S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

跳至解决方案
1,807 次查看
347996379
Contributor III

Hi, this is how I can close the problem after installing the IAR Eclipse Plugin, recreating a project, and then compiling the problem.

pastedImage_1.png

ilinkCommandLine_S32K146OFBMU_iar.xcl

pastedImage_2.png

标记 (3)
0 项奖励
回复
1 解答
1,685 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,686 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

0 项奖励
回复