S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

ソリューションへジャンプ
2,468件の閲覧回数
347996379
Contributor III

Hi, this is how I can close the problem after installing the IAR Eclipse Plugin, recreating a project, and then compiling the problem.

pastedImage_1.png

ilinkCommandLine_S32K146OFBMU_iar.xcl

pastedImage_2.png

タグ(3)
0 件の賞賛
返信
1 解決策
2,346件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,347件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

0 件の賞賛
返信