S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for ARM v2018.R1 After installing the IAR Eclipse Plugin, configure the output, output the IAR linker, output converter (Output Converter) to generate S19/HEX/BIN file, and compile error

Jump to solution
2,433 Views
347996379
Contributor III

Hi, this is how I can close the problem after installing the IAR Eclipse Plugin, recreating a project, and then compiling the problem.

pastedImage_1.png

ilinkCommandLine_S32K146OFBMU_iar.xcl

pastedImage_2.png

Tags (3)
0 Kudos
Reply
1 Solution
2,311 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

View solution in original post

0 Kudos
Reply
1 Reply
2,312 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that your target - S32K146_OFBMU_iar.out is opened or in use by another application. Or you dont' have permissions to be able delete existing .out file. 

Jiri 

0 Kudos
Reply