S32DS for ARM 2018R1 license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for ARM 2018R1 license

Jump to solution
36,127 Views
BoxLi
NXP Employee
NXP Employee

Hi:

My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me? 

Thanks.

 

binli_0-1654501988529.png

 

0 Kudos
Reply
1 Solution
36,103 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I've extended your entitlement. Please refresh or re-activate your installation.

Best Regards,

Mike

View solution in original post

93 Replies
9,714 Views
NiceHyuny
Contributor I

Hi, my licence is expired, can you help me to extend it?

The number is 

4F70-F0A3-101C-3C96

 

Thank u so much.

0 Kudos
Reply
9,583 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I have extended this entitlement through 2025. Please use the activation code to receive the new license.

Best Regards,

Mike

0 Kudos
Reply
7,317 Views
Jaydenyzhu
Contributor I

Dear,

my license of S32 Design Studio for ARM Version 2018.R1 has expired. Could you please extend it for me? 

Activation Code D5D0-D801-AB24-58DF

Thanks a lot.

0 Kudos
Reply
7,452 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hello, @Jaydenyzhu 

I have extended this entitlement through 2026.

Please use the activation code to receive the new license.

Best Regards,

- Mehul Patel

0 Kudos
Reply
7,554 Views
Jaydenyzhu
Contributor I

Thank you very much. Now everything is working correctly. Thank you again.

0 Kudos
Reply
10,335 Views
atranzillo93
Contributor III

Hi, my licence is expired, can you help me to extend it?

The number is 

B361-6887-8BBF-ED12

 

Moreover, also for my collegue Anna D'Alessio: 

E735-6A42-FED4-6005

 

Thank u so much.

Anita

0 Kudos
Reply
10,527 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Both entitlements have been extended through 2025. Please use the activation code to re-activate your installations.

Best Regards,

Mike

0 Kudos
Reply
10,991 Views
valeriaalessi
Contributor II

Good morning,

my license of S32DS for ARM 2018R1 IDE has expired. Could you please extend it for me? 

In attachment you can find the current licence expired.

Thanks a lot.

Valeria

0 Kudos
Reply
10,784 Views
mikedoidge
NXP Employee
NXP Employee

Hello @valeriaalessi,

I checked the license server. It reported that you had exceeded the maximum number of returns. I have reset the return count. The issue should now be resolved. Please try once more.

Mike

0 Kudos
Reply
10,751 Views
valeriaalessi
Contributor II

Good morning,

I tried to re-activate with the same license number but it continues to tell me that the license is for another feature. However, the second error about exceeded number of returns does not come out again, after the first one.

Could you help me?

Thanks a lot.

Valeria

0 Kudos
Reply
11,103 Views
mikedoidge
NXP Employee
NXP Employee

Hello @valeriaalessi,

I have manually returned the license from the server side. When you receive the offer to return the license, please choose 'Yes'. Sometimes there is some setting which does not get reset properly and this will force it to be reset. After this, and with my action to return the license, you should be able to activate without issue.

Best Regards,

Mike

0 Kudos
Reply
11,085 Views
valeriaalessi
Contributor II

Good morning!

The issue is solved!

Thanks a lot.

Valeria

11,154 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I have extended your license through 2025. Please refresh from the Help->NXP Licenses menu or reactivate using the same activation code as before.

Best Regards,

Mike

0 Kudos
Reply
11,438 Views
valeriaalessi
Contributor II

Good morning,

I tried to activate again the license, with the same number as before, but it tells me that the license is for another feature. Then, if I click on return, a error message appears (see attachments).

Could you help me please?

Thanks a lot!

Valeriaerror_1.PNGerror_2.PNG

0 Kudos
Reply
36,104 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I've extended your entitlement. Please refresh or re-activate your installation.

Best Regards,

Mike

3,895 Views
e-look_see
Contributor I

Hi, My S32 Design Studio for ARM v2018 R1 License has already expired,could you help to extend it?Thanks! Activation Code: 3EF3-981A-CE8D-45C3

0 Kudos
Reply
4,338 Views
KerwinCao
Contributor I

Hello, my license of S32 Design Studio for ARM Version 2018.R1 expiration soon

Could you please extend it ? Thanks. 

My activation Code: C617-86A4-65B7-F3D9

Thanks a lot

0 Kudos
Reply
4,908 Views
Xuchengcheng
Contributor I

Hello, my license of S32 Design Studio for ARM Version 2018.R1 expiration soon

Could you please extend it ? Thanks. 

My activation Code: 516A-3379-0522-6A9D

Thanks a lot

0 Kudos
Reply
5,560 Views
csuiil
Contributor I

Hi:

My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me? 

Thanks.

==========================================

Item DescriptionS32 Design Studio


Order NumberS32DS_2018_R1_100931407

Purchase Order Number

Total Number of Licenses:100

Activation Code  C625-7579-0C28-63DC

License Applicable to Product(s):

Version Description
R1 2018 S32 Design Studio (View EULA) 3.1 S32 Design Studio (View EULA)


100 Available

 


 
 
 
0 Kudos
Reply
7,533 Views
HoganLiu
Contributor I

Dear,

my license of S32 Design Studio for ARM Version 2018.R1 has expired. Could you please extend it for me? 

Activation Code: E03E-A0CC-D45D-88C8

Thanks a lot

.

0 Kudos
Reply
7,706 Views
liamtsen
Contributor I

Hi, my licence is expired, can you help me to extend it?

The number is 

Thanks a lot.

Tags (1)
0 Kudos
Reply