Hi:
My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me?
Thanks.
Solved! Go to Solution.
Hello,
I've extended your entitlement. Please refresh or re-activate your installation.
Best Regards,
Mike
Thank you very much. Now everything is working correctly. Thank you again.
Hi, my licence is expired, can you help me to extend it?
The number is
Moreover, also for my collegue Anna D'Alessio:
Thank u so much.
Anita
Hello,
Both entitlements have been extended through 2025. Please use the activation code to re-activate your installations.
Best Regards,
Mike
Hello @valeriaalessi,
I checked the license server. It reported that you had exceeded the maximum number of returns. I have reset the return count. The issue should now be resolved. Please try once more.
Mike
Good morning,
I tried to re-activate with the same license number but it continues to tell me that the license is for another feature. However, the second error about exceeded number of returns does not come out again, after the first one.
Could you help me?
Thanks a lot.
Valeria
Hello @valeriaalessi,
I have manually returned the license from the server side. When you receive the offer to return the license, please choose 'Yes'. Sometimes there is some setting which does not get reset properly and this will force it to be reset. After this, and with my action to return the license, you should be able to activate without issue.
Best Regards,
Mike
Good morning!
The issue is solved!
Thanks a lot.
Valeria
Hello,
I have extended your license through 2025. Please refresh from the Help->NXP Licenses menu or reactivate using the same activation code as before.
Best Regards,
Mike
Good morning,
I tried to activate again the license, with the same number as before, but it tells me that the license is for another feature. Then, if I click on return, a error message appears (see attachments).
Could you help me please?
Thanks a lot!
Valeria
Hello,
I've extended your entitlement. Please refresh or re-activate your installation.
Best Regards,
Mike
Hello, my license of S32 Design Studio for ARM Version 2018.R1 expiration soon
Could you please extend it ? Thanks.
My activation Code: C617-86A4-65B7-F3D9
Thanks a lot
Hello, my license of S32 Design Studio for ARM Version 2018.R1 expiration soon
Could you please extend it ? Thanks.
My activation Code: 516A-3379-0522-6A9D
Thanks a lot
Hi:
My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me?
Thanks.
==========================================
Item DescriptionS32 Design Studio
Order NumberS32DS_2018_R1_100931407
Purchase Order Number
Total Number of Licenses:100
Activation Code C625-7579-0C28-63DC
License Applicable to Product(s):
Version Description
R1 2018 S32 Design Studio (View EULA) 3.1 S32 Design Studio (View EULA)
100 Available
Dear,
my license of S32 Design Studio for ARM Version 2018.R1 has expired. Could you please extend it for me?
Activation Code: E03E-A0CC-D45D-88C8
Thanks a lot
.
Hi, my licence is expired, can you help me to extend it?
The number is
Hi, @liamtsen ,
I have extended your license through end of December 2028.
Please refresh the activation to use it.
Thank you. Best regards.
- Mehul Patel
Hello,
My S32 Design Studio for ARM v2018.R1 License has already expired. Could you please help to extend it? Thanks!
Activation Code: B7B1-173F-51BA-13A2
Best regards,
Sarah
My S32 Design Studio for ARM 2018_R1 would expired in 4 days, could you help to extend it? thanks;
ActivationId: 799E-5E79-910F-6C57