An error occurred when adding the S32K3 Real-Time Drivers Update Sites in S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An error occurred when adding the S32K3 Real-Time Drivers Update Sites in S32 Design Studio

5,774件の閲覧回数
Panpan
Contributor I

Hi Team,

An error occurred when adding the S32K3 Real-Time Drivers Update Sites(SW32K3_RTD_4.4_2.0.3_DS_updatesite_D2302.zip) in S32 Design Studio(V3.5), as shown below:

Panpan_0-1679023820774.png

Looking forward to your replay.

Thanks.

0 件の賞賛
返信
10 返答(返信)

5,756件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

S32K3 RTD v.2.0.3 is delivered as an Update Site for S32 Design Studio "S32 Design Studio IDE v3.4 Update 3".

 

B.R.

VaneB

0 件の賞賛
返信

5,744件の閲覧回数
Panpan
Contributor I

Hi VaneB,

Might I ask a question?

How to install S32K3 Real-Time Drivers for S32 Design Studio IDE v3.5?

 

Best Regards.

0 件の賞賛
返信

5,728件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

I suggest you download the S32DS v.3.4. If you still want to use v.3.5, take a look at the below community posts:

0 件の賞賛
返信

5,719件の閲覧回数
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your help.

I have installed the S32DS v.3.4. 

An error occurred when building the S32K344_HSE_OTA(SW32K3_OTADEMO_0.8.0) project, it seems to be missing the StandardTypes.h/S32K344_MU.h/Compiler.h etc. file, where can I find these file? or do you know the solution?

Panpan_0-1679466882359.png

 

Looking forward to your reply.

Best Regards.

0 件の賞賛
返信

5,696件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

For the S32K344_HSE_OTA project, you must have installed the Real Time Drivers v1.0.0 in S32DS v.3.4 and the S32K344 with AB_SWAP HSE firmware.

To run the project:

  1. Import the project to your S32DS workspace (File -> Import... -> General -> Existing Projects into Workspace)
  2. Build the project (right-click on project name -> Build project)
  3. Go to Run/Debug and select the desired debug configuration, and click on Launch.
  4. The PRACTICE script will halt the code at main().
  5. Type Go and enter
  6. Code will halt at Random Number Generation Demo (Demo_RandomNumberGeneration())
  7. Type Go and enter (to execute demo)
  8. Code will halt at Key Provisioning Demo (Demo_KeyProvisioning())
  9. Type Go and enter (to execute demo)
  10. Code will halt at Authentication Demo (Demo_Authentication())
  11. Type Go and enter (to execute demo)
  12. Code will halt at Symmmetric Cipher Demo (Demo_SymmetricCipher())
  13. Type Go and enter (to execute demo)
  14. Code will halt at Hash Demo (Demo_Hash())
  15. Type Go and enter (to execute demo)
  16. Code will halt at OTA Update Demo (Demo_OtaUpdate())
  17. Type Go and enter (to execute demo)
  18. Type CONTINUE to execute the practice script.
  19. RESET is issued to the device, and the OTA Update application will execute.
0 件の賞賛
返信

5,685件の閲覧回数
Panpan
Contributor I

Hi @VaneB 

 

Sorry to bother you, I have anther question to ask you.

For the S32K344_HSE_OTA project, it indicates the HW requires the S32K3XXEVB-Q172 and P&E debug tool. Where and how the P&E debug tool can be bought?

And how the Trace32 and Multi GHS software can be downloaded?

 

Looking forward to your reply.

Best Regards.

0 件の賞賛
返信

5,669件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Panpan 

If you are using an EVB, it includes two options for debugging. You can connect a debugger to the 20-pin Cortex Debug D ETM Connector with TRACE or the 10-pin Cortex Debug JTAG Connector (depending on your board) and the on-board S32K3 debugger (see the below image).

 

VaneB_1-1679614353779.png

Also, I attached some links to HOWTOS that will be useful for you.

0 件の賞賛
返信

5,655件の閲覧回数
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your reply.

I am planning to buy the S32K3X4EVB-T172 evaluation board, I need to purchase the TRACE connector from the third party. Right?

And is there a soft simulation environment for S32K3X4?

 

Best Regards.

0 件の賞賛
返信

5,645件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

5,688件の閲覧回数
Panpan
Contributor I

Hi @VaneB 

 

Thank you for your help, I solved the problem.

 

Best Regards.

0 件の賞賛
返信