S32 Design Studio for ARM 2018.R1 - Update 7 available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio for ARM 2018.R1 - Update 7 available

S32 Design Studio for ARM 2018.R1 - Update 7 available

 

 

 

nxp.png

Product Release Announcement

Automotive Microcontrollers and Processors

S32 Design Studio for ARM® 2018.R1 

Update 7

S32DS_Logo_official_2016_scaled.png  

 

 

 

What is new?

  • S32K1xx SDK BETA 2.9.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148.  Also included is AMMCLIB 1.1.13 for S32K11x and S32K14x. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6)

pastedImage_2.png

Installation instructions

The update is available for  (via Eclipse Updater) or offline installation (direct download link)

 pastedImage_1.png

  • offline installation:  
    • go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip filepastedImage_3.png
    • Start S32DS and go to "Help" -> "Install New Software..."
    • Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step
      pastedImage_4.png
    • Select all available items and click "Next" button.

 

This will starts the update installation process.

标签 (1)
评论

If I want to install the up7, I need to install the up1~6?

Hello,

As this is a cumulative update, it includes all previous updates. So it is not necessary to install the previous updates prior to installing update 7.

Best Regards,

Mike

无评分
版本历史
最后更新:
‎09-04-2018 09:23 AM
更新人: