One or more Launch Configurations need to be updated?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

One or more Launch Configurations need to be updated?

Jump to solution
1,642 Views
jeffcharles
Contributor III

Hi,

I just installed CW10.7 the other day. The Development Studio gives the following warning when I build a new project based on MC9S12ZVL32. After I click the OK button, it reports a error. How to solve this problem?

pic001.PNG

pic002.PNG

1 Solution
1,572 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Your issue is probably caused because of wrong installation path.  

Did you change the default installation path for CodeWarrior?

It should be located in "C:\Freescale" directory.

So, the solution is to install the CodeWarrior again, but into a default folder.

I hope it helps you.

Best Regards,

Diana

View solution in original post

1 Reply
1,573 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Your issue is probably caused because of wrong installation path.  

Did you change the default installation path for CodeWarrior?

It should be located in "C:\Freescale" directory.

So, the solution is to install the CodeWarrior again, but into a default folder.

I hope it helps you.

Best Regards,

Diana