One or more Launch Configurations need to be updated?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

One or more Launch Configurations need to be updated?

ソリューションへジャンプ
1,156件の閲覧回数
jeffcharles
Contributor III

Hi,

I just installed CW10.7 the other day. The Development Studio gives the following warning when I build a new project based on MC9S12ZVL32. After I click the OK button, it reports a error. How to solve this problem?

pic001.PNG

pic002.PNG

1 解決策
1,086件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Your issue is probably caused because of wrong installation path.  

Did you change the default installation path for CodeWarrior?

It should be located in "C:\Freescale" directory.

So, the solution is to install the CodeWarrior again, but into a default folder.

I hope it helps you.

Best Regards,

Diana

元の投稿で解決策を見る

1 返信
1,087件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Your issue is probably caused because of wrong installation path.  

Did you change the default installation path for CodeWarrior?

It should be located in "C:\Freescale" directory.

So, the solution is to install the CodeWarrior again, but into a default folder.

I hope it helps you.

Best Regards,

Diana