Where can I find Processor Expert examples and tutorials in Driver Suite?
How to configure the processor component to match my hardware?
Adding Processor Expert to C Project (without SDK in PEx Driver Suite)
Adding Processor Expert to C Project (with SDK in PEx Driver Suite)
AN4819 - Building a Project using IAR Eclipse Plugin - This application note provides steps to configure IAR Eclipse plugin and using Processor Expert (PEx) together with IAR build tool chain.
AN4913 - Building and Debugging a project using Keil MDK-ARM Eclipse plug-in - This application note provides steps to configure Keil MDK-ARM Eclipse plug-in and using Processor Expert together with Keil build tool chain.
Processor Expert Tools in Microcontroller Driver Suite - Training Videos
Thank you.
The Microcontroller Driver Suite will not be extended with new parts lik the K65. You can use Kinetis Design Studio V3.x for this, see
This offers (with the SDK V1.3) MK65 support:
With this, KDS v3.x (I recommend KDS V3.2, see https://mcuoneclipse.com/2016/04/02/nxp-kinetis-design-studio-v3-2-0/). Be aware that the future is with the Kinetis SDK and the SDK V2.0, see https://mcuoneclipse.com/2016/01/29/first-nxp-kinetis-sdk-release-sdk-v2-0-with-on-demand-package-bu....
I hope this helps,
Erich
Thank you Erich. I was able to access what I needed once I transferred to KDS V3.2 and installed SDK V1.3.