Importing Example Projects
Select File > Import from CodeWarrior menu. The Import dialog appears. Select General / Existing Projects into Workspace and click Next. Select the Select root directory option and click Browse. Browse to the following location of CodeWarrior installation directory:
<PExDrv 10_0_2>\eclipse\ProcessorExpert\Projects
Select the folder containing the example projects if you want to import multiple projects, or the specific example project.
Click OK.
If you have selected the folder, the list of the example projects available in the folder appears in the Projects area. Check the checkbox adjacent to the project(s) you want to import.
Select the Copy projects into workspace checkbox to create an independent copy of the project into the workspace.
Click Finish.
Typical Component Usage
Examples of using generated code can be found on Typical usage page of the components. This page is provided within a component help. To get this help use the component’s pop-up menu command Help on component or browse the component in the Components User Guide within the Eclipse help system at Processor Expert Software - Microcontrollers Driver Suite > Manuals. The Typical usage page is available as a part of documentation for every LDD or high level component.