Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

ソリューションへジャンプ
2,704件の閲覧回数
jeffreygraves
Contributor III

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

(ie similar to fsl_usb_device_msd_class or fsl_usb_device_hid_class)

タグ(3)
1 解決策
2,045件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,045件の閲覧回数
michaelsteffenf
NXP Employee
NXP Employee

Mark, Is this still on track to be released in Q3 using the KSDK1.3?

0 件の賞賛
返信
2,045件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have checked the current status and the fsl_usb_device_cdc_class PEx component support has been postponed. This PEx component will not be available in KSDK 1.3.0 release in September. But the Kinetis SDK USB CDC drivers are available, see for example documentation in KSDK_1.2.0\doc\usb\ folder (these USB CDC drivers can be used in any Kinetis project).

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,045件の閲覧回数
michaelsteffenf
NXP Employee
NXP Employee

Marek,

Is there some documentation or guide on implementing our USB CDC Class driver into an existing KSDK PEx project.  I've got a customer using PEx for the entire project and he wants to use the PEx CDC component, but its not available, nor will be available in KSDK 2.0.  How can he implement the example USB CDC project into his PEx project?

Mike

2,045件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Michael,

I have asked Processor Expert development team to provide USB CDC support (example, user guide).

Best Regards,

Marek Neuzil

2,045件の閲覧回数
F50SC
Contributor III

Hi Marek

As per Mike's last comment we have a similar project...can Freescale provide a step by step guide on how to implement USB CDC in a PEx + KSDK1.2 + MQX project.

Regards

Jerome

0 件の賞賛
返信
2,046件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

0 件の賞賛
返信