Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

跳至解决方案
4,101 次查看
jeffreygraves
Contributor III

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

(ie similar to fsl_usb_device_msd_class or fsl_usb_device_hid_class)

标记 (3)
1 解答
3,442 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,442 次查看
michaelsteffenf
NXP Employee
NXP Employee

Mark, Is this still on track to be released in Q3 using the KSDK1.3?

0 项奖励
回复
3,442 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have checked the current status and the fsl_usb_device_cdc_class PEx component support has been postponed. This PEx component will not be available in KSDK 1.3.0 release in September. But the Kinetis SDK USB CDC drivers are available, see for example documentation in KSDK_1.2.0\doc\usb\ folder (these USB CDC drivers can be used in any Kinetis project).

Best Regards,

Marek Neuzil

0 项奖励
回复
3,442 次查看
michaelsteffenf
NXP Employee
NXP Employee

Marek,

Is there some documentation or guide on implementing our USB CDC Class driver into an existing KSDK PEx project.  I've got a customer using PEx for the entire project and he wants to use the PEx CDC component, but its not available, nor will be available in KSDK 2.0.  How can he implement the example USB CDC project into his PEx project?

Mike

3,442 次查看
marek_neuzil
NXP Employee
NXP Employee

Hi Michael,

I have asked Processor Expert development team to provide USB CDC support (example, user guide).

Best Regards,

Marek Neuzil

3,442 次查看
F50SC
Contributor III

Hi Marek

As per Mike's last comment we have a similar project...can Freescale provide a step by step guide on how to implement USB CDC in a PEx + KSDK1.2 + MQX project.

Regards

Jerome

0 项奖励
回复
3,443 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

0 项奖励
回复