Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

Jump to solution
4,104 Views
jeffreygraves
Contributor III

Is a KSDK_1.1.0 based fsl_usb_device_cdc_class PEx component forthcoming?

(ie similar to fsl_usb_device_msd_class or fsl_usb_device_hid_class)

Tags (3)
1 Solution
3,445 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

View solution in original post

0 Kudos
Reply
6 Replies
3,445 Views
michaelsteffenf
NXP Employee
NXP Employee

Mark, Is this still on track to be released in Q3 using the KSDK1.3?

0 Kudos
Reply
3,445 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have checked the current status and the fsl_usb_device_cdc_class PEx component support has been postponed. This PEx component will not be available in KSDK 1.3.0 release in September. But the Kinetis SDK USB CDC drivers are available, see for example documentation in KSDK_1.2.0\doc\usb\ folder (these USB CDC drivers can be used in any Kinetis project).

Best Regards,

Marek Neuzil

0 Kudos
Reply
3,445 Views
michaelsteffenf
NXP Employee
NXP Employee

Marek,

Is there some documentation or guide on implementing our USB CDC Class driver into an existing KSDK PEx project.  I've got a customer using PEx for the entire project and he wants to use the PEx CDC component, but its not available, nor will be available in KSDK 2.0.  How can he implement the example USB CDC project into his PEx project?

Mike

3,445 Views
marek_neuzil
NXP Employee
NXP Employee

Hi Michael,

I have asked Processor Expert development team to provide USB CDC support (example, user guide).

Best Regards,

Marek Neuzil

3,445 Views
F50SC
Contributor III

Hi Marek

As per Mike's last comment we have a similar project...can Freescale provide a step by step guide on how to implement USB CDC in a PEx + KSDK1.2 + MQX project.

Regards

Jerome

0 Kudos
Reply
3,446 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

The fsl_usb_device_cdc_class PEx component will be available in KSDK 1.3.0 release this year (Q3/2015).

Best Regards,

Marek Neuzil

0 Kudos
Reply