恩智浦其他产品知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Other NXP Products Knowledge Base

讨论

排序依据:
********************************************************************************************************* * This simple example code has been written for the FRDM-KL25Z + FRDM-FXS-MULT2-B * boards and demonstrates how to use the embedded magnetic threshold detection * function in conjunction with the auto-wake/sleep mode for reducing current * consumption of the FXOS8700CQ. * * The magnetic threshold is set to 100uT (1000 counts) on the X and Y axis. * Once this threshold is exceeded, the FXOS8700CQ is waken up and an interrupt * is generated on the INT1 pin. If the magnetic field is below this threshold * within the 20ms period, the FXOS8700CQ goes back to sleep mode and also * generates an interrupt on the INT1 pin. *********************************************************************************************************
查看全文
****************************************************************************************************** * This code has been written for the NXP FRDM-KL25Z + FRDM-STBC-AGM04 boards * and demonstrates how to read the acceleration (MMA8652FC), magnetic (MAG3110) * and angular rate (FXAS21002C) data using an interrupt technique. * * All sensors are controlled via I2C by default. * * I2C slave addresses: * MMA8652FC -> 0x1D * MAG3110 -> 0x0E * FXAS21002C -> 0x20 * * J7 selects MCU I2C bus for SDA: * 2:3 -> I2C_SDA1 (PTC2) * * J8 selects MCU I2C bus for SCL: * 2:3 -> I2C_SCL1 (PTC1) * * INT1_8652 connected to PTD4, INT1_MAG3110 connected to PTA5 pin and * INT1_21002 connected to PTA4 pin. ***************************************************************************************************** Original Attachment has been moved to: FRDM-KL25Z-FRDM-STBC-AGM04-Basic-read-using-I2C-and-interrupts.rar
查看全文
*************************************************************************************************** * The PCF2129AT is a CMOS Real Time Clock (RTC) and calendar with an integrated * Temperature Compensated Crystal Oscillator and a 32.768 kHz quartz crystal * optimized for very high accuracy and very low power consumption. * Detailed Description: * This simple example code has been written for the FRDM-KL25Z + OM13513 * boards and demonstrates how to set and read the time/date on the PCF2129AT * using the SPI (do not forget to remove the JP1 jumper) interface. * * In this example the time to be set is Wednesday, February 8 2017, 2:45 PM. * * Connection:    FRDM-KL25Z       OM13513 * VDD               J9-4                       P2-2 * GND               J9-18                    P2-1 * MOSI              J2-8                      P2-5 * MISO              J2-10                    P2-6 * SCLK              J2-12                    P2-4 * CS                  J2-6                      P2-7 ***************************************************************************************************
查看全文
Hi, Trying download and debug in IAR for MAC57D54H from NXP but get an error as: "Warning:Stack pointer is setup to incorrect alignment.Stack addr=0xFFFFFFFF" What would be the reason?
查看全文
Subject:  Info on FET BUK7909-75AIE Description:  The datasheet for part number BUK7909-75AIE describes it as qualified to AEC standard for use in automotive critical applications.  It also says it is Q101 compliant.  We are not familiar with these automotive standards but would like to know if samples have been tested for either these or similar qualification tests: Lifetesting Tempeature Cycling HAST or 85/85. I am expecting the automotive qual to meet or exceed these requirements, but need to be sure that device samples or devices from the same process have had qualification testing performed.  Please comment. Also, we need to know if there is an MSL rating for this part?  Finally, what is the terminal finish?  What is the long-term availability.  WE are looking to use these to replace an obsolete FET from IR/Infineon, and we want to be sure it will remain available.
查看全文
Four live demonstrations are presented: Timing Attack; Simple Power Analysis; Fault Attack, and finally an RFID Relay Attack demo. Timing Attack demo The Timing Attack demo shows the importance of securely implementing a PIN verification. If a PIN verification is implemented with operations which are not time-invariant - for example an if-else construction - it is possible to identify when an incorrect PIN digit is being compared by observing the timing information of the corresponding EM side-channel measurement. By iterating through all possible values of a PIN digit the correct character will be identified in a maximum of 10 attempts. To make the PIN query secure, a time-invariant comparison has to be implemented. For example, a bitwise XOR comparison and subsequent OR operation for all PIN digits, ensures the same time is taken for all possible comparisons. This scheme is illustrated in the block diagram.             Simple Power Analysis demo The RSA-Algorithm implemented in the Simple Power Analysis demo application is reduced to a simple 8-Bit implementation for illustrative purposes. The physical smart card interface used is contact-based. By monitoring the voltage drop across a shunt resistor it is possible to measure the power consumption of an RSA operation on a digital oscilloscope. Observation of the resulting measurements reveal that it is possible to visually distinguish  single square operations from square and multiply operations. By iteratively logging this sequence of operations, the bits of the exponent, that is the secret key, can be directly identified. By using countermeasures like the square and always multiply algorithm, the decoding of the exponent bits can be prevented and the key protected. The square and always multiply algorithm is illustrated in the block diagram.    Fault Attack demo The Fault Attack demo shows what can happen at software execution, if a flashlight is fired on a decapsulated chip which has no security measures. With simple tools – a mechanical grinding tool and some chemical etchant - it is possible to expose the surface of the chip and crudely inject photons into the sensitive silicon substrate. In this case the flashlight causes a skip in the execution of the PIN verification code if the flash is discharged close to the surface at the correct moment. In normal function expiration the UserPin is either correct or incorrect and access to the data is granted or denied accordingly. With a successful flashlight attack it doesn’t matter which value for UserPin is entered - after several tries the attacker skips the query and has access to the secret data.    RFID Relay Attack demo The RFID Relay Attack demo demonstrates a new paradigm in relay attacks in the context of software emulated smartcards on mobile devices. Previous conditions about proximity of the attacker to the victim and the time when the victim is approached, are negated. With a software emulated smartcard on a mobile device an attacker can intercept and relay the transaction of a potential victim remotely. This new attack paradigm greatly enhances the value of this attack for criminals, and consequently will result in greater malware development efforts. Additional Information on the individual attacks
查看全文
******************************************************************************** * Detailed Description: * This example shows how to use the CTU module triggered from eTimer0 module channel 2. * * For closer details on how CTU works I suggest you to check application note * MPC5643LPWM_ADC_concept * https://community.freescale.com/docs/DOC-102559 * * This example sets eTimer0 channel2 for PWM signal generation. * This signal is than used to send MSR trigger to CTU module * Example contains also simple CTU module driver initialization * CTU scheduler submodule is toggling with external pin based on CTU triggers * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P, * silicon mask set 1N65H * Target :  internal_FLASH* ******************************************************************************** Original Attachment has been moved to: Example-MPC5744P-CTU-eTimer-v1_1-GHS614.zip
查看全文
This video shows the necessary configurations to flash a binary file to a target, in this case the FRDM-KL25
查看全文
This simple method, commonly used by RF engineers every day, is effective for creating a fast change of frequency range in a demo circuit, when you only have something close to work with. Your ability to use Freescale RF Power products as drop-ins is increased! In addition to being able to purchase a demonstration board, you can download any of the available DXF files for the PCB layout and order the board and list of materials for your production line. In many cases, you may be able to save money by choosing, testing, and qualifying your own list of less costly components. The initial design work is done with a Freescale demo board! The tuning, manufacturing and qualification process is all that is left to you. Thanks for choosing Freescale RF Power!
查看全文
In Window Builder the string table is one of the key elements of the resource manager. This application notes gives tips and tricks to ease the use of string tables.
查看全文
With the release of PEG 2.3.13 a newly created widget is available in PEG, called the "Swipe" widget. This application note describes features of the widget and how to make use it with Window Builder and PEG runtime library.
查看全文
This application note describes the changes of the Window Builder code generator that have been released in the latest PEG revision (2.3.13). To fix a bug in the code generator it had become necessary to introduce some changes. The attached document describe the changes in more detail and explain how to deal with them to avoid messing up user code interleaved in the generated code.
查看全文
Q: How should I start to evaluate PEG? A:   Download: Desktop and Hardware Demos       Request for Window Builder  -  The free download is the full version of Window Builder, but no source code is provided, so applications can only be developed on provided compiled libraries (this by default is Windows, but can be extended to a EVB such as the Tower System).        Request for further evaluation please contact Freescale sales or distributor representative. Q: Is PEG software supported on NON-Freescale and Freescale silicon? A: Yes, PEG Software can be licensed for for NON-Freescale and Freescale silicon. There is a discount when used with Freescale silicon. Q:  Is the cost limited to 10,000 pieces? A:  There are 4 licensing models.       1) PEG Base Single Product/MCU (3 seats, <=10,000 units, 1 year support) is specific to the processor used AND the specific name and model of the customer end product.      2) Upgrade - Unlimited Run-time for PEG Base:  There are NO limits on the number of run-time units for the PEG Base Single Product/MCU      3) Upgrade - Same MCU across  Product Family (+3 seats, unlimited run-time): Supports a family of customer end products that use the same processor      4) Upgrade - Multi MCU across  Product Family (+6 seats, unlimited run-time): Supports a family of customer end products that use multiple processors Q: Is technical support included? A:  One year of support is included with the purchase of a license and can always renew. Q: How does the actual GUI image (in the frame buffer) get updated through interrupt routines or some other method. A:  PEG implemented a scheduler that runs at a defined rate (20 times per second by default) and quickly checks a messaging queue.  If updates to the image are required, then the appropriate actions are taken to update the screen. Q: How is the frame buffer decided on?  Does PEG do it as needed or does the designer set the size and update as needed? A: PEG will define the require space for the frame buffer depending on the screen resolution, color depth, and number of buffers (i.e double-buffering, multiple surfaces, etc…) Q: Do we have examples of wave form generation code with anti-aliasing filters? A: There are examples of PEG drawing a variety of graphs (in the demo folder of PEG). Q: What drivers hardware and screen drivers are supported? A: PEG screen drivers can be developed for virtually any processor/controller. The list here includes devices for which drivers currently exist. Q: How can I purchase PEG? A: You can purchase it direct please contact sales@swellsoftware.com or from a number of distributors/re-sellers:      - AIC Japan      - eCOS      - eSOL      - Express Logic      - Green Hills Software      - Microdigital      - Quadros      - Arrow      - Future      - Advent     
查看全文
How can I distinguish between various MSC8154/MSC8156 devices? You can read the System Part and Revision ID Register (SPRIDR) from address  to get the part ID and revision ID numbers. Device             SPRIDR[PARTID] MSC8154                0x8304 MSC8154EC           0x831C MSC8154E             0x830C MSC8156               0x8302 MSC8156EC           0x831A MSC8156E             0x830A Revision           SPRIDR[REVID] Rev. 1                       0x0000 Rev. 2                       0x0001 [ return to top ] My configuration sets up the L2 unified cache/M2 memory to 256KB of M2 and 256 KB of L2 cache.  Does this mean L2 cache is 8 ways of 32 KB each? No. The L2/M2 is 512 KB, arranged in 8 ways of 64 KB each way. In your configuration, the L2 cache becomes 4 ways. Each way is still 64 KB. [ return to top ] Does an M3 ECC event trigger an interrupt? M3 memory is ECC-protected so a single-bit error is detected and corrected, therefore an interrupt is not necessary. [ return to top ] The L2 cache features 4 L2 software prefetch channels.  Are there 4 software prefetch channels per core or is this the total number per device? The L2 cache is private for each core, therefore the 4 software prefetch channels are per core. Each core configures its own set of L2 software prefetch registers. Each core can only configure its own L2. The L2 software prefetch registers cannot be configured externally from the DSP subsystem. [ return to top ] Do I need an I2C serial EEPROM for loading of the Reset Configuration Word (RCW)? No, there are other options for loading of the RCW besides the I2C serial EEPROM. Multiplexed RCW loading option(RCW_SRC[0:2]=000) - all 64-bits of the RCW are loaded in four passes using the external pins RC[15:0]  using the /RCW_LSEL[0:3] pins as lane select signals. Reduced RCW loading option (RCW_SRC[0:2]=011) - some bits of the RCW are latched from external pins and some bits are loaded from default hard-coded values. [ return to top ] How does MSC8156 MAPLE-B TVPE support Viterbi and Turbo decoding? Turbo and Viterbi decoding are supported by MSC8156 MAPLE-B TVPE in same µcode. You can initialize the Maple with one TVPE standard, plus some Viterbi parameters. Then you can use different Buffer Descriptors for Turbo and Viterbi. Note that MAPLE-B doesn't support multiple Turbo standards with the same µcode because Maple µcode is standard specific and a µcode re-load is required to switch from one standard to another. So supporting a mixture of users of different standard in real time cannot be done with current MAPLE-B.  Turbo and Viterbi decoding are supported in same µcode, since Viterbi decoding parameters are fully configurable and are not standard related. [ return to top ] I want to use the Debug and Profiling Unit (DPU) in the MSC8156 to log information into the virtual trace buffer. I have set up the DPU registers for core 0. How do I set up the DPU for the other cores 1/2/3/4/5 since there is only one set of DPU registers? Each DSP subsystem includes a DPU. Each core can access its own DPU registers using the same physical addresses. [ return to top ] I only need to reset an individual core in the MSC8156. How can I do that? All cores are reset together. There is not a method to reset a particular core in the MSC8156. [ return to top ] The MSC8156 Reference Manual shows the default DDR1 and DDR2 memory address spaces are 512 MB. How do I change the memory space to 1 GB? The MSC8156 Reference Manual shows the DDR address spaces as follows: 0x40000000–0x5FFFFFFF      DDR1 Memory (default value)                                               512 M 0x60000000–0x7FFFFFFF      Reserved.  Used for DDR1 memory if configured for 1 GB.      512 M 0x80000000–0x9FFFFFFF      DDR2 Memory (default value)                                               512 M 0xA0000000–0xBFFFFFFF     Reserved. Used for DDR2 memory if configured for 1 GB.       512 M After reset, the default DDR1 and DDR2 memory space is 512 MB. To increase to 1GB DDR memory range, you need to configure the CLASS registers as follows: For DDR1 memory controller, change C0EAD5 from the reset value of 0x0005FFFF to 0x0007FFFF [ return to top ] What is the maximum heat sink attachment force to avoid damaging the solder balls? Detailed information about the Flip-Chip Plastic Ball Grid Array (FC-PBGA) package type devices (MSC8144 and MSC8156) can be found in this document FC-PBGAPRES.pdf The maximum heat sink attachment force is 4 Newtons (10 lb force). [ return to top ] What does the NO_INC bit indicate in the DMA buffer descriptor BD_ATTR field? When would you use this? You can set NO_INC if you want to transfer to or from the same address. The address will not be incremented. For example, if you want to fill memory with data from a single memory location, you will need to set NO_INC for the source. However, the destination will have the NO_INC bit cleared. [ return to top ] If a MSC8156 DMA port A or B bus error happens, i.e., DMAERR[PAE] or DMAERR[PBE] bit is set, can I clear these bits and continue with the DMA operation? A port error will freeze the DMA channel so clearing the error bit has no effect. In this case, the DMA channel needs to be reinitialized before it can be used again. [ return to top ] If a DMA BD size 0 error occurs, i.e., DMAERR[BDSZ] is set, to indicate that the buffer descriptor field BD_SIZE is cleared, how can I tell which DMA channel is associated with the error? The DMAERR register does not indicate which channel accessed the BD with size 0. However, you can check the DMACHCRx registers to determine which channel did not finish the transfer by checking if the active ACT bit is high. A channel that does not encounter the error will finish (ACT bit gets cleared). [ return to top ] .
查看全文
See a demonstration of PEG Software to develop graphical user interfaces (GUI) for consumer, industrial and automotive display applications.
查看全文
See an overview of PEG software for developing graphical user interfaces (GUI) for consumer, industrial and automotive display applications.
查看全文
The following wikis provide useful “how to” and FAQ information not available on Freescale websites or forums. The links below provide useful design resources for product designers and users. eGUI PEG GUI StarCore DSPs
查看全文
The PEG GUI wiki provides useful “how to” and FAQ information not available on Freescale websites or forums. The links listed below provide useful design resources for product designers and users. PEG GUI discussions under Freescale Other Solutions in the Freescale Community (all spaces) PEG GUI videos PEG GUI FAQ Website
查看全文