Subject: Info on
FET BUK7909-75AIE
Description: The
datasheet for part number BUK7909-75AIE
describes it as qualified to AEC standard for use in automotive critical
applications. It also says it is Q101
compliant. We are not familiar with
these automotive standards but would like to know if samples have been tested
for either these or similar qualification tests:
Lifetesting
Tempeature Cycling
HAST or 85/85.
I am expecting the automotive qual to meet or exceed
these requirements, but need to be sure that device samples or devices from the
same process have had qualification testing performed. Please comment.
Also, we need to know if there is an MSL rating for this
part? Finally, what is the terminal
finish? What is the long-term
availability. WE are looking to use
these to replace an obsolete FET from IR/Infineon, and we want to be sure it
will remain available.