NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
This video demonstrates how to: SPI Master configuration SPI Slave configuration Ping-Pong data message Data visualization via FreeMASTER
View full article
  1 Every great build starts with "Hello World" Every engineer remembers their first “Hello World” — that small, satisfying moment when an idea typed on a screen suddenly comes to life on a real machine. This series is a take on that same feeling, only this time the “machine” is a car. It’s a demonstrator that looks and behaves like a real vehicle, showcasing the combined use of tools from both the NXP and MathWorks ecosystems. This demo has been showcased at several events, including most recently at the MathWorks booth during Embedded World 2026 and MathWorks Automotive Conference, where the demo video that accompanies this series was filmed. Think of these articles as a guided tour through how the whole thing comes together, piece by piece. ▶ Watch the demo in action — presented at the MathWorks booth, Embedded World 2026 2 Table of Contents • Every great build starts with Hello World • From a model on a laptop to silicon on the bench • From the steering wheel to every node • And it grew up along the way • Built to be rebuilt — and learned from • A demonstrator, not a blueprint • The article series — one domain at a time 3 From a model on a laptop to silicon on the bench How does a car end up running on NXP silicon, starting from a model on a laptop? That’s where the NXP Model-Based Design Toolbox (MBDT) comes in. It acts as the bridge between the MathWorks ecosystem — Simulink and MATLAB — and NXP’s processors and embedded tools. An application is designed and modeled in Simulink, MBDT generates optimized code for the chosen NXP target, and that code is deployed straight onto the hardware. The main advantage of this approach is what it allows before any board is involved: an application can be validated and tuned in simulation first, and hardware that isn’t physically present can simply be simulated in its place. The results: early issue detection, shorter development cycles, and a faster time to market — backed by a toolchain that has been validated end to end. NXP Model-Based Design Toolbox One Pager Figure 1. NXP Model-Based Design Toolbox One Pager 4 From the steering wheel to every node At the heart of the demo is a driver-in-the-loop setup: a physical steering wheel and a set of foot pedals feed signals directly into the simulation, where a virtual car is driven in simulation, into an environment developed through a RoadRunner simulated environment. From there, a clear hierarchy carries every input down to the hardware. The main node — an S32N processor — sits at the center: it communicates with the host PC running the simulation and makes the vehicle-level decisions. It then hands those decisions to a zonal node that acts as a gateway, fanning the signals out to the end nodes that handle each function — the front and rear lights, the front and rear parking sensors, the radar, and the steering rack, and, on the traction side, the battery management system and motor control. The effect is immediate and physical: steering and acceleration in the virtual world set the model on the table moving; shifting into reverse spins the motors up in the right direction; and when an obstacle appears behind the physical car, it stops on its own, with the rear lights turning red across every node — just like a production vehicle. Throughout, a live dashboard built with NXP’s FreeMASTER Lite shows the vehicle state as it happens, from the reverse camera to the parking sensors, blending signals from the virtual world with readings from the physical hardware. Figure 2. Demo architecture — main node (S32N), zonal gateway, and end nodes. 5 And it grew up along the way Behind all of these are the core functions of a real car — lighting, parking sensors, steering rack, motor control, and battery management — spread across roughly ten microcontrollers and processors and sixteen NXP evaluation boards and reference designs. There’s no need to unpack every component here, because each one earns its own dedicated article series later on. What’s worth knowing is how it all grew: this didn’t start as today’s car. It began as a battery management system (BMS), then gained cloud connectivity, then motor control — which evolved into a full traction inverter demo — and from there the remaining vehicle domains, from body and lighting to chassis and parking, were layered on one by one until it became a complete vehicle topology. In other words, existing MathWorks and model-based examples were assembled, domain by domain, into a car. 6 Built to be rebuilt — and learn from Why go to all this trouble? Mostly to document the work, share the thinking behind it, and show how to actually use MBDT. A big part of the appeal is that everything runs on NXP evaluation boards, which means the whole thing can be reproduced. There’s no need to redo a complex custom hardware design before starting; the same boards can be picked up to get going right away. That also makes the demo a hands-on learning platform: a place to explore the model-based workflow by doing one domain at a time. Note: A word on scope — this is a proof of concept that demonstrates the development workflow, not production firmware as it stands today. A great path forward is NXP’s CoreRide, which you can read more about on this page: Software-Defined Vehicle Development: NXP CoreRide Platform — but that part will not be covered in this series. Whether the field is automotive, electrification, industrial automation, or robotics — or simply an interest in model-based development — there should be something here worth taking away. 7 A demonstrator, not a blueprint One last note on how to read all of this. This car is a demonstrator, not a reference design. It was built with the hardware that happened to be on hand, so some of the boards and NXP solutions used aren’t necessarily the optimal fit for a given function — for a specific job, a different microcontroller might serve better. The point was never to say “use exactly these parts.” The point is the steps and the approach: the workflow itself, and how the pieces fit together. With that in mind, the articles below each take a part of this build and show how it’s done. Welcome to “Hello World” with the Model-Based Design Toolbox. 8 The article series — one domain at a time Each part of the demo car gets its own dedicated write-up, grouped into the twelve tracks below. As articles go live, the placeholders will be replaced with links. Bookmark this page — it will keep growing. NXP MBDT — How-To & Introduction What is Model-Based Design Toolbox? How to install Model-Based Design Toolbox? MBDT Setup and How-to run an application Develop an MBDT application workflow Create a new model and configure it for NXP Hardware Create a new configuration project using the S32CT How to MBDT Dio Port/Pins FreeMASTER & FreeMASTER Lite Introduction to FreeMASTER Using FreeMASTER block in Simulink Visualize and control variables in FreeMASTER Create web dashboard with FreeMASTER Lite Parking sensors Overview SW & HW Environment Logic Control (Main model overview) Front & Rear Lights System Overview SW & HW Environment Logic Control (Main model overview) Motor Control Overview SW & HW Environment Logic Control Architecture (Main model overview) Battery Management Systems Overview SW & HW Environment Logic Control (Main model overview) Steering Overview SW & HW Environment Logic Control (Main model overview) Radar Overview SW & HW Environment Processing Chain - NXP Radar SDK Main Node Overview SW & HW Environment Logic Control (Main model overview) Zone Node Overview SW & HW Environment Logic Control (Main model overview) Software & Integration Creating virtual vehicle with MathWorks Overview SW & HW Environment Logic Control Creating Virtual Scenes & Scenarios with MathWorks (RoadRunner & Unreal Engine)  Processor-in-the-Loop (PIL) What is next? Export to & Debug generated code to S32 Design Studio IDE Other Guides Getting Started with FRDM-A-S32K312 using Model-Based Design  A1: Interacting with Digital Inputs Outputs on MR-CANHUBK344 A2: Sending data via UART and monitoring signals with FreeMASTER A3: Controlling LED intensity with ADC and PWM A4: Communicating over the CAN Bus   Note: This index is updated as new articles are published.
View full article
Introduction The following article shows a basic configuration and model for S32K396BMS-EVB that configures the SPI to communicate with the MC33CD1030 MSDI IC mounted on the evaluation board.   Prerequisite software The following software tools were used to develop and deploy the application onto the S32K396BMS-EVB board. MATLAB® R2024b or later Simulink ® MATLAB ® Coder™ Simulink ® Coder™ Embedded Coder ® Support Package for ARM ® Cortex ® -M Processors S32K3 MBDT Toolbox Version 1.4.0 BMS MBDT Toolbox Version 1.2.0 FreeMASTER Run-Time Debugging Tool   Prerequisite hardware The application is developed for the following hardware*: S32K396BMS-EVB Debug probe (used to deploy the example and to connect the FreeMASTER application to the board) 12V power supply   Configuration project In this chapter, I show most important settings that must be to allow the MCU to enter standby mode and to be able to wake up and switch to RUN mode again. For more details, please download the files attached and consult the configuration project.   Pins configuration   For the CD1030, only the SPI pins must be configured; LPSPI3 PCS1: PTF18 (OUTPUT) LPSPI3 CLOCK: PTF13 (OUTPUT) LPSPI3 SIN: PTF12 (INPUT) LPSPI3 SOUT: PTF15 (OUTPUT)   Figure 1. Configuration Pins tab - LPSPI pins   Peripherals configuration Platform component The interrupt must be configured for the LPSPi3. To configure it, please go to PLATFORM -> Interrupt Controller and add a new entry into the table, as below. Figure 2. Configuration Platform Component - Enable LPSPI3 interrupt   MCU Component The peripheral clock must be enabled and it can be done from the MCU component -> McuModuleConfiguration -> McuModeSettingsConf. Figure 3. Configuration MCU Component - Enable LPSPI3 peripheral clock   SPI Component The MCU communicates with MC33CD1030 over the LPSPI3. First step is to configure the Spi -> SpiGeneral -> SpiPhyUnit Figure 4. Configuration SPI Component - SpiPhyUnit (LPSPI3)   Then, the Spi->SpiDriver must be configured. Important! The frame size of the SPI messages: It must be 32-bit wide and MSB. Figure 5. Configuration SPI Component - SpiChannel   Figure 6. Configuration SPI Component - SpiExternalDevice   Figure 7. Configuration SPI Component - SpiJob   Figure 8. Configuration SPI Component - SpiSequence   Model configuraiton The Simulink model used to communicate with the MC33CD1030 can be seend in the picture below. It can also be found in the achieve attached to this article. The initialization of the model sets the AsyncMode to interrupt. Figure 9. Simulink Model - Initialization subsystem   The application executes the following tasks at each step: Set up the External Buffer for the LPSPI3 SpiChannel_CD1030. The input for the block must be an array of 4 uint8 elements (in total 4 bytes - 32bit). The control word is the last element, while the first 3 elements are the configure words. The Dest Data output is a data story memory configured as uint8 with the size equal to 4.  Send the command to the MC33CD1030 IC and receive the previous result in CD1030_RecvData_SG data store Increment a variable to check that the application is running   Figure 10. Simulink Model - Full Overview   Validation To validate the application, the FreeMASTER tool is used to connect to the board and initiate the sequence to enter standby mode. To connect the board, you can use the LPUART1 (J6 connector), baud rate 115200. If everything is properly configured, in the FreeMASTER you should see the following in the Variable Watch: The SPI_SetAsyncMode_Status, CD1030_SetupEB_Status and SPI_Transmit_Status should all be 0. The CD1030_RecvData_SG (BIN) and CD1030_RecvData_SG (HEX) should display the content of the CD1030's register 0x3E Read switch status registers SG. The step_counter should increment at each step execution. Figure 11. FreeMASTER Project - Variable Watch   To test that the CD1030 is working, I connect the J10_6 (SG0 - KEY_ON_DIN) to either GND or VCC and we can see that the last bit of the register changes.  Figure 12. FreeMASTER Project - J10_6 connected to GND  Figure 13. FreeMASTER Project - J10_6 connected to VCC   Conclusion   In this article, I presented a basic implementation that allows the S32K396 communicate with the MC33CD1030 IC over the SPI. For further details, please consult the MC33CD1030 reference manual.
View full article
Table of Contents 1. Introduction 2. Requirements 2.1 Software Required 2.2 Hardware Required 3. NXP Account Login 4. Installation 4.1 PEmicro Driver Installation 4.2 FreeMASTER Installation 4.3 MATLAB® Installation 4.4 MATLAB® Add-Ons Installation 4.5 MBDT for S32K3 v1.8.0 Installation 5. Running a Demo from the MBDT Examples for S32K3 6. Running a Motor Control Demo using MBDT 7. Conclusion 1. Introduction This article aims to help new users prepare and install the necessary software and hardware to use the FRDM Automotive S32K312 with the latest  Model-Based Design Toolbox for S32K3 version 1.8.0. Note: These steps can also be followed with any NXP Evaluation Board from the supported list referenced in the toolbox documentation. S32K312MINI‑EVB Renamed to FRDM‑A‑S32K312: Now part of the FRDM Automotive Ecosystem under its new name, the board keeps the same hardware and adds full ecosystem compatibility for flexible, scalable development.     2. Requirements   2.1 Software Required MATLAB® R2023b or later, with the following Add-ons: AUTOSAR Blockset Embedded Coder Support Package for ARM Cortex-M Processors Motor Control Blockset NXP_Support_Package_S32K3 Stateflow NXP Model-Based Design Toolbox for S32K3 version 1.8.0 FreeMASTER Run-Time Debugging Tool PEmicro Hardware Interface Drivers   2.2 Hardware Required FRDM-A-S32K312 Development Board MCSPTE1AK344 Motor Control Kit, which includes: Sunrise motor  DEVKIT-MOTORGD  12V power supply USB Type-C cable   3. NXP Account Login Open Software Licensing: Support, make sure you are logged into your NXP Account, and select: Click on My NXP Account. Select Software Licensing and Support. Then click on View accounts: These steps will ensure that you are properly authenticated with your NXP Account before proceeding with step 4.5 MBDT for S32K3 v1.8.0 Installation. Keep the page open for the login to persist.   4. Installation Note: Before proceeding, make sure you have full access to your PC or Laptop. Some installers require local admin rights. Contact your IT department to assist you with installation.   4.1 PEmicro Driver Installation After downloading the PEmicro Hardware Interface Drivers: Open the installer package and select the default Destination Folder: Click on Install and then wait for it to finish successfully. Connect the USB cable to your PC and the FRDM Automotive S32K312 board: Open Device Manager to check OpenSDA and the COM port number. OpenSDA - CDC Serial Port → note this COM port number: Note: The COM port number may differ on your system.   4.2 FreeMASTER Installation Download the  FreeMASTER Run-Time Debugging Tool:   Open the installer FMASTERSW32.exe Click Next, then select all available products: Use the default installation path: C:\NXP\FreeMASTER 3.2 Wait for the installation to complete.   4.3 MATLAB® Installation First, check whether MATLAB® R2023b or later is already installed. If so, you can skip this section. For this tutorial, MATLAB® R2025b is downloaded from MathWorks®: Download the matlab_R2025b_Windows.exe (246 MB) file. A MathWorks® Account login is required. After signing in, select the installation directory; the default is C:\Program Files\MATLAB\R2025b For minimum requirements, install the following products: MATLAB® Simulink® AUTOSAR Blockset Embedded Coder MATLAB® Coder Motor Control Blockset Simulink® Coder Stateflow By default, Select All is enabled during install: Wait for the installation to finish. After installation, open MATLAB® and change the default Add-ons path to a shorter path such as C:\MathWorks .   4.4 MATLAB® Add-Ons Installation Open Add-On Explorer and install: Embedded Coder Support Package for ARM Cortex-M Processors NXP Support Package for S32K3 (NXP_Support_Package_S32K3)   4.5 MBDT for S32K3 v1.8.0 Installation After installing the support package, run the following command in MATLAB®: sp_s32k3.nxp.setup(); Select version 1.8.0; the installer will check prerequisites: If any toolboxes are missing, install them before continuing. Click Download to proceed. The Download button opens the Software Terms and Conditions dialog; if the page is not loading properly, follow the steps in 3. NXP Account Login. After reading, click I Agree. Download the SW32_MBDT_S32K3_1.8.0_D2512.mltbx file (approx. 1.6 GB): Once the download completes, browse to the location of the SW32_MBDT_S32K3_1.8.0_D2512.zip file: Click Install to proceed and accept the license agreement. After a few minutes, the dialog will display: Installation successfully completed! Click Next. Select an option such as Open S32K3 Root Folder. MATLAB®'s current folder will change to the root of the toolbox. Click Finish to close the installer. The current folder in MATLAB® is now C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K3 :     5. Running a Demo from the MBDT Examples for S32K3 Navigate to C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K3\S32K3_Examples\demos\s32k3xx_uart_leds_s32ct Open the model s32k3xx_uart_leds_s32ct.mdl . Click on Hardware Settings: Go to Hardware Board Settings → Hardware → Select Configuration Project Template: For the FRDM-A-S32K312 select Custom: S32K312MINI-EVB S32 Config Tool. A Warning Dialog will appear; click OK. Wait for the configuration update to complete. Click on Apply and close the Configuration Parameters window. Press Build, Deploy & Start (CTRL+B) to generate the code: After the build completes successfully, the executable is downloaded to the board. Open a terminal application and connect to the board's COM port at 115200 baud: Pressing r, g, or b on the keyboard toggles the corresponding RGB LED on the board.   6. Running a Motor Control Demo using MBDT Navigate to C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K3\S32K3_Examples\mc\PMSM Open the folder s32k312_mc_pmsm_2sh_s32ct : Open the model s32k312_mc_pmsm_2sh_s32ct.mdl : Press Build, Deploy & Start (CTRL+B) to generate the code. After the executable file is downloaded to the board: Disconnect the FRDM-A-S32K312 board from the PC. Insert the DEVKIT-MOTORGD on top of the FRDM-A-S32K312, ensuring proper pin alignment. Plug in the 12V power supply to the DEVKIT-MOTORGD. Reconnect the USB Type-C cable to the FRDM-A-S32K312.  The RGB LED and User Buttons are on the top side, the Reset Button is on the left side, while the 12V power, Motor Phases, and USB Type-C are on the right side.    Open FreeMASTER s32k312_mc_pmsm_2sh_s32ct.pmpx : Press GO to connect at 115200 baud. In the App Control tab, press On and set Speed Required to 1000 RPM: Apply a small mechanical load to the motor (friction force to the motor shaft) and observe the iABC currents. Here is a short video with the steps above explained:   7. Conclusion These steps conclude the Getting Started with FRDM Automotive S32K312 using the Model-Based Design Toolbox guide. For more details, refer to: s32k312_mc_pmsm_2sh_s32ct_example_readme.html The corresponding example_readme.html for the selected model. Thank you for your time, Stefan V.
View full article
  Product Release Announcement Analog & Automotive Embedded Systems NXP Model-Based Design Toolbox for S32K3 – version 1.7.0 img_0-1713952962606.png     The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3 version 1.7.0. This release supports automatic code generation for S32K3 peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3 Automotive Microprocessors. This new product adds support for S32K310, S32K311, S32K312, S32K314, S32K322, S32K324, S32K328, S32K338, S32K341, S32K342, S32K344, S32K348, S32K358, S32K364, S32K366, S32K374, S32K376, S32K388, S32K394 and S32K396 MCUs, and part of their peripherals, based on RTD MCAL components (ADC, CAN, DIO, FEE, GPT, I2C, ICU, LIN, MEM, MCL, PWM, SPI, UART), and support for the GD3162 Gate Driver based on the S32K396 GD3162 Software. In this release, we have also updated the RTD, S32 Configuration Tools, AMMCLib, FreeMASTER, and MATLAB support for the latest versions. The product comes with over 180 examples, covering all the features and functionalities of the toolbox, including new demos for motor control applications.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=7608021   Technical Support: NXP Model-Based Design Toolbox for S32K3 issues will be tracked through the NXP Model-Based Design Tools Community space.   Release Content: Automatic C code generation from MATLAB® for NXP S32K3 derivatives: S32K310 S32K311 S32K312 S32K314 S32K322 S32K324 S32K328 S32K338 S32K341 S32K342 S32K344 S32K348 S32K358 S32K364 S32K366 S32K374    S32K376    S32K388    S32K394  S32K396   Support for the following peripheral components and functions: ADC CAN DIO eTPU FEE GD3162 GPT I2C ICU LIN MCL (including DMA support) MEM Memory read/write PWM Profiler Registers read/write SPI UART   New RTD version supported (6.0.0)   Integrates S32K396 GD3162 v2.0.2 The toolbox enables access to the GD3162 gate driver for S32K396 derivatives from Simulink models, by delivering a library block (Gd3162) that generates code on top of GD3162 components API.   New S32 Configuration Tools version supported (2024.R1.8)😎   Integration with EB tresos v29.0.0   Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB tresos to configure peripherals/pins/clocks   Default Configuration Project Templates targeting all the supported S32K3 derivatives The toolbox delivers default configuration projects, available in both S32 Configuration Tools and EB tresos, covering an initial enablement of the on-board peripherals, pins, and clocks, for all the supported S32K3 derivatives. The desired template, which represents the starting point for enabling the hardware configuration of the application, can be selected via a dropdown widget.   Support for creating and using Custom Project Templates The toolbox provides support to use and create custom project templates. This could be very useful when having a custom board design – offering the possibility to create the configuration for it only once. After it is saved as a custom project template, it can be used for every model that is being developed.   Such custom projects, addressing specific hardware designs are offered inside the current version of the toolbox to integrate the following EVBs: MCTPTX1AK324 S32K344-WB S32K396-BGA-DC1 MR-CANHUBK344, alongside a set of examples specifically created to target this hardware design and a series of articles (available on NXP Community) demonstrating how to use the toolbox features and functionalities for creating applications for custom boards.   The toolbox has been tested and validated on the official NXP Evaluation Boards     S32K31XEVB-Q100     S32K312EVB-Q172     XS32K3X2CVB-Q172     XS32K3X4EVB-Q257     XS32K3XXEVB-Q172     MR-CANHUBK344             S32K3X4EVB-T172      S32K344-WB        XS32K3X8CVB-Q172     S32K388EVB-Q289             XS32K396-BGA-DC     XS32K396-BGA-DC1   Integrates the Automotive Math and Motor Control Library release 1.1.41 All functions in the Automotive Math and Motor Control Functions Library v1.1.41 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   S32 Design Studio integration We provide the feature of importing the code generated from a Simulink model inside the S32 Design Studio IDE. This functionality can be useful if the model needs to be integrated into an already existing project or for debug purposes.   Simulation modes We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) including AUTOSAR SW-C deployment External mode   GD3162 Applications To demonstrate the integration and support of the GD3162 gate driver IC, we have included a reference Simulink application that configures six GD3162 devices in   a daisy-chain topology using SPI communication. The setup enables sequential initialization, configuration, and status monitoring of each GD3162 device using the S32K396 as a controller MCU.   Motor Control Applications The toolbox provides examples for 1-shunt and 2-shunt PMSM and BLDC motor control applications, supporting both S32 Configuration Tools and EB  tresos. Each of the examples provides a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. The toolbox also demonstrates the integration of the Motor Control Blockset in developing such applications.   For demonstrating the S32K3 eTPU Software integration, we have included a PMSM application where the FOC algorithm runs on the main CPU of the S32K396 MCU, while the analog sensing, software resolver, and PWM signals generation are offloaded to the eTPU co-processor.   The motor control applications were developed and validated on the MCSPTE1AK344 and MCSPTR2AK396 Motor Control kits.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b R2025a   Examples for every peripheral/function supported More than 180 examples showcasing: I/O Control Timers and scheduling Communication (CAN, I2C, LIN, SPI, UART) Memory handling Motor Control applications (BLDC and PMSM) AMMCLib FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3 MCUs and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for S32K3 version 1.7.0 is fully integrated with MATLAB® environment.   Target Audience: This release (1.7.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3 MCUs and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
  Product Release Announcement Automotive Embedded Systems NXP Model-Based Design Toolbox for S32K3 – version 1.6.0 img_0-1713952962606.png     The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3 version 1.6.0. This release supports automatic code generation for S32K3 peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3 Automotive Microprocessors. This new product adds support for S32K310, S32K311, S32K312, S32K314, S32K322, S32K324, S32K328, S32K338, S32K341, S32K342, S32K344, S32K348, S32K358, S32K364, S32K366, S32K374, S32K376, S32K388, S32K394 and S32K396 MCUs, and part of their peripherals, based on RTD MCAL components (ADC, CAN, DIO, FEE, GPT, I2C, ICU, LIN, MEM, MCL, PWM, SPI, UART), and support for the eTPU co-processor based on the S32K3 eTPU Software. In this release, we have also updated the RTD, S32 Configuration Tools, AMMCLib, FreeMASTER, and MATLAB support for the latest versions. The product comes with over 180 examples, covering all the features and functionalities of the toolbox, including new demos for motor control applications.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=6626551   Technical Support: NXP Model-Based Design Toolbox for S32K3 issues will be tracked through the NXP Model-Based Design Tools Community space.   Release Content: Automatic C code generation from MATLAB® for NXP S32K3 derivatives: S32K310 S32K311 S32K312 S32K314 S32K322 S32K324 S32K328 S32K338 S32K341 S32K342 S32K344 S32K348 S32K358 S32K364 S32K366 S32K374    S32K376    S32K388    S32K394  S32K396   Support for the following peripheral components and functions: ADC CAN eTPU DIO FEE GPT I2C ICU LIN MEM MCL (including DMA support) PWM SPI UART Memory read/write Registers read/write Profiler   New RTD version supported (5.0.0)   Integrates S32K3 eTPU Software v2.0.0 CD01 The toolbox enables access to the eTPU co-processor of the S32K36x/S32K39x derivatives from Simulink models, by delivering a library of blocks that generate code on top of eTPU components APIs: Etpu MotorControl Rdc_Checker   New S32 Configuration Tools version supported (2024.R1.7 Update 😎😎   Integration with EB tresos v29.0.0   Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB tresos to configure peripherals/pins/clocks   Default Configuration Project Templates targeting all the supported S32K3 derivatives The toolbox delivers default configuration projects, available in both S32 Configuration Tools and EB tresos, covering an initial enablement of the on-board peripherals, pins, and clocks, for all the supported S32K3 derivatives. The desired template, which represents the starting point for enabling the hardware configuration of the application, can be selected via a dropdown widget.   Support for creating and using Custom Project Templates The toolbox provides support to use and create custom project templates. This could be very useful when having a custom board design – offering the possibility to create the configuration for it only once. After it is saved as a custom project template, it can be used for every model that is being developed.   Such custom projects, addressing specific hardware designs are offered inside the current version of the toolbox to integrate the following EVBs: S32K344-WB S32K396-BGA-DC1 MR-CANHUBK344, alongside a set of examples specifically created to target this hardware design and a series of articles (available on NXP Community) demonstrating how to use the toolbox features and functionalities for creating applications for custom boards.   The toolbox has been tested and validated on the official NXP Evaluation Boards     S32K31XEVB-Q100     S32K312EVB-Q172     XS32K3X2CVB-Q172     XS32K3X4EVB-Q257     XS32K3XXEVB-Q172     MR-CANHUBK344             S32K3X4EVB-T172      S32K344-WB        XS32K3X8CVB-Q172     S32K388EVB-Q289             XS32K396-BGA-DC     XS32K396-BGA-DC1   Integrates the Automotive Math and Motor Control Library release 1.1.39 All functions in the Automotive Math and Motor Control Functions Library v1.1.39 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   S32 Design Studio integration We provide the feature of importing the code generated from a Simulink model inside the S32 Design Studio IDE. This functionality can be useful if the model needs to be integrated into an already existing project or for debug purposes.   Simulation modes We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) including AUTOSAR SW-C deployment External mode   Motor Control Applications The toolbox provides examples for 1-shunt and 2-shunt PMSM and BLDC motor control applications, supporting both S32 Configuration Tools and EB  tresos. Each of the examples provides a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. The toolbox also demonstrates the integration of the Motor Control Blockset in developing such applications.   For demonstrating the S32K3 eTPU Software integration, we have included in this release a PMSM application where the FOC algorithm runs on the main CPU of the S32K396 MCU, while the analog sensing, software resolver, and PWM signals generation are offloaded to the eTPU co-processor.   The motor control applications were developed and validated on the MCSPTE1AK344 and MCSPTR2AK396 Motor Control kits.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b   Examples for every peripheral/function supported More than 180 examples showcasing: I/O Control Timers and scheduling Communication (CAN, I2C, LIN, SPI, UART) Memory handling Motor Control applications (BLDC and PMSM) AMMCLib FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3 MCUs and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for S32K3 version 1.6.0  is fully integrated with MATLAB® environment.   Target Audience: This release (1.6.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3 MCUs and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
    Product Release Announcement Automotive Embedded Systems NXP Model-Based Design Toolbox for S32Z/E – version 1.3.0   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32Z/E version 1.3.0. This release supports automatic code generation for ARM Cortex-R52 and DSP/ML processor cores from MATLAB and Simulink for NXP S32Z/E Automotive Real-Time Processors. This new release supports S32Z/E2 families and its cores (Real-Time ARM Cortex-R52 cores and DSP/ML processor). It also supports Multicore, 41 Operators highly optimized for DSP/ML processor, Processor-in-Loop Simulation mode, RTD components (ADC, PWM, DIO, CAN, UART, GPT), FreeMASTER, AMMCLib, and execution profiling. The product comes with 120 examples, covering all DSP/ML processor Operators and demonstrating the usage of the peripherals (e.g.: I/O control, timers and scheduling, communication) and multicore concurrent execution.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=6450481   Technical Support: NXP Model-Based Design Toolbox for RADAR issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content: Automatic C code generation from MATLAB® for NXP S32Z2/E2 packages, including rev. B0 S32E2xx-bga975 S32Z2xx-bga594 S32Z2xx-bga400 Automatic C code generation from MATLAB® for NXP S32Z2/E2 cores ARM Cortex-R52 Cluster 0 and Cluster 1 cores DSP/ML processor Multicore support using Concurrent Execution from Simulink Homogeneous multicore execution between ARM Cortex-R52 Cluster 0 and Cluster 1 cores using IPCF Heterogenous multicore execution between ARM Cortex-R52 Cluster 0 Core 0 and SPF2 core using OpenAMP MCAL components supported (based on RTD version 2.0.0) ADC PWM DIO CAN UART GPT Software-in-the-Loop and Processor-in-the-Loop (SIL/PIL) simulation modes MATLAB scripts   Simulink models Includes MATLAB API and Simulink Library blocks for the 41 Operators highly optimized for DSP/ML processor Includes AMMCLib (v1.1.38) blocks and examples FreeMASTER support and examples Support for MATLAB versions: R2022a R2022b R2023a R2023b R2024a 120 examples: 41 Operators for DSP/ML processor Multicore I/O control Timers and scheduling Communication (CAN) SiL, PiL FreeMASTER   For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® experience by allowing customers to evaluate and use ARM Cortex-R52 cores and DSP/ML processor from NXP’s S32Z/E Realt-Time Processors and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for S32Z/E version 1.3.0 is fully integrated within MATLAB® environment.   Target Audience: This release (1.3.0) is intended for technology demonstration, evaluation purposes, and prototyping on NXP S32Z/E Real-Time Processors and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
  Product Release Announcement Automotive Embedded Systems NXP Model-Based Design Toolbox for S32M2 – version 1.1.0   The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32M2 version 1.1.0. This release supports automatic code generation for S32M2 peripherals and applications prototyping from MATLAB/Simulink for NXP S32M2 Automotive Microprocessors. This product adds support for S32M41, S32M242, S32M43, S32M244, S32M274, S32M276 MCUs and part of their peripherals, based on RTD MCAL components (ADC, AE, DIO, CAN, Can_Trcv, DPGA, GDU, GPT, LIN, LIN_Trcv, MCL, PWM, MCL, MCU, PORT, QDEC, SPI, UART). In this release, we have also added support for FreeMASTER, AMMCLib, and MATLAB support for the latest versions. The product comes with over 85 examples, covering all supported peripherals, and Simulink simulation modes Software-in-the-Loop, Processor-in-the-Loop, and External Mode. Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=6481361 Technical Support: NXP Model-Based Design Toolbox for S32M2 issues will be tracked through the NXP Model-Based Design Tools Community space. Release Content: Automatic C code generation from MATLAB® & Simulink® for NXP S32M2 derivatives: S32M241 S32M242 S32M243 S32M244 S32M274 S32M276 Support for the following peripherals (MCAL components): ADC AE CAN CAN_Trcv DIO DPGA GDU GPT ISR LIN LIN_Trcv MCL MCU MEMORY PROFILER PWM PORT QDEC SPI UART Profiler in PIL mode Provides 2 modes of operation Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tool or EB Tresos to configure peripherals/pins/clocks Provides Motor Control examples MBDT for S332M2 1.1.0 provides examples for PMSM sensorless, open loop and closed-loop hall sensors motor control applications, supporting S32 Configuration Tools. Each of them has a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. Integrates the Automotive Math and Motor Control Library version 1.1.38 All functions in the Automotive Math and Motor Control Functions Library v1.1.38 are supported as blocks for simulation and embedded target code generation. Integration with FreeMASTER MBDT for S332M2 1.1.0 delivers several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications. Support for Custom Default Project MBDT for S332M2 1.1.0 provides support for users to create their own custom default project. This could be very useful when having a custom board design – the configuration for it needing to be created only once. After that configuration is saved as a custom default project, it can be used for other models that are developed. Support for custom board initialization MBDT for S332M2 1.1.0 generates the components’ peripherals initialization function calls as configured in the Board Initialization window, which can be customized to each Simulink model. This feature allows users to set a custom order for the components initialization, the insertion of the Custom code sequences, or share the custom initialization with multiple Simulink models via the Export and Import functionality. Integration with S32 Config Tools version v1.7 Integration with S32 Design Studio MBDT for S332M2 1.1.0 automatically generates the <model_name>_Config folder, next to the Simulink model location, providing user the opportunity to easily import the generated code from Simulink into S32 Design Studio. Each time the code is generated, the  <model_name>_Config folder is updated with the new changes. Toolbox also provides a mechanism to launch an S32 Design Studio instance, with the imported generated code project in the Project Explorer tab from S32DS. Simulation modes       Toolbox provides support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode      Support for application execution profiling Custom Linker File and Startup Code Users can choose to use custom files for this process, from the Build Options group which can be found in the Target Hardware Resources, as illustrated in the image below. Examples for every peripheral/function supported       We have added over 60 examples, including: CDD Blocks (Ae, Dpga, Gdu, Mcl, Qdec) Communication (Can, Lin, Spi, Uart) AMMCLib IO Blocks (Adc, Dio, Pwm) ISR Blocks (Hardware Interrupt Handler) MCAL Blocks (Gpt) Utility Blocks (FreeMASTER, Memory, Profiler, Registers) Software-in-the-Loop / Processor-in-the-Loop / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached. MATLAB® Integration Support for MATLAB® versions R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b   The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32M2 MCUs and evaluation board solutions out-of-the-box with:   Target Audience This release (MBDT for S32M2 1.1.0) is intended for technology demonstration, evaluation purposes, and prototyping of S32M2 MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt DEMO Motor Control Rapid Prototyping on NXPs S32M2 with MathWorks and the Model-Based Design Toolbox This training shows how to design and develop motor control algorithms with Simulink® (MathWorks) and the Model-Based Design Toolbox for S32M2. Presentation introduces NXP’s S32M2 family, an integrated solution for 12V Motor Control and show how to access and configure the MCU peripherals making the Simulink® model hardware-aware and ready to generate, build and deploy the application on the target. The FreeMASTER software tool is used to control and monitor the algorithms running on the S32M2. First application focuses on a simple scalar control (also known as open-loop control or Volts per Hertz control) algorithm for a permanent magnet synchronous motor (PMSM). Second application shows how MATLAB and Simulink works together with the MBDT for S32M2 focusing on a workflow of implementing a predictive maintenance motor control application. Toolbox is used to acquire data from an accelerometer mounted on the motor. The motor is spinning at various speeds, and the vibrations are monitored using FreeMASTER. Data is transferred to MATLAB, where is preprocessed and a Support Vector Machine is trained. Then the resulted classifier is transferred to Simulink where together with the Model-Based Design Toolbox for S32M2 code is generated and deployed on the MCU. For more details about the demo mentioned above, please check this webinar a full demo description.        
View full article
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for RADAR – version 1.0.0   The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for RADAR version 1.0.0. This release supports automatic code generation for ARM Cortex-A53, NXP SPT Accelerator and NXP LAX Accelerator cores from MATLAB for NXP S32R45 Automotive Microprocessors. This release adds support for code generation and execution on both LAX cores,  OpenMP code generation for parallel execution of for loops, and Processor-in-the-Loop (PIL) simulation, improves the code generation and Radar processing demo, and adds support for new exponential, logarithmic, min, max, and thresholding LAX kernels. The product comes with 60+ examples, covering the supported RSDK SPT and LAX Kernels from MATLAB API and demonstrating the programming of the LAX accelerator from MATLAB environment.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=6450491   Technical Support: NXP Model-Based Design Toolbox for RADAR issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content: Automatic C code generation from MATLAB® for NXP S32R45: ARM Cortex-A53 NXP LAX Accelerator Code generation and execution on both LAX cores Support for execution of RSDK SPT kernels: rangeFFT, dopplerFFT, NonCohComb Support Linux application build and run NXP Auto Linux BSP 37.0 for S32R45 Includes MATLAB API for additional RSDK LAX Kernels highly optimized for LAX accelerator add, sub, mul, div, times, cT, inv abs, abs2, sqrtAbs, conj, norm, norm2 diag, eye, zeros, ones, find, sort exp, log, log2, log10, min, max, thresbit cospi, sinpi, tanpi, cispi, sincpi acospi, asinpi, atanpi, atan2pi Processor-in-the-Loop (PIL) simulation mode Improved code generation and reduced memory usage Support for Radar SDK version 1.2.0 Support for MATLAB versions: R2023a R2023b R2024a R2024b More than 60 examples showcasing the supported functionalities: Cholesky Gauss-Newton Eigen (new) Kalman Filter Linear Regression Large Matrix Multiplication Navier-Stokes QR Factorization (updated) MUSIC DoA (updated) Radar processing demo – Automated Driving Toolbox scenario (updated) Standalone and Processor-in-the-Loop (PIL) simulation Range FFT, Doppler FFT, and Non-Coherent Combining offloaded to NXP SPT accelerator MUSIC DoA offloaded to NXP LAX accelerator     Radar processing demo – RoadRunner Toolbox scenario (new) Processor-in-the-Loop (PIL) simulation     For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® experience by allowing customers to evaluate and use ARM Cortex-R52 core, NXP SPT Accelerator, and NXP LAX Accelerator from NXP’s S32R45 processor and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for RADAR version 1.0.0 is fully integrated with MATLAB® environment.   Target Audience: This release (1.0.0) is intended for technology demonstration, evaluation purposes, and prototyping on NXP S32R45 Processors and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt    
View full article
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.3.0 RFP   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.3.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32R41x, and S32S2xx MCUs. This new product adds support S32R41 Cut 1.1 and S32G3, C++ code generation for S32G2 and S32G3,  Radar examples for S32R41, and support for MATLAB versions R2021a - R2023b for running in Software-in-the-Loop and Processor-in-the-Loop modes.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=3742498   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32G3xx derivatives: S32G399A Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 (including Cut 1.1) Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Supported Evaluation Boards GoldBox 2 Development Platform (S32G-VNP-RDB2 Reference Design Board) GoldBox 3 Development Platform (S32G-VNP-RDB3 Reference Design Board) X-S32R41-EVB Development Board GreenBox 2 Development Platform Support for MATLAB® versions: R2021a R2021b R2022a R2022b R2023a R2023b S32G2 and S32G3 support: SIL and PIL simulation modes with code execution profiling. C++ code generation. S32R41 support: SIL and PIL simulation modes. Code execution profiling using PMU cycle counter. Tools updates: S32 Flash Tool v2.1.4, S32 Debugger v3.5 Includes an Example library with 20+ examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL) MathWorks Automotive Adaptive Cruise Control Using FMCW and MFSK Technology examples ported to S32R41: MSFK Radar Range and Speed Estimation of Multiple Targets FMCW Radar Multiple Targets Range and Speed Estimation       GUI to help you setup the toolbox and the evaluation board:       For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32G3xx, S32S2xx, and S32R41 MCUs and evaluation board solutions out-of-the-box with: Model-Based Design Toolbox for S32M2xx version 1.3.0 is fully integrated with MATLAB® environment in terms of installation:     Target Audience This release (1.3.0 RFP) is intended for technology demonstration, evaluation purposes and prototyping of S32G2xx, S32G3xx, S32R41, and S32S2xx MCUs and Evaluation Boards..   Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt      
View full article
Introduction With the latest advances in microcontrollers, they are getting faster and more efficient, being able to successfully run complex algorithms in a reasonable time. One important category are Artificial Intelligence algorithms. Using both NXP ® and MathWorks ® ecosystem, the steps to deploy an AI algorithm to NXP hardware are simplified and straight forward. The article provides guidance on how to implement a State-of-Charge (SoC) estimation algorithm based on a feedforward deep learning network developed by Mathworks' experts (Battery State of Charge Estimation in Simulink Using Deep Learning Network). The algorithm is then deployed on i.MX RT1060 Evaluation Kit using NXP Model Based Design Toolbox for I.MX RT. As the main objective of the article is to demonstrate how to run an AI algorithm on NXP evaluation board, the example is ran in Processor-in-the-Loop (PIL) simulation mode. This type of simulation represents an important step in the validation process of an algorithm, corner cases can be easily replicated as the input data can be directly loaded from MATLAB's workspace. The execution of the algorithm is done on the microcontroller. For a more detailed overview of the execution of the algorithm, code profiling options can be enabled to generate a report which details execution times.   What BMS is Battery Management System (BMS) is a critical component in battery-driven devices, such as electric vehicles. Their main objective is to ensure that the battery pack remains in an optimal and safe operating mode. At the core of the most tasks, the BMS must compute the State-of-Charge (SoC) estimation. To make a precise estimation, the algorithm requires an accurate model of the actual cells, which are difficult to characterize. An alternative to this approach is to create data driven models of the cell using AI methods such as neural networks.   Deep Learning Toolbox The Deep Learning Toolbox™ developed by Mathworks provides a framework for deep neural networks to be used in algorithms. It enables the user to use convolutional neural networks (ConvNets, CNNs) and long short-term memory (LSTM) networks to perform classification and regression on image, time-series and text data. The network and layer graphs are not mandatory to be created in MathWorks ecosystem, as other frameworks can be used, such as TensorFlow™ 2, TensorFlow-Keras, PyTorch ® .   Prerequisite Software To create, build and deploy a Simulink Model onto the i.MX RT RT1060 EVK, the following software is required: MATLAB R2022a Deep Learning Toolbox Simulink ® MATLAB ® Coder™ Simulink ® Coder™ Embedded Coder ®  Support Package for ARM Cortex-M Processors i.MX RT MBD Toolbox (version 1.3.0)   Prerequisite hardware The hardware required for this example is i.MX RT1060 Evaluation Kit. The i.MX RT1060 crossover MCUs are part of the EdgeVerse™ edge computing platform. The core of the MCU is a Arm ® Cortex ® -M7 core at 600 MHz. The device is fully supported by NXP’s MCUXpresso Software and Tools, a comprehensive and cohesive set of free software development tools.   Model - Overview The BatterySOCSimulinkEstimation model included in the Deep Learning Toolbox computes the SoC estimation using two methods: first method uses a neural network and the second one uses the extended Kalman filter algorithm. By plotting data generated by these two estimations and comparing it to the true values, it is possible to validate that the FNN predicts the SoC with an accuracy of 3 within a temperature range between -10 C and 25 C.   Note! Before making any modification to the model included in the toolbox, it is recommended to create a backup of the example in order to be able to revert to the original state. For this example, the predictions are done on the i.MX RT1060 evaluation board in PIL mode while the Kalman filter is locally computed on the computer. Referenced Model From the original model, the FNN block must be added in a new blank model. As the newly created model is used in a Referenced model, an input port must be added to received data (make sure the Port dimensions is set to 5), and one output port to return the data computed. The other settings for all these 3 blocks can be left default. Next, in the Model Settings the following changes must be made: Hardware Implementation Hardware Board: NXP MIMXRT1062xxxxA Target Hardware Resources Download Type: OpenSDA OpenSDA drive: Click on browse and select the partition assigned to the IMXRT1060 PIL Communication interface: Serial Interface Hardware UART: LPUART1 Serial port: The COM port assigned to the board (it can be found by using Device Manager or by running serialportlist command in MATLAB Command Window) Baudrate: 115200 Code generation Verification Check Enable portable word sizes   Top model Based on the BatterySOCSimulinkEstimation model included in the Deep Learning Toolbox, the FNN block must be removed (either deleted or commented). A ModelReference subsystem must be added to the model. In the Block Parameters of the ModelReference subsystem, select the model created and configured above. Simulation Mode must be set to Processor-in-the-Loop (PIL). Another modification that must be done is the sample time of the nnInput Data Read Memory block which must be changed from 0 (continuous) to -1 (inherited).   Next, in the Model Settings the following changes must be made: Hardware Implementation Hardware Board: NXP MIMXRT1062xxxxA Target Hardware Resources Download Type: OpenSDA OpenSDA drive: Click on browse and select the partition assigned to the IMXRT1060 PIL Communication interface: Serial Interface Hardware UART: LPUART1 Serial port: The COM port assigned to the board (it can be found by using Device Manager or by running serialportlist command in MATLAB Command Window) Baudrate: 115200 Code generation Verification Check Enable portable word sizes   Deployment and validation Now that both models (top model and referenced model) are configured, SIL/PIL manager can be opened from the APPS tab in Simulink. In the SIL/PIL tab, the simulation must be selected to SIL/PIL only (red rectangle) and the System Under Test to Model Blocks in SIL/PIL mode (blue rectangle). Before the simulation is started, the BatterySOCSimulinkEstimation_ini.m script must be executed to load the necessary data into MATLAB's workspace. The script can be found next to the Simulink Model included in the Deep Learning Toolbox. From the top model, the SOC scope can be opened to display the generated data. The simulation can be started from the RUN button within the scope. Note! Diagnostic Viewer can provide important information if there are any errors within the models. If the simulation is successfully deployed on the target, the data plotted into the scope should look like this:   Code profiling Code profiling is an important tool to validate an algorithm as it provides important information about the execution time. The time is measured by the timer configured in Model Settings -> Hardware Implementation -> Hardware board settings -> Target hardware resources -> Profiling Timers. By default, the PIT timer, channel 0, is used. The Code generation can be enabled from Model Settings -> Code Generation -> Verification -> Code execution time profiling -> Measure task execution time. The generated report can either be Coarse (referenced models and subsystems only) or Detailed (all function call sites). When the simulation is completed, a small window is opened. The Profiling report can be opened by clicking on the view the full code execution profiling report.   Conclusion The NXP and Mathworks ecosystems enable the users to deploy an Artificial Intelligence algorithm onto the NXP hardware. In the end, I strongly recommend the users interested in BMS and Artificial Intelligence to watch the Deploying a Deep Learning-Based State-Of-Charge (SOC) Estimation Algorithm to NXP S32K3 Microcontrollers webinar hosted by Javier Gazzarri (MathWorks) and Marius Andrei (NXP).   EdgeVerse and NXP are trademarks of NXP B.V. All other product or service names are the property of their respective owners. © 2023 NXP B.V. Arm, Cortex are trademarks and/or registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere. The related technology may be protected by any or all of patents, copyrights, designs and trade secrets. All rights reserved. PyTorch, the PyTorch logo and any related marks are trademarks of The Linux Foundation. MATLAB, Simulink, Stateflow and Embedded Coder are registered trademarks and MATLAB Coder, Simulink Coder, Deep Learning Toolbox are trademarks of The MathWorks, Inc. See mathworks.com/trademarks for a list of additional trademarks. TensorFlow, the TensorFlow logo and any related marks are trademarks of Google Inc.
View full article
        Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.2.0 RFP       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.2.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32S2xx, and S32R41 MPUs. This new product adds support for new MATLAB versions R2022a and R2022b for running in Processor-in-the-Loop mode.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13897177   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 Supported Evaluation Boards GoldBox Development Platform (S32G-VNP-RDB2 Reference Design Board) GreenBox II Development Platform X-S32R41-EVB Development Board Support for MATLAB versions: R2020a R2020b R2021a R2021b R2022a R2022b Tools update for S32R41: S32 Flash Tool v2.1 S32 Debugger v3.5 Simulation mode: We provide support for Software-in-Loop (SIL) and Processor-in-Loop (PIL) simulation mode with code execution profiling: Includes an Example library with 16 examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL) GUI to help you setup the toolbox and the evaluation board :     For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32S2xx, and S32R41  processors and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for HCP version 1.2.0 (RFP) is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.2.0 RFP) is intended for technology demonstration, evaluation purposes, and prototyping S32G2xx, S32S2xx, and S32R41 and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt    
View full article
        Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.1.0 RFP       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.1.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32S2xx, and S32R41 MPUs. This new product adds support for running Processor-in-Loop and Software-in-Loop simulation on S32R41 (ARM Cortex-A53).   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/product?child_plneID=683951   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 Supported Evaluation Boards GoldBox Development Platform (S32G-VNP-RDB2 Reference Design Board) GreenBox II Development Platform X-S32R41-EVB Development Board Support for MATLAB versions: R2020a R2020b R2021a R2021b Simulation mode: We provide support for Software-in-Loop (SIL) and Processor-in-Loop (PIL) simulation mode with code execution profiling:   Includes the HEV demo (S32G2xx, S32S2xx):   Includes the RADAR demo - MFSK Radar Range and Speed Estimation on Multiple Targets (S32R41), in collaboration with Gamax Laboratory Solutions Kft.:   Includes an Example library with 16 examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL)   GUI to help you setup the toolbox and the evaluation board :     For more details, features and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32S2xx, and S32R41  processors and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for HCP version 1.1.0 (RFP) is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.1.0 RFP) is intended for technology demonstration, evaluation purposes and prototyping S32G2xx, S32S2xx, and S32R41 and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt    
View full article
General Installer and Setup  How to install the license of MBDT for S32K3?  How to setup the S32K344 toolbox and EVB?  How to export the generated code to S32DS3.4? Export generated projects in MBDT for s32k3XX  Programming methods MBDT for S32k3 using P&E Multilink Custom code usage SENT Protocol Support in S32K3 MBDT Custom project usage How to use custom project configuration Sequential reset S32K344-Q172 sequential reset SIL / PIL / External Mode External mode External mode example wouldn't compile after update  S32K3X4EVB-Q257 with MBDT PIL Example: Not able to run Simple PIL S32CT example Peripherals ADC How to add a new ADC channel using the external configuration tool  SPI How to send 32 bit frames  DIO S32K3x4-Q172P_with_MBDT_Blink_Project DIO and PWM configuration issues ICU PWM Duty cycle measurement PWM PWM raising edge and falling edge detection Interrupt based PWM generation CAN FreeMASTER over CAN connection issue  Apps Motor Control SPI configuration MODEL based design tool box- 32 bit instruction (SIMULINK) 
View full article
          Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.1.0 RTM     Austin, Texas, USA December 20, 2021 The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.1.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K344 and S32K312 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A battery cell controller (& MC33664PHY). In this release, we have also added 2 new motor control applications (for both PMSM and BLDC), as well as updated FreeMASTER, AMMCLib, and GCC compiler to the latest versions. The product comes with over 100 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=12920897   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K344 S32K312   Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A battery cell controller & MC33664PHY The toolbox provides support for the MC33775A and MC33664. The MC33775A is a lithium-ion battery cell controller IC designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33664 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high speed isolated communication network. The ready-to-run example provided with the MBDT for S32K3 shows how to communicate between the S32K344 and the MC33775A via the MC33664 transceiver. The MCU configures the battery cell controller to perform Primary and Secondary chains conversion, reads the cell voltages conversion results from the MC33775A, and displays the values to the user over the FreeMaster.     Added new motor control examples The toolbox provides examples for both 3-shunt PMSM and BLDC motor control applications. Each of them has a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization.     Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.     Support for AUTOSAR blockset (SW-C deployment) Updated to the latest version of RTD (v1.0.0) and GCC(v10.2) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.26: All functions in the Automotive Math and Motor Control Functions Library v1.1.26 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a R2021b   S32Design Studio Integration We provide a simple mechanism to let users the opportunity to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.     Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 100 examples, including: Motor control applications (PMSM and BLDC) Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode   For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.1.0 is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.1.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt    
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to S32K3xx Product Family.
View full article
Product Release Announcement EDGE PROCESSING  NXP Model-Based Design Toolbox for i.MX RT Crossover MCUs – version 1.2.0     The Edge Processing Tools Team at NXP Semiconductors is pleased to announce the release of the Model-Based Design Toolbox for i.MX RT 1xxx Series version 1.2.0. This release supports automatic code generation for peripherals and applications prototyping from MATLAB/Simulink for NXP’s i.MX RT 117x, 106x & 101x Series of crossover MCUs.   NXP Download Location https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   MATHWORKS Download Location https://www.mathworks.com/matlabcentral/fileexchange/81051-nxp-support-package-imxrt1xxx   Version 1.2.0 Release Content Automatic C code generation based on MCUXpresso SDK 2.9.1/2.9.2 drivers and MCUXpresso Configuration Tools 9.0 initializations from MATLAB®/Simulink® for: i.MX RT 1176: MIMXRT1176DVMAA,MIMXRT1176AVM8A,MIMXRT1176CVM8A i.MX RT 1175: MIMXRT1175DVMAA,MIMXRT1175AVM8A,MIMXRT1175CVM8A i.MX RT 1173: MIMXRT1173CVM8A i.MX RT 1172: MIMXRT1172DVMAA,MIMXRT1172AVM8A,MIMXRT1172CVM8A i.MX RT 1171: MIMXRT1171DVMAA,MIMXRT1171AVM8A,MIMXRT1171CVM8A i.MX RT 1061: MIMXRT1061CVJ5A,MIMXRT1061CVL5A,MIMXRT1061DVJ6A,MIMXRT1061DVL6A i.MX RT 1062: MIMXRT1062CVJ5A,MIMXRT1062CVL5A,MIMXRT1062DVJ6A,MIMXRT1062DVL6A i.MX RT 1064: MIMXRT1064CVJ5A,MIMXRT1064CVL5A,MIMXRT1064DVJ6A,MIMXRT1064DVL6A i.MX RT 1011: MIMXRT1011CAE4A,MIMXRT1011DAE5A   Multiple options for configuration of MCU packages, Build Toolchain and embedded Target Connections are available via Simulink Model Configuration UI       Multiple MCU peripherals and Drivers supported. The following subsystems highlighted in red as supported in Simulink environments in various forms: blocks, files, options i.MX RT 117x derivatives   i.MX RT 106x derivatives i.MX RT 101x derivatives     Basic and Advanced Simulink Block configuration modes via MCUXpresso Configuration Tools 9.0 UIs for Pins, Clocks, and Peripherals       MATLAB/Simulink versions 2019a – 2021b are supported for Design, Simulation, Code Generation, and Deployment of applications on i.MX RT 117x,106x & 101x Series. Other i.MX RT devices will be supported in future versions of the toolbox. Support for Software-in-Loop (SiL), Processor-in-Loop (PiL), and External Mode; RTCESL – Real-Time Control Embedded Software Motor Control and Power Conversion Libraries (limited support designed for Motor Control applications). A future update will enhance the number of functionalities supported by Simulink.     Simulink Example library with more than 190 models to showcase various functionalities:   Integrated PMSM Motor Control Sensor/Sensor-less application for both IMXRT1060-EVK and IMXRT1170-EVK:     Target Applications with MATLAB/Simulink This release of the Model-Based Design Toolbox can be used to design, build, and test applications from multiple domains: INDUSTRIAL AC Meters Motion Control Robotics HMI SMART CITY/HOME Video Surveillance Identification Appliances Speakers   AUTOMOTIVE HVAC ECU     Target Audience This release is intended for technology demonstration, evaluation purposes, and prototyping for i.MX RT 1xxx MCUs and their corresponding Evaluation Boards: EVK-MIMXRT1170 EVK-MIMXRT1060 EVK-MIMXRT1064 EVK-MIMXRT1010   Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt Technical by System Tools: https://web.microsoftstream.com/channel/618ab630-c8da-4fa8-ade8-5aa70a353124    
View full article
In this video we show how to build, simulate and test a speed estimator based on Hall Sensors for a BLDC motor. The estimator is first tested under Matlab Simulink environment and then ported into the Open Loop Control Simulink model and tested on the MPC5744P Development Kit with FreeMASTER over CAN interface.   We discuss about: - How to compute the speed; - How to build a speed estimator based on Hall sensors; - Step-by-step model building an enhancements; NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows how to navigate within the integration Matlab help for NXP's Model-Based Design Toolbox for S32K1xx. The following items will be highlighted: Getting HELP Open Examples Support via Community
View full article