Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
MCUXpresso Config Tool for MCUXpresso IDE Clone an Example Project from MCUXpresso IDE The following steps will guide you through the manipulation of the general-purpose outputs. The example sets up a CTimer to generate a PWM signal and change between two LEDs. Find the Quickstart Panel in the lower left-hand corner and click on Import SDK example(s) Sabina_Bruce_14-1767120564749.png Click on the FRDM-MCXN947 board to select that you want to import an example that can run on that board, and then click on Next Sabina_Bruce_15-1767120575767.png Use the arrow button to expand the  driver_examples  category, then expand the ctimer examples, click on the check box next to  ctimer_match_interrupt_example  to select it. To use the UART for printing (instead of the default semihosting), Select UART as the SDK Debug Console checkbox under the project options. Then, click on Finish Sabina_Bruce_16-1767120587691.png Click on the  “frdmmcxn947_ctimer_match_interrupt_example”  project in the Project Explorer View and build, compile, and run the demo as described in the previous section Sabina_Bruce_17-1767120603466.png You should see the BLUE and RED LED changing back and forth Terminate the debug session Use MCUXpresso IDE Pins Tools to Modify Example Note: Previously, you had to clone an SDK project like in the previous step. Open the pins tool by selecting “ConfigTools” on the top right hand of the file explorer window and then select “ Open Pins” Sabina_Bruce_2-1767120490131.png The pins tool should now display the pin configuration for the ctimer project Sabina_Bruce_3-1767120490074.png In the Pins view deselect “Show dedicated pins” and “Show no routed pins” checkboxes to see only the routed pins. Routed pins have a check in a green box next to the pin name. The functions selected for each routed pin are highlighted in green Sabina_Bruce_4-1767120490861.png In the current configuration, PIO3_2 and PIO3_3 are routed as the outputs of the CTimer. Let’s add a third Ctimer Match output and enable the Green LED Select “Show no routed pins” to see the other options. To enable the third Ctimer Match Output, browse the column for Ctimer and select and output. In this example, we will select, Ctimer4 Match 2 on PIO3_6. Select the item in the Ctimer column to enable Sabina_Bruce_5-1767120490102.png Now, let’s route the Green LED. In the search box type “green” so that the routed pin for this LED is shown. Finally, click the box under the GPIO column. The box will highlight in green, and a check will appear next to the pin Sabina_Bruce_6-1767120489892.png Next configure the GPIO pin as an output in the “Routing Details” window Sabina_Bruce_7-1767120490064.png Now it’s time to implement these changes into the project by exporting the new updated pin_mux.c and pin_mux.h files that are generated by the Pins tool. Click on Update Project in the menu bar Sabina_Bruce_8-1767120490018.png The screen that pops up will show the files that are changing and you can click on “diff” to see the difference between the current file and the new file generated by the Pins tool. Click on “OK” to overwrite the new files into your project Sabina_Bruce_9-1767120490120.png Let’s add some additional code to the example. Open  simple_match_interrupt.c  file and add the following macros for the third ctimer output. Sabina_Bruce_10-1767120489936.png Add the Green LED functions as well. Sabina_Bruce_11-1767120491994.png Some additional code to be implemented will be the third ctimer’s callback, this can be copied from  ctimer_match1_callback  and modify the content to match2. To be able to visually identify the new ctimer, we will remove one of the previous ctimers as shown Sabina_Bruce_12-1767120492171.png The main function will need to include the initialization of both the Green LED and the Ctimer Sabina_Bruce_13-1767120490811.png Build and download the project as done in the previous section Run the application. You should now see the Green and Blue LED blinking back and forth Terminate the debug session
記事全体を表示
MCUXpresso IDE 25.6 書き込み MCXW716C 失敗:プロセッサはセキュアモードです、EraseSector タイムアウト (6000ms) PC=0xFFFF MCUXpresso IDE 25.6 MCXW716Cへの焼込みに失敗しました:プロセッサはセキュア モードです、EraseSector タイムアウト (6000ms) PC=0xFFFFFFFE、ChecksumSectors Ef(38) 各位、私は MCUXpresso IDE + LinkServer を使用してNXP MCXW716C (パネル: FRDM-MCXW71 / または自研パネル) をダウンロードした際に、次のようなエラー メッセージが発生しました。 软ハードウェア環境 IDE:MCUXpresso IDE 25.6.136 LinkServer: RedlinkMulti ドライバ v25.6 (2025年6月26日 ビルド1017) 调试器:パネルダウンロードMCU-LINK 搭載 (r0E3) CMSIS-DAP V3.117 接続方式:SWD コア片: MCXW716CxxxA システム:Windows [バージョン番号可选] 工程/例:[例 frdmmcxw71_lpi2c_read_fxls896x_accel_value_transfer] 复现步骤 打开工程并通常编译生成 AXF/ELF 点击デバッグ(またはダウンロード/烧录) LinkServer は正常に接続されていますが、消去/書き込み段階で障害が発生しています 关键日志(截取)   プロセッサはセキュアモードです...フラッシュドライバ「ChecksumSectors」のアドレス0x00000000に23936バイトを書き込み中 エラー 'Ef(38): フラッシュ操作でエラーが返されました (ログを参照)' ... ドライバ「EraseSector」タイムアウト (6000 ms) PC: FFFFFFFE 现象说明 チップとフラッシュを正常に認識可能:フラッシュ バリアント「FMU 1MB」が検出されました ただし、プロセッサはセキュアモードです 続いて、フラッシュ ドライバの操作段階でのチェック:ChecksumSectors Ef(38) 最终 EraseSector 擦除扇区超過時間 6000ms 、PC 表示0xFFFFFFFE 我想确认/请教的问题 プロセッサーはセキュア モードになっています。MCXW716C では通常、何を意味しますか? 安全寿命期間/安全構成に入ったことを示し、フラッシュの擦過と调试を制限しますか? このような状況に対して、正しい代替方法は何ですか?大量消去 / 回復 / 安全でないフローが必要かどうか? PC: 0xFFFFFFFE は、フラッシュ ドライバ跑飛/HardFault/调试访问安全ドメイン隔離による「無能 PC」であるかどうかを確認できますか? LinkServer v25.6 + MCXW716C で EraseSector タイムアウトのようなものに遭遇しましたか? 充電可能な情報(必要に応じて) [安全例/TrustZone/セキュア ブート構成を使用するかどうか:是/否/不确定] [コア片は否か曾经烧录过安全相关固片/配置区:是/否/不确定] [谝试过的操作:SWD 周波数の低下、回線/换口、断電重启、按住复位连接続、换 LinkServer バージョン等] 完全な LinkServer ログ / 工程 / 最小复现步骤を提供可能 感大家の指差す。 ボード設計 Re: MCUXpresso IDE 25.6 烧录 MCXW716C 失败:processor is in secure mode,EraseSector timeout(6000ms) PC=0x こんにちは@向明月 セキュアプロビジョニングツールをダウンロードできると思います。 MCUXpresso セキュアプロビジョニングツール | NXP Semiconductors そして、w71 ワークスペースを作成します。 Harry_Zhang_1-1766737112192.png そしてそれを消します。 Harry_Zhang_0-1766737059406.png これがお役に立てれば幸いです。 BR ハリー
記事全体を表示
S32K344 boot跳转APP出现hard fault wzy__1024_0-1766554505966.png 如图所示,使用S32K344产品进行boot跳转App入口地址出现hard fault故障,附件txt为boot和appflash分区的链接文件,压缩包内含有boot和app的map文件以及hex文件,请技术支持帮助看一下问题出在哪里 Re: S32K344 boot跳转APP出现hard fault 你好@wzy__1024 看来你正在跳转到RESET向量所在的地址。但不是指向RESET向量指向的地址: lukaszadrapa_0-1767369649781.png 因此,地址 0x443004 并不是入口点,而是指向入口点的指针。 此致, 卢卡斯
記事全体を表示
零件编号 MMG3014NTl 的标记 亲爱的支持者 MMG3014NTl 的实际标记与数据表不符,在标记中,第二行标记有 7 个字符,而数据表显示只有 6 个字符。请参考随附的照片以供参考。请告知这是否正常和有效。谢谢 Re: Marking for the part number MMG3014NTl 亲爱的支持者 我想跟进我对部件号MMG3014NTl 标记的询问。 数据表 中的 标记(第二行包含六个字符的标记)与实际产品标记(第二行包含七个字符的标记)不一致。因为数据表中没有具体说明第二行标记的确切格式或字符数。 请告知这是否正常和有效。谢谢 isagani_0-1766569064692.png
記事全体を表示
[S32K344] 版本失败:RTD 7.0.0 中缺少包含路径 (std_Types.h)(autosar r23-11) 大家好 我在为S32K344新建的"Greenfield" 项目中遇到了一个长期存在的问题,即代码生成后,标准包含路径没有自动添加到项目设置中。 我的环境 芯片:S32K344(BGA257) 集成开发环境:S32 Design Studio(最新版本) RTD 版本:Autosar R23-11 V7.0.0 开发软件包:S32K344 开发软件包 复制步骤 我为 S32K344 创建了一个全新的应用项目。 我打开了配置工具(.mex)。 在 “外围设备/元器件” 视图中,我添加了以下元器件: BaseNXP(必填) 平台(用于中断/IntCtrl) Eth_43_GMAC(以太网驱动程序) 我配置了元器件(启用基本设置)并保存了配置。 我点击"更新代码"生成源文件。生成成功。 我点击了版本(锤子)按钮。 问题:版本立即失败,出现多个 " 致命错误 ",这表明找不到基本的 AUTOSAR 和 RTD 标头。编译器似乎不知道恩智浦 RTD 库的位置。 错误日志(控制台输出): 明文文本(Plaintext)   fatal error: Std_Types.h: No such file or directory fatal error: Eth_GeneralTypes.h: No such file or directory fatal error: Mcal.h: No such file or directory fatal error: S32K344_SIUL2.h: No such file or directory ... make: *** [generate/src/subdir.mk:71: generate/src/OsIf_Cfg.o] Error 1 观察结果:我通过文件资源管理器手动验证了文件夹结构。丢失的文件(如 Std_Types.h在 BaseNXP 元器件文件夹中)确实存在于项目/ SDK 结构中的磁盘上。但是,这些路径不会自动添加到项目中。 我的问题是我是否缺少一个特定的步骤或复选框来强制 "配置工具 "更新 "项目包含路径"?还是 RTD 7.0.0 的已知问题?整合? 如果能帮助我自动修复包含路径,我将不胜感激。 顺祝商祺! Re: [S32K344] Build fail: Missing Include Paths (Std_Types.h) with RTD 7.0.0 (AUTOSAR R23-11) 嗨,@VaneB、 谢谢你的调查。 我又深入研究了一下项目属性,发现了一条特定的错误信息,这似乎是 include 路径无法自动注入的根本原因。 能否请您检查一下在您的工作项目中是否也出现了同样的行为? 1.SDK 错误请进入项目属性 -> SDK。确保选中"Show all SDKs"。然后,将鼠标光标悬停在选中的 PlatformSDK_S32K3... 项上。 在我这边,工具提示显示了以下错误: 错误:由于不支持项目所需的工具链,因此无法附加 SDK。 您是否也看到了这个错误工具提示,或者对您来说没有问题? 2。您的安装环境要验证我是否缺少特定的软件包或更新,您能否确认: 扩展:你已经安装了哪些扩展/软件包?(最好能提供"S32DS 扩展和更新" 的截图或列表)。 项目创建:你究竟是如何设置应用程序项目的?您是否更改了向导中的任何设置(例如有关工具链或库支持的设置),还是使用了默认设置? 3.文件检查为了 100% 确定:文件 Std_Types.h 是否已被删除?是否实际存在于磁盘上的 RTD include 文件夹中?(我想是的,因为你的版本可以正常运行,但我想排除我这边安装失败的可能性)。 感谢您的支持! 顺祝商祺! Re: [S32K344] Build fail: Missing Include Paths (Std_Types.h) with RTD 7.0.0 (AUTOSAR R23-11) 你好@nikovntv 我使用相同的设备和 RTD 版本从头开始创建了一个项目。在外围设备工具中,我添加了以下元器件:BaseNXP、平台、端口、Dem、EthTrcv 和 Eth_43_GMAC,我还解决了配置工具报告的所有配置问题。 在 main.c文件中,我只添加了以下内容: #include "Mcal.h" #include "Mcu.h" #include "Port.h" #include "Eth_43_GMAC.h" #include "OsIf.h" 建立项目后,没有报告任何错误。 能否请您确认一下配置工具中是否有任何错误,或者是否缺少任何需要添加依赖关系的驱动程序? BR、VaneB Re: [S32K344] Build fail: Missing Include Paths (Std_Types.h) with RTD 7.0.0 (AUTOSAR R23-11) 你好@nikovntv 此错误通常是由不兼容的软件包引起的。请确保选择适用于 Arm 的 32 位裸机工具链的恩智浦 GCC 10.2,并在创建项目时选择 RTD 7.0.0 作为 SDK。
記事全体を表示
使用 ISP 在 imx8mp 上使用 MIPI-CSI2 捕获偏差 最近,我们已经从基于 ISI 的管道捕获转向使用 ISP。这样做的目的是用软件而不是硬件来执行除渣器。 ISI 版本的驱动程序正常工作,可以在两个独立的 4 线 mipi-csi2 接口上支持两个传感器实例。分辨率和位深度也不吓人(1920x1200、8 或 10 位)。 除了开放 vvcam 服务所需的额外 ioctl 之外,ISP 版本的驱动程序与 ISI 版本的驱动程序相同。链接 vvcam 的传感器接口驱动程序/库似乎也成功启动并运行。调整后的 xml 和 json 配置文件似乎也是正确的。 isp_media_server 适用于我们传感器的一个或两个实例,安装了所有正确的系统驱动程序和传感器驱动程序(imx8_media_dev、我们的驱动程序、vvcam_video、vvcam_dwp 和 vvcam_isp)。它没有报告任何错误,并为每个传感器正确安装了一个 /dev/videoX 实例。 使用 gstreamer 或 video_test 工具也可以在正确的模式下启动正确的传感器。然而,我们所得到的却是错误的。 随附的是输出到监测的 video_test 捕获。当通过 isp_media_server 而不是使用 ISI/设备树方法间接完成时,mipi 设置似乎不正确。它似乎缺少 SOF 标头并且捕获不对齐。 以下是我们使用的版本: 基于 Varascite SOM 的 imx8mp Kirkstone yocto 版本 内核 v5.15.60 isp-imx-4.2.2.18.0 kernel-module-isp-vvcam-4.2.2.18.0 如果能找到这些设置的配置位置,那就太好了。 我的假设是设备树,但除了禁用ISI和启用ISP之外,这种情况没有改变。 非常感谢。 - 奥利弗 Re: Mipi-csi2 capture misalignment using ISP on imx8mp 请向我提供测试记录,您是否尝试过其他格式?有区别吗? Re: Mipi-csi2 capture misalignment using ISP on imx8mp 抱歉,主题发布时附件未被采纳.... Re: Mipi-csi2 capture misalignment using ISP on imx8mp @joanxie,谢谢你的回复。传感器是 ar0234,其中 isp0 上的第一个传感器是单色变体,而 isp1 上的传感器是彩色(拜耳)变体。在引擎盖下驱动传感器的方式没有区别。 日志有点没用,因为没有任何故障。但无论如何,随附的是 isp_media_server 的输出结果。不知道还有哪些日志会令人感兴趣。 两个传感器(彩色或单色)之间没有真正的变化,我也没想到会有这样的变化,因为两个传感器的捕获数据和配置会相同。如果我将捕获分辨率从 10 位更改为 8 位,则会有区别。损失较少(一个图像中只有 3 个重复图像,而不是 5 个左右),但 SOF 仍有偏差,同样存在错位。见附图。 很抱歉捕获的质量很差,我实际上是在用手机拍屏幕的照片。但我认为这已经清楚地说明了问题所在。 Re: Mipi-csi2 capture misalignment using ISP on imx8mp 谢谢你的提醒,我不知道 ISP 只能播放 1080p。这其实不是一个问题,因为我可以通过 ISI 运行单声道摄像机,而只需通过 ISP 运行彩色摄像机。 不过,我现在一次只运行一台相机。 我将查看 ar0144 驱动程序,看看是否有任何明显区别。您知道 ar0144 驱动程序需要哪个版本的内核/vvcam/isp 吗? Re: Mipi-csi2 capture misalignment using ISP on imx8mp 你是同时用双摄像头捕获的吗?双摄像头也有同样的问题吗?逐个测试如何?让我提醒一下,如果您需要同时使用双 ISP,只能支持到 1080p 分辨率,所以我建议您可以逐个测试,我们已经验证了 ar0144,也许您可以参考一下,检查您的设置是否正确,检查 vvcam 驱动程序是否设置正确。 https://github.com/nxp-imx-support/meta-imx8mp-isp-ar0144 您也可以参考 AN 了解如何设置单色 Re: Mipi-csi2 capture misalignment using ISP on imx8mp 参考你的描述,你需要仔细检查你的摄像头驱动程序,ar0144 软件包基于 6.1.22
記事全体を表示
s32k312 hse work abnormal when enable gcc -O1 Hi NXP expert,     1. i am using s32k312 hse to do a rsa verify function,  i store the rsa public key in NVM catalog  ``` { HSE_ALL_MU_MASK,  HSE_KEY_OWNER_CUST,   HSE_KEY_TYPE_RSA_PUB, 2,  HSE_KEY2048_BITS }, ```    2. it can verify in default project, which in settings, gcc optimization is  None (-O0)   3.  i want to shrink the binary size, and change gcc settings to -O1,  no else changed. then the function returns  failed (0x55a5a164) how to solve this problem    thanks. Re: s32k312 hse work abnormal when enable gcc -O1 Hi victory, Based on your description, it sounds very similar to the issue described in the S32K3常见问题检查列表(Check list)-V1.2-20251113.docx:  4.32 编译器优化设置不当导致HSE服务失败问题 4.32 编译器优化设置不当导致HSE服务失败问题.png Please note that during the Christmas holiday period, our support response times may be longer than usual. In some cases, your request might be addressed after the New Year. Thank you for your understanding. Best Regards, Robin
記事全体を表示
PoP ピンをサポートする i.MX6Q .BSDL ファイルですか? こんにちは。NXP には、PoP RAM に接続する部品の上部にあるピンを含む、i.MX6Q PoP バリアント用の .BSDL ファイルがあるでしょうか?最終目標は、部品上の RAM ピンをカバーする境界スキャン テストを開発し、ソフトウェア スイート内で RAM の機能テストを実行することです。高性能クアッドコア ARM プロセッサ | NXP Semiconductors のダウンロード ページで IMX6Q_PoP_BSDL.bsdl を見つけましたが、PoP ピンが含まれていません。使用中の部品番号はMCIMX6Q7CZK08ADです。 i.MX6Quad Re: i.MX6Q .BSDL file with PoP pin support? 弊社が提供できるのは以下のものだけです: 高性能クアッドコア ARM プロセッサ | NXP Semiconductors   image - 2025-12-22T172657.843.png
記事全体を表示
IMX8MP と sec-dsim.cサポート こんにちは、 MIPI DSI 経由で imx8MP にコネクテッドされたパネルを起動しようとしています。DSI ブリッジ ドライバのソースを調べていたところ、ドライバが fslc ブランチから「消えた」ことに気付きました。 これは私が確認した最後の発生です: https://github.com/Freescale/linux-fslc/commits/5.15-2.2.x-imx/drivers/gpu/drm/bridge/sec-dsim.c 現在このブランチを使用しています: linux-imx_5.10.72_2.2.0 ドライバは最近のブランチのどこに移動しましたか?Samsung バージョンとの統合に向けた動きが見られます。 ありがとうございます! Re: IMX8MP and sec-dsim.c support こんにちは、 私も同じことを思っていました。これを解決しましたか?なぜ pl_tx_done ではなく ph_tx_done を待つのでしょうか。 Re: IMX8MP and sec-dsim.c support これは問題ないようです。クロック有効化シーケンスにバグがあり、SOコマンドが送信されていないことが判明しました。 Re: IMX8MP and sec-dsim.c support ドライバはまだここに存在します、よかった!気になるSOは変わってないのでこちらで質問させていただきます。https://github.com/nxp-imx/linux-imx/blob/29549c7073bf72cfb2c4614d37de45ec36b60475/drivers/gpu/drm/bridge/sec-dsim.c#L695 「」 if (packet.payload_length) { /* Long Packet case */ reinit_completion(&dsim->pl_tx_done); /* write packet payload */ sec_mipi_dsim_write_pl_to_sfr_fifo(dsim, packet.payload, packet.payload_length); /* write packet header */ sec_mipi_dsim_write_ph_to_sfr_fifo(dsim, packet.header, use_lpm); ret = wait_for_completion_timeout(&dsim->ph_tx_done, MIPI_FIFO_TIMEOUT); if (!ret) { dev_err(dsim->dev, "wait payload tx done time out\n"); return -EBUSY; } } ``` リセット中です dsim->pl_tx_done ただし、次のものを待っています: wait_for_completion_timeout(&dsim->ph_tx_done, これは正しいですか?ハードウェアは長いパケットに対して pl_tx と ph_tx の両方に割り込みを生成しますか? Re: IMX8MP and sec-dsim.c support こんにちは、 新しい git からカーネルが利用可能かどうかを確認する必要があります。 https://github.com/nxp-imx よろしくお願いします。
記事全体を表示
[乱用] 投稿者: @JohnKlug / ボード: imx-プロセッサ / 報告者: qzgopv qzgopv は、 @JohnKlug が投稿した 「Could not invoke dnf for external kernel module in Yocto kirkstone」という 投稿について、以下の理由で報告しました: 理由:盗作 詳細: 投稿リンク: https://community.nxp.com/t5/i-MX-Processors/Could-not-invoke-dnf-for-external-kernel-module-in-Yocto/mp/1627964#M203740 投稿者: @JohnKlug |メール著者 報告者: qzgopv |メールレポーター 報告された投稿には 2 件の返信があります。
記事全体を表示
SPI DMA 传输大容量数据时,S32K312 uart AsyncReceive 回调事件总是出错 你好 在 S32K312 S32DS3.5 RTD4.0.0 项目中,SPI0 和 SPI1 采用 DMA 模式,UART1 采用中断模式。 当同步发送或异步接收 12 字节的帧时,UART1 运行良好。 但 SPI DMA 传输大容量数据时,uart AsyncReceive 回调事件总是出错。 有什么建议吗? Re: S32K312 uart AsyncReceive callback event is always error when SPI DMA transfer mass data 是的,这是中断优先级问题,Uart1 在提高优先级后才能工作。 非常感谢! Re: S32K312 uart AsyncReceive callback event is always error when SPI DMA transfer mass data 您好, SPI DMA 突发期间 UART 异步接收错误可能有以下原因: 1.中断优先级问题 - 由于 DMA 完成或其他 ISR 具有相同或更高的优先级,因此 UART RX 中断不能迅速得到服务。 - 结果:UART RX FIFO 溢出 → 超限或成帧错误。 确保 LPUART1_IRQn 比所有与 DMA 相关的 IRQ(如 DMATCDx_IRQn)具有更高的优先级(数值上更低)。 确认中断分组允许抢占。 2。DMA 的总线占用情况 - 用于 SPI 的 eDMA 信道在大突发期间会使 AXBS 交叉条达到饱和。 - CPU 和外设寄存器访问(包括 UART RX 处理)延迟,增加了 ISR 延迟。 配置 SPI DMA 通道以允许 eDMA 引擎停滞(BWC 设置)   BR, Petr
記事全体を表示
[ABUSE] Post By: @JohnKlug / Board: imx-processors / Reported by: hylhmda hylhmda has reported the post Could not invoke dnf for external kernel module in Yocto kirkstone posted by @JohnKlug for the following reasons: Reason: Harassment Details: https://www.e123.hk/zh-hant/e-center/group/topic/933211"> https://www.spinsheet.com/racing-team-log/pharmacy-online-3"> https://www.spinsheet.com/racing-team-log/pharmacy-online-3"> https://totalhockeymanagement.com/pharmacy-online-2"> https://www.itconnecta.es/pharmacy-online-8"> https://museusvalenciades.grupotecopy.es/en/node/2360"> http://xn--80ab2anoq0a.xn--p1ai/art/pharmacy-online-0"> https://new.roger24.de/pharmacy-online-6"> https://www.danduo168.com/en/artworks/693/pharmacy-online-2"> http://kalyterizoi.gr/foreis/pharmacy-online-4"> https://chitapage.ru/catalog/17222"> https://lotteryobzor.com/forum/pharmacy-online-10"> http://hubram.cz/content/pharmacy-online-11"> https://jeunescathos-bxl.org/fr/content/pharmacy-online-0"> https://investor18.ru/investors/pharmacy-online-5"> https://direct.needshub.com/node/28207"> https://direct.needshub.com/node/28207"> https://www.onlyhomebuyers.com/for-sale-by-owner-homes/la/77"> https://theanubianwar.com/node/6402"> http://www.beautynbrushes.com/services-provided/bundle-color-vitalitymythicls"> https://new.roger24.de/pharmacy-online-6"> https://ng.nycc.org/content/pharmacy-online-2"> https://rahuldolas.com/forum/general-discussion/topic/729/pharmacy-online"> https://slp.millingtonpubliclibrary.org/content/pharmacy-online-8"> https://www.old.ts3bots.de/node/1024"> http://old-namur.jeunescathos.org/fr/content/pharmacy-online-30"> https://backend.dawahnigeria.com/audit/304766"> https://recruitment.kenet.or.ke/node/2040"> http://dev.nikol-buket.com/content/pharmacy-online-0"> https://rahuldolas.com/forum/general-discussion/topic/729/pharmacy-online"> http://stage.isupportveterans.org/node/5264"> http://ru.ph-ed-plus.nspu.ru/article/17947"> https://golemobuchino.com/content/2467/pharmacy-online"> https://theanubianwar.com/node/6402"> https://investor18.ru/investors/pharmacy-online-5"> https://www.e123.hk/zh-hant/e-center/group/topic/933211"> http://www.dachpedigrees.com/owner-breeder/pharmacy-online-4"> https://theanubianwar.com/node/6402"> https://oregonweddingday.com/your-couple-name-2370"> https://recruitment.kenet.or.ke/node/2040"> Post link: https://community.nxp.com/t5/i-MX-Processors/Could-not-invoke-dnf-for-external-kernel-module-in-Yocto/m-p/1627964#M203740 Post author: @JohnKlug | Email Author Reported by: hylhmda | Email Reporter The reported post has 2 replies.
記事全体を表示
复制: 关于 EB32.0.0 Im/Exporter 的问题 本帖复制自 此处 嗨,团队、 我的客户舍弗勒希望导出 arxml 文件。我在 EB32.0.0 上试过,该工具会报告一些奇怪的错误。 同样的程序也适用于 EB 29 和 K3 RTD。 您能帮忙检查一下这个问题吗? 此致, Liek EB TRESOS 许可证 优先级:中等 来源:恩智浦内部来源:恩智浦内部 Re: Copy: Issue about EB32.0.0 Im/Exporter 你好@Luis_Garabo 首先,请参阅 RTD 发行说明,以验证哪个 EB Tresos 版本已通过相应的 RTD 版本进行了验证。 必须使用发行说明中指定的经过验证的 EB Tresos 版本,以确保功能正确和运行稳定。
記事全体を表示
[ABUSE] Post By: @JohnKlug / Board: imx-processors / Reported by: wsmjdwen wsmjdwen has reported the post Could not invoke dnf for external kernel module in Yocto kirkstone posted by @JohnKlug for the following reasons: Reason: Misleading or False information Details: https://whs6570.com/node/2090"> https://www.e123.hk/zh-hant/e-center/personal-wall/81576/933330"> https://www.danduo168.com/en/artworks/692/pharmacy-online-5"> https://www.albatrosplus.ru/pharmacy-online-9"> https://www.rapidservice.com.ec/es/content/1-carga-pesada-14482"> https://okwiki.ru/catalog/pharmacy-online-4"> https://www.lawtech.ru/subscribe/26814-16102025"> https://www.availcalendar.com/calendar/25583"> https://www.itconnecta.es/pharmacy-online-12"> https://www.musicinafrica.net/newsfeed/213463/373416"> https://www.cableman.ru/node/84341"> https://www.horecascout.nl/vacatures/5441/pharmacy-online"> http://hr-life.ru/node/53784"> http://kalyterizoi.gr/foreis/pharmacy-online-5"> https://auc.org.ua/faq/28092025-2124"> http://lsdsng.com/node/4271"> https://www.jobwebby.ilovemarkso.com/domainasname-anthony-gmbh/pharmacy-online"> https://www.spinsheet.com/century-club-log/pharmacy-online-4"> https://spdm.dambo.me/forums/miscellaneous/news-and-announcements/pharmacy-online-0"> https://ufa-help.ru/content/pharmacy-online-14"> http://pbgpersonnel.ru/forum/pharmacy-online-0"> https://totalhockeymanagement.com/pharmacy-online-11"> https://darkmetal2039.com/history/pharmacy-online-26"> http://lsdsng.com/node/4271"> http://hubram.cz/content/pharmacy-online-12"> http://hr-life.ru/node/53784"> http://ysrp.bnl.bm/review/pharmacy-online-5"> http://ph-ed-plus.nspu.ru/article/17933"> http://www.sccu.chula.ac.th/node/919"> https://reflexologie-cerilly.fr/en/node/4245"> https://satto.vtranet.com/binh-luan-389"> https://dev.beautynbrushes.com/services-provided/marley-twists-maroonimmortalep"> https://www.vgame.ca/node/46849"> https://www.inserthere.me/sitereview/pharmacy-online"> https://www.castnblastadvisor.com/outfitters/pharmacy-online-0"> https://localautosforsale.com/local-autos/tx/96/daihatsu/1500-classic-4wd/2001/8697"> https://darkmetal2039.com/history/pharmacy-online-26"> https://spdm.dambo.me/forums/miscellaneous/news-and-announcements/pharmacy-online-0"> https://reflexologie-cerilly.fr/en/node/4245"> https://enki.ua/advert/16925"> Post link: https://community.nxp.com/t5/i-MX-Processors/Could-not-invoke-dnf-for-external-kernel-module-in-Yocto/m-p/1627964#M203740 Post author: @JohnKlug | Email Author Reported by: wsmjdwen | Email Reporter The reported post has 2 replies.
記事全体を表示
pn557 upgrading OS from Android 13 to Android 15 我们一直在开发具有PN553和PN557 NFC功能的Android 15设备。 (系统Android版本为15,之前一直是Android版本为13,这次我们需要为PN557升级) NFC移植的参考源代码具体从链接网址获取源代码。 问题1: 请告诉我应该参考哪个具体链接获取源代码,期待您给一个地址。 问题2: 源代码同时支持PN553和PN557? 还是,它只支持PN557? 期待您们的回复,谢谢! DSC Re: pn557 upgrading OS from Android 13 to Android 15 遗憾的是,PN557 没有 Android 15 移植指南。我们只有 PN7160 和 PN7220 的端口指南。 PN7160/PN7220 – Android 15 移植指南 回复: pn557 upgrading OS from Android 13 to Android 15 PN557 信息不公开。我找不到该产品的驱动程序源代码和文档。我想你可以向当地的恩智浦代理商和恩智浦营销部门查询这个产品,申请支持。 回复: pn557 upgrading OS from Android 13 to Android 15 嗨,吉米: 感谢您的耐心回复和解释!那么,我能理解 PN557 产品本身支持升级/移植到 Android 15,但你的官方团队没有为 PN557 提供专用的移植指南吗?期待您的回复!谢谢!
記事全体を表示
S32K144 中 PDB 触发信号 ADC 采样的问题 问题描述: PDB0 的 ADC0 采样由 FTM2 的触发信号触发,PDB1 的 ADC1 采样由 FTM3 的触发信号触发。 TerenceBill_0-1764836681353.png FTM2 和 FTM3 的 PWM 频率设为 10 kHz。FTM 模块的时钟 频率为 80 MHz,配置为 对称上下计数模式 TerenceBill_1-1764836759584.png ADC0 有 4 个通道,ADC1 有 5 个通道,触发信号是在背靠背模式下实现的。 禁用 ADC 硬件平均时,采样工作正常,但启用 4 采样硬件平均时,采样工作会出现异常。 ADC0 时钟配置为 40 MHz,采样时间短,这不应影响 PDB 触发信号。此外,FTM 触发信号在 ADC 中断中被禁用,在 PDB 中断中重新启用。 此外,在调试过程中设置断点时,基于 ADC 中断的数据采集可以正常工作,但在连续运行时却无法运行。 PDB1 和 PDB0 之间的冲突会是根本原因吗?   我的问题如下: FTM2 和 FTM3 均设置为 10 kHz,分别用作触发信号以启动 PDB0 和 PDB1。如果 ADC 完成中断发生冲突,是否会导致 PDB 出现序列错误? 使用 ADC 硬件平均时,PDB 触发信号模式有任何预防措施吗? 为什么在调试期间设置断点时可以进入 ADC 中断并获取采集数据,而在全速运行期间却无法进入 ADC 中断?在这种情况下应如何进行调试? 调试期间,ADC 的 4 采样硬件平均配置基本上可在 1000 个 PDB CNT 周期内完成,因此也应在 8000 个 PDB CNT 周期内完成。       TerenceBill_2-1764836803497.png TerenceBill_3-1764836814845.png TerenceBill_4-1764836828111.png TerenceBill_5-1764836842107.png TerenceBill_6-1764836854604.png TerenceBill_7-1764836864124.png TerenceBill_8-1764836877431.png TerenceBill_9-1764836937974.png Re: The Problem of PDB Triggering ADC Sampling in S32K144 您好, FTM2 和 FTM3 均设置为 10 kHz,分别用作触发信号以启动 PDB0 和 PDB1。如果 ADC 完成中断出现冲突,这会导致 PDB 中的序列错误吗? 答:除非出现序列错误,否则应确保在新触发信号出现之前及时读取 ADC 结果寄存器。 使用 ADC 硬件平均时,PDB 触发信号模式有任何预防措施吗? 答:可以正常工作,特别是在使用背靠背的情况下。 为什么在调试期间设置断点时可以进入 ADC 中断并获取采集数据,而在全速运行期间却无法进入 ADC 中断?在这种情况下应如何进行调试? 答:没有确切的设置和使用的代码,很难说 BR, Petr
記事全体を表示
組み込みシステム開発におけるベストDevOpsプラクティス 皆さん、 組み込みシステム開発における DevOps の実装に関するベストプラクティスについて議論したいと思いました。組み込みシステムには特有の課題があることは誰もが知っていますが、DevOps の原則を組み合わせ、適切なDevOps ソリューションを活用することで、ワークフローを大幅に改善することができます。 私が役に立つと思ったいくつかの方法を以下に示します。 自動ビルドとCI/CD 組み込みシステムでは、自動ビルド パイプラインの設定が非常に重要です。CI/CD を使用すると、テスト、フラッシュ、実際のデバイスへのデプロイメントを自動化できるため、エラーを早期に検出できます。 ファームウェアとハードウェアのバージョン管理 ファームウェアをソフトウェアのように扱う – バージョン管理に Git または同様のツールをハードウェア抽象化レイヤー (HAL) とともに使用すると、ソフトウェアとハードウェアの両方の依存関係を同期して管理するのに役立ちます。 ハードウェア・イン・ザ・ループ(HIL)による継続的インテグレーション HIL テストを CI パイプラインに統合すると、シミュレートされた環境だけでなく、実際のシナリオに対しても検証できるようになります。これにより、実際のハードウェアでのみ発生する問題を検出できるようになります。 組み込みソフトウェアのコンテナ化 ソフトウェア環境のレプリケーションに Docker または同様のツールを使用すると、組み込みプラットフォームで作業する場合でも、開発、テスト、展開の各フェーズ全体で一貫性が確保されます。 あなたのご意見や、効果的だとわかった追加の実践方法をぜひお聞かせください。組み込み開発ワークフローに DevOps をどのように統合していますか? DSC Re: Best DevOps Practices for Embedded Systems Development 私たちはまさにあなたが提案していることを実行しようとしています。具体的な方法についてのアドバイスはありますか?
記事全体を表示
kw45 CAN 接收 您好,NXP团队, 我正在使用 KW45B41Z-EVK 板,我的目标是在这个 BLE 板上实现 CAN 通信(包括发送和接收) 我修改了 flexcan_interrupt_transfer 示例,删除了对第二个节点的依赖,并尝试进行双向通信。但是,只有传输功能能正常工作。 此外,当使用原始的flexcan_interrupt_transfer项目并从CAN流量生成器(使用相同的帧ID和为接收配置了相同的CAN信道)发送帧时,板仍然无法接收任何帧。 在这两种情况下,问题都是板无法接收 CAN 帧。您能帮我找出可能的原因并指导我解决这个问题吗? Re: kw45 CAN Reception 你好,你好,希望你一切都好、 您能帮我们描述一下代码中实施的修改吗? 您能帮助我们确认以下内容吗? 您使用的是哪个版本的 SDK? 你使用的是 1 个 KW45B41Z-EVK 板还是 2 个板?未作修改的示例是否能按预期使用 2 个 KW45B41Z-EVK? KW45B41Z-EVK 的 J9 上是否有为 P5V_CAN 供电的 12V 电源? 能否分享一下运行示例时的终端视图?非常感谢 顺祝商祺! 路易斯 Re: kw45 CAN Reception 您好, 很抱歉打扰您,首先问题已经解决。看来我正在使用的流量生成器出现了故障,无法在总线上传输帧。 除此以外,Rx 现在工作正常。谢谢你的快速回复。
記事全体を表示
i.MX8ULP の A コアと DDR 周波数を下げる方法 i.MX8ULP の A コア周波数と DDR 周波数の両方を下げたいです。 これを実現する方法と、どのレジスタまたは構成を変更する必要があるかを教えてください。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは、 次のアプリケーションノート (4.3 DVFS の使用) を参照してください。 i.MX 8ULPの消費電力の最適化 よろしくお願いいたします。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは@JorgeCas DVFS を使用しており、A コアの CPU 周波数を下げたいと考えています。現在、周波数は808MHzあたりを表示しており、これをできるだけ下げたいと思っています。 以下は私が取得したログです: root@imx8ulp-9x9-lpddr4-evk:~# echo 1 > /sys/devices/platform/imx8ulp-lpm/enable [ 467.490570] DDR enter low frequency mode root@imx8ulp-9x9-lpddr4-evk:~# mhz 808 MHz, 1.2392 nanosec clock A コア周波数を下げる方法と、どの設定または構成を変更する必要があるかを教えてください。 ありがとうございます。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは、 アプリケーションノートによると、imx8ulp-evk-nd.dtb デバイス ツリーを使用する必要がありますが、ログを見ると、9x9 ボードを使用しているため、変更を行うためのデバイス ツリーがありません。 これを参考にしてデバイスツリーを変更し、もう一度試してください。 https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx8ulp-evk-nd.dts よろしくお願いいたします。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP ありがとう@JorgeCas root@imx8ulp-9x9-lpddr4-evk:~# echo 1 > /sys/devices/platform/imx8ulp-lpm/enable root@imx8ulp-9x9-lpddr4-evk:~# mhz 655 MHz, 1.5267 nanosec clock 参考までに、.dtsを更新しましたファイルを変更し、A コアの周波数を 650 MHz まで下げることができるようになりました。A コアの周波数をさらに下げて、理想的には 200 MHz 程度にしたいと思っています。これを実現する方法を教えてください。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは、 残念ながら、Cortex - A コアの周波数を 650 MHz 未満に下げる方法についてのドキュメントはありません。 アプリケーション ノートによると、最小動作電圧 VDD_DIG1/2 (最小動作周波数) で動作しており、弊社のエンジニアは前回の投稿で、PLL ではより低い周波数は提供されないとコメントしました。 PLL レジスタを手動で変更してみることもできます。 よろしくお願いいたします。 Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは、 @JorgeCas ご説明ありがとうございます。Cortex-A コアの PLL でサポートされる最も低い周波数は 650 MHz であると理解しています。 消費電力をさらに削減するために、PLL 構成を手動で変更することを検討したいと思います。i.MX8ULP 上の Cortex-A クロックを制御する PLL (レジスタまたはクロック パス) と、周波数を 650 MHz 未満に下げる場合に推奨される設定や制約があるかどうかを教えてください。 PLL レジスタを安全に変更するためのガイダンスやドキュメントがあれば、大変助かります。 よろしくお願いします、 ヤシュ Re: How to Reduce A-Core and DDR Frequency on i.MX8ULP こんにちは@JorgeCas 、 i.MX8ULP の PLL 設定を変更して Cortex-A コア周波数を 650 MHz 未満に下げることに関する以前の質問を確認します。レビューする機会があったかどうか確認したかったのです。どのようなご指導でもいただければ幸いです。 ありがとう、 ヤシュ
記事全体を表示
kw45 功率低 嗨,nxp: 1。kw45 中的 NBU 内核会在所有电源模式下进入睡眠状态还是处于空闲状态 2。是否有可能在睡眠模式(超低功耗)下进行 NBU。 3.当没有数据要传输时,NBU 内核是否会自动切换到空闲/电源模式 4.空闲模式对 NBU 意味着什么。根据"KW45_WK47_MCXW71_MCXW72_BLE_power_profile_calculator_v1 中的工作表说明。34 " 所有电源模式(睡眠、深度睡眠、掉电等),当 NBU 处于IDLE状态时,最低功耗为 1.1 uA 这意味着什么。 电路板设计 核心与内存 Re: Low power in kw45 你好,路易斯、 低功耗参考设计代码是否在除EVK板之外的任何自定义硬件上进行了测试,因为它不在我们的定制板上运行,仅供参考,我们已经根据EVK匹配了Circuit。连接后很快就会断开,但在 EVK 中,它会一直连接到提供数据。 此外,低功耗启用宏 glowpowerEnble 如果被禁用,将无法再次启用。如果启用,则无法再次禁用。特别是 app_preinclude.h 中的 sdk 宏的一些链接问题、未在其他文件中检查。那么,有没有其他办法 应该有关于如何在自定义板上使用 sdk 的指南,如果有,请给我链接 还有一件事关于1,需要考虑的所有参数是什么。固件和 sdk 2.硬件东西,可以让低功耗代码在定制主板上运行 所有 sdk 中的开发者指南、低功耗连接框架指南均为旧版 MCU,请提供 kw45 Re: Low power in kw45 你好 根据应用笔记 AN13230 K inetis KW45 和 K32W1 低功耗蓝牙功耗分析表 2,在应用层面,NBU 的电源模式表明 NBU 在所有可用的深度睡眠模式下均处于禁用状态。 有关 NBU 电源模式的更多信息,请参阅 AN13230 中的第 3.1.1 章。 你能不能帮我们解释一下你在评论 " 中指的是什么 NBU 在睡眠模式(超低功耗)" 中可能做什么? 在第 2 章中,指示 NBU 可以在睡眠模式、深度睡眠模式、掉电模式、深度掉电模式等任何状态下处于活动状态。 在第 3.1 章中指出,当系统处于空闲状态时,系统会进入低功耗电源模式,所有软件层都同意这一点;每次发生同步或异步事件并需要处理时,系统都会退出低功耗电源模式。 在表 2 中,深度睡眠模式概述了进入这些状态所需的条件。引用的表格用作计算器来估算这些条件的值,将在测试期间使用。 顺祝商祺! 路易斯 Re: Low power in kw45 以上信息我已经知道了,但是有没有什么指南可以帮助我们将低功耗参考设计外设 sdk 代码移植到定制板上的端口,我请你不要给出通用答案 Luis,我的问题是,当我修改这个代码来发送连续的虚拟数据而不是单个温度或电池时,它会在连接 1 或 2 秒后断开连接。在 Evk 板上,它可以连续发送而不会断开连接。自定义板电路遵循您的硬件推荐指南。那么,我们在软件方面需要考虑什么呢? 是的,我们正在使用下面的例子。 低功率参考设计_ble_中央参考系统和低功率参考设计_ble_外围参考系统 Re: Low power in kw45 您能否确认在未对自定义板进行任何修改的情况下使用示例代码时是否会出现断开连接问题? 此外,您能否描述一下代码中实施的修改? 在第 3 章中,运行低功耗参考设计外设应用程序表明 SW2 可以停止广告,你能帮我们检查一下是否没有触发信号 SW2 来停止广告吗? 至于软件方面的考虑,应用配置包含了外设示例中软件应用程序接口的描述。 你可以验证 " GapprestartAdvAfterConnect " 是否设置为 1;在外围设备示例中,这会在连接结束时重启广告模式;以及 " gapprestartScanAfterConnect " 设置为 1,因为连接结束时设备会切换回扫描模式。 顺祝商祺! 路易斯 Re: Low power in kw45 你好 SDK中提供的示例已使用恩智浦开发板进行了验证。KW45硬件设计建议公开版中包含的设计建议对基于开发板的定制板具有所有必要要求,即基于开发板的定制板可以与开发板相同的功能运行,包括SDK示例。 您能否帮助我们确认您使用的是Lowpower_reference_design_ble_central_freertos和Lowpower_reference_design_ble_peripheral_freertos示例,或者具体说明您测试的是哪个示例? 您能否帮助我们确认"glowpowerEnble" 中的宏是否为 gAppLowpowerEnabled_d? 要使用SDK中提供的低功耗示例,我建议查看MCUXpresso SDK文档页面以获取示例,该页面包含低功耗参考设计中心应用程序——MCUXpresso SDK文档和低功耗参考设计外设应用程序——MCUXp resso SDK文档;此外,示例中的自述文件中提供了更多信息。 有关低功耗连接的最新文档,请参阅以下链接:LowP ower — MCU Xpresso SDK 文档 顺祝商祺! 路易斯 Re: Low power in kw45 你好 要将低功耗参考设计外设应用程序与 BT2 中的 coincell 电池连接起来,可以在代码中测试以下修改: 在app_config.c中文件中修改gAdvParams,输入gAdvConnectableUndirected_c作为advertisingType,确保不要输入gAdvNonConnectable_c 作为 else 场景,也可以在app_preinclude.h 中将其定义为 0。 确认 app_preinclude.h 中的 gAppUsePairing_d 和 gAppUseBonding_d 定义为 1 另外,您能否与我们分享一下您在 KW45B41Z-EVK 中的跳线配置? 关于板配置,你能否帮助我们确认是否设置了以下跳线: 跳线 JP42 打开 跳线 JP5 为 1-2 短路配置 跳线 JP14 已连接 跳线 JP10 位于 2-3 [旁路配置] 位置 有关跳线配置和说明的更多信息,请参阅KW45B41Z-EVKUM表 5 和表 8(电源)。 如果这对你有用,请告诉我你的发现、 顺祝商祺! 路易斯
記事全体を表示