Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32K344 Mini-EVB 上的以太网引脚冲突 您好,团队、 我正在使用S32K344 Mini-EVB进行以太网连接活动。从用户手册中我可以看到,PTD16 引脚用于 MDC,PTD17 引脚用于 MDIO。但当我在 S32DS 中进行以太网引脚配置时,我看到 PTD16 只能路由到 MDIO,而 PTD17 则路由到 MDC,而且我还从 S32K344_IOMUX 中验证了这一点,从该 excel 中我还可以看到 PTD16 --> MDIO 和 PTD17 --> MDC。 那么,用户手册文件中是否有错误,如果有,是否会影响以太网通信。 Re: Ethernet Pin Conflict on S32K344 Mini-EVB 你好@MySterio_1、 是的,你说得对。引脚 MDC 和 MDIO 对调。我已经报告过——它将在下一个版本的 UM12406 中修复——发布日期尚不清楚。 请随时参考我与此主板相关的 LwIP 示例:示例 S32K344 EMAC LWIP Fre eRTOS miniEVB S32DS 3.6.1 RTD 6.0.0   顺祝商祺! 帕维尔
記事全体を表示
HSE_b: Not allowed to import RSA key to RAM I'm trying to understand how to use the key import service by importing a single 1024-bit RSA public key into the RAM catalog, but the server responds HSE_SRV_RSP_NOT_ALLOWED. My test application formats the RAM key catalog as follows: { { muMask = HSE_MU0_MASK | HSE_MU1_MASK, groupOwner = HSE_KEY_OWNER_ANY, keyType = HSE_KEY_TYPE_RSA_PUB, numOfKeySlots = 2, maxKeyBitLen = HSE_KEY1024_BITS, }, { muMask = HSE_MU0_MASK | HSE_MU1_MASK, groupOwner = HSE_KEY_OWNER_ANY, keyType = HSE_KEY_TYPE_ECC_PUB_EXT, numOfKeySlots = 2, maxKeyBitLen = HSE_KEY256_BITS, }, { muMask = 0, groupOwner = 0, keyType = 0, numOfKeySlots = 0, maxKeyBitLen = 0 }, } and I get server reply HSE_SRV_RSP_OK. I then try to import an RSA key with the following key info: { keyFlags = HSE_KF_USAGE_VERIFY, keyBitLen = HSE_KEY1024_BITS, keyCounter = 0x0, smrFlags = 0x0, keyType = HSE_KEY_TYPE_RSA_PUB, specific = { pubExponentSize = 4, } } and my request is as follows: { targetKeyHandle = 0x20000, pKeyInfo = 0x20401f74, pKey = { 0x210034b4, 0x21003534, 0x0}, keyLen = { 0x80, 0x4, 0x0}, } . I have set HSE_RAM_PUB_KEY_IMPORT_POLICY_ATTR_ID to HSE_KM_POLICY_ALLOW_RAM_PUB_KEY_IMPORT, and read it back as the same. LC attribute is 0x04, HSE error flags are 0x0000, HSE status flags are 0x0B60. Firmware version reads as 0x0F SoC ID 0x0000 FW type 0x02 major 0x32 minor 0x00 patch. Re: HSE_b: Not allowed to import RSA key to RAM Hi @Emma_G-gbg  Your parameters are correct, I can see nothing wrong there. If you have super user rights, it’s not even necessary to set that attribute. I was testing something very similar yesterday, so I just slightly updated my code to import 1024bit RSA public key with 4-bytes public exponent. It looks like this: Notice that it’s not necessary to set pubExponentSize when importing RSA public key. HSE ignores this parameter. It uses keyLen[1] instead. Parameter pubExponentSize is used when reading the keyInfo by service HSE_SRV_ID_GET_KEY_INFO. This is what I got when I read the keyInfo of that key: Isn’t that just data cache issue? Could you try to disable data cache to see if it makes a difference? Regards, Lukas Re: HSE_b: Not allowed to import RSA key to RAM Thank you, I had missed filling in cipher and auth key handle information, I hadn't checked so I thought HSE_INVALID_KEY_HANDLE would be zero. It's currently working with at least some of the values in cached memories, with cache maintenance operations before and after service calls. Since we are adding HSE services to an existing project we are precluded from changing the cache structure, but so far everything has worked as long as we make sure it's actually written to the shared memory, although I did also try disabling the cache for the relevant memories, which made no difference.
記事全体を表示
如何通过 UART 接收不同长度的数据? 嘿 ! 我使用的是 s32k144 评估板,我使用 UART_PAL 库使用 MODBUS 协议通过 UART 接收数据。我在 while 循环中使用了 thenon 阻塞 uart_receivedata() API,并使用回调检查接收事件和接收数据。 在我确定要接收的数据长度之前,一切都很正常,但当要接收的数据长度不固定,而且每次都不一样时,我该怎么办呢? 我看到了许多相同的主题,但没有一个主题提供了绝对的解决方案,我请求您指导我一个正确的解决方案,如果可能的话,请提供相同的代码/屏幕截图。 我附上了一张截图,在开关语句中,不同情况下接收数据的长度是不确定的。 请@Robin_Shen为我们提供解决方案。 此致, 阿达尔什 Re: How to receive data of varying length over UART? 你好,我想问一下你们是否解决了在 485 上接收变长数据的问题。我目前也遇到了同样的问题,但一直无法解决。 Re: How to receive data of varying length over UART? 本指南中还缺少一样东西,但@Robin_Shen发送的链接中却有。我也会把它写在这里。 6.在 LPUART_DRV_StartReceiveDataUsingInt() 函数中,启用 CTRL[IDLE]。 非常感谢@Adarshnanda制作这份指南! Re: How to receive data of varying length over UART? HI 我正在尝试通过 LPC804 的 UART 接收数据,并使用 mcuxpresso ide,请问谁能提供代码并告诉我接收数据的步骤。 Re: How to receive data of varying length over UART? 嘿,@Robin_Shen、 我查看了该主题,它对我很有效。唯一令人困惑的是,该主题中有些答案与通过 DMA 接收数据有关,有些则与通过中断接收数据有关。 如果想使用 INTERRUPTS 实现 UART_IDLE_LINE_RECEIVE,让我总结一下需要遵循的步骤。 请注意,我们需要添加 LPUART 驱动程序。 1.在 LPUART_DRV_INIT 函数中,必须配置外设寄存器,以启用 IDLE LINE INTERRUPT& 设置 IDLE 标志设置前接收的空闲字符数。你应该看看参考手册。我已将其配置为 8 个空闲字符& ,在此附上截图。 2.在 LPUART_DRV_IRQHandler 中,必须检查 IDLE_LINE_DETECT 标志是否设置& ,如果设置了,则调用 LPUART_DRV_RxIdleCallback 函数(默认情况下没有,用户需要定义)。请注意 - 需要在启动 IRQ_Handler 时调用此函数。 3.在文件 - (callbacks.h) 的枚举 - uart_event_t 中,定义一个事件 UART_EVENT_IDLE_DETECT。 4.定义 LPUART_DRV_RxIdleCallback& 并提供其函数原型。 5.之后,您就可以在应用程序中使用它了。 谢谢@Robin_Shen & 我希望这对其他人有所帮助。 此致, 阿达尔什 Re: How to receive data of varying length over UART? 你好,阿达什、 很抱歉,最近的 S32K1 SDK/RTD 驱动程序没有实现空闲检测功能。您是否参考过S32K144 LPUART IDLE 线路中断配置中的讨论? 您需要更改 SDK 驱动程序,才能获得 LPUART 空闲线中断。 祝好, Robin ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"Mark Correct" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请另开新主题,并参考已关闭的主题。 ------------------------------------------------------------------------------- Re: How to receive data of varying length over UART? 7。调用 LPUART_DRV_GetReceiveStatus 函数来计算接收的长度,调用 LPUART_DRV_AbortReceivingData 函数以在处理第一帧后重新开始接收数据,这样接收缓冲区从 0 开始。 这是我添加的内容。现在调试成功了。感谢专家们分享之前的内容。谢谢大家。
記事全体を表示
S32G:为什么 QSPI_IP_HyperflashProgram 每 2 字节发送一次写入命令? 专家们好 CTM: 法雷奥 平台:S32G3 模块:RTD 5.0.0QLP04 Fls 驱动程序 客户报告说,他们遇到的或非闪存写入吞吐量明显低于预期。 客户可能想知道为什么 QSPI_IP_HyperflashPro gram 函数 2 字节以 2 字节传输数据。看来这就是瓶颈所在。 是否有专家能就这一问题提供帮助? 感谢你的支持 狮子座 RTD Re: S32G: why the Qspi_Ip_HyperflashProgram sends write command for every 2 bytes? 你好@Nhi_Nguyen 谢谢您的帮助。但是在我们的驱动程序中一次写入 2 字节对客户来说太慢了吗?怎样才能提高性能? BR、 狮子座 Re: S32G: why the Qspi_Ip_HyperflashProgram sends write command for every 2 bytes? 你好@LeoLiAP、 这是因为 Hyperbus 支持以下两种类型的数据发送: 驱动程序支持将单个字写入内部缓冲(您的代码是每个地址数据的单个字),然后调用命令将缓冲区发送到 Fls(写入缓冲区)。 顺祝商祺! Nhi Re: S32G: why the Qspi_Ip_HyperflashProgram sends write command for every 2 bytes? 你好@LeoLiAP、 写入 2 字节遵循 Hyperbus 协议,所以我知道我们无法改变这一点。但 SW 团队将改进代码以节省时间,相关票据为ARTDCMEM-1247。 顺祝商祺! Nhi
記事全体を表示
Vision ML with the FRDM-MCXN947 The MCX N microcontroller family includes an eIQ Neutron N1-16 NPU for accelerating neural network models. The FRDM-MCXN947 development board can be combined with a camera and LCD screen to showcase running TinyML vision models on a microcontroller.   MCX N Camera Hardware Setup: The following hardware is used: MCX N FRDM Development Board - FRDM-MCXN947 OV7670 camera (with optional wide-angle lens) NXP LCD-PAR-S035  There are three small modifications needed for the FRDM-MCXN947 board for camera support. Without this modification the camera colors will be incorrect and tinted red.   Change SJ16, SJ26, and SJ27 found on the back of the Rev B board to connect pin 3 (the dashed side) so that it looks like the following:          Then connect the camera and LCD to the FRDM-MCXN947: Plug in the OV7670 camera into J11. It should line up with the orange box.                            Connect the LCD-PAR-S035 LCD into J12. It should be flush with the bottom so that the top 2 rows of pins are left hanging off the edge. Also note that on some LCD-PAR-S035 boards those top two rows of pins are not installed.          It should look like the following when complete           Also as the camera and Ethernet pins are shared, if you need to use the Ethernet+Camera at the same time please see this NXP Community post. MCX N Vision ML Examples: The NXP Application Code Hub contains several vision AI/ML examples: Face Detect Face Detect with Zephyr Multiple Person Detection  CIFAR10 Fashion MNIST There are also Multimedia Processing Pipeline (MPP) examples inside the MCX N MCUXpresso SDK that demonstrate more examples of using vision AI/ML on MCX N. These examples are only available for VSCode/GCC in the Repository-Layout SDK package. Note: It is recommended to use MCUXpresso SDK 25.09 for these examples. The MPP issues in the 25.12 and 26.03 MCUXpresso SDK releases should be fixed in the upcoming MCUXpresso SDK 26.06.  MCX N ML Vision Lab: The attached eIQ Neutron NPU for MCX N Lab Guide - Face Detect.pdf lab document walks through the steps to download an example Face Detect ML project from the NXP Application Code Hub and use the eIQ Neutron Compiler tool to convert a model. It also describes how to update the eIQ and Neutron software libraries in an older MCUXpresso SDK project to work with the latest eIQ Neutron SDK libraries. It is recommended to go through the general MCX N NPU Lab Guide first and then do the attached Face Detect lab second.  The lab is also included below: 1  Lab Overview This document will demonstrate the acceleration provided by the eIQ Neutron NPU using the Multiple Face Detection demo for the FRDM-MCXN947 found on the NXP App Code Hub. The demo will run with the non-NPU optimized model and then the performance can be compared to the NPU optimized version of that same model. It also demonstrates how the NPU optimized version of the face detect model was generated. This lab is written for MCUXPresso IDE but the same basic steps can be used for VSCode or GCC. This lab will also cover how to update the Neutron NPU libraries in the project, as the original Face Detect example uses an older Neutron library version. It is highly recommended to complete the eIQ Neutron NPU for MCX N Lab Guide before starting this lab. 2  Software and Hardware Installation This section will cover the hardware and software needed for this lab. 2.1 Hardware The following hardware is required for this lab: MCX N FRDM Development Board - FRDM-MCXN947 OV7670 camera (with optional wide-angle lens) NXP LCD-PAR-S035 2.2 NXP Software Installation          Install MCUXpresso IDE v25.6 or later. Download the latest eIQ Neutron SDK Download and unzip the latest MCUXpresso SDK for FRDM-MCXN947 using MCUXpresso SDK builder Search for the FRDM-MCXN947 board Then click on Others On the SDK builder page, make sure to select the “eIQ” middleware and that the MCUXpresso IDE toolchain is selected. Then click on Build SDK.   Then click on the Download button and accept the license agreement to download the zip file. 3   Face Detection Example 3.1 Download Face Detect Demo from App Code Hub The code for this lab can be found on the NXP Application Code Hub hosted on Github, and we can use MCUXpresso IDE to directly import the Face Detection example from App Code Hub. Drag-and-drop the FRDM-MCXN947 SDK zip file into the Installed SDKs window, located on a tab at the bottom of the screen named “Installed SDKs”. You will get the following pop-up, so hit OK. Once imported, the Installed SDK tab will look something like this:  In the Quickstart Panel found in the lower left corner, click on Import from Application Code Hub.. In the dialog box that pops up there are many filters available to filter for different devices and types of demos. But since the name of the demo we are interested in is already known, the search box will be faster. Select the AI/ML category and then type in “face detection” and then click on the “Multiple face detection on mcxn947” demo. Make sure you don’t accidently click on the “Multiple Person Detection” demo. On the popup that comes up, click on GitHub link at the top. At that point the Next button at the bottom will become clickable so click on that. The next screen displays the possible branches. In this case there is only main so just click on the Next button at the bottom to go with the default. The next dialog box determines the location on your computer where the code will be downloaded to. You can leave it at the default location if desired or click on Browse to pick your own location. Then click on Next. The next screen will download the code and ask about importing the project. Click on Next to go with the default Import existing Eclipse projects option. Then finally on the last screen click on Finish to import the project into your MCUXPresso IDE workspace. You may get the following warning due to the project being made on an older version of the SDK. Then hit OK to accept the using the newest version.  15. It should look like the following when done: 3.2 Convert Model The demo is already using a model that was converted to take advantage of the eIQ Neutron NPU. This purpose of this section of the lab is to teach new NXP users how that model was converted. Unzip the eIQ Neutron SDK package in a directory of your choosing.   Optionally add \eIQ_NeutronSDK_ \bin to your executable path so that the neutron-compiler utility can be directly called from the command line. Back in MCUXpresso IDE, find the location of the original non-converted model used for this demo by right clicking on the face_detect.tflite file in source/model/ and going to Utilities->Open directory browser here. Copy the directory location as it will be used in the next step Open a Windows Command prompt and navigate to the directory where the model was at from the previous step             Use the Neutron Compiler to convert the Face Detection model: neutron-compiler --input face_detect.tflite --output face_npu.tflite --target mcxn94x 3.3 Update eIQ Neutron Libraries The Face Detect ACH example uses an older version of the eIQ Neutron libraries, and so it needs to be updated to match the Neutron libraries in newest eIQ Neutron SDK since the model was converted with that version of the Neutron Compiler tool. In the frdmmcxn947_multi_face_detection project, right click on the eiq folder and go to Utilities->Open directory browser here Overwrite the Neutron files from the eIQ Neutron SDK folder into your project to update the Neutron libraries to the latest version: File Name Source Directory in eIQ Neutron SDK Target Directory in MCUXpresso SDK libNeutronDriver.a target\mcxn94x\board\ eiq\neutron\mcxn\cm33 libNeutronFirmware.a target\mcxn94x\board\ eiq\neutron\mcxn\cm33 NeutronDriver.h target\mcxn94x\driver\include\ eiq\neutron\driver\include NeutronErrors.h target\mcxn94x\common\include\ eiq\neutron\common\include After the new Neutron libraries are copied over, clean the project to ensure the new libraries will be used 3.4 Board modifcations There are some hardware modifications to the MCX FRDM board required for this demo since the camera pins are muxed with the Ethernet pins and the Ethernet functionality is the default. The board version can be determined by scanning the QR code on the back of the MCX FRDM board with your phone. Most people will have Rev B boards. Rev A: Remove the R157, R158, and R159 resistors from the back of the Rev A board so that it looks like the following: Rev B: Change SJ16, SJ26, and SJ27 found on the back of the Rev B board to connect pin 3 (the dashed side) so that it looks like the following: 3.5 Connect the camera and LCD Plug in the OV7670 camera into J11. It should line up with the orange box. Connect the LCD-PAR-S035 LCD into J12. Note that some older LCD-PAR-S035 LCDs may have an extra set of pins soldered on, and in that case the extra 2 rows of pins should be hanging off the edge like in the photo below.             It should look like the following when complete 3.6 Run Models Now open up model_data.s by double clicking on it, and then modify line 43 to point to the original (non NPU converted) model file named face_detect.tflite. This particular project uses the .tflite file directly. Build the project by clicking on the Build icon in the Quickstart Panel Then download and run the project by clicking on the Debug icon in the Quickstart Panel You should see the demo working with an inference time of 817ms printed on the LCD display. Note: The default camera on the OV7670 is not very wide angle so you have to hold it fairly far back. There are wide-angle lenses that can be purchased to make it easier to demonstrate. Note: After POR there may be some glitching on the camera due to the fact the camera is expecting 2.8V but the board is at 3.3V and the initial HSYNC signal was missed. Press the reset button (SW1) and it should fix any camera issue.  Now let’s use the Neutron optimized model by opening model_data.s again and this time selecting the NPU converted model face_npu.tflite Recompile and reprogram the board. You’ll see it is significantly faster with a 22ms inference time, a 37x improvement! 4  Conclusion This lab demonstrated how the eIQ Neutron NPU on MCX N devices can significantly decrease inference time on quantized models and the steps to generate a NPU optimized model using the command line tools. Also explore the other App Code Hub ML examples available online. FRDM-Training MCXN NPU|ML
記事全体を表示
What is the meaning of FLEXIO_CTRL[DBGE] The reference manual wording on DBGE is a bit short with only "Enables the FLEXIO operation in Debug mode" What happens if it is disabled and you debug code? Trying to figure out what debug operations are safe when using FLEXIO and debugging FLEXIO drivers. I guess it is NOT safe to let the debugger read SHIFTBUFn in receive mode or any other hardware register with read sideeffect, not even by accidently howering over it in the debugger. Re: What is the meaning of FLEXIO_CTRL[DBGE] Hi @Henrik-Wires  If the "Enable FLEXIO operation in debug mode" is disabled, the FLEXIO module stops when the debugger stops the CPU. All FIexIO activity is freeze until execution resumes. This topic has also been discussed in the following thread: Does it means that flexio can't work in debug mode? BR, VaneB Re: What is the meaning of FLEXIO_CTRL[DBGE] Does that also mean that it is safe to access the FLEXIO registers using the debugger if DBGE is disabled, or will reading SHIFTBUFn with the debugger disturb the Shift Status Flag SHIFTSTAT[SSF] Re: What is the meaning of FLEXIO_CTRL[DBGE] Hi @Henrik-Wires  As stated in the S32K3 reference manual, the SHIFTBUFn register must be read only when the corresponding SHIFTSTAT[SSF] flag is set. Re: What is the meaning of FLEXIO_CTRL[DBGE] Hi @Henrik-Wires  Could you please clarify what this will be used for or what kind of analysis you are trying to achieve? Re: What is the meaning of FLEXIO_CTRL[DBGE] Can I somehow block S32DS from attempting to access registers? Only briefly howering over a pointer to SHIFTBUFn makes the debugger access the value which disturbs the FLEXIO state by clearing SHIFTSTAT[SSF] Re: What is the meaning of FLEXIO_CTRL[DBGE] Hi @Henrik-Wires  The IDE itself does not block access to registers. That kind of protection can be implemented using the MPU or XRDC; however, I do think that approach aligns with what you are trying to achieve. Instead, you could monitor when SHIFTSTAT[SSF] is set and then verify whether the corresponding SHIFTBUFn register contains the expected value. Re: What is the meaning of FLEXIO_CTRL[DBGE] I am exploring, writing and debugging a custom low level FLEXIO driver. Experienced odd results while debugging which I suspect is due to S32DS fetching SHIFTBUFn register values while stepping thru the driver, disturbing the SHIFTSTAT[SSF] state and resulting in lost events. Re: What is the meaning of FLEXIO_CTRL[DBGE] The driver obviously monitors SHIFTSTAT and access SHIFTBUFn accordingly. My issue is that it that stepping over the driver code with S32DS can trigger a debug read of SHIFTSTAT, which seems to disturb the state held in that register. For example when howering with the mouse over a pointer to SHIFTSTAT. If I carefully avoid touching any such pointers with the debugger then the driver works. I had hope that disabling DBGE would allow the debugger to access SHIFTSTAT without disturbing the **bleep**FSTAT register state, but from your response this is not the case. Re: What is the meaning of FLEXIO_CTRL[DBGE] Hi @Henrik-Wires  Disabling the DBGE bit does not prevent the debugger from disturbing registers such as SHIFTSTAT, because DBGE does not control debug read behavior. Instead, DBGE controls whether the peripheral keeps running when the core is halted.
記事全体を表示
iMX RT700 EVK accessing SDIO Card Trying to access 1.8V SDIO card on RT700 EVK. Set jumpers JP65 and JP66 to 1-2 using a sample enhanced with debug statements. SDCARD fatfs freertos example. Card inserted. SDCARD fatfs freertos example. Card inserted. --- SD Card Init --- SD card init failed! Status: 1834 Possible causes: - Card doesn't support 1.8V signaling - Voltage switch failed - Card communication error Trying basic card detection... OCR: 0x 0 Flags: 0x 0 Re: iMX RT700 EVK accessing SDIO Card Hi @MikeAtPhantom , Thank you so much for your interest in our products and for using our community. Please carefully check the readme file. I did a test for you, the SDK demo runs okay. HW: MIMXRT700-EVK    JP65 1-2 connected SW:  mimxrt700evk_sdcard_fatfs_freertos_cm33_core0 SD:    SanDisk  Ultra   32G Please use Recommend SD Cards , and try to run the example again. Best Regards MayLiu
記事全体を表示
i.MX RT1060 API の LPSPI_MasterTransferEDMA は 24 ビットのフレーム サイズをサポートしていませんか? LPSPI を使用して DMA 経由で 24 ビット フレームを書き込もうとしています。アプリケーションは重要ではありませんが、私の例では、メモリから外部 DAC にデータを送信することです。私はこれを DMA で動作させたいと思っています。なぜなら、最終的には TCD のリンク リストを PIT と一緒に使用して、CPU オーバーヘッドなしで DAC を継続的に更新するためです。これは外部 ADC および DAC を使用する一般的なアプリケーションです。16 ビット DAC/ADC には 24 ビットのフレーム要件があることも一般的です (上位バイトはコマンド用、下位バイトはデータ用)。uint8_t データを使用して転送を 3 バイトに分割するのではなく、uint32_t データを使用して 24 ビットのフレーム サイズで送信し、先頭バイトを無視します。 さて、LPSPI と DMA の構成に移ります。 1.imxRT1060 SDK の API LPSPI_MasterInit 関数の lpspi_master_config_t 構造を使用すると、 bitsPerFrame を 24 に設定できます。DMA を使用せずに標準転送を行う場合、これは問題ではありません。 2. ただし、API の LPSPI_MasterTransferEDMA 関数で DMA を使用する場合、24 ビット フレーム サイズのケースは eDMA ハードウェアによって処理またはサポートされませんか?LPSPI_MasterTransferEDMALite では、DMA 転送幅は edma_transfer_config_t 構造体で設定されます。具体的には、srcTransferSize フィールドと destTransferSize フィールドは、SPI フレーム サイズ (bytesPerFrame) から導出される bytesEachRead 値と bytesLastWrite 値に基づいて構成されます。 /* LPSPI_MasterTransferPrepareEDMALite */ uint32_t bytesPerFrame = ((base->TCR & LPSPI_TCR_FRAMESZ_MASK) >> LPSPI_TCR_FRAMESZ_SHIFT) / 8U + 1U; if (bytesPerFrame <= 4U) { handle->bytesEachWrite = (uint8_t)bytesPerFrame; // for 24bit frames = 3 handle->bytesEachRead = (uint8_t)bytesPerFrame; // .... handle->bytesLastRead = (uint8_t)bytesPerFrame; // .... } /* now back in LPSPI_MasterTransferEDMALite */ switch (handle->bytesEachRead) //bytes each transfer { case (1U): transferConfigRx.srcTransferSize = kEDMA_TransferSize1Bytes; transferConfigRx.minorLoopBytes = 1; if (handle->isByteSwap) { addrOffset = 3; } break; case (2U): transferConfigRx.srcTransferSize = kEDMA_TransferSize2Bytes; transferConfigRx.minorLoopBytes = 2; if (handle->isByteSwap) { addrOffset = 2; } break; case (4U): transferConfigRx.srcTransferSize = kEDMA_TransferSize4Bytes; transferConfigRx.minorLoopBytes = 4; break; default: transferConfigRx.srcTransferSize = kEDMA_TransferSize1Bytes; transferConfigRx.minorLoopBytes = 1; assert(false); break; } デフォルトのケースが発生し、3 バイトのケースは処理されないためエラーが発生します。EDMAハードウェアは3バイト転送をサポートしていますか?基本的に、uint32_tのデータとフレームを3バイトとして扱い、最上位バイトを無視してDMA転送を行いたいのですが、可能ですか? Re: i.MX RT1060 API's LPSPI_MasterTransferEDMA does not support 24bit framesize? こんにちは@azoneさん、 弊社の製品にご興味をお持ちいただき、またコミュニティをご利用いただき誠にありがとうございます。 次のリンクを確認してください。eDMA は 1、2、4、8、16、32、64 バイトの転送サイズをサポートしており、24 ビット (3 バイト) の転送サイズはサポートしていないことが説明されています。 MCUXpresso SDK APIリファレンスマニュアル: EDMA: 拡張ダイレクトメモリアクセス (eDMA) コントローラドライバ よろしくお願いいたします。 メイリュー Re: i.MX RT1060 API's LPSPI_MasterTransferEDMA does not support 24bit framesize? わかりました。確認してくれてありがとう。これで、動作させるために時間を無駄にすることがなくなりました。したがって、唯一の方法は、すべてをuint8_tデータとしてkLPSPI_MasterPcsContinuousで3バイトとして送信することです。これは他のすべてのペリフェラルでも同じ方法で実行しているので問題ありませんが、16ビットDAC実装の場合は不要なオーバーヘッドが発生します。ありがとうございます。
記事全体を表示
NXP mpc5744p MCUボードと開発キットMotorGDボードの3Dモデル こんにちは、みんな、 mpc5744p MCU や DevKit motorGD ボードなどの NXP 製品を含む新しいテストベンチを開発しています。 私はテストベンチ用にプロフェッショナルな 3D 画像を入手しようとしており、次の 3D ファイルが必要です: 1. mpc5744p MCUボード 2. DevKit モーターGDボード NXPのウェブサイトで検索したら、.zipファイルを見つけました。レイアウト用のファイルがありましたが、Easyeda を使用して開くことができませんでした。 1. LAY-29379_B.zip 2. LAY-29333_E.zip どなたか、これらを開くか、2 つのボードの 3D モデル ファイルを取得するのを手伝っていただけませんか。 ありがとう、良い一日をお過ごしください! Re: 3d Model of NXP mpc5744p MCU Board & Devkit MotorGD Board こんにちは、 NXPのウェブサイトで検索したら、.zipファイルを見つけました。レイアウト用のファイルがありましたが、Easyeda を使用して開くことができませんでした。 1. LAY-29379_B.zip 2. LAY-29333_E.zip これらは、Candace: allegro で設計されたレイアウト ファイルです。 レイアウトデザインから 3D モデルを抽出できるとは思っていません。 私は次の方法を見つけました: EAGLE + Fusion 360 .brdファイルを開くEAGLE のファイル。 Fusion 360 Sync 機能を使用します。 Fusion 360 → EAGLE デザインをインポートに移動します。 コンポーネントを含む完全な 3D PCB モデルを生成します。 機械統合のために STEP (.step) または IGES としてエクスポートします。 レイアウトデザインから 3D モデルを抽出できるとは思っていません。 500MB 程度の STEP ファイルをコミュニティ経由で共有することはできません。 よろしくお願いいたします。 ピーター Re: 3d Model of NXP mpc5744p MCU Board & Devkit MotorGD Board こんにちは、 petervlnaさん ご返信ありがとうございます。 提案された解決策をEagle + Fusion 360を使用して試しましたが、残念ながら、ファイルを開くことができないことを示すエラーが発生しました (下の画像を参照)。EasyEDA、Altium、KiCadなどの他の PCB ソフトウェアを使用する場合にも、同じ問題が発生します。 この時点で、 .STEP 形式の 2 つのボードの 3D モデルが緊急に必要です。これらのファイルを、 Google Drive、OneDrive、MEGAなどのクラウド ストレージ サービスやその他の便利なプラットフォーム経由で直接提供していただければ幸いです。 改めましてサポートありがとうございます。ご返信をお待ちしております。 よろしくお願いします、 アハメド Re: 3d Model of NXP mpc5744p MCU Board & Devkit MotorGD Board こんにちは、 はい、そのような場合は、NXP サポートにチケットを送信してください。 このようなファイルを取得するには、NXP との有効な NDA も締結する必要があります。 当社のサポート ポータルでは 2GB のファイルが許可されており、以前にも STEP ファイルを共有したことがあるため、STEP モデルをサポート ポータル経由で共有することが可能です。 内部ファイルを当社の公式システム外で共有することはできません。 よろしくお願いいたします。 ピーター Re: 3d Model of NXP mpc5744p MCU Board & Devkit MotorGD Board こんにちは、 petervlnaさん ご提案ありがとうございます。番号 (CASE: 00756530) でCASEを開設しました。 できるだけ早くファイルを入手したいと考えています。 どうもありがとう。 よろしくお願いします、 アハメド
記事全体を表示
S32K312 uart AsyncReceiveコールバックイベント情報は、SPI DMAが大量のデータを転送するときに常にエラーになります。 こんにちは、 S32K312 S32DS3.5 RTD4.0.0 プロジェクトでは、SPI0 と SPI1 は DMA モードで動作し、UART1 は割り込みモードで動作します。 UART1 は、12 バイトのフレームを同期送信または非同期受信するときに正常に動作します。 しかし、SPI DMA が大量のデータを転送する場合、uart AsyncReceive イベント情報は常にエラーになります。 何か提案はありますか? Re: S32K312 uart AsyncReceive callback event is always error when SPI DMA transfer mass data はい、それは割り込み優先度の問題です。Uart1 は優先度を上げた後に動作します。 本当にありがとう! Re: S32K312 uart AsyncReceive callback event is always error when SPI DMA transfer mass data こんにちは、 SPI DMA バースト中の UART 非同期受信エラーの原因としては、以下のことが考えられます。 1. 割り込み優先度の問題 - DMA 完了または他の ISR の優先度が同等かそれ以上であるため、UART RX 割り込みはすぐには処理されません。 - 結果: UART RX FIFO がオーバーフロー → オーバーランまたはフレーミング エラー。 LPUART1_IRQn がすべての DMA 関連 IRQ (例: DMATCDx_IRQn) よりも高い優先度 (数値的に低い) を持つことを確認します。割り込みグループ化によりプリエンプションが許可されることを確認します。 2. DMAによるバスの占有 - SPI の eDMA チャネルは、大きなバースト中に AXBS クロスバーを飽和させる可能性があります。 - CPU およびペリフェラル レジスタ アクセス (UART RX 処理を含む) が遅延され、ISR レイテンシが増加します。 eDMAエンジンのストールを許可するようにSPI DMAチャネルを構成する(BWC設定)   BR、ペトル
記事全体を表示
LPC1768+SSP0+GPDMA 的一些问题 为什么在 SSP0 中打开 DMACR 并将一些数据传输到 BUF 之后,DMACR 被 RESET 为零,SSP0DR 一直在变化,但是 BUF 数据保持不变。在中断期间我还尝试重新打开 DMACR,但是 BUF 数据仍然没有变化。 以下是代码配置: #define SPI_RX_LEN 5386 extern U8 SPIRXBUF[SPI_RX_LEN]; void DMAInit_SPI_RX(U8 *destAddr, U32 len) { U32 part1 = (len> 4095) ?4095 : len; U32 part2 = (len> 4095) ?(len - 4095) : 0;// 拆分传输(单通道最大 4095字节)   lpc_sc->pconp |= (1<< 29); // 使能gpdma时钟 LPC_GPDMA->DMACConfig |= (1<< 0);//使能 GPDMA LPC_GPDMA->DMACIntTCClear |= 0x01; // 清除通道0传输完成标志 LPC_GPDMA->DMACIntErrClr |= 0x01; // 清除通道0错误标志   // 链表项1:传输part1字节 lli[0].srcAddr= (u32)&lpc_ssp0->dr; // 源:spi0 数据寄存器 lli[0].destAddr= (U32)destAddr; // 目的:缓冲区起始 lli[0].control= (part1& 0x0FFF) // 传输大小(字节数) | (0x00<< 12) // 源突发大小 | (0x00<< 15) // 目的发大小 | (0x00<< 18) //源数据宽度 | (0x00<< 21) //目的数据宽度 | (0x00<< 26) //源地址不变(外设寄存器)。 | (0x01<< 27) //目的地址自增 | (1u<< 31); // 使能中断   // 链表项2:传输part2字节(若需要) if (part2> 0) { lli[0].nextLLI = (U32)&lli[1]; // 指向链表项2 lli[1].srcAddr= (u32)&lpc_ssp0->dr; lli[1].destAddr= (U32)(destAddr + part1); // 缓冲区偏移 lli[1].control= (part2& 0x0FFF) // 传输大小(字节数) | (0x00<< 12) // 源突发大小 | (0x00<< 15) // 目的发大小 | (0x00<< 18) //源数据宽度 | (0x00<< 21) //目的数据宽度 | (0x00<< 26) //源地址不变(外设寄存器)。 | (0x01<< 27) //目的地址自增 | (1u<< 31); // 使能中断 lli[1].nextLLI= 0; // 结束链表 } else { lli[0].nextLLI = 0; }   // 配置 DMA 通道 0 LPC_GPDMACH0->DMACCConfig = 0; LPC_GPDMACH0->DMACCLLI = (U32)&lli[0]; // 链表起始地址 LPC_GPDMACH0->DMACCSrcAddr = lli[0].srcAddr;// 源地址(spi0 dr) LPC_GPDMACH0->DMACCDestAddr = lli[0].destAddr; // 目的地址 LPC_GPDMACH0->DMACCControl = lli[0].control; // 控制字 LPC_GPDMACH0->DMACCConfig = (0x01<< 15) //中断错误 | (0x01<< 14) //终端计数中断 | (0x02<< 11) // 传输类型:外设到内存 | (0x00<< 6) //目的外设:存储器 | (0x01<< 1) // 源外设:SSP0 RX(参考手册) | (0x01<< 0); // 通道使能   GPDMAEnabe(); }     void DMA_IRQHandler(void) { if(LPC_GPDMA->DMACIntTCStat& 0x01) // 通道0传输完成 { LPC_GPDMA->DMACIntTCClear = 0x01; // 清除标志 //SSPSlave_Init(); // run_lamp_glitter; // lpc_ssp0->dmacr |= (1<< 0); // LPC_GPDMACH0->DMACCConfig |= (0x01<< 0); LPC_GPDMA->DMACConfig |= (1<< 0);//使能 GPDMA 时间++; } if(LPC_GPDMA->DMACIntErrStat& 0x01) // 通道0错误 { LPC_GPDMA->DMACIntErrClr = 0x01; // 清除标志 } } void SSPSlave_Init(void) { lpc_sc->pconp |= (1<< 21); /* 打开 ssp 电源 */ /***************************************************************** * 初始化 SSP 的通讯方式,设置数据长度为 8bit,帧格式为 SPI,SCK 为低有效、 * 数据在sck 的第二个时钟沿采样,设置位速率。 ******************************************************************/ LPC_SSP0->CR0 = (0x00)<< 😎 | /* 设置spi位速率*/ (0x01<< 7) | /* CPHA 时钟输出相位 */ (0x00<< 6) | /* CPOL 时钟输出极性 */ (0x00<< 4) | /* FRF 帧格式 00=SPI,01=SSI, */ /* 10=Microwire,11=保留 */ (0x07<< 0); /* DSS 数据长度,0000-0010=保留 */ /* 0011=4位,0111=8位,1111=16位*/ lpc_ssp0->cpsr = 2; /* 时钟分频寄存器*/   LPC_SSP0->CR1 = (0x00<< 3) | /* SOD 从机输出禁能,0=允许 */ (0x01<< 2) | /* MS 主从选择,1=从机 */ (0x01<< 1) | /* SSE SSP使能,1=使能 */ (0x00<< 0); /* LBM 回写模式 */   sysTimeDlay(5); lpc_ssp0->dmacr |= (1<< 0);   } LPC17xx Re: LPC1768+SSP0+GPDMA some problem 你好@Lee_Lee 我认为 DMA 正在 "读取空的 SSP FIFO",但由于访问宽度不正确,数据没有正确写入内存。 您目前的配置是 (0x00<< 18)// 源数据宽度(0x00<< 21)// 目的数据宽度 但在 LPC 中: SSP 的 DR 寄存器是一个 16 位寄存器 即使使用 8 位 SPI 模式,对 SSP0->DR 的 DMA 访问仍必须是 16 位访问。 DMA 实际上没有将数据正确写入内存 结果是 BUF 保持不变。 因此,我认为您可以尝试将源代码和 des 宽度改为 16。 BR 哈利
記事全体を表示
FlexGUI-PF8X PF8200 的编程问题 亲爱的; 当我使用 FlexGUI-PF8X 离线工具为 PF8200 的固件 (SC33PF8200KKES) 编程时,报告了以下问题: 脚本解析失败(格式错误)。具体信息见图 1。 我可以正常使用 PF8100 进行刻录和写入。 谢谢! 致以最崇高的敬意 Re: Programming issue with FlexGUI-PF8X PF8200 我没测试OTP 的script我测试了TBB script是可以运行的,在GUI 选择TBB 以后 我用的是10.0.0的GUI 版本 Re: Programming issue with FlexGUI-PF8X PF8200 Dear;          好的,我按照最新的GUI后测试一下。谢谢!         Best Regards! Re: Programming issue with FlexGUI-PF8X PF8200 TBB 的那个脚本能运行吗? 不行的话现在最新的GUI! GUI PMIC软件|汽车|恩智浦半导体 Re: Programming issue with FlexGUI-PF8X PF8200 Dear;         固件见附件。谢谢!         Best Regards! Re: Programming issue with FlexGUI-PF8X PF8200 能发我看看是哪个script吗? Re: Programming issue with FlexGUI-PF8X PF8200 Dear;         该次烧写的固件是直接NXP官网下载的,谢谢!       Best Regards! Re: Programming issue with FlexGUI-PF8X PF8200 不会,我也是WIN11 Re: Programming issue with FlexGUI-PF8X PF8200 看这个附件的文档里面有更新的FW,从第12页开始看4 Installing and configuring software and tools 。 Re: Programming issue with FlexGUI-PF8X PF8200 Dear;          我现在使用的是windows 11操作系统,我看这个软件支持的操作系统是windows 10或windows 7,这个是否会影响GUI的正常工作?谢谢!           Best Regards! Re: Programming issue with FlexGUI-PF8X PF8200 Dear;          谢谢您的支持,已经搞定了,谢谢!          Best Regards!
記事全体を表示
IMX8MQ 摄像机 mipi 问题 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 我正在 imx8mq-EVK 板上开发摄像头 mipi 驱动程序,我的摄像机输出数据是 RAW-10 位。 当我参考 ov5640 驱动程序代码时,我遇到了以下问题。 1. 在 “驱动程序/媒体/平台//mxc/捕获/mx6s_捕获.c” 中,有一些寄存器如下所示,但我无法在参考手册中找到有关以下寄存器的任何线索。(来自查看代码,我知道这些寄存器的基地址是0x0x30A90000) #define CSI_CSICR1 0x0 #define CSI_CSICR2 0x4 #define CSI_CSICR3 0x8 #define CSI_STATFIFO 0xC #define CSI_CSIRXFIFO 0x10 #define CSI_CSIRXCNT 0x14 #define CSI_CSISR 0x18 #define CSI_CSIDBG 0x1C #define CSI_CSIDMASA_STATFIFO 0x20 #define CSI_CSIDMATS_STATFIFO 0x24 #defineCSI_CSIDMASA_FB1 0x28 #define CSI_CSIDMASA_FB2 0x2C #define CSI_CSIFBUF_PARA 0x30 #define CSI_CSIIMAG_PARA 0x34 #define CSI_CSICR18 0x48 #define CSI_CSICR19 0x4c 2. 同样的问题,在参考手册中找不到有关以下寄存器(0x180~0x198)的任何介绍。(基地地址为 0x30A70000)。 in"driver/media/platform/imx8/mxc-mipi-csi2_yav.c" 、 printk("MIPI CSI2 HC IGNORE_VC 0x180 = 0x%x\n", readl(csi2dev->base_regs + 0x180)); printk("MIPI CSI2 HC VID_VC 0x184 = 0x%x\n", readl(csi2dev->base_regs + 0x184)); printk("MIPI CSI2 HC FIFO_SEND_LEVEL 0x188 = 0x%x\n", readl(csi2dev->base_regs + 0x188)); printk("MIPI CSI2 HC VID_VSYNC 0x18C = 0x%x\n", r eadl(csi2dev->base_regs + 0x18C)); printk("MIPI CSI2 HC VID_SYNC_FP 0x190 = 0x%x\n", readl(csi2dev->base_regs + 0x190)); printk("MIPI CSI2 HC VID_HSYNC 0x194 = 0x%x\n", readl(csi2dev->base_regs + 0x194)); printk("MIPI CSI2 HC VID_HSYNC_BP 0x198 = 0x%x\n", readl(csi2dev-base_regs + 0x198)); 3. 在参考手册中,提到了一些 " 数据类型 ",如下所示, " 13.6.3.6.4 RAW10(数据类型 = 0x2B)" 如何将值 0x2B 设置为数据类型? 我的参考手册版本是: 名称:i.MX 8M 双/8M 四极管/8M 四核应用处理器参考手册 文件编号:IMX8MDQLQRM 修订版 0, 01/2018 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: IMX8MQ Camera mipi Question 我曾在多个 i.MX8MQ MIPI-CSI 启动器上看到过这种确切的行为--驱动程序通常看起来很好,但当显示/HDMI 端启动时,由于 CSI-2 通道映射、数据类型或时钟树中的细微问题而发生故障。 在 i.MX8MQ 上,CSI-2 接收器的要求极为严格: 正确的数据类型匹配(RAW10 vs RAW8 vs YUV422) 正确的车道极性 + 映射 DISP/HDMI PLL 切换后,传感器时钟保持稳定 正确的 pinctrl(许多板在 GPIO 模式下意外离开了数据通道) 如果出现上述任何一种不匹配情况,CSIS 块会保持 "流 "状态,但会静默地丢弃所有数据包--看起来与您描述的情况非常相似。 作为参考,以下是我们开发的一些上游 MIPI/CSI 摄像头驱动程序,它们显示了在 i.MX8 级 SoC 上通常可以解决这个问题的确切的 DT 模式和 CSI 设置顺序: Linux-next https://web.git.kernel.org/pub/scm/linux/kernel/git/next/linux-next.git/commit/?id=fa9e6df636fb8b3b27570f38c53640c9e2b02f79中的 MIPI 传感器驱动程序示例 Zephyr 中的另一个传感器(用于比较 MIPI/时钟序列) https://github.com/zephyrproject-rtos/zephyr/commit/c784481ca039ccd606a192ee07bc83f6b0117e59 媒体管道更新示例(CSI 路由 + 格式协商) https://web.git.kernel.org/pub/scm/linux/kernel/git/next/linux-next.git/commit/?id=9d382f6a9978916317b3fb4ef07b5fec684adde0 如果您正在设计完整的相机流水线(传感器 → MIPI → CSI-2 → ISP/显示屏),本深入探讨可能会对您有所帮助: https://siliconsignals.io/blog/v4l2-camera-stack-step-by-step-guide-for-custom-devices/ https://www.kernel.org/doc/html/v4.9/media/kapi/v4l2-intro.html Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好 [email protected]、 您能详细说明需要做哪些更改才能解决这些问题吗? 对我来说,每个像素都缺少 4 位。我已经为我的问题启动了一个主题。请看一看。 https://community.nxp.com/message/1195672 提前感谢! 瓦西姆 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 我也遇到了同样的问题。 有人在接收 10 位系统时解决了这个问题吗? 此致, 雅各 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好 [email protected]、 您能分享一些关于如何解决该问题的信息吗?我问这个问题是因为我们也面临着类似的问题,如果能了解更多关于你们如何解决问题的信息就更好了。是平台方面的问题还是传感器方面的问题? 提前感谢! 锡瓦拉姆 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,伦卡、 感谢您的答复。 我已经解决了这个问题。 还有一个问题令我困惑 、 我一直认为 MIPI CSI 驱动程序每帧应该接收 1280000 字节(1280*800*10 位/8),但实际上是 1024000 字节(1280x800)。我不知道原因。 根据 RM (imx6) 如下所示,对于 RAW10,数据大小应为 (n * 像素 * 5/4) 字节。 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,杨、 我不建议你在设备树中更改 MIPI PHY 时钟。你写道,你的摄像机是 1280x800,60fps,灰色 10 位。双通道,我想电路板支持包。不直接支持这个配置。你还写道,一段时间后图像就错位了。根据我的经验,如果没有为给定的分辨率正确设置摄像机寄存器,如果相机时钟不稳定,就会发生这种情况。尽管如此,你不需要使用 iMX6 文档/源代码来获得 iMX8 系列微控制器。你能不能提供 0x3800 ~ 0x3815 和 0x3035 ~ 0x3037 范围内的寄存器设置? 我在将 720p 分辨率设置为 60fps 时也遇到了问题。我将尝试联系相机所有者,寻求有关此类配置的帮助。 亲切的问候, Lenka Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,伦卡、 感谢您的帮助。 目前,我能收到一张完整的图像,但图像并不稳定。1 分钟后,图像将错位。相机传感器供应商建议修改 MIPI-CSI 像素时钟,如您所知,RM 中没有关于 MIPI CSI 的有用信息。我在恩智浦网站上找到了一些文件,如下所示,但我仍然很困惑,因为这些文件是针对 iMX6 的。 https://www.nxp.com/files-static/32bit/doc/app_note/AN5305.pdf 根据该文件、 我尝试修改 "IMX8MQ_CLK_CSI1_PHY_REF_DIV "为<178560000> ,但在 linux 系统文件中验证后发现并不匹配。 我的问题是 、 1.IMX8MQ_CLK_CSI1_PHY_REF_DIV " 是 MIPI 时钟,对吗? 2 'IMX8MQ_CLK_CSI1_CORE_DIV' 和'IMX8MQ_CLK_CSI1_ESC_DIV' , 用途是什么? 3.如何修改 'IMX8MQ_CLK_CSI1_PHY_REF_DIV' 的值,使其完全符合我的要求? 我的相机是 1280x800、60fps、灰色 10 位。双车道 我还评论了 "基地址切换 "功能,否则内核将打印"基地址切换更改错误" 。我不确定这种行为是否必要。 谢谢。 杨青 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,杨、 1.这些寄存器与 iMX8 上实现的任何寄存器都不匹配。 2.iMX8 尚不支持这些寄存器。 3.数据类型禁用寄存器(偏移量0x38)用于输入数据类型重设,但可以忽略。如果将摄像头和 ISI 寄存器正确设置为目标数据类型,那么也应该可以正常工作。 如果您还有其他问题,请随时提出。 祝你好运 伦卡 Re: IMX8MQ Camera mipi Question <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,杨 关于 1. iMX8M MIPI-CSI 4 通道配置 对于其他问题(未在参考手册中描述),可能建议 向 NXP 当地营销办事处申请。注意,将有新的参考手册修订版 提供最新信息。 问候 igor ----------------------------------------------------------------------------------------------------------------------- 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
Trace32デバッグを使用したS32K388 拝啓、 Trace32 を使用して S32K388 をデバッグしたいと思います。Trace32 プラグインをインストールするには、以下のリンクにアクセスしました。 https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-Lauterbach-TRACE32-debugger-plug-in-into-S32/ta-p/1112237 その後、Trace32 デバッグ構成を使用して、シングルコア プロジェクトとマルチコア プロジェクトの両方の新しいプロジェクトを作成しました。 しかし、Trace32 を使用してデバッグしようとすると、常にエラー メッセージが表示されます。 また、複数のコアをデバッグする場合、 M7_1_0.elfとM7_2_0.elfをプログラムできないという問題が発生します。 これをテストするのを手伝っていただけますか? ありがとうございます。 BR、 ショーン・ウー Re: S32K388 using Trace32 debug こんにちは、 S32DS から直接どのように動作するのかはわかりません。動作させることができなかったからです。 しかし、私はS32DSを使ってTrace32 powerviewを起動したことがありませんでした。 T32 フォルダーから PowerView を起動し、メニューからプログラミング スクリプトを実行するだけです。 ここにはプログラミング スクリプトがあります。Powerview で実行し、デバイスをプログラムするだけです。 その間に、S32DS 経由で CAN を使って起動して実行できるかどうかを確認します。 よろしくお願いいたします。 ピーター Re: S32K388 using Trace32 debug こんにちは、 petervlnaさん s32k38x.cmmとs32k38x.bin(おそらくあなたのフォルダ内のこの名前を私に知らせてもらえますか?このファイルはありません。 ありがとうございます。 BR、 ショーン・ウー Re: S32K388 using Trace32 debug こんにちは、 プライベートメッセージで送信しました。 よろしくお願いいたします。 ピーター Re: S32K388 using Trace32 debug 親愛なるペテヴルナ様 ご協力いただきありがとうございます。 BR、 ショーン・ウー Re: S32K388 using Trace32 debug 親愛なるpetervlna様 私はあなたの s32k38x.cmm を使用していますが、うまく動作します。ご協力いただきありがとうございます。 BR、 ショーン・ウー
記事全体を表示
AHBによるフラッシュ書き込みアクセス こんにちは。mimxrt1050 コントローラと NOR フラッシュ QSPI でフラッシュ書き込みアクセスがサポートされているかどうかを知りたいです。これは HyperFlash でのみ利用可能であると読みましたが、確認したいと思います。 よろしくお願いします。 ブートROM|ブート|フラッシュ コアとメモリ Re: Flash write access with AHB こんにちは、Sam。現在、IP 操作は動作していますが、NOR フラッシュ QSPI は AHB を使用したフラッシュ書き込みをサポートできますか? Re: Flash write access with AHB @vanessa_dis MIMXRT1050 の FlexSPI コントローラは、QSPI NOR フラッシュの読み取り、書き込み、消去操作を完全にサポートしています。EVK ボードで使用するには、デフォルトの HyperFlash チップからスイッチするためのハードウェアの変更のみが必要です。 https://www.nxp.com/docs/en/application-note/AN12108.pdfQSPIフラッシュからのブートを有効にする方法 Re: Flash write access with AHB こんにちは、 私はAHBアドバンストハイパフォーマンスバスを恐れています Re: Flash write access with AHB @vanessa_dis あなたの言いたいことは分かりました。 はい、i.MX RT1050 および RT1060 シリーズの FlexSPI コントローラは、AHB バスを使用した外部 QSPI NOR フラッシュへの書き込みアクセスを完全にサポートしています。この機能は HyperFlash に限定されません。 FlexSPIコントローラは、シリアルNORフラッシュ(QSPIをカバー)、HyperFlash、HyperRAMなど、さまざまな外部メモリタイプをサポートする柔軟なアーキテクチャで設計されています。 。コントローラは、サポートされているこれらのデバイスに対して、AHBバスを介してメモリマップされた読み取りおよび書き込みアクセスを提供します。 。 https://www.nxp.com/docs/en/nxp/application-notes/AN12239.pdf Re: Flash write access with AHB HAB(ハイアシュアランスブーツ)の詳細をお問い合わせいただきましたか? https://spsdk.readthedocs.io/en/stable/images/hab.html 安全なアクセスで以下の AN を参照してください (申し訳ありませんが、直接送信することはできません。アクセスを申請するか、地元の営業/FAE にお問い合わせください)。 AN12681 i.MX RT10xxでHABセキュアブートを使用する方法 [AN979510]
記事全体を表示
MCUXpresso IDEとSDKのインストール (日本語ブログ) 0. この記事は? NXPのマイコン用ソフトウェア開発環境MCUXpressoとそのSDKは無料で提供されていて,誰でも簡単にインストール可能!すぐにサンプル・コードを動かしてみることができます.😃 このブログ記事は,MCUXpresso IDEとSDKのインストール方法をステップ・バイ・ステップで紹介します. ※ この記事では使用する基板の例としてFRDM-MCXA153を使います インストール手順の解説動画を公開しました.視聴はこちらのリンクから.   目次 0. この記事は? 1. MCUXpresso IDEって? 2. nxp.comへのログイン 3. MCUXpresso IDEのインストール 4. SDKのインストール 4.1 MCUXpresso IDEの起動とワークスペース 4.2 SDKのインストール手順 4.3 準備完了! 5. おまけ:このまま基板の動作を試してみるには 参考資料 1. MCUXpresso IDEって? NXPが提供している汎用マイコンの各種サンプル・コードは,NXPが無料で提供するソフトウェア開発環境:MCUXpressoで動作するように作られています. このMCUXpressoには「MCUXpresso IDE (以下IDE)」と「MCUXpresso VisualStudio Code (以下VSC)」の2種類があり,IDEはすべての機能をひとつにまとめたアプリケーション.VSCはMicrosoft社が提供するVisualStudio Codeのプラグインとして提供されています. このブログではこの2種類のうち,IDEとSDKのインストールの方法を紹介します. IDEはWindows,macOS,Linuxで動作し,いずれのOSでも同じユーザ・インターフェースでの操作が可能です. MCUXpressoで動作するサンプル・コードを試してみるには,まずその準備としてIDEをインストールし,さらに動作させるマイコン/基板(ターゲット)のSDKをインストールしておかなければなりません. IDEはIntegrated Development Environmentの略で,統合開発環境アプリケーションです.このアプリケーションにはソースコードを編集するエディタをはじめ,コンパイラやリンカといったツールチェーン,コードをプロジェクト単位にまとめて,さまざまな設定と一緒に管理してくれるソフトウェアなどが含まれています. SDKはSoftware Development Kitの略で,マイコン・チップ毎に必要なドライバ・コード,設定情報が含まれています.SDKは作成しようとするマイコン・チップや基板(ターゲット)ごとにインストールしておかなければなりません. ではこれらのインストール方法をステップごとに解説しましょう. この記事はmacOSを用いた例となっていますが,WindowsやLinuxでもほぼ同じ操作でインストールできます. 2. nxp.comへのログイン これ以降の作業を行うには,あらかじめnxp.comにログインしておかなくてはなりません. もしまだ nxp.com のアカウントをお持ちでない場合には,先に登録を済ませたのちにログインしてください. MyNXPアカウントの登録方法はこちら 3. MCUXpresso IDEのインストール IDEのインストーラをMCUXpresso IDEのダウンロードサイトからダウンロードします.このダウンロードにはnxp.comでのユーザ登録が必要なので,もしまだであればあらかじめ済ませておきましょう. MCUXpresso IDEのダウンロードサイト行き「ダウンロード」ボタンを押す. ページがスクロールし,ダウンロードページへのリンク・ボタンが表示される.この「ダウンロード」ボタンを押す. MCUXpresso IDEのリンクをクリック. 利用規約が表示される.問題がなければ「I Agree (同意)」ボタンを押す. 自分が使うOSに合わせたインストーラを選んでリンクをクリック. ダウンロードするインストーラはLinuxならファイル名末尾の拡張子が「.deb.bin」のものを.Windowsなら「.exe」を. macOS用は拡張子が「.pkg」ですが2種類あります.M1以降のMシリーズ(Arm)プロセッサ搭載のMacなら「MacOSX - aarch64」,インテルCPU搭載のMacなら「MacOSX - 86-64」をダウンロードします. ※ バージョン番号が違う場合は読み替えてください ダウンロードが完了したら,インストーラを起動.表示される手順に従ってインストールを完了させます.   4. SDKのインストール   4.1 MCUXpresso IDEの起動とワークスペース MCUXpresso IDEのインストールが完了したら,MCUXpresso IDEを起動します. macOSでは,起動後にワークスペースをどこにするか聞いてきます(ガイド動画2:49付近).ワークスペースとは作業を行うためのフォルダです. デフォルトではユーザ・フォルダの中の,「Documents」の中に新しいフォルダが作られます. ※ 下図はデフォルト設定表示の例.この例ではdemoというユーザ名で作業しているので「/Users/demo/..」のような指定となっています.  ワークスペース(フォルダ)はユーザ・フォルダの中なら好きな場所にできます.下図の例ではユーザ・フォルダの中に「mcux」を作り,さらにその中で「project0」という名のワークスペースが作られます. 4.2 SDKのインストール手順 起動(起動とワークスペースを指定を完了)すると,下図のようなウェルカム表示が現れるのでこの中の「Download and Install SDKs」をクリック. しばらくサーバへの問い合わせを行ったあと,下図のような表示となります.このデフォルトの表示状態では右側と下側の表示が隠れてしまっているので,ウィンドウのサイズを拡げるか,表示を適宜スクロールします. ウィンドウサイズを拡げて表示域を確保 表示右上部の検索フィールドに,使用する基板やマイコンの型番を入力. ここでは例としてFRDM-MCXA153を使うので「A153」を入力した.その結果,FRDM-MCXA153基板が候補として表示された. FRDM-MCXA153基板を選択すると「Install」ボタンがハイライト表示されるので,これをクリック インストール中はダイアログボックスが表示される インストールが完了すると,ウェルカム表示に戻る. この表示をタブのクローズボタンで閉じる. IDEのデフォルト表示状態になる. 下部中央の表示枠(ペイン)のInstalled SDKタブにインストールされたSDKが表示される 4.3 準備完了! これで準備は整いました! 左上のペイン内の「Project Explorer」で,新しいプロジェクトを作成したり,SDKやGitHubまたはダウンロードしてきたプロジェクトをインポートして実行してみることが可能です. 5. おまけ:このまま基板の動作を試してみるには SDKにはサンプル・コードが含まれています. ここまでFRDM-MCXA153を例としてSDKをインストールしたので,そのままこの中にあるサンプル・コードを試してみることにします. まず基板とコンピュータをUSBケーブルで接続しておきます.FRDM-MCXA153では「MCU-Link」の表示のあるUSBコネクタを使います(写真参照). IDEの左上ペイン内,Project Explorerタブにある「Import SDK example(s)...」をクリック. インストールされているSDKが表示されるので「Next>」をクリック. サンプル・コードのリストが表示される. LEDチカチカ(=Lチカ)の例が「driver_examples」→「gpio」→「gpio_led_output」にあるので,下図のように階層をたどってチェックマークを入れ,「Finish」ボタンを押す. サンプル・コードがインポートされた. 青い虫のアイコン(Start debugging project)をクリック. ターゲットを選択するダイアログボックスが現れるので,表示された基板の情報を確認して「OK」ボタンを押す. コードがビルドされ,マイコンのフラッシュ・メモリに書き込まれます.そのあとコードが実行できる状態で一時停止. 黄色の四角とと緑の三角が組み合わさったアイコン(Resume)をクリックすると,基板上でコードが実行されます. このサンプル・コードはGPIO(General Purpose Input/Output = 汎用入出力)ピンにHIGHとLOWを交互に出すものでした.このピンが赤色のLEDに繋がれているので,LEDが点滅します. 参考資料 解説動画:さぁはじめよう!MCUXpresso IDE 関連情報:MCUXpresso for VSCとSDKのインストール (日本語ブログ) 変更履歴: 2025-05-07:初版 2025-06-26:「nxp.comへのログイン」の項を追加 2025-10-28:リンクの訂正 2025-11-10:リンクの更新 2025-11-14:インストール手順解説動画へのリンクを追加 / 参考資料の項を追加 2025-11-18:冒頭部の画像と使用基板の注釈追加.動画リンク画像変更 2026-03-17:「MCUXpresso IDEって?」の項の図を訂正 2026-04-05:「MCUXpresso IDEの起動とワークスペース」の項を追加 2026-07-24:章番号と目次を追加.「0. この記事は?」内,動画紹介リンクの強調  ========================= 本投稿の「Comment」欄にコメントをいただいても、現在返信に対応しておりません。 お手数をおかけしますが、お問い合わせの際には「NXPへの技術質問 - 問い合わせ方法 (日本語ブログ)」をご参照ください。 (既に弊社NXP代理店、もしくはNXPとお付き合いのある方は、直接担当者へご質問いただいてもかまいません。) NXPのマイコン:MCXシリーズのソフトウェア開発にはMCUXpresso IDEが無料で使えます. またさまざまなMCUXpresso IDEで使えるサンプル・コードが提供されています.ここではIDEとSDKのインストールの手順を解説します. これを読めば,誰でも簡単に開発環境&SDKをインストールできて,サンプル・コードまで動かすことができます! General Purpose Microcontrollers MCUXpresso MCUXpresso IDE MCX 日本語ブログ
記事全体を表示
由 nxp_mbdToolbox_s32K3 创建的版本无法通过 Freemaster 与 MCSPTE1AK344 通信 订购了全新的 mcspte1ak344,安装了所需的所有工具/软件(S32DS、RTD、SDK、Freemaster、Minwin)。 成功使用 nxp_mbdToolbox_s32K3\ S32K3_Examples\ mc\ 下的所有模型创建版本并通过 matlab2025a 下载到 MCSPTE1AK344 但是,当打开相应的 freemaster pmpx 文件时,无法与 MCSPTE1AK344 通信、 始终显示错误消息 " 在任何通信端口 UART " 上均未检测到主板。 检查完窗口/设备管理器后,OpenSDA-CDC 串行端口 (http://www.pemicro.com/opensda)(COM10) 检测到,其驱动程序显示为 windows 能找到的最佳驱动程序。 并安装了另一个名为 Jungo 的驱动程序,包括 PEMicro OpenSDA 调试驱动程序和 pemicrowindrvr。 到目前为止,只有从 mcb_open_loop 创建的版本才能让 freemaster 以 115200 bps 的速度找到板,所有使用其他 MBD 模型从示例中构建的版本都无法让 FreeMaster 找到板。 请大家帮忙 Re: Build created by NXP_MBDToolbox_S32K3 fail to communicate with MCSPTE1AK344 via Freemaster 你好@mchuang、 正如我们之前讨论的那样,其中一个问题是由运输引起的,由于运输过程中的振动,GD3000 板与 S32K344-T172 板接触不当。 为了解决这个问题,我们始终建议将 GD3000 板正确插入 S32K344-T172 板的顶部,按压接头并确保其插入良好。 如果连接不良,则 S32K344 可能无法通过 SPI 与 GD3000 芯片通信;如果一切正常,则板载 RGBLED 将亮起,并根据启动/停止/故障情况显示不同的颜色。 MCSPTE1AK344 开发套件入门中有相关信息 | NXP 半导体 顺祝商祺! Stefan V.
記事全体を表示
使用 usbdm 对 68HC912B32 编程 我正在尝试对一块装有这种芯片的旧板进行编程,但是对这个微控制器系列来说是全新的,所以不胜感激。 我下载并安装了 USBDM_4_12_1_340_Win.msi Windows 软件,并运行了"USBDM Memory Dump" 应用程序,转储了 68HC912B32 芯片上的闪存(地址范围 0x8000-0xFFFF)。 我还查看了"HCS12 Programmer" 或"Flash programmer" 应用程序,但其下拉菜单列表中没有 MC912B32 芯片。我还用 " Detect Chip " 按钮尝试了 " 设备选择 " 但它无法检测到我的芯片。 我不需要完整的开发环境/集成开发环境,只需要能够转储闪存、更换损坏的微控制器并用转储的程序对新微控制器进行编程。 这个 4 岁的https://community.nxp.com/t5/OSBDM-and-TBDML/program-the-HC12-B-Family-of-MCU/td-p/1324102这个问题很有趣,但并没有提供解决方案。 我的首选操作系统是 Linux 而不是 Windows,因此我非常乐意尝试基于 Linux 的解决方案。 对如何安装一个有效的编程环境有什么想法吗? 非常感谢 汤姆-克兰 Re: Programming a 68HC912B32 with usbdm 嗨,@pgo、 感谢您的跟进。我取得了一些进展。 Code Warrior 5.2 不支持 68HC912B32 的解决方案是安装 Code Warrior 5.1。这里建议https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-Development-Studio-for-HCS12-X-Microcontrollers/m-p/603056。 在 5.1 版中(见所附屏幕截图 Code-warrior2-run-as-administrator-MC68HC912B32+USBDM.jpg),MC68HC912B32 芯片已出现并可以选择。 但是,"连接 "下拉菜单中没有列出 USBDM 或 TBDML 选项。 在重新安装 Code Warrior 5.1 后,我重新安装了 USBDM 及其驱动程序,并将 USBDM 插入电脑。 为了检查 USBDM 未出现在 "代码勇士连接 "菜单中是否是因为 USBDM 不支持 68HC912B32,我尝试选择了 USBDM 支持的其他芯片。 我选择了 MC9S12A128B。 现在 “连接” 菜单增加了 3 个条目:" TBDML ", " HCS 串行监测 " & " USBDM "。请参阅所附屏幕截图 Code-warrior2-MC68HC9S12A128B+USBDM.jpg。 除了尝试修改 USBDM Tcl 代码以支持 68HC912B32 外,是否还有任何其他软件/硬件应用程序或其他选项可与 USBDM pod 一起使用以对该芯片进行编程? 如果没有,是否有其他支持 S/W 的硬件/软件选项可以让我对 68HC912B32 的闪存进行编程? 我的板只有用于调试/编程的 6 针 BDM 插槽 —— 所以必须假设制造商最初就是这样编程的,除非它是在焊接之前断路完成的,这似乎不太可能... 谢谢! 汤姆 Re: Programming a 68HC912B32 with usbdm 嗨,汤姆 很抱歉,我已经无法访问 Codewarrior(或 Windows!),因此无法亲自检查。 当我在恩智浦网站(https://www.nxp.com/products/68HC912B32)上搜索 68HC912B32 时,最终会找到您下载的 Codewarrior 版本,因此这似乎是正确的版本。 我不知道为什么 B32 没有出现。 对不起! Re: Programming a 68HC912B32 with usbdm 嗨,Pgo、 感谢您的跟进。 我已经部分拆解了之前转储的图像,所以应该可以拼凑出一个 .asm文件放入代码勇士项目中。 我找不到 Codewarrior 第 6 版的下载地址,但还是从https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-development-studio-for-hcs12x-microcontrollers-classic-ide-v5-2:CW-HCS12X下载了。 链接。 它被列为版本 5.2,重要的是,在 " 支持的设备 " 的 " Expand All " 复选框下列出了 68HC912B32。 安装 + 运行应用程序并检查版本号,显示的是 5.9 而不是 5.2。请参见所附截屏图片。 正在调用 " 启动对话框..." 和 " 创建新项目 " 提供了一个可选择芯片系列的弹出窗口。请参阅所附的截屏图片。 它只列出了 HCS12 & HCS12X 系列。 将这些节目扩展到家庭成员。请参阅所附的截屏图片。不出所料,其中没有 HCS912B32。 是我做错了什么,还是漏掉了什么显而易见的东西? 非常感谢 汤姆-克兰 Re: Programming a 68HC912B32 with usbdm 嗨,汤姆 很抱歉,USBDM 编程器不太可能适用于对您的芯片进行编程。 正如其他主题所指出的,这需要开发 TCL 脚本来完成基本工作(芯片启动、大量擦除等),并开发目标代码来完成块编程。 这是一项艰巨的工作,而且不能保证这种方法一定有效,因为 USBDM 采用的方法可能与早期的芯片不兼容。 可以使用位于 https://github.com/podonoghue/usbdm-eclipse-makefiles-build 的代表为 Linux 版本 USBDM。 我认为最好的办法是检查 Codewarrior V6(我认为)是否支持该芯片的 TBDML(USBDM 与之兼容)。 我不确定这是否允许独立编程,而不是从源代码进行调试开发。 仅适用于窗口。 再见
記事全体を表示
使用EB配置FS23驱动时报错 您好,我在配置FS2303驱动时,EB出现如图一的错误提示。但是我在图二的地方已经添加了相关通知函数。同时图三提示的错误也不知道怎样产生的。我使用的是 Autosar4.4   版本2.0的S32K3 mcal驱动和Autosar4.7 版本1.0的FS23 MCAL驱动。我想请问一下上述问题是两个版本不兼容导致的问题吗? Re: 使用EB配置FS23驱动时报错 好的,谢谢您的回复 Re: 使用EB配置FS23驱动时报错 嗨@夏超 从release note里面来看,你所使用的版本确实是不兼容的。 FS23 SBC AUTOSAR R21-11 版本 1.0.0 FS23 SBC Autosar 4.4 版本 0.8.0
記事全体を表示
RW612 FlexSPI PORTB1 アクセス RW612 チップセットを外部 XIP モードで使用しています。コードは FlexSPI PortA1 から実行され、PSRAM (APS6404L) を FlexSPI PortB1 に接続しています。SDKs (25.06 バージョン) が提供する構成を使用してポート B1 にアクセスしています。 PSRAM ID を読み取ろうとすると、PortB1 (CLCK/CS) で信号アクティビティが表示されません。 これらの信号が欠陥のある部品によって保持されていないことを確認するために、SPARM を取り外しました。 これは、APS6404 が DQS 信号を使用しないという事実に関係していますか? DQS を使用しないように PortB1 を構成するにはどうすればよいでしょうか? FlexSPI が PortA1 アクセス用に初期化された後は、FLEXSPI_Init 関数を呼び出すことができないことがわかっています。 ご協力とお時間をありがとうございました。 Re: RW612 FlexSPI PORTB1 access こんにちは、ローマン。 ご協力ありがとうございます。この問題は、バスの実行中に FlexSPI クロックを設定しようとしたことに関連していました。次の行をコメント アウトしました。 CLOCK_EnableClock( kCLOCK_Flexspi ); BOARD_SetFlexspiClock(FLEXSPI、5U、3U); FlexSPI ポート B1 は現在実行されており、AHB キャッシュを使用して PSRAM への書き込み/読み取りをCAN。 助けてくれてありがとう、本当に感謝してるよ。 Re: RW612 FlexSPI PORTB1 access こんにちは@khalidL 。 下の画像のように、MCU 設定で PSRAM メモリ セクションを定義しましたか? プロジェクトのアプリケーション コード ハブ投稿に記載されている手順を必ず実行し、問題が解決しない場合はお知らせください。 Re: RW612 FlexSPI PORTB1 access こんにちは、ローマン。 ご協力とご協力に感謝いたします。上記の例をプロジェクトに統合する過程で、次の問題が発生しました。メインから関数「 __RAMFUNC(SRAM) status_t BOARD_InitPsRam(void) 」を呼び出すと、コードがサイレントにクラッシュします。 リンカーファイル(main_data.ldt、main_txt.ldt および noinit_noload_section.ldt)board.cをコピーするファイル?BOARD_InitPsRam が RAM に正しくコピーされなかったためにコードがクラッシュしたのではないかと思います。 お時間を割いてご協力いただき、改めて感謝申し上げます。 Re: RW612 FlexSPI PORTB1 access この例は私のボードでは動作します。ご協力ありがとうございます。 Re: RW612 FlexSPI PORTB1 access こんにちは@khalidL 、お元気ですか。 アプリケーション コード ハブには、外部 NOR フラッシュからの XIPに関する例があります。共有されたリンクからサンプルをテストして、プロジェクト要件に適合するかどうかをお知らせください。 プロジェクトを MCUXpresso IDE にインポートするには、「アプリケーション コード ハブからインポート」オプションをクリックします。(このサンプルには SDK バージョン 2.16.00 が必要です) アプリケーション コード ハブ ウィンドウに入ったら、サンプルの名前 (外部 NOR フラッシュからの XIP およびマルチポート FlexSPI モジュールを使用した外部 pSRAM の構成) を検索し、それを選択して「Github リンク」をクリックし、「次へ >」ボタンが使用できるようになるまで待ちます。 「次へ > 」ボタンをクリックしたら、手順に従って Git リポジトリからプロジェクトをインポートします。最後に、プロジェクトがワークスペースで使用できるようになると、セットアップでフラッシュしてテストできるようになります。 これが役に立つかどうか教えてください。
記事全体を表示