FXOS8700CQ is not generating Data ready interrupt on INT1 Hi, I am using Hexiwear development kit. I have configured FXOS8700CQ to generate Data ready interrupt on INT1 (PTC1). But the INT1 interrupt never triggered. FXOS8700CQ configuration is mentioned below. Please let me know, am i missing some thing? fxos_status_t FXOS_Init( handleFXOS_t* fxosHandle, const settingsFXOS_t* fxosSettings ) { /** * initialize intern structures, * which will be used from now on */ uint8_t chip_ID = 0x00; uint8_t tmp[1] = {0}; memcpy( (void*)&self, (void*)fxosHandle, sizeof(self) ); memcpy( (void*)&settings, (void*)fxosSettings, sizeof(settings) ); statusI2C_t status = I2C_Init( &(self.protocol), settings.address, settings.baudRate_kbps ); if ( STATUS_I2C_SUCCESS != status ) { return status; } else { statusI2C_t devStatus = STATUS_I2C_SUCCESS; devStatus |= I2C_ReadReg( &(self.protocol), WHO_AM_I_REG, &chip_ID); if(kFXOS_WHO_AM_I_Device_ID == chip_ID) { /** go to standby */ devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp); devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, tmp[0] & (uint8_t)~ACTIVE_MASK); devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp); if ((tmp[0] & ACTIVE_MASK) == ACTIVE_MASK) { catch( CATCH_I2C ); } devStatus |= I2C_WriteReg(&(self.protocol), F_SETUP_REG, F_MODE_DISABLED); // Disable the FIFO devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG2, MOD_HIGH_RES); // /* enable auto-sleep, low power in sleep, high res in wake */ devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG1, (M_RST_MASK | M_OSR_MASK | M_HMS_MASK)); devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG2, (M_HYB_AUTOINC_MASK)); devStatus |= I2C_WriteReg(&(self.protocol), XYZ_DATA_CFG_REG, FULL_SCALE_4G); // +/-4g range with 0.244mg/LSB devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG4, 0x01); // Enable DRDY interrupt devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG5, INT_CFG_DRDY_MASK); devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG3, WAKE_FF_MT_MASK); devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, HYB_ASLP_RATE_0_8HZ | HYB_DATA_RATE_100HZ | ACTIVE_MASK); devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp); if ((tmp[0] & ACTIVE_MASK) != ACTIVE_MASK) { catch( CATCH_I2C ); } if ( STATUS_I2C_SUCCESS != devStatus ) { catch( CATCH_I2C ); } } return devStatus; } } //Interrupt configuration /** create basic tasks */ status |= HostInterface_Init(); SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK; // Turn on clock to Port C module PORTC_PCR1 |= (0|PORT_PCR_ISF_MASK | PORT_PCR_MUX(0x1) | PORT_PCR_IRQC(0xA)); // PC1 is configured for falling edge interrupts //Enable PORTC interrupt on NVIC NVIC_SetPriority( PORTC_IRQn, HEXIWEAR_TAP_IRQ_PRIO); Thanks, J. Chandra Sekhar Re: FXOS8700CQ is not generating Data ready interrupt on INT1 Hello Chandra,
I do recommend performing the reset just writing 0x40 to the CTRL_REG2 register.
Could you please make sure the INT1 pin is connected to your MCU/MPU input pin? Is your input pin configured for falling edge interrupts?
Regards,
David Re: FXOS8700CQ is not generating Data ready interrupt on INT1 Hi, To perform Soft reset, i have used below code. But this command resulting the STATUS_I2C_ERROR. fxos_status_t FXOS_SoftReset() { statusI2C_t i2cStatus = I2C_WriteReg( &(self.protocol), FXOS_CTRL_REG2, RST_MASK ); if ( STATUS_I2C_SUCCESS != i2cStatus ) { return STATUS_FXOS_PROTOCOL_ERROR; } else { return STATUS_FXOS_SUCCESS; } } Thanks, J. Chandra Sekhar Re: FXOS8700CQ is not generating Data ready interrupt on INT1 Hello Chandra,
Thank you for using the community.
Your device configuration seems correct. I just want to recommend applying a reset to all registers before device the configuration.
Could you please make sure the INT1 pin is connected to your MCU/MPU input pin? Is your input pin configured for falling edge interrupts?
Regards,
David Re: FXOS8700CQ is not generating Data ready interrupt on INT1 Hi, Thanks for your response. I have checked the code and configured similarly in my Hexiwear board. But still the same, FXOS8700CQ sensor is not generating interrupt. const gpio_input_pin_user_config_t Acc_cfg[] = { { .pinName = ACC_INT1, .config.isPullEnable = false, .config.pullSelect = kPortPullDown, .config.isPassiveFilterEnabled = false, .config.isDigitalFilterEnabled = false, .config.interrupt = kPortIntDisabled }, { .pinName = ACC_INT2, .config.isPullEnable = false, .config.pullSelect = kPortPullDown, .config.isPassiveFilterEnabled = false, .config.isDigitalFilterEnabled = false, .config.interrupt = kPortIntDisabled }, { .pinName = GPIO_PINS_OUT_OF_RANGE, } }; //Configured Pin 1 of PORTC as input GPIO_DRV_Init( Acc_cfg, NULL ); //Sensor configuration devStatus |= I2C_ReadReg( &(self.protocol), WHO_AM_I_REG, &chip_ID); if(kFXOS_WHO_AM_I_Device_ID == chip_ID) { /** go to standby */ FXOS_GotoStandby(); devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp); devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, tmp[0] & (uint8_t)~ACTIVE_MASK); devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp); if ((tmp[0] & ACTIVE_MASK) == ACTIVE_MASK) { catch( CATCH_I2C ); } devStatus |= I2C_WriteReg(&(self.protocol), XYZ_DATA_CFG_REG, FULL_SCALE_2G); // +/-2g range with 0.244mg/LSB devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG1, (0x1F)); // Hybrid mode (accelerometer + magnetometer), max OSR devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG2, 0x20); // M_OUT_X_MSB register 0x33 follows the OUT_Z_LSB register 0x06 (used for burst read) devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG2, 0x02); // High Resolution mode devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG3, 0x00); // Push-pull, active low devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG4, 0x01); // Enable DRDY interrupt devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG5, 0x01); // DRDY interrupt routed to INT1 - PTC1 devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, 0x35); // ODR = 3.125Hz, Reduced noise, Active mode FXOS_SetActive(); if ( STATUS_I2C_SUCCESS != devStatus ) { catch( CATCH_I2C ); } } //Interrupt handler void PORTC_IRQHandler(void) { PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR); /** Write your code here ... */ /* Unblock the task by releasing the semaphore. */ portBASE_TYPE taskToWake = pdFALSE; if (pdTRUE==xSemaphoreGiveFromISR(xReadRawDataSemaphore, &taskToWake)) { FXOS8700CQ_DataReady = 1; if (pdTRUE == taskToWake) { vPortYieldFromISR(); } } } //Task to read data from sensor void ReadRawData(task_param_t param) { xReadRawDataSemaphore = xSemaphoreCreateBinary(); if( xReadRawDataSemaphore == NULL ) { configASSERT(0); } for(;;) { /*Block waiting for the semaphore to become available. */ if( xSemaphoreTake( xReadRawDataSemaphore, LONG_TIME ) == pdTRUE ) { if(FXOS8700CQ_DataReady) { FXOS8700CQ_DataReady = 0; FXOS_ReadRawData(&AccelMagData[0]); } vPortYieldFromISR(); } } } Trying this from few days, but no luck. Request your support. Thanks, J. Chandra Sekhar Re: FXOS8700CQ is not generating Data ready interrupt on INT1 Hello Chandra,
I hope all is great with you. Thank you for using the NXP communities.
In this case, I highly recommend using the following bare metal project as a reference for your design:
FXOS8700CQ - Bare metal example project
I hope this information helps.
Regards,
David
View full article