RDBESSK358BMU CAN4 normal mode issue Hi NXP team, I am working with the RDBESSK358BMU board and trying to bring up CAN using FlexCAN4 with the onboard CAN-FD transceiver. At the end of post you can see my code. I also selected the pins in S32 Design Studio based on my understanding of the board documentation and schematic, but it still does not work. My current understanding is: PTC30 → CAN4_TX PTC31 → CAN4_RX PTA7 → CAN_STB PTD8 → CAN-FD_EN PTD9 → CAN-FD_ERR In S32DS pin configuration, I selected them as follows according to my interpretation: PTC30 / CAN4_TX PTC31 / CAN4_RX PTD8 as GPIO Output PTA7 as GPIO Output PTD9 as GPIO Input However, the setup is still not working. I want to use normal mode only with the real external transceiver and real CAN bus. I do not want loopback mode. Also, when I try to run in normal mode, the board seems to reset. 1- Do you have a complete working example for: RDBESSK358BMU FlexCAN4 normal mode external CAN transceiver enabled correct pin settings correct S32DS configuration 2- If possible, could you please provide: a full working example project or a minimal but complete initialization example including: clock init pin mux CAN transceiver control pins FlexCAN4 init start mode transmit example in normal mode My current code is as bellow also, the pin setting in S32DS is attached. Thank you. Saman **************************************************************** #include "Mcal.h" #include "OsIf.h" #include "FlexCAN_Ip.h" #include "FlexCAN_Ip_Cfg.h" #include "Clock_Ip.h" #include "Clock_Ip_Cfg.h" #include "Siul2_Port_Ip.h" #include "Siul2_Port_Ip_Cfg.h" volatile int exit_code = 0; int main(void) { Flexcan_Ip_DataInfoType txInfo; uint8 txData[8] = {1U, 2U, 3U, 4U, 5U, 6U, 7U, 8U}; /* Clock init */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* Pin init */ Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0); /* OSIF init */ OsIf_Init(NULL_PTR); /* CAN4 init */ FlexCAN_Ip_Init(4U, &FlexCAN_State0, &FlexCAN_Config0); /* Start CAN controller */ FlexCAN_Ip_SetStartMode(4U); /* CAN frame info */ txInfo.msg_id_type = FLEXCAN_MSG_ID_STD; txInfo.data_length = 8U; txInfo.fd_enable = FALSE; txInfo.fd_padding = 0U; txInfo.enable_brs = FALSE; txInfo.is_polling = TRUE; txInfo.is_remote = FALSE; for (;;) { (void)FlexCAN_Ip_SendBlocking(4U, 0U, &txInfo, 0x123U, txData, 1000U); for (volatile uint32 i = 0U; i < 1000000U; i++) { } } return exit_code; } Re: RDBESSK358BMU CAN4 normal mode issue Hello @samansaki,
You can select the "Switch package" option inside the Pins tool, and select the 172HDQFP package:
Best regards, Julián Re: RDBESSK358BMU CAN4 normal mode issue Hi Julián, I currently have a problem in the debug stage of my code. The reset issue I mentioned is related to switching to normal mode, which I will ask about later as a separate issue. For now, I would like to solve the debug problem first. I want to debug my code step by step, set breakpoints, and check the registers. Specifically, I want to verify registers such as: SIUL2 GPDO / GPDI MSCR / IMCR configuration FlexCAN registers From the BMU board documentation (S32K358, 172-MQFP), I expect: PTD8 -> pin 64 -> CAN_EN PTD9 -> pin 63 -> CAN_ERR PTA7 -> pin 100 -> CAN_STB PTC30 -> pin 101 -> CAN4_TX PTC31 -> pin 103 -> CAN4_RX However, I noticed that when I select the S32K358 family in S32DS, the tool automatically assigns a default part number (S32K358 in 289-BGA), while my board uses the 172-MQFP package. Because of this, the pin mapping is different, and I cannot reliably check the registers during debugging. I searched in S32DS but could not find where to manually change the part number/package. I have attached a screenshot showing this issue. Best regards, Saman Re: RDBESSK358BMU CAN4 normal mode issue Hi @samansaki,
Your general configuration seems to be correct. How are you testing the CAN communication? Are you using something like the PCAN USB analyzer?
You can look through our community for some existing examples regarding RDBESSK358BMU or S32K358 in general, for example:
[RD-K358BMU]How to get example alike CAN and compile
CAN receive problem: RDK358BMU board
How to enable VCU CAN on RD-K358BMU
Now, regarding this sentence: "Also, when I try to run in normal mode, the board seems to reset." Could you clarify what this means? At which point in the application does the board reset?
Best regards, Julián Re: RDBESSK358BMU CAN4 normal mode issue Hi @samansaki,
Could you share how are you testing CAN communication? Are you using a PCAN USB analyzer? Are you able to scope the bus?
Unfortunately, I do not have the board with me right now, but I can share some S32K3X8 EVB CAN example if needed. Just help me sharing S32DS + RTD versions.
Anyway, RDBESSK358BMU board uses the TJA1463ATK CAN interface, which is operated by two control pins, STB_N and EN. For NORMAL mode, set HIGH levels on both STB_N and EN.
You can do this by writing 1 to the pin:
Siul2_Dio_Ip_WritePin(STB_N_PORT, STB_N_PIN, 1U);
Siul2_Dio_Ip_WritePin(EN_PORT, EN_PIN, 1U);
Other than that, basic configuration looks OK.
You could also check that the bit timing matches both nodes on the bus (Whatever you are using to test, eg. another board, PCAN USB, etc.)
Best regards, Julián Re: RDBESSK358BMU CAN4 normal mode issue Hi Julian Thank you for your nice answer. Regarding my main problem, I checked the examples you provided, and now I’m trying to send a very simple CAN message using FlexCAN on S32K358, but I’m stuck and not sure where the issue is. I have been debugging this for quite some time, but I still cannot figure out what’s wrong. My goal is simply to periodically send a basic CAN frame (8 bytes) using one TX message buffer. Please take a look at my code below, as well as the attached screenshots from S32DS (registers, pin configuration, etc.): #include "Mcal.h" #include "Clock_Ip.h" #include "Siul2_Port_Ip_Cfg.h" #include "Siul2_Port_Ip.h" #include "FlexCAN_Ip.h" #define TX_MB_IDX 0U #define MSG_ID 0x123U uint8 txData[8] = {1,2,3,4,5,6,7,8}; uint32 canStatus; Flexcan_Ip_DataInfoType tx_info = { .msg_id_type = FLEXCAN_MSG_ID_STD, .data_length = 8u, .fd_enable = FALSE, .fd_padding = FALSE, .enable_brs = FALSE, .is_polling = TRUE, .is_remote = FALSE }; int main(void) { Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0); FlexCAN_Ip_Init(INST_FLEXCAN_4, &FlexCAN_State0, &FlexCAN_Config0); FlexCAN_Ip_SetStartMode(INST_FLEXCAN_4); while (1) { canStatus = (uint32)FlexCAN_Ip_Send(INST_FLEXCAN_4, TX_MB_IDX, &tx_info, MSG_ID, txData); txData[0]++; for (volatile uint32 i = 0; i < 1000000U; i++) { } } }
記事全体を表示