I am using MiMxRT1020 development kit.. I want to update firmware via TCP with bootloader. As soon as I receive my new firmware I want to reset application and I want to jump to the bootloader mode. But NVIC_SystemReset() is not working. So I can not update my firmware. Here is sample of my code.
if(ack_offset == 0xffff) {
/* received complete firmware */
osDelay(2000);
__disable_irq();
/* reset application */
NVIC_SystemReset();
}
@Sabina_Bruce that is not a proper test!
If you look at the NVIC_Reset inline function, you will see that the attempt at reset is followed by an infinite loop:
for(;;) {}So you have not proved the reset works. You need to test an application that has actual reset capability and without debug pod attached.
@meeras - Have you resolved this issue?
I'm also seeing an apparent reset failure on RT1024.
Also FYI see this similar issue and patch for M55 etc. ARM cores:
https://github.com/ARM-software/CMSIS_6/issues/195
I'm going to try applying ARM's CMSIS patch.
Interested to hear what you've found!
Thanks,
Best Regards, Dave
Hello ,
Hope you are doing well.
I have tested this one my end without any issue.
I used the simple hello world example. Placed the NVIC_SystemReset after it prints hello world.
It will not reach the next printf as it resets the application.
I am using the latest IDE and SDK version.
Best Regards,
Sabina
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------