Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
SPI Communication Issue with TC6 SPI Protocol Hello, I am implementing SPI communication between the S32K144 MCU and MAC-PHY (LAN8650). For Control Transaction Write/Read (where the master writes/reads a register value to/from the slave), the process follows the TC6 SPI protocol as shown in the image below: Before stepping forward to actual register read/write to MAC-PHY, I thought of testing it with some dummy data and verify it by probing in at MOSI of S32K144 and SDI of MAC-PHY(LAN8650) chip. With that I could successfully send 16 bit and 32 bit data, but whereas no data transactions happening for 64 bit transfer.  As per above picture inorder to read/ write the slave register it should be 64 bits(Control header + Data) or higher. The working code 32 bits dummy data transfer is as follows :  #include "S32K144.h" /* include peripheral declarations S32K144 */ uint32_t tx_32bits = 0xFD00FD00; //uint32_t tx_32bits_array[2] = {0xFD00, 0X1010}; uint32_t LPSPI0_32bits_read; /* Returned data in to SPI */ void LPSPI0_init_master(void) { PCC->PCCn[PCC_LPSPI0_INDEX] = 0; /* Disable clocks to modify PCS ( default) */ PCC->PCCn[PCC_LPSPI0_INDEX] = 0xC6000000; /* Enable PCS=SPLL_DIV2 (40 MHz func'l clock) */ LPSPI0->CR = 0x00000000; /* Disable module for configuration */ LPSPI0->IER = 0x00000000; /* Interrupts not used */ LPSPI0->DER = 0x00000000; /* DMA not used */ LPSPI0->CFGR0 = 0x00000000; /* Defaults: */ /* RDM0=0: rec'd data to FIFO as normal */ /* CIRFIFO=0; Circular FIFO is disabled */ /* HRSEL, HRPOL, HREN=0: Host request disabled */ LPSPI0->CFGR1 = 0x00000001; /* Configurations: master mode*/ /* PCSCFG=0: PCS[3:2] are enabled */ /* OUTCFG=0: Output data retains last value when CS negated */ /* PINCFG=0: SIN is input, SOUT is output */ /* MATCFG=0: Match disabled */ /* PCSPOL=0: PCS is active low */ /* NOSTALL=0: Stall if Tx FIFO empty or Rx FIFO full */ /* AUTOPCS=0: does not apply for master mode */ /* SAMPLE=0: input data sampled on SCK edge */ /* MASTER=1: Master mode */ LPSPI0->TCR = 0x1100001F; /* Transmit cmd: PCS1, 32 bits, prescale func'l clk by 4, etc*/ /* CPOL=0: SCK inactive state is low */ /* CPHA=0: On the rising edge of SCLK the data is captured, while on the falling edge of SCLK the data will change /* PRESCALE=2: Functional clock divided by 2**2 = 4 */ /* PCS=1: Transfer using PCS1 */ /* LSBF=0: Data is transfered MSB first */ /* BYSW=0: Byte swap disabled */ /* CONT, CONTC=0: Continuous transfer disabled */ /* RXMSK=0: Normal transfer: rx data stored in rx FIFO */ /* TXMSK=0: Normal transfer: data loaded from tx FIFO */ /* WIDTH=0: Single bit transfer */ /* FRAMESZ=31: # bits in frame = 31+1=32 */ LPSPI0->CCR = 0x04090808; /* Clock dividers based on prescaled func'l clk of 100 nsec */ /* SCKPCS=4: SCK to PCS delay = 4+1 = 5 (500 nsec) */ /* PCSSCK=4: PCS to SCK delay = 9+1 = 10 (1 usec) */ /* DBT=8: Delay between Transfers = 8+2 = 10 (1 usec) */ /* SCKDIV=8: SCK divider =8+2 = 10 (1 usec: 1 MHz baud rate) */ LPSPI0->FCR = 0x00000003; /* RXWATER=0: Rx flags set when Rx FIFO >0 */ /* TXWATER=3: Tx flags set when Tx FIFO <= 3 */ LPSPI0->CR = 0x00000009; /* Enable module for operation */ /* DBGEN=1: module enabled in debug mode */ /* DOZEN=0: module enabled in Doze mode */ /* RST=0: Master logic not reset */ /* MEN=1: Module is enabled */ } void LPSPI0_tx_32bits (uint32_t send) { while((LPSPI0->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0); /* Wait for Tx FIFO available */ LPSPI0->TDR = send; /* Transmit data */ LPSPI0->SR |= LPSPI_SR_TDF_MASK; /* Clear TDF flag */ } uint32_t LPSPI0_rx_32bits (void) { uint32_t recieve = 0; while((LPSPI0->SR & LPSPI_SR_RDF_MASK)>>LPSPI_SR_RDF_SHIFT==0); /* Wait at least one RxFIFO entry */ recieve= LPSPI0->RDR; /* Read received data */ LPSPI0->SR |= LPSPI_SR_RDF_MASK; /* Clear RDF flag */ return recieve; /* Return received data */ } void PORT_init (void) {   //Master:   PCC->PCCn[PCC_PORTB_INDEX] |= PCC_PCCn_CGC_MASK;   PORTB->PCR[2] |= PORT_PCR_MUX(3); /*Port B2: MUX = ALT3, SCK*/   PORTB->PCR[3] |= PORT_PCR_MUX(3); /*Port B3: MUX = ALT3, SIN*/   PORTB->PCR[4] |= PORT_PCR_MUX(3); /*Port B4: MUX = ALT3, SOUT*/   PORTB->PCR[5] |= PORT_PCR_MUX(3); } int main(void) { uint32_t counter = 0; volatile int i; WDOG_disable(); SOSC_init_8MHz(); /* Initialize system oscillator for 8 MHz xtal */ SPLL_init_160MHz(); /* Initialize SPLL to 160 MHz with 8 MHz SOSC */ NormalRUNmode_80MHz(); /* Init clocks: 80 MHz sysclk & core, 40 MHz bus, 20 MHz flash */ LPSPI0_init_master(); PORT_init(); for (;;) { LPSPI0_tx_32bits(tx_32bits); LPSPI0_32bits_read = LPSPI0_rx_32bits(); } return 0; } Note : For 64 bit data transfer, I changed TCR[FRAMESZ]=3F and changed respective data types and values. My questions are: 1. Is S32K144 doesnt support whole 64 bit transfer in one go? [In S32K1xx Series Reference Manual, Rev. 14 at start of page 1623 it means as the maximum frame size is 32 bits?] 2. If it supports only 32 bits, then kindly help me the way that on how to transfer >=64 bits of data. 3. Else if it supports 64 bits, then kindly point me out the changes i have to perform in the above code. Thanks in advance! Re: SPI Communication Issue with TC6 SPI Protocol Hello @Muthappan_Viswanthan  I'm really glad to hear that I was able to help for a change, since I'm usually the one receiving help.   If you have any further questions, feel free to leave a reply 🙂 Re: SPI Communication Issue with TC6 SPI Protocol Thanks for your reply. Rightnow, Iam using older version of S32 DS and doing baremetal programming. But thought of switching to newer version and using RTD, this might helpful for me in that case. Thanks again! Re: SPI Communication Issue with TC6 SPI Protocol Hi, Finally its working and the issue is with header as you stated. Actually, I read like we should set the parity bit to "1'" if we have odd number of 1's between bit 31:1 and thus in my case I didnt set it. After your comment I just deep dive into it and got to know that my understanding is wrong. Thanks for lightning up.! Re: SPI Communication Issue with TC6 SPI Protocol Hello,   I'm responding to your post as I have experience implementing the TC6 protocol using the LAN8651 MAC-PHY chip from Microchip on the S32K314 MCU.   In my case, I used RTD 4.0.0 with S32 Design Studio 3.5, and configured the LPSPI driver as follows.   Based on this LPSPI driver, you should be able to configure a uint8_t tx and rx buffer with 12 elements and perform SPI communication accordingly. ex) uint8_t spiRxBuffer[12], uint8_t spiTxBuffer[12] Re: SPI Communication Issue with TC6 SPI Protocol Hi, a delay in SCK should not be an issue. Check if there are right number of clock periods in words. To say more capture full frame in scope/analyzer. I guess you have wrong parity bit calculated. You wrote "The header seems to be correct, example I used "0x30000c00" for IMASK0." But this time parity bit should be set to have odd number of "1" in header. BR, Petr Re: SPI Communication Issue with TC6 SPI Protocol Thanks for your help so far.  I made the changes to transfer as 3x 32bit words for both read & write. As per the statement from LAN8650 datasheet "When performing control writes, the register data sent over SDI is also echoed back over SDO", I am not getting echoed data as same as what I transmitted during write and read operations. The modified code is as below: void lan8650_write_imask0(uint32_t value) { uint32_   t header = build_ctrl_header(1, 0x00, 0x000C, 0); uint32_t read_tx_header2 = 0; uint32_t read_tx_data2 = 0; CS_LOW(); LPSPI0_tx_32bits(header); // Write header (void)LPSPI0_rx_32bits(); //Read dummy bytes LPSPI0_tx_32bits(value); // Write data read_tx_header2 = LPSPI0_rx_32bits(); // Read Header Echo LPSPI0_tx_32bits(0x00000000); // Write dummy data read_tx_data2 = LPSPI0_rx_32bits(); // Read data Echo CS_HIGH(); } uint32_t lan8650_read_imask0(void) { uint32_t header = build_ctrl_header(0, 0x00, 0x000C, 0); uint32_t rx_header = 0; uint32_t rx_data = 0; CS_LOW(); LPSPI0_tx_32bits(header); // Send header (void)LPSPI0_rx_32bits(); // Dummy data LPSPI0_tx_32bits(0x00000000); // Dummy to clock header rx_header = LPSPI0_rx_32bits(); // Read Header Echo LPSPI0_tx_32bits(0x00000000); // Dummy to clock data rx_data = LPSPI0_rx_32bits(); // Read data CS_HIGH(); return rx_data; } And I measured the SPI lines of LAN8650 with scope and the observations are:  1. CS is LOW for the entire duration of 3x 32bits transfer. 2. SCK not seems to be continuous. After each 32bits transfer SCK is in LOW for some time and then starting back. [Refer below picture channel 2 (green) waveform ] 3. SDI line has the same 32bit header, 32 bit data and 32 bit dummy data which I sent from S32K144 MOSI. 4. SDO echoes "0xC000 0000" during header transmission (Ignored data),  "0xC000 0001" during both data & dummy data transmission which expected to be header & data as per datasheet.   The header seems to be correct, example I used "0x30000c00" for IMASK0. So, whether that delay in SCK between each 32 bits makes an issue? Re: SPI Communication Issue with TC6 SPI Protocol Hi, code looks normal, but I think a protocol looks little bit different. There should be 3 words transferred for single register writing/reading For both read and write, the Control Header sent to the LAN8650/1 over SDI is always echoed back to the SPI host over SDO. When performing control writes, the register data sent over SDI is also echoed back over SDO. Thus for write you send header, data, dummy words, For read you send header, dummy, dummy words. So try that, measure SPI lines with scope /analyzer to know real frames. Also check header is correct. BR, Petr Re: SPI Communication Issue with TC6 SPI Protocol Hello, I used 2 a) [ set FRAMESZ to 31 for 32bit frame size and control CS manually and fill data registers as per desired number of word transfer.] with some dummy data and it worked. Now, when I tried with my actual task where I need to communicate with LAN8650 chip, I should write/read by sending control header first where the respective address should be present: For this purpose I used the below code :  #include "S32K144.h" /* include peripheral declarations S32K144 */ #define CS_LOW()    (PTB->PCOR = (1 << 5))  // Clear bit to pull CS low #define CS_HIGH()   (PTB->PSOR = (1 << 5))  // Set bit to pull CS high       //System registers (MMS = 0) const TC6Reg TC6ADR_RESET      = { .mms = 0x00, .addr = 0x003 }; const TC6Reg TC6ADR_CONFIG0    = {.mms = 0x00, 0x0004}; const TC6Reg TC6ADR_STATUS0    = {.mms = 0x00, 0x0008}; const TC6Reg TC6ADR_IMASK0     = {.mms = 0x00, 0x000C}; const TC6Reg TC6ADR_PLCACTL0   = {.mms = 0x04, 0xCA01}; const TC6Reg TC6ADR_PLCACTL1   = {.mms = 0x04, 0xCA02}; const TC6Reg TC6ADR_PLCASTAT   = {.mms = 0x04, 0xCA03}; const TC6Reg TC6ADR_MAC_NCR    = {.mms = 0x01, 0x0000}; const TC6Reg TC6ADR_MAC_NCFGR  = {.mms = 0x01, 0x0001};   uint32_t tx_16bits = 0xFD00FD00; uint32_t tx_32bits_array[2] = {0xFD00, 0X1010}; uint32_t LPSPI0_16bits_read; /* Returned data in to SPI */ uint16_t lan8650_phy_id = 0; uint32_t tx_upper = 0xFD00FD00; uint32_t tx_lower = 0x1010ABCD; uint32_t rx_upper, rx_lower;   // Calculates odd parity for a 32-bit word (excluding bit 0) uint8_t calculate_parity(uint32_t word31to1) {    uint8_t count = 0;    int i;    for (i = 1; i < 32; i++) {        if ((word31to1 >> i) & 0x01) count++;    }    return (count % 2 == 0) ? 0 : 1;  // Return 0 if even (to make odd) }   uint32_t build_ctrl_header(uint8_t wnr, uint8_t mms, uint16_t addr, uint8_t num_regs) {    uint32_t header = 0;    header |= (0U << 31);                 // DNC = 0 (Control)    header |= (0U << 30);                 // HDRB = 0 (Ignored on write)    header |= ((wnr & 0x01) << 29);       // WNR: 1 = write, 0 = read    header |= (0U << 28);                 // AID = 0 (auto-increment)    header |= ((mms & 0x0F) << 24);       // MMS = memory map select    header |= ((addr & 0xFFFF) << 8);     // Register address    header |= ((num_regs & 0x7F) << 1);   // Length (in registers), shifted to [7:1]    uint8_t parity = calculate_parity(header & 0xFFFFFFFE); // Clear bit 0 for parity calc    header |= parity; // Set bit 1 to make parity odd    return header; }     void LPSPI0_init_master(void) { PCC->PCCn[PCC_LPSPI0_INDEX] = 0; /* Disable clocks to modify PCS ( default) */ PCC->PCCn[PCC_LPSPI0_INDEX] = 0xC6000000; /* Enable PCS=SPLL_DIV2 (40 MHz func'l clock) */   LPSPI0->CR = 0x00000000; /* Disable module for configuration */ LPSPI0->IER = 0x00000000; /* Interrupts not used */ LPSPI0->DER = 0x00000000; /* DMA not used */ LPSPI0->CFGR0 = 0x00000000; /* Defaults: */ /* RDM0=0: rec'd data to FIFO as normal */ /* CIRFIFO=0; Circular FIFO is disabled */ /* HRSEL, HRPOL, HREN=0: Host request disabled */ LPSPI0->CFGR1 = 0x00000001; /* Configurations: master mode*/ /* PCSCFG=0: PCS[3:2] are enabled */ /* OUTCFG=0: Output data retains last value when CS negated */ /* PINCFG=0: SIN is input, SOUT is output */ /* MATCFG=0: Match disabled */ /* PCSPOL=0: PCS is active low */ /* NOSTALL=0: Stall if Tx FIFO empty or Rx FIFO full */ /* AUTOPCS=0: does not apply for master mode */ /* SAMPLE=0: input data sampled on SCK edge */ /* MASTER=1: Master mode */ LPSPI0->TCR = 0x1100001F; /* Transmit cmd: PCS3, 16 bits, prescale func'l clk by 4, etc*/ /* CPOL=0: SCK inactive state is low */ /* CPHA=0: On the rising edge of SCLK the data is captured, while on the falling edge of SCLK the data will change /* PRESCALE=2: Functional clock divided by 2**2 = 4 */ /* PCS=3: Transfer using PCS3 */ /* LSBF=0: Data is transfered MSB first */ /* BYSW=0: Byte swap disabled */ /* CONT, CONTC=0: Continuous transfer disabled */ /* RXMSK=0: Normal transfer: rx data stored in rx FIFO */ /* TXMSK=0: Normal transfer: data loaded from tx FIFO */ /* WIDTH=0: Single bit transfer */ /* FRAMESZ=31: # bits in frame = 31+1=32 */ LPSPI0->CCR = 0x04090808; /* Clock dividers based on prescaled func'l clk of 100 nsec */ /* SCKPCS=4: SCK to PCS delay = 4+1 = 5 (500 nsec) */ /* PCSSCK=4: PCS to SCK delay = 9+1 = 10 (1 usec) */ /* DBT=8: Delay between Transfers = 8+2 = 10 (1 usec) */ /* SCKDIV=8: SCK divider =8+2 = 10 (1 usec: 1 MHz baud rate) */ LPSPI0->FCR = 0x00000003; /* RXWATER=0: Rx flags set when Rx FIFO >0 */ /* TXWATER=3: Tx flags set when Tx FIFO <= 3 */ LPSPI0->CR = 0x00000009; /* Enable module for operation */ /* DBGEN=1: module enabled in debug mode */ /* DOZEN=0: module enabled in Doze mode */ /* RST=0: Master logic not reset */ /* MEN=1: Module is enabled */     }     void LPSPI0_tx_32bits (uint32_t send) { while((LPSPI0->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0); /* Wait for Tx FIFO available */ LPSPI0->TDR = send; /* Transmit data */ LPSPI0->SR |= LPSPI_SR_TDF_MASK; /* Clear TDF flag */ }       uint32_t LPSPI0_rx_32bits (void) { uint32_t recieve = 0;   while((LPSPI0->SR & LPSPI_SR_RDF_MASK)>>LPSPI_SR_RDF_SHIFT==0); /* Wait at least one RxFIFO entry */ recieve= LPSPI0->RDR; /* Read received data */ LPSPI0->SR |= LPSPI_SR_RDF_MASK; /* Clear RDF flag */ return recieve; /* Return received data */ }   void SOSC_init_8MHz(void) {  SCG->SOSCDIV=0x00000101; /* SOSCDIV1 & SOSCDIV2 =1: divide by 1 */  SCG->SOSCCFG=0x00000024; /* Range=2: Medium freq (SOSC between 1MHz-8MHz)*/  /* HGO=0: Config xtal osc for low power */ /* EREFS=1: Input is external XTAL */  while(SCG->SOSCCSR & SCG_SOSCCSR_LK_MASK); /* Ensure SOSCCSR unlocked */  SCG->SOSCCSR=0x00000001; /* LK=0: SOSCCSR can be written */  /* SOSCCMRE=0: OSC CLK monitor IRQ if enabled */ /* SOSCCM=0: OSC CLK monitor disabled */ /* SOSCERCLKEN=0: Sys OSC 3V ERCLK output clk disabled */ /* SOSCLPEN=0: Sys OSC disabled in VLP modes */ /* SOSCSTEN=0: Sys OSC disabled in Stop modes */ /* SOSCEN=1: Enable oscillator */  while(!(SCG->SOSCCSR & SCG_SOSCCSR_SOSCVLD_MASK)); /* Wait for sys OSC clk valid */ } void SPLL_init_160MHz(void) {  while(SCG->SPLLCSR & SCG_SPLLCSR_LK_MASK); /* Ensure SPLLCSR unlocked */  SCG->SPLLCSR = 0x00000000; /* SPLLEN=0: SPLL is disabled (default) */  SCG->SPLLDIV = 0x00000302; /* SPLLDIV1 divide by 2; SPLLDIV2 divide by 4 */  SCG->SPLLCFG = 0x00180000; /* PREDIV=0: Divide SOSC_CLK by 0+1=1 */  /* MULT=24: Multiply sys pll by 4+24=40 */ /* SPLL_CLK = 8MHz / 1 * 40 / 2 = 160 MHz */  while(SCG->SPLLCSR & SCG_SPLLCSR_LK_MASK); /* Ensure SPLLCSR unlocked */  SCG->SPLLCSR = 0x00000001; /* LK=0: SPLLCSR can be written */  /* SPLLCMRE=0: SPLL CLK monitor IRQ if enabled */ /* SPLLCM=0: SPLL CLK monitor disabled */ /* SPLLSTEN=0: SPLL disabled in Stop modes */ /* SPLLEN=1: Enable SPLL */  while(!(SCG->SPLLCSR & SCG_SPLLCSR_SPLLVLD_MASK)); /* Wait for SPLL valid */ } void NormalRUNmode_80MHz (void) { /* Change to normal RUN mode with 8MHz SOSC, 80 MHz PLL*/  SCG->RCCR=SCG_RCCR_SCS(6) /* PLL as clock source*/  |SCG_RCCR_DIVCORE(0b01) /* DIVCORE=1, div. by 2: Core clock = 160/2 MHz = 80 MHz*/  |SCG_RCCR_DIVBUS(0b01) /* DIVBUS=1, div. by 2: bus clock = 40 MHz*/  |SCG_RCCR_DIVSLOW(0b10); /* DIVSLOW=2, div. by 3: SCG slow, flash clock= 26 2/3 MHz*/  while (((SCG->CSR & SCG_CSR_SCS_MASK) >> SCG_CSR_SCS_SHIFT ) != 6) {}  /* Wait for sys clk src=SPLL */ }  /* TXWATER=3: Tx flags set when Tx FIFO <= 3 */     void WDOG_disable (void){  WDOG->CNT=0xD928C520; /*Unlock watchdog*/  WDOG->TOVAL=0x0000FFFF; /*Maximum timeout value*/  WDOG->CS = 0x00002100; /*Disable watchdog*/ } void PORT_init (void) { //Master: PCC->PCCn[PCC_PORTB_INDEX] |= PCC_PCCn_CGC_MASK; PORTB->PCR[2] |= PORT_PCR_MUX(3); /*Port B2: MUX = ALT3, SCK*/ PORTB->PCR[3] |= PORT_PCR_MUX(3); /*Port B3: MUX = ALT3, SIN*/ PORTB->PCR[4] |= PORT_PCR_MUX(3); /*Port B4: MUX = ALT3, SOUT*/ //PORTB->PCR[5] |= PORT_PCR_MUX(3); PORTB->PCR[5] |= PORT_PCR_MUX(1); PTB->PDDR |= (1<<5); PTB->PSOR |= (1<<5);     }   void lan8650_write_reset(void) {    uint32_t header = build_ctrl_header(1, 0x00, 0x0003, 0); // Write to RESET reg    CS_LOW();    LPSPI0_tx_32bits(header); (void)LPSPI0_rx_32bits();     // Write header    LPSPI0_tx_32bits(0x00000001); (void)LPSPI0_rx_32bits(); // Write data    CS_HIGH(); } void lan8650_write_imask0(uint32_t value) {    uint32_t header = build_ctrl_header(1, 0x00, 0x000C, 0);    CS_LOW();    LPSPI0_tx_32bits(header); (void)LPSPI0_rx_32bits();    LPSPI0_tx_32bits(value);  (void)LPSPI0_rx_32bits();    CS_HIGH(); } uint32_t lan8650_read_imask0(void) {    uint32_t header = build_ctrl_header(0, 0x00, 0x000C, 0);    uint32_t data = 0;    CS_LOW();    LPSPI0_tx_32bits(header); (void)LPSPI0_rx_32bits(); // Send header    LPSPI0_tx_32bits(0x00000000);                       // Dummy to clock data    data = LPSPI0_rx_32bits();                          // Get data    CS_HIGH();    return data; }     int main(void) {       uint32_t imask_read_value;     volatile int i;       // Usual system and SPI setup       WDOG_disable();       SOSC_init_8MHz();       SPLL_init_160MHz();       NormalRUNmode_80MHz();       PORT_init();           // Configure SPI pins       LPSPI0_init_master();  // Init LPSPI master       // Small delay before starting (optional)       for ( i = 0; i < 100000; i++); // Optional delay           // Write RESET           lan8650_write_reset();           // Optional delay to allow reset to complete           for ( i = 0; i < 100000; i++);           // Unmask all interrupts           lan8650_write_imask0(0x00000000);           // Read IMASK0 to verify           imask_read_value = lan8650_read_imask0();           // Set breakpoint here to inspect imask_read_value           while (1) { }       return 0;   } Here, I am trying to Write 0x00000000 to IMASK0 register address and trying to readback the same address in order to ensure the value has been written properly. But I got value has 0xC0000001 instead of 0xC0000000. (IMASK0 has 31 to 16 bits as reserved and Read-Only bits thus 0xC000 can be fixed even i try to write it as 0, thus we can neglect that) But the lower 16 bits are R/W and thus it should be 0.   For debugging purpose, in the above code I set breakpoint in the last while loop and it successfully hits (above picture) thus seems like write and read happening proper (not 100% sure, my assumption) but the value read is wrong.  I tried all possibilities and still couldn't find where it went wrong. Kindly guide me to solve this issue.  Thanks in advance.     Re: SPI Communication Issue with TC6 SPI Protocol Hi, yes, lpspi allows sending/receiving frame that has size larger that 32 bits. There could be several ways to do that. 1. set FRAMESZ to be multiple of 32, as per your need, how many words have to be transferred (up to 128) 2. set FRAMESZ to 31 for 32bit frame size and a) control CS manually and fill data registers as per desired number of word transfer. You can refer to below code  https://community.nxp.com/t5/S32K/S32K146-LPSPI-with-ADXL314/m-p/1826209/highlight/true#M32845 b) use continuous selection, refer to https://community.nxp.com/t5/S32K/Continuous-Transfer-LPSPI-S32K14x/td-p/1830165 For sure above codes need to be modified for 32bit transfer. Hope it helps. BR, Petr
記事全体を表示
FRDM-MCXN947 RTC Hello, I'm working on my data logger with FRDM-MCXN947, and I'm going to use the RTC module available on the board to record the time. I would like to ask, is it necessary to connect an external battery (and if so how), in case the main power supply is not connected via usb-c? Board Design Development Board MCXN Power Re: FRDM-MCXN947 RTC Hi, Thank you so much for your interest in our products and for using our community. Yes, you need an external battery to maintain the count of the time record. You need to connect the battery on VDD_BAT according to the Table 1. Power domain operating requirements section from UG10092 MCXNx4x Hardware Design Guide. Additional documentation: 2.1.1 Power supply configuration section from UM12018 FRDM-MCXN947 Board User Manual. Hope it helps you. Have a nice day!
記事全体を表示
调试器的“堆使用情况(FreeRTOS)”选项卡如何工作? 查看 MCUXpresso 屏幕截图,我有一个 125 kB 的 FreeRTOS 堆。标签的图形显示一切正常,但是如果我把数字加起来,标签的列表似乎显示它已经全部用完了。我理解错了吗? 此外,当特定内存块没有像其他内存块一样指定给 FreeRTOS 任务时,“已分配”是什么意思? 回复:调试器的堆使用情况(FreeRTOS)选项卡如何工作? 至于更新 IDE,我可能无法做到这一点,直到项目完成(很快)。 声明的分配解释是有意义的。谢谢您的回复。 回复:调试器的堆使用情况(FreeRTOS)选项卡如何工作? 如果堆仅配置为 125 kB(configTOTAL_HEAP_SIZE),FreeRTOS 动态内存分配器如何提供超过 135 kB 的内存? 重复我的第二个问题:当特定内存块没有像其他内存块一样指定给 FreeRTOS 任务时,“已分配”是什么意思?
記事全体を表示
RW612 SDK - mbedTLS gcm.c 针对未使用的静态数据发出警告 我正在为 RW612 构建一个应用程序。我已经合并了 mbedTLS 库,因为它出现在 AWS 影子示例中。但是,当我构建它时,gcm.c 会发出警告,指出两个函数 gcm_gen_table() 和 gcm_mult() 被定义成静态但未被使用。出现这种情况的原因是 NXP 添加了 MBEDTLS_AES_GCM_STARTS_ALT、MBEDTLS_AES_GCM_UPDATE_ALT 等来定义标准 mbedTLS GCM 函数的替代函数,但并没有排除标准函数使用的静态函数。 我附上了 gcm.c 的原始版本,以及不会对未使用的静态变量发出警告的修复版本。请检查并将这些修改纳入您的下一个版本中,谢谢。 达娜·M.
記事全体を表示
带有 PCA9451 的 I.MX93 的 PMIC_ON_REQ 控制 尊敬的恩智浦社区: 我们想询问 I.MX93 的PMIC_ON_REQ信号的控制机制,因为我们正在使用PCA9451 PMIC和I.MX9322CVX 。以下是我们的具体问题: 上电期间 当我们提供NVCC_BBSM_1P8电压时, PMIC_ON_REQ信号自动变高。该信号连接到 PMIC 以启动上电序列。这个理解正确吗? 掉电期间 我们可以使用软件将PMIC_ON_REQ信号拉低以允许PMIC进入关机过程吗? 如果可以,那么如何实现呢? 我们可以在哪里找到相关流程或文档? 电池电量检测 我们的电池旨在检测 I.MX93 的运行状态。当I.MX93断电时,电池会自动关闭电源。 是否有推荐的引脚来监控此状态(来自 I.MX93 或 PCA9451)? 3.1如果电池还没有断电,但是PMIC已经完成断电过程,此时NVCC_BBSM_1P8仍然由电池供电。PMIC_ON_REQ信号会自动再次拉高吗? 感谢您的支持和澄清。 顺祝商祺!
記事全体を表示
如何使用多种语言来检测唤醒词和检测词??? 我知道当我检测启动词和命令时它目前以一种语言检测,但我如何检测两种语言? 例如,我想检测英文的“Hi, NXP”和韩文的“Hi, NXP”。
記事全体を表示
PCF8523T 在一段时间后对 I2C 无响应 我们遇到一个问题,PCF8523T 上的 I2C 接口在一段时间后变得无响应(命令后无 ACK)。 为了加速,我们以~800kbps(~10 倍客户速度)的速度运行该设备超过 4 小时,每秒 10 笔交易,并进入这种状态,因此重现它并非易事。 我们知道 PCF8523T 无法处理双启动条件,从数据表中可以看出: “对于此设备,不允许重复启动。因此,必须释放 STOP 在下一次“开始”之前。”我们不会这样做,虽然已经验证过,但可能会出现故障。 我们相信,当这种情况发生时,VCC 和 VBAT 电源都是稳定的。 此设备上是否存在任何已知问题,即 I2C 将停止响应,这与 VBAT/VCC 切换无关? 通过电源循环,VCC 和 VBAT I2C 都可以再次工作,但是有没有什么方法,比如通过多个 SCL 周期重置内部状态机? 回复:PCF8523T 在一段时间后对 I2C 无响应 作为信息,“意外”写入登记册确实是个问题。 作为额外信息,它看起来像<~0.5V,需要同时在 VBAT 和 VDD 上施加电压,才能使上电复位功能起作用,将寄存器设置重置为默认值 回复:PCF8523T 在一段时间后对 I2C 无响应 这似乎是一个软件错误,确切的根本原因正在调查中。 DMA 用于 I2C 数据传输,并且不知何故(有时)跳过了 DMA 传输(和 I2C 数据)开头的一个字节,因此“Control_3”获得了“秒”的值,因此在 32 到 59 之间写入任何秒数都会将 RTC 转换为“直接切换模式”,并且由于 VBAT>VCC,这意味着 I2C 通信丢失。 如果写入的秒数在 0 到 31 之间时发生数据丢失,则是安全的。 我们会保持这个话题开放,直到我们确定这是问题所在,但我们会在几天内确定。 确实很奇怪的错误,但还是感谢您的输入! 回复:PCF8523T 在一段时间后对 I2C 无响应 我们已经更接近问题的核心了。 参考 RTC.PNG 文件中先前发布的原理图。 齐纳二极管 D404(DDZ9690)是 5.6v 齐纳二极管。 D405 在超低电流下的正向电压为~0.2V。 随着时间的推移,VBAT 电压在许多情况下将接近 5.4V,高于 VCC(5V) 我们将 Control_3 寄存器中的 PM[2:0] 设置为 0x0,这给出了 PCF8523T 的电源和电源模式之间切换的“标准模式”。 但有时我们似乎会无意中将 RTC 模式更改为“直接切换模式”,并且当 VBAT>VCC 时,I2C 通信停止工作。 知道什么原因会导致这种故障吗? 回复:PCF8523T 在一段时间后对 I2C 无响应 您好,您能否将地址从 0xD0 更改为 0xA2,并告诉我问题是否仍然存在? 回复:PCF8523T 在一段时间后对 I2C 无响应 附件是示意图。 C407 不是 NXP 推荐的(1µF 而不是 3.3µF),但当电压移除时,斜率远低于 0.7V/ms 在这种情况下,电压永远不会被消除。 RTC 周围的一些组件: ABS07-32.768KHZ-7-T7pF晶体 KW-5R5C334H-R超级电容器 BSS138 N-MOSFET 两条 I2C 线直接连接到 MPC5517EAVLU66 引脚 31:PH1/AN26/EMIOS21/SDA_A 引脚 32:PH0/AN27/EMIOS20/SCL_A 回复:PCF8523T 在一段时间后对 I2C 无响应 您能分享一下您的示意图吗? 回复:PCF8523T 在一段时间后对 I2C 无响应 感谢这份内容丰富的文件。 不幸的是,我们既没有保持低 SDA 信号,也没有保持 SCL 信号。当这种情况发生时,它们都很高。 我们已经尝试过“恢复总线的顺序是发送 9 个时钟脉冲加上 STOP 信号。”的建议 但这并没有帮助。 当查看通信时,它的行为就像 RTC 上的 I2C 完全没有响应。
記事全体を表示
如何在 S32K116 上配置多个 UART 外设? 大家好, 背景:S32 DS 3.4 软件和示例 S32K1xx SDK RTM v4.0.3 示例项目 --> lin_slave_s32k116 和 lpuart_echo_s32k116。 我想使用 2 个 UART 外设,LPUART1 用于 LIN 通信,LPUART0 与 arduino uno 协同工作。 在我的应用程序中,每当我从主机发送 lin 信号时,从机 s32k116 EVB 都应该响应并从 LPUART0 发送一些字符串值以便与 arduino 通信。我尝试合并 lin_slave 和 lpuart_echo 这两个示例,但没有成功。 任何建议或帮助都将不胜感激! 提前致谢!! 谢谢与问候, 桑托什   回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 是的,你是对的! 我改变了一些时钟配置,现在它可以按预期工作了。 谢谢与问候, 桑托什 回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 非常感谢您的快速回复! 你是对的,跳线 J15 引脚 2 与 gnd 短路。当我进一步按照 j15 的示意图操作时。我注意到 C143 电容器短路,需要更换。 谢谢与问候, 桑托什 回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 感谢您的回复! 是的,我用万用表测量了MCU的电源,除非我把跳线J15从原位拔掉,否则就不会有电源输入。拔掉跳线J15后,电压显示为5V,D1的红色LED也亮了。 之前一直都好好的,不知道现在怎么不行了。我连MCU开机都没发热。 您知道如何对电路板进行硬件重置吗?或者这是 MCU 的问题吗? 谢谢与问候, 桑托什 回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 非常感谢您的回复,我会尽快向您更新。 目前,我遇到了一些与主板硬件相关的问题。即使我将跳线 J107 置于 2-3 位置,MCU 也无法通电,但如果我将跳线 J15 从其位置 1-2 移除,它就会打开。您是否知道如何对主板进行硬件重置,或者您对这个问题还有其他建议吗? 问候, 桑托什 回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 有关于此问题的任何更新吗?或者您是否需要任何其他文件或信息来处理此问题? 如果您有任何需要,请告诉我,我很乐意提供。 我期待您的回复。 此致, 桑托什 回复:如何在S32K116上配置多个UART外围设备? 你好@danielmartynek , 感谢您的回复! 请查看附件中的 zip 文件,其中包含此消息下方项目所需的所有文件。 在我的应用程序中,我想在接收到一些 lin 信号时从不同的外设发送一些 UART 信号,而我在这个项目中遇到的问题是,我看不到任何 LED 对 lin 信号做出响应,也没有从另一个 UART 外设观察到任何消息,例如欢迎消息和逻辑分析仪上对 lin 信号的响应。 当我用不同的项目尝试相同的示例时,它按预期工作。我不确定是否可以在同一个代码中合并两个示例,或者我是否必须使用 freeRTOS 来实现这种方法? 如果我遗漏了什么,请告诉我吗? 我期待您的回复。 谢谢与问候, 桑托什
記事全体を表示
MCUXpressoでプロキシと証明書を設定して、アプリケーションコードハブからコードをダウンロードする方法は? 私の質問はタイトルと同じです。 私のPCにはプロキシと証明書があるため、MCUXpressoのApplication Code Hubからプロジェクトをインポートできません。この問題を解決するためにどのように設定できますか? 私はgithubからソースコードを引き出すことができるという考えを持っています https://github.com/nxp-appcodehub/dm-fashion-mnist-recognition-on-mcxn947 その後、このコードを添付の画像としてファイルからインポートします。それがうまくいくかどうかはわかりません。通常、アプリケーション ハブからのプロジェクトには、カメラなどの追加のデバイスが必要になるためです。その時点で確認する追加のデバイスはありません。 この状況についてアドバイスをお願いします。ありがとうございます。 Re:MCUXpressoでプロキシと証明書を設定して、アプリケーションコードハブからコードをダウンロードする方法は? もちろん、ありがとう。わかりました。
記事全体を表示
[i.MX 8 MP] 关于使用 ISP 和新传感器的问题 您好。 我正在查看一些移植指南并有几个问题。 使用带有新传感器的 ISP 是否需要相机校准文件(XML)? 用于生成 XML 文件的 ISP 校准工具是免费提供的吗? 我可以在不使用相机校准文件的情况下将 MIPI-CSI 流传递给 ISP 吗? 我不熟悉嵌入式 Linux(yocto)。 谢谢! 回复:[i.MX 8 MP] 关于使用 ISP 和新传感器的问题 你好。@roxanne41watts 谢谢你回答我的问题。 基本上,我明白如果我使用 ISP,我就需要 xml。 首先,我想尝试使用图像传感器接口(ISI)捕获 RAW 图像。 谢谢! 回复:[i.MX 8 MP] 关于使用 ISP 和新传感器的问题 您好!我很乐意解答您的问题。 相机校准文件(XML):是的,相机校准文件(XML)通常需要与新传感器一起使用 ISP(图像信号处理)。该文件包含重要的校准数据,确保 ISP 正确处理图像。 ISP 校准工具:一些 ISP 校准工具是免费提供的。例如,GitHub 上的 Infinite-ISP Tuning Tool 是一款免费的基于控制台的 ISP 调整应用程序。但是,可用性可能因您所使用的特定 ISP 和传感器而异。 MIPI-CSI 流到 ISP:通常不建议在不使用相机校准文件的情况下将 MIPI-CSI 流传递到 ISP,因为校准数据对于准确的图像处理至关重要。然而,某些设置可能允许绕过某些校准步骤,但这不是常见的做法,可能会导致不理想的结果。 嵌入式 Linux (Yocto):Yocto 是一个开源项目,它提供模板、工具和方法来帮助您为嵌入式产品创建基于 Linux 的定制系统。它有点技术性,但有大量资源和社区可以帮助您入门。
記事全体を表示
如何在 Linux 中使用帧缓冲区更新 epdc 显示? 我正在使用带有 epdc 显示子卡(IMXEBOOKDC5)的 IMX8ULP EVK。使用 Linux 映像启动后,epdc 显示器无法使用帧缓冲区进行更新。当检查显示器 pmic 的电源使能引脚时,它仍然保持低电平,即使我写入帧缓冲区(与使用 android 映像相比,每当我更新帧缓冲区 fb0 时,此引脚都会变高)。 此外,我比较了 android 和 linux 源代码中的帧缓冲区驱动程序 C 文件(drivers/video/fbdev/mxc/mxc_epdc_v2_fb.c)。我发现 android 中有一个函数(mxc_epdc_update_data)用于从用户空间更新数据。 回复:如何在 Linux 中使用帧缓冲区更新 epdc 显示? 嗨志明, 謝謝您的支持。 回复:如何在 Linux 中使用帧缓冲区更新 epdc 显示? 你好@Namitha_zcs Linux 驱动程序中的 fb 更新函数是mxc_epdc_fb_send_update并在mxc_epdc_fb_ioctl中定义,如果在用户空间使用MXCFB_SEND_UPDATE ,则会调用更新函数。 此致, 志明
記事全体を表示
使用断点进行调试而不停止所有中断 大家好, 我在没有操作系统的iMXRT-1064上开发了一个应用程序。该应用程序的各种功能包括 EtherCAT 主站,并通过定时器中断维持通信。 我想使用断点来暂停代码执行,以便检查变量值或验证逻辑流程。然而,当遇到断点时,所有中断和代码执行也会停止,导致 EtherCAT 连接断开。 有没有办法设置断点来暂停主执行但仍允许某些中断(例如处理 EtherCAT 通信的中断)继续运行? 感谢您的帮助! 回复:使用断点进行调试而不停止所有中断 你好@EdwinHz , 谢谢你的回答。最后一个问题:如果我开始采用 FreeRTOS 并启用多线程,是否可以使用调试器暂停一个线程,同时让其他线程继续运行? 谢谢!
記事全体を表示
LPC55C3xピン配置多重化 LPC55C3xは、複数のペリフェラルを必要とする新製品の潜在的なマイクロコントローラとして評価しているところです。各ピンのピン多重化/代替機能を評価して、これらのデバイスでペリフェラル リストが可能かどうかを確認する必要があります。過去のNXPのデータシートとリファレンスマニュアルには、各ピンと利用可能な代替機能を定義する表が含まれていました。LPC55C3x リファレンス マニュアルのセクション 6.2 (ピン配置) には、次のように記載されています。 「ピン配置については、添付の「LPC553xピン機能」スプレッドシートを参照してください。 そのようなスプレッドシートを見つけることができません。それがどこにあるかについてのリンクや場所を誰でも提供できますか? -リック 日時:LPC55C3xピン配列多重化 どういたしまして! 日時:LPC55C3xピン配列多重化 それは確かに役に立ちました!ありがとうございます。
記事全体を表示
i.MX93 M33 固件 ELE(EdgeLock Enclave)API 支持 - 缺少 S3MU 驱动程序 我正在开发一个需要在 M33 固件中独立使用 ELE(EdgeLock Enclave)网络安全功能的项目。经过 SDK 分析,我发现 缺少文件: drivers/fsl_s3mu.c/.h-S3MU 驱动程序实现驱动程序/fsl_ele_base_api.c-ELE 基本 API 板/evkmimx9352/driver_examples/s3mu/-S3MU 示例 i.MX93 架构是否支持通过 S3MU 进行 M33 到 ELE 的直接通信? 是否有替代方法或技术文档? Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 已在系统邮件中回复您。 此致 哈维 回复: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 像 i.MX93 这样的 SoC 只有一个 Cortex-M33 内核,启用 ELE 功能是否会与定制 MCU 固件开发相冲突?换句话说,启用 ELE 后,是否会锁定 M33,从而阻止上传定制的 MCU 固件? Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 谢谢您的答复。 我知道你们提供的补丁文件主要是针对 i.MX95 的 M7 内核,但我的问题主要是针对只有 M33 内核的 SoC,如 i.MX93。 是否可以在M33上开发我的自定义固件并在其上调用和使用与ELE相关的网络安全功能? 谢谢! Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 向您发送了带有演示的系统邮件,请在邮件中查看。 此致 哈维 Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 这个例子似乎是在解释 TrustZone 的用例,但我更感兴趣的是在 i.MX93 的 M33 内核上进行开发。我想在此固件上进行开发并使用与 ELE 相关的网络安全功能。这可行吗? 谢谢。 Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver 希望这些例子能有所帮助。 此致 哈维
記事全体を表示
MCXN-947 的 FlexPWM 输入捕获示例 有没有可用于 FlexPWM 输入捕获的示例? 时钟|计时器 FRDM 培训 MCX N Re: flexPWM INPUT CAPTURE EXAMPLE FOR MCXN-947 你好@embedabu 感谢您的提问。 没有基于 FlexPWM 的捕获演示。但是,SDK 下有一个 CTimer 捕获演示可供参考。 请注意使用SDK v25.06。 谢谢! BR 爱丽丝
記事全体を表示
se050 initial configuration Hi, I am trying to communicate with the EdgeLock se050 chip. I am using the NXP “Plug & Trust Middleware Mini Package” and I have been able to compile and execute the example they provide. I can read the version of the chip, but when I try to read an object I get an error and the example cant continue, in ht ex_sss_entry before preparing for the digest sign. My assumption is that the I2C communication is correct, but maybe the authentication is not, and that’s why I cant access to se050 objects. I would like to ask you if you do some first configuration to this chip, which authentication method do you use and if there are any credentials that we can use. Kind regards, Iván Re: se050 initial configuration It seems the hardware connection does not enabled. Maybe you should check the I2C connection and enable GPIO. You can refer to the EdgeLock SE05x Quick start guide with Raspberry Pi for help. What kind of Hardware platform you are using? Re: se050 initial configuration Hi @ivangonzalezcano , Thanks for the info! I just replied your private ticket on the same topic, but if you prefer to discussing it here, it is also fine with me. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: se050 initial configuration Hi @Kan_Li,  I am using a SE050F variant. Thank you. Re: se050 initial configuration Hi @ivangonzalezcano , What is the SE050 variant you are using to play with the mini MW? Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
由于缺少许可证,无法安装 APU 编译器 你好,AP 软件专家、 福特客户正在安装用于 QNX 的 S32V234 VSDK 1.5.5,但他们无法安装 APU Compiler v1.0 b657,因此他们询问如何才能获得许可证。 此致 于 优先级:中等 Re: Could not install APU Compiler due to missing license @jiri_kral、 明白了,感谢您的帮助,我将关闭该票! 于 Re: Could not install APU Compiler due to missing license 您好, 兰迪的激活密钥是5B4B-73EC-F2E2-81B0 Re: Could not install APU Compiler due to missing license @jiri_kral 谢谢您的帮助!我的 APU 编译器许可证现在运行良好,但 Randy([email protected])看不到他的驾照。他如何访问 APU 编译器的下载链接? 于 Re: Could not install APU Compiler due to missing license 你好、 这两个许可证的有效期均已延长。 Re: Could not install APU Compiler due to missing license @jiri_kral、 您是否愿意为"[email protected]"颁发许可证? 并将我的"[email protected]"? 于 Re: Could not install APU Compiler due to missing license @jiri_kral 我已将用户名通过电子邮件发送给您。谢谢您的帮助! 于 Re: Could not install APU Compiler due to missing license 你好、 客户的 NXP ID 是什么?通常是电子邮件地址。
記事全体を表示
MIPI-CSI-2 とベイヤーパターンカメラ (RAW10) を使用した i.MX93 こんにちは、 カスタムの i.MX93 ベースのボードを持っています。提供されている CSI-2 インターフェースを使用して、ベイヤーパターン カメラ (IMX327) で RAW10 データを転送したいと考えています。 デバイスツリーの設定とプレスリリース、製品ニュース-ctlの設定はSO far正しいのですが、パイプラインを開始するとdwc-mipi-csi2からIRQストームが発生し、「 IPIインターフェース致命的イベント情報」カウンタが増加します。INT_ST_IPI_FATALレジスタの値は0x2aで、IPI FIFOオーバーフローを示しています。IPIがIRQを1つも持っていないため、ISIにデータをプッシュしていないのではないかと考えています。 https://community.nxp.com/t5/i-MX-Processors/About-settings-to-operate-ov5640camera-on-i-MX93EVK/mp/1716885/highlight/true#M212016を参照何らかの特別な設定があるようです。これらの値をRAW10に適合させようとしましたが、CAMERA_MUX[DATA_TYPE]の値0x31(ユーザー定義16)について疑問がありました。CSI-2 データ型 RAW10 の場合、これが 0x2b ではなくユーザー定義であるのはなぜですか? IPI エラーの原因は何でしょうか?この問題をさらにデバッグするにはどうすればよいでしょうか? 感謝と敬意を表します。 アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) アップデートはありますか?Omnivision 9732でも同じ問題が発生しています Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは@brian14さん、 i.MX93 と RAW10/12 Bayer データを出力するカメラ センサでも同じ問題が発生しています。 何かアイデアや提案はありますか? よろしくお願いします。 Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは、 連絡あった?もう1ヶ月が経ちました。 ありがとう、アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは、 このトピックに関して何かニュースはありますか? ありがとう、そしてよろしく。 アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは@steinaさん、 NXP サポートにお問い合わせいただきありがとうございます。 このCASEについては社内チームで検討し、できるだけ早くお問い合わせいたします。 すてきな一日を!
記事全体を表示
S32DS for ARM 2018R1 ライセンス こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1のライセンスの有効期限が切れました。 延長していただけますか? アクティベーションコード00B2-2243-F93D-50F1 よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: 0255-52A3-B9BE-AB0C よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM V2.2 のライセンスが 13 日後に期限切れになります。確認して延長を手伝っていただけますか? Arm用S32 Design Studio アクティベーションID: 97B6-8CB8-3FC0-851A 評価日数: 13 機能バージョン: 2.2 機能のステータス: 評価 (13 日間) ありがとうございます。 Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license はい、うん Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ARM V2.2 ライセンスの有効期限が切れました。 ライセンスを延長していただけますか? アクティベーションID: DD5C-6F03-8AE4-7ECA SOありがとう。 Re: S32DS for ARM 2018R1 license S32 プラットフォーム 3.4 の S32DS のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます。アクティベーションコード C5A1-5B94-2A38-9034 Re: S32DS for ARM 2018R1 license こんにちは: おはようございます!S32dsのライセンスが期限切れです。ライセンスの延長をお願いできますか?ソフトウェアバージョンは2.2です。 本当にありがとうございます!あなたの助けが必要です! Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード:349D-19F8-FFD7-7F10 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード592C-8B75-D563-0CAE Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license S32DS for ARM 2018R1 のライセンスの有効期限が切れました。延長をお願いしたいです。どうもありがとうございます。 コード9DD9-3E3B-4AA1-1DE3 S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DE17-8B75-A725-CBC3 Re: S32DS for ARM 2018R1 license S32DS for Power Win32 v2017 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか?「このライセンスを返却することはできません」というヒントです。返品しようとすると、「 よろしくお願いします。 Re: S32DS for ARM 2018R1 license S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?アクティベーションコード D429-1EC2-B799-7507 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは: S32 Design Studio for Power Architecture ® v2.1 - Windows/Linuxのライセンス IDE の有効期限が切れました。確認と延長を手伝っていただけますか? アクティベーションコード DDD9-023A-976E-CD88 ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認と延長を手伝っていただけますか?アクティベーションコード DDD9-023A-976E-CD88 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license こんにちは、S32 Design Studio for ARM v2.2 ライセンスの有効期限はすでに切れています。延長してもらえますか? ありがとうございます! アクティベーションコード: 2D6B-DC21-07CF-F125 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは: 私の免許証 S32DS for Arm v2.2 IDE の有効期限がもうすぐ切れます。確認して延長していただけませんか? ありがとうございます。 アクティベーションコード: BC11-7022-0D21-E460 回复: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 4777-90EB-DAF6-AE57 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018 R1 のライセンスが期限切れです。延長してもらえますか? アクティベーションコード: 6EC6-15B7-7227-97F6 ありがとうございます。 カルロ 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM V1.3 のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license 問題は解決しました。ありがとうございます Re: S32DS for ARM 2018R1 license S32DS ライセンスの拡張を手伝ってください。アクティベーションコード: FF84-9C7B-EFCB-6595。ありがとうございます! Re: S32DS for ARM 2018R1 license こんにちは、 あなたのアカウントを確認しましたが、すべてのライセンスは有効でアクティブ化されています。S32DS PA では異なるアクティベーション キーを使用しましたが、問題はありません。 Re: S32DS for ARM 2018R1 license ソフトウェアフィードバック:(ライセンスがありません) Re: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限がすでに切れていますが、延長することはできますか? ありがとうございます! アクティベーションコード: 77FC-3B94-A7DC-54EE Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: FF84-9C7B-EFCB-6595 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。ARM 2018R1 用に S32DS を再インストールしました。 オフラインでアクティベートすると、activation.xml に「ライセンスを生成CANません。すでに期限が切れています」と表示されます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスが期限切れになりました。延長していただけますか? アクティベーションコード: FC1A-4C29-3203-9C08 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v3.5 のライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8A8B-9E9B-F34E-2603 回复: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Arm v2.2 ライセンスはすでに期限切れです。延長してもらえますか? ありがとうございます! アクティベーションコード: D0BA-0474-25E0-F056 S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます!アクティベーションコード: 3EF3-981A-CE8D-45C3 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 3EF3-981A-CE8D-45C3 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: C617-86A4-65B7-F3D9 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 0384-6363-91F6-CB8E Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8238-B154-F160-0911 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 516A-3379-0522-6A9D どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 0D34-286B-9EE6-E692 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: DE63-F9AF-C189-5399 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 ========================================== 商品の説明S32 Design Studio 注文番号S32DS_2018_R1_100931407 注文番号 ライセンスの総数:100 アクティベーションコード C625-7579-0C28-63DC 製品に適用されるライセンス: バージョンの説明 R1 2018 S32 Design Studio (EULA を表示) 3.1 S32 Design Studio (EULA を表示) 100個入手可能       Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM v2.2 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード F1B3-2017-8F0D-17BE よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @acirillo さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32S 2018のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @linxwhut さん、 両方のライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @Detective さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: C819-045E-F1F8-61B7 Re: S32DS for ARM 2018R1 license こんにちは。私と同僚の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限が切れてしまいました。ライセンスの延長を手伝っていただけますか?ありがとう アクティベーションコード:82DF-FC84-F43A-1EF0 アクティベーションコード:5EBA-DE62-DCF0-02A9 Re: S32DS for ARM 2018R1 license こんにちは、ホーガンさん。 有効期限を2027年まで延長しました。現在のコードで再度アクティブ化してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとうございます Re: S32DS for ARM 2018R1 license よろしくお願いします。 Re: S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとう 。 Re: S32DS for ARM 2018R1 license こんにちは、 @J_Garyさん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: E971-3802-1E3D-5BA6 Re: S32DS for ARM 2018R1 license こんにちは、 @liamtsenさん、 あなたのライセンスを2028年12月末まで延長しました。 使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちはサラさん ライセンスが延長されました。アクティベーション コードをもう一度試してください。 よろしくお願いします、 マイク 回复: S32DS for ARM 2018R1 license こんにちは、 @Hanshengさん あなたのライセンスを2027年末まで延長しました。使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1 ライセンスの有効期限がすでに切れています。延長にご協力いただけませんか? ありがとうございます! アクティベーションコード: B7B1-173F-51BA-13A2 よろしくお願いいたします。 サラ Re: S32DS for ARM 2018R1 license こんにちは、 @1772137309 。 あなたのライセンスを2028年末まで延長しました。 S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: B0A4-688C-2AD6-79EE Re: S32DS for ARM 2018R1 license こんにちは、 @ScreenUserさん、 ライセンスの有効期限を 2027 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 6C82-9208-D1F2-C38F Re: S32DS for ARM 2018R1 license こんにちは、 ライセンスの有効期限を 2026 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは: S32DS_Power_Win32_v2.1 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 Re: S32DS for ARM 2018R1 license どうもありがとうございます。今はすべて正常に動作しています。改めて感謝申し上げます。 Re: S32DS for ARM 2018R1 license こんにちは、ハオさん あなたの免許を3年間延長しました。S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは、 @Jaydenyzhu 私はこの権利を2026年まで延長しました。 新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 - メフル・パテル S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコードD5D0-D801-AB24-58DF よろしくお願いします。 Re: S32DS for ARM 2018R1 license My S32 Design Studio for Arm 2018_R1 の有効期限が 4 日後に切れますが、延長してもらえますか?ありがとう; アクティベーションID: 799E-5E79-910F-6C57 Re: S32DS for ARM 2018R1 license こんにちは、Gen Liさん あなたの免許を3年間延長しました。 現在のアクティベーション コードを使用して再度アクティベーションしてください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license おはよう、 S32 Design Studio for Power Architecture バージョン 2.1 IDE のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード DBA1-317C-5265-7E4F よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、Mehul_Patelさん S32DS が動作するようになりました。ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん あなたのライセンスを2026年12月末まで延長しました。 アクティベーションを更新してください。 ありがとう。敬具。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 アクティベーションコードはD876-C313-75B1-2E1B です。ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 @cjgyf さん、 あなたの権利を2025年12月末まで延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん ライセンスを再アクティブ化できるように、 S32DS for Arm v2018のアクティベーション コードを共有していただけますか。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license 私のライセンスも期限切れ(9DE8-C6AE-8B6B-952B)なのですが、延長していただけますか?よろしくお願いいたします! Re: S32DS for ARM 2018R1 license こんにちは、NXPの専門家の皆さん。 S32DS for Arm v2018 のライセンスの有効期限が切れ、ライセンスが返却されましたが、現在ライセンスが欠落していることが示されています。ライセンスの延長にご協力ください。どうぞよろしくお願いいたします。 デビッド Re: S32DS for ARM 2018R1 license こんにちは、マイク 遅れてごめんなさい。どうもありがとうございます。今はすべて正常に動作しています。 敬具 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。同じコードで再度アクティベートしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 09D2-DE37-6529-87FB よろしくお願いします。 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 この権限のサーバー ログを確認しました。返却されたライセンスの最大数に達したことが報告されています。カウントをリセットした、SO今は動作するはずです。同僚にもう一度試してもらってください。 また、同僚が次のリンクを使用して NXP.com アカウントにログインすると、独自のライセンスを取得できることにも注意してください。 https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、マイク 再アクティベーションは現在私の PC では機能していますが、以前は同じライセンスが機能していた同僚の他の PC では機能しなくなりました。同僚にもライセンスを拡張することは可能ですか?それとも、新しいライセンスを取得することは可能ですか?NXP アカウントは次のとおりです。 [email protected] [email protected] よろしくお願いします。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license 本当にありがとう、マイク。 敬具 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 あなたの権利を延長しました。新しい有効期限を受け取るSOライセンスを更新してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう。 S32DS for ARM 2018R1 のライセンスが期限切れになります。延長していただけますか?添付ファイルでご覧いただけます。 ありがとうございます。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは、 私はこの権利を2025年まで延長しました。新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 4F70-F0A3-101C-3C96 本当にSOありがとう。 Re: S32DS for ARM 2018R1 license ありがとう、マイク。 良い一日を! Re: S32DS for ARM 2018R1 license こんにちは、 両方の権利は2025年まで延長されました。インストールを再アクティベートするには、アクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は B361-6887-8BBF-ED12 さらに、私の同僚のアンナ・ダレッシオにも: E735-6A42-FED4-6005 本当にSOありがとう。 アニタ Re: S32DS for ARM 2018R1 license こんにちは@zhanglei327さん、 あなたの権利を2025年まで延長しました。インストールをライセンス サーバーと同期するには、[ヘルプ] -> [NXP ライセンス] メニューにある [更新] ボタンを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、 私の免許証はもうすぐ期限切れになります。 Re: S32DS for ARM 2018R1 license おはよう! 問題は解決しました! よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 サーバー側からライセンスを手動で返却しました。ライセンスの返却のオファーを受け取ったら、「はい」を選択してください。場合によっては、適切にリセットされない設定があり、強制的にリセットされることがあります。この後、ライセンスを返却すれば、問題なくアクティベートできるはずです。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 同じライセンス番号で再アクティブ化を試みましたが、ライセンスは別の機能用であるというメッセージが表示され続けます。ただし、最初のエラーの後、戻り値の回数を超えたことに関する 2 番目のエラーは再び発生しません。 助けていただけますか? よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 ライセンスサーバーを確認しました。返品の最大数を超えたと報告されました。返品カウントをリセットしました。これで問題は解決されるはずです。もう一度お試しください。 Mike Re: S32DS for ARM 2018R1 license おはよう、 以前と同じ番号でライセンスを再度アクティブ化しようとしましたが、ライセンスは別の機能用であると表示されます。その後、「戻る」をクリックすると、エラー メッセージが表示されます (添付ファイルを参照)。 助けていただけますか? よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。[ヘルプ] -> [NXP ライセンス] メニューから更新するか、以前と同じアクティベーション コードを使用して再アクティベーションしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 S32DS for Arm 2018R1 IDEs のライセンスが期限切れになりました。延長していただけますか? 添付ファイルで、現在のライセンスの有効期限が切れていることをCAN確認できます。 よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは、 あなたの権利を延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license 私も期限が切れてしまいました。延長していただけますか?ありがとうございます。 回复: S32DS for ARM 2018R1 license 私の番号も延長していただけますか?ありがとうございます。私の番号(A9DC-778F-BAF6-8677)は有効期限が切れています。 回复: S32DS for ARM 2018R1 license ARM V2.2 用 S32DS の公式延期を要求します。 A467-A14C-CD17-0852 Re: S32DS for ARM 2018R1 license S32DS Power V2.1 ライセンスの有効期限が切れました。 ライセンスを延長していただけますか? アクティベーションID: 1C02-6C5E-91A6-0F19 SOありがとう。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM v2.2 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 回复: S32DS for ARM 2018R1 license こんにちは。ARM バージョン v2.2 の S32 Design Studio ライセンスの有効期限が近づいています。 詳しく説明していただけますか?ありがとうございます。 私のアクティベーションコードは95F3-8275-56B8-B07Dです どうもありがとうございます。 Re: S32DS for ARM 2018R1 license tem 説明S32 Design Studio for ARM v2018 注文番号S32-DS-ARM_v2018_169264627 您能帮我延長许可证的有效期吗?激活码EBF4-DE52-80C0-FD65 非常感谢。 Re: S32 Design Studio for ARM v2.2 license马上过期了,申请延长 注文ID / ライン # S32DS-IDE-Arm-V2-X_186201937 / 1 履行された数量 1 アクティベーションコード 2107-4B0B-EBCA-A774 製品 S32 Arm v2.2 Design Studio ホスト 647F47BFF507631C69881D8FA0244925EE42B3D7 注文日 2022年8月15日
記事全体を表示
S32K1xx LIN Stack LDF parser Hi team, The customer is using an NXP S32K118 EVB with the LIN stack (LIN 2.0 protocol) and encountering terminal errors when loading a new LDF (LIN Description File). The same LDF works fine in CANoe, but not in NXP Design Studio.   Error: "Issue: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes. Level: Error Type: Tool problem Tool: Peripherals Origin: Peripherals Resource: Sources Information: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes." Occurs for sporadic frames that encapsulate unconditional frames. Error disappears when the sporadic frame name is manually added to the  configurable_frames  list — which is unexpected behavior. Is this a Design Studio issue, a limitation of the NXP LIN stack, or a problem in the LDF file? Why does the tool require sporadic frames in  configurable_frames , when this isn’t standard per LIN 2.0? Thank you, BR, Daniel LIN_STACK Re: S32K1xx LIN Stack LDF parser Hi @danielmartynek , Can you share the LDF file used by the customer? From LIN spec I read the following, which I understand that all frames shall be listed in Configurable Frames, even sporadic frames. BR Liviu
記事全体を表示