2139388_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2139388_en-US

2139388_en-US

S32K1xx LIN Stack LDF parser

Hi team,

The customer is using an NXP S32K118 EVB with the LIN stack (LIN 2.0 protocol) and encountering terminal errors when loading a new LDF (LIN Description File). The same LDF works fine in CANoe, but not in NXP Design Studio.

 

  • Error: "Issue: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes.
    Level: Error
    Type: Tool problem
    Tool: Peripherals
    Origin: Peripherals
    Resource: Sources
    Information: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes."
  • Occurs for sporadic frames that encapsulate unconditional frames.
  • Error disappears when the sporadic frame name is manually added to the configurable_frames list — which is unexpected behavior.

Is this a Design Studio issue, a limitation of the NXP LIN stack, or a problem in the LDF file?

Why does the tool require sporadic frames in configurable_frames, when this isn’t standard per LIN 2.0?


Thank you,

BR, Daniel

LIN_STACKRe: S32K1xx LIN Stack LDF parser

Hi @danielmartynek ,


Can you share the LDF file used by the customer?

From LIN spec I read the following, which I understand that all frames shall be listed in Configurable Frames, even sporadic frames.

lyxye_0-1753364292558.png



BR

Liviu

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:23 AM
Updated by: