Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Regarding Boot Configuration Settings on MIMXRT1170 Dear NXP Support Team, I have a couple of questions regarding the boot configuration settings for our project: Can we use BOOT_CFG[0:11] as individual functions when booting from fuses? When using the "Boot from Fuses" settings, do the BOOT_CFG[0:11] pins need to be pulled down or set to any specific state? I have attached images for your reference. Please update me as soon as possible. Your assistance in clarifying these points would be greatly appreciated. I appreciate your support. Best regards, Sagar Re: Regarding Boot Configuration Settings on MIMXRT1170 Fuses cannot be re-written. It is suggested to use the fuse configuration once you are completely sure that the parameters are correct.  Even with the fuse configuration you are able to enter serial download mode if boot_mode pin is available.  The ROM will behave like this: Boot_Mode is configured in Boot From Fuses (b00) - BT_FUSE_SEL = 0, No application in boot device, BootROM enters serial downloader mode - BT_FUSE_SEL = 1, valid application in boot device, BootROM gets all boot device info from fuse Boot_Mode is configured in Internal Boot (b10) - BT_FUSE_SEL = 0, valid application in boot device, BootROM gets boot device info from boot_cfg pins. - BT_FUSE_SEL = 1, valid application in boot device, BootROM gets all boot device info from fuse Best regards, Omar Re: Regarding Boot Configuration Settings on MIMXRT1170 Hello @Omar_Anguiano , Thank you for the quick reply. I have another query: if we use Boot from Fuses, can we change it later if we want to? Is Serial Downloader and Internal Boot compulsory? If we set the fuses, can we change the fuse settings afterward? In the reference design file, it is mentioned that the Boot Mode selection header should be used only during the development phase. We use Boot Selection settings during the development phase, but after finalizing the production phase, we switch to Boot from Fuses. What happens if we want to change the bootloader and firmware again after setting Boot from Fuses? Thanks  Sagar Re: Regarding Boot Configuration Settings on MIMXRT1170 If using boot from fuses then the boot_cfg pins can be used for other purpose as the ROM will read the values from the fuses instead of the GPIOs. The state of the pins can be as a normal pin as the state of the GPIO will not be read on that mode. Best regards, Omar
View full article
What is the use of the dcf_config.c file under the board folder of the S32K396 project? Re: What is the use of the dcf_config.c file under the board folder of the S32K396 project? Hi .@danielmartynek, Is there a way to modify DCF clients using DCD tools? Re: What is the use of the dcf_config.c file under the board folder of the S32K396 project? Hi @qingwang_a, There is S32K3xx_DCF_clients.xlsx attached to the Reference Manual. You can refer to these excel calculators for MPC57xx, It is similar to the S32K3 DCF. https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC57xx-DCF-records/ta-p/1114884 Here is this C40_Ip RTD example that writes a new DCF record. https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-DCF-POR-WDG-EN-DS35-RTD300/ta-p/1849816 Regards, Daniel Re: What is the use of the dcf_config.c file under the board folder of the S32K396 project? Thank you for your reply. Do you have any examples or documentation on using DCD_tool to modify dcf_client? Re: What is the use of the dcf_config.c file under the board folder of the S32K396 project? Hi @qingwang_a, This is configurable in DCD Regards, Daniel
View full article
CodeWarrior 2.1およびCodeWarrior 10.6 PEドライバ PEドライバ(multilink_universal_install_12.2)はCodeWarrior 2.1 IDEで使用できますが、CodeWarrior 10.7では使用できませんので、12.7をインストールする必要があります。PEドライバはCodeWarrior 2.1 IDEとCodeWarrior 10.7 IDEの両方で使用できますか? Re:CodeWarrior 2.1およびCodeWarrior 10.6 PEドライバ ご回答をよろしくお願い申し上げます。 Re:CodeWarrior 2.1およびCodeWarrior 10.6 PEドライバ ITが見つかりません elf.file 、elfファイルをパスに再読み込みします Re:CodeWarrior 2.1およびCodeWarrior 10.6 PEドライバ ご返信いただきありがとうございます Re:CodeWarrior 2.1およびCodeWarrior 10.6 PEドライバ こちらから入手できるP&Eパッチのインストールをお試しいただけますか。 https://www.pemicro.com/downloads/download_file.cfm?download_id=463 これにより、互換性のあるすべての PEmicro インターフェイスのサポートが CW MPC55xx/56xx v2.10 に更新されます Stan
View full article
CodeWarrior 2.1 和 CodeWarrior 10.6 PE 驱动程序 PE 驱动程序(multilink_universal_install_12.2)可以在 CodeWarrior 2.1 IDE 上使用,但不能在 CodeWarrior 10.7 上使用,必须安装 12.7。PE 驱动程序是否可以在 CodeWarrior 2.1 IDE 和 CodeWarrior 10.7 IDE 上使用? 回复:CodeWarrior 2.1 和 CodeWarrior 10.6 PE 驱动程序 非常感谢! 回复:CodeWarrior 2.1 和 CodeWarrior 10.6 PE 驱动程序 找不到 elf.file,请重新加载 elf 文件到路径 回复:CodeWarrior 2.1 和 CodeWarrior 10.6 PE 驱动程序 谢谢你的回复 回复:CodeWarrior 2.1 和 CodeWarrior 10.6 PE 驱动程序 您可以尝试安装此处提供的 P&E 补丁吗? https://www.pemicro.com/downloads/download_file.cfm?download_id=463 这应该更新所有兼容 PEmicro 接口的支持到 CW MPC55xx/56xx v2.10 Stan
View full article
S32G3 bsp38 u-boot loads PFE firmware Hi, I am using BSP38 and have programmed the fip.s32-sdcard file to the eMMC. During the U-Boot boot process, I encountered a failure loading the PFE firmware, returning -1. According to the output of mtd list, the PFE firmware should be located at address 0x0000030a0000-0x000004000000. I used Flashtool to program the s32g_pfe_class.fw file to address 0x30a0000 and set the pfengfw variable in the environment. Despite these steps, the PFE firmware still fails to load. Could you provide guidance on the correct steps to ensure that U-Boot loads the PFE firmware properly? Thanks, XD => print pfengfw pfengfw=0x30a0000 => pfeng info Failed to get speed of XPCS for emac1_xpcs** No partition table - mmc 0 ** PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -1 PFE mode: enable emac0: sgmii emac1: sgmii emac2: rgmii fw: '0x30a0000' (from env) => Re: S32G3 bsp38 u-boot loads PFE firmware Hello, @XD  Thanks for the reply. I've checked the related document, but seems currently no related script found, from my opinion, you may directly use the partation table of pre-built full images, then copy the PFE firmware to correct place. Sorry for your inconvenience. BR Chenyin Re: S32G3 bsp38 u-boot loads PFE firmware Hi Chenyin, Thank you for your reply. Do you have the partition table or the script to generate the image for reference? Thanks, XD Re: S32G3 bsp38 u-boot loads PFE firmware Hello, @XD  Thanks for the post. Yes, the uboot loads the PFE firmware from the partition 1. Currently, from the BSP UM, only the full disk image that generated from Yocto build includes both FIP and PFE firmware. BR Chenyin Re: S32G3 bsp38 u-boot loads PFE firmware It appears that the eMMC lacks a partition, and U-Boot requires a FAT partition to load the firmware file. Is there a way to generate a file that includes both the FIP and PFE firmware? Alternatively, is there another method to enable U-Boot to locate the firmware file? Thanks, XD
View full article
文档_OTA_安全启动_88MW320 没有文档,只有示例。请帮我找到所需的文件 回复:Documentation_OTA_Secure-Boot_88MW320 你好, 请提供一些解释工作流程的文档,或者任何通用的secureboot.c,secureboot.h 和 boot.c 和 boot.h文件对我来说很有用。 此外,如果有文档解释 MQTT 和 HTTP 流程,那将会非常有帮助。@DanielRuvalcaba 回复:Documentation_OTA_Secure-Boot_88MW320 你好, 那么引导加载程序呢?是否有特定的 boot.c 文件?和 boot.h 或 secureboot.c 和 secureboot.h 此外,除了 SDK 包中的文档之外,还有其他可用的东西吗?我需要一些用于 HTTP、MQTT 的应用程序开发。 回复:Documentation_OTA_Secure-Boot_88MW320 您好,我正在使用适用于RDMW320-R0 (88MW320_xx_xxxx) 的 SDK 版本 2.9.13,该版本是从 MCUXpresso SDK 构建器下载的 问题是,当我下载与 SDK 一起生成的文档时,我没有获得有关 OTA、自定义引导加载程序开发、安全启动、HTTP/HTTPS、MQTT、MbedTLS 和类似 API 的应用程序说明或其他内容的详细信息。
View full article
IMX8MP - PMIC 故障 大家好, 我们在设计中使用 IMX8M,并使用 PCA9450 PMIC 为其供电。我们的设备在 12VDC 上运行。我们面临的问题是,如果设备使用12V电池供电,那么在设备开启关闭的许多时候,PMIC IC就会损坏。在这里,我们的观察是,只有PMIC受到损坏,没有其他IC或元器件有任何问题。如果我们更换 PMIC,那么板就会开始工作。我们检查了电源设计,没有发现问题。有人遇到过类似问题吗?如何才能解决问题。 谢谢。 PMIC Re: IMX8MP - PMIC Failure 嗨,@Dip_2783! 请确保遵循正确的开机和掉电顺序。如果处理器或 PMIC 正在开启或关闭,则任何电压轨都不应保持激活状态。此外,电源轨不应连接到任何可能干扰 PMIC 或处理器输入/输出的外设。 如果您愿意,可以通过我们的案例门户申请方案审查。我们可以帮助验证您的连接,并提出必要的更改建议。 致以最崇高的敬意, Chavira Re: IMX8MP - PMIC Failure 你好,@Chavira、 关于电源轨连接。大家都知道,5VDC 用于给 PMIC 供电。 3.3VDC 和 1.8VDC 用作上拉或外设集成电路电源。 电源轨 VPP_2V5 用于为 DDR4& 供电,而 VPP_2P85 则用于以太网 PHY。 我们观察到的是,设备在直流电和PoE上可以正常运行,但是当它使用12V电池供电时,它可以多次平稳运行,但有时在开启/关闭时它会突然停止工作。只有在电池上才会出现这种故障,在其他任何电源上都不会出现。 谢谢  Re: IMX8MP - PMIC Failure 嗨,@Dip_2783! 我注意到有几个电源轨(3.3VDC、1.8VDC、VPP_2V85 和 VPP_2V5)始终保持激活状态。 这些电源信号不应连接到任何直接与处理器接口的外设上,尤其是在上电/掉电过程中。 能否请您提供连接详情或示意图,说明这些电源轨的走向? 此外,您能否确认这些电源信号在关机期间是否会干扰 PMIC?这有可能解释我们观察到的问题。 期待您的反馈。 顺祝商祺! 查维拉 Re: IMX8MP - PMIC Failure 你好,查维拉、 请参见所附的 FYR 示意图。 请注意,我们在 VIN+ 和 VIN- 上连接 12V 电池。 此致 浸渍 Re: IMX8MP - PMIC Failure 嗨,@Dip_2783! 感谢您联系恩智浦支持中心! 能否请您提供示意图,说明电池是如何连接到 PMIC 的? PMIC 上的 VSYS 引脚最大支持 6V 输入电压。您如何降低 12V 电池的电压,以确保其保持在安全工作范围内(6V 或更低)? 期待收到您的电路图,以便我们为您提供进一步的帮助。 致以最崇高的敬意, Chavira
View full article
无法使用 Segger j-link V9 调试器调试 S32k311 微控制器 我一直在使用 Elekronika India 的评估板开发基于 s32k311 MCU 的 18s 电池管理系统 解决方案。Segger j-link V9-G JTAG 调试器用于闪存和调试。 但当我们调试示例代码时,闪存闪烁后,PC 进入随机 RAM 位置,而不是主函数。附上图片供您参考。除主断点外,没有其他断点。但电脑没有停在主内存,而是转到随机内存位置并停在那里。我用 S32k311 的另一个示例代码进行了尝试,得到了相同的输出结果。   请提出解决方案。   Re: Unable to debug S32k311 mcu using Segger j-link V9 debugger 问题出在 JTAG 适配器板上的 Segger 连接器上。它无法在调试会话之前 RESET 控制器。现在已经解决了。 Re: Unable to debug S32k311 mcu using Segger j-link V9 debugger 你好 但是,当我们调试示例代码时,闪存闪烁后,PC 会进入随机 RAM 位置,而不是进入主函数 好吧,我觉得很奇怪。内核将执行加载的指令。而不是一些随意的人。 在您的软件系统中必须执行一些分支(跳转)到该 RAM 位置。要执行分支,必须在核心寄存器中定义 RAM 位置。 如果按步骤进行调试,就会看到指向 RAM 的分支发生的确切位置及其先决条件。 但电脑没有停在主内存,而是转到随机内存位置并停在那里。我用 S32k311 的另一个示例代码进行了尝试,得到了相同的输出结果。 是的,如果没有达到主断点,就不会在主断点停止。 由于另一个示例给出了相同的结果,因此如果您使用我们的 EVB,可能是电路板上的一些跳线设置。 我们为 EVB 提供了入门指南,其中介绍了所有必要的硬件设置。 但启动调试只会告诉你问题出在哪里。 顺祝商祺! Peter Re: Unable to debug S32k311 mcu using Segger j-link V9 debugger 请查找 gdb 服务器日志以供参考
View full article
替代 LPC1768 系列的推荐微控制器系列是什么? 您好, 请就 LPC17xx 系列的精确引脚对引脚替换提出建议。 我有现有的设计,修改硬件是个问题,但我有很多使用 LPC2148 外围设备(UART、I2C、计时器等)的代码(很多),哪个新系列与外设软件兼容? 建议用于新设计的哪个系列具有大致相当的能力(内存大小、速度、外设等)? Re: What is the recommended microcontroller series that replaces the LPC1768 series? 我也有同样的问题,而且现在已经过去快 5 年了。 新设计应该使用哪个系列的微控制器? Re: What is the recommended microcontroller series that replaces the LPC1768 series? HI LPC1768 是 LPC2368 的替代品。而 LPC1769 则是 LPC1768 的替代品。唯一不同的是最大时钟频率(120Mhz)。内存较少的替代品是LPC1766。LPC4078是更换LPC176x的选项。(http://www.nxp.com/products/microcontrollers/core/cortex_m4_m4f/LPC4078FBD100.html) 请注意,LPC4078 的版本时间为 2013 年,寿命为 15 年。 我们的建议是 LPC546xx 或 LPC540xx MCU 系列,基于 220MHz 的 Cortex M4 内核(带有可选的辅助 Cortex M0+ 内核)、类似的外围设备、高达 512KB 的闪存和高达 200KB 的内存。请在以下链接中查看更多信息:https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus:MC_1414576688124 LPC546xx 和 LPC540xx 不是 LPC17xx 的引脚对引脚替代品 祝您愉快 张俊
View full article
人工智能与人类智能有何不同? Brolly Academy 提供广泛的 IT 潮流课程,旨在为学生提供宝贵的技能和 100% 就业援助。 以下是您可以在布罗利学院探索的 50 门热门 IT 课程 我们在海得拉巴提供最好的generateai 培训 Re: How does AI differ from human intelligence? 有趣的讨论人工智能的优势在于快速处理大量数据,而人类智能则增加了直觉、情感和对上下文的理解。两者都有独特的能力,将它们结合起来往往能找到最有效的解决方案。值得探讨的好话题!https://vignesh156.aiskills.in/   Re: How does AI differ from human intelligence? "有见地的讨论!人工智能在数据处理和模式识别方面非常出色,但人类智能在创造力、同理心和道德判断力方面仍处于领先地位。将这两种优势结合起来,才是真正的力量所在。       Re: How does AI differ from human intelligence? 欢迎来到 Brollyai,您在掌握未来技术方面值得信赖的合作伙伴 Brollyai 成立于 2021 年,其诞生源于一个愿景,即在有抱负的技术爱好者与快速发展的人工智能世界之间架起一座桥梁。我们专用于在最前沿的人工智能领域提供一流的教育和实践培训。 我们的团队拥有丰富的知识和 15 年的行业经验。我们经验丰富的教师对最新的技术进步有着深刻的理解,确保学生获得最高质量的教育和培训。 我们提供: 在布罗莱艾,我们的专长是 生成式人工智能: 潜入创造性人工智能应用的世界,从图像生成到高级自然语言处理。 提示工程: 学习设计有效提示的艺术和科学,以充分发挥人工智能模型的潜力。 机器学习: 全面了解从基础概念到高级算法的机器学习技术。 我们提供最好的 培训在海德拉巴 Re: How does AI differ from human intelligence? 速度& 处理能力--人工智能可以在数秒内分析海量数据集,而人类则需要更长的时间。 模式识别--人工智能擅长从数据中发现人类无法识别的复杂模式。 决策--人类使用推理和直觉,而人工智能则依赖算法和统计模型。 适应性--人工智能会随着数据的增多(机器学习)而不断改进,但人类可以将创造力和情境应用于新问题。 错误处理--人工智能可以减少人为错误,但在处理模棱两可或不完整的数据时可能会遇到困难,而人类可以更好地解释这些数据。 在 数据分析人工智能提高了效率,但人类智慧对于战略思考和决策至关重要 Re: How does AI differ from human intelligence? 人工智能与人类智慧截然不同!人类从经验和情感中学习,从而产生创造力和直觉。相比之下,人工智能依赖于数据和算法,因此在特定任务中表现出色,但在新情况下灵活性较差。虽然我们可以驾驭复杂的社会动态并具有自我意识,但人工智能却无法真正理解或感受。 https://generativeaimasters.in/prompt-engineering-course-in-hyderabad/"> 海得拉巴的及时工程课程
View full article
使用 MCUXpresso 对 PN7642 进行编程 你们好 我在 MCUXpresso(v24.12.148)上使用 #PN7642(开发套件)时遇到两个问题、SDK 版本 2.12.5) 首先,我无法将kGPIO_I2CM_SDA和kGPIO_I2CM_SCL引脚用作输出引脚。尝试将它们设置为高电平,结果是 0.5 V 电平。 我尝试将 SPIM 引脚作为输出,结果没有问题。 第二个问题是,我无法使用 Peripheral+ 视图查看寄存器值。当我在调试模式下停止控制器时,所有寄存器都是红色的。只有计时器元器件向我显示一些值。什么原因会导致这种情况? 顺祝商祺! 奥利弗 Re: Programming PN7642 with MCUXpresso 你好@MPEngineering 这应该与 IDE 有关。您可以使用中间变量 (reg_value) 进行调试。也就是说,可以读取外设寄存器的值并将其赋值给 reg_value,然后将 reg_value 添加到调试窗口。此时,您可以看到寄存器的值。建议您尝试一下。 Re: Programming PN7642 with MCUXpresso 我想知道最近写入控制器的寄存器值。 根据我的理解,我使用 Peripherals+ 视图来显示最近的数值。 因此,在调试模式下停止控制器,应该能看到这些值,但我只看到红色突出的寄存器,没有看到值。 问题出在哪里? 顺祝商祺! Re: Programming PN7642 with MCUXpresso 你好@MPEngineering 应该如下所示: Re: Programming PN7642 with MCUXpresso 嘿,KaiLi、 明白了 那么注册视图又是什么呢?请看附图。 顺祝商祺! Re: Programming PN7642 with MCUXpresso 你好@MPEngineering 应配置寄存器 PCRM_PADOUT (0xBB),将 SDA/SCL 设置为通用 GPIO,然后将这两个引脚配置为高电平或低电平输出。
View full article
S32K314 亲爱的先生 我们是第三方编程器制造商,已经支持代码闪存和数据闪存块编程。 我们有一位客户希望对 UTEST 块(0x1B00_0000~x1B00_1FFF)进行编程。 是否有任何编程文档(编程过程和方法)可供参考? 代码闪存和数据闪存的编程方法是否相同? 谢谢! Re: S32K314 你好@gary_yang 您可以查看本文件"3.5 节。UTEST 部门".这可能会回答你的大部分问题: https://www.nxp.com/webapp/Download?colCode=AN13388&location=null 我想强调的是:这是无法删除的 OTP 内存。有些区域是预留的,有些区域用于设备配置,有些区域是留给客户/应用程序使用的。 如应用笔记中所述,请参阅 S32K3 参考手册中附带的 S32K3xx_DCF_client.xlsx。"UTEST Memory Map" 页面描述了相关内容。 问候, Lukas
View full article
LS1017 - XSPI_B読み取りエラー NXPサポートチームの皆様、こんにちは。 LS1017 デバイスの XSPI_B インターフェースで読み取りの問題があります。 ハードウェア情報/セットアップ: CPU XSPI_BはマイクロセミFPGAにコネクテッド CPU プラットフォーム周波数 = 400 MHz、CPU 速度 = 1500 MHz --> XSPI Errata A-050568 は適用されません 単一のポイントツーポイント接続(トレース長約70mm、±2mmに一致) DDRモード 50 MHz (100Mbit) LS1017ではIPモードコマンドのみが使用されます DQSはFPGAによって駆動されます - 読み取りストローブ(MCR0[RXCLKSRC]==3) DQS サンプリング ポイントの DLL は次のように設定されます: SLVDLYTARGET=0xF; DLLEN=0x1; OVRDEN=0x0; DLLxCR の他のフィールドはリセット値 (すべてゼロ) として保持されます CS-Signalのみが4.75kのプルアップ抵抗を持っています PCBレベルでの信号整合性のシミュレーションは良好に見える エラー/テスト関数: 最初に、LS1017 (VxWorks オペレーティング システム) 上のテスト機能がランダム パターンを生成し、それを FPGA 内のテスト メモリに 1 回書き込みます。 書き込みトランザクションが完了すると、関数は FPGA テスト メモリからパターンを定期的に読み取り、それを元の値 (読み取りループあたり 512 バイト) と比較します。 添付されているのは、エラーを示すテスト関数のコンソール出力の例です。 テストメモリの内容を5000回読み取って検証してみました。このCASE、最初の 1207 回の実行ではエラーは発生しませんでした。実行 1208 にエラーが含まれていました。 エラーパターンには顕著な特徴があります。 エラーは64バイト整列(=IPコマンド長)で発生します --> (添付の例:オフセット384/64=6) エラーはちょうど64バイト長です(=IPコマンド長) -->(添付の例:オフセット448-384=63 64 個のエラー バイトのうち、2 バイトごとにのみエラーがあります --> DQS の立ち下がりエッジですか? 2番目のバイトが64バイト全体でシフトされているようです オフセット384-391が予想されます: 0x d5 79 23 80 52 56 5e 4d オフセット384-391実際: 0x d5 8a 23 79 52 80 5e 56 他のテスト関数の実行では、エラーは同じ特徴を持ちますが、実行とオフセットが異なります。 私の質問: 過去に同様の読み取り問題を経験したことがありますか リファレンスマニュアルの図 187。DQS は A_SCLK/B_SCLK と位相を合わせて描画されますが、実際には DQS の立ち上がり/立ち下がりエッジはラウンドトリップ時間 + FPGA リードタイムによってシフトされます。(CASEでは8〜10 nsの大きさ)。内部の DQS サンプリング メカニズム / DLL 遅延ラインがどのように機能しているかについて、詳しい情報を提供していただけますか?(例: DLL のタイムベース) データシート表49。パラメータ T/2 を使用したCS 出力ホールド時間/CS 出力遅延の式が含まれています。Tは同じ表で前述したFSCKの期間ですか?FSCK = シリアル ルート クロック?--> このCASE、T=10ns でしょうか? データシート図32.: FlexSPI DDRモード2 = (MCR0[RXCLKSRC]=0x3)? 表48のTFSIDVW値はMCR0[RXCLKSRC]=0x3のDDRモードにも適用されます。 よろしくお願いいたします。 SL QorIQ LS1デバイス Re: LS1017 - XSPI_B read errors こんにちは@Stefan_L このメールがあなたのお元気を願っています。 これは同期の問題かもしれません。 いくつか質問させてください。 セクションの注記を考慮しましたか? 18.5.14.4 サンプリング用のDLL構成: シリアルルートクロックが100MHz未満の場合、DLLは遅延のためシリアルルートクロックの半サイクルにロックすることができません。 遅延チェーンではセル数が制限されます。代わりに、DLL を次のように構成する必要があります。 — オーバーデン=0x1 — OVRDVAL=N; DLL 内の各遅延セルは約 75 ps ~ 225 ps です。DLL遅延チェーンの遅延は(N * Delay_cell_delay)、N は最大値に基づいて設定する必要があります。現在のプロジェクトがサポートしているDDR周波数、N = 17、これは推奨値であることに注意してください。実際のアプリケーションで障害が発生した場合は調整が必要になることがあります。 — DLLxCRの他のフィールドはリセット値(すべてゼロ)のままにしておく必要があります LS1017 からのルート クロック信号の波形を提供していただけますか? QorIQ LS1028A リファレンス マニュアル、Rev. 0、12/2019 のセクション「18.6.6 FPGA デバイスでのアプリケーション」の情報を考慮しましたか? 素晴らしい一日をお過ごしください。 BR、 ヘクトル5世
View full article
How can TJA1465 determine that the current wake-up cause is a specific frame wake-up I would like to ask the experts, TJA1465 is only configured with WUF. When I perform a specific frame wake-up, how can I determine the current wake-up cause? I can be sure that the CW bit will be set to 1, but there are other messages being sent on the bus, and CW will also be set to 1, which will cause interference. Are there any other ways or registers to determine the wake-up cause Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up The two wake-up distinctions are set in advance via CPNC / PNCOK, and he has a wake pin for local wake-ups. The TJA1465 supports remote wake-up via a CAN wake-up pattern (WUP) or selective wake-up via a CAN wake-up frame (WUF). --- So it's wake up with wake pin, configured with CPNC / PNCOK that is selected to wake up, do not configure CPNC / PNCOK to wake up is WUP wake up, explain clearly? Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up Thank you very much for your answer. Maybe I didn't describe it clearly. I have already implemented Specific Frame Wake-up (WUF). When the ECU is awakened, I would like to know if there is a way to determine through register setting or other methods that the reason for the wake-up is due to this specific frame, because there are other wake-up sources in the entire network that need to be distinguished Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up These two wakeups are still fundamentally different see below, as well as the settings before the wakeup: CAN wake-up pattern (WUP) The CAN wake-up pattern (WUP) is used for two purposes. To activate CAN biasing in CAN Offline mode (transition from CAN offline to CAN OfflineBias) To trigger a CAN wake-up event The following conditions must be met to trigger a wake-up event via a CAN WUP. The CAN transceiver is in CAN Offline or CAN OfflineBias mode CAN wake-up enabled (CWE = 1) CAN wake-up frame detection (WUF) deactivated (CPNC = 0 or PNCOK = 0)   CAN wake-up frame (WUF) CAN partial networking through selective wake-up detection allows a device in a CAN network to be selectively woken up in response to a wake-up frame (WUF) on the CAN bus. Selective wake-up detection uses one of two filtering methods. Identifier-only filtering (PNDM = 0) Identifier + data length code + data mask filtering (PNDM = 1) The following conditions must be met to enable CAN WUF functionality. CAN biasing needs to be activated (CAN OfflineBias, CAN ListenOnly or CAN Active mode). CAN wake-up enabled (CWE = 1) CAN partial networking configuration completed (PNCOK = 1) CAN partial networking enabled (CPNC = 1) No CAN partial networking error detected (CPNERRS = 0)
View full article
S32DS RTD3.0.0 IDEsのスタック問題 こんにちは: 質問があります。MEX ファイルの各コンポーネントまたは変数を変更するたびに、S32DS IDEs ツールが非常に遅くなるということです。 S32DS IDE ツールの車載生成コードや、それを閉じることができる関連構成はありますか? たとえば、CANハードウェア オブジェクトのシーケンスを移動したいのですが、ステップを移動するたびにしばらく停止してしまいます。本当に困っています。 よろしくお願いします。 BR、ビルウェン Re: S32DS RTD3.0.0 IDE tool stuck problem これまでこれをやったことがないので、問題がないとは保証できません。インストール中に問題が発生した場合はお問い合わせください。 Re: S32DS RTD3.0.0 IDE tool stuck problem こんにちは@Robin_Shen : ご返信ありがとうございます。 S32DSv3.6.1 + S32K3 RTD 3.0.0 は使用できますか?出来ますか?私たちは RTD3.0.0 をベースに BMS を開発しているので、RTD6.0.0 に変更する場合には多くの労力が必要になります。一時的に、他の実装に重点を置きたいと考えています。 ありがとう BR、ビルウェン Re: S32DS RTD3.0.0 IDE tool stuck problem S32DSv3.6.1 + S32K3 RTD 6.0.0 をインストールして、MCAL プロジェクトでペリフェラルを構成するパフォーマンスが向上するかどうかを確認することをお勧めします。 Re: S32DS RTD3.0.0 IDE tool stuck problem こんにちは@Robin_Shen : すでに3.5.14にアップデートしましたしかし、まだ非常に遅く、Xmx を 12G に変更しても、同じようです。 他に何か提案はありますか?それともS32DS 3.6バージョンを使うべきでしょうか? よろしくお願いします。 BR、ビルウェン Re: S32DS RTD3.0.0 IDE tool stuck problem この問題は S32DS アップデート 12 以降で修正されました。それ以降のバージョンにアップデートすることをお勧めします。 オンラインで更新することもできます。S32DS拡張機能と更新を開き、 S32 Design Studio プラットフォーム パッケージとS32 Design Studio プラットフォーム ツール パッケージを更新します。 または、S32DS Update 12 ( SW32_S32DS_3.5.12_D2405.zip ) などのオフライン更新パッケージをダウンロードします。 または、JVM メモリを拡張します。同様の場所 C:\NXP\S32DS.3.5\eclipse\s32ds.ini に移動し、-Xmx パラメータを 8Gb に増やします。 Re: S32DS RTD3.0.0 IDE tool stuck problem こんにちは、Robin_Shen: ご返信ありがとうございます。 私のソフトウェア環境はS32DS 3.5とRTD 3.0.0です。S32DS をバージョン 3.5 から 3.6 にアップデートする必要があるということでしょうか? ありがとう BR、ビルウェン Re: S32DS RTD3.0.0 IDE tool stuck problem こんにちは、BillWenさん。 S32K3 RTD 3.0.0何年も前にリリースされました。 お客様には常に、リリース ノートに記載されている最新の RFP 品質の S32K3 RTD と S32DS バージョンを使用することをお勧めします。 この問題は S32DS v3.5 アップデート 12 で修正されました。 よろしくお願いします、 ロビン --------------------------------------------------------------------------------- 注記: - この投稿があなたの質問への回答である場合は、「解決策として承認」ボタンをクリックしてください。ありがとう! - Threadは最後の投稿から7週間フォローされます。それ以降の返信は無視されます。 後ほど関連する質問がある場合は、新しいThreadを開いて、閉じたThreadを参照してください。 ---------------------------------------------------------------------------------
View full article
NTAG 424 DNA即使锁定还能被擦除吗? 您好,我想使用 NTAG 424 DNA 标签包含在产品中,并使用 URL 来访问其他详细信息。我想锁定这些标签,以便在发货后任何人都无法更改或删除它们。 我尝试了 NXP TagWriter Android 应用程序中的锁定功能,包括“软保护”和“锁定标签”。这两种方法都可以有效防止将不同的数据写入标签。但是,我仍然可以使用“擦除至出厂默认设置”功能来擦除内容。在此之后,标签显示为“空”内容,并且由于它们被锁定,我无法再次在其上书写,因此它们实际上变得毫无用处。 有没有其他方法可以锁定它们,使它们无法被删除?也许使用不同的软件? 顺便说一句,我也尝试使用“密码保护”来保护这些标签的写入,但我一直收到错误消息,提示这些标签不支持该功能。 当我扫描一个首先受到软保护然后被擦除并且现在不可写的标签时,我附加了 TagInfo 的输出。 谢谢,如有任何见解我将不胜感激。 回复:NTAG 424 DNA 即使锁定仍然可以被擦除吗? 你好@dgobera ,祝你有个愉快的一天! 非常感谢您对我们的产品感兴趣。 为了能够再次写入“已擦除为出厂默认设置”的标签,您可以尝试使用 NXP TagWriter 应用程序的“删除保护”功能,这在复制您描述的过程时对我有用,之后您应该能够再次将 NDEF 写入标签。 为了防止标签被覆盖或擦除,必须更改标签内 NDEF 文件的写访问权限,此过程在NTAG 424 DNA 数据表的第 8.2.3.3 和 11.7 节中进行了描述。为了执行此过程,我建议看一下我们推荐的RFIDDiscover软件应用程序,该应用程序是一种与PEGODA 非接触式智能卡读卡器一起使用的工具,并提供了一种探索 NTAG 424 DNA 和其他智能卡功能的简便方法。 请注意,为了访问该工具,您需要签署一份保密协议 (NDA),因为该软件是 NXP 安全资源的一部分。 谨致问候, 丹尼尔。
View full article
S32K344 Flash Memory Erase Cycles life   #define FLS_MASTER_ID                0U #define FLS_BUF_SIZE                 80U #define FLS_SECTOR_ADDR              0x00600000U #define FLS_SECTOR_TEST              C40_CODE_ARRAY_0_BLOCK_2_S256    void FlashWrite()  {      /* Unlock sector if needed */     if (STATUS_C40_IP_SECTOR_PROTECTED == C40_Ip_GetLock(FLS_SECTOR_TEST))     {         C40_Ip_ClearLock(FLS_SECTOR_TEST, FLS_MASTER_ID);     }       /* Erase sector */     C40_Ip_MainInterfaceSectorErase(FLS_SECTOR_TEST, FLS_MASTER_ID);     do     {         C40Status = C40_Ip_MainInterfaceSectorEraseStatus();     }     while (STATUS_C40_IP_BUSY == C40Status);     /* Check job result */     Fls_ExampleAssert(STATUS_C40_IP_SUCCESS == C40Status);       /* Write data */     C40_Ip_MainInterfaceWrite(FLS_SECTOR_ADDR, FLS_BUF_SIZE, TxBuffer, FLS_MASTER_ID);     do     {         C40Status = C40_Ip_MainInterfaceWriteStatus();     }     while (STATUS_C40_IP_BUSY == C40Status);     /* Check job result */     Fls_ExampleAssert(STATUS_C40_IP_SUCCESS == C40Status);       /* Compare the data in memory with TxBuffer */     C40Status = C40_Ip_Compare(FLS_SECTOR_ADDR, FLS_BUF_SIZE, TxBuffer);     /* Check job result */     Fls_ExampleAssert(STATUS_C40_IP_SUCCESS == C40Status);      }   I am Calling this function FlashWrite() for every 1 Minute and MCU is working 24HRs so considering that how much flash memory life i'll get. Also let me know how to calculate it?   S32K344-WB   Re: S32K344 Flash Memory Erase Cycles life Dear  @lukaszadrapa and @narsimh_kamath  Thanks for the detailed information and calculations. This is what i was looking for. Re: S32K344 Flash Memory Erase Cycles life Thank you @lukaszadrapa  The simplified calculation & insight you offer is very helpful! It does look like if the interval for writing 32B data were increased from 'every 1 min' to ' every 2 min' , then certainly the desired EEPROM emulation can be achieved with a 15 year lifetime. Would you agree? Re: S32K344 Flash Memory Erase Cycles life There's 128KB of data flash. Even if I do not consider any overhead caused by Emulated EEPROM mechanism: "data flash size" / "user data" = 128KB / 2KB = 64 updates So, the data flash will be full just after 64 updates. We can perform 100,000 cycles on data flash, so it will gives us 6,400,000 updates. Doing this every 1 minute for 24 hours a day for 15 years: 6,400,000 / 60 / 24 / 365 = 12 years But that's ideal situation without any EEE overhead. Fee needs additional data in flash, so it will be less than 12 years. If you add additional 1MB from code flash: 1024KB / 2KB = 512 updates We can perform 1000 cycles on code flash: 512,000 updates 512,000 / 60 / 24 / 365 = 1 year So, this also does not make a difference. If you want to know the endurance exactly (with EEE overhead), you can find section "3.6.9 Endurance calculation" in Fee user manual. c:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Fee_TS_T40D34M50I0R0\doc\RTD_FEE_UM.pdf But you are not able to reach 15 years in this use-case. Regards, Lukas Re: S32K344 Flash Memory Erase Cycles life Hi @lukaszadrapa , thanks. I notice we now support FEE in the latest MBDT for S32K3 (V1.6.0) . Could you help share some insight to the calculation involved for estimating if a certain use-case is feasible or not (in terms of Flash / emulated EEPROM specifications for S32K3). E.g. , if I need to write 2KB of data every 1 minute for 24 hours a day for 15 years , can this be supported assuming I am able to use FEE & can implement a round-robin sector scheme? Re: S32K344 Flash Memory Erase Cycles life Hi @jerryrig  This is 1MB block on S32K344, so this specification applies:   I can see you are erasing still the same sector in a loop. And because one sector erase == one P/E cycle, you have only 1000 cycles available. So, if you erase the same sector each minute, you have less than 17 hours. To achieve much better numbers, I would consider to use data flash block which provides  100,000 cycles and I would use EEPROM Emulation feature. There's Autosar Fee driver in RTD for this (notice that it's not available in non-Autosar Ip layer). Regards, Lukas
View full article
S9KEAZシリーズをMCUXPRESSOに 親愛なる皆さん。 これは、S9KEAZN32ACLC MCU用のプロジェクトをMCUXpressoに作成する方法ですか?つまり、SDKを作成し、それを明白にビルドするという標準的な方法を使用しているのでしょうか? それとも、「generic M0+」エントリを使用するのでしょうか? ヒントは大歓迎です。 よろしくお願いいたします。 ジョルジェコン Re:MCUXPRESSOにS9KEAZシリーズ ありがとう、張。それは明らかです。 Re:MCUXPRESSOにS9KEAZシリーズ こんにちは、ジョルジェコン、 MCUXPRESSOはS9KEAZシリーズをサポートしていません。S32DSに対応した車載用マイコンです https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-design-studio-for-arm:S32DS-ARM 関連する BSP とドライバは、このページの「組み込みソフトウェア」にあります https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/automotive-mcus/ultra-reliable-kea-automotive-microcontrollers-mcus-based-on-arm-cortex-m0-plus-core:KEA お役に立てば幸いです。 張 俊
View full article
Camera tuning on i.MX8M Quad Hello, I'd like to know if i.MX8M Quad supports camera tuning inside If i.MX8M Quad does not support camera tuning, Customer always have to apply the pre-tuned Camera Module with i.MX8M Quad? Thank you. Best regards, Andy i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Re: Camera tuning on i.MX8M Quad Hello, Thank you for your quick reply. Best regards, Andy Re: Camera tuning on i.MX8M Quad Hello, The Mx8Mplus support camera tunning trough ISP module that is not present on MX8MQ. Regards
View full article
如何基于RTOS使用S32G-VNP-RDB3(s32g399a)的PFE功能? 我们正在基于 RTOS 开发 S32G-VNP-RDB3 (s32g399a)。我知道我们需要使用 PFE 来使用多个以太网端口,但 PFE 需要应用单独的驱动程序,而我不知道该怎么做。 重新表述我的问题如下。 1.如何在S32G-VNP-RDB3(s32g399a)中使用PFE功能? 2. 有没有 PFE 的 PTP 和 TIME Aware Shaper 功能的演示文件? 如果有人知道如何使用它,请帮助我......请帮忙...... 回复:如何基于RTOS使用S32G-VNP-RDB3(s32g399a)的PFE功能? 你好 !非常感谢您的回复。 关于 Q1 当我从该页面(链接:S32G3 安全车辆网络处理器 | NXP 半导体)获取 tresos 时,我无法获得有关许可证的任何确认。相反,我从可以下载不同版本的地方下载了版本 29,检查了激活码,激活了它,并且正在使用它。 关于 Q2 和 Q3 由于缺乏文档,我在使用和开发它时遇到了困难。我会尝试检查相关的发行说明。 感谢您的帮助。如有其他问题,我将创建一个新会话来询问。
View full article