Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
LS1043A MSI interrupts Dear Sirs, I am developing a bare metal PCIe Controller (RC) driver for LS1043A, using a LS1043ARDB board. I successfully: - setup all outbound ATUs programming (using LS1043A Linux device tree addresses for system and PCIe addresses and limits). - discover PCIe bus endpoint and setup them (BARs, etc). - setup GIC. - test endpoint legacy interrupts. Now, I am stuck on MSI interrupts. I am using LS1043A PCIe controller #3 (@ 0x3600000h), and an AX99100 serial/parallel device or an I350 ethernet endpoint, both supporting MSI. I setup all MSI capability registers on endpoints, and attempted to deliver the MSI interrupt in two different ways: A) without any inbound ATU, writing in the endpoint MSI address register the address of the SCFG_G2MSIIR register (0x1573000). B) with an inbound ATU, writing in the endpoint MSI address register the PCIe bus address that the inbound ATU maps to 0x1573000 on the system bus. In both cases, no interrupt is delivered to GIC. If I write by CPU to the SCFG_G2MSIIR (0x1573000) I see the proper interrupt (192,187,188,or 189) be delivered depending on the data value I write (0, 1, 2 or 3); therefore, I assume my GIC is properly configured and SCFG is working. What am I missing to have working MSI interrupts from endpoints? Best regards Eco Re: LS1043A MSI interrupts dear Eco56, For MSI interrupts on LS1043A PCIe controller, the proper configuration requires: - The MSI address register in your endpoint devices should point to SCFG_G2MSIIR register (0x1573000) as you've attempted. - Ensure the proper GIC interrupt line is configured for the corresponding PCIe controller #3 (interrupt 192, 187, 188, or 189 as you noted). - The PCIe controller must have MSI capability enabled in its configuration space. - Verify that the inbound ATU window is correctly mapping the PCIe address space to the system memory where SCFG_G2MSIIR (0x1573000) is located. - Ensure the ATU window size is sufficient and properly aligned. - Check that transaction attributes are properly configured (No Snoop and Relaxed Ordering should be set to 0). - For your direct approach without inbound ATU: Since you can write directly to SCFG_G2MSIIR and see interrupts delivered to GIC, your GIC configuration appears correct. Try enabling the Bus Master capability for your endpoints to ensure they can initiate memory write transactions. Also verify that the endpoints' MSI capability registers are properly configured, particularly the MSI Enable bit. BR LFGP Re: LS1043A MSI interrupts Dear Sirs, I'm facing the same problem using the LS1043ARDB, and I believe I’m still missing something on the RC side. I’m testing with PCIe controller #2 (same behavior observed on controller #3). For controller #2 I’m using SCFG_G2MSIIR = 0x1572000. First of all, if I manually write from the CPU to 0x1572000, I correctly receive the MSI interrupt on the GIC, so the SCFG and GIC configuration look fine, as reported in eco56. Also, I am enabling No‑Snoop = 1 and the coherency mapping, as described in the LS1043A documentation. When I program the i350 endpoint to generate MSI: If I don’t configure any inbound iATU, as soon as the device triggers MSI I receive interrupt 160 (PCIe config/error interrupt). This makes me think the MSI Memory Write TLP is reaching the RC, but the RC is not able to translate it properly. (if I use legacy interrupt, it trigger the proper legacy interrupt) If I configure an inbound iATU, the config/error interrupt disappears, but I still don’t receive any MSI on the GIC. This is the inbound iATU configuration:     writel(0x80000000, pcie_rc->dbi + 0x900);       writel(0x00000000, pcie_rc->dbi + 0x904);       writel(0x01570000, pcie_rc->dbi + 0x90C);       writel(0x00000000, pcie_rc->dbi + 0x910);     writel(0x01573FFF, pcie_rc->dbi + 0x914);     writel(0x01570000, pcie_rc->dbi + 0x918);       writel(0x00000000, pcie_rc->dbi + 0x91C);       writel(0x80000000, pcie_rc->dbi + 0x908); With this configuration, I’m defining an inbound memory window that maps the PCIe address range 0x01570000 – 0x01573FFF into the same range on the system bus, so that inbound PCIe Memory Write transactions targeting 0x1572000 (SCFG_G2MSIIR for controller #2) should be translated and forwarded to the SCFG block. With this inbound window enabled, I no longer see the PCIe error interrupt, which seems to confirm that the inbound MSI write is now accepted by the RC. However, I still do not see any MSI interrupt being delivered to the GIC when the endpoint generates MSI. Could you please confirm if this setup is correct, or if there is any additional RC‑side configuration required to get MSI delivered to the GIC? Riccardo
View full article
LPC1754 USB 大容量存储器 我用 LPC1754 设计了一块主板,并通过 spi 将或非闪存 W25Q64 连接到它。由于使用 cmsis 文件系统无法将 或非 闪存格式化为 FAT16,我在我的项目中使用了 chan 的 FatFS,并添加了带有 cmsis 驱动程序的 keil mdk USB 设备大容量存储。连接电脑时可以正确显示设备描述符并且 Ii 被识别为大容量存储设备,但是 Windows 无法正确指定磁盘扇区的数量。形成和探索它是不可能的。 我用 f_mkfs 功能在固件中格式化了它,我几乎可以肯定 chan 的 FatFs 在我的项目中工作正常。 我想知道是否有人有过相关经验? 在线调试 Re: LPC1754 usb mass storage 你好@jalilisahar 也许以下是一个可能的原因。请检查。 默认情况下,Windows USB 大容量存储类 (MSC) 预计逻辑块大小为 512 字节。 您的 W25Q64 是 或非 闪存(64 Mbit = 8 MB),具有以下物理特征: 页面 = 256 字节擦除扇区 = 4 KB 如果 USB MSC 中的 SCSI READ CAPACITY (10) 命令未返回长度为 512 字节的区块长度,或者 FatFS diskio 层未将媒体抽象为 512 字节的扇区,Windows 将无法正确计算磁盘扇区的总数。 BR 爱丽丝
View full article
Lpspi_Ip_SyncTransmit 中的延迟 在 Lpspi_Ip_SyncTransmit 函数的开头和结尾我都遇到了这些意想不到的延迟。你可以在随附的图片中看到我所描述的痕迹。红色信号是我在 Lpspi_Ip_SyncTransmit 函数之前设置的 LED,然后在之后立即清除。如你所见,Lpspi_Ip_SyncTransmit 实际占用的时间中只有大约 25% 是传输数据。请注意,追踪中的 "DIN" 是 MISO。奇怪的是,在数据开始计时之前,它会保持高电平很长时间。这可能是什么原因造成的?我禁用了所有的 DevErrorDetect 标志,但它没有解决这个问题。有趣的是,有一次我将 LED 切换移动到仅包围 Lpspi_Ip_SyncTransmit() 中的 Lpspi_Ip_ClearCS() 函数,然后它在数据传输结束和 CS 被钳位之前增加了显著的延迟。 我曾怀疑问题是否出在 LED 的设置上,因为这将导致测试失败,但即使没有 LED 的切换,MISO 线路在传输前仍会保持很长时间的高电平,这看起来很奇怪。 Re: Delays in Lpspi_Ip_SyncTransmit HI 您使用的是哪种 S32K3? CORE_CLK 的频率是多少? 什么是 RTD 版本? RTD 附带代码包,你可以在其中找到包含每个 API 执行时间的 RTD_SPI_ProfileReport.xlsx。例如SyncTransmit ...\SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_QualityPackage\SPI\RTD_SPI_ProfileReport.xlsx 祝好, Robin ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"ACCEPT AS SOLUTION" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请另开新主题,并参考已关闭的主题。 ------------------------------------------------------------------------------- Re: Delays in Lpspi_Ip_SyncTransmit 我在 nxp 目录中没有找到您提到的 ProfileReport 文件。 我将优化功能调至 O3,延迟时间大大减少。不过,实际 SPI 通信时间周围的额外时间仍与时钟移动的时间差不多。 Re: Delays in Lpspi_Ip_SyncTransmit 请点击下载 S32K3 标准软件-> 汽车软件 -s32K3/S32M27x-Cortex-M 的实时驱动程序-> s32k3_s32m27x 实时驱动程序 ASR R21-11 版本 6.0.0 RTD_SPI_ProfileReport.xlsx中SyncTransmit的执行时间与测量结果很接近。 Re: Delays in Lpspi_Ip_SyncTransmit 我正在使用 RTD 6.0.0 和 S32k311。核心时钟频率为 120MHz。以下是 SPI 设置。 Re: Delays in Lpspi_Ip_SyncTransmit 好的,谢谢。我找到了。你是说我的结果在意料之中?我所看到的似乎与此相差无几。 Re: Delays in Lpspi_Ip_SyncTransmit 好的,感谢您提供的信息。 Re: Delays in Lpspi_Ip_SyncTransmit 是的,您的测试结果与 RTD_SPI_ProfileReport 的结果非常接近。 热门帮助:S32K3xx 如何优化 APP 代码以获得更高性能 注意 RTD 6.0.0 是使用-OS 配置版本和测试的。建议使用版本说明中所示的编译器选项。 因此,在使用与最初测试的优化级别或工具链不同的驱动程序时,我们无法保证驱动程序的功能。此外,对 RTD 的任何修改都不在我们的支持范围之内。
View full article
SR150 UWBIoT TWR 测距 - phRangingMesr.rssi 始终为 0。DS-TWR 是否支持 RSSI 或需要 CCC/RSSI? 你好 我正在使用恩智浦SR150 UWBIoT MCUx SDK(v04.08.01),并将demo_ranging_controller+demo_ranging_controlee应用程序用于 DS-TWR 测距。 测距距离和信噪比打印正确,但RSSI 始终报告为 0,无论测距距离或天线状况如何。 输出示例(取自 PrintUtility.c→ printRangingData()): TWR[0].distance = 135 cm TWR[0].rssi= 0 使用的代码: pRangingData->ranging_meas.range_meas_twr[i].rssi 我在文档中找不到必须通过宏或配置启用TWRRSSI(RANGE_DATA_NTF)的任何地方。 供应商 SNR 字段正常工作,但phRangingMesr_t 中的 rssi 成员从未填充。 我的问题 SR150 在正常 TWR 测距会话 (RANGE_DATA_NTF) 中是否支持 RSSI? (任何参数,如 NXP_EXTENDED_NTF_CONFIG、PHY 配置、会话类型等) 。 如果不是,那么RSSI 仅在以下情况下可用是否正确? CCC_RANGE_DATA_NTF(CCC/CSA 我的)— Q8.8 RSSI_RX1/RSSI_RX2 TEST_RX_NTF / TEST_PER_RX_NTF(射频测试模式) - Q8.8 RSSI 值 是否有推荐的方法在同一个数据包上同时获取距离和真实校准 RSSI? 任何官方确认或文件指针都将非常有用。 现在,信噪比打印正常,但在所有测距测试中,RSSI 仍为 0。 谢谢! Re: SR150 UWBIoT TWR ranging – phRangingMesr.rssi always 0. Is RSSI supported in DS-TWR or requires 你好 希望你一切顺利。很抱歉给您带来不便,但由于该产品的信息受 NDA(保密协议)保护,因此不对外公开。 如需了解有关该芯片的更多信息,请联系在代理商网络中提供的代理商之一?或者,如果您有任何直接联系人帮助您获得此设备,请与他们联系。 如果您正在寻找有关我们 UWB 产品的信息,或者您对该技术感兴趣,我建议您查看我们合作伙伴(Trimension UWB 合作伙伴)提供的开发套件和模块。 如果您对这些套件/模块感兴趣,您需要直接与他们联系,了解他们可以提供的流程和支持,因为这项技术的支持途径就是通过他们。 文档和软件由相应的 UWB 模块合作伙伴分发。选择模块后,您将被引导到我们合作伙伴的页面,在那里您可以访问数据表、应用笔记和所需的支持 此致, 里卡多
View full article
安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 你好,恩智浦: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗, 可以幫忙看看log 是啥麼問題?感謝! 错误: ==== 许可证列表结束。==== ==== 32-bit license service installation log start: ==== Returned: 1 Console: C:\Users\ericclsung\AppData\Local\Temp\I1764729332\Windows>cd"C:\Users\ericclsung\AppData\Local\Temp\036160.tmp\cll\i86" C:\Users\ericclsung\AppData\Local\Temp\036160.tmp\cll\i86>cllSvrUtility.exe -installService LAXCompiler -installService LAXCompiler -installService(LAXCompiler) was successful 错误:系统找不到指定的路徑。 ==== 32 位许可证服务安装日志结束。==== XMLScriptWriter:没有跳过任何安装对象 8. final log file name=C:\NXP\S32DS.3.4\_S32Design Studio for S32 Platform 3.4_installation\Logs\S32_Design_Studio_for_S32_Platform_3.4_Install_12_03_2025_10_38_16.log Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 你好、 能否提供您的恩智浦 ID?我试过您的电子邮件地址,但系统中没有这个地址。 Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 您好 NXP ,能否检查一下您的系统中是否有这封电子邮件 ID:[email protected]? Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 你好、 对不起,[email protected]也不是活动或非活动账户 。 Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 你好,恩智浦 您能再次检查我的 NXP ID 吗?我已经完成了我的个人资料。 Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 嗨,埃里克、 我检查了两个电子邮件地址,但系统中仍然没有该账户。您有激活码吗? Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 您好,恩智浦, 您指的是 S32 Design Studio v.3.4 版激活码吗?还是其他激活码? Re: 安裝S32DS.3.4_b201217_win32.x86_64.exe 失敗 你好、 抱歉耽搁了。是的,S32DS v3.4 激活码。
View full article
Wakeup Source Recognition after function reset from standby mode in MCAL - S32K3 RTD Customer Company*: HERO MOTOCORP - NORMALIZED Project Name*: N/A Customer Contact Point* (Name & Email): Aryan Kumar [email protected] SW Package Info*: S32K3_S32M27x Real-Time Drivers ASR R21-11  HW* (Board/Chipset/Platform): S32K3XX (S32K344) SW Version*: Version 6.0.0 Hello team,  I have a customer trying to know wakeup source after standby exit in MCAL. I have seen this other post talking about the process and which APIs to use. Basically, Dan mentioned (in this post: Solved: Question about the WISR with S32K3 MCAL RTD5.0.0 - NXP Community) that Icu_Init() will clear flags if called before Platform_Init(), meaning checking wake-up source with callback looks like a limitation of the RTDs. Also, Icu_GetInputState() uses global variables that needs to be initialized by Icu_Init(). Meaning that customer can only call Wkpu_Ip_GetInputState() function to check the WISR flags.  So, if I understand correctly, there are 3 ways to read wake-up source: 1. Enabling Platform after standby exit, and MCU will jump to WKPU_IRQn and service the WKPU channel. If callback is needed, customer can implement workaround by assigning Wkpu structure: Wkpu_Ip_u32ChState[0].chInit = TRUE; Wkpu_Ip_u32ChState[0].notificationEnable = TRUE; Wkpu_Ip_u32ChState[0].WkpuChannelNotification = IcuSignalNotification_Wkpu; This works as expected. 2. Calling Wkpu_Ip_GetInputState() after standby exit, as Icu_GetInputState() cannot be called before Icu_Init(), but Icu initialization clears WISR flags. However, when entering the function, if both WISR & IREER bits are enabled for the requested channel, WISR is not cleared:  If I understand correctly, these are cleared upon calling Icu_Init(), correct? 3. Directly reading WISR/WISR_64 registers. These three methods use either baremetal or IP layer. I have two questions: How to correctly implement Wkpu_Ip_GetInputState()? Is there a fix or implementation for MCAL layer, in either 6.0.0 or 7.0.0? If so, can you share the implementation? I've attached the project I used to test this, WKPU[42] is configured. SW is S32DS v3.6.4 + RTD 6.0.0. Best regards, Julián Priority: MEDIUM S32_CONFIG_TOOL S32_FLASH_TOOL S32DS Source: Direct Customer Re: Wakeup Source Recognition after function reset from standby mode in MCAL - S32K3 RTD Hi @DanNguyenDuy, Thank you for the quick response, Dan! I will inform customer. Best regards, Julián Re: Wakeup Source Recognition after function reset from standby mode in MCAL - S32K3 RTD Hi @Julián_AragónM, 1. Follow AUTOSAR requirements, the Icu module doesn't provide functions that can check wakeup source directly at the MCAL layer. Icu will transfer wakeup source information to EcuM module and this module will check wakeup source. In RTD driver, EcuM is a stub module. Follow " Specification of ECU State Manager AUTOSAR CP R21-11": 2. In Icu configuration, when user enable "IcuWkpuStandbyWakeSupport" then Icu_Init() will not clear WISR flags. In your project, to check wakeup source in the Wkpu_Ip layer, you can refer to the below code: When call Platform_Init(NULL_PTR); before Icu_Init(), I saw that somehow the WISR flags were erased. So, I called this function after Icu_Init() function. Best regards, Dan
View full article
S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode がハードフォールトを引き起こしている ETAS は GM と協力して SDV2 プロジェクトに取り組んでおり、以下の問題が発生しています。 ツールのバージョン: HSEファームウェアバージョン: ** HSE_FW_S32K344_12.2.76.0 ** LLSI インターフェース バージョン: ** LLSI_SW32K3XX_0_9_9_PRC ** 静的 MCAL バージョン: SW32K3_RTD_R21-11_6.0.0_P03 (GM暗号) SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506 (汎用MCAL) 問題の説明: Mem_Inflsで散発的な問題が見つかりました C40_Ip_AccessCodeの MCAL モジュール。 構成パラメータ: Mem-Load-アクセス-Code-On-JobStart --> 有効 フラッシュ書き込み要求が発生したとき C40_Ip_AccessCodeがRAMにコピーされる RAMから実行される ハードフォールト発生 デバッグ結果: この行からフラッシュ操作をトリガーした後 "C40_Ip_pFlashBaseAddress[C40_Ip_Instance]->MCR |= FLASH_MCR_EHV_MASK;" この行がRAMから実行されると、この行で問題が発生していることがわかりました。 「 ( 0U == ( local_C40_Ip_pFlashBaseAddress [ C40_Ip_Instance ]-> MCRS & FLASH_MCRS_DONE_MASK)) " 「 C40_Ip_pFlashBaseAddress 」このポインター配列は Const-Global であり、コードフラッシュに格納されます。 フラッシュ ドライバが別の要求を実行しているときにフラッシュにアクセスしようとすると、ハード障害が発生します。 根本的な原因: NXP Mem_Infls関数「C40_Ip_AccessCode」 RAM から実行されているものは、書き込み/消去操作の実行中にフラッシュにアクセスしています。 ERAS-FBL チームによる修正案: 内部にポインタのローカル配列を作成する 「C40_Ip_アクセスコード」 CodeFlashに保存されたものを使用する代わりに FLASH_Type * local_C40_Ip_pFlashBaseAddress [FLASH_INSTANCE_COUNT] = IP_FLASH_BASE_PTRS;" このローカル ポインタ配列を使用して、フラッシュ レジスタにアクセスします。 この修正/パッチはテスト済みで、問題はもう発生していません。 修正のためのコード変更は添付のスクリーンショットでCAN確認できます。 適用した修正が問題なく、CAN使用できるかどうかを確認したかったのです。 RAMから実行しているのに、なぜ同時にCodeFlashにアクセスしているのでしょうか?上記のコメントで示したアセンブリを見ると、コードフラッシュから配列にアクセスしようとしていることが分かります。これがハードフォールトの原因です。RAMに保存されている配列のみを使用する場合、この問題は発生しません。 追加メモ: MemAcCallback は構成されていない、SO この CASE は NULL_PTR になります。 これは、一般的な Mem_Infls 構成のスクリーンショットです。 優先度: 中 RTD 出典: 直接お客様 Re: S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode causing hard-fault より詳細なスクリーンショットを添付します: C40_Ip_AccessCodeがロードされ、 Mem_43_INFLS_AcLoadedフラグをチェックするか、フラッシュとRAMのアセンブリをチェックすることができます。 R1--> レジスタを確認してください。コード フラッシュに C40_Ip_pFlashBaseAddress のアドレスがあり、その内容をロードすると、ハード フォールトが発生します。 フラッシュステータスペリフェラルのスクリーンショットでもすべてを確認できます。 Mem_Inflsモジュールの完全な設定は、添付のzipファイルにCANあります。 Re: S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode causing hard-fault こんにちは、 @cuongnguyenphu さん、 ご確認ありがとうございます。参考までに、以下の画像をすべて再度アップロードしました。 Re: S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode causing hard-fault C40_Ip_AccessCode のこの問題を発見してくださった@vamsilankaに感謝します。 問題とご提案を理解しました。ただし、これらの画像を再度アップロードしていただけますでしょうか?問題を解決するには、RTD チーム用のチケットを作成してもらいます。現在の画像は解像度が低く、 Re: S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode causing hard-fault @vamsilanka 確認と修正のために開発チームにチケットを作成しました: https://jira.sw.nxp.com/browse/ARTDCMEM-821 その理由は、 C40_Ip_pFlashBaseAddressがフラッシュコードで定義されているためです。 回避策として、RAM に保存されるローカル ポインターを作成し、問題を解決できます CAN SO。   Re: S32K3 RTD-6.0.0 Mem_Infls C40_Ip_AccessCode causing hard-fault こんにちは、 @cuongnguyenphu さん、 このトピックに関して迅速なご返答を頂きありがとうございます。お客様に状況をお知らせします。
View full article
HSE Firmware Install Hi, I want to try to use HSE. I download HSE_DEMOAPP_S32K3XX_0_2_6_0 HSE_FW_S32K3XX_0_2_6_0, HSE_FW_S32K312_0_2_40_0. ENV: S32DS IDE 3.5, RTD 4.0.0, HSE_DEMOAPP_S32K3XX_0_2_6_0 HSE_FW_S32K3XX_0_2_6_0, HSE_FW_S32K312_0_2_40_0. I have some problem: from readme.pdf It says only trace32 is supported, how to use JLINK SWD to install HSE FW? at NXP website, I do not find  AN744810 “HSE FW install for S32K3xx” at secure files section. how to write HSE feature flag to UTEST at 0x1B000000? what is the usage of Demoapp? it is just for install HSE FW? If I want to use EB29 + IDE3.5+ RTD4.0 for application project how to use HSE module?  Re: HSE Firmware Install #Hello,@VaneB  I am working on the S32K3X4EVB-T172 board and trying to install the HSE firmware  The HSE firmware flashing is successful, but my application always stops at if (FALSE == checkHseFwFeatureFlagEnabled()) { /* Stuck here */ } So HSE FW initialization does not proceed. I checked the UTEST region (0x1B000080), and I am getting the value 0xffffffff please review out project and image and helps us proceed with this  Thank you  Re: HSE Firmware Install Hi @BigSun  The HSE FW installation steps are the same for all S32K3 variants. So the code for S32K344 can be ported to S32K312.  Regarding the UTEST sector, this is an OTP (One Time Programmable). This causes the erase operations not to be allowed. You can only append new data or configuration and read data. The process to write data in the UTEST Sector is the same process used to program data in other blocks. The unlocking process is also the same but with the difference that the UTEST sector has its own register PFCBLKU_SPELOCK[SLCK] to lock or unlock the sector from program operations. Unfortunately, as all the documentation of the HSE is under NDA (Non-Disclosure Agreement) the information is not public and we can not share it.  If you have never accessed the secure files follow the guide below. NXP SECURE ACCESS RIGHTS FIRST-TIME USER REGISTRATION GUIDE Re: HSE Firmware Install Hi, the S32K3_HSE_DemoExamples_1_0_0 mentioned above only support S32K344, but now I use S32K312 and need to debug with JLINK SWD. for the HSE FW install, I do not know how to write HSE feature flag with JLINK now. for HSE install manual is secure file , now I have no access permission. I have to ask questions in this community. Re: HSE Firmware Install Hi @BigSun  The available HSE examples are provided with the HSE Demo App for Lauterbach TRACE32 and S32K3 MCUs for General Purpose HSE Demo Examples for PEMicro. These packages offer different use-case scenarios and examples to showcase the capabilities of the HSE FW in various devices. The application note: HSE FW install for S32K3xx can be downloaded from S32K3 Microcontrollers for Automotive General Purpose and found in Documentation > Secure Files (under NDA (Non-Disclosure Agreement)). Also, you can find an S32K3xx HSE with RTD Training.  Additionally, refer to the available S32K3_M27x CRYPTO_43_HSE Driver examples provided with the RTDs, and the USER Manual and Integration manual that can be found in the file installed by the RTD.exe, for example, C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0_P12\eclipse\plugins\Crypto_43_HSE_TS_T40D34M40I0R0\doc. B.R. VaneB
View full article
lwip_freeRTOS_s32K344:版本配置问题报告:FreeRTOS 示例项目 问题:FreeRTOS 和 lwIP 示例项目编译失败,出现"致命错误:FreeRTOS.h:没有此类文件或目录" 平台:S32 Design Studio 3.6.2 目标:S32K344 (S32K3 Platform) 受影响项目: free_rtos、 lwip_freertos 示例应用程序 环境验证 已安装元器件(已确认): ✅ S32 Design Studio:版本 3.6.2 ✅ 平台 SDK S32K3:包括 FreeRTOS 和 lwIP TCP/IP 协议栈 ✅ FreeRTOS 源位置: 源代码 观察到版本错误: ../src/main.c:19:10: 致命错误:FreeRTOS.h:没有此类文件或目录 19 | #include"FreeRTOS.h" | ^~~~~~~~~~~~ 编译终止。 手动添加路径时的层叠错误 将 FreeRTOS 包含路径手动添加到版本设置中时: 初始 FreeRTOS.h 标头 出现新的错误 ,原因是缺少二级依赖关系: portmacro.h (ARM Cortex-M7 端口特定定义) FreeRTOS 示例的正确项目导入步骤是什么? Re: lwip_freeRTOS_s32k344 : Build Configuration Issue Report: FreeRTOS Example Projects 你好@Sachin05 你能否提供你安装的 RTD 版本和 FreeRTOS 代码包版本?此外,您能否分享一下导入示例的步骤?这将有助于我更好地了解您的设置,并确认是否有任何遗漏。 BR、VaneB Re: lwip_freeRTOS_s32k344 : Build Configuration Issue Report: FreeRTOS Example Projects 你好@VaneB RTS 版本 FreeRTOS 软件包版本 按照 S32 Design Studio 3.6.2 的标准恩智浦示例导入程序进行导入IDE: 已打开 S32 Design Studio 3.6.2 IDE 导航至控制面板 →"创建或导入项目" 已选定:"示例中的 S32DS 项目" 筛选/搜索参数: 类别:TCP/IP 堆栈(或中间件) 设备系列:S32K3X4 示例名称: lwip_freertos (或类似的变体,如 free_rtos_tcpip)。 从列表中选择示例 点击"完成" 导入工作区 在首次尝试版本之前,未对导入的项目进行任何自定义修改。 问候,萨钦
View full article
Ntag216のパスワード保護の削除 Ntag216 でパスワード保護を削除しようとしましたが、失敗しました。パスワードは次のように設定します。たとえば、パスワードは「abcd」、パックは「C5 C5」、書き込み保護のみ、 パスワード: A2:E5:61:62:63:64 パック: A2:E6:C5:C5:00:00 AUTHO セット: A2:E3:04:00:00:00 E4 を設定しませんでした。E4 バイトは次のとおりです。 00:05:00:00 パスワード保護を解除しようとしたとき、私は 1B:61:62:63:64 タグはこう返信しました: C5:C5 次に、次のコマンドで AUTHO ビットを設定しようとしました。 A2:E3:04:00:00:FF エラー: エラー: I/O障害 パスワード保護を解除するにはどうすればいいですか?正しいバイト値とコマンドと手順は何ですか? NTAG213_215_216 NFCフロントエンド・ソリューション Re: Removing password protection in Ntag216 こんにちは@mnhpias あなたの調子が良いといいのですが。 NTAG216 のテスト構成に使用しているソフトウェアは何ですか?確認ですが、AUTH0 を設定しようとした直後 (パスワード認証が成功) に「エラー: I/O 障害」がスローされますか? 空の NTAG で同じ手順をテストできる可能性はありますか?これは、手順に影響を与える可能性のある構成を排除しようとするものです。 よろしくお願いいたします。 エドゥアルド。 Re: Removing password protection in Ntag216 こんにちは、 ACCESS バイト内の PROT ビットを 1b に設定すると、パスワードで保護された読み取りおよび書き込みアクセスが定義されます。このバイトに 80h を書き込むと正常になります。 私の理解では、パスワードによる読み取り/書き込み保護を解除して、すぐにメモリにアクセスしようとしているということですが、これは正しいですか?パスワード認証が成功すると、パスワード保護を解除せずにメモリの読み取り/書き込みが可能になります。このアプローチを実現しようとしているのでしょうか? よろしくお願いいたします。 エドゥアルド。 Re: Removing password protection in Ntag216 親愛なる@EduardoZamora様、 私はNfc Tools Android アプリの NFC コマンド ツールを使用していましたが、これが問題になっている可能性があります。その後、Android アプリ (kotlin コード) で試してみましたが、問題なく動作し、これらのコマンドを使用してパスワード保護を削除できるようになりました。「I/O エラー」エラーは発生しません。 もう一つ質問があります。読み取り保護のために、次の操作を実行しました。 パスワード認証、1B:61:62:63:64 セットE3、A2:04:00:00:04 E4、A2:E4:80:05:00:00 を設定 これは機能し、ページ 04 からのすべてのページが読み取り保護されるようになりました。この手順は正しい手順ですか? 今は、読むためにこれをやっています: パスワード認証、1B:61:62:63:64 E3、A2:04:00:00:FF を設定 E4、A2:E4:00:05:00:00 を設定 読み取りおよび書き込み保護が削除されました。この後、タグから NDEF テキストを読み取ろうとすると、エラーが表示され、テキストは読み取られません。しかし、タグをもう一度タップして読むと、CAN読みます。 しかし、読み取りおよび書き込み保護を解除した後、カードを再度タップせずにすぐにタグを読み取るという永続的な操作が必要です。これをどうやって行うのでしょうか?
View full article
T1024 PCS 链路建立调试 当客户的以太网PCS无法连接时,本文将提供基于T1024的逐步调试指南。 许多以太网接口由 SerDes 配置,因此需要确认链路错误究竟是由 SerDes 还是由 PCS 本身引起的。本文将提供一些线索。 Serdes Lane&pins 首先检查您正在使用的是哪一条 SerDes 通道,并在《QorIQ T1024 参考手册》中确认对应的 SerDes 通道。如下面的配置,用户在 RCW[128:136] 中设置 SRDS_PRCTL_S1=0x05B,应用程序将利用 SGMII.m1 和 SGMII.m2。 本文将以SGMII.m1为用户案例,现在SGMII将在帧管理器MAC1中。 请检查 SerDes 通道分配以确认使用的是哪一条 SerDes 通道。以 SGMII.m1 为例,其对应的通道引脚名称为 SD1_TX3P/N 和 SD1_RX3P/N,可认为这是通道 3。 MAC 编号与 SerDes 通道编号无关,请查阅相应的表格以确定具体引脚。 任何使用此以太网的硬件测试都应与引脚相关,请参阅以下的元器件引脚编号。 您可以测试该通道的 RX 引脚眼图,以确认频率是否正确。如果您将该通道设置为 SGMII 1.25G,可以通过眼图确认信号速率是否配置正确。 上面的眼图仅显示SerDes的速度。 在环回测试看似正常时,这一点尤为重要,因为它可能仍然无法与其他设备正常连接。 如何确认 SerDes 链路已建立 请在《QorIQ T1024 参考手册》中查找对应的通道寄存器。 在本使用场景中采用的是通道 3,因此需要读取通道 3 的寄存器,以确认 SerDes 通道 3 是否正常运行。例如如下: # 3号通道 md.l 0xFFE0EA8C0 1 - aa611080 # LN3GCR0 md.l 0xFFE0EA8C4 1 - 101c4019 # LN3GCR1 md.l 0xFFE0EA8CC 1 - 00002800 # LN3SSCR0 md.l 0xFFE0EA8D0 1 - 0f0fc01f # LN3RECR0 md.l 0xFFE0EA8D4 1 - 0f0f0fa8 # LN3RECR1 md.l 0xFFE0EA8D8 1 - 00003006 # LN3TECR0 md.l 0xFFE0EA8E0 1 - 39000400 # LN3TTLCR0 md.l 0xFFE0EA8E4 1 - 00000000 # LN3TTLCR1 md.l 0xFFE0EA8F4 1 - 00000000 # LN3TCSR1 md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3 SerDes_LNnTCSR3 是一个重要的调试测试寄存器,CDR_LCK 用于检查 CDR 是否锁定。 CDR_LCK=0表示未检测到有效的比特流。作为测试,您可以将通道置于环回模式 LN2TCSR3[LPBK_EN]=01。CDR 应锁定在数字环回模式(内部环回)。否则,设备本身可能会出现问题。 所以,如果您能把 LPBK-EN 设置为“01”环回模式,它会在环回模式下将 SerDes 自身的 TX 和 RX 信号设置为排除外部信号,然后再检查 CDR_LCK,如果是 1,SerDes 本身就运行良好。总之,CDR_LCK 应该始终被置位。 在 “md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3” 的输出中,CDR_LCK=0,怀疑问题发生在 SerDes 端。 正常状态应为: => md fe0ea8fc 1 fe0ea8fc:08000000 如何确认 PCS 链路已建立 有关 MAC 和 PHY 寄存器的详细信息,请参阅《T1024DPAArm,QorIQ T1024 数据路径加速架构 (DPAA) 参考手册》 在DPAARM中找到偏移地址。 对于 SGMII,MAC 地址应为 offset+0x1000。 请按照《T1024DPAARM》中第 6.5.4 节“MDIO 以太网管理接口使用说明”的指示来读取 MDIO 寄存器。 在本应用场景中,接口为 SGMII1、MAC1,此时 MAC1 的地址为 FM1_mEMAC1:4E_0000,对应的 FM1_mEMAC1 MDIO 寄存器起始地址为 4E_1000h。 本例协议采用 SGMII,读取时应按照《T1024DPAARM》6.5.4.3 节“Clause 22 读取流程”的步骤执行。 6.5.4.3 第 22 条阅读流程 1) 等待 MDIO_CFG[BSY] = 0。 2) 用正确的 PHY_ADDR 和 REGISTER_ADDR 写入 MDIO_CTL,并设置第 16 位。 3) 等待 MDIO_CFG[BSY] = 0。 4) 如果寻址的 PHY 没有响应,则设置 MDIO_CFG[MDIO_RD_ER]。 否则读取 MDIO_DATA 值。 在本使用场景下,应读取 MDIO_SGMII_SR,您可以在《QorIQ T1024 参考手册》30.5.5 节 “1000Base-KX PCS MDIO 内存映射/寄存器定义”中查阅该寄存器的具体定义 关键位如下: 以下是本使用场景的结果: 读取 MDIO_SGMII_SR 时,请使用能够满足延迟时间要求的手动输入。 如果您无法手动输入,请按照流程进行操作,“等待 MDIO_CFG[BSY] = 0”再读取 MDIO_DATA 值。 读取SGMII1 MDIO寄存器 === Serdes 测试 1 === 0xFFE0EA8FC 值:0x08000000 转储 PCS0 寄存器 0xFFE4E1030-0xFFE4E103C: 0x40001408 0x00000000 0x00001340 0x00001340 选择 0x8002,devmem 0xFFE4E1034 32 0x8002 Read: 0x00000083 选择0x8003,devmem 0xFFE4E1034 32 0x8003 读取:0x0000E400 选择 0x8001,devmem 0xFFE4E1034 32 0x8001 Serdes0 状态:0x00000029 选择 0x8001 devmem 0xFFE4E1034 32 0x8001 Serdes0 状态:0x0000002D 选择 0x8001,devmem 0xFFE4E1034 32 0x8001 Serdes0 状态:0x0000002D 第一次没有链路,LINK_STAT 为 0(0x00000029),然后变为 1(0x0000002D)。 现在 PCS 链路已建立,硬件环回检查流程也已完成。
View full article
关于 MPC5777C DCF_UTEST_REE_TMPSNS 配置后 PMC_SELF_TEST 失败的查询 我正在使用 MPC5777C 芯片配置 UTEST 的 PMC 温度传感器 RESET 事件启用控制 DCF。我将 LDPLS 位设置为 1 以在 PMC_REE_TD 寄存器中加载 DCF 客户端数据,我将 TEMPSNS0 和 TEMPSNS2 都设置为 0 以禁用由温度传感器引起的 RESET 事件。 -> DCF 配置如下:dcf_utest_ree_tmpsns: ldpls(1), tmpsns2(0), tmpsns0(0) 在此状态下向 MPC5777C 供电时,PMC_SELF_TEST_UM_VD_REG 的 ST_RESULT 显示单片机自检失败。在配置 DCF 之前,结果总是 PASS,但在配置之后,记录为 Failed。这种行为因我们生产的板而异。 例如,在板 1 上,它总是在配置 DCF 之后失败,而在板 2 上,它总是在配置 DCF 之后通过(两个板始终在 DCF 配置之前通过)。 我的问题是 1.我想了解我配置的 DCF 中的 LDPLS、TEMPSNS0 和 TEMPSNS2 设置如何影响 PMC 自检操作和结果。具体而言,当温度传感器 RESET 事件被禁用时,自检有时会失败甚至通过,这是否正常? 2。如果我已经配置了 DCF,那么在启动顺序之后在应用程序区域重新配置 PMC 设置,然后再次执行自检是否正确? 我一直都很感谢你善意而有益的回复。
View full article
FEE(K3)データ処理に関する質問 こんにちはチーム S32K3のFEEデータ取り扱い情報についてお伺いしてもよろしいでしょうか? 1.FeeBlockSize = 10 B の場合、ヘッダーやその他のメタデータを追加した後に DataFlash に書き込まれる実際のサイズはどれくらいですか? 2. Fee_MainFunction を 1 回実行すると、いくつの単位のデータ (FlsPageSize 単位) が書き込まれますか?(HW 書き込み操作は、FlsPageSize で設定された値に基づいて実行されますか?) 書き込み操作は、デフォルトで 32 ビットに設定されている「仮想ページ サイズ」に基づいていると思います。したがって、サイズが 10 バイトの場合、32 バイトが書き込まれます。 Fee_MainFunction は実行されるたびに、32 バイト (仮想ページ サイズ) 単位で動作します。 これで理解できましたか? よろしくお願いします。 RTD 出典: 直接お客様 Re: Question about FEE(K3) Data handling こんにちは@Luke_Chun 、 1.FeeBlockSize = 10 B の場合、ヘッダーやその他のメタデータを追加した後に DataFlash に書き込まれる実際のサイズはどれくらいですか? => DataFlash に書き込まれるブロック n データの実際のサイズ: 実際のサイズ = n * FEE_VIRTUAL_PAGE_SIZE (ブロックサイズ < FEE_VIRTUAL_PAGE_SIZE)の場合 { 1 の場合 } それ以外 { if((ブロックサイズ % FEE_VIRTUAL_PAGE_SIZE) == 0U) { n = ブロックサイズ/FEE_VIRTUAL_PAGE_SIZE; } それ以外 { n = ブロックサイズ/FEE_VIRTUAL_PAGE_SIZE + 1; } } 例: FeeBlockSize = 10 バイト、FEE_VIRTUAL_PAGE_SIZE = 8 の場合 --> ドライバはデータを 2 回に分けて書き込みます。1 回目: 8 バイトのデータを書き込みます。2 回目: 残りの 2 バイトのデータ + 6 バイトのパディング データ (0xFF) を書き込みます。 FeeBlockSize = 10 バイト、FEE_VIRTUAL_PAGE_SIZE = 16 の場合 --> ドライバは 1 回でデータを書き込みます: 10 バイトのデータ + 6 バイトのパディング データ (0xFF) を書き込みます 2. Fee_MainFunction を 1 回実行すると、いくつの単位のデータ (FlsPageSize 単位) が書き込まれますか?(HW 書き込み操作は、FlsPageSize で設定された値に基づいて実行されますか?) => 私の答え: Mem_Acc レイヤー ( MemAcc_CalculateLengthTransfer 関数内)では、ブロック データの長さが計算され、JobInfo->LengthChunk に割り当てられます。 この変数は下位層で使用されます - Mem_INFLS (ユーザーが料金ブロック用に内部フラッシュを構成した場合)。Mem_INFLS レイヤーでは、Mem_43_INFLS_IPW_ComputeWriteLength 関数を介してオフセットとアドレスに基づいて長さが再度計算されます (フラッシュ メモリへの書き込み前)。 SO、長さの値はアドレスとブロックのサイズによって異なるため、状況に応じた正しい長さの値はありません。 よろしくお願いいたします。 ダン
View full article
i.MX 数据表中 NVCC 的含义 你好 我正在查看 i.MX 数据表,经常看到以 NVCC_* 开头的引脚名称。 能否请您解释一下 NVCC 代表什么? 此外,名称中包含 NVCC 的徽章有何意义? 感谢您的支持。 顺祝商祺! Re: Meaning of NVCC in i.MX Datasheet 您指的是哪种产品? NVCC 是"Nominal Voltage Common Collector" 的缩写,NVCC_* 引脚是为一组 I/O 焊盘(如 GPIO、UART、SPI 等)提供电压的电源引脚。 如 NVCC_SD 为 SD 卡接口引脚供电。 Re: Meaning of NVCC in i.MX Datasheet 你好,丽塔、 谢谢您的解释。我所指的产品是 i.MX93。 我知道 NVCC 代表标称电压共集电极,而 NVCC_* 引脚是为特定 I/O 组(如 GPIO、UART、SPI)提供电压的电源引脚。NVCC_SD 为 SD 卡接口供电的例子非常有用。 感谢您的支持。 致以最诚挚的问候, tkato Re: Meaning of NVCC in i.MX Datasheet 你好@tkato, 不客气。 如有任何疑问,您可以创建新的主题,与我们自由联系。 祝您有美好的一天 顺祝商祺! Rita
View full article
PN532 标签仿真 NFC 工具显示 NULL 所有数据 目前正在使用 PN532 (UM0701-02 ) 模块接口,通过基于 IRQ 状态模型的 SPI 通信与 STM32WL 微控制器连接。我将一步步解释我是如何处理状态机的 第 1 步: SPI 配置 - 时钟 2Mhz 和 8 位模式 第 2 步: 在启动 PN532 模块后,我发送了 SMA 配置,然后正在等待第一个 IRQ 的 ACK,之后我将等待第二个 IRQ 的 SMA 配置响应。我没有收到任何错误信息。请注意我使用的以下配置 pn532_packetbuffer[0] =pn532_command_samconfiguration; pn532_packetbuffer[1] = 0x01;// 正常模式; pn532_packetbuffer[2] = 0x14;// 超时 50ms * 20 = 1 秒 pn532_packetbuffer[3] = 0x01;// 使用 IRQ 引脚! 步骤 3:收到 SMA 配置回复后, 。 我已经开始发送 TgTarget 启动命令。对于这条命令,我只收到 ACK,当电话接近模块时,我才收到回复。 uint8_tcommand[] ={ pn532_command_tginitastarget、 5,// 模式:仅 PICC,仅被动 0x04, 0x00, // SENS_RES 0x00, 0x00, 0x00,// NFCID1 0x20, // SEL_RES 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,// FeliCaParams 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,// NFCID3t 0,//一般字节的长度 0//历史字节的长度 }; 如果(uidPtr != 0) {//如果设置了 uid,则将 3 个字节复制到 nfcid1 memcpy命令 + 4, uidPtr、 3); }} 这条命令也得到了成功的回复。 因此,现在我有了手机 NFC 信息,如 NFC 支持类 注:到此为止,我得到了正确的 IRQ Assert、ACK 和命令回复。 第 4 步: 响应后,我将开始发送 TgGetTarget 命令(0x86)。第一次,比如当我将手机靠近 PN532 时,得到的响应为 0x87,错误代码为 0x13。像 RF 版本一样。之后,我尝试了两种方法来恢复通信。最初的方法是发送 Inrelease 命令 0x52、0x00,然后获取 IRQ,并得到 53 和 0x00 的响应。然后再次发送 TgTartget Command Initi 命令,就像再次执行步骤 3 一样。请注意,在这之后的一段时间里,我得到了对 0x86 的正确回复。 现在我还有一个问题,在我发送 Inrelease 或 TgTarget 命令后,NFC Tools Mobile 显示的所有数据,如序列号和其他信息都显示为零。并展示 felica 技术。但使用的是 ISO1884A A 类卡枚举。 现在我想知道为什么会出现这种情况。如果我遗漏了任何序列。请尽快为我们提供指导。我们正处于项目收尾阶段。 已经有人向我推荐了表格,但我没有得到答复 互联标签解决方案 接触式智能卡读卡器芯片 HITAG读卡器IC 面向读卡器系统的MIFARE SAM NFC 控制器解决方案 NFC 前端解决方案 NFC读卡器库 Re: PN532 Tag emulation NFC Tools showing NULL all the data 请问谁能对此问题提供支持 Re: PN532 Tag emulation NFC Tools showing NULL all the data 我并不想存储任何数据。首先,我发送带有所需参数的 0x8C(TgInitAsTarget)命令,然后等待 0x8D 响应。我正确收到了 0x8D 响应。之后,我发送 TgGetData (0x86) 命令,希望收到状态为 0x00 的 0x87,但大多数时候收到的是状态为 0x13 的 0x87。出现这种情况时,我再次发送 TgInitAsTarget (0x8C) 命令,再次收到正确的 0x8D 响应。这次,当我发送 0x86 时,我收到了状态为 0x00 的 0x87 以及 APDU 数据。这种行为在摩托罗拉和 Realme 等较新的手机上运行正常,但在较旧的三星手机上,我总是在 0x86 之后收到状态为 0x13 的 0x87,即使在多次间隔之后也是如此。收到 0x8D 后,我尝试以不同的时间间隔发送 0x86,例如 1 毫秒、10 毫秒、20 毫秒、50 毫秒、80 毫秒、100 毫秒、120 毫秒和 140 毫秒,但在较旧的三星设备上我仍然收到 0x13。如有遗漏,请指教。还要注意一件事,如果我得到 0x87、0x13 我也尝试过轮询,那时我得到 0x29。 Re: PN532 Tag emulation NFC Tools showing NULL all the data 这是因为没有内存来存储数据。 请参阅应用笔记中的第 3.3.7.2 章 Re: PN532 Tag emulation NFC Tools showing NULL all the data 我们仍然面临这个问题,请任何人支持解决这个问题。我不知道我们会遇到什么问题。
View full article
使用 testpmd 的 DPDK LX2162A SoM 全部 TX 0 你好 我们目前正在开发一款由 SolidRun(ClearFog LX2162A LX2-Lite 开发平台)开发的基于 LX2162A SOM 的板,最终目标是让 Open vSwitch 与 DPDK 一起运行。软件方面,我们使用的是厂家提供的基于 Ubuntu 22.04(内核 5.15)或 Ubuntu 24.04(内核 6.6)的镜像。我们使用 nxp-qoriq/dpdk 编译了正确的内核版本。我们使用提供的 dynamic_dpl.sh 脚本使用该板提供的两个 25G 接口创建了一个 DPRC(我们还尝试了两个 10G 端口和 1G 端口,它们都有如下所述的相同问题)。 我们想使用 dpdk-testpmd 测试 DPDK 下的转发是否有效。我们用同一根电缆连接了两个 25G 端口,使它们直接相连。我们使用该命令进行了测试: dpdk-testpmd -l 0-3 -n 1 -- --portmask 0x3 --nb-cores=1 --txq=1 --rxq=1 --tx-first --auto-start 我们在装有英特尔网卡的 x86 系统上测试了相同的设置,使用相同的命令,我们看到数据包被正确转发。 然后,我们还尝试使用带有 dpni-dpni 参数的 dynamic_dpl.sh 脚本来创建两个直接连接的 dpni 对象,而不使用任何 dpmacs,但结果仍然一样。在尝试用 OVS 配置此设置时,我们无法与测试系统建立任何链接。使用带有内核驱动程序的 OVS 时,我们可以成功配置桥接器,但速度上限大约为 5 GBit/s 如果您能就此事提供任何指导,我们将不胜感激。
View full article
启用硬件加密引擎 你好,先生、 目前我正在使用恩智浦Layerscape 1046ARDB套件,在该套件中,我正在使用名为InnTel IPsec-MB的软件加密设备执行L2FWD-Crypto代码。此外,TLS 也与它并行运行,以进行密钥交换 现在,我想将我的代码移植到工具包中,目的是使用硬件加密引擎。下面是我提出的相关问题。 Q1) 如何启用套件中的硬件加密引擎? 我目前的命令是 meson 安装版本--crossfile config/Arm/arm64-dpaa-linux_gcc-denableDrivers=总线/dpaa、mempool/dpaa、crypto/dpaa_sec 但只有在 "驱动程序 "部分出现了 dma、raw、crypto dpaa,而在 "已启用驱动程序 "部分却没有出现。 如何解决? Q2) DPDK 早期版本中提供了 KNI,而新版本中却没有。那么,为此提供的替代方案是什么呢? Re: Enable Hardware Crypto Engine 你好 我已经在内核模块中启用了 CAAM。现在我遇到的问题是 : Q1) (最后几行输出dmesg | grep -i caam) 设备 caam-keygen 已注册 caam_jr 17300000.jr : 冲洗作业环 2 失败。 探测 17300000.jr 失败,错误 -5。 Q2) 对于 af-xdp,来自eno1端口的流量是这样处理的 sudo ethtool -L eno1 combined 2 # 添加一条流量规则,将指向端口 443 的 TCP 流量引导到 RX 队列 1 sudo ethtool -N eno1 flow-type tcp4 dst-port 443 action 1 ./dpdk_app ... --vdev="net_af_xdp0,iface=eno1,start_queue=1,queue_count=1"... nb_rx = rte_eth_rx_burst(portid、 0, pkts_burst, MAX_PKT_BURST); 在这里,我给出了数据传输的特定端口号。 请标明查询内容。 Re: Enable Hardware Crypto Engine 你好 问题 1) 启用硬件加密引擎:问题似乎出 在你的 meson 版本 命令上。要在 DPDK 中支持 DPAA 加密加速,您需要正确包含 DPAA 网络安全驱动程序。检查是否安装了所需的依赖项和正确的 Linux 头文件。命令中的语法看起来正确,但您可能需要确保版本环境具有所有必要的先决条件。 尝试在命令中添加 DPAA 高效密码学标准驱动程序的完整路径: ``` meson setup 版本 --crossfile config/Arm/arm64_dpaa_linux_gcc -Denable_drivers=总线/dpaa,mempool/dpaa,crypto/dpaa_sec ``` 如果你在启用的驱动程序部分仍然看不到它,请验证 DPAA 加密加速器已正确初始化您的内核以及所需的 DPDK 库已正确安装。 Q2) 关于 KNI(内核网卡接口)替代方案: 在较新的 DPDK 版本中,KNI 已被弃用和移除。推荐的替代方案是: 1. AF_XDP(地址系列 eXpress 数据路径)- 提供高性能数据包处理接口 2. AF_PACKET - 用于数据包处理的标准套接字接口 3. Virtio-user - 适用于用户空间网络应用程序 对于与 L2fwd-crypto 并行运行的 TLS 密钥交换的特定用例,AF_XDP 作为 KNI 替代品可能会提供最佳性能特征。   此致
View full article
NXP汽车以太网:10BASE-T1(S)基础知识(日文博客) 介绍 这次我们将解释 10Mbps 车载以太网 10BASE-T1(S) 的基础知识。 1. 背景 首先,我将解释10BASE-T1(S)标准诞生的背景。 到目前为止, CAN已广泛应用于高速工业和汽车网络。 另一方面,由于大容量通信的需求,Ethernet也开始被引入。 然而,两种方法的通信速度都是 ・CAN FD(0.5M~8Mbps) ・100BASE-T1 (100Mbps) 存在约10Mbps的差距。 CAN FD 速度不够快,而 100BASE-T1 以太网又太贵也太快了。 在许多应用场景中,100BASE-T1 性能过剩,因此需要以合理的成本获得良好的性能,而 10BASE-T1 正是针对这些领域而设计的。 与 10BASE-T1 类似,还有一种名为 CAN XL(10M 至 20Mbps)的新标准,可以覆盖 10Mbps 的范围。我们将在其他场合对此进行详细解释。 2. 10BASE-T1(L)和10BASE-T1(S) IEEE 802.3cg 规范为 10Mbps 范围提供了两种类型的以太网。PHY规范已定义。 10BASE-T1 L:工业 点对点 传输距离1000 m(L表示Long) 全双工通信 10BASE-T1 S :用于汽车 点对点 传输距离:一对一通信15米(S代表短距离) 半双工通信 * 选项:全双工通信 *选项:半双工通信,多点连接(总线连接,最多 8 个节点) 多点传输采用一对双绞线,传输距离为25米,短截线长度为10厘米。 可选:PLCA(物理层碰撞避免)。如果未实现 PLCA,则使用 CSMA/CD(载波感知/碰撞检测)。 未假定使用中继器(最初的 10BASE 假定使用四个中继器连接) 3. 10BASE-T1(S)的优势 兼容 100BASE-T1/1000BASE-T1 车载网络可以与以太网系统统一。 更简单的架构 无需协议转换 减少设计工时 降低 100BASE-T1/1000BASE-T1 的成本 允许使用廉价的电线和连接器 半双工模式,差动曼彻斯特编码 与全双工相比,功能更少/更简单(无需 PHY 控制、简化时钟恢复、无需链路控制、无需链路监视器、无需自动协商、无需 DFE/FFE(判决反馈均衡器/前馈均衡器)、无需基线漂移校正、无需 AGC(自动增益控制)、简化 ADC(模数转换器))。 多点配置 显著减少网络配置所需的交换机/PHY数量 PLCA 提供比 CSMA/CD 和 TDMA 更高效的冲突控制 → 低延迟 4. 10BASE-T1(S) 的用途 以下是一些 10BASE-T1(S) 适用于的车载应用示例。 写作 前大灯、尾灯、氛围灯、内饰灯的LED控制 前照灯中使用的矩阵式 LED 包含数万个 LED,使用传统的 CAN(最大 1Mbps)很难控制它们,但 10BASE-T1S 可以控制它们。 利用LED灯进行高分辨率符号显示和视频投影,照亮路面。 传感器 近距离声纳和各种环境传感器等 执行器 车门车窗、座椅电机等。 音频 扬声器和麦克风音频传输 以上只是一个例子,预计未来价格低廉且易于使用的 10BASE-T1(s) 将有各种各样的用途。 5-1. 主要特性:多点连接 10BASE-T1(S) 除了像 1000BASE-T1 和 100BASE-T1 一样支持菊花链连接外,还支持多点连接,这大大降低了网络配置成本。 如上图所示,即使节点数量相同,与菊花链相比,多点连接也能显著减少所需的以太网交换机和 PHY 的数量。 5-2. PLCA选项的主要特点 对于菊花链连接,由于是一对一链路,因此不存在数据冲突问题;但在多点连接配置中,多个节点共享总线,因此需要数据冲突预防机制。10BASE-T1(S) 也可以使用一种名为 PLCA 的冲突预防技术。 采用仲裁方法,利用PLCA(物理层冲突避免)来避免数据冲突。 由管理设备为每个已连接的设备分配唯一的节点 ID;并依次为各 PHY 授予传输机会。 节点 ID 可以赋值为 0 到 254。 如果未实施PLCA,则CSMA/CD PHY传输机会以轮询方式确定。 ID=0 的节点(被指定为主节点)在总线上发出 BEACON 信号。该 BEACON 信号标志着新一轮传输机会的开始。 当具有其他 ID 的节点收到信标时,它会等待自己的传输机会。 每个节点在发送数据包之前,都会在传输机会期间发送 COMMIT 信号。 每个节点只有在时隙与其自身 ID 匹配时才开始传输(如果 TO_TIMER 周期已过,节点也可以跳过传输机会)。 →与TDMA(时分多址)不同,它不会因为打包未使用的时隙而浪费时间。 COMMIT 请求会停止其他节点的定时器 (TO_TIMER),并让它们等待数据包。 这样,通过将每个节点的通信时间除以时间,就可以避免冲突。 6. 10BASE-T1(S) PHY 和 100BASE-T1/1000BASE-T1 的 比较 在OSI参考模型中的位置 IEEE 802.3cg 定义的 10BASE-T1(S) 对应于 OSI 参考模型的物理层 (PHY),就像 100BASE-T1 和 1000BASE-T1 一样。 从主机控制器通过MII接收的数据会发送到以太网线路。接收过程则相反。 *恩智浦提供主机控制器和10BASE-T1(S)兼容的PHY器件。 物理层模块 下图所示为 10BASE-T1(S) 的 PHY 模块。该配置与 100BASE-T1 和 1000BASE-T1 基本相同,即主机控制器通过 MII 输入的数据经 PCS 编码,PMA 转换为模拟信号,然后发送到传输路径。接收过程则相反。   PCS区块 PCS 与 100BASE-T1/1000BASE-T1 的主要区别在于,PCS 执行 PLCA 冲突控制。 此外,编码使用的是DME,而不是PMA。 DME(差分曼彻斯特编码) 10BASE-T1(S) 使用 DME 的主要原因是降低成本,其主要特点如下: 10Base-T1(S)的DME信号比100BASE-T1等使用的PAM信号成本更低。 由于DME内置时钟,其0和1电平之间的转换频率高于PAM,即使0和1连续出现,同步丢失的可能性也更小。这有助于降低产品成本。 PMA块 PMA模块执行D/A转换和校正控制。 从下面的框图可以看出,10BASE-T1(S) 中许多模块已被消除(或简化),这简化了设备设计并有助于降低成本。 电缆 使用 10BASE-T1(S) 可以采用价格低廉的以太网电缆。 10BASE-T1(S) 使用一对(两根电缆)非屏蔽双绞线 (UTP) 电缆。 (与 100BASE-T1/1000BASE-T1 以太网线相比,可以显著减轻重量并节省空间。) 到目前为止,我们已经解释了支持 10Mbps 范围的 10BASE-T1(S) 汽车以太网 PHY。 希望您能够理解我们是如何降低成本的,以及我们采取的各种措施。 参考信息 NXP 车载以太网网页 TJA1410,10BASE-T1S PMD 收发器网页 =========================​ 我们目前无法 回复 此帖子“ 评论”部分的评论。 对于由此造成的不便,我们深表歉意。如有任何疑问, 请 参考“ 如何就 技术问题 联系 NXP ( 日语 博客 ) ” 。 (如果您已经是 恩智浦的 分销商或 与 恩智浦 有业务往来 ,您可以直接咨询负责人。) 本页概述了车载以太网 10BASE-T1S 的基本知识。 汽车以太网 界面 日本博客
View full article
什么是电源? - 入门指南 - 第 5 部分:电源管理集成电路 (PMIC) 和单板计算机 (SBC)(日语博客) 在最后一期中,我们将探讨“PMIC ”和“ SBC”。 首先,关于PMIC 。 PMIC是电源管理集成电路的缩写,它是一种用于管理电源的集成电路( IC ) 。 通常,PMIC包含多个电源,例如线性稳压器和开关稳压器,并且还能够监控电源的异常情况,并在预定的时间打开和关闭每个电源。 安装的电源数量和类型各不相同;例如,处理器的 PMIC大约会安装 10 个电源。 下图 摘自 NXP.jp ,显示 PCA9452 配备 了 六个开关稳压器 ( BUCKx) 和五个线性稳压器 ( LDOx)。管理这些电源的功能 是“逻辑控制”。 另一方面,下图所示的PCA9420配备了两个开关稳压器( SWx )和两个线性稳压器( LDOx)。它比PCA9452小得多。   PMIC 的优势在于将多个电源及其管理功能集成到单个 IC 中,从而无需为每个电源设计单独的电路即可轻松管理电源。 还有一些 PMIC 是预先配置好的,可以针对特定处理器进行优化,因此只需连接其中一个 PMIC 即可操作处理器。 另请参阅这篇博客文章。 NXP “电源”概述页   接下来,我们来谈谈SBC 。 SBC代表系统基础芯片,指的是为系统提供基础的芯片(在本例中指的是集成电路) 。与电源管理集成电路 (PMIC) 类似,它具有多个电源,能够监控这些电源,并能够按预定时间开启和关闭电源。不同之处在于,它还内置了用于更大型系统控制的功能,例如通信收发器(如CAN收发器和LIN收发器)、看门狗定时器和复位控制。 同样,下图是NXP.jp提供的SBC FS23图的复制品。 除了一个开关稳压器(HVBUCK )和两个线性稳压器( HVLDOx)之外,它还具有一个 CAN FD 收发器、一个 LIN 收发器和一个看门狗定时器。   单板计算机 (SBC) 的优势在于它比电源管理集成电路 (PMIC) 具备更广泛的功能。这意味着您只需在电路板上放置一个 SBC 即可实现所需的系统,而无需像使用 PMIC 那样在电路板上排列许多单独的集成电路。 上文我们已经解释了电源管理集成电路(PMIC)和单板计算机(SBC)的优势。请选择最适合您应用场景的器件。 到目前为止,我们已经用五篇文章讲解了电源的相关知识。为了方便初学者理解,我们着重介绍了电源的工作原理,而省略了详细的操作原理和公式。 如果您想了解更多详情,请尝试使用描述中的关键词进行搜索。 以往的文章可从NXP “电源”摘要页面(日语博客)访问,请查看。 ========================= 我们目前无法回复此帖子“评论”部分的评论。 对于由此造成的不便,我们深表歉意。如有任何疑问,请参阅“ NXP技术问题-如何联系我们(日语博客) ”。 (如果您已经是恩智浦的分销商或与恩智浦有合作关系,您可以直接询问负责人。) 如果您想知道“什么是电源?”,本页总结了您需要了解的第一件事。 在第五部分中,我们将解释 PMIC(电源管理集成电路)和 SBC(系统基础芯片)。 (阅读时间:5分钟) 采购和市场营销中心 日本博客
View full article
在 SDK_25_06_00_RD-RW612-BGA 中失败 亲爱的先生们 我有一个 RD-RW612-BGA 板:IPA-2A/1A V3。 而且,如果我使用最初的软件开发工具包,即 SDK_2_13_3_RD-RW612-BGA,其固件位于 components/conn_fwloader/fw_bin 元器件中。 如果我使用 rw61x_sb_wifi_a1.bin 或 rw61x_sb_ble_a1.bin,SDK 2.13.3 中的 wifi 示例可以正常工作。如果我使用 rw61x_sb_wifi_a2.bin/rw61x_sb_ble_a2.bin,使用 FW 运行的示例将无法下载。 现在,我们想改用最新的 SDK,但发现 SDK 25.06 没有 rw61x_sb_xxxx_a1.bin,只有 rw61x_sb_xxxx_a2.bin。当然,SDK的版本还可以,但是下载固件时一切都失败了。 请告诉我在哪里可以找到 SDK 25.06 中的相关 rw61x_sb_xxxx_a1.bin,就像我们在 SDK 2.13.3 中做的那样。 此致, /ckhsu 产品:WiFi RW6XX 协议:BLE -> 连接性 Re: Fail in SDK_25_06_00_RD-RW612-BGA 您好, 问题是 RW612ET/A1IK 已经停产。这意味着它不再受支持。 如果您不想使用 FRDM-RW612。您可以使用我们合作伙伴的另一个板。 此致, 丹尼尔 Re: Fail in SDK_25_06_00_RD-RW612-BGA 您好, 我想答案意味着我拥有的 V3 板只能使用旧的 SDK,无法使用另一个最新的 SDK。是否正确? 此致, /ckhsu Re: Fail in SDK_25_06_00_RD-RW612-BGA 您好, 推荐的 RW612 开发板是 FRDM-RW612。我建议你看一看。 关于您的问题,您使用的是 A1 版本,这是一个旧的 SoC 版本。看起来 RD-RW612-BGA 板的 V3 版本仍在使用这个变体。V4 使用 A2 SoC 变体(与 FRDM 板相同)。最新的 SDK 版本仅包含 A2 版本。你需要升级板才能使用最新的固件。 此致, 丹尼尔
View full article