Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Technical Feasibility Assessment: Supporting 32-bit Applications and 32-bit Qt GUI on i.MX8M Plu Hi NXP Technical Support Team, [Project Background] We are developing a production project based on the i.MX8M Plus platform. Our current software stack is: - Target SoC: i.MX8M Plus (Cortex-A53, ARMv8-A 64-bit) - BSP / Yocto Version: Yocto Project 5.0 (Scarthgap) / meta-imx - Linux Kernel: 6.6 (AArch64) [Customer Requirement] Our end-customer has raised a new requirement: they need to run both 32-bit Linux applications and 32-bit Qt GUI applications on this 64-bit Linux OS environment (due to legacy 32-bit dependencies/codebase from older platforms). To evaluate whether this requirement is commercially and technically feasible, could you please clarify NXP's official stance on the following points: 1. Feasibility of 32-bit Applications & 32-bit Qt: Does NXP officially support running 32-bit user-space applications—specifically 32-bit Qt GUI applications—on a 64-bit i.MX8M Plus kernel via Yocto Multilib or any other official mechanism? 2. Availability of 32-bit Hardware Acceleration & Qt Libraries: If this is feasible: a) Does NXP provide 32-bit user-space GPU acceleration binaries (e.g., a 32-bit version of `imx-gpu-viv` for EGL/GLES) and VPU binaries compatible with i.MX8M Plus on a 64-bit kernel? b) Does NXP provide official Yocto recipes, BSP support, or validated configurations for building a 32-bit Qt stack (`lib32-qtbase`, `lib32-qtdeclarative`, etc.) on the i.MX8 family? 3. Performance & Rendering Limitations (If Acceleration is Absent): If 32-bit proprietary GPU drivers are NOT provided for i.MX8M Plus, is running a 32-bit Qt GUI via software rendering (e.g., LinuxFB, software Mesa/llvmpipe) officially recommended or considered production-ready by NXP for commercial products? 4. Official Recommendation / Solution: If running hardware-accelerated 32-bit Qt on i.MX8M Plus is not supported, what is NXP's official statement and recommended architectural solution for customers migrating legacy 32-bit applications/Qt to the i.MX8M Plus platform? A formal statement from NXP will serve as our official engineering and architectural baseline for the customer. Looking forward to your reply! Thanks and regards i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux Yocto Project Re: Technical Feasibility Assessment: Supporting 32-bit Applications and 32-bit Qt GUI on i.MX8M Plu Hi, Thank you very much for the prompt and clear explanation! This fully clarifies the architectural boundaries of the i.MX 8M Plus BSP regarding 32-bit user-space components and GPU/multimedia acceleration. We will follow NXP's official recommendation and push forward with the native AArch64 deployment for our customer's Qt and application stack. Thanks again for your support! I have marked your reply as the accepted solution. Best regards, Re: Technical Feasibility Assessment: Supporting 32-bit Applications and 32-bit Qt GUI on i.MX8M Plu Hi @DADAXIN  Our BSP for the I.mx8mp is a 64-bit version. It is compiled and tested exclusively for AArch64, covering components such as the Vivante GPU user-space libraries (EGL/OpenGL ES/Vulkan), the VPU, and Qt 6 (provided via meta-qt6). Using 32-bit Qt with hardware acceleration on the i.MX 8M Plus falls outside the scope of the BSP release and is not a supported configuration. Our recommended approach is to recompile it as a native AArch64 applications/Qt. If a 32-bit solution is a hard requirement, please contact our Professional Services following below link: https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT B.R
View full article
i.MX RT1176: GPTの最大周波数 GPTの最大周波数 #RT1176 を知りたいです。GPTのキャプチャ機能を使って信号の周波数を測定したいと思っています。これまではMCUを使っていましたが、タイマーの最大周波数STM32H7 240MHzで、低く感じます。だから高い周波数タイマーを持つMCUが欲しいです。しかしRT1170のデータシートにはGPTの導入がありません。 Re: i.MX RT1176: Maximum frequency of the GPT @长亭様 i.MX RT1176にご関心をお寄せいただきありがとうございます。 GPTの最大動作クロック周波数は240 MHzで、この情報は i.MX RT1170リファレンスマニュアルで確認できます: よろしくお願いします、 シェリー
View full article
ペリフェラル Toolでのedma4エラーメッセージがSD 26 09 00以降に発生しています 皆様、 SDK 26.06.00以降、ペリフェラル Toolを使ってDMA周辺機器を追加しており、完璧に動作し、今も問題ありません。しかし、SDK 26.09.00以降はペリフェラル Toolでエラーメッセージが表示されます: 問題点:EDMAドライバはツールチェーン/IDEsプロジェクトに存在しません。プロジェクトはコンパイルできません! レベル:誤差 タイプ:検証 ツール:ツールチェーン/IDEプロジェクト 起源:ペリフェラル 対象:ツールチェーン/IDEプロジェクト:cm33_core0 リソース: platform.drivers.edma4 私はEDMAコンポーネントを直接使用していません。私はlpspi_edmaコンポーネントを使用していますが、私の記憶が正しければ、これにはedmaコンポーネントも含まれています。 私の主な質問は、lpspi_edma 2.1.4 を使用することです。SPI設定でDMAを実装するのは最新の方法でしょうか(私のSDKウィザードでは2.10.14がEDMAとして、バージョン2.10.13も同様です)?確かに、プロジェクトは問題なくコンパイルされ、実行されます。 私の.mex言う: Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2421543" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>親愛なるセレステへ、</P><P>はい、MCXN947を使用しています。</P></DIV></DIV></LINGO-BODY><LINGO-SUB id="lingo-sub-2421536" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</LINGO-SUB><LINGO-BODY id="lingo-body-2421536" slang="en-US" mode="CREATE"><P>こんにちは、 <A href="<A href="<A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A>" target="_blank"><A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A></A>" target="_blank">@PAChristiaans さん</A>、</P> <P>投稿ありがとうございます。</P> <P>質問に答える前に、MCXN947を使っているかどうか確認していただけますか?</P> <P>BR</P> <P>セレステ</P></LINGO-BODY><lingo-sub id="lingo-sub-2422493" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2422493" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、 <A href="<A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A>" target="_blank">@PAChristiaans さん</A>、</P> <P>ご辛抱いただきありがとうございます。こちら側でいくつかテストを行ったところ、同様の問題を再現することができました。</P> <P>テストによると、SDKに提供されているドライバーバージョンは正しいです。この問題は、設定ツールペリフェラルツールのeDMAコンポーネント検証に関連しているようです。この件は、さらなる調査のために設定ツールチームにエスカレーションします。</P> <P>最新情報があれば随時お知らせします。</P> <P>BR</P> <P>セレステ</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423302" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2423302" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、 <A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank">@PAChristiaans さん</A>、</P> <P>理由が分かった。新しいSDK 26.09にはplatform.drivers.edma4ドライバが含まれていません。これは、ソフトウェアチームがコンポーネント名を <STRONG>platform.drivers.edma_unified</STRONG>に変更したためです。MCXN947はedma4ドライバが搭載されている古いSDKsでサポートされていたため、古いSDKsとの後方互換性があるため、すべてのオプションを提供しています。プロジェクトに使っているドライバを正確に選ぶべきです。</P> <P>下の画像をご覧ください。</P> <P><SPAN class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1792751388672.png" style="width: 400px;"><span class="lia-inline-image-display-wrapper" image-alt="Celeste_Liu_0-1792751388672.png" style="width: 400px;"><img src="<A href="https://community.nxp.com/t5/image/serverpage/image-id/398421iB582FD0BF6C76349/image-size/medium?v=v2&px=400" target="_blank">https://community.nxp.com/t5/image/serverpage/image-id/398421iB582FD0BF6C76349/image-size/medium?v=v2&px=400</A>" role="button" title="Celeste_Liu_0-1792751388672.png" alt="Celeste_Liu_0-1792751388672.png" /></span></SPAN></P> <BR /> <P>ツールチェーンプロジェクトのフィルターを選択すると、正しいドライバのみが提示されます:</P> <P><SPAN class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1792751421202.png" style="width: 400px;"><span class="lia-inline-image-display-wrapper" image-alt="Celeste_Liu_1-1792751421202.png" style="width: 400px;"><img src="<A href="https://community.nxp.com/t5/image/serverpage/image-id/398422i03C5C91ED1058759/image-size/medium?v=v2&px=400" target="_blank">https://community.nxp.com/t5/image/serverpage/image-id/398422i03C5C91ED1058759/image-size/medium?v=v2&px=400</A>" role="button" title="Celeste_Liu_1-1792751421202.png" alt="Celeste_Liu_1-1792751421202.png" /></span></SPAN></P> <P>お役に立てば幸いです。</P> <P>BR</P> <P>セレステ</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423396" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2423396" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、セレステさん。</P><P>ご回答いただき、誠にありがとうございます。<BR />私はMCUXpresso 25.6とSDK 26 09 00 FRDM MCXN947を使っていますが、クライアント上では少し見た目が異なります。<BR />実際のfsl_edma.cを見てみるとドライバーファイルは正しいと思いますが、なぜかUIが違って見えます。<BR />繰り返しますが、プロジェクトのコンパイル自体には問題は発生していませんが、エラーメッセージが表示されます。安全に無視してもいいのでしょうか?</P><P>敬具</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423678" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool こんにちは、 @PAChristiaans さん、 はい。スクリーンショットを見る限り、これはエラーではなく警告のようなので無視しても大丈夫です。 UIの違いについては、統合されているMCUXpresso Config Toolsのバージョンが異なることが原因である可能性があります。私はバージョン26.09を使用しています。 アップデートについては、MCUXpresso IDEリンク内の「設定ツールの更新 」を参照してください。もちろん、現在のバージョンが問題なく動作しているなら、更新しなくても使い続けることもできます。 お役に立てば幸いです。 BR セレステ
View full article
RW612 WPA2-Enterprise再認証 – PTKインストール前のEAPOL TX完了 こんにちは、 Zephyr 4.3とHostap/wpa_supplicantを使用したRW612ベースの製品上でWPA2-Enterprise / IEEE 802.1Xを実装しています。 初期認証はPEAP/MSCHAPv2およびEAP-TLSの両方で正しく動作します。EAP-TLSは、PSA/ELSで保護された非エクスポート型の秘密鍵でも動作します。 特にWi-Fiのインプレース再認証時に問題が発生することが確認されています。 観測されたシーケンス: RADIUS アクセス-受け入れ → EAPの成功 → 4ウェイハンドシェイク → APがメッセージ3を再送信します → Wi-Fi接続が途絶えました →デバイスは再接続し、再び認証に成功します 現在の証拠は、最終的なEAPOL-Key応答の送信と新しいPTKの設置の間に順序の問題の可能性を示唆しています。 PTKの更新処理は、最終的なEAPOLフレームが送信待ちの状態であっても、続行できるようです。 私たちは、以下のことを保証するサポートされたメカニズムを見つけようとしました。 最終的なEAPOLキーフレーム送信が完了しました 前に 新しいPTKのインストール しかし、RW612のWi-Fiドライバ/ファームウェアパス内でEAPOL TX完了コールバック、TXキュードレイン/フェンス、または同等のAPIは見つかりませんでした。 診断実験としてのみ、PTKのインストール前に100ミリ秒の遅延を追加することで、PEAPおよびEAP-TLSの再認証試行が複数回、中断なく完了することができました。固定遅延は、生産上の解決策とは考えていません。 もう少し詳しく教えていただけますか: ファームウェアによってEAPOLデータフレームが実際に送信されたかどうかを知るための、サポートされているAPIはありますか? - PTKを更新する前に使うべきテキストラキューのフラッシュ/ドレインやキーインストールフェンスはありますか? - これはRW612のWi-Fiドライバ/ファームウェアにおける既知の制限や既知の問題ですか? - この問題に対応する新しいドライバやWi-Fiファームウェアはありますか? テスト済みバージョン: RW612ドライバ:v1.3.r52.z_up.p11 Wi-Fiファームウェア:18.99.6.p47 必要に応じて詳細なトレースやベンダー発行パッケージをご提供いたします。 ありがとう。RW612 Re: RW612 WPA2-Enterprise reauthentication – EAPOL TX completion before PTK installation こんにちは、 @sukrusinan さん。お元気でお過ごしでしょうか。 あなたのセットアップやケースシナリオをよりよく理解するために、以下の情報を共有していただけませんか? あなたのアプリケーションで使われているベース例を共有してください。Zephyr Wi-FiのShellですか? この設定は以前、このままの状態で正常に動作したことがありますか?もし実装されているなら、どのような変更が施されたのか教えていただけますか? 認証が失敗した場合の端末ログを提供します。 RADIUSサーバーとして何を使用していますか? どのAPモデルを使っていますか? Zephyrの最新バージョン(4.4.2)でこの動作を再現できますか? ご要望の情報をお知らせください。 Re: RW612 WPA2-Enterprise reauthentication – EAPOL TX completion before PTK installation こんにちは、 @RomanVR さん。 ご返信ありがとうございます。 ご依頼いただいた情報は下記に記載しております。 1. 基本適用 これはNXP RW612ベースのデバイス向けにカスタムされたZephyrアプリケーションです。 これはZephyr Wi-Fi Shellのサンプルに直接基づいているわけではありません。使用するもの: 標準的なZephyr Wi-FiマネジメントAPI Hostap/wpa_supplicant NXP RW612 Wi-Fiドライバ 標準のWi-Fiシェルとwpa_cliは、診断目的でのみ有効になっています。 2. この設定は以前にも正常に機能したことがありますか? 初期のWPA2-エンタープライズ認証は以下の両方で正しく動作します: PEAP/MSCHAPv2 EAP-TLS 再起動して再接続するのも有効です。 問題は具体的にはWi-Fiのインプレース再認証にあります。現在の設定では、シームレスなインプレース再認証が安定して動作していません。 失敗したCASE: initial authentication succeeds -> RADIUS Access-Accept -> EAP succeeds -> in-place reauthentication is triggered -> Wi-Fi link is lost -> IPv4 is removed -> device reconnects automatically -> authentication and connectivity recover 再認証中にネットワーク接続が中断されたため、これは失敗と判断します。 この問題は、PEAP/MSCHAPv2とEAP-TLSの両方で再現されています。 3. ターミナルログ 添付ファイルは、以下の端末のデータを匿名化したものです。 PEAP/MSCHAPv2再認証失敗 EAP-TLS再認証失敗 キャプチャされたデータには、認証情報、鍵、内部アドレス、SSID、MACアドレス、またはプライベート証明書情報は含まれていません。 現在のログレベルでは、フレームごとのEAPOL送信完了時刻や詳細なPTKインストールタイミングは利用できません。 4. RADIUSサーバー Ubuntu上で動作するFreeRADIUS。 5. アクセスポイント WPA2-Enterprise を使用する Ubiquiti UniFi U6 Pro。 6. Zephyr 4.4.2 Zephyr 4.4.2でのハードウェアテストはまだ実施していません。 公式v4.4.2ソースの独立したチェックアウトを作成しました。しかし、現在の統合にはバージョンピン留めのZephyr/Hostapアダプターが含まれており、これらのパッチは4.4.2にはクリーンに適用されません。 したがって、変更のみ ZEPHYR_BASEは 有効な比較にはなりません。統合はまず4.4.2 HostapおよびNXP HALリビジョンに移植されなければ、意味のあるハードウェアA/Bテストを行うことはできません。 この調査の正確な結果を記載した短いメモを添付いたしました。 現在テスト済みのバージョン: Zephyr: 4.3.0 based Hostap: 2.11 NXP Wi-Fi driver: v1.3.r52.z_up.p11 Wi-Fi firmware: 18.99.6.p47 また、以下の点についてもご助言いただければ幸いです。 RW612のWi-Fiドライバ/ファームウェアは、EAPOL-Keyフレームの送信を次のPTK/キー更新前に完了させることを保証するサポートメカニズムを提供していますか? 特に、サポートされている機能はありますか? EAPOL/データTX完了コールバック、 TXキューのドレインまたはフラッシュ、 ファームウェア同期/フェンス、 あるいは、ドキュメント化されたキー更新順序保証はありますか? このような仕組みがすでにRW612スタックに存在しているのか、それともこの動作にドライバやファームウェアの修正が必要なのかを判断しようとしています。 添付のログは、EAP認証が成功した後のリンク中断のみを示しています。それだけでは内部ファームウェアの根本原因を特定するものではありません。 よろしくお願いいたします。 Re: RW612 WPA2-Enterprise reauthentication – EAPOL TX completion before PTK installation こんにちは、 @sukrusinan さん。追加情報を共有していただきありがとうございます。 提供された情報は、その行動が発生する状況を理解するのに役立ちます。アプリケーションは完全にカスタムなので、問題のデバッグや分析が複雑になります。したがって、この動作がより簡単な例で再現可能かどうか、またどのように行うかをご確認いただけると、私たちの側で再現できるよう助かります。 さらに、根本原因を絞り込むために、同じRW612アプリケーションが別のアクセスポイントでも報告された挙動を再現しているかどうか、確認していただけますか? さらに調査するために、可能であれば以下のログを共有していただけませんか: AP(Ubiquiti)のログには、再認証と4ウェイハンドシェイクのやり取りが記録されている。 スニファによる通信失敗の試みを、無線経由で独自にキャプチャした。 この情報は、RW612スタックのEAPOL TX補完動作やキー更新順序付けの動作をさらに評価すべきかどうかを判断するのに役立ちます。 Re: RW612 WPA2-Enterprise reauthentication – EAPOL TX completion before PTK installation こんにちは、 ご提案ありがとうございます。いくつかの進展があり、同じRW612ハードウェア上で最小限のZephyr PEAP/MSCHAPv2アプリケーションで問題を再現できるようになりましたが、関連のない製品サービスは削除されています。 私たちの体制: Zephyr 4.3.0/ Hostap 2.11 NXP Wi-Fiドライバ v1.3.r52.z_up.p11 無線ファームウェア 18.99.6.p47 UniFi U6 Pro / FreeRADIUS 初期PEAP認証は正しく動作し、RADIUSアクセス承認、DHCP、pingも含まれます。しかし、インプレース再認証は再度アクセス承認を受け取り、その後Wi-Fiリンクを切断して最終的に再接続します。 EAPOL鍵の送信とペアワイズ鍵のインストールとの間のタイミングについて調査した。最小限のアプリケーションを用いて、再認証前から連続ICMP監視(250ミリ秒間隔)を伴ったA/B/A/Bテストを実施しました。 設定 Ping応答 リンクの中断 0ミリ秒の遅延、試行1回目 131/288 27.844秒 100ミリ秒の遅延、試行1回目 288/288 観察されなかった 0ミリ秒の遅延、2回目の試行 159/288 27.840秒 100ミリ秒の遅延、2回目の試行 288/288 観察されなかった 100ミリ秒の遅延は、後続のペアワイズキーインストール要求の前に導入されました。これはタイミングに敏感な相互作用を示唆しているが、固定遅延は適切な解決策とは考えていない。 また、以前に発生したEAP-TLS再認証失敗時のUniFi AP側のEAPOLログと、独立したOTAキャプチャも収集しました。OTAキャプチャでは、ステーションからAPにM4が送信されたことが示されています(キー情報0x030a、リプレイカウンタ4)。しかし、APが受信したか受け入れたか確認できず、スニッファーのAP側のカバレッジも不完全です。 新しいr54ドライバとそれに対応するファームウェアを調べましたが、現在HostapのスケジュールスキャンやROC/クッキーAPIの互換性の問題でポートがブロックされており、ハードウェアでのテストはまだしていません。 いくつかポイントを明確にしていただけますか? 新しいペアワイズキーをインストールする前に、EAPOLキーの送信が完了していることを確認するためのサポートされているメカニズムはありますか? 現在のドライバやファームウェアのバージョンで、既知の再認証やキー更新の問題はありますか? どのRW612ドライバ、ファームウェア、Zephyr/Hostapの組み合わせをおすすめしますか?この不具合を修正するアップデート版やパッチはありますか? EAPOL TXの完了とキーのインストール状況を確認するためのファームウェアのトレースやコールバックはありますか? 別のアクセスポイントベンダーとのテストはまだ実施中です。 最小限のアプリケーションテスト結果、AP側のEAPOL要約、RADIUSイベント情報、独立したOTAキャプチャ結果を含むZIPファイルを添付しました。キャプチャデータとAPログは、READMEに記載されているとおり、別々のテストセッションから取得したものです。 必要に応じて、最小限の再生ソースや生のキャプチャもプライベートで共有可能です。 私たちの主な目標は、シームレスなWi-Fi再認証を実現するための確実な解決策を見つけることです。 Re: RW612 WPA2-Enterprise reauthentication – EAPOL TX completion before PTK installation こんにちは、 @sukrusinan さん。返信が遅くなり申し訳ありません。 ログを共有してくださりありがとうございます。確認した上で、認証失敗の根本原因を特定するために以下のポイントが必要です。 別のAPでテスト: これにより、再認証失敗が別のAPで再現可能かどうかを判断でき、監視された動作を分離するのに役立ちます。 PEAP障害時の同期OTAキャプチャ: 共有されたOTAの抜粋は別のEAP-TLSセッションからのもので、PEAP APログとは関連付けられません。これは、APがM4を拒否している理由が、M4がAPにとって無効なフォーマットであるかどうかを分析するのに役立ちます。 最小限の再現: 最小限のZephyrアプリケーションでこの挙動を再現する手順を教えていただけますか?これは、こちら側で再現を試みる際に役立つでしょう。 ご質問について: 最新のZephyrバージョンで作業し、下流リポジトリ(リンク追加)でZephyrメインリポジトリにはないバグ修正をテストすることが推奨されます。 ソフトウェアの仕組みに関しては、この挙動が別のAPでも存在するかを判断する必要があります。したがって、別のAPベンダーでテストを実行することは可能ですが、STA側の状況をより詳細に把握するために、以下のデバッグログを有効にしてみてください。 CONFIG_WIFI_NM_WPA_SUPPLICANT_LOG_LEVEL_DBG CONFIG_WIFI_NM_WPA_SUPPLICANT_DEBUG_LEVEL ご依頼いただいた検査結果についてお知らせください。
View full article
需要帮助解决 imx95lpd5evk 启动问题 我刚拿到一块imx95lpd5evk主板,它无法启动,请问如何才能启动? 目前的设置是,我将启动开关 SW7 设置为 0010,以便从 eMMC 启动。 我已将 IMX-MIPI-HDMI 板连接到 Mini SAS 连接器 J14,并通过 HDMI 线连接到监测。 当我将 USB-C 调试线连接到我的电脑时,电脑甚至都检测不到它,设备管理器中甚至没有显示未知设备。 现在我打开板,本以为屏幕上会像快速入门指南里说的那样出现企鹅,但我却没有看到任何企鹅。屏幕只有黑色。开机后我只看到风扇转了,仅此而已。 我有个疑问,即使imx95宕机,调试功能是否也应该正常工作?因为我怀疑我的工作笔记本电脑的USB接口是否被禁用,这才是导致问题的原因。 我这块板上的eMMC芯片是不是空的?因为企鹅并没有如期而至。 请问有人能指导我接下来该怎么做吗? Re: Need help on imx95lpd5evk booting 实际上这是我的失误,现在已经解决了,主板正在启动。 感谢你的回复 Re: Need help on imx95lpd5evk booting 你好, 请您提供一下交换机(SW7)的图片,并按照“连接USB调试线”章节中的步骤操作,然后分享终端的输出结果。
View full article
Need help on imx95lpd5evk booting i just got the imx95lpd5evk board, it is not booting, help to make it boot the current set up is i have kept the boot switch SW7 as 0010 for booting from emmc i have connected a imx-mipi-hdmi board to the mini sas connector J14, and an hdmi to a monitor. when i connect a usb c debug cable to my pc, it is not even detecting, like i am not even getting unknown device in the device manager. and now i turn on the board expecting to get the penguins on the screen, as the quick start guide says, but i am not getting any penguins. The display is black only. after turning on i am seeing the fan getting on thats all. and i have a doubt is the debug supposed to work even when the imx95 is down? because i have doubt if the usb of my work laptop is disabled, which is causing the issue. is the emmc given in my board empty by any chance? because the penguins are not coming as expected. can someone guide me on how to move forward. Re: Need help on imx95lpd5evk booting actually it was some mistake on my part, and it is resolved, the board is booting now. Thank you for your reply Re: Need help on imx95lpd5evk booting Hello, Could you please share a picture of your switch (SW7), and follow the steps of chapter Connect USB debug cable, and share the output of the terminal. 
View full article
S32K3 AES Key Provisioning after ADKP protection Hello Team, We have enabled SHE Based Secure Boot on S32K platform. Also we are protecting JTAG interface by programming ADKP password and Advancing Life Cycle to OEM.  May i know if I can re-provision AES keys (Key Catlog is already aligned for AES keys) to device with ADKP protection enabled with Life Cycle in OEM.  Or do we need to set Life Cycle to IN_FIELD? Also, do Specify what should be the OWNER type for KEY to be updated? Thank You, Bhushan Re: S32K3 AES Key Provisioning after ADKP protection Hi @Bhushan1312  The keys can be updated also in OEM_PROD or in IN_FIELD life cycle but it depends on user rights, Host Identity (HID) and key owner. In HSE firmware reference manual rev. 2.8, see please: Table 42. Key group owners 6.2.3.2  Key Selection This section is important: “• If the host is granted with Super User (SU) rights, the owner of the target key handle must match the host identity (HID) (see Execution Rights (Super User vs. User)) If the host has User rights, the owner of the target key handle must be HSE_KEY_OWNER_CUST if LC is CUST_DEL, or HSE_KEY_OWNER_OEM if LC is OEM_PROD” Then there are tables 47, 48 and 49 which explain if authentication and encryption is needed based on user rights when importing a key to empty slot or when updating a key. For example, if you elevate to super user rights using authorization key owned by CUST, you can import or update CUST keys also in OEM_PROD. But you can’t import keys owned by OEM before the life cycle is advanced to OEM_PROD. That’s because you don’t have OEM authorization key yet. Regards, Lukas
View full article
i.MX RT1176:GPT 的最大频率 我想知道RT1176的GPT最大频率。我想使用GPT的捕获功能来测量信号频率。之前我用的是STM32H7单片机,但它的定时器最大频率只有240MHz,我觉得太低了。所以我需要一个定时器频率更高的单片机。但是RT1170的数据手册里没有提到GPT。 Re: i.MX RT1176: Maximum frequency of the GPT 亲爱的@长亭, 感谢您对 i.MX RT1176 的关注。 GPT 的最大工作时钟频率为 240 MHz,您可以在 i.MX RT1170 参考手册中找到此信息: 此致, 雪莉
View full article
ADKP保護後のS32K3 AESキープロビジョニング こんにちは、チームの皆さん、 S32Kプラットフォーム上でSHEベースのセキュアブートを有効にしました。また、ADKPパスワードのプログラミングとOEMへのライフサイクル推進などでJTAGインターフェースを保護しています。 AESキー(Key CatlogはすでにAESキーにアライメントされています)を、OEMのライフサイクルでADKP保護を有効にしたデバイスに再プロビジョニングできるか教えていただけますか? それとも、ライフサイクルをIN_FIELDに設定する必要があるのでしょうか? また、更新するキーの所有者タイプを指定してください。 ありがとうございました。 ブーシャン Re: S32K3 AES Key Provisioning after ADKP protection こんにちは、@Bhushan1312さん キーはOEM_PRODやライフサイクルIN_FIELD更新可能ですが、ユーザー権限、ホスト識別(HID)、キー所有者に依存します。 HSEファームウェアのリファレンスマニュアルでは、2.8を参照してください。 表42。主要なグループ所有者 6.2.3.2キー選択 このセクションは重要です。 「• ホストにスーパーユーザー(SU)権限が付与された場合、ターゲットキーハンドルの所有者はホストの識別子(HID)と一致しなければなりません(実行権(スーパーユーザー対ユーザー)を参照) ホストがユーザー権を持っている場合、LCがCUST_DELの場合はターゲットキーハンドルの所有者がHSE_KEY_OWNER_CUSTされ、LCがOEM_PRODの場合はHSE_KEY_OWNER_OEM」とされています。 次に、表47、48、49があり、キーを空スロットにインポートする際や鍵を更新する際にユーザー権限に基づく認証や暗号化が必要かどうかを説明しています。 例えば、CUSTが所有する認可キーを使ってスーパーユーザー権利に昇格した場合、OEM_PRODでもCUSTキーをインポートまたは更新できます。 しかし、ライフサイクルがOEM_PRODに進むまではOEM所有の鍵をインポートすることはできません。それは、まだOEM認証キーをお持ちでないためです。 よろしくお願いいたします。 ルーカス
View full article
Compulab IOTDIN-IMX8- C 1800QM-D4-N32 CAN performance issues Hello Team, We are currently evaluating CAN communication performance on a CompuLab ARM-based platform using the onboard CAN interface exposed through the terminal I/O block. During our testing, we have observed significantly higher CPU utilization on the ARM platform compared to our x86-based system under similar CAN network conditions: x86 platform: approximately 30% CPU utilization CompuLab ARM platform: approximately 45% CPU utilization For comparison, when using a PEAK USB CAN adapter with compulab, the overall performance appears to be better, and the CPU utilization is lower than with the onboard CAN interface. Our CAN network configuration is as follows: CANopen network with 18 nodes. CAN bitrate used: 250 kbps SocketCAN with txqueuelen set to 2000 Communication consists primarily of PDO messages Message periodicity ranges from 100 ms to 10 seconds The shortest update interval currently used is 100 ms CAN-FD is not enabled The same application software and CAN configuration are used on both x86 and ARM platforms We would like to better understand: What factors could contribute to the higher CPU consumption observed on the ARM platform? Are there any known limitations or optimization recommendations for the onboard CAN controller/driver on this platform? Are there specific CAN driver, interrupt handling, buffering, or kernel-level tuning parameters that should be reviewed? Could differences between the onboard CAN controller and the PEAK USB CAN adapter explain the observed performance gap? Are there any recommended profiling or diagnostic methods that would help identify the primary source of CPU load? Our objective is to achieve performance on the ARM platform comparable to what we observe on x86 systems while maintaining the current network load and message rates. We would greatly appreciate any guidance, recommendations, or best practices for improving CAN performance on this platform. Thank you for your support. Re: Compulab IOTDIN-IMX8- C 1800QM-D4-N32 CAN performance issues Hello @JyothiKrao  Hope you are doing very well. There is not enough information to identify a platform-specific limitation yet. The exact CompuLab model, SoC, kernel version, CAN driver, and interface configuration are required before recommending a controller-specific workaround. In particular, we should confirm whether the interface uses FlexCAN or another controller, whether RX FIFO or mailbox mode is selected, and whether the driver supports any receive offload mechanism. We recommend first comparing the following measurements on both systems: Actual CAN traffic: frames per second, bytes per second, bus utilization, and the number of PDOs transmitted and received. CAN errors and drops: ip -details -statistics link show can0 and the controller/driver statistics. Interrupt load: /proc/interrupts , /proc/softirqs , and the CPU on which the CAN interrupt is running. Process and kernel load: top -H , pidstat -t , and, if available, perf top or perf record while the same traffic is active. CPU frequency and governor: verify that both platforms are operating at their expected frequency and that frequency scaling is not affecting the comparison. Best regards, Salas.
View full article
Which Matter Branch/Release should i use Hello,  I'm a bit confused with which matter branch to pick i see a release v1.6.0.0.1 and a branch v1.6-branch-imx_matter_2026_q2, which is the suggested one to use in iMX93 running in Linux env, is there any Major change between these 2 branches that i need to pay attention to? __PRESENT __PRESENT Re: Which Matter Branch/Release should i use Hi @eldhokk  You should use v1.6-branch-imx_matter_2026_q2. The v1.6.0.0.1 release is intended for MCU platforms (FreeRTOS/Zephyr). B.R Re: Which Matter Branch/Release should i use Hi @pengyong_zhang, I would like to know use of this branch and how it differs connectedhomeip other than ELE and groupcast and couple of examples, I don't see any difference between them and v1.6-branch-imx_matter_2026_q2 looks outdated compared to connectedhomeip releases  __PRESENT __PRESENT
View full article
AN15071: where to download the demo and tool? Hello NXP team, AN15071 Rev 1.0 (CMIS over I3C on MCX N947) refers to the mcxn947_optical_module_cmis_over_i3c_demo project and to cmis_test_tool.exe in its scripts folder, but the only link in the document is the USB-to-I3C bridge repository. Where can the demo source and the PC tool be downloaded, or when will they be published? Thank you for your support, Charles Dias FRDM-Training Hands-On Training MCXN Re: AN15071: where to download the demo and tool? Hello @Celeste_Liu , I'll create the ticket. Thank you for your help! Re: AN15071: where to download the demo and tool? Hello @CharlesDias , Thanks for your post. The AN15071 demo and related tool will be uploaded to the Application Code Hub. The upload process is still ongoing, and they are expected to be available in mid-November. If this is urgent, you can contact us by creating a private ticket. If the demo has already passed our internal scan, I can request to send to you before the official release. Hope it helps. BR Celeste
View full article
AN15071: デモ版とツールはどこからダウンロードできますか? NXPチームの皆様、こんにちは。 AN15071 Rev 1.0 (MCX N947 上の I3C 経由の CMIS) は、 mcxn947_optical_module_cmis_over_i3c_demoプロジェクトとその scripts フォルダー内のcmis_test_tool.exeを参照していますが、ドキュメント内の唯一のリンクは USB-to-I3C ブリッジのリポジトリです。 デモソースとPCツールはどこでダウンロードできるのか、またいつ公開されるのか? サポートありがとうございます。 チャールズ・ディアス FRDMトレーニング ハンズオン・トレーニング MCX N Re: AN15071: where to download the demo and tool? こんにちは、 @CharlesDias さん、 投稿ありがとうございます。 AN15071デモおよび関連ツールは アプリケーションコードハブにアップロードされます。アップロード作業は現在も進行中であり、11月中旬には利用可能になる予定です。 緊急の場合は 、プライベートチケットを作成してお問い合わせください。デモがすでに内部スキャンを通過している場合は、正式リリース前に送付をお願いできます。 お役に立てば幸いです。 BR セレステ Re: AN15071: where to download the demo and tool? こんにちは、 @Celeste_Liu さん。 チケットを作成します。 助けてくれてありがとう!
View full article
Code compression MPC556 Hi there. I'm working on a legacy MPC556 microcontroller where I don't have an option to change it. I need any code compressor. Reading MPC555UM, I could find the following at 4.3.1: "Compression is done off line by a special compressor tool, using a fixed vocabulary instruction based algorithm, optmized for the PowerPC instruction set." I've searched for some compiler or even other tool to compress my C code but I've no idea which one I must use. I saw somebody mentioning about Squeezard compressor but I couldn`t find it to download or even buy it. Is there something I can do to compress my C code ? It can be any tool (compiler with a compression option or compressor software) even in case I need to buy it! My last option will be to develop by my own but I don't know how tough is that. Re: Code compression MPC556 Hi, colleague! Have you managed to find any information about the code compression mechanism? Please contact with me [email protected] Re: Code compression MPC556 Hi @juninholiveira90  I'm sorry but the tools and documentation for code compression are not available anymore. Also MPC555/556 are already in End Of Life status, the device is no longer manufactured, so it's not supported anymore. Regards, Lukas
View full article
Could not connect to core / wire ack fault FRDM-MCXA153 I have accidently configured pins 49 and 50 to something else, without realising they are used for the debug probe as well which now means I can't access debug anymore. I changed them back to default but code now won't go to MCU because it doesn't find the core. The probe exists and the MCU seems healthy, I tried the reset and ISP pins to no avail. also tried mass erasing flash but its not possible because of the same fault. This is what I'm currently struggling with: Wire Ack Fault Ee(42). Could not connect to core No connection to chip's debug port Also tried the preconnect script but it did not work. Maybe if I can find a way to get to ROM mode? not sure, any advice is welcome. Development Board Re: Could not connect to core / wire ack fault FRDM-MCXA153 Hi @Luca28  Thanks for the detailed information. Since the issue appeared after changing the pin configuration and the debugger can no longer connect to the core, I would suggest trying to recover the device through ISP mode first. Please try entering ISP mode by holding the ISP button while resetting or power-cycling the board. Then, instead of starting a debug session, please use MCUXpresso Secure Provisioning Tool or blhost to check whether the device can be detected in ISP mode. Please refer to this link Re: FRDM-MCXA153 Suddenly started reporting an error on debug attempt - NXP Community BR Harry
View full article
Compulab IOTDIN-IMX8-C 1800QM-D4-N32 CAN 性能问题 各位团队成员,大家好! 我们目前正在使用通过终端 I/O 模块暴露的板载 CAN 接口,在基于 CompuLab ARM 的平台上评估 CAN 通信性能。 在测试过程中,我们观察到,在类似的 CAN 网络条件下,ARM 平台上的 CPU 利用率明显高于基于 x86 的系统: x86平台: CPU利用率约为30%。 CompuLab ARM平台: CPU利用率约为45%。 相比之下,当使用PEAK USB CAN 适配器和 compulab时,整体性能似乎更好,CPU 利用率也比使用板载 CAN 接口时更低。 我们的CAN网络配置如下: 具有18 个节点的 CANopen 网络。 CAN总线比特率: 250 kbps SocketCAN,txqueuelen 设置为 2000 通信主要通过PDO消息进行。 消息周期范围为100 毫秒至 10 秒 目前使用的最短更新间隔为100 毫秒 CAN-FD 未启用 x86 和 ARM 平台使用相同的应用软件和 CAN 配置。 我们希望更好地了解: 哪些因素可能导致 ARM 平台上的 CPU 占用率较高? 该平台上的板载 CAN 控制器/驱动程序是否存在任何已知的限制或优化建议? 是否有需要检查的特定 CAN 驱动程序、中断处理、缓冲或内核级调优参数? 板载 CAN 控制器和 PEAK USB CAN 适配器之间的差异是否可以解释观察到的性能差距? 是否有推荐的我的或诊断方法可以帮助确定 CPU 负载的主要来源? 我们的目标是在 ARM 平台上实现与 x86 系统相当的性能,同时保持当前的网络负载和消息速率。 我们非常感谢您能提供任何关于提高该平台上 CAN 性能的指导、建议或最佳实践。 感谢您的支持。 Re: Compulab IOTDIN-IMX8- C 1800QM-D4-N32 CAN performance issues 你好@JyothiKrao 希望你一切都好。 目前信息不足,无法确定是否存在平台特定的限制。在推荐针对特定控制器的变通方案之前,需要确切的 CompuLab 型号、SoC、内核版本、CAN 驱动程序和接口配置。具体来说,我们应该确认接口是否使用 FlexCAN 或其他控制器,是否选择 RX FIFO 或邮箱模式,以及驱动程序是否支持任何接收卸载机制。 我们建议首先比较两个系统上的以下测量结果: 实际 CAN 流量:每秒帧数、每秒字节数、总线利用率以及发送和接收的 PDO 数量。 CAN 错误和丢包: ip -details -statistics link show can0 以及控制器/驱动程序统计信息。 中断负载: /proc/interrupts 、 /proc/softirqs 以及运行 CAN 中断的 CPU。 进程和内核负载: top -H 、 pidstat -t ,以及(如果可用) perf top 或 perf record 同时保持相同的流量处于活动状态。 CPU 频率和调速器:验证两个平台是否都在预期的频率下运行,并且频率缩放是否影响比较结果。 顺祝商祺! 萨拉斯。
View full article
コード圧縮 MPC556 やあ。私はレガシーのMPC556マイクロコントローラを扱っていて、変更オプションがありません。コード圧縮ツールが必要です。MPC555UMを読んでみると、4.3.1で次のような記述が見つかりました。「圧縮は、PowerPC命令セットに最適化された固定語彙命令ベースのアルゴリズムを使用する専用の圧縮ツールによってオフラインで行われます。」 Cコードを圧縮できるコンパイラや他のツールを検索しましたが、どれを使えばいいのか全くアイデアがありません。Squeezardコンプレッサーについて言及している人を見かけたのですが、ダウンロードも購入もできませんでした。Cコードを圧縮する方法はありますか?圧縮オプション付きのコンパイラやコンプレッサーソフトウェアなど、どんなツールでも使えますし、購入が必要になった場合にも対応できます! 最後の手段は自分で開発することですが、それがどれほど大変なことなのか分かりません。 Re: Code compression MPC556 こんにちは、同僚さん!コード圧縮の仕組みに関する情報は何か見つかりましたか?どうかお問い合わせください [email protected] Re: Code compression MPC556 こんにちは、@juninholiveira90 申し訳ありませんが、コード圧縮のためのツールやドキュメントはもう利用できません。 また、MPC555/556はすでにエンドサービス状態にあり、製造中でサポートされていません。 よろしくお願いいたします。 ルーカス
View full article
我应该使用哪个 Matter 分支/版本? 你好, 我有点困惑该选择哪个 Matter 分支。我看到有v1.6.0.0.1版本和一个分支v1.6-branch-imx_matter_2026_q2 ,后者是建议在 Linux 环境下运行的 iMX93 上使用的分支。这两个分支之间有什么需要注意的重大变化吗? __展示 __展示 Re: Which Matter Branch/Release should i use 嗨@pengyong_zhang , 我想了解这个分支的用途,以及它与connectedhomeip除了 ELE 和 groupcast 之外的其他区别,并举几个例子。我看不出它们之间有什么区别,而且v1.6-branch-imx_matter_2026_q2版本看起来比 connectedhomeip 的其他版本要旧。 __展示 __展示 Re: Which Matter Branch/Release should i use 嗨@eldhokk 你应该使用 v1.6-branch-imx_matter_2026_q2。v1.6.0.0.1版本适用于 MCU 平台(FreeRTOS/Zephyr)。 B.R
View full article
iMX8QM - 中断/触发 a72 核心 CPU 您好,NXP, 我们成功启动了带有 a72 核心的 VARISCITE iMX8QM VAR-SOM-SYMPHONY 板,仅使用引导加载程序。引导加载程序日志如下: => CPU列表 错误:获取温度失败!(误差 = -19) 0: cpu@0 NXP i.MX8QM RevB A53 频率为 0 MHz - 传感器数据无效 错误:获取温度失败!(误差 = -19) 1:CPU@1 NXP i.MX8QM RevB A53 频率为 0 MHz - 传感器数据无效 错误:获取温度失败!(误差 = -19) 2:CPU@2 NXP i.MX8QM RevB A53 频率为 0 MHz - 传感器数据无效 错误:获取温度失败!(误差 = -19) 3:CPU@3 NXP i.MX8QM RevB A53 频率为 0 MHz - 传感器数据无效 4:CPU@100 NXP i.MX8QM RevB A72,频率 1596 MHz,温度 54°C 5:CPU@101 NXP i.MX8QM RevB A72,频率 1596 MHz,温度 54°C => 但是我们无法使用SGI中断/Poke CPU,设备树如下所示: gic:中断控制器@51a00000 { 兼容 = "arm,gic-v3"; reg = <0x0 0x51a00000 0 0x10000>, /* GIC Dist */       <0x0 0x51b00000 0 0xC0000>, /* GICR */       <0x0 0x52000000 0 0x2000>,  /* GICC */       <0x0 0x52010000 0 0x1000>,  /* GICH */       <0x0 0x52020000 0 0x20000> /* GICV */ #中断单元 = <3> 中断控制器; interrupts = ; interrupt-parent = <&gic>; };   设备树需要做任何更改吗?     Re: iMX8QM - Interrupt/Poke the a72 Core CPU 嗨@kamohan 这个问题与设备树关系不大。SGI 无法传递给内核;原因可能在于目标内核的上电状态或 GIC 初始化。 这是 ATF 中的代码,请确保使用 PSCI CPU_ON 和 SMC 为 A72 上电。 int imx_pwr_domain_on(u_register_t mpidr) { int ret = PSCI_E_SUCCESS; unsigned int cluster_id = MPIDR_AFFLVL1_VAL(mpidr); unsigned int cpu_id = MPIDR_AFFLVL0_VAL(mpidr); sc_pm_set_resource_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); sc_pm_req_low_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); if (sc_pm_set_resource_power_mode(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], SC_PM_PW_MODE_ON) != SC_ERR_NONE) { ERROR("core %d power on failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } if (sc_pm_cpu_start(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], true, CPU_START_ADDR) != SC_ERR_NONE) { ERROR("boot core %d failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } return ret; } void imx_pwr_domain_on_finish(const psci_power_state_t *target_state) { #if (!defined COCKPIT_A53) && (!defined COCKPIT_A72) uint64_t mpidr = read_mpidr_el1(); if (CLUSTER_PWR_STATE(target_state) == PLAT_MAX_OFF_STATE) cci_enable_snoop_dvm_reqs(MPIDR_AFFLVL1_VAL(mpidr)); #endif plat_gic_pcpu_init(); plat_gic_cpuif_enable(); } U-Boot 只使用主核心;辅助核心不会进入 U-Boot。此外,U-Boot 不启用 IRQ,也不在 NS 端配置 GIC CPU 接口,因此 U-Boot 无法接收 SGI 信号。 此致, 志明
View full article
SWO Data Watch Not Working on FRDM-MCXN947 Hello NXP Community, I am using MCUXpresso IDE 25.6 with the FRDM-MCXN947 development board. All other SWO features, including ITM Console output, interrupts, profiling, and counters, are working correctly. However, SWO Data Watch does not display live variable values or generate plots. I tested a simple program with global volatile variables that update continuously. The variables display the correct values in the debugger while paused and continue updating during execution (shown in the global variables), but SWO Data Watch remains empty or displays zero values. I have attached a screenshot of the SWO Trace Configuration. The SWO clock speed is set to 12.0 MHz, and the trace clock is enabled in the Clock Configuration tool. SWO trace statistics show good bytes with no bad bytes, and the trace configuration appears active. This is the simple code Iam using -  #include #include "fsl_common.h" #include "fsl_clock.h" #include "board.h" volatile uint32_t trace_counter = 0; volatile uint32_t trace_ramp = 0; volatile uint32_t trace_wave = 0; int main(void) { BOARD_InitBootClocks(); while (1) { trace_counter++; trace_ramp += 10U; if (trace_ramp >= 1000U) { trace_ramp = 0U; } trace_wave = (trace_wave == 0U) ? 100U : 0U; SDK_DelayAtLeastUs(100000U, CLOCK_GetFreq(kCLOCK_CoreSysClk)); } } Screenshots are attached for better clarification. Could this be a limitation or compatibility issue with SWO Data Watch on the MCXN947 in MCUXpresso IDE 25.6? Are any additional target, probe, or watchpoint configurations required to enable live variable monitoring? Thank you for your help. FRDM-MCXN947  MCXN Re: SWO Data Watch Not Working on FRDM-MCXN947 Hello @sidsal , Thanks for your post. After checking internally, I can confirm this is a known issue in MCUXpresso IDE v25.06 for arm33 core.   The issue comes from a difference in the DWT unit. The MCXN947 uses a Cortex-M33 core (Armv8-M). Its DWT comparator registers are designed differently from those on Cortex-M3/M4 (Armv7-M). Because of this, the comparators are not set up correctly for data tracing on this core. No data trace packets are generated, so the SWO Data view stays empty or shows zero. As NXP is currently focusing its development efforts on MCUXpresso for VS Code as the recommended development environment, we are unable to provide a confirmed schedule for an new MCUXpresso IDE release containing a fix at this time. Sorry for the inconvenience caused. BR Celeste
View full article