Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
SWO Data Watch Not Working on FRDM-MCXN947 Hello NXP Community, I am using MCUXpresso IDE 25.6 with the FRDM-MCXN947 development board. All other SWO features, including ITM Console output, interrupts, profiling, and counters, are working correctly. However, SWO Data Watch does not display live variable values or generate plots. I tested a simple program with global volatile variables that update continuously. The variables display the correct values in the debugger while paused and continue updating during execution (shown in the global variables), but SWO Data Watch remains empty or displays zero values. I have attached a screenshot of the SWO Trace Configuration. The SWO clock speed is set to 12.0 MHz, and the trace clock is enabled in the Clock Configuration tool. SWO trace statistics show good bytes with no bad bytes, and the trace configuration appears active. This is the simple code Iam using -  #include #include "fsl_common.h" #include "fsl_clock.h" #include "board.h" volatile uint32_t trace_counter = 0; volatile uint32_t trace_ramp = 0; volatile uint32_t trace_wave = 0; int main(void) { BOARD_InitBootClocks(); while (1) { trace_counter++; trace_ramp += 10U; if (trace_ramp >= 1000U) { trace_ramp = 0U; } trace_wave = (trace_wave == 0U) ? 100U : 0U; SDK_DelayAtLeastUs(100000U, CLOCK_GetFreq(kCLOCK_CoreSysClk)); } } Screenshots are attached for better clarification. Could this be a limitation or compatibility issue with SWO Data Watch on the MCXN947 in MCUXpresso IDE 25.6? Are any additional target, probe, or watchpoint configurations required to enable live variable monitoring? Thank you for your help. FRDM-MCXN947  MCXN Re: SWO Data Watch Not Working on FRDM-MCXN947 Hello @sidsal , Thanks for your post. After checking internally, I can confirm this is a known issue in MCUXpresso IDE v25.06 for arm33 core.   The issue comes from a difference in the DWT unit. The MCXN947 uses a Cortex-M33 core (Armv8-M). Its DWT comparator registers are designed differently from those on Cortex-M3/M4 (Armv7-M). Because of this, the comparators are not set up correctly for data tracing on this core. No data trace packets are generated, so the SWO Data view stays empty or shows zero. As NXP is currently focusing its development efforts on MCUXpresso for VS Code as the recommended development environment, we are unable to provide a confirmed schedule for an new MCUXpresso IDE release containing a fix at this time. Sorry for the inconvenience caused. BR Celeste
View full article
i.MX RT1176 eDMA:错误时停止机制设置的 CR[HALT] 无需任何软件写入即可清除。 你好, 我们正在调查运行在 PX4 飞行器上的 NuttX 的 i.MX RT1176(rev B0)的 eDMA 错误。 控制器板(fmu-v6xrt)。NuttX 中已找到并修复了错误的触发信号,但是 我们观察到一些eDMA行为,这些行为无法用参考手册解释,我们希望 理解它。 背景(公开报告): https://github.com/apache/nuttx/issues/20881 修复已合并到 apache/nuttx 项目中: https://github.com/apache/nuttx/pull/20893 ## 配置 - eDMA(用于 LPSPI、LPI2C 和 LPUART;不是 eDMA_LPSR) - CR[HOE] = 1(出错时停止),CR[EDBG] = 1 - 已启用散射/聚集;已启用次级环路通道链接 (ELINK) - 使用的通道:LPSPI1/2/3、LPI2C1/2/3、LPUART3/4/5/6/8/10 ## 发生了什么 驱动程序错误导致在 LPUART 上执行有效的 TCD 后,将 TCD 与 CITER = BITER = 0(分散/聚集)关联起来。 TX通道。我们在错误中断处理程序中捕获了 eDMA 寄存器,然后清除它们。 错误信息: - ES[NCE] 已设置,故障通道 = LPUART TX 通道,TCD CITER = BITER = 0 - CR = 0x432(已设置 HALT) 稍后我们从线程上下文(中断之外)读取 CR 时,它是 0x412(HALT 清除)。 同一信道上出现了成对的错误。大多数配对中,两个错误都出现在同一位置。 毫秒,但在某些配对中,第二个错误发生在第一个错误之后 1-269 毫秒。在这些情况下 LPSPI 和 LPI2C 传输停止的时间几乎与两者之间的时间间隔相同。 错误(例如,268 毫秒间隙 / 270.2 毫秒中断)。 软件的功能 - CR 只在初始化时写入一次。之后没有代码会写入 CR[HALT] = 0。 - 在错误中断处理程序中,驱动程序会为通道写入 CERR,然后终止程序。 该通道上的传输:CEEI、CERQ、TCD CSR = 0、TCD DLASTSGA = 0。 参考手册(修订版)5) 将 CR[HOE] 描述为:“任何错误都会导致 eDMA 引擎写入 1 到 HALT 场。随后,eDMA 引擎会忽略所有服务请求,直到您写入为止。 将 0 设置为 HALT 场。我们的观察结果与此不符,因为 HALT 在没有任何任何变化的情况下就变成了 0。 软件编写。 ## 问题 1.当 CR[HOE] = 1 时,在什么条件下 CR[HALT] 会被清除而无需对 CR 进行软件写入? 例如,写入 CERR 或 CERQ,或者激活或终止另一个通道。 2. 当 CR[HALT] = 1 时,如果一个子循环已经在执行,会发生什么? 渠道,以及在此期间收到的服务请求?他们是迷路了吗?还是…… HALT 清除后是否需要继续维护? 3.在错误处理程序将 CERQ 和 TCD CSR = 0 写入故障通道后,会发生什么? 是否会在 1-269 毫秒后在同一通道上引发第二次 NCE? 4. 对于多个外设共享 eDMA 的系统,NXP 是否建议 HOE = 0 或 HOE = 1?如果 HOE = 1,预期的恢复操作是否是在错误处理程序中写入 CR[HALT] = 0? 我们在 i.MX RT1170 芯片勘误表(修订版)中没有找到关于此的勘误。1.6)。我们可以分享 如果需要,可以提供寄存器捕获方法以及测量的更多详细信息。 谢谢! i.MXRT Re: i.MX RT1176 eDMA: CR[HALT] set by Halt-On-Error clears without any software write to C 嗨@宫胁, 感谢您的联系!您是否尝试过在RT1176 rev B0开发板上使用MCUXpresso SDK示例程序来重现此问题?我认为这是一种将 eDMA 行为与 NuttX 驱动程序和 PX4 工作负载分离的有效方法。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
View full article
どのMatterブランチ/リリースを使うべきか こんにちは、 どのMatterブランチを選ぶべきか少し混乱しています。iMX93でLinux環境で動く際に推奨されている v1.6-branch-imx_matter_2026_q2 と、この2つのブランチ間で注目すべき大きな違いはありますか? __現在 __現在 Re: Which Matter Branch/Release should i use こんにちは@pengyong_zhangさん このブランチの用途と、ELEとgroupcast以外のconnectedhomeipとの違い、そしていくつかの例を知りたいのですが、両者の違いが全く分かりません。v1.6-branch-imx_matter_2026_q2はconnectedhomeipのリリースと比べて古くなっているように見えます。 __現在 __現在 Re: Which Matter Branch/Release should i use こんにちは、 @eldhokkさん v1.6-branch-imx_matter_2026_q2 を使用してください。v1.6.0.0.1のリリースはMCUプラットフォーム(FreeRTOS/Zephyr)向けに設計されています。 B.R
View full article
guiguider2.0.1不能创建C模拟器 我把guiguider2.0.1安装在了win10上  可以正常安装和运行  生成代码也正常 在生成C模拟器的时候会提示错误如下: 我想知道是因为我的系统win10(要求win11),还是其它问题产生的? Re: guiguider2.0.1不能创建C模拟器 嗨@tbg 感谢您提供错误日志。 GUI Guider 2.0.1 正式支持 Windows 11(64 位)。 从日志来看,C 模拟器运行失败的原因是捆绑的 GCC/MinGW 编译器无法执行其 cc1 元器件: cc.exe:致命错误:无法执行“cc1”:CreateProcess:没有该文件或目录 因此,我首先建议在 Windows 11 上测试 GUI Guider 2.0.1。如果同样的问题仍然存在,我们可以进一步调查工具链/安装环境。 BR 哈里
View full article
无法连接到核心/线路确认故障 FRDM-MCXA153 我不小心将引脚 49 和 50 配置成了其他用途,却没有意识到它们也用于调试探针,这意味着我现在无法再访问调试功能了。我已将它们改回默认值,但现在代码无法发送到 MCU,因为它找不到内核。探针存在,MCU 看起来也正常,我尝试了 RESET 引脚和 ISP 引脚,但都无济于事。也尝试过批量擦除闪存,但由于同样的故障,无法完成。 这就是我目前遇到的困难: 线路确认故障 Ee(42)。无法连接到核心网 未连接到芯片的调试端口 我也尝试过预连接脚本,但是没有成功。也许我能找到进入 ROM 模式的方法?不太确定,欢迎大家提供建议。 开发板 Re: Could not connect to core / wire ack fault FRDM-MCXA153 嗨@Luca28 感谢您提供如此详细的信息。 由于该问题是在更改引脚配置后出现的,并且调试器无法再连接到内核,我建议先尝试通过 ISP 模式恢复设备。 请尝试按住 ISP 按钮,同时 RESET 或重启板,进入 ISP 模式。然后,请不要启动调试会话,而是使用 MCUXpresso 安全配置工具或 blhost 检查是否可以在 ISP 模式下检测到设备。 请参考此链接 回复:FRDM-MCXA153 在调试尝试时突然开始报告错误 - NXP 社区 BR 哈里
View full article
代码压缩 MPC556 你好呀。我正在使用一款老旧的MPC556微控制器,没有办法更换它。我需要一款代码压缩器。阅读MPC555UM手册时,我在4.3.1节中找到了以下内容:“压缩是由一个特殊的压缩工具离线完成的,该工具使用基于固定词汇表指令的算法,并针对 PowerPC 指令集进行了优化。” 我一直在寻找一些编译器或其他工具来压缩我的 C 代码,但我不知道应该使用哪一个。我看到有人提到Squeezard压缩器,但我找不到下载或购买的地方。有什么办法可以压缩我的C代码吗?可以是任何工具(带有压缩选项的编译器或压缩软件),即使我需要购买它也没关系! 我的最后一个选择是自己开发,但我不知道这有多难。 Re: Code compression MPC556 嗨,同事!你找到任何关于代码压缩机制的信息了吗?请联系我:[email protected] Re: Code compression MPC556 你好@juninholiveira90 很抱歉,代码压缩的工具和文档已不再提供。 此外,MPC555/556 已经停产,该设备不再生产,因此不再提供支持。 此致, Lukas
View full article
Compulab IOTDIN-IMX8- C 1800QM-D4-N32 CAN パフォーマンスの問題 こんにちは、チームの皆さん、 現在、端末I/Oブロックを通じて露出したオンボードCANインターフェースを用いて、CompuLabのARMベースプラットフォーム上でCAN通信性能を評価しています。 テスト中、同様のCANネットワーク条件下で、ARMプラットフォームのCPU利用率はx86ベースのシステムに比べて著しく高いことが観察されました。 x86プラットフォーム: 約 30%のCPU使用率 CompuLab ARMプラットフォーム: 約 45%のCPU使用率 比較として、 ピークUSB CANアダプターとコンピュラブを組み合わせると、全体的な性能が優れており、CPUの使用率もオンボードCANインターフェースより低く見えます。 私たちのCANネットワーク構成は以下の通りです: 18ノードからなるCANopenネットワーク。 使用中のCANビットレート: 250 kbps txqueuelenを2000に設定したSocketCAN コミュニケーションは主にPDOメッセージで構成される メッセージの送信間隔は100ミリ秒から10秒までです。 現在使用されている最短更新間隔は100ミリ秒です。 CAN-FDは有効になっていません x86およびARMプラットフォームの両方で、同じアプリケーションソフトウェアとCAN構成が使用されています 私たちは以下の点についてより深く理解したいと考えています。 ARMプラットフォームで観察される高いCPU消費量に寄与する要因は何でしょうか? このプラットフォーム上のオンボードCANコントローラ/ドライバに関して既知の制限や最適化の提案はありますか? 特定のCANドライバ、割り込み処理、バッファリング、またはカーネルレベルのチューニングパラメータは確認すべきでしょうか? オンボードのCANコントローラとピークUSBのCANアダプターの違いが、観察された性能差の説明になるのでしょうか? CPU負荷の主な原因を特定するのに役立つ推奨されるプロファイリングや診断方法はありますか? 私たちの目標は、現在のネットワーク負荷とメッセージレートを維持しつつ、x86システムで見られる性能と同等のパフォーマンスをARMプラットフォーム上で達成することです。 このプラットフォームでのCANパフォーマンス向上のためのガイダンス、推奨、ベストプラクティスをいただけると大変ありがたいです。 再開まで今しばらくお待ちください。 Re: Compulab IOTDIN-IMX8- C 1800QM-D4-N32 CAN performance issues こんにちは、 @JyothiKraoさん お元気でお過ごしのことと思います。 プラットフォーム固有の制限を特定するには、まだ十分な情報がありません。コントローラ固有の回避策を推奨する前に、正確なCompuLabモデル、SoC、カーネルバージョン、CANドライバ、インターフェース構成が必要です。特に、インターフェースがFlexCANを使用しているか他のコントローラを使用しているか、RX FIFOまたはメールボックスモードを選択しているか、ドライバが受信オフロード機構をサポートしているかを確認する必要があります。 まず、両システムにおける以下の測定値を比較することをお勧めします。 実際のCANトラフィック:フレーム数/秒、バイト数/秒、バス利用率、送受信PDO数。 CANエラーとドロップ: ip -details -statistics link show can0 とコントローラ/ドライバの統計。 割り込み負荷: /proc/interrupts 、 /proc/softirqs 、およびCAN割り込みが動作するCPUです。 プロセスとカーネルの負荷: top -H 、 pidstat -t 、および、利用可能な場合は、同じトラフィックがアクティブな間、 perf top または perf record 。 CPU周波数とガバナー:両方のプラットフォームが期待される周波数で動作し、周波数のスケーリングが比較に影響していないかを確認しましょう。 よろしくお願いいたします。 サラス。
View full article
FRDM-MCXN947 上的 SWO 数据监视功能无法正常工作 NXP社区的各位朋友,大家好! 我正在使用MCUXpresso IDE 25.6和FRDM-MCXN947开发板。 SWO 的其他所有功能,包括 ITM 控制台输出、中断、性能分析和计数器,均运行正常。但是, SWO 数据监视器不显示实时变量值,也不生成图表。 我测试了一个简单的程序,其中包含持续更新的全局易失性变量。暂停时,这些变量在调试器中显示正确的值,并且在执行过程中持续更新(显示在全局变量中),但 SWO 数据监视器仍然为空或显示零值。 我已附上 SWO 跟踪配置的屏幕截图。SWO 时钟频率设置为12.0 MHz ,并且在时钟配置工具中启用了跟踪时钟。SWO 跟踪统计信息显示只有有效字节,没有坏字节,并且跟踪配置似乎已激活。 这是我使用的简单代码 - #include #include "fsl_common.h" #include "fsl_clock.h" #include "board.h" volatile uint32_t trace_counter = 0 ; volatile uint32_t trace_ramp = 0 ; volatile uint32_t trace_wave = 0 ; int main ( void ) { BOARD_InitBootClocks () ; 当( 1 ) { trace_counter ++; trace_ramp += 10 U ; 如果( trace_ramp >= 1000 U ) { trace_ramp = 0 U ; } trace_wave = ( trace_wave == 0 U ) ?100 U : 0 U ; SDK_DelayAtLeastUs ( 100000U , CLOCK_GetFreq ( kCLOCK_CoreSysClk ) ) ; } } 附上屏幕截图以便更好地说明。 这会不会是 MCUXpresso IDE 25.6 中 MCXN947 上的 SWO 数据监视器存在限制或兼容性问题?要启用实时变量监测,是否需要任何额外的目标、探针或观察点配置? 感谢您的帮助。 FRDM-MCXN947 MCX N Re: SWO Data Watch Not Working on FRDM-MCXN947 你好@sidsal , 感谢您的帖子。 经内部核实,我确认这是MCUXpresso IDE v25.06(arm33内核)中已知的问题。 问题出在DWT单位的不同上。MCXN947 使用 Cortex-M33 内核( Armv8-M )。它的 DWT 比较器寄存器设计与 Cortex-M3/M4 ( Armv7-M ) 上的不同。因此,该核心上的比较器没有正确设置,无法进行数据跟踪。没有生成数据跟踪包,因此 SWO 数据视图保持为空或显示为零。 由于恩智浦目前正集中精力开发基于 VS Code 的 MCUXpresso,并将其作为推荐的开发环境,因此我们暂时无法提供包含此修复程序的 MCUXpresso IDE 新版本发布的具体时间表。由此造成的不便,敬请谅解。 BR 塞莱斯特
View full article
iMX8QM - Interrupt/Poke the a72 Core CPU Hello NXP, We were able to bringup VARISCITE iMX8QM VAR-SOM-SYMPHONY Board with a72 core conly in bootloader.. the bootloader logs are as below, => cpu list Error: get temperature failed! (error = -19) 0: cpu@0 NXP i.MX8QM RevB A53 at 0 MHz - invalid sensor data Error: get temperature failed! (error = -19) 1: cpu@1 NXP i.MX8QM RevB A53 at 0 MHz - invalid sensor data Error: get temperature failed! (error = -19) 2: cpu@2 NXP i.MX8QM RevB A53 at 0 MHz - invalid sensor data Error: get temperature failed! (error = -19) 3: cpu@3 NXP i.MX8QM RevB A53 at 0 MHz - invalid sensor data 4: cpu@100 NXP i.MX8QM RevB A72 at 1596 MHz at 54C 5: cpu@101 NXP i.MX8QM RevB A72 at 1596 MHz at 54C => But we  are unable to Interrupt/Poke the cpu using SGI, the device tree is as below, gic: interrupt-controller@51a00000 { compatible = "arm,gic-v3"; reg = <0x0 0x51a00000 0 0x10000>, /* GIC Dist */       <0x0 0x51b00000 0 0xC0000>, /* GICR */       <0x0 0x52000000 0 0x2000>,  /* GICC */       <0x0 0x52010000 0 0x1000>,  /* GICH */       <0x0 0x52020000 0 0x20000>; /* GICV */ #interrupt-cells = <3>; interrupt-controller; interrupts = ; interrupt-parent = <&gic>; };   Are there any changes to be done for Device Tree?     Re: iMX8QM - Interrupt/Poke the a72 Core CPU Hi @kamohan  This issue has little to do with the Device Tree. The SGI cannot be delivered to the kernel; the cause likely lies in the target core's power-on state or GIC initialization. Here is code in ATF, please make sure you are using PSCI CPU_ON with SMC to power on the A72. int imx_pwr_domain_on(u_register_t mpidr) { int ret = PSCI_E_SUCCESS; unsigned int cluster_id = MPIDR_AFFLVL1_VAL(mpidr); unsigned int cpu_id = MPIDR_AFFLVL0_VAL(mpidr); sc_pm_set_resource_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); sc_pm_req_low_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); if (sc_pm_set_resource_power_mode(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], SC_PM_PW_MODE_ON) != SC_ERR_NONE) { ERROR("core %d power on failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } if (sc_pm_cpu_start(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], true, CPU_START_ADDR) != SC_ERR_NONE) { ERROR("boot core %d failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } return ret; } void imx_pwr_domain_on_finish(const psci_power_state_t *target_state) { #if (!defined COCKPIT_A53) && (!defined COCKPIT_A72) uint64_t mpidr = read_mpidr_el1(); if (CLUSTER_PWR_STATE(target_state) == PLAT_MAX_OFF_STATE) cci_enable_snoop_dvm_reqs(MPIDR_AFFLVL1_VAL(mpidr)); #endif plat_gic_pcpu_init(); plat_gic_cpuif_enable(); } U-Boot uses only the primary core; the secondary core does not enter U-Boot. Additionally, U-Boot does not enable IRQs and does not configure the GIC CPU interface on the NS side, so SGI signals cannot be received within U-Boot. Best Regards, Zhiming
View full article
i.MX RT1176 eDMA: CR[HALT] set by Halt-On-Error clears without any software write to C Hello, We are investigating eDMA errors on an i.MX RT1176 (rev B0) running NuttX on a PX4 flight controller board (fmu-v6xrt). The trigger of the errors has been found and fixed in NuttX, but we observed eDMA behavior that we cannot explain from the Reference Manual, and we would like to understand it. Background (public report): https://github.com/apache/nuttx/issues/20881 Fix merged in apache/nuttx: https://github.com/apache/nuttx/pull/20893 ## Configuration - eDMA (the one serving LPSPI, LPI2C and LPUART; not eDMA_LPSR) - CR[HOE] = 1 (Halt On Error), CR[EDBG] = 1 - Scatter/gather enabled; minor-loop channel linking (ELINK) enabled - Channels in use: LPSPI1/2/3, LPI2C1/2/3, LPUART3/4/5/6/8/10 ## What happened A driver bug linked a TCD with CITER = BITER = 0 (scatter/gather) after a valid TCD on LPUART TX channels. We captured the eDMA registers in the error interrupt handler, before clearing the error: - ES[NCE] set, failing channel = an LPUART TX channel, TCD CITER = BITER = 0 - CR = 0x432 (HALT set) When we read CR later from thread context (outside the interrupt), it was 0x412 (HALT clear). The errors came in pairs on the same channel. In most pairs both errors were in the same millisecond, but in some pairs the second error came 1-269 ms after the first. In those cases the LPSPI and LPI2C transfers stopped for almost the same time as the gap between the two errors (for example, 268 ms gap / 270.2 ms interruption). ## What the software does - CR is written only once, at initialization. No code writes CR[HALT] = 0 afterwards. - In the error interrupt handler, the driver writes CERR for the channel, then terminates the transfer on that channel: CEEI, CERQ, TCD CSR = 0, TCD DLASTSGA = 0. The Reference Manual (Rev. 5) describes CR[HOE] as: "any error causes the eDMA engine to write 1 to the HALT field. Subsequently, the eDMA engine ignores all service requests until you write 0 to the HALT field." Our observation does not match this, because HALT became 0 without any software write. ## Questions 1. With CR[HOE] = 1, under what conditions is CR[HALT] cleared without a software write to CR? For example, writing CERR or CERQ, or activating or terminating another channel. 2. While CR[HALT] = 1, what happens to a minor loop that is already executing on another channel, and to service requests that arrive during that time? Are they lost, or are they held and serviced after HALT is cleared? 3. After the error handler has written CERQ and TCD CSR = 0 on the failing channel, what can cause a second NCE on the same channel 1-269 ms later? 4. For a system where several peripherals share the eDMA, would NXP recommend HOE = 0 or HOE = 1? If HOE = 1, is the expected recovery to write CR[HALT] = 0 in the error handler? We have not found an erratum about this in the i.MX RT1170 Chip Errata (Rev. 1.6). We can share the register capture method and more details of the measurement if that helps. Thank you. i.MXRT Re: i.MX RT1176 eDMA: CR[HALT] set by Halt-On-Error clears without any software write to C Hi @miyawaki , Thanks for the reaching out! Have you tried with some MCUXpresso SDK demo on an RT1176 rev B0 board to reproduce this issue? I think it would be a useful way to separate eDMA behavior from the NuttX driver and PX4 workload.  Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
Guiguider 2.0.1 cannot create a C simulator. I installed guiguider 2.0.1 on Windows 10, and it installed and ran normally, and the code generation was also normal. However, when generating the C simulator, I encountered the following error: I want to know if it's because my system is Windows 10 (which requires Windows 11), or if there's some other problem? Re: guiguider2.0.1不能创建C模拟器 HI @tbg  Thanks for providing the error log. GUI Guider 2.0.1 officially supports Windows 11 (64-bit). From the log, the C simulator fails because the bundled GCC/MinGW compiler cannot execute its cc1 component: cc.exe: fatal error: cannot execute 'cc1': CreateProcess: No such file or directory Therefore, I would first recommend testing GUI Guider 2.0.1 on Windows 11. If the same issue still occurs there, we can further investigate the toolchain/installation environment. BR Harry
View full article
AN15071:在哪里可以下载演示版和工具? 您好,NXP团队, AN15071 Rev 1.0(MCX N947 上的 CMIS over I3C)提到了mcxn947_optical_module_cmis_over_i3c_demo项目及其脚本文件夹中的cmis_test_tool.exe ,但文档中唯一的链接是 USB 转 I3C 桥接存储库。 演示源代码和PC工具在哪里可以下载?或者它们何时发布? 感谢您的支持, 查尔斯·迪亚斯 FRDM 培训 动手实践培训 MCX N Re: AN15071: where to download the demo and tool? 你好@Celeste_Liu , 我会创建工单。 感谢您的帮助! Re: AN15071: where to download the demo and tool? 你好@CharlesDias , 感谢您的帖子。 AN15071 演示和相关工具将上传到应用程序代码中心。上传过程仍在进行中,预计将于 11 月中旬上线。 如果情况紧急,您可以创建私人工单与我们联系。如果演示版已经通过了我们的内部审核,我可以申请在正式版本前发送给您。 希望对您有所帮助。 BR 塞莱斯特
View full article
コア/配線認証の故障FRDM-MCXA153に接続できませんでした 誤ってピン49と50を別のものに設定してしまい、それがデバッグプローブにも使われていることに気づかず、その結果デバッグにアクセスできなくなりました。デフォルトに戻しましたが、コードがMCUに行けません。コアが見つからないからです。プローブは存在し、MCUも正常そうです。リセットやISPピンも試しましたが効果はありませんでした。フラッシュメモリの一括消去も試みましたが、同じ不具合のため不可能でした。 私が現在抱えている問題は以下のとおりです。 ワイヤACK障害 Ee(42)コアに接続できませんでした チップのデバッグポートに接続されていません プリコネクトスクリプトも試してみましたが、うまくいきませんでした。ROMモードに移行する方法を見つけられればいいのですが?よくわからないので、アドバイスをいただけると嬉しいです。 開発ボード Re: Could not connect to core / wire ack fault FRDM-MCXA153 こんにちは、 @Luca28さん 詳細な情報ありがとうございます。 ピン設定を変更した後に問題が発生し、デバッガがコアに接続できなくなったため、まずISPモードでデバイスを復旧することをおすすめします。 ボードのリセットまたは電源の再投入を行う際に、ISPボタンを押し続けながらISPモードに入ってみてください。その後、デバッグセッションを開始する代わりに、MCUXpressoセキュアプロビジョニングツールやblhostを使ってISPモードでデバイスが検出可能かどうかを確認してください。 こちらのリンクを参照してください Re: FRDM-MCXA153 デバッグ試行時に突然エラーが報告され始めた - NXPコミュニティ BR ハリー
View full article
SWOデータウォッチがFRDM-MCXN947で動作しない こんにちは、NXPコミュニティの皆さん、 私は MCUXpresso IDE 25.6 と FRDM-MCXN947 開発ボード を使っています 。 ITMコンソール出力、割り込み、プロファイリング、カウンタなど、その他のSWO機能はすべて正常に動作しています。しかし、 SWOデータウォッチでは、リアルタイムの変数値が表示されず、グラフも生成されません。 継続的に更新されるグローバルな揮発性変数を含むシンプルなプログラムをテストしました。これらの変数は、一時停止中はデバッガで正しい値を表示し、実行中も更新され続けます(グローバル変数に表示されます)。しかし、SWO Data Watchは空のままか、ゼロ値を表示します。 SWOトレース設定のスクリーンショットを添付しました。SWOのクロック速度は12.0MHzに設定されており、クロック設定ツールでトレースクロックが有効になっています。SWOトレース統計では、不良バイトはなく、正常バイトのみが表示され、トレース設定は有効になっているようです。 これが私が使用しているシンプルなコードです。 #include #include "fsl_common.h" #include "fsl_clock.h" #include "board.h" volatile uint32_t trace_counter = 0 ; volatile uint32_t trace_ramp = 0 ; volatile uint32_t trace_wave = 0 ; int main ( void ) { BOARD_InitBootClocks () ; ( 1 )​ { trace_counter ++; trace_ramp += 10 U ; if ( trace_ramp >= 1000 U ) { trace_ramp = 0 U ; } trace_wave = ( trace_wave == 0 U ) ?100 U : 0 U ; SDK_DelayAtLeastUs ( 100000 U , CLOCK_GetFreq ( kCLOCK_CoreSysClk )) ; } } より分かりやすくするために、スクリーンショットを添付しました。 これはMCUXpresso IDE 25.6のMCXN947上のSWO Data Watchとの制限や互換性の問題でしょうか?リアルタイム変数監視を有効にするために、追加のターゲット、プローブ、またはウォッチポイントの設定が必要ですか? 助けてくれてありがとう。 FRDM-MCXN947 MCX N Re: SWO Data Watch Not Working on FRDM-MCXN947 こんにちは、 @sidsal さん、 投稿ありがとうございます。 内部で確認したところ、これはMCUXpresso IDE v25.06のarm33コアで既知の問題であることが確認できました。 問題は、DWT単位の違いに起因する。MCXN947はCortex-M33コア(Armv8-M)を使用しています。DWTコンパレータレジスタはCortex-M3/M4(Armv7-M)のものとは異なる設計です。そのため、このコア上のデータトレース用にコンパレータが正しく設定されていません。データトレースパケットは生成されないため、SWOデータビューは空のままかゼロのままになります。 NXPは現在、推奨開発環境として MCUXpresso for VS Code の開発に注力しているため、修正を含む新しいMCUXpresso IDEリリースの確定スケジュールは現時点で提供できません。ご不便をおかけして申し訳ありません。 BR セレステ
View full article
Guiguider 2.0.1 では C 言語シミュレータを作成できません。 Windows 10にguiguider 2.0.1をインストールしたところ、インストールと実行は正常に完了し、コード生成も正常でした。しかし、Cシミュレータを生成する際に、以下のエラーが発生しました。 私のシステムがWindows 10(Windows 11が必要)だからなのか、それとも他に何か問題があるのか知りたいです。 Re: guiguider2.0.1不能创建C模拟器 こんにちは、 @tbgさん エラーログをご提供いただきありがとうございます。 GUI Guider 2.0.1は公式にWindows 11(64ビット)をサポートしています。 ログから、Cシミュレータが失敗するのは、バンドルされているGCC/MinGWコンパイラがcc1コンポーネントを実行できないためです。 cc.exe: 致命的なエラー: 'cc1' を実行できません: CreateProcess: そのようなファイルやディレクトリはありません したがって、まずWindows 11でGUI Guider 2.0.1をテストすることをお勧めします。同じ問題が依然として起きている場合は、ツールチェーンやインストール環境をさらに調査できます。 BR ハリー
View full article
i.MX RT1176 eDMA: CR[HALT]は、Halt-On-Errorによって設定され、Cへのソフトウェア書き込みなしでクリアされます こんにちは、 私たちは、PX4便でNuttXを搭載している i.MX RT1176(回転B0)のeDMAエラーを調査しています コントローラボード(FMU-V6XRT)。エラーのトリガーはNuttXで発見・修正されていますが リファレンス・マニュアルから説明できないeDMAの挙動を観察し、 理解するために。 背景(公開レポート): https://github.com/apache/nuttx/issues/20881 修正がapache/nuttxにマージされました: https://github.com/apache/nuttx/pull/20893 ## 構成 - eDMA(LPSPI、LPI2C、LPUARTをサービスするもの;eDMA_LPSRではない) - CR[HOE] = 1(エラーで停止)、CR[EDBG] = 1 - 散乱/ギャザー対応;マイナーループチャネルリンク(ELINK)有効 - 使用チャネル:LPSPI1/2/3、LPI2C1/2/3、LPUART3/4/5/6/8/10 ## どうしたの ドライバーのバグにより、LPUART上で有効なTCDが実行された後にCITER = BITER = 0(散布/採集)とTCDが連結されました TXチャネル。エラー割り込みハンドラでeDMAレジスタをキャプチャしてからクリアします。 エラー: - ES[NCE] 設定、故障チャネル = LPUART TX チャネル、TCD CITER = BITER = 0 - CR = 1 0x432(停止集合) 後でThreadコンテキスト(割り込み外)からCRを読み取ったときは0x412(HALTクリア)でした。 エラーは同じチャネル上でペアで発生しました。ほとんどのペアでは、両方のエラーが同じでした ミリ秒単位だが、一部のペアでは、2番目のエラーは最初のエラーから1〜269ミリ秒後に発生した。そういう場合 LPSPIとLPI2Cの転送は、両者の間隔とほぼ同時期に停止しました エラー(例:268 ms ギャップ / 270.2 ms 中断)。 ## ソフトウェアが何をするか - CRは初期化時に一度だけ書き込まれます。その後、CR[HALT] = 0 と書き込むコードはありません。 - エラー割り込みハンドラで、ドライバはチャネルに対してCERRを書き込み、その後 そのチャネルでの転送:CEEI, CERQ, TCD CSR = 0, TCD DLASTSGA = 0。 リファレンス・マニュアル(改訂版)5) CR[HOE]を次のように説明しています。「エラーが発生すると、eDMAエンジンが書き込みます 1. HALT分野へ。その後、eDMA エンジンは、あなたが書き込むまで全てのサービス要求を無視します。 HALTフィールドに0を投入します。しかし、私たちの観察はこれと一致しません。なぜなら、HALTが 0 なしに 0 になるからです。 ソフトウェアが書く。 ## 質問 1.CR[HOE] = 1の場合、CR[HALT]はソフトウェアによるCR書き込みなしにどのような条件下でクリアされますか? 例えば、CERRやCERQの書き込み、あるいは別のチャネルの有効化や終了などです。 2. CR[HALT] = 1の場合、すでに別のループで実行中のマイナーループはどうなるのか その期間中に届くサービス要請に対して、チャネルやサービスに対応できるのでしょうか?彼らは迷子なのか、それとも HALTが解除された後に保管および整備されるのか? 3.エラーハンドラが故障チャネルにCERQとTCD CSR = 0を書き込んだ後、 同じチャネルで1〜269ms後に2回目のNCEが発生する原因? 4. 複数のペリフェラルがeDMAを共有するシステムの場合、NXPはHOE = 0を推奨しますか? HOE = 1?HOE = 1 の場合、エラーハンドラに CR[HALT] = 0 を書き込むことが想定される回復処理ですか? i.MX RT1170 チップの正誤表 (Rev.1.6)。私たちは共有できます レジスタキャプチャ方法と測定の詳細について教えてください。 よろしくお願いします。 i.MX RT Re: i.MX RT1176 eDMA: CR[HALT] set by Halt-On-Error clears without any software write to C こんにちは@宮脇、 ご連絡いただきありがとうございます!RT1176 rev B0ボードでMCUXpresso SDKのデモを使ってこの問題を再現してみましたか?これはeDMAの動作をNuttXドライバやPX4のワークロードから分離する有効な方法だと思います。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
View full article
iMX8QM - a72コアCPUへの割り込み/ポーク こんにちは、NXPさん。 ブートローダーで72コアのみを使用してVARISCITE iMX8QM VAR-SOM-SYMPHONYボードを起動することができました。ブートローダーのログは以下のとおりです。 => CPUリスト エラー: 温度の取得に失敗しました!(誤差 = -19) 0: cpu@0 NXP i.MX8QM RevB A53 0 MHz - センサーデータが無効です エラー: 温度の取得に失敗しました!(誤差 = -19) 1: cpu@1 NXP i.MX8QM RevB A53 0 MHz - センサーデータが無効です エラー: 温度の取得に失敗しました!(誤差 = -19) 2: cpu@2 NXP i.MX8QM RevB A53 0 MHz - センサーデータが無効です エラー: 温度の取得に失敗しました!(誤差 = -19) 3: cpu@3 NXP i.MX8QM RevB A53 0 MHz - センサーデータが無効です 4: CPU@100 NXP i.MX8QM RevB A72、1596 MHz、54℃ 5: CPU@101 NXP i.MX8QM RevB A72、1596 MHz、54℃ => しかし、SGIを使用してCPUを割り込み/ポークすることはできません。デバイスツリーは以下のとおりです。 gic: interrupt-controller@51a00000 { 互換 = "arm,gic-v3"; reg = <0x0 0x51a00000 0 0x10000>, /* GIC Dist */       <0x0 0x51b00000 0 0xC0000>, /* GICR */       <0x0 0x52000000 0 0x2000>,  /* GICC */       <0x0 0x52010000 0 0x1000>,  /* GICH */       <0x0 0x52020000 0 0x20000>; /* GICV */ #interrupt-cells = <3>; 割り込みコントローラ; 割り込み = interrupt-parent = <&gic>; };   デバイスツリーに変更を加える必要はありますか?     Re: iMX8QM - Interrupt/Poke the a72 Core CPU こんにちは、 @kamohanさん この問題はデバイスツリーとはほとんど関係がありません。SGIはカーネルに提供できません。原因はおそらくターゲット コアの電源オン状態 やGIC初期化にあります。 以下はATFのコードです。A72の電源を入れるには、PSCI CPU_ONとSMCを使用していることを確認してください。 int imx_pwr_domain_on(u_register_t mpidr) { int ret = PSCI_E_SUCCESS; unsigned int cluster_id = MPIDR_AFFLVL1_VAL(mpidr); unsigned int cpu_id = MPIDR_AFFLVL0_VAL(mpidr); sc_pm_set_resource_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); sc_pm_req_low_power_mode(ipc_handle, cluster_id == 0 ? SC_R_A53 : SC_R_A72, SC_PM_PW_MODE_ON); if (sc_pm_set_resource_power_mode(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], SC_PM_PW_MODE_ON) != SC_ERR_NONE) { ERROR("core %d power on failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } if (sc_pm_cpu_start(ipc_handle, ap_core_index[cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id], true, CPU_START_ADDR) != SC_ERR_NONE) { ERROR("boot core %d failed!\n", cpu_id + PLATFORM_CLUSTER0_CORE_COUNT * cluster_id); ret = PSCI_E_INTERN_FAIL; } return ret; } void imx_pwr_domain_on_finish(const psci_power_state_t *target_state) { #if (!defined COCKPIT_A53) && (!defined COCKPIT_A72) uint64_t mpidr = read_mpidr_el1(); if (CLUSTER_PWR_STATE(target_state) == PLAT_MAX_OFF_STATE) cci_enable_snoop_dvm_reqs(MPIDR_AFFLVL1_VAL(mpidr)); #endif plat_gic_pcpu_init(); plat_gic_cpuif_enable(); } U-Bootはプライマリコアのみを使用し、セカンダリコアはU-Bootには関与しません。さらに、U-BootはIRQを有効にしず、NS側のGIC CPUインターフェースの設定も行わないため、U-Boot内でSGI信号を受け取ることができません。 よろしくお願いします、 志明
View full article
LS1028A custom board does not boot after removing CPLD — RCW configured by pull-up/pull-down resisto Hi NXP Support, We have started designing our own board based on the LS1028A. In this design, we removed the CPLD, and the RCW is configured using pull-up/pull-down resistors. The LS1028A POR reset is controlled by a reset IC with a 200 ms reset delay. From our measurements, all board power rails, clocks, and reset signals are present, but the processor does not boot. We do not know the reason. Could you please help analyze the possible cause? Thanks. Re: LS1028A custom board does not boot after removing CPLD — RCW configured by pull-up/pull-down res The most probable causes are: Incorrect cfg_rcw_src resistor strap settings due to the removal of the CPLD. RESET_REQ_B being unintentionally connected into the reset path. Please verify that RESET_REQ_B is not tied to PORESET_B. PORESET_B timing issues caused by the reset IC. Per the datasheet, the PORESET_B rise/fall time should not exceed one SYSCLK period. An invalid or inaccessible RCW image in the selected boot source. External circuitry preventing HRESET_B from being released. We recommend temporarily selecting a hard-coded RCW boot mode and verifying whether CodeWarrior can successfully connect to the device through CWTAP. This would help isolate whether the issue is related to the RCW boot path or to the reset hardware implementation. Thanks. Re: LS1028A custom board does not boot after removing CPLD — RCW configured by pull-up/pull-down res We removed the CPLD on the LS1028A. The power-up sequence follows the reference board circuit. The RCW is configured by pull-up/pull-down resistors, selecting hardware-encoded boot. All other configurations are also set by pull-up/pull-down resistors. In our measurements, the rise of PORESET_B does not exceed one clock cycle, and the reset duration is 200 ms. HRESET_B goes high and then low. However, the LS1028A does not boot normally, and no clock is output on SDHC1_CLK. Re: LS1028A custom board does not boot after removing CPLD — RCW configured by pull-up/pull-down res Let me confirm when you set hardware-encoded mode the HRESET_B could not get high at the end. If so, it is possible that this is a hardware issue. Please test the waveforms of PORESET_B, HRESET_B, RESET_REQ and ASLEEP following the LS1028A Reference Manual, 4.8.6 Power-On Reset Sequence Timing. It's better to test the SYSCLK and POR configs pins at the same time, and compare them against the timing requirements to confirm when the hardware issue occurs. Thanks
View full article
S32k342: Bctudmabuffer がデータで更新されていません。 こんにちは、 ADC0に10チャネル対応にPIT、BCTU、DMA(Ch6)を設定しました。 レジスタ値LISTCHRとFIFO1DR、MSR(10進数)を確認しました MSR:32768、 TRGCFG[23] :268477184 MCR: 67305600 FIFO1DR: 781516942 LISTCHR[0] : 2162725 LISTCHR[1] : 65576 LISTCHR[2] : 6 LISTCHR[3] : 327687 LISTCHR[4] : 2147909636 FIFCR: 16777216 FIFOERR: 151060480 FIF0SR: 0 FIFOCNTR: 15 Autosar MCALのDMAチャプニング6を設定し、例コードを使った https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-... 質問は、bctudma バッファで DMA ウォーターマーク通知とデータを取得できないことです。 何が不足しているのか、ご教示ください。 ありがとう Re: S32k342: Bctudmabuffer is not updating with data. 私はAUTOSAR MCALを使っています。 転送設定も設定する必要がありますか? また、転送 API を呼び出す必要があります。Mcl_SetDmaChannelTransferList と Mcl_SetDmaCHannelCommand を MCL_DMA_CH_START_REQUEST とともに呼び出します。 Re: S32k342: Bctudmabuffer is not updating with data. 現在、私はパスを使用しており、これに関する共有設定を持っています。 PIT_CH0 → TRGMUX → BCTU_Trg23 → ADC0/Adc1 → DMA 私にさせてください。 最後に使う道を紹介します: PIT_CH0 - TRGMUX - BCTU_Trg23 ADC0(5チャネル) - FIFO1 - eDMA PIT_CH1 - TRGMUX - BCTU_Trg47 - ADC1(5チャネル) - FIFO2 - eDMA この設定についても教えてください。 Re: S32k342: Bctudmabuffer is not updating with data. 私はRTD 3.0.0を使用しています。 Re: S32k342: Bctudmabuffer is not updating with data. Bctu 設定: ADC: DMA: また、BCT、PIT、EDMAなどの周辺時計も対応可能ですDMAMUX_0 Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 詳細を教えていただきありがとうございます。 レジスタの値だけでは、何が不足しているかを判断するのは難しい。ADC変換がBCTU FIFOに達しているように見えるため、問題はBCTU→DMA要求パス、DMAチャネル構成、またはDMAMUXの設定に関連している可能性があります。 以下のいずれかを教えていただけますか: 問題を再現する簡略化されたテストプロジェクト、または S32構成ツールの設定画面のスクリーンショット: ADC BCTU DMA/eDMA DMAMUX PIT また、ご利用のRTDバージョンをお知らせください。 構成や簡略化されたプロジェクトを使えば、作業中の例と比較して、欠落や誤った設定をより効率的に特定できます。 BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 転送設定やそれに対応するコードは必要ありません。転送設定はドライバで行います。 Rmコンポーネントを通してDMAMUXの設定と初期化も行いましたか?こんなものを用意しておくべきです… 希望するチャネルを選択しています。次に、コード内で Rm init を呼び出します。 #include "CDD_Rm.h" /* HLD RMドライバ経由でDMAMUXを初期化してください */ Rm_Init(&Rm_Config); BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. はい、やっています。 また、Rm_Initも実行しています。 Re: S32k342: Bctudmabuffer is not updating with data. 以前に共有したすべての設定です。 Adc: Adc 0 と 1 の両方で、呼び出し API Adc_EnableCtuControlMode を使用して制御モードを使用します。 Adc_CtuEnableHwTrigger も呼び出す必要がありますか?私はまだ呼び出していません。 Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 詳細を教えていただきありがとうございます。 これまでの情報からは根本原因を特定するのは難しいです。レジスタダンプだけでは、問題がBCTU、DMA、DMAMUX、またはソフトウェア構成にあるかどうかを特定するには不十分です。 確認すべき追加事項がいくつかあります。 DMA割り込みは有効になっており、正しく設定されていますか? ADC BCTUの制御モードとトリガーモードのどちらを使用していますか? DMAウォーターマーク通知は、BCTU制御モードを使用している場合にのみ利用可能ですのでご注意ください。トリガーモードを使用している場合、DMAウォーターマーク通知は表示されません。 問題を分析するために、以下の内容を教えていただけますか: 問題を再現する簡略化されたスタンドアロンプロジェクト、または 関連するS32設定ツールの設定(ADC、BCTU、DMA/DMAMUX、PIT)のスクリーンショットと関連コード一式を添付してください。 理想的には、完全に簡略化されたプロジェクトがあれば、構成を確認し、動作中の参照例と比較することがより効率的に行えるでしょう。 BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 提供されたスクリーンショットからは、明らかな問題は見当たりません。 プロジェクトと使用したコードを共有していただいたので、意図したトリガーシナリオをテストするために、いくつか作成してみましょう。 BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. 設定を確認してください。 Re: S32k342: Bctudmabuffer is not updating with data. はい、お願いします。コードを共有するのは難しいので、s32k342 用のテストプロジェクトを作成してください。 ありがとうございます。 Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 最後に、ご指定の構成に合わせてADC HLDのデモを行いました。 トリガーパス: PIT0_CH0 -> TRGMUX -> BCTU Trigger 23 -> ADC0(5チャネル) -> BCTU FIFO1 -> eDMA(ch0) PIT1_CH1 -> TRGMUX -> BCTU Trigger 47 -> ADC1(5チャネル) -> BCTU FIFO2 -> eDMA(第16チャンネル) ここに掲載されています:https://community.nxp.com/t5/S32K-Knowledge-Base/Example-FRDM-A-S32K344-PIT-ADC-BTCU-ControlMode-FIFO-DMA-HLD/ta-p/2420432 お役に立てば幸いです。 BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. 感謝、 確認して、改めてご連絡いたします。 Re: S32k342: Bctudmabuffer is not updating with data. サンプルコードを確認しましたが、動作しません。 Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 データが更新されたのを確認しました BR、ペトル Re: S32k342: Bctudmabuffer is not updating with data. 返事いただけますか? Re: S32k342: Bctudmabuffer is not updating with data. こんにちは、 BCTUリストに記載されているチャネルはBCTU制御モードでのみ使用され、ADCユニットのグループで定義されたチャネルは通常または注入変換に使用されます。AdcHwUnitのグループとチャネルは、この例で使われていなくても単純に省略することはできません。 ポート内でADCチャネルを定義する必要はありません。ADCパスは常に有効なので、ポート設定は不要です。一般的に、ADCチャネルはポート設定を必要としません。 バッファのずれに関してですが、当初はラウターバッハでテストしたところ、バッファは予想通り正しく表示されました。 S32DS内部では、コードの実行が停止するとデータの順序が乱れる。デバッグモード中にPITが継続的に実行されるように設定されていたことが原因だと分かりました。デバッグ中にPITをフリーズできるように設定を変更してください。 バッファの定義も間違っていました。正しくはuint16_tとして宣言する必要がありました。 すると、S32DSでもバッファが正しく表示されるようになります。 BR、ペトル     Re: S32k342: Bctudmabuffer is not updating with data. あなたと同じチャネルを設定しましたが、BCTUDMAバッファが更新されているのが確認できます。 それでも、Adc0/1チャネルのアライメントはどうやってしたのか、なぜADC0のVREFL/HデータがADC1のVREFL/Hチャネルと一致しないのかは理解できません。P0も同じですか?また、ポートで設定する必要のない内部チャネルもありますが、P7やP0のように外部チャネルがあるのに、なぜポート内で設定されなかったのでしょうか?チャネル(10)を設定したいのですが、BCTUでどうやってアライメントすればいいですか?また、設定にはないp7とp0としてポート設定も必要ですか? なぜADC0/1の全チャネルをADC構成アレイに含めていないのですか?なぜADC0/1ごとにチャネルが1つだけなのですか?
View full article
IMX95 A55 Bare Metal Development Hello everyone, I am working on bringing up a bare-metal application directly on the Arm Cortex-A55 cluster of an NXP i.MX95 (using the i.MX95 EVK / custom board). While much of the ecosystem documentation focuses on Linux (Yocto) or running real-time tasks on the Cortex-M7/M33 cores, I want to execute low-level code directly on the A55 core(s) without an underlying OS kernel. Is there anybody have done this(which IDE, debug probe)or Do you know this is a good approach? FRDM-IMX95  iMX95  Re: IMX95 A55 Bare Metal Development Hello @thehk  This approach is possible, but it is not supported by NXP because of the complexity of the architecture. Also, you can try Zephyr for i.MX95 in Cortex A55 core. Best regards, Salas.
View full article