Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
How do I implement Secure Boot on the i.MX95? I completed the secure boot process on imx8mp. Secure boot is achieved using HABv4 on an 8mp. Does imx95 also use HABv4 to implement secure boot? When compiling flash.bin, I did not see information such as CSF block or sld hab block. How do I perform a secure boot on IMX95? Re: How do I implement Secure Boot on the i.MX95? Hello @yyn  I hope you are doing very well. Please take a look to the introduction_ahab in the U-boot documentation. There is explained the Secure Boot process of the i.MX9 family. Best regards, Salas. Re: How do I implement Secure Boot on the i.MX95? Hello, Just adding a practical reference here for anyone else working on Secure Boot with the i.MX95. As mentioned above, the i.MX95 uses AHAB rather than the HABv4 approach used on the i.MX8MP, so the signing and boot authentication workflows are different. At RidgeRun, we've documented a step-by-step guide for implementing Secure Boot on the i.MX95 using Yocto, covering AHAB key generation, SRK fuse table generation, image signing with NXP's CST, and validation of signed boot images. It also includes an alternative signing workflow using PKCS#11 and SoftHSM2. The guide uses the Toradex Verdin i.MX95 as its reference platform and focuses on development-stage signing and validation, without programming security fuses or closing the device. For anyone looking for a hands-on reference alongside NXP's documentation, you can find it here: https://developer.ridgerun.com/wiki/index.php/RidgeRun_Platform_Security_Manual/Getting_Started/NXP_i.MX95/Yocto_Build_Process/Secure_Boot Hope this is useful to others working on i.MX95 security! Best Regards
View full article
NCF3321AHF 数据手册 需要NCF3321AHF器件的数据手册。 Re: NCF3321AHF datasheet 你好, 您请求的文件属于机密文件,受保密协议 (NDA) 约束,仅可通过安全文件访问。请参考以下指南访问安全文件: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 如果您还有其他问题,请告诉我。 此致, 阿隆德拉
View full article
imx8mp Android System Fast Boot Solution 你好! 我参考Android System Fast Boot Solution - Study and Summary of Hibernate_v1.pdf 在imx8mp android14  源码是source imx-android-14.0.0_1.0.0/imx_android_setup.sh 修改完会出现GPU的报错,详情见附件,这个需要怎么解决 Re: imx8mp Android System Fast Boot Solution Hi @jieh朱 The default BSP GPU driver code does not support execution upon GPU hibernation and power-on; NXP has not tested this. You can refer to the power-on/power-off handling of `echo mem`, but `echo disk` requires separate verification of GPU driver and buffer recovery. Best Regards, Zhiming
View full article
NCF3321AHF datasheet need datasheet for NCF3321AHF part. Re: NCF3321AHF datasheet Hello,  The document you are asking for is confidential, under NDA and is available through Secured Files only, use the following guide to gain access to secured files: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf Please let me know if you have further issues Best regards,  Alondra
View full article
FRDM-i.MX93 Support for Yocto Kirkstone Hi, We are currently using Yocto Kirkstone on our i.MX8MQ project and would like to evaluate the same image on the FRDM-i.MX93 board. The meta-imx-frdm repository appears to support Scarthgap. Is there an official Kirkstone-compatible branch or BSP available for FRDM-i.MX93? If not, is there any recommended approach to enable FRDM-i.MX93 support with Kirkstone? Thank you. Yocto Project Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @Zhiming_Liu , Thank you for your response. We are currently using the NXP Kirkstone BSP (LF5.15.71_2.2.0) for our i.MX8MQ project. Could you please clarify whether this BSP can be used as the starting point for porting the meta-imx-frdm layer to Kirkstone? Also, is there a recommended Kirkstone branch or release of the NXP BSP that already includes the necessary i.MX93 processor support? Our objective is to run our existing Kirkstone-based project image on FRDM-i.MX93, with the necessary board-specific modifications. Thank you for your guidance. With regards Ajil Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @ap3415  A Yocto release is needed to port the meta-imx-frdm layer to Kirkstone. Best Regards, Zhiming Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @ap3415  You may try using the Kirkstone-based BSP release lf-5.15.71-2.2.2  and porting the FRDM-i.MX93 configurations from the Scarthgap-based meta-imx-frdm layer. In addition to the machine configuration, please also review the corresponding U-Boot configuration, kernel device tree, board-support patches and recipe dependencies. Since this combination has not been officially validated, some adaptation may be required due to the differences between the Kirkstone and Scarthgap BSP versions. Best Regards, Zhiming
View full article
FRDM-i.MX93 Yocto・カークストーン対応 こんにちは、 現在、i.MX8MQプロジェクトでYocto Kirkstoneを使用しており、同じ画像をFRDM-i.MX93ボード上で評価したいと考えています。 meta-imx-frdm リポジトリはScarthgapをサポートしているようです。FRDM-i.MX93用の公式のKirkstone互換ブランチやBSPはありますか? もしそうでなければ、KirkstoneでFRDM-i.MX93のサポートを有効にするための推奨方法はありますか? よろしくお願いします。 Yocto Project Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは@Zhiming_Liuさん ご返信ありがとうございます。 現在、i.MX8MQプロジェクトではNXP Kirkstone BSP(LF5.15.71_2.2.0)を使用しています。 このBSPをmeta-imx-frdmレイヤーをKirkstoneに移植する出発点として使えるのか、教えていただけますか? また、必要なi.MX93プロセッササポートが既に含まれている、KirkstoneのおすすめのNXP BSPブランチやリリースはありますか? 私たちの目標は、既存のKirkstoneベースのプロジェクトイメージを、必要なボード固有の変更を加えた上で、FRDM-i.MX93上で実行することです。 ご指導ありがとうございました。 に関して アジル Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは、 @ap3415さん Meta-imx-frdmレイヤーをKirkstoneに移植するにはYoctoリリースが必要です。 よろしくお願いします、 志明 Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは、 @ap3415さん KirkstoneベースのBSPリリースlf-5.15.71-2.2.2を使用し、Scarthgapベースのmeta-imx-frdmレイヤーからFRDM-i.MX93構成を移植してみてください。 マシンの設定に加えて、対応するU-Boot設定、カーネルデバイスツリー、ボードサポートパッチ、レシピ依存関係も確認してください。この組み合わせは公式に検証されていないため、カークストーン版とスカースギャップ版のBSPの違いにより、何らかの調整が必要になる場合があります。 よろしくお願いします、 志明
View full article
NCF3321AHFデータシート NCF3321AHF部品のデータシートが必要です。 Re: NCF3321AHF datasheet こんにちは、 ご依頼の文書は機密であり、NDAの下でSecured Filesを通じてのみ利用可能です。以下のガイドをご利用ください。Secure Filesへのアクセスは以下のガイドをご利用ください: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 他に問題があればお知らせください よろしくお願いします、 アロンドラ
View full article
How do I implement Secure Boot on the i.MX95? 我在imx8mp 上完成了 安全启动的流程。 8mp 上使用 HABv4 实现安全启动。 imx95 也是使用HABv4实现安全启动吗? 编译flash.bin  没有看到 CSF block ,sld hab block 等信息。 我应该如何完成 imx95 的安全启动? Re: How do I implement Secure Boot on the i.MX95? 你好@yyn 希望你一切都好。 请参阅 U-boot 文档中的 introduction_ahab 部分。 本文解释了 i.MX9 系列的安全启动过程。 顺祝商祺! 萨拉斯。 Re: How do I implement Secure Boot on the i.MX95? 你好, 这里补充一点实用参考,供其他使用 i.MX95 进行安全启动的人员参考。 如上所述,i.MX95 使用的是 AHAB 而不是 i.MX8MP 上使用的 HABv4 方法,因此签名和启动认证工作流程有所不同。 在 RidgeRun,我们编写了一份使用 Yocto 在 i.MX95 上实现安全启动的分步指南,涵盖了 AHAB 密钥生成、SRK 熔丝表生成、使用 NXP 的 CST 进行映像签名以及对已签名启动映像的验证。它还包括使用 PKCS#11 和 SoftHSM2 的替代签名工作流程。 该指南以 Toradex Verdin i.MX95 为参考平台,重点关注开发阶段的签名和验证,而不涉及网络安全熔丝的编程或设备的关闭。 如果您想在参考 NXP 官方文档的同时获取一些实际操作方面的资料,可以在这里找到: https://developer.ridgerun.com/wiki/index.php/RidgeRun_Platform_Security_Manual/Getting_Started/NXP_i.MX95/Yocto_Build_Process/Secure_Boot 希望这对其他从事 i.MX95 网络安全研究的人有所帮助! 顺祝商祺!
View full article
imx8mp Android システムファストブートソリューション 你好! 我参考Android システム高速ブート ソリューション - Hibernate_v1.pdf の調査と概要 imx8mp android14 で  源码是source imx-android-14.0.0_1.0.0/imx_android_setup.sh GPU の不具合が発生する可能性があるため、アクセサリの修正が完了しました。これには解決が必要です Re: imx8mp Android System Fast Boot Solution こんにちは@jieh朱 デフォルトのBSP GPUドライバコードは、GPUの休止状態および電源投入時の実行をサポートしていません。NXPはこの点についてテストを行っていません。`echo mem`の電源投入/電源オフ時の処理については参考になりますが、`echo disk`ではGPUドライバとバッファのリカバリについて別途検証が必要です。 よろしくお願いします、 志明
View full article
KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example Dear NXP Support, I would like to inquire about the low power functionality of the KW47. Environment MCU: KW47 SDK: SDK_26_03_00_KW47-EVK IDE: IAR Embedded Workbench RTOS: FreeRTOS Hardware: Custom Board Our goal is to reduce power consumption while operating as a BLE Peripheral. I have attached a diagram illustrating the intended behavior. Please note that the figure is a conceptual illustration and does not represent actual current consumption values. It is intended to show the expected relationship between Deep Sleep operation and BLE-related events. The intended behavior is as follows: Deep Sleep is used as the low power mode. Advertising transmission is handled by the BLE stack and SDK. Low power operation is enabled immediately after startup. The device automatically enters Deep Sleep when FreeRTOS enters the Idle state. While operating as a BLE Peripheral and continuing advertising, the CPU enters Deep Sleep whenever it becomes idle. The device wakes only when BLE stack processing is required, such as during Advertising Events, Connection Requests, or Connection Events, and returns to Deep Sleep after the required processing has completed. Based on the Low Power Application Developers Guide, it appears that Bluetooth LE applications can use Deep Sleep even while advertising. However, we could not determine which SDK example project should be used as a reference for this implementation. Could you please advise on the following points? What is the recommended approach to achieve the behavior described above? Which SDK example project should be used as a reference? Is there any example that automatically enters Sleep/Deep Sleep while advertising and automatically wakes up when BLE events occur? What is the recommended behavior while a BLE connection is established? Is it recommended to enter Deep Sleep between Connection Intervals, or should the device remain active while connected? Thank you for your support. Best regards,     Protocol: Bluetooth Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example Hi Habib, Thank you for the information and for sharing AN14554. I will review the document, especially Sections 3.2.1 and 4.2.2.6, to better understand the recommended low-power software configuration and Deep Sleep behavior during BLE connection. I appreciate your support. Best regards, hyama Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example Hello @hyama, Please refer to AN14554, which provides the configuration steps to achieve an optimized low-power profile while maintaining high system performance. It also describes the measurement setup and procedures used to measure the current consumption of the KW47. Specifically, Section 3.2.1 describes the recommended software configuration for low-power operation. this example is available in both baremetal and FreeRTOS versions. Also, section 4.2.2.6 covers the connection mode measurements and confirms that the device enters Deep Sleep between Connection Intervals.  BR, Habib
View full article
Fuses programming on 8ULP - for booting from eMMC Hello everybody, Recently I spent some time for trying to program Fuses on an 8ULP board to get it booted from eMMC. These findings might be helpful for those who need to perform this: Manual Procedure: Boot into U-Boot via UUU, stop autoboot, then: => fuse prog -y 4 1 0x00400000 => fuse prog -y 3 7 0x00008000 => reset After reboot, verify: => fuse read 4 1 Word 0x00000001: 00400000 => fuse read 3 7 Word 0x00000007: 00008000 Disconnect USB, power cycle - board boots from eMMC. UUU script: uuu_version 1.2.39 # prog-boot-fuses-evk.lst # Programs eMMC-boot fuses (Boot Config and BT_FUSE_SEL) on a CLEAN EVK-board 8ULP #SDPS: boot -f flash.bin SDPS: boot -f u-boot-imx8ulp-evk-uuu.imx SDPV: delay 2000 #SDPV: write -f flash.bin -skipspl SDPV: write -f u-boot-imx8ulp-evk-uuu.imx -skipspl SDPV: jump FB: ucmd fuse prog -y 4 1 0x00400000 FB: ucmd fuse prog -y 3 7 0x00008000 i.MX8ULP Re: Fuses programming on 8ULP - for booting from eMMC For anyone visiting this page while searching for the fuse map for the imx8ulp, it's attached as the reference manual (IMX8ULPRM) as a spreadsheet. It's not retrievable when viewing in a browser, you must use a PDF viewer like Okular. This is a bad trend by NXP to hide documentation like this. I also encountered the 'feature' when searching for pinmux options for the imx8ulp, which were attached to the Data Sheet (IMX8ULPCEC).
View full article
熔丝在 8ULP 上编程-用于从 eMMC 启动 大家好 最近我花了一些时间尝试在 8ULP 板上对 熔丝 进行编程,让它从 eMMC 启动。 这些发现可能会对需要进行这项工作的人有所帮助: 手动程序: 通过 UUU 启动 U-Boot,停止自动启动,然后: = > 熔丝 prog-y 4 1 0x00400000 = > 熔丝 prog-y 3 7 0x00008000 = > RESET 重新启动后,进行验证: => 熔丝 read 4 1 字 0x00000001: 00400000 => 熔丝 read 3 7 Word 0x00000007: 00008000 断开 USB 连接,重启电源-从 eMMC 启动主板。 UUU 脚本: uuu_version 1.2.39 # prog-boot-fuses-evk.lst # 在 CLEAN EVK-Board 8ULP 上编程 eMMC-boot 熔丝(启动配置和 BT_FUSE_SEL) #SDPS: 启动 -f flash.bin SDPS: 启动 -f u-boot-imx8ulp-evk-uuu.imx SDPV: delay 2000 #SDPV: write -f flash.bin -skipspl SDPV: write -f u-boot-imx8ulp-evk-uuu.imx -skipspl SDPV: jump FB: ucmd 熔丝 prog -y 4 1 0x00400000 FB: ucmd 熔丝 prog -y 3 7 0x00008000 i.MX8ULP Re: Fuses programming on 8ULP - for booting from eMMC 对于任何在搜索 imx8ulp 的 fuse map 时访问此页面的用户,它以电子表格的形式作为参考手册 (IMX8ULPRM) 附上。在浏览器中查看时无法读取,必须使用像 Okular 这样的 PDF 查看器。NXP 这样做隐藏文档,是一种不好的做法。我在查找 imx8ulp 的引脚复用选项时也遇到了这个“功能”,这些选项附在数据手册 (IMX8ULPCEC) 中。
View full article
imx8mp 安卓系统快速启动解决方案 你好! 我参考Android系统快速启动解决方案-Hibernate_v1的学习与总结.pdf 在imx8mp android14  是源码imx-android-14.0.0_1.0.0/imx_android_setup.sh 修改完成会出现GPU的报错,详情见附件,这个需要怎么解决 Re: imx8mp Android System Fast Boot Solution Hi @jieh朱  默认BSP的GPU驱动代码不支持GPU休眠重新上电执行,NXP没有测试过。可以参考 echo mem 的上下电处理,但 echo disk 必须单独验证 GPU 驱动和缓冲区的恢复。 Best Regards, Zhiming
View full article
KW47 在 BLE 广播期间进入深度睡眠状态 - 推荐方法和参考示例 尊敬的NXP技术支持: 我想咨询一下KW47的低功耗功能。 环境 MCU:KW47 SDK:SDK_26_03_00_KW47-EVK IDE:IAR Embedded Workbench 实时操作系统:FreeRTOS 硬件:定制板 我们的目标是在作为 BLE 外设运行时降低功耗。 我附上了一张图表,说明了预期的行为。 请注意,该图为概念示意图,并不代表实际的当前消耗值。其目的是展示深度睡眠操作与 BLE 相关事件之间的预期关系。 预期行为如下: 深度睡眠模式用作低电源模式。 广告传输由 BLE 协议栈和 SDK 处理。 启动后立即启用低功耗模式。 当 FreeRTOS 进入IDLE状态时,设备会自动进入深度睡眠状态。 当 CPU 作为 BLE 外围设备运行并持续广播时,CPU 会在空闲时进入深度睡眠状态。 设备仅在需要 BLE 协议栈处理时才会唤醒,例如在广播事件、连接请求或连接事件期间,并在所需处理完成后返回深度睡眠。 根据低功耗应用开发者指南,蓝牙低功耗应用即使在广播期间也可以使用深度睡眠模式。但是,我们无法确定应该使用哪个 SDK 示例项目作为此实现的参考。 请您就以下几点提供建议? 为实现上述行为,推荐采用什么方法? 应该使用哪个 SDK 示例项目作为参考? 是否有任何示例可以在广播时自动进入睡眠/深度睡眠状态,并在发生 BLE 事件时自动唤醒? 建立 BLE 连接时,建议采取哪些行为?是否建议在连接间隔期间让设备进入深度睡眠状态,还是应该在连接期间保持设备处于活动状态? 感谢您的支持。 顺祝商祺!     协议:蓝牙 Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example 你好,哈比卜, 感谢您提供的信息和分享 AN14554。 我将仔细阅读该文档,特别是第 3.2.1 节和第 4.2.2.6 节,以便更好地了解推荐的低功耗软件配置和 BLE 连接期间的深度睡眠行为。 感谢您的支持。 此致, 海马 Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example 你好@hyama , 请参考AN14554 ,其中提供了在保持高系统性能的同时实现优化低功耗我的的配置步骤。它还描述了用于测量 KW47 电流消耗的测量装置和程序。 具体而言,第 3.2.1 节描述了低功耗运行的推荐软件配置。此示例在裸机和 FreeRTOS 版本中均可用。此外,4.2.2.6 节涵盖了连接模式的测量,并确认设备在连接间隔期间进入深度睡眠状态。 BR, 哈比卜
View full article
i.MX95でセキュアブートを実装するにはどうすればよいですか? imx8mpのセキュアブートプロセスを完了しました。 セキュアブートは、8mp上でHABv4を使用して実現されます。 imx95もセキュアブートの実装にHABv4を使用していますか? flash.binをコンパイルした際、CSFブロックやsld habブロックなどの情報は表示されませんでした。 IMX95でセキュアブートを実行するにはどうすればよいですか? Re: How do I implement Secure Boot on the i.MX95? こんにちは@yyn お元気でお過ごしのことと思います。 U-ブート のドキュメントにある introduction_ahab をご覧ください。 i.MX9ファミリーのSecure Bootプロセスについて説明しています。 よろしくお願いいたします。 サラス。 Re: How do I implement Secure Boot on the i.MX95? こんにちは、 i.MX95でセキュアブートに取り組んでいる他のユーザーのために、実用的な参考情報としてここに追加しておきます。 前述の通り、i.MX95はi.MX8MPで使われているHABv4方式ではなくAHABを使用しているため、署名と起動認証のワークフローが異なります。 RidgeRunでは、Yoctoを使ったi.MX95へのSecure Boot実装に関するステップバイステップガイドを公開しており、AHABキー生成、SRKヒューズテーブル生成、NXPのCSTによるイメージ署名、署名付きブートイメージの検証をカバーしています。また、PKCS#11とSoftHSM2を使用した代替署名ワークフローも含まれています。 ガイドはToradex Verdin i.MX95を参考プラットフォームとして使用し、セキュリティヒューズのプログラミングやデバイスのクローズを行わず、開発段階での署名と検証に焦点を当てています。 NXPのドキュメントに加えて実践形式の参考資料を探している方は、こちらでご覧いただけます: https://developer.ridgerun.com/wiki/index.php/RidgeRun_Platform_Security_Manual/Getting_Started/NXP_i.MX95/Yocto_Build_Process/Secure_Boot i.MX95のセキュリティに取り組んでいる方々の参考になれば幸いです! よろしくお願いいたします。
View full article
i.MX 93 AHAB Keys revocation procedure doubts Hello, we are working on SRK revocation for an i.MX93 product that is updated over the air, and we could not find a complete description of the procedure. We have read the thread imx93: SRK revocation (https://community.nxp.com/t5/i-MX-Processors/imx93-SRK-revocation/td-p/1827004), the Reference Manual (§9.5.1.3.2.3, SRK revoke) and AN14954, and we would like to confirm a few points. 1. ahab_commit in the field In the thread above, a container signed with SRK2 and Revocations = 0x1 did not revoke SRK1 until ahab_commit 0x10 was run. We would like to understand how the commit is meant to be used on devices that receive later updates: - Is it enough to run the commit once, after the container carrying the revoke mask has been authenticated? - Or can the commit be left permanently in the boot command once at least one key has been revoked, so that any build installed afterwards applies the revocation? Is it safe and without effect when there is nothing new to commit? - Must the containers of later builds keep the same srk_revocations value (the Reference Manual says the ELE checks that the revoke bits in the container match what is already set in the fuses), and which containers have to carry it (the boot container and the OS container)? 2. Multiple or cross revocation A container signed with one SRK can revoke a different one (as in the thread). Can the revoke mask contain several bits, including all the other SRKs? Is there a check in the ELE that prevents a container signed with a compromised SRK from revoking the remaining ones, or is this something that has to be handled by key management? 3. Checking the revocation state Is there a supported way to know which SRKs are revoked, from U-Boot or from Linux? With fuse sense most words beyond bank 6 return ERROR on our board, and the nvmem interface shows zeros for them. Would a functional check (authenticating a small container signed with each SRK and looking at the ELE events) be a reasonable approach? 4. fuse override for tests From AN14954 we understood that the shadow fuses can be overridden in OEM Open without burning the e-fuses. Does the ELE use the shadow value of the SRK hash fuses when authenticating containers, so that the signing chain can be tested this way without writing the hash? And is there any way to simulate a revocation with this mechanism? 5. SRK table after closing The hash covers the whole SRK table (4 keys). Once the hash is written, can the table still be changed (guess no since they are fused), even for positions that were left empty at the time? So basically, is it possible to only write 2 keys and add 2 later? We understand that part of the fuse information is covered by the Security Reference Manual under NDA. If so, a pointer to the relevant document or section, or even a high-level description of the procedure, would already help a lot. Given the upcoming Cyber Resilience Act, key revocation is going to become a standard requirement for many products, so a clear public description would be very valuable Thanks in advance
View full article
i.MX 93 AHABキーの失効手続きに関する疑問 こんにちは、 現在、i.MX93製品のSRK取り消しを進めており、無線で更新されていますが、手順の完全な説明は見つかりませんでした。私たちはThread imx93を読みました:SRK取り消し(https://community.nxp.com/t5/i-MX-Processors/imx93-SRK-revocation/td-p/1827004)、リファレンス・マニュアル(§9.5.1.3.2.3、SRK取り消し)、およびAN14954。いくつかの点を確認したいと思います。 1. 現場でのahab_commit 上記のThreadでは、SRK2とRevocations = 0x1で署名されたコンテナは、ahab_commit 0x10実行されるまでSRK1を取り消しませんでした。私たちは、コミットが後のアップデートを受けるデバイスでどのように使われるのかを理解したいと考えています。 - リヴォークマスクを搭載したコンテナが認証された後、コミットを一度実行するだけで十分でしょうか? - あるいは、少なくとも1つのキーが取り消された後も、コミットをブートコマンドに永久に残し、SO、その後インストールされたビルドがその取り消しを適用できるようにできますか?新しい行動がなければ安全で効果がないのでしょうか? - 後のビルドのコンテナは同じsrk_revocations値を保持しなければなりませんか?(リファレンス・マニュアルによると、ELEはコンテナ内のリボークビットがヒューズに既に設定されているものと一致しているかを確認します)、どのコンテナ(ブートコンテナとOSコンテナ)がそれを運ぶ必要がありますか? 2. 複数またはクロスの取り消し 1つのSRKで署名されたコンテナは、別のSRKを取り消すことができます(Threadのように)。リヴォークマスクは他のすべてのSRKを含めて複数のビットを含めることはできますか?ELEに、侵害されたSRKで署名されたコンテナが残りのSRKを取り消すのを防ぐチェック機能はありますか?それとも鍵マネジメントが処理しなければならないのでしょうか? 3. 取り消し状態の確認 どのSRKが取り消されたか、U-BootからかLinux側で確認できるサポートされた方法はありますか?ヒューズセンスを使うと、バンク6以降のほとんどのワードはボード上でエラーを返し、nvmemインターフェースではそれらに対してゼロが表示されます。機能チェック(各SRKに署名された小さなコンテナを認証し、ELEイベント情報を確認する)は妥当な方法でしょうか? 4. 試験用のヒューズオーバーライド AN14954から、OEM Openではシャドウヒューズを上書きしてもeヒューズを焼き切れないと分かりました。ELEはコンテナ認証時にSRKハッシュヒューズのシャドウ値を使い、ハッシュを書かずにこの方法で署名チェーンをテストできるのでしょうか?この仕組みを使って、免許の取り消しをシミュレートする方法はありますか? 5. 閉鎖後のSRKテーブル このハッシュはSRKテーブル全体(4つのキー)をカバーしています。ハッシュが書き込まれた後、テーブルは(フュージョンされているのでおそらく無理です)変更できますか?その時点で空いた位置でも?SO、2つのキーだけを書いて後で2つ追加することは可能でしょうか? 信管情報の一部はNDAに基づくセキュリティリファレンスマニュアルでカバーされていると理解しています。もしそうなら、関連する文書やセクションへのポインタ、あるいは手順の高レベルの説明があれば、すでに大いに役立ちます。今後のサイバーレジリエンス法(Cyber Resilience Act)を踏まえ、キーの取り消しは多くの製品で標準的な要件となるため、明確な公開説明は非常に価値があります 前もって感謝します
View full article
KW47 BLEアドバタイジング中のディープスリープ - 推奨アプローチと参考例 NXPサポートの皆様、 KW47の低電力機能についてお伺いしたいのですが。 環境 MCU:KW47 SDK:SDK_26_03_00_KW47-EVK IDE:IAR Embedded Workbench RTOS: FreeRTOS ハードウェア: カスタムボード 私たちの目標は、BLEペリフェラルとして運用する際の消費電力を削減することです。 意図した動作を示す図を添付しました。 この図は概念的な図解であり、実際の現在の消費量を表すものではないことにご注意ください。これは、ディープスリープ作戦とBLE関連イベント情報との期待される関係を示すことを目的としています。 意図された動作は以下のとおりです。 ディープスリープは低電力モードとして使用されます。 広告の送信はBLEスタックとSDKによって処理されます。 起動直後から低消費電力動作が有効になります。 FreeRTOSがアイドル状態になると、デバイスは自動的にディープスリープ状態に入ります。 BLEペリフェラルとして動作し、広告を続けている間、CPUはアイドルになるとディープスリープに入ります。 デバイスはBLEスタックプロセッシングが必要な場合のみ、例えば広告イベント情報、接続リクエスト、接続イベント情報の際にのみ起動し、必要なプロセッシングが完了するとディープスリープに戻ります。 Low Power Application Developers Guideによると、Bluetooth LEアプリケーションは広告中でもディープスリープを利用できるようです。しかし、この実装の参照としてどのSDKサンプルプロジェクトを使うべきかは判断できませんでした。 以下の点についてアドバイスいただけますか? 上記のような動作を実現するための推奨されるアプローチは何ですか? どのSDK例プロジェクトを参考にすべきでしょうか? 広告中に自動的にスリープ/ディープスリープに入り、BLEイベント情報が発生すると自動的に起きる例はありますか? BLE接続確立時の推奨される動作は何ですか?接続間隔の間にディープスリープに入るのが推奨されますか?それともコネクテッド中はデバイスはアクティブのままにすべきでしょうか? 再開まで今しばらくお待ちください。 よろしくお願いいたします。     プロトコル:Bluetooth Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example こんにちは、ハビブさん。 情報提供とAN14554の共有、ありがとうございます。 特に3.2.1および4.2.2.6のセクションを確認し、BLE接続時の推奨される低消費電力ソフトウェア構成とディープスリープの挙動をよりよく理解します。 サポートいただき感謝します。 よろしくお願いします、 ヒヤマ Re: KW47 Deep Sleep During BLE Advertising - Recommended Approach and Reference Example こんにちは、 @hyama さん。 最適な低消費電力プロファイルを実現しつつ、高いシステム性能を維持するための設定手順については、 AN14554を参照してください。また、KW47の電流消費量を測定するために使用された測定設定と手順についても説明しています。 具体的には、セクション3.2.1は低消費電力動作のための推奨ソフトウェア構成を説明しています。このサンプルは、ベアメタル版とFreeRTOS版の両方で利用可能です。また、4.2.2.6項では接続モードの測定について説明し、接続間隔中にデバイスがディープスリープ状態に入ることを確認しています。 BR、 ハビブ
View full article
MCUXpresso Tooltime Episodes NXP LinkedIn Live series Tool Time: practical embedded development, on demand Catch up on conversations and demonstrations featuring NXP development tools, SDK workflows, board enablement, debugging, visualization, configuration and user-interface design. Browse past episodes See how the MCUXpresso ecosystem comes together Tool Time brings developers closer to the software and workflows used to build with NXP microcontrollers. Across the series, the episodes cover MCUXpresso SDK releases, VS Code integration, CMake and Kconfig projects, Configuration Tools, GUI Guider, FreeMASTER, LinkServer, Serial Memory Tool, MCUXpresso Installer, cloud connectivity and FRDM board expansion. Use this replay library to explore each topic, meet the hosts and guests, and go directly to the available LinkedIn episode. What the series provides Focused sessions on MCUXpresso tools and embedded-development workflows Topics spanning setup, configuration, build systems, debug, visualization and prototyping Conversations with NXP specialists and ecosystem guests Direct links to rewatch each available episode on LinkedIn Watch past episodes Choose an episode and select Watch on LinkedIn. Newest episodes are listed first. NOVEMBER 2026   |   EMBEDDED UI with GUI GUIDER From Prompt to Embedded UI with GUI Guider Describe the GUI you want and let AI help bring the concept to life. Host: Mike Susen   Guest: Zhenhua Luo Watch on LinkedIn OCTOBER 2026   |   AGENTIC AI Introducing our new Agentic AI Toolkit Explore how AI agents can discover, understand and use products to help improve customer enablement. Host: Kyle Dando   Guest: Marius-Lucian Andrei Watch on LinkedIn SEPTEMBER 2026   |   HARDWARE EXPANSION Adding a click shield to a FRDM board (G-Knob) A Tool Time episode focused on adding a G-Knob click shield to a FRDM board. Host: Kyle Dando   Guest: Patrik Fillner Watch on LinkedIn AUGUST 2026   |   INSTALLATION MCUXpresso Installer A focused discussion and demonstration of MCUXpresso Installer. Host: Jose Ocampo Hernandez   Guest: Alexandra Maracine Watch on LinkedIn JULY 2026   |   SERIAL MEMORY Serial Memory Tool A Tool Time session featuring the Serial Memory Tool. Host and guest: Patrik Fillner Watch on LinkedIn JUNE 2026   |   DEBUG LinkServer A focused episode covering LinkServer. Host: Kyle Dando   Guest: Cristian Lupascu Watch on LinkedIn MAY 2026   |   DATA VISUALIZATION FreeMASTER data visualization A Tool Time session focused on FreeMASTER data visualization. Host: Kyle Dando   Guest: Patrik Fillner Watch on LinkedIn APRIL 2026   |   EMBEDDED GUI GUI Guider A focused discussion and demonstration of GUI Guider. Host: Kyle Dando   Guest: Mike Susen Watch on LinkedIn MARCH 2026   |   CONFIGURATION MCUXpresso Configuration Tools A Tool Time episode focused on MCUXpresso Configuration Tools. Host: Patrik Fillner   Guest: Petr Hradsky Watch on LinkedIn FEBRUARY 2026   |   CLICK BOARDS 6 clicks A Tool Time episode titled “6 clicks.” Host: Kyle Dando   Guest: Stella Or Watch on LinkedIn JANUARY 2026   |   BUILD CONFIGURATION CMake and Kconfig projects on FRDM-MCXN947 A session on CMake and Kconfig projects using the FRDM-MCXN947. Host: Kyle Dando   Guest: Jose Ocampo Hernandez Watch on LinkedIn DECEMBER 2025   |   CLOUD CONNECTIVITY Bluetooth to Cloud on MCX W71 and RW612 A Bluetooth-to-cloud project running on the MCX W71 and RW612. Host: Kyle Dando   Guest: Chris Gammell, Golioth Watch on LinkedIn NOVEMBER 2025   |   RELEASE HIGHLIGHTS SDK 25.10, VS Code and Configuration Tools A session covering the 25.10 SDK release, VS Code integration and streamlined Configuration Tools. Host: Kyle Dando   Guest: Jose Ocampo Hernandez Watch on LinkedIn OCTOBER 2025   |   SERIES OVERVIEW MCUXpresso IDEs, SDK, Configuration and Security A session covering MCUXpresso IDEs, SDK, Configuration Tools and security tooling. Host: Kyle Dando Replay link not listed Episode links open LinkedIn in a new browser tab. LinkedIn sign-in may be required to view some replays. Application Code Hub FreeMASTER LinkServer MCUXpresso Config Tools MCUXpresso for VS Code MCUXpresso SDK
View full article
Flexcan callback is not executed ocassionally I have implemented flexcan callback to receive FLEXCAN_EVENT_RX_COMPLETE and FLEXCAN_EVENT_TX_COMPLETE events. When RX event is generated, the received can buffer is copied into a queue. And when TX event is generated a can_available flag is set to true to send the next can frame.  Please find the code snippet below void flexcan1_callback(uint8 instance, Flexcan_Ip_EventType eventType, uint32 buffIdx, const Flexcan_Ip_StateType *flexcanState) { (void)flexcanState; (void)buffIdx; if (eventType == FLEXCAN_EVENT_RX_COMPLETE) { can_frame_t cebms_can_frame = {.type_e=CAN_EXTD_ID}; if (buffIdx == can_md_idx_rx_u8[CAN_STD_ID]) { cebms_can_frame.type_e = CAN_STD_ID; } xQueueSendFromISR(chg_rx_queue[1], (const void*)&cebms_can_frame, &xHigherPriorityTaskWoken); FlexCAN_Ip_Receive(instance, buffIdx, &rxData[instance][cebms_can_frame.type_e], FALSE); } else if ((FLEXCAN_EVENT_TX_COMPLETE == eventType)) { can_tx_available[instance] = TRUE; } }       boolean Can_Tx(uint8_t instance, can_frame_t* can_frame) { uint16_t can_timeout = 0xFFFFU; boolean can_return = FALSE; while ((can_tx_available[instance] == FALSE) && (can_timeout)) { can_timeout--; } if (can_tx_available[instance] == TRUE) { can_tx_available[instance] = FALSE; FlexCAN_Ip_Send(instance, can_md_idx_tx_u8[can_frame->type_e], &can_data_info[can_frame->type_e], can_frame->id.u32, (uint8 *)&can_frame->data.u8a); can_return = TRUE; printf("SUCCESS: 0x%08X", (unsigned int)can_frame->id.u32); } else { printf("FAILED: 0x%08X", (unsigned int)can_frame->id.u32); } return can_return; }   Here, sometimes when I try to transmit multiple can frames sequentially using the above function, FAILED is printed multiple times for those can ids in the sequence for approx 20 seconds. And suddenly can frames start getting transmitted and SUCCESS is printed. I have also attached a CAN logger to verify this, and the result is same on the CAN logger. When FAILED is printed, no messages are seen on the CAN logger.   Please help me out on this matter and whether my implementation is correct or not.   Thanks Gauri   #s32k311 #flexcan   Re: Flexcan callback is not executed ocassionally Hello @geeznxp, I will assume RTD 3.0.0 is used (based on you post history). I will also assume your other node is the PCAN-USB analyzer. From your description, I cannot immediately diagnose your application, however, here are some points to check: 1. Is can_tx_available declared as volatile? Since it is written inside an ISR (TX_COMPLETE callback) and read inside a task-level while-loop. Without the volatile qualifier, the compiler is free to cache false or never reload the variable in other iterations. 2. The ~20 second interval may also point to a bus-off event. Add a bus-off error case in the callback, to detect and handle the bus-off event.  3. I would also check ESR1 registers in the interval where FAILED is printed multiple times. Lastly, general points to check, CAN bus termination, bit rate configuration, FlexCAN_Ip return value, FlexCAN error callback registered. Best regards, Julián
View full article