Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
电路板支持包。 中的 A53 核心频率 大家好,社区和NXP导出团队! 电路板支持包。 48 手册中有关于 A53 核心时钟的信息,如下所示。 root@s32g399aevb3:/sys/设备/system/cpu/cpufreq/policy0/# cat scaling_available_frequencies 48148 54166 61904 72222 86666 104000 136842 200000 371428 1300000 我的问题是,为什么时钟频率直接从 1.3G 降到 371M,而没有 866/650 可选?是不是有什么特殊原因? 顺祝商祺! 光宇 Re: A53 core frequency in S32G3 BSP 你好, @Guangyu_D 感谢分享。 1. 从现有文件来看,我没有看到对此有任何特殊考虑。 2. 目前的结果是由最初实现中引入的原始频率采样策略引起的,它在允许的频率范围的限制之间选择均匀间隔的分频器,而不是均匀间隔的频率。这自然会在高频端产生稀疏的频率点,在低频端产生更密集的频率点。 BR 陈银
View full article
HSE option Hello, For some export purpose, we would like to remove the HSE (crypto parts) module. I did not find any reference whithout HSE module in your lists, do you confirm that no S32G2 or S32G3 references are available without HSE (crypto parts) module? B.R. Re: HSE option Hello, @COLLIN_O  Thanks for the post. From the latest product introduction of both S32G2/3, HSE is included in all of the variants listed. BR Chenyin
View full article
FS26スタンバイ NXPのエキスパートの方、こんにちは。FS26に関連する問題が発生しました。 テストの結果、FS26がスタンバイモードに移行できないことが判明しました。シングルステップ実行は継続されますが、FS26はスタンバイモードに移行できません。Sbc_fs26_SetOperatingMode()インターフェースがフルスピードで実行されるたびにリセットが発生します。ハードウェアウェイク信号は削除されており、リセットピンには他の信号は接続されていません。 小型エンジンドライバー Re: FS26 standby こんにちは、チェンシュウ どの状態からスタンバイ状態に切り替えましたか? 実行したコマンドを教えていただけますか? Re: FS26 standby こんにちは、ご協力ありがとうございました。問題は解決しました。 テストの結果、ウェイクアップ時間が5ms未満の場合、M_WIO_FLGレジスタの読み取り値が0となり、ウェイクアップソースが読み取れないことが判明しました。この点についてご回答いただけますでしょうか?よろしくお願いいたします。 Re: FS26 standby こんにちは、チェンシュー 新しいトピックについては、新しいチケットを送信してください! https://support.nxp.com/s/?language=en_US
View full article
FRDM-MX95 PRO software packages? I was wondering what OS software packages will be available for the MX95 PRO?  Will Android AAOS be available for it as a demo image?  Is there anyone we can communicate with about what will specifically be available? Re: FRDM-MX95 PRO software packages? currently, only linux 6.18.20_2.0.0 demo images for imx95 frdm pro Embedded Linux for i.MX Applications Processors | NXP Semiconductors you can download demo images from the link above, for android, I checked the board file, the latest android 16.0.0_2.0.0 is based on kernel 6.18.20_2.0.0, so should support frdm pro, but this version android hasn't verified on this board yet, only 19x19 evk and 15x15 frdm Re: FRDM-MX95 PRO software packages? Any news if we will get android automotive on the frdm-mx95 or would we have to upgrade to frdm-mx95 pro version? Re: FRDM-MX95 PRO software packages? let me confirm auto android team again, the owner is on vacation, and come back office in next week, any update I will let you know it Re: FRDM-MX95 PRO software packages? refer to the link as below https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-applications-processors:ANDROID-AUTO auto android demo images are only for imx95 19x19 evk Re: FRDM-MX95 PRO software packages? Are there any plans for android or AAOS?  Seems weird that the FRDM MX95 Pro wouldn't have an AAOS version especially since the Evaluation board 19x19 has been discontinued and benched.  Is there a reason the pro being a 19x19 processor wouldn't work as the evaluation board. Re: FRDM-MX95 PRO software packages? Thanks. There seems to be a genuine lack of Android automotive support. The frdm has a lot of potential but without additional support from nxp we are left on our own. From my understanding the evk has been dropped from support from toradex and discontinued. With the frdm pro having the same hardware there should be some support. We need the BSP which would make building the images a lot easier. Re: FRDM-MX95 PRO software packages? Is there any way i can contact them to ask a question? Or could they give us some instructions on how to compile the new frdm pro board, maybe they can provide the board package file to make it easier for us to compile? Re: FRDM-MX95 PRO software packages? unfortunately, got information from auto android team that they haven't any plan to support any imx95 frdm board Re: FRDM-MX95 PRO software packages? since they don't have plan to support this yet, I don't think they can offer any packages to build Re: FRDM-MX95 PRO software packages? Even though it isn't listed yet, I just wanted to let the community know that I was able to flash Android 16.0.0_2.0.0 (L6.18.20_2.0.0 BSP) to eMMC, and it ran fine on my FRDM-IMX95-PRO board.  AOSP Android 16 worked well enough that I could deploy my own custom Trusty applet and have a corresponding Android app communicate with it afterward. I just saw Android 17.0.0_1.0.0 (L6.18.37_2.1.0 BSP) posted on the NXP website today (if Android 16 worked, I'm guessing Android 17 should work as well too)
View full article
FRDM-MX95 PRO 软件套装? 我想知道MX95 PRO会有哪些操作系统软件版本可用?是否会提供Android AAOS的演示镜像?我们能否联系到相关人员,了解具体有哪些服务或产品可供选择? Re: FRDM-MX95 PRO software packages? 目前,仅提供适用于 imx95 frdm pro 的 Linux 6.18.20_2.0.0 演示镜像。 适用于 i.MX 应用处理器的嵌入式 Linux | 恩智浦半导体 您可以从上面的链接下载演示镜像。对于安卓系统,我检查了开发板文件,最新的安卓 16.0.0_2.0.0 基于内核 6.18.20_2.0.0,因此应该支持 FRDM Pro,但这个版本的安卓系统尚未在该开发板上验证过,目前只验证过 19x19 EVK 和 15x15 FRDM。 Re: FRDM-MX95 PRO software packages? 请问frdm-mx95是否会支持Android Automotive?还是必须升级到frdm-mx95专业版? Re: FRDM-MX95 PRO software packages? 请参考以下链接。 https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-automotive-os-for-i-mx-applications-processors:ANDROID-AUTO 自动安卓演示图片仅适用于 imx95 19x19 evk Re: FRDM-MX95 PRO software packages? 我再确认一下安卓自动团队的情况,负责人正在休假,下周才会回来上班,有任何更新我会通知你。 Re: FRDM-MX95 PRO software packages? 是否有针对安卓或AAOS系统的计划?FRDM MX95 Pro 没有 AAOS 版本似乎很奇怪,尤其是考虑到评估板 19x19 已经停产并停止测试。19x19处理器的Pro版为什么不能用作评估板? Re: FRDM-MX95 PRO software packages? 我可以通过什么方式联系他们询问问题? 或者他们能否给我们一些关于如何编译新的frdm pro板的说明?也许他们可以提供板包文件,以便我们更容易地进行编译? Re: FRDM-MX95 PRO software packages? 很遗憾,我从安卓汽车团队那里得知,他们没有任何支持IMX95 FRDM主板的计划。 Re: FRDM-MX95 PRO software packages? 谢谢。目前看来,Android车载系统确实缺乏支持。frdm 具有很大的潜力,但如果没有 nxp 的额外支持,我们就只能靠自己了。据我了解,Evk 已停止获得 Toradex 的支持并停产。由于 frdm pro 与 frdm pro 采用相同的硬件,因此应该可以获得一些支持。我们需要电路板支持包。,它可以让构建镜像变得更加容易。 Re: FRDM-MX95 PRO software packages? 由于他们目前还没有支持这方面的计划,我认为他们无法提供任何构建代码包,软件包。 Re: FRDM-MX95 PRO software packages? 虽然还没有被列入名单,但我只是想告诉大家,我已经成功地将Android 16.0.0_2.0.0 (L6.18.20_2.0.0 电路板支持包。)刷入 eMMC,并且在我的FRDM-IMX95-PRO板上运行良好。 AOSP Android 16 运行良好,我可以部署自己的自定义 Trusty 小程序,并让相应的 Android 应用随后与其通信。 我今天在NXP网站上看到了Android 17.0.0_1.0.0 (L6.18.37_2.1.0 电路板支持包。) (如果Android 16可以运行,我猜Android 17也应该可以运行)。
View full article
界面隐藏问题guiguider2.0.1 guiguider2.0.1创建一个界面使用在界面右侧属性中添加hidden标志,有时候会导致其他界面也看不见,且无法恢复只能重新启动软件才可以, 回复: 界面隐藏问题guiguider2.0.1 你好@ZYQ 谢谢你提供的信息。 我可以重现这个问题。 我已经将此事报告给了我们的GUIGUIDER团队。 BR 哈里
View full article
マルチコアプロジェクトにおける追加MPU領域の設定 私は基本的に2つのSDKsのサンプルを組み合わせたプロジェクトを作っています。私はRT1170-EVKB SDKのバージョン26.09.00を使っています。このプロジェクトのアイデアは、マルチコアの例とLVGLの例を取り、M7コアがグラフィックスを実行し、その後プログラムを実行するM4コアと通信することです。そのために、SDKsの例を挙げました: freertos_message_buffers(プライマリとセカンダリの両方)をベースプロジェクトとして使用します。その後、lvgl_guider_cm7プロジェクトのコードやドライバーファイルをコピー&ペーストして、ゆっくりとグラフィックを追加しています。 私はlvgl_guider_cm7 mcux_config.hを保持しています同じファイルにしてPXPとVGLiteを使ったようにします。そのためには、フレームバッファをキャッシュ以外の場所に配置する必要があります。SDKの例で使われている共有メモリも非キャッシュに配置する必要があります。こうなると、ディスプレイにアーティファクト(本来あるべきでないオブジェクトに小さな線が入る現象)が発生します。 __USE_SHMEMプリプロセッサを外すことで直せますが、当然ながらマルチコア通信が失敗します。原因はBOARD_EarlyConfigMPU関数にあると考えています。関数の中には、次のような部分があります。 #elif defined(__MCUXPRESSO) #if defined(__USE_SHMEM) extern uint32_t __base_rpmsg_sh_mem; extern uint32_t __top_rpmsg_sh_mem; uint32_t nonCacheStart = (uint32_t)(&__base_rpmsg_sh_mem); uint32_t size = (uint32_t)(&__top_rpmsg_sh_mem) - nonCacheStart; #else extern uint32_t __base_NCACHE_REGION; extern uint32_t __top_NCACHE_REGION; uint32_t nonCacheStart = (uint32_t)(&__base_NCACHE_REGION); uint32_t size = (uint32_t)(&__top_NCACHE_REGION) - nonCacheStart; #endif このセクションでは、__USE_SHMEMプリプロセッサに基づいて、共有メモリまたは通常の非キャッシュのいずれかの非キャッシュを定義します。関数のさらに下では、MPU領域を次のように宣言しています: volatile uint32_t i = 0; ... while ((size >> i) > 0x1U) { i++; } if (i != 0) { /* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */ BOARD_EARLY_ASSERT(!(nonCacheStart % size)); BOARD_EARLY_ASSERT(size == (uint32_t)(1 << i)); BOARD_EARLY_ASSERT(i >= 5); /* Region 10 setting: Memory with Normal type, not shareable, non-cacheable */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_NONCACHE, nonCacheStart); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, i - 1); } 今度は、MPU内の両方の領域を定義して、LVGLがアーティファクトなしで動作し、rpmsgメッセージバッファが通信できるようにしたいと考えています。私の記憶領域は以下の通りです: 私が試みたのは、上記のコードを修正して両方のMPUリージョン定義を実行することでした。例えば: #elif defined(__MCUXPRESSO) extern uint32_t __base_NCACHE_REGION; extern uint32_t __top_NCACHE_REGION; uint32_t nonCacheStart = (uint32_t)(&__base_NCACHE_REGION); uint32_t nonCacheSize = (uint32_t)(&__top_NCACHE_REGION) - nonCacheStart; #if defined(__USE_SHMEM) extern uint32_t __base_rpmsg_sh_mem; extern uint32_t __top_rpmsg_sh_mem; uint32_t rpmsgShmemStart = (uint32_t)(&__base_rpmsg_sh_mem); uint32_t rpmsgShmemSize = (uint32_t)(&__top_rpmsg_sh_mem) - rpmsgShmemStart; #endif この方法だと、通常の非キャッシュ領域は常に定義され、共有メモリ領域は使用される場合にのみ定義される。MPUのリージョン定義を次のように修正しました: volatile uint32_t i = 0; ... while ((nonCacheSize >> i) > 0x1U) { i++; } if (i != 0) { /* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */ BOARD_EARLY_ASSERT(!(nonCacheStart % nonCacheSize)); BOARD_EARLY_ASSERT(nonCacheSize == (uint32_t)(1 << i)); BOARD_EARLY_ASSERT(i >= 5); /* Region 10 setting: Memory with Normal type, not shareable, non-cacheable */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_NONCACHE, nonCacheStart); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, i - 1); } #if (__USE_SHMEM) i = 0; while ((rpmsgShmemSize >> i) > 0x1U) { i++; } if (i != 0) { /* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */ BOARD_EARLY_ASSERT(!(rpmsgShmemStart % rpmsgShmemSize)); BOARD_EARLY_ASSERT(rpmsgShmemSize == (uint32_t)(1 << i)); BOARD_EARLY_ASSERT(i >= 5); /* Region 16 setting: Memory with Normal type, not shareable, non-cacheable */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_SHMEM, rpmsgShmemStart); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, i - 1); } #endif この作業を行う際に、board.h 内に追加の MPU 領域用のマクロを作成しました。こんな感じで: #define BOARD_MPU_REGION_SHMEM (16) /* rpmsg shared memory */ これらの変更を加えたことで、LVGLはアーティファクトなしで描画できるようになったが、マルチコア通信は依然として失敗する。マルチコア通信を動かすM4Threadにブレークポイントを設けました。時には最初にメッセージを受信したことを通知してトリガーされますが、メッセージデータが誤っているため、そのメッセージデータに関連するコードは実行されません。ブレークポイントが数回トリガーされると、それ以降は二度とトリガーされなくなります。 このプロジェクトを実行するために、MPU領域の定義など、何か見落としている点はありますか? Re: Multicore Project setup of an additional MPU region 変更はプライマリコアにのみ適用されました。プライマリコアはBOARD_EarlyConfigMPUを実行し、セカンダリコアはBOARD_ConfigMPUを実行するため、セカンダリコアの機能には、プライマリコアに変更を加えた動作が既に含まれています。以下は、セカンダリコアがハードウェア初期化時に実行する処理の一部です。 #elif __CORTEX_M == 4 void BOARD_ConfigMPU(void) { #if defined(__CC_ARM) || defined(__ARMCC_VERSION) ... #elif defined(__MCUXPRESSO) extern uint32_t __base_NCACHE_REGION; extern uint32_t __top_NCACHE_REGION; uint32_t nonCacheStart = (uint32_t)(&__base_NCACHE_REGION); uint32_t nonCacheSize = (uint32_t)(&__top_NCACHE_REGION) - nonCacheStart; #elif defined(__ICCARM__) || defined(__GNUC__) ... #endif #if defined(__USE_SHMEM) #if defined(__CC_ARM) || defined(__ARMCC_VERSION) ... #elif defined(__MCUXPRESSO) extern uint32_t __base_rpmsg_sh_mem; extern uint32_t __top_rpmsg_sh_mem; uint32_t rpmsgShmemStart = (uint32_t)(&__base_rpmsg_sh_mem); uint32_t rpmsgShmemSize = (uint32_t)(&__top_rpmsg_sh_mem) - rpmsgShmemStart; #elif defined(__ICCARM__) || defined(__GNUC__) ... #endif #endif そして関数の後半では次のようになります。 uint32_t i = 0; /* Only config non-cacheable region on system bus */ assert(nonCacheStart >= 0x20000000); ... while ((nonCacheSize >> i) > 0x1U) { i++; } if (i != 0) { /* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */ assert(!(nonCacheStart % nonCacheSize)); assert(nonCacheSize == (uint32_t)(1 << i)); assert(i >= 5); /* Region 0 setting: Memory with device type, not shareable, non-cacheable */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_NONCACHE, nonCacheStart); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, i - 1); } #if defined(__USE_SHMEM) i = 0; while ((rpmsgShmemSize >> i) > 0x1U) { i++; } if (i != 0) { /* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */ assert(!(rpmsgShmemStart % rpmsgShmemSize)); assert(rpmsgShmemSize == (uint32_t)(1 << i)); assert(i >= 5); /* Region 1 setting: Memory with device type, not shareable, non-cacheable */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_RPMSG_SHMEM, rpmsgShmemStart); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, i - 1); } #endif どちらのプロジェクトも、プリプロセッサで__USE_SHMEMが定義されています。以下は、セカンダリコアのメモリ構成です。 他に何か見落としている点があるのでしょうか?それとも、私の変更方法が間違っているのでしょうか?メインプロジェクトの設定にある「リンカースクリプトの管理」セクションに何か追加する必要はありますか?機会があれば、EVK-Bボード上で動作するプロジェクトの.zipをアップロードして、問題を確認したり再現したりできると思います。 Re: Multicore Project setup of an additional MPU region こんにちは、 @CMoran さん。 あなたの理解は理にかなっていますが、あなたが言及した変更がCM7とCM4の両方のコアに適用されたかどうかは明確ではありませんでした。各コアにはboard.hの定義があり、そこで、それぞれがMPUの独自の構成を使用して、初期ハードウェア初期化時にセットアップを行います。ご指摘の変更がプライマリコアのみに適用された場合、コアがメモリ領域を均等に扱わない可能性があり、その結果、このような予期せぬ動作が発生すると考えられます。 変更が両方のコアに適用され、MPU設定が一致していることを確認してください。また、両方のプロジェクトのプリプロセッサ定義で__USE_SHMEMが設定されていることも確認してください。 Re: Multicore Project setup of an additional MPU region こちらが.zipファイルですその中には、M7およびM4プロジェクトが含まれている。修正しても結局うまくいかなかったので、修正前の状態のままにしておきました。この例では、ターミナルを開いて中央のボタンを押すと、m7コアとm4コアの両方からメッセージが表示されます。画面上を移動する設定アイコンには、説明されているように多数の不具合が発生しています。 m7プロジェクトから__USE_SHMEMプリプロセッサを削除すると、設定アイコンの不具合は解消されますが、マルチコア通信が失敗します。 上記で適用した変更を加えることで設定アイコンも修正されますが、マルチコア通信は失敗します。 このデモで使用されているスクリーンはRK055HDMIPI4MA0です。 Re: Multicore Project setup of an additional MPU region 残念ながら、新しいメモリ領域定義を作成する前に: #define BOARD_MPU_REGION_SHMEM (16) /* rpmsg shared memory */ 私は単に、キャッシュ以外の用途で定義済みのメモリ領域を再利用していただけです。 #define BOARD_MPU_REGION_NONCACHE (10) /* Noncacheable space in application */ そして、私も同じ結果になった。非キャッシュ領域に合わせて、新しいメモリ領域の定義を10に変更しました。コア同士の通信はうまくいかなかった。 ブレークポイントを使用して両方のコアでrpmsg共有メモリの開始位置とサイズを確認しましたが、両方とも正しい開始位置(0x20340000)とサイズ(0x10000)でした。両方のコアのARM_MPU_RASR()関数の4番目のパラメータを1に変更し、その領域が「共有可能」であることを示すようにしました。相変わらず成果は出ていない。あなたかチームメンバーの方に時間があれば、私のプロジェクトのコードを別の返信に投稿しましたので、ご覧ください。試せばいいアイデアが尽きかけています。 Re: Multicore Project setup of an additional MPU region こんにちは、 @CMoran さん。 わかった。最初の返信に戻りますが: あなたは、メモリ領域の新しい定義を作成したと述べました。 #define BOARD_MPU_REGION_SHMEM (16) /* rpmsg shared memory */ しかし、ARM_MPU_RBAR() の定義では、MPU_RBAR_REGION_Msk が使用されており、これは 15 と定義されています。 #define MPU_RBAR_REGION_Msk (0xFUL /*<< MPU_RBAR_REGION_Pos*/) CM7では、地域の数を16と定義しており、0~15の番号が付けられている。 つまり、実際にはリージョン0を設定しているのです。 Re: Multicore Project setup of an additional MPU region こんにちは、 @CMoran さん。 プロジェクトをビルディングし、その結果生まれた.ldのメモリ領域を分析した後、LVGLのフレームバッファとマルチコアメッセージバッファが、非連続した物理メモリであるためマージできない別々のメモリ領域に配置されている領域が見えます。 LVGLフレームバッファ用のNCACHE_REGION(アドレス0x81000000、16MB、SDRAM内) マルチコアメッセージバッファ用のrpmsg_sh_mem(アドレス0x20340000、64KB、OCRAM内) とはいえ、MPUリージョン7は現在、キャッシュ可能なノーマルメモリとして0x20300000〜0x2037FFFF KB(512KB)をカバーしており、この範囲にはrpmsg_sh_mem領域も含まれます。これにより、共有メモリがキャッシュ可能になり、あなたが見ているようなコア間通信エラーが発生する可能性があります。リージョン7のサイズを縮小して、すでにキャッシュできないリージョン3にrpmsg_sh_memが落ちるようにすることは、既存ドライバのMPUレベルの変更なしにメッセージバッファの適切な機能を確保する簡単な解決策かもしれません。 Re: Multicore Project setup of an additional MPU region こんにちは、 @EdwinHzさん あなたの提案を少し試してみました。MPUのリージョン7(OCRAM2)を512KBから256KBに変更しました。 /* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */ MPU->RBAR = ARM_MPU_RBAR(BOARD_MPU_REGION_OCRAM_B, 0x20300000U); MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB); __USE_SHMEM プリプロセッサを削除した後、rpmsg_sh_mem は MPU 領域 3 にフォールスルーしますが、これは既にキャッシュ不可として定義されています。私が作成したデモは、意図したとおりに動作するようになりました。
View full article
HSEオプション こんにちは、 輸出目的のため、HSE(暗号化部分)モジュールを削除したいと考えています。あなたのリストにはHSEモジュールなしの参照情報が見当たりませんでしたが、HSE(暗号化部品)モジュールなしのS32G2またはS32G3の参照情報は存在しないということでしょうか? B.R. Re: HSE option こんにちは、 @COLLIN_O 投稿ありがとうございます。 最新のS32G2/3製品導入以降、HSEは記載されたすべてのバリアントに含まれています。 BR チェイン
View full article
SPI通信による「s32k31XEVB-Q100評価ボード」 こんにちは、 私はs32k31XEVB-Q100評価ボードを持っており、S32とFS23間のSPI通信を実装しようとしています。 私のPIN設定: PTB0 -> lpspi0_pcs0 PTC8 -> lpxpi0_sck PTC9 ->lpxpi0_sin PTB1 -> lpxpi0_sout ペリフェラルではLpspiを追加しました /* SPI */ /* Time to transfer all frame data */ #define BCC_MSG_SIZE 4U #define RX_BUFFER_SIZE 4U #define TIMEOUT ((uint32)1000000UL) #define NUMBER_OF_BYTES (10) uint16 numberOfBytes = BCC_MSG_SIZE; static void handleSPI(void) { static int counterSPI = 0; __attribute__(( aligned(32) )) uint8_t rxBuffer[BCC_MSG_SIZE] = {0x00};// = {0,0,0,0,0,0,0,0,0,0,0,0}; /* Buffer for receiving. */ __attribute__(( aligned(32) )) uint8_t txBuffer[BCC_MSG_SIZE] = {0x00}; /* Transmission buffer. */ /* M_DEV_PROG_ID * */ txBuffer[0] = 0x01 << 1; // General status flags ( Register address / Read/Write) txBuffer[1] = 0x00; // Read Data txBuffer[2] = 0x00; // Read Data txBuffer[3] = 0x00; // CRC if (counterSPI++ >= 5000000) { counterSPI = 0; lpspi_status = Lpspi_Ip_SyncTransmit(&MASTER_EXTERNAL_DEVICE, &txBuffer[0], &rxBuffer[0], numberOfBytes, 100000); } } int main(void) { /* Write your code here */ Clock_Ip_StatusType clockStatus; clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); if (CLOCK_IP_SUCCESS != clockStatus) { exit_code = -1; } /* Initial Pins */ Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* Initial ISR */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(FlexCAN0_0_IRQn); /* already enabled in IntCtrl_Ip - Interrupt Controller */ //IntCtrl_Ip_EnableIrq(FlexCAN0_1_IRQn); //IntCtrl_Ip_EnableIrq(FlexCAN0_2_IRQn); //IntCtrl_Ip_EnableIrq(FlexCAN0_2_IRQn); FlexCAN_Ip_Init(INST_FLEXCAN_0, &FlexCAN_State0, &FlexCAN_Config0); FlexCAN_Ip_SetRxIndividualMask(INST_FLEXCAN_0,RX_MB_IDX,0xFFFFFFFF); FlexCAN_Ip_ConfigRxMb(INST_FLEXCAN_0, RX_MB_IDX, &rx_info, Rx_MSG_ID); FlexCAN_Ip_SetStartMode(INST_FLEXCAN_0); //FlexCAN_Ip_Receive(INST_FLEXCAN_0,RX_MB_IDX,&rxData,false); lpspi_status = Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_0); /* update Transfer Mode */ //Lpspi_Ip_UpdateTransferMode(MASTER_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); for(;;) { handleSPI(); handleCAN(); handleLED(); if(exit_code != 0) { break; } } return exit_code; } 今、私はロジックアナライザーをボード上のJ39にコネクテッドしました。 このコードの実行結果は次のとおりです。 さて、いくつか質問があります。 1) 値を正しい順序で送信していますか? 2) データを読み取るだけの場合でも、CRCを送信する必要がありますか? 3) このボード上のFS23のどのレジスタが固定データを返しますか?あるいは、答えを検証するために知っているデータはありますか? 4) CLKでは時々CLKが通常より長くなっているのを見かけます。 SPI通信を正常に動作させるためのヒントを何か教えていただけますか? Re: SPI Communication on "s32k31XEVB-Q100 Evaluation Board" こんにちは、ジョン。 以下のコメントをご覧ください。 ここではFS23のみをサポートしており、S32Kはサポートしていないので、FS23の視点からお答えします。 さて、いくつか質問があります。 1) 値を正しい順序で送信していますか? [gw]読み取りおよび書き込み操作の詳細な形式については、回答2を参照してください。 また、READ/WRITE/CRC に関する詳細は MCU コミュニケーションの16-5ページもAN12149 をご覧ください 2) データを読み取るだけの場合でも、CRCを送信する必要がありますか? [gw]はい、SPI通信フレーム形式は以下の通りです:CRCはデフォルトで存在し無効化できません。読み書き操作中は、最上位ビット(MSB)が最初に送信され、最下位ビット(LSB)が最後に送信されます。SPIがアイドル状態、つまりCSBピンがハイ状態のとき、MISOは高インピーダンス状態になります。 AN14129ページで11ページ16ページにINIT CRCおよび通常のCRC計算方法を紹介します。 それらは異なる。 3) このボード上のFS23のどのレジスタが固定データを返すのか?それとも答えを検証するために知っているデータ? [gw] M_DEV_PROG_ID アドレスは  0x01 4) CLKでは、時々、clkが通常よりも長くなっているのが見られます。 [gw]CSがローに変わるときの波形をテストするとCLCKはハイになりますが、タイミング図ではローになっています。
View full article
FRDM-i.MX93 支持 Yocto Kirkstone 您好, 我们目前正在 i.MX8MQ 项目中使用 Yocto Kirkstone,并希望在 FRDM-i.MX93 板上评估相同的映像。 The meta-imx-frdm代码库似乎支持 Scarthgap。是否有官方的 Kirkstone 兼容分支或电路板支持包。可用于 FRDM-i.MX93? 如果没有,是否有推荐的方法可以在 Kirkstone 中启用 FRDM-i.MX93 支持? 谢谢! Yocto Project Re: FRDM-i.MX93 Support for Yocto Kirkstone 嗨@Zhiming_Liu , 感谢您的反馈, 我们目前在 i.MX8MQ 项目中使用的是 NXP Kirkstone 电路板支持包。 (LF5.15.71_2.2.0)。 请问这个电路板支持包是否可以作为将 meta-imx-frdm 层移植到 Kirkstone 的起点? 另外,是否有推荐的 Kirkstone 分支或 NXP 电路板支持包。版本,其中已经包含了必要的 i.MX93 处理器支持? 我们的目标是在 FRDM-i.MX93 上运行我们现有的基于 Kirkstone 的项目镜像,并进行必要的针对特定电路板的修改。 感谢您的指导。 关于 阿吉尔 Re: FRDM-i.MX93 Support for Yocto Kirkstone 你好@ap3415 需要 Yocto 版本才能将 meta-imx-frdm 层移植到 Kirkstone。 此致, 志明 Re: FRDM-i.MX93 Support for Yocto Kirkstone 你好@ap3415 您可以尝试使用基于 Kirkstone 的 电路板支持包。版本 lf-5.15.71-2.2.2,并将 FRDM-i.MX93 配置从基于 Scarthgap 的 meta-imx-frdm 层移植过来。 除了机器配置之外,请同时检查相应的 U-Boot 配置、内核设备树、板级支持补丁和配方依赖项。由于此组合尚未得到官方验证,因此由于 Kirkstone 和 Scarthgap 电路板支持包。版本之间的差异,可能需要进行一些调整。 此致, 志明
View full article
8ULP 上でのヒューズプログラミング - eMMC からのブート用 みなさんこんにちは、 最近、8ULPボードのヒューズをプログラムして、eMMCから起動できるようにするために時間を費やしました。 これらの調査結果は、以下のような作業を行う必要がある方にとって役立つかもしれません。 手動手順: UUU 経由で U-Boot を起動し、自動起動を停止してから、次の手順を実行します。 => fuse prog -y 4 1 0x00400000 => fuse prog -y 3 7 0x00008000 => リセット 再起動後、以下を確認してください。 => ヒューズ読み取り 4 1 ワード 0x00000001: 00400000 => ヒューズ読み取り 3 7 ワード 0x00000007: 00008000 USBケーブルを外し、電源を入れ直すと、ボードはeMMCから起動します。 UUUスクリプト: uuu_version 1.2.39 # prog-boot-fuses-evk.lst # クリーンなEVKボード8ULP上でeMMCブートヒューズ(ブート構成とBT_FUSE_SEL)をプログラムする #SDPS: boot -f flash.bin SDPS: boot -f u-boot-imx8ulp-evk-uuu.imx SDPV: 遅延 2000 #SDPV: write -f flash.bin -skipspl SDPV: write -f u-boot-imx8ulp-evk-uuu.imx -skipspl SDPV: ジャンプ FB: ucmd fuse prog -y 4 1 0x00400000 FB: ucmd fuse prog -y 3 7 0x00008000 i.MX8ULP Re: Fuses programming on 8ULP - for booting from eMMC IMX8ULPのヒューズマップを探している際にこのページを訪れる方のために、リファレンス・マニュアル(IMX8ULPRM)としてスプレッドシートとして添付されています。ブラウザで閲覧する場合は取得できません。OkularのようなPDFビューアを使用する必要があります。NXPがこのようなドキュメントを隠すという悪い傾向です。私も、データシート(IMX8ULPCEC)に添付されていたimx8ulpのピンマルチプレクサオプションを検索した際に、この「機能」に遭遇しました。
View full article
i.MX 93 AHAB 密钥撤销程序疑问 你好, 我们正在研究如何撤销通过空中升级的 i.MX93 产品的 SRK,但我们找不到完整的程序说明。我们已经阅读了 imx93: SRK 撤销主题( https://community.nxp.com/t5/i-MX-Processors/imx93-SRK-revocation/td-p/1827004 )、参考手册(§9.5.1.3.2.3,SRK 撤销)和 AN14954,我们想确认以下几点。 1. ahab_commit 在字段 在上面的线程中,使用 SRK2 签名且 Revocations = 0x1 的容器直到运行 ahab_commit 0x10 才撤销 SRK1。我们想了解在接收后续更新的设备上,该提交应该如何使用: - 在携带撤销掩码的容器通过身份验证后,运行一次提交是否足够? - 或者,一旦至少撤销了一个密钥,是否可以将该提交永久保留在启动命令中,以便之后安装的任何版本都会应用撤销操作?如果没有新的版本可提交,这样做是否安全无害? - 后续版本的容器是否必须保持相同的 srk_revocations 值(参考手册中说 ELE 会检查容器中的撤销位是否与熔丝中已设置的值匹配),以及哪些容器必须携带该值(启动容器和操作系统容器)? 2. 多次或交叉撤销 使用一个 SRK 签名的容器可以撤销另一个 SRK(如线程中所示)。撤销掩码可以包含多个比特,包括所有其他 SRK 吗?ELE 中是否有检查机制来防止使用被泄露的 SRK 签名的容器撤销其余的 SRK,还是说这必须由密钥管理来处理? 3. 检查撤销状态 是否有官方支持的方法可以从 U-Boot 或 Linux 中知道哪些 SRK 被撤销了?使用熔丝感知时,我们板上第 6 个库之后的大多数字都会返回 ERROR,并且 nvmem 接口会显示为零。功能性检查(验证每个 SRK 签名的小容器并查看 ELE 事件)是否是一种合理的方法? 4. 测试用的熔丝位覆盖 从 AN14954 中我们了解到,在 OEM Open 中可以覆盖影子熔丝,而无需烧毁电子熔丝。ELE 在验证容器身份时是否使用 SRK 哈希熔丝的影子值,以便无需写入哈希即可测试签名链?那么,有没有办法利用这种机制模拟撤销操作呢? 5. SRK 表收盘后 哈希值涵盖整个 SRK 表(4 个键)。哈希表写入后,即使当时的位置是空的,该表还能更改吗(估计不能,因为它们是融合的)?所以基本上,是否可以只写入 2 个密钥,以后再添加 2 个密钥? 我们了解到,部分熔丝信息受保密协议约束,并已写入网络安全参考手册。如果是这样,提供相关文档或章节的链接,甚至是流程的概要描述,都会有很大的帮助。鉴于即将生效的《网络弹性法案》,密钥撤销将成为许多产品的标准要求,因此,一份清晰的公开说明将非常有价值。 提前致谢
View full article
How do I implement Secure Boot on the i.MX95? I completed the secure boot process on imx8mp. Secure boot is achieved using HABv4 on an 8mp. Does imx95 also use HABv4 to implement secure boot? When compiling flash.bin, I did not see information such as CSF block or sld hab block. How do I perform a secure boot on IMX95? Re: How do I implement Secure Boot on the i.MX95? Hello @yyn  I hope you are doing very well. Please take a look to the introduction_ahab in the U-boot documentation. There is explained the Secure Boot process of the i.MX9 family. Best regards, Salas. Re: How do I implement Secure Boot on the i.MX95? Hello, Just adding a practical reference here for anyone else working on Secure Boot with the i.MX95. As mentioned above, the i.MX95 uses AHAB rather than the HABv4 approach used on the i.MX8MP, so the signing and boot authentication workflows are different. At RidgeRun, we've documented a step-by-step guide for implementing Secure Boot on the i.MX95 using Yocto, covering AHAB key generation, SRK fuse table generation, image signing with NXP's CST, and validation of signed boot images. It also includes an alternative signing workflow using PKCS#11 and SoftHSM2. The guide uses the Toradex Verdin i.MX95 as its reference platform and focuses on development-stage signing and validation, without programming security fuses or closing the device. For anyone looking for a hands-on reference alongside NXP's documentation, you can find it here: https://developer.ridgerun.com/wiki/index.php/RidgeRun_Platform_Security_Manual/Getting_Started/NXP_i.MX95/Yocto_Build_Process/Secure_Boot Hope this is useful to others working on i.MX95 security! Best Regards
View full article
NCF3321AHF 数据手册 需要NCF3321AHF器件的数据手册。 Re: NCF3321AHF datasheet 你好, 您请求的文件属于机密文件,受保密协议 (NDA) 约束,仅可通过安全文件访问。请参考以下指南访问安全文件: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 如果您还有其他问题,请告诉我。 此致, 阿隆德拉
View full article
imx8mp Android System Fast Boot Solution 你好! 我参考Android System Fast Boot Solution - Study and Summary of Hibernate_v1.pdf 在imx8mp android14  源码是source imx-android-14.0.0_1.0.0/imx_android_setup.sh 修改完会出现GPU的报错,详情见附件,这个需要怎么解决 Re: imx8mp Android System Fast Boot Solution Hi @jieh朱 The default BSP GPU driver code does not support execution upon GPU hibernation and power-on; NXP has not tested this. You can refer to the power-on/power-off handling of `echo mem`, but `echo disk` requires separate verification of GPU driver and buffer recovery. Best Regards, Zhiming
View full article
NCF3321AHF datasheet need datasheet for NCF3321AHF part. Re: NCF3321AHF datasheet Hello,  The document you are asking for is confidential, under NDA and is available through Secured Files only, use the following guide to gain access to secured files: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf Please let me know if you have further issues Best regards,  Alondra
View full article
FRDM-i.MX93 Support for Yocto Kirkstone Hi, We are currently using Yocto Kirkstone on our i.MX8MQ project and would like to evaluate the same image on the FRDM-i.MX93 board. The meta-imx-frdm repository appears to support Scarthgap. Is there an official Kirkstone-compatible branch or BSP available for FRDM-i.MX93? If not, is there any recommended approach to enable FRDM-i.MX93 support with Kirkstone? Thank you. Yocto Project Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @Zhiming_Liu , Thank you for your response. We are currently using the NXP Kirkstone BSP (LF5.15.71_2.2.0) for our i.MX8MQ project. Could you please clarify whether this BSP can be used as the starting point for porting the meta-imx-frdm layer to Kirkstone? Also, is there a recommended Kirkstone branch or release of the NXP BSP that already includes the necessary i.MX93 processor support? Our objective is to run our existing Kirkstone-based project image on FRDM-i.MX93, with the necessary board-specific modifications. Thank you for your guidance. With regards Ajil Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @ap3415  A Yocto release is needed to port the meta-imx-frdm layer to Kirkstone. Best Regards, Zhiming Re: FRDM-i.MX93 Support for Yocto Kirkstone Hi @ap3415  You may try using the Kirkstone-based BSP release lf-5.15.71-2.2.2  and porting the FRDM-i.MX93 configurations from the Scarthgap-based meta-imx-frdm layer. In addition to the machine configuration, please also review the corresponding U-Boot configuration, kernel device tree, board-support patches and recipe dependencies. Since this combination has not been officially validated, some adaptation may be required due to the differences between the Kirkstone and Scarthgap BSP versions. Best Regards, Zhiming
View full article
FRDM-i.MX93 Yocto・カークストーン対応 こんにちは、 現在、i.MX8MQプロジェクトでYocto Kirkstoneを使用しており、同じ画像をFRDM-i.MX93ボード上で評価したいと考えています。 meta-imx-frdm リポジトリはScarthgapをサポートしているようです。FRDM-i.MX93用の公式のKirkstone互換ブランチやBSPはありますか? もしそうでなければ、KirkstoneでFRDM-i.MX93のサポートを有効にするための推奨方法はありますか? よろしくお願いします。 Yocto Project Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは@Zhiming_Liuさん ご返信ありがとうございます。 現在、i.MX8MQプロジェクトではNXP Kirkstone BSP(LF5.15.71_2.2.0)を使用しています。 このBSPをmeta-imx-frdmレイヤーをKirkstoneに移植する出発点として使えるのか、教えていただけますか? また、必要なi.MX93プロセッササポートが既に含まれている、KirkstoneのおすすめのNXP BSPブランチやリリースはありますか? 私たちの目標は、既存のKirkstoneベースのプロジェクトイメージを、必要なボード固有の変更を加えた上で、FRDM-i.MX93上で実行することです。 ご指導ありがとうございました。 に関して アジル Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは、 @ap3415さん Meta-imx-frdmレイヤーをKirkstoneに移植するにはYoctoリリースが必要です。 よろしくお願いします、 志明 Re: FRDM-i.MX93 Support for Yocto Kirkstone こんにちは、 @ap3415さん KirkstoneベースのBSPリリースlf-5.15.71-2.2.2を使用し、Scarthgapベースのmeta-imx-frdmレイヤーからFRDM-i.MX93構成を移植してみてください。 マシンの設定に加えて、対応するU-Boot設定、カーネルデバイスツリー、ボードサポートパッチ、レシピ依存関係も確認してください。この組み合わせは公式に検証されていないため、カークストーン版とスカースギャップ版のBSPの違いにより、何らかの調整が必要になる場合があります。 よろしくお願いします、 志明
View full article
NCF3321AHFデータシート NCF3321AHF部品のデータシートが必要です。 Re: NCF3321AHF datasheet こんにちは、 ご依頼の文書は機密であり、NDAの下でSecured Filesを通じてのみ利用可能です。以下のガイドをご利用ください。Secure Filesへのアクセスは以下のガイドをご利用ください: https://www.nxp.com/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 他に問題があればお知らせください よろしくお願いします、 アロンドラ
View full article
How do I implement Secure Boot on the i.MX95? 我在imx8mp 上完成了 安全启动的流程。 8mp 上使用 HABv4 实现安全启动。 imx95 也是使用HABv4实现安全启动吗? 编译flash.bin  没有看到 CSF block ,sld hab block 等信息。 我应该如何完成 imx95 的安全启动? Re: How do I implement Secure Boot on the i.MX95? 你好@yyn 希望你一切都好。 请参阅 U-boot 文档中的 introduction_ahab 部分。 本文解释了 i.MX9 系列的安全启动过程。 顺祝商祺! 萨拉斯。 Re: How do I implement Secure Boot on the i.MX95? 你好, 这里补充一点实用参考,供其他使用 i.MX95 进行安全启动的人员参考。 如上所述,i.MX95 使用的是 AHAB 而不是 i.MX8MP 上使用的 HABv4 方法,因此签名和启动认证工作流程有所不同。 在 RidgeRun,我们编写了一份使用 Yocto 在 i.MX95 上实现安全启动的分步指南,涵盖了 AHAB 密钥生成、SRK 熔丝表生成、使用 NXP 的 CST 进行映像签名以及对已签名启动映像的验证。它还包括使用 PKCS#11 和 SoftHSM2 的替代签名工作流程。 该指南以 Toradex Verdin i.MX95 为参考平台,重点关注开发阶段的签名和验证,而不涉及网络安全熔丝的编程或设备的关闭。 如果您想在参考 NXP 官方文档的同时获取一些实际操作方面的资料,可以在这里找到: https://developer.ridgerun.com/wiki/index.php/RidgeRun_Platform_Security_Manual/Getting_Started/NXP_i.MX95/Yocto_Build_Process/Secure_Boot 希望这对其他从事 i.MX95 网络安全研究的人有所帮助! 顺祝商祺!
View full article