Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Demo EthernetAnalyzer FRDM-A-S32K344 RTD 7.0.1 S32K344 Embedded Ethernet Analyzer Demo with LVGL Overview This article presents an embedded Ethernet Analyzer demo for the S32K344 MCU and the FRDM-A-S32K344 development board.The application captures received and transmitted Ethernet frames and displays them directly on an LCD-PAR-S035 touchscreen. It provides a compact, stand-alone view of Ethernet traffic without requiring the captured frames to be transferred to a host PC.The demo is available in two variants: Bare-metal lwIP application FreeRTOS lwIP application Both variants use the same Ethernet Analyzer, frame parser and graphical application layers.   Figure 1: Complete FRDM-A-S32K344 and LCD-PAR-S035 hardware setup Motivation PC-based packet analyzers remain the preferred solution for detailed network debugging. However, the frames visible to a PC capture application may depend on the Ethernet adapter and its driver configuration.For example, some adapters may process or remove an IEEE 802.1Q VLAN tag before the frame is delivered to the capture application. This can make analysis of VLAN-tagged traffic less straightforward. Automotive Ethernet applications may also use an IEEE 802.1CB redundancy tag, commonly referred to as an R-TAG.The purpose of this demo is to provide a direct view of the Ethernet frames processed by the S32K3 Ethernet interface and to make basic VLAN and R-TAG inspection available directly on the development board.The application is intended as a compact demonstration and debugging aid. It is not intended to replace a full-featured PC packet analyzer.   Main Features The application provides: Capture of received Ethernet frames Capture of transmitted Ethernet frames Configurable RX and TX capture Storage of frame snapshots in a bounded internal buffer Graphical frame list Selection and inspection of individual frames Hexadecimal frame data view Basic decoding of: Source and destination MAC addresses EtherType IEEE 802.1Q VLAN tags IEEE 802.1CB R-TAGs ARP IPv4 ICMP VLAN, R-TAG and multicast display filters RX and TX activity indication Start, pause, resume, stop and clear controls Capacitive touchscreen operation Preserved lwIP TCP/IP connectivity   Figure 2: Frame list with standard Ethernet traffic  Figure 3: Frame list with VLAN and R-TAG traffic  Frame Details A captured frame can be selected from the frame list and opened in the Frame Details screen. This screen provides decoded information about the selected frame together with a hexadecimal data dump. The raw frame data can therefore be compared with the decoded Ethernet, VLAN, R-TAG and higher-layer protocol fields.   Figure 4: Frame Details screen showing decoded fields and hexadecimal data Capture Settings The Capture Settings screen can be used to enable or disable RX and TX capture and to select the types of frames displayed by the application.The available display filters include VLAN-tagged frames, R-TAG frames and multicast frames.   Figure 5: Capture Settings screen Software Architecture The Ethernet capture path is separated from frame decoding and graphical processing. The RX and TX hooks copy a bounded frame snapshot into an application-managed ring buffer. The captured frame is subsequently decoded and displayed from the application context. LVGL functions are not called directly from the Ethernet RX or TX processing context. GUI refresh and activity indication are deferred to the graphical application processing path. The main application-specific software layers are: App.c/.h Application initialization and periodic processing of the LCD, touchscreen, LVGL and Ethernet Analyzer GUI. eth_analyzer.c/.h Frame capture, capture state control, filtering and storage of RX and TX frame snapshots. eth_analyzer_parser.c/.h Parsing and decoding of Ethernet, VLAN, R-TAG and selected higher-layer protocol fields. eth_analyzer_gui.c/.h Connection between the analyzer data model and the LVGL graphical interface.   For a detailed description of the project structure, software components, hardware connections and configuration, refer to the comments in src/main.c. Graphical Application The graphical interface uses LVGL 9.4.0 and was designed using NXP GUI Guider 2.0.1.The GUI Guider-generated screens, widgets and event handlers are stored separately from the custom GUI callbacks and Ethernet Analyzer application logic. This separation allows the graphical screens to be modified in GUI Guider while keeping the custom application layers maintainable. Font Roboto Mono is used for selected frame information and hexadecimal data. The generated LVGL font data retains the original SIL Open Font License 1.1 terms. The original GUI Guider project is included with this article, allowing the graphical application to be modified and regenerated using GUI Guider 2.0.1.   TCP/IP Connectivity The original lwIP TCP/IP functionality is preserved. The example uses the following static IPv4 address 192.168.0.209 Connectivity can be verified from a host configured for the same IPv4 subnet. ping 192.168.0.209 The ping response time may vary while the captured frame list is being refreshed. GUI rendering and blocking LCD transfers temporarily occupy processing time, but the TCP/IP stack remains operational.   Hardware The demo was developed and tested with: S32K344 MCU FRDM-A-S32K344 development board LCD-PAR-S035 display ST7796S LCD controller GT911 capacitive touchscreen controller The display is connected through LPSPI. The touchscreen uses LPI2C together with GPIO signals for interrupt and reset control. Detailed signal connections and hardware configuration are documented in main.c and README.md in the attached projects. Software Requirements NXP S32 Design Studio for S32 Platform 3.6.6 S32K3 RTD 7.0.1 FreeRTOS for S32K3 11.1.0 TCP/IP Stack for S32K3 5.0.0 LVGL 9.4.0 NXP GUI Guider 2.0.1 The attached project packages include README.md, Dependencies.txt, applicable software bill of materials files, license texts and the NXP disclaimer.   Porting to Other Boards The Ethernet Analyzer, parser and GUI layers were intentionally separated from the board-specific LCD, touchscreen and Ethernet initialization.This architecture can be adapted to other S32K3-based FRDM or evaluation boards. Porting requires board-specific changes, including: MCU and board configuration Ethernet controller and PHY setup Pin multiplexing Clock configuration LCD and touchscreen connections RTD and TCP/IP Stack configuration Available flash and RAM resources The project should therefore be treated as a reusable integration reference rather than as a drop-in project for every S32K3 board.   Known Limitations This project is a demonstration application and has several intentional limitations: The internal capture buffer has a finite capacity. Only a bounded portion of each frame is stored. Frame capture and GUI rendering consume MCU processing time. LCD transfers use blocking LPSPI communication. RX and TX indicators are informational and may not visibly represent every individual event. The protocol parser supports selected Ethernet and higher-layer fields only. The analyzer is not intended to provide the capture performance or protocol coverage of a dedicated PC-based packet analyzer. The application has not been designed or qualified as a production monitoring solution.   Attached Projects The following project variants are provided:   Demo_EthernetAnalyzer_BareMetal_FRDM_A_S32K344_v1_0_RTD701 Demo_EthernetAnalyzer_FreeRTOS_FRDM_A_S32K344_v1_0_RTD701 The original GUI Guider project is also included: Demo_EthernetAnalyzer_GUI_Guider_v1_0_GG201 The GUI project can be opened and modified using NXP GUI Guider 2.0.1. It contains the screens, widgets, events, custom callbacks and graphical assets used by the Ethernet Analyzer application. After modifying the graphical application, copy the contents of the GUI Guider generated and custom output directories into the corresponding src/gui_guider directories of the BareMetal or FreeRTOS project. The GUI Guider project package includes the applicable license information and software component documentation. This article presents BareMetal and FreeRTOS variants of an embedded Ethernet Analyzer demo for the S32K344 MCU. The application captures RX and TX Ethernet frames and displays them directly on an LCD-PAR-S035 touchscreen, including basic decoding of VLAN and IEEE 802.1CB R-TAG information and hexadecimal inspection of individual frames. The graphical interface uses LVGL 9.4.0 and was created with NXP GUI Guider 2.0.1.
View full article
ASA紧急警报处理和音频源切换 我们的主要问题是,当车辆从 DAB 收到紧急警报,而其他媒体源(例如通过蓝牙/CarPlay/Android Auto 播放的 Spotify 或 FM 广播电台)处于活动状态时,车辆的行为会如何。   具体来说,我们希望您能就以下几点提供技术说明:   自动信号源切换:当用户正在收听 FM 广播或 Spotify 时,如果通过 DAB 收到 ASA 紧急警报,系统如何自动切换到 DAB 紧急公告并显示相关警报信息?   系统职责:哪个元器件负责实现此行为?警报检测和触发信号是由 ASA 芯片本身处理,还是 DAB 接收器/主机需要一个控制接口,使其能够中断当前活动的媒体源并切换到 DAB 音频?   车辆集成:DAB接收器是直接控制音频源和显示,还是向车辆的信息娱乐系统发送警报通知或触发信号,然后由车辆的信息娱乐系统执行源切换并显示警报?   标准与实施:相关的 ASA/DAB 标准是否定义了这种行为以及接收器与车辆信息娱乐系统之间所需的接口,还是这些实施细节留给了接收器制造商和车辆 OEM?   技术要求:为了确保紧急警报能够覆盖当前活动的媒体源,是否需要任何特定的硬件接口、软件 API、控制信号或信息娱乐集成要求?   我们的目标是了解此功能是否主要由 ASA 接收器/解码器提供,或者是否需要与车辆的信息娱乐系统进行额外集成。   任何相关的技术文档、系统架构图或实施指南都将不胜感激。 Re: ASA Emergency Alert Handling and Audio Source Switching 你好 osmanistlink10 感谢您对恩智浦产品的关注。 与您的问题相关的NXP产品部件号是多少?
View full article
能源革命系统评测:它真的有效吗? 如果您正苦于无法预测的停电、不断上涨的每月电费,或者只是想为您的家人建立一个可靠的离网能源备用系统,那么您并不孤单。 最近,能源革命系统在互联网上引起了轰动。这本书被宣传为一本循序渐进的 DIY 指南,教普通人如何在家制造清洁、便携式发电机,这在在线技术论坛和社区留言板上引发了广泛的讨论。 事实上,用户和 DIY 技术爱好者正在NXP 社区论坛和技术问答网站等平台上热烈讨论该系统,询问这些 DIY 磁线圈原理是否真的能转化为现实世界的家庭电力。 在这篇令人震惊的评论中,我们将深入探讨能源革命系统究竟是什么,它是如何运作的,它包含什么,以及它是否真的能在 2026 年兑现其承诺。 产品快速概览 产品名称:能源革命系统 类别:替代能源/DIY家居改造/离网电力 格式:电子蓝图、分步操作手册和高清视频指南 组装时间: 2至4小时(适合初学者) 官方门户网站:点击此处访问官方能源革命系统 退款保证: 60 天(100% 无条件退款) 等级: ⭐⭐⭐⭐⭐ (4.8/5) 什么是能源革命系统? 能源革命系统是一个全面的数字化教学蓝图,旨在指导初学者组装一台静音、轻便且经济高效的能源发电机。 与昂贵、噪音大、耗油的商用发电机不同,该装置专注于使用易于获取的硬件部件(如磁线圈、电线、电池储能组和标准逆变器)来捕获电流。 目标很简单: 大幅降低您的水电费:使用自发电为日常电子产品、照明设备和家用电器供电。 紧急停电保护:在恶劣天气导致电网瘫痪时,准备好安全、适合室内使用的备用电源。 它的工作原理是什么? 其核心机制依赖于基本的电转换和谐振原理。该程序会向您展示如何将磁能捕获装置连接到深循环电池。 能量捕获:线圈结构能够高效地捕获微小的电荷。 存储:能量持续输入到您的电池储能系统中。 逆变器转换:简单的电源逆变器可以将直流电转换为标准的家用交流电。 即插即用:您可以将家用电源插座、充电器、灯具、风扇和小电子产品直接插入本机。 由于它无需内燃即可运行,因此不会产生任何有害烟雾,而且运行完全静音,因此可以在客厅、卧室或公寓内安全使用。 本指南包含哪些内容? 当您从官方网站订购时,即可立即获得以下数字下载权限: 高分辨率蓝图和图表:易于阅读的原理图,显示每个连接和电线规格。 完整的五金材料清单:一份详细的清单,告诉你应该在当地的五金店(如家得宝、劳氏或当地电子产品商店)购买哪些零件,才能获得最优惠的价格。 高清演示视频教程:一步一步的视频说明,展示从开始到结束的组装过程。 维护和扩展手册:延长电池寿命和排除设置故障的指南。 它真的有效吗?(令人震惊的真相) 是的,它确实有效——前提是你的期望值要现实一些。 如果你指望花费 100 美元自制一个工作台就能立即为一栋五居室豪宅或一台工业空调机组供电,那你肯定会失望的。然而,正如成千上万的 DIY 建造者和社区论坛用户所证实的那样,如果按照蓝图建造,它可以提供非常可靠的辅助电源。 它非常适合为普通家用电器、LED 照明、Wi-Fi 路由器、电视屏幕和手机充电器供电,从而大大减轻电表负荷,每年为您节省数百美元的电费。 优点和缺点 优点 大幅降低成本:立即降低您的每月电费支出。 100% 静音安全:无噪音电机或危险的一氧化碳气体。 适合初学者:无需任何电气方面的知识——清晰的视频指南将引导您完成每个步骤。 60 天退款保证:您可以完全无风险地试用本指南两个月。 缺点 需要自行组装:您必须单独购买硬件零件,并花费 2 到 3 个小时进行组装。 仅提供电子版:通过即时 PDF 和视频下载以电子方式交付。 最终结论:2026年还值得购买吗? 由于电网不稳定且电价达到历史新高,掌控家庭能源需求是一个明智之举。能源革命系统提供简单易懂、万无一失的蓝图,将看似复杂的 DIY 建造项目变成一个有趣的周末项目。 我们提供60 天退款保证,您没有任何损失,却能获得真正的能源独立。 立即领取您的专属折扣! 不要等到下一次大风暴或电价飙升才去寻求电力保障。今天就迈出通往能源自由的第一步! 👉 点击这里访问官方能源革命系统网站,立即领取您的 2026 年折扣!
View full article
コードを生成できません コード生成プロセスが停止します。 Re: 无法生成代码 この問題は解決しましたか? Re: 无法生成代码 こんにちは、 @Cui5222 さん。 お使いのGUI Guiderのバージョンは何ですか?本当にインターネットにコネクテッドのですか?GUI Guiderを管理者として実行してみてはどうでしょうか?
View full article
Which neutron-converter matches i.MX95 BSP LF6.6.52_2.2.x? Toolkit 1.14 has no Linux_6.6.52 folder We are enabling the Neutron NPU on a Toradex Verdin iMX95, B0 silicon, running the Yocto reference multimedia image from Toradex BSP 7.7.0. This is not Torizon. The kernel is 6.6.142-7.7.0-devel, based on NXP LF6.6.52_2.2.2. /dev/neutron0 exists, and the driver probes. The image did not ship the Neutron firmware. We installed "NeutronFirmware.elf" and "NeutronKernels.bin" from nxp-imx/neutron, branch lf-6.6.52_2.2.0. The userspace delegate and Neutron libraries were built from the same branch. label_image runs in a container and reaches the NPU. eIQ Toolkit 1.14.0, installer EIQ-TOOLKIT-WIN-1.14.0 dated 28 January 2025, has no Linux_6.6.52 converter. The newest Linux converter in that install is Linux_6.6.36_2.1.0. Converting mobilenet_v1_1.0_224_quant.tflite with --target imx95 produces a model whose microcode is 0x5bfe0804. At runtime the 6.6.52 stack reports: microcode version mismatch! 0x5bfe0804 (expected 0xa186aaf2) The delegate is created, and one node is delegated, but the classification scores are empty. The same model on the CPU, without the Neutron delegate, correctly returns "military uniform" for grace_hopper.bmp. Replacing the firmware and the userspace libraries with the lf-6.6.36_2.1.0 versions removes the mismatch, then the 6.6.52 kernel driver fails the job with a failure to create a neutron inference job, Neutron Driver internal fault code 442. The 6.6.36 library cannot talk to this kernel. The eIQ Toolkit release notes say the Neutron converter for i.MX95 BSP LF6.6.52_2.2.x is available only in eIQ Toolkit 1.14. The 1.14 installer we have does not contain it. Which converter binary produces microcode 0xa186aaf2 for this BSP, and in which eIQ Toolkit or Neutron SDK package is it shipped? Re: Which neutron-converter matches i.MX95 BSP LF6.6.52_2.2.x? Toolkit 1.14 has no Linux_6.6.52 fold Hi @Giorgos_Sofroniou  The prebuilt converter is only availble on eIQ Ubuntu version. Best Regards, Zhiming
View full article
Energy Revolution System Review: Does It Actually Work? If you are struggling with unpredictable power outages, rising monthly electricity bills, or simply want to build a reliable off-grid energy backup for your family, you are not alone. Recently, the Energy Revolution System has taken the internet by storm. Promoted as a step-by-step DIY guide that teaches everyday people how to build a clean, portable power generator at home, it has sparked massive debates across online tech forums and community message boards. In fact, users and DIY tech enthusiasts are heavily discussing this system on platforms like the NXP Community Forum and tech Q&A sites, asking whether these DIY magnetic coil principles genuinely translate into real-world household power. In this shocking review, we take a deep dive into what the Energy Revolution System really is, how it works, what you get inside, and whether it actually delivers on its promises in 2026. Quick Product Overview Product Name: Energy Revolution System Category: Alternative Energy / DIY Home Improvement / Off-Grid Power Format: Digital Blueprints, Step-by-Step Manuals & HD Video Guides Assembly Time: 2 to 4 Hours (Beginner-Friendly) Official Portal: Click Here to Access the Official Energy Revolution System Money-Back Guarantee: 60 Days (100% Unconditional Refund) Rating: ⭐⭐⭐⭐⭐ (4.8/5) What Is the Energy Revolution System? The Energy Revolution System is a comprehensive, digital instructional blueprint designed to guide beginners through assembling a silent, lightweight, and cost-effective energy generator. Unlike expensive, loud, and gas-guzzling commercial generators, this setup focuses on capturing electrical current using easily sourced hardware parts—such as magnetic coils, wiring, a battery storage bank, and a standard inverter. The goal is simple: Slash Your Utility Costs: Use self-generated power to run everyday electronics, light fixtures, and appliances. Emergency Blackout Protection: Have a safe, indoor-friendly power backup ready when the power grid goes down during severe weather. How Does It Work? The core mechanism relies on basic electrical conversion and resonance principles. The program shows you how to connect a magnetic energy capture unit to a deep-cycle battery. Energy Capture: The coil configuration captures small electrical charges efficiently. Storage: Energy feeds continuously into your battery storage bank. Inverter Conversion: A simple power inverter converts the DC charge into standard AC household electricity. Plug & Play: You can plug household power strips, chargers, lamps, fans, and small electronics directly into the unit. Because it operates without internal combustion, it produces zero hazardous fumes and runs completely silent, making it safe to use inside your living room, bedroom, or apartment.  What Do You Get Inside the Guide? When you order from the official website, you gain immediate digital download access to: High-Resolution Blueprints & Diagrams: Easy-to-read schematics showing every connection and wire gauge. Complete Hardware Materials Checklist: A detailed list telling you exactly what parts to buy at local hardware stores (like Home Depot, Lowe's, or local electronics shops) for the best price. HD Walkthrough Video Tutorials: Step-by-step video instructions showing the assembly from start to finish. Maintenance & Expansion Manuals: Guidance on extending battery life and troubleshooting your setup. Does It Actually Work? (The Shocking Truth) Yes, it does work—provided you have realistic expectations. If you expect a $100 DIY bench build to instantly power a whole 5-bedroom mansion or industrial AC unit, you will be disappointed. However, as thousands of DIY builders and community forum users have confirmed, when built according to the blueprints, it delivers a very reliable supplementary power source. It excels at powering regular household electronics, LED lighting, Wi-Fi routers, TV screens, and phone chargers—taking significant load off your electric meter and saving you hundreds of dollars on utility bills each year. Pros and Cons Pros Drastic Cost Reduction: Lower your monthly electricity expenses right away. 100% Silent & Safe: No noisy motors or dangerous carbon monoxide fumes. Beginner Friendly: No prior electrical background required—clear video guides walk you through every step. 60-Day Money-Back Guarantee: Try the guide for two full months completely risk-free. Cons Assembly Required: You must buy the hardware parts separately and dedicate 2 to 3 hours to building it. Digital Format Only: Delivered electronically via instant PDF and video downloads. Final Verdict: Is It Worth Buying in 2026? With power grid instability and electricity prices reaching record highs, taking control of your home's energy needs is a smart move. The Energy Revolution System provides simple, foolproof blueprints that turn a seemingly complex DIY build into a fun weekend project. Backed by a 60-day money-back guarantee, you have nothing to lose and real energy independence to gain. Claim Your Discounted Access Today! Don't wait for the next major storm or price surge to leave you without power. Take the step toward energy freedom today! 👉 CLICK HERE to Visit the Official Energy Revolution System Website & Claim Your 2026 Discount Today!
View full article
无法生成代码 生成代码会卡住 Re: 无法生成代码 请问此问题有解决吗 Re: 无法生成代码 你好@Cui5222 , 你使用的是哪个版本的GUI Guider?你确定你已连接到互联网吗?您能否尝试以管理员身份运行 GUI Guider?
View full article
どのNeutronコンバータがi.MX95 BSP LF6.6.52_2.2.xに一致しますか?Toolkit 1.14にはLinux_6.6.52フォルダはありません 私たちは、Toradex Verdin iMX95、B0シリコン上でNeutron NPUを有効にしており、Toradex BSP 7.7.0のYoctoリファレンスマルチメディアイメージを実行しています。これはトリゾンではありません。カーネルはNXP LF6.6.52_2.2.2をベースにした6.6.142-7.7.0-develです。/dev/neutron0が存在し、ドライバーがプローブします。 そのイメージにはNeutronのファームウェアは付属していません。「NeutronFirmware.elf」をインストールしました。およびNXP-IMX/Neutronの「NeutronKernels.bin」、LF-6.6.52_2.2.0の分岐です。ユーザースペースデリゲートとNeutronライブラリは同じブランチから構築されました。label_imageはコンテナ内で実行され、NPUに到達します。 eIQツールキット1.14.0、2025年1月28日付のインストーラーEIQ-TOOLKIT-WIN-1.14.0にはLinux_6.6.52コンバータがありません。そのインストールで最新のLinuxコンバータはLinux_6.6.36_2.1.0です。mobilenet_v1_1.0_224_quant.tflite を変換中--target imx95 はマイクロコードが0x5bfe0804のモデルを生成します。実行時に6.6.52スタックは以下を報告します。 マイクロコードのバージョンが一致しません!0x5bfe0804 (期待値 0xa186aaf2) 委任先は作成され、1つのノードが委任されましたが、分類スコアは空です。同じモデルのCPU上で、Neutronデリゲートなしではgrace_hopper.bmpの「軍服」を正しく返します。 ファームウェアとユーザー空間ライブラリをlf-6.6.36_2.1.0に置き換えるバージョンは不一致を除去し、その後6.6.52カーネルドライバは中性子推論ジョブの作成に失敗し、Neutron Driver 内部故障コード442を発生させます。6.6.36ライブラリはこのカーネルと通信できません。 eIQ Toolkitのリリースノートによると、i.MX95 BSP LF6.6.52_2.2.x用のNeutronコンバーターはeIQ Toolkit 1.14でのみ利用可能とされています。私たちが持っている1.14インストーラーには、それは含まれていません。 どのコンバーターバイナリがこのBSP用のマイクロコード0xa186aaf2を生成しており、どのeIQ ToolkitやNeutron SDKパッケージに出荷されているのでしょうか? Re: Which neutron-converter matches i.MX95 BSP LF6.6.52_2.2.x? Toolkit 1.14 has no Linux_6.6.52 fold こんにちは、 @Giorgos_Sofroniou さん。 プリビルドのコンバーターは eIQ Ubuntu 版のみで利用可能です。 よろしくお願いします、 志明
View full article
ASA Emergency Alert Handling and Audio Source Switching Our main question concerns the behavior of the vehicle when an emergency alert is received from DAB while another media source is active, such as Spotify via Bluetooth/CarPlay/Android Auto or an FM radio station.   Specifically, we would appreciate your technical clarification on the following points:   Automatic Source Switching: When an ASA emergency alert is received over DAB while the user is listening to FM radio or Spotify, how does the system automatically switch to the DAB emergency announcement and display the relevant alert information?   System Responsibility: Which component is responsible for this behavior? Is the alert detection and triggering handled by the ASA chip itself, or does the DAB receiver/head unit need a control interface that allows it to interrupt the currently active media source and switch to DAB audio?   Vehicle Integration: Does the DAB receiver directly control the audio source and display, or does it send an alert notification or trigger signal to the vehicle's infotainment system, which then performs the source switching and displays the alert?   Standards and Implementation: Does the relevant ASA/DAB standard define this behavior and the required interface between the receiver and the vehicle infotainment system, or are these implementation details left to the receiver manufacturer and vehicle OEM?   Technical Requirements: Are there any specific hardware interfaces, software APIs, control signals, or infotainment integration requirements necessary to ensure that an emergency alert can override the currently active media source?   Our objective is to understand whether this functionality is primarily provided by the ASA receiver/decoder or whether additional integration with the vehicle's infotainment system is required.   Any relevant technical documentation, system architecture diagrams, or implementation guidelines would be greatly appreciated. Re: ASA Emergency Alert Handling and Audio Source Switching Hi osmanistlink10 Thanks for your interest in NXP products. What's the NXP product part number related your questions?
View full article
无法生成c语言代码 当组件超过30个的时候,无法生成代码,软件卡住不动,等好长时间也没用 Re: 无法生成c语言代码 是的,GUI Guider 1.10.0 项目不能在 2.0.0 中直接打开,也不能自动升级。具体请参考:Tutorials — GUI Guider Documentation Re: 无法生成c语言代码 新版本的guiguider导入不了之前旧版本做的界面设计吗?我这点击导入没有反应,我之前用的是1.10.1-GA版本。 Re: 无法生成c语言代码 应该是的,我还没有试,但是我看内部ticket关了。等我空了给你测试下。 Re: 无法生成c语言代码 好的,最新版的不限组件数量吗 Re: 无法生成c语言代码 Hello @J_T @iyutong  这个问题在GUI-Guider的最新版 v2.0.x得到解决,可以在GUI Guider | NXP 半导体下载试用。 BR Celeste Re: 无法生成c语言代码 请问该问题解决了吗? Re: 无法生成c语言代码 好的,了解,我会报告给相关team。 Re: 无法生成c语言代码 最新版1.9.1,也问题依旧,卡这不动,但1.9.1是在50个的时候开住的 最新版1.9.1最新版1.9.1 Re: 无法生成c语言代码 你好,感谢发帖。方便提供更多细节吗?你用的哪个版本的gui-guider。只是添加三十个以上的组件就可以100%复现这个问题吗? 麻烦您帮忙提供更多信息,以便我更好的复现并把情况反映到相关team。感谢理解!
View full article
C言語コードを生成できません コンポーネントが30個を超えると、コードが生成されず、ソフトウェアがフリーズし、長時間経過しても何も起こりません。 Re: 无法生成c语言代码 はい、GUI Guider 1.10.0このプロジェクトはバージョン2.0.0では直接開くことができず、自動アップグレードもできません。詳細は「チュートリアル - GUI Guiderドキュメント」を参照してください。 Re: 无法生成c语言代码 新しいバージョンのGuiGuiderでは、古いバージョンで作成したインターフェースデザインをインポートできないのでしょうか?インポートボタンをクリックしても何も反応がありません。以前はバージョン1.10.1-GAを使用していました。 Re: 无法生成c语言代码 そうであるはずです。まだ試していませんが、内部チケットがクローズされているのを確認しました。時間があるときにテストしてみます。 Re: 无法生成c语言代码 最新バージョンでは、コンポーネントの数に制限はないのでしょうか? Re: 无法生成c语言代码 こんにちは@J_T @iyutong この問題は、GUI-Guiderの最新バージョンであるv2.0.xで解決されています。最新バージョンは、GUI Guider | NXP Semiconductorsからダウンロードして試用できます。 BR セレステ Re: 无法生成c语言代码 この問題は解決しましたか? Re: 无法生成c语言代码 わかりました。担当部署に報告します。 Re: 无法生成c语言代码 最新バージョンの1.9.1でも同じ問題が残っています。フリーズして動かなくなりますが、バージョン1.9.1では50ユニットでロックが解除されます。 最新版1.9.1最新バージョン1.9.1 Re: 无法生成c语言代码 こんにちは、投稿ありがとうございます。もう少し詳しい情報をお聞かせいただけますか?お使いのgui-guiderのバージョンは何ですか?30個以上のコンポーネントを追加するだけで、この問題を100%再現することは可能でしょうか? 問題の再現性を高め、関係部署に報告するために、もう少し詳しい情報をご提供いただけますでしょうか?ご理解いただきありがとうございます。
View full article
Unable to generate code The code generation process gets stuck. Re: 无法生成代码 Has this problem been resolved? Re: 无法生成代码 Hi @Cui5222, What version of GUI Guider are you using? Are you certain you are connected to the internet? Could you try running GUI Guider as administrator? 
View full article
エネルギー革命システムレビュー:本当に効果があるのか? 予測不能な停電や月々の電気料金の高騰、あるいはファミリのために信頼できるオフグリッドのエネルギーバックアップを構築したい方は、一人ではありません。 最近、エネルギー革命システムがインターネット上で爆発的な人気を博している。家庭でクリーンでポータブルな発電機の組み立て方を教えるステップバイステップのDIYガイドとして宣伝されており、オンラインのテックフォーラムやコミュニティの掲示板で大きな議論を巻き起こしています。 実際、ユーザーやDIY技術愛好家はNXPコミュニティフォーラムや技術系プラットフォーム&Aサイトなどでこのシステムについて活発に議論し、これらのDIY磁気コイルの原理が本当に家庭用電力に繋がるかどうかを問い合っています。 この衝撃的なレビューでは、エネルギー革命システムとは一体何なのか、どのように機能するのか、その中身は何なのか、そして2026年に実際にその約束が果たされるのかどうかを徹底的に検証します。 簡単な製品概要 製品名: エネルギー革命システム カテゴリ: オルタナティブエネルギー / DIYホーム改修 / オフグリッド電源 形式:デジタル設計図、ステップバイステップマニュアル、HDビデオガイド 組み立て時間: 2~4時間(初心者向け) 公式ポータル:公式エネルギー革命システムにアクセスするにはこちらをクリックしてください。 返金保証: 60日間(100%無条件返金) 評価: ⭐⭐⭐⭐⭐ (4.8/5) エネルギー革命システムとは何ですか? エネルギー革命システムは、初心者でも静かで軽量、かつ費用対効果の高い発電機を組み立てられるよう設計された、包括的なデジタル設計図です。 高価で騒音が大きく、燃費の悪い業務用発電機とは異なり、このシステムは磁気コイル、配線、バッテリーバンク、標準的なインバーターなど、入手しやすいハードウェア部品を使用して電流を収集することに重点を置いています。 目標は単純だ。 光熱費を大幅に削減:自家発電した電力を使って、日常的に使用する電子機器、照明器具、家電製品を動かしましょう。 停電時の緊急対策:悪天候などで電力網が停止した場合に備え、安全で屋内でも使用できる予備電源を用意しておきましょう。 それはどのように機能しますか? その中核となるメカニズムは、基本的な電気変換と共振の原理に基づいている。このプログラムでは、磁気エネルギー回収ユニットをディープサイクルバッテリーに接続する方法を説明します。 エネルギー捕捉:コイル構造により、微弱な電荷を効率的に捕捉します。 蓄電:エネルギーはバッテリー蓄電バンクに継続的に供給されます。 インバータ変換:シンプルなパワーインバータは、直流(DC)電荷を標準的な家庭用交流(AC)電力に変換します。 プラグ&プレイ: 家庭用の電源タップ、充電器、ランプ、扇風機、小型電子機器を直接ユニットに接続できます。 内燃機関を使用しないため、有害な排気ガスを一切発生させず、完全に静かに作動するため、リビングルーム、寝室、アパートなど、室内での使用も安全です。 ガイドブックには何が含まれていますか? 公式ウェブサイトから注文すると、以下のデジタルダウンロードへのアクセスを即座に得られます: 高解像度設計図と図面:すべての接続箇所と電線サイズを示す、読みやすい回路図。 ハードウェア材料の完全なチェックリスト: ホームデポ、ローズ、地元の家電店などでどの部品を最良の価格で買えばよいかを詳細に示したリストです。 HD高画質ウォークスルービデオチュートリアル:組み立ての最初から最後までを段階的に解説するビデオ説明。 メンテナンスおよび拡張マニュアル:バッテリー寿命の延長方法とセットアップのトラブルシューティングに関するガイダンス。 それは本当に効果があるのか?(衝撃の真実) はい、効果はあります。ただし、現実的な期待を持つことが前提です。 もし100ドルのDIYベンチビルドで5ベッドルームのマンションやインダストリアルエアコンを即座に動かせると期待しているなら、期待がっかりするでしょう。しかし、何千人ものDIYビルダーやコミュニティフォーラムのユーザーが確認しているように、設計図に従って作ると非常に信頼性の高い補助電源を提供します。 通常の家庭用電子機器、LED照明、Wi-Fiルーター、テレビ画面、携帯電話の充電器に優れており、電気メーターの負荷を大幅に軽減し、年間数百ドルの光熱費を節約できます。 長所と短所 メリット 大幅なコスト削減:毎月の電気料金をすぐに削減できます。 100%静かで安全:騒音の出るモーターや危険な一酸化炭素ガスは一切ありません。 初心者向け:電気に関する予備知識は一切不要です。分かりやすいビデオガイドがすべての手順を丁寧に解説します。 60日間返金保証:ガイドを2ヶ月間、完全にリスクなしでお試しください。 短所 組み立て必須: ハードウェア部品は別途購入し、2〜3時間かけて組み立てる必要があります。 デジタル形式のみ: PDFおよびビデオの即時ダウンロードにより電子的に配信されます。 最終結論:2026年に購入する価値はあるのか? 電力網の不安定さや電気料金が過去最高値に達する中、ご自宅のホームのエネルギー需要をコントロールすることは賢明な選択です。エネルギー革命システムは、一見複雑そうなDIY作業を楽しい週末プロジェクトに変えるための、シンプルで確実な設計図を提供します。 60日間の返金保証付きなので、失うものは何もありません。得られるのは、真のエネルギー自立です。 今すぐ割引アクセスを申請しましょう! 次の大きな嵐や価格高騰で停電に見舞われるまで待ってはいけません。今日からエネルギーの自由への第一歩を踏み出しましょう! 👉 こちらをクリックして公式エネルギー革命システムウェブサイトにアクセスし、今すぐ2026年の割引を申請しましょう!
View full article
Unable to generate C language code When there are more than 30 components, code cannot be generated, the software freezes, and nothing happens even after a long time. Re: 无法生成c语言代码 Yes, GUI Guider 1.10.0The project cannot be opened directly in version 2.0.0, nor can it be automatically upgraded. Please refer to: Tutorials — GUI Guider Documentation for details. Re: 无法生成c语言代码 Can't the new version of GuiGuider import interface designs created in the old version? I'm not getting any response when I click import. I was using version 1.10.1-GA before. Re: 无法生成c语言代码 It should be. I haven't tried it yet, but I see the internal ticket is closed. I'll test it for you when I have time. Re: 无法生成c语言代码 Okay, is the latest version unlimited in the number of components? Re: 无法生成c语言代码 Hello @J_T @iyutong This issue has been resolved in the latest version of GUI-Guider, v2.0.x, which can be downloaded and tried from GUI Guider | NXP Semiconductors . BR Celeste Re: 无法生成c语言代码 Has this problem been resolved? Re: 无法生成c语言代码 Okay, I understand. I will report it to the relevant team. Re: 无法生成c语言代码 The latest version, 1.9.1, still has the same problem; it's stuck and won't move, but version 1.9.1 unlocks at 50 units. 最新版1.9.1The latest version 1.9.1 Re: 无法生成c语言代码 Hello, thank you for posting. Could you provide more details? Which version of gui-guider are you using? Is it possible to 100% reproduce this problem simply by adding more than thirty components? Could you please provide more information so I can better reproduce the issue and report it to the relevant team? Thank you for your understanding!
View full article
哪个中子变流器与 i.MX95 电路板支持包 LF6.6.52_2.2.x 匹配?工具包 1.14 没有 Linux_6.6.52 文件夹。 我们正在 Toradex Verdin iMX95, B0 芯片上启用 Neutron NPU,运行来自 Toradex 电路板支持包。 7.7.0 的 Yocto 参考多媒体映像。这不是Torizon。内核版本为 6.6.142-7.7.0-devel,基于 NXP LF6.6.52_2.2.2。/dev/neutron0 存在,驱动程序会进行探测。 该镜像未包含 Neutron 固件。我们安装了“NeutronFirmware.elf”以及来自 nxp-imx/neutron 分支 lf-6.6.52_2.2.0 的“NeutronKernels.bin”。用户空间代理库和 Neutron 库都是从同一分支构建的。label_image 在容器中运行并到达 NPU。 eIQ 工具包 1.14.0安装程序 EIQ-TOOLKIT-WIN-1.14.0(日期为 2025 年 1 月 28 日)没有 Linux_6.6.52 变流器。该安装中最新的 Linux 变流器是 Linux_6.6.36_2.1.0。正在转换 mobilenet_v1_1.0_224_quant.tflite使用 --target imx95 参数会生成一个微代码为 0x5bfe0804 的模型。运行时,6.6.52 版本堆栈报告: 微代码版本不匹配!0x5bfe0804(预期为 0xa186aaf2) 已创建委托,并委托了一个节点,但分类分数为空。在 CPU 上,如果没有 Neutron 委托,相同的模型可以正确地为 grace_hopper.bmp 返回“军装”。 将固件和用户空间库替换为 lf-6.6.36_2.1.0版本删除了不匹配项,然后 6.6.52 内核驱动程序因无法创建中子推理作业而导致作业失败,中子驱动程序内部故障代码 442。6.6.36 库无法与此内核通信。 eIQ Toolkit 版本说明指出,i.MX95 电路板支持包。 LF6.6.52_2.2.x 的 Neutron 变流器仅在 eIQ Toolkit 1.14 中可用。我们拥有的 1.14 安装程序中不包含它。 哪个变流器二进制会为该电路板支持包。生成微代码 0xa186aaf2?它包含在哪个 eIQ Toolkit 或 Neutron SDK 软件包中? Re: Which neutron-converter matches i.MX95 BSP LF6.6.52_2.2.x? Toolkit 1.14 has no Linux_6.6.52 fold 你好@Giorgos_Sofroniou 预建变流器仅在eIQ Ubuntu版本上可用。 此致, 志明
View full article
gAdvertisingStateChanged_cは、どの広告リクエストが完了したかを示していますか? こんにちは、 gAdvertisingStateChanged_cイベントについて質問があります。 Gap_StartAdvertising()またはGap_StopAdvertising()が呼び出されると、アプリケーションはgAdvertisingStateChanged_cイベントを待ってから次の操作に進みます。 しかし、受信したgAdvertisingStateChanged_cイベント情報が過去のGap_StartAdvertising()リクエストに対応しているのか、それとも以前のGap_StopAdvertising()リクエストに対応しているのかを確実に判断する方法はありますか? 例えば、広告状態の変更リクエストがほぼ同時に発行された場合、アプリケーションは特定の gAdvertisingStateChanged_c イベント情報をトリガーした API 呼び出しと関連付けることができるでしょうか? それとも、アプリが独自の州情報を維持して、保留中の広告リクエストを追跡することが推奨されるのでしょうか? ありがとうございます。 プロトコル:Bluetooth Re: Does gAdvertisingStateChanged_c indicate which advertising request completed? こんにちは、 ご説明いただきありがとうございます。 gAdvertisingStateChanged_c自体は、それが広告の開始要求によってトリガーされたのか、停止要求によってトリガーされたのかを示していないことが、今理解できました。ビーコンの例を確認すると、アプリケーションは内部で期待状態(例えばmAdvertisingOnやmAppTargetStateなどの変数を用いて)を追跡し、自身の状態機械に基づいてイベント情報を解釈しているようです。 ご支援ありがとうございます。このThreadは閉じます。 よろしくお願いいたします。 Re: Does gAdvertisingStateChanged_c indicate which advertising request completed? こんにちは、 @hyama さん。お元気でお過ごしでしょうか。 gAdvertisingStateChanged_cイベントには、広告の開始/停止コールによってトリガーされたかどうかを示す情報は含まれていません。推奨されているのは、アプリケーションが独自の状態を維持し、さらなる変更を追跡することです。 開発の参考として、 wireless_examples/bluetooth/beaconのSDK例を参照することをお勧めします。そこにはソフトウェア定義フラグを通じて広告イベント情報を追跡する実装が含まれています。 これが役に立つかどうか教えてください。
View full article
ASA緊急警報処理およびオーディオソース切り替え 主な質問は、Bluetooth/CarPlay/Android 車載経由でSpotifyやFMラジオ局など、他のメディアソースが稼働している間にDABから緊急警報が届いた際の車載の挙動に関するものです。   具体的には、以下の点について技術的なご説明をいただければ幸いです。   自動ソース切り替え:ユーザーがFMラジオやSpotifyを聴いている間にDABでASA緊急警報が受信された場合、システムはどのようにして自動的にDAB緊急アナウンスに切り替わり、関連するアラート情報を表示するのでしょうか?   システム責任:この動作の原因はどのコンポーネントにあるのでしょうか?アラートの検出やトリガーはASAチップ自体が処理しているのか、それともDABレシーバやヘッドユニットが、現在アクティブなメディアソースを中断してDABオーディオにスイッチできる制御インターフェースが必要なのでしょうか?   車載統合:DABレシーバはオーディオソースと表示を直接制御するのか、それとも車載のインフォテインメントシステムにアラート通知やトリガー信号を送り、その後ソース切り替えを行いアラートを表示するのか?   規格と実装:関連するASA/DAB標準はこの挙動やレシーバと車載インフォテインメントシステム間の必要なインターフェースを定義しているのか、それともこれらの実装の詳細はレシーバメーカーや車載OEMに委ねられているのか?   技術的要件:緊急警報が現在アクティブなメディアソースを上書きできるようにするために、特定のハードウェアインターフェース、ソフトウェアAPI、制御信号、またはインフォテインメント統合の要件はありますか?   私たちの目的は、この機能が主にASAレシーバ/デコーダーによって提供されているのか、それとも車載のインフォテインメントシステムとの追加統合が必要なのかを理解することです。   関連する技術ドキュメント、システムアーキテクチャ図、実装ガイドラインなどがあれば大変ありがたいです。 Re: ASA Emergency Alert Handling and Audio Source Switching こんにちは、osmanistlink10さん NXP製品にご関心いただきありがとうございます。 質問の際、NXPの製品部品番号は何ですか?
View full article
ECU BUS PRO ブートローダーを実装しようとしています。   バイナリファイルからMCUにデータをロードする必要があり、ECU BUS PROがこの機能を果たすことは理解しています。 しかし、最新バージョン(現在ECU BUS PRO 0.8.15を使用)では、バイナリファイルを添付するオプションがありません。 この機能は以前のバージョンでは利用可能だったようです。古いバージョンはどこで見つけてダウンロードできますか? これを実現するための代替案はありますか? Re: ECU BUS PRO こんにちは、 現在、 s32k342用のブートローダーを開発中です。開発はRTDバージョン6.0で行われています。(同じRTDバージョンはs32k344のブートローダー構築にも使用されており、これは機能し、ECUBUS Pro経由でアプリケーションをフラッシュする作業も完了しています) バス・マスタでCAN通信を確認しました。リクエスト0x02 10 03に対して、レスポンス0x02 50 03を受け取りました。 現在、Ecubus Proを介した通信に問題が発生しています。ECUBUS Proで同じリクエストを送信すると、バスエラーまたは上位レイヤータイムアウトが発生します。 私は以下のデバッグ作業を行いました。 CANのIDとそのフォーマットを照合しました。 user_config.h:CAN_RX:0x731、CAN_TX=0x739 EcuBus proインターフェース:CAN_TX=0x731、CAN_RX = 0x739 両CASEとも標準CANIdを使用しています ボーレート:500kbps、 CANビットタイミング: S32DSでg_RXCANMsgバッファをリアルタイムで監視すると、テスターからの要求メッセージがバッファに格納されます。 なぜバス・マスタで応答を受け取れるのに、EcuBus Proには返答が送られないのでしょうか? フラッシュ撮影中に他に注意すべき点はありますか?   ありがとう、 アキラ。 Re: ECU BUS PRO こちらをお試しください: https://app.whyengineer.com/examples/nxp_bootloader/readme.html Re: ECU BUS PRO こんにちは、 @parksuhun さん。 1.GitHubのEcuBusのリリースタブ(Releases · ecubus/EcuBus-Pro)に入り、すべてのプレビュビュスリリースを見つけることができます。 2. AN12323 S32K1xx Firmware updates – Application Noteも参照できます。ここではブートローダーとファームウェアアップデートの基本を説明しており、一方のボードがCAN経由でFWアップデートを送信し、もう一方のボードが更新されるデモも含まれています。 よろしくお願いします、 ジュリアン
View full article
Does gAdvertisingStateChanged_c indicate which advertising request completed? Hello, I have a question regarding the gAdvertisingStateChanged_c event. When Gap_StartAdvertising() or Gap_StopAdvertising() is called, the application waits for the gAdvertisingStateChanged_c event before proceeding to the next operation. However, is there a reliable way to determine whether a received gAdvertisingStateChanged_c event corresponds to a previous Gap_StartAdvertising() request or a previous Gap_StopAdvertising() request? For example, if advertising state change requests are issued close together, can the application correlate a specific gAdvertisingStateChanged_c event with the API call that triggered it? Or is it recommended that the application maintain its own state information to track pending advertising requests? Thanks. Protocol: Bluetooth Re: Does gAdvertisingStateChanged_c indicate which advertising request completed? Hello, Thank you for the clarification. I understand now that gAdvertisingStateChanged_c itself does not indicate whether it was triggered by an advertising start or stop request. After reviewing the beacon example, it appears that the application keeps track of the expected state internally (for example, by using variables such as mAdvertisingOn or mAppTargetState) and interprets the event based on its own state machine. Thank you for your support. I will close this thread. Best regards, Re: Does gAdvertisingStateChanged_c indicate which advertising request completed? Hello @hyama, hope you are doing well. The gAdvertisingStateChanged_c event does not contain information indicating whether it was triggered by an advertising start/stop call. The recommendation is that the application maintain its own state and further changes tracked. For reference on your development, I'd suggest referring to the SDK example at: wireless_examples/bluetooth/beacon, as it contains an implementation that tracks the advertising events through a software-defined flag. Please let me know if this helps.
View full article
ECU BUS PRO I am trying to implement a Bootloader.   I need to load data from a binary file into the MCU, and I understand that ECU BUS PRO performs this function. However, in the latest version (currently using ECU BUS PRO 0.8.15), there is no option to attach a binary file. It seems that this feature was available in older versions. Where can I find and download an older version? Are there any alternative solutions to achieve this? Re: ECU BUS PRO Hi,  I am currently working on bootloader for s32k342. The development is done in RTD version 6.0.  (The Same RTD version is used to build bootloader for s32k344, which is functional and flashing application via ECUBUS Pro was completed) I verified the CAN communication in bus master. For Request 0x02 10 03, I am getting response 0x02 50 03.  Now I am facing problem in Communicating through Ecubus Pro. The same request send on ECUBUS Pro gives me Bus error or Upper layer timeout.  I did the following debugging: Cross checked the CAN IDs and its format in user_config.h: CAN_RX:0x731, CAN_TX= 0x739 EcuBus pro interface: CAN_TX=0x731, CAN_RX = 0x739 Both the cases uses Standard CANId Baudrate:500kbps, CAN bit timing:   Monitored the g_RXCANMsg buffer on real time in S32DS, the request msg from the tester is stored in the buffer. Why No response is being send back to EcuBus Pro when I can receive the response in Bus master? Is there anything else to be taken care while flashing?   Thanks,  Akhila. Re: ECU BUS PRO try this: https://app.whyengineer.com/examples/nxp_bootloader/readme.html Re: ECU BUS PRO Hi @parksuhun, 1. You can go into EcuBus' release tab in github (Releases · ecubus/EcuBus-Pro) where you can find all of the preivous releases. 2. You can also refer to the AN12323: S32K1xx Firmware updates – Application Note, which explains the bootloader and firmware update basics, as well as including a demo where one board sends a FW update through CAN, and the second board is updated. Best regards, Julián
View full article