Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
s32k396 Basic Secure Boot qeustion On a 32K396, HSE FW 0.2.50.0 FULL_MEM is used, and the current lifetime is CUST_DEL. Testing Process: Initially, the system ran normally. Then, the address 0x00453FF0 within the authentication range was changed from 0xFF to 0xFE, while keeping the AppBL Header, authentication tag, and IVT unchanged. The IVT bootCfgWord was set to 0x00000009. After powering off and on again, a J-Link Attach connection was used, without downloading the image, and RAM/ECC initialization during connection was disabled using an empty SetupTarget. At this point, the PC stopped at 0x2040012E. The instructions from 0x2040012C to 0x2040012E are WFI and branches that jump back to WFI, consistent with the JTAG Recovery wait loop. Currently, no user Secure Recovery application is configured. Question: Please confirm the complete handling process and reliable criteria for this version after BSB authentication failure: Why is GPR3 bit5 still 0 even after entering the JTAG Recovery waiting loop? Is it related to the fact that this bit only indicates "SBAF boot application kernel into Recovery" and the current recovery path is triggered by HSE FW? And which status bit or error message should be used to clearly confirm that the failure is due to AppBL authentication failure? Re: s32k396 Basic Secure Boot qeustion Thank you for the detailed test description. The statement that no user Secure Recovery application is configured may be important here. Could you please clarify how the recovery flow is intended to work in your configuration? In particular: What recovery action is expected after the AppBL authentication failure if no Secure Recovery application is configured? Was JTAG Recovery explicitly configured and enabled? Is the observed WFI loop itself considered unexpected, or is the concern only that GPR3[5] remains cleared? Please provide the relevant recovery configuration and the HSE/SBAF status information read immediately after connecting with J-Link. The observed WFI loop may be expected if no user Secure Recovery application is configured. Therefore, please first clarify the intended recovery flow and the expected device behavior after the AppBL authentication failure. Re: s32k396 Basic Secure Boot qeustion We observed that bit 5 of gpr3 was not set. This is a flag bit, and the manual states that it should be set to 1 in recovery mode. Why didn't it recover? Detailed tests are attached.
View full article
LInux CAAMドライバは=mではなく=yでコンパイルされています Linux 6.18.2_1.0.0まではCONFIG =yモードでCAAMドライバをコンパイルできていました。しかし、最近のLinux 6.18.20_2.0.0やLinux 6.18.37_2.1.0では、カーネル内蔵証明書エラーが発生しました。 CRYPTO_DEV_FSL_CAAM_PKC、セキュア、信頼された鍵のオン/オフなどのCAAM設定を変更してみました。これで証明書がCAAMとは独立するはずですが、SILL CERTIFICATEはCAAMドライバーを=mモードにするまで壊れています。 CAAMドライバーを=yとして使うことは可能ですか?私はi.MX7を使用しています。ありがとう Re: LInux CAAM driver compiled =y instead of =m この問題が発生するかどうかを確認するには、「CONFIG_TRUSTED_KEYS_CAAM」を無効にして「n」に設定してください。 SDKsのデフォルトビルド設定で、以下の情報を見つけました。 # CONFIG_TRUSTED_KEYS_CAAM が設定されていません Re: LInux CAAM driver compiled =y instead of =m おそらく6.18.2では既に動作していなかったのでしょう。よくわからない。6.12.xでは確かに動作したはずです。 CAAM_DEBUGを有効にして、 zcat /proc/config.gz | grep CAAM # CONFIG_CRYPTO_DEV_FSL_CAAM_DMA が設定されていません CONFIG_TRUSTED_KEYS_CAAM=y CONFIG_CRYPTO_DEV_FSL_CAAM_COMMON=y CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y CONFIG_CRYPTO_DEV_FSL_CAAM_KEYBLOB_API_DESC=y CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO=y CONFIG_CRYPTO_DEV_FSL_CAAM=y CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG=y CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9 # CONFIG_CRYPTO_DEV_FSL_CAAM_INTC が設定されていません CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y CONFIG_CRYPTO_DEV_FSL_CAAM_PRNG_API=y CONFIG_CRYPTO_DEV_FSL_CAAM_BLOB_GEN=y CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y # CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API_TEST が設定されていません # CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST が設定されていません CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y CONFIG_CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE=7 CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST=m dmesgでこれが表示されます [ 0.600724] caam 30900000.crypto: entropy-delay property missing in DT [ 0.600757] caam 30900000.crypto: device ID = 0x0a16030000000000 (Era 8) [ 0.600776] caam 30900000.crypto: job rings = 3, qi = 0 [ 0.609580] sdhci-esdhc-imx 30b40000.mmc: Got CD GPIO [ 0.614915] caam algorithms registered in /proc/crypto [ 0.615107] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto [ 0.615138] caam 30900000.crypto: rng crypto API alg registered prng-caam [ 0.615157] caam 30900000.crypto: registering rng-caam [ 0.615184] 01: operation [ 0.615198] 02: fifo_store [ 0.615217] rng job desc@: (ptrval): b0800004 82500002 60340010 81cf2500 ......P...4`.%.. [ 0.615405] 01: operation [ 0.615423] 02: fifo_store [ 0.615440] rng job desc@: (ptrval): b0800004 82500002 60340010 8126fac0 ......P...4`..&. [ 0.616325] Device caam-keygen registered [ 0.620411] caam-snvs 30370000.caam-snvs: ipid matched - 0x3e [ 0.620477] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state [ 0.621041] hid: raw HID events driver (C) Jiri Kosina [ 0.621217] usbcore: registered new interface driver usbhid [ 0.621230] usbhid: USB HID core driver [ 0.624128] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 (8000000f) counters available [ 0.627983] NET: Registered PF_INET6 protocol family [ 0.629380] Segment Routing with IPv6 [ 0.629471] In-situ OAM (IOAM) with IPv6 [ 0.629630] NET: Registered PF_PACKET protocol family [ 0.629705] Bridge firewalling registered [ 0.629717] can: controller area network core [ 0.629795] NET: Registered PF_CAN protocol family [ 0.629810] can: raw protocol [ 0.630378] Key type dns_resolver registered [ 0.637395] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 1 supported-hw 0x4 0x2 [ 0.638671] Registering SWP/SWPB emulation handler [ 0.649825] Loading compiled-in X.509 certificates [ 0.650591] 07: operation [ 0.651164] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA [ 0.674771] 01: operation [ 0.674791] 02: fifo_store [ 0.674811] rng job desc@: (ptrval): b0800004 82500002 60340010 8126fac0 ......P...4`..&. [ 0.679492] Problem loading in-kernel X.509 certificate (-22) Re: LInux CAAM driver compiled =y instead of =m はい、CAAMは原理的にi.MX7上で=yである場合があります。私は、=m の回避策を i.MX7 CAAM の要件ではなく、依存関係/ビルドの回帰の証拠として扱います。 LF6.18.20_2.0.0ビルドの最初の証明書エラーを正確に貼り付ければ、どのKconfig/Makefile依存関係が原因かを追跡し、特定のNXPやアップストリームパッチでバックポートが必要なかどうかを判断できます。 Re: LInux CAAM driver compiled =y instead of =m 信頼済みキーのオン/オフを含む関連設定をすべて変更してみましたが、CAAMを=mモードに切り替えるまで変化はありませんでした。 Re: LInux CAAM driver compiled =y instead of =m もしそうなら、Yocto SDKと同様にCAAMドライバー=mの設定をしてください。 Re: LInux CAAM driver compiled =y instead of =m 質問はyの問題に関するものでした。明らかに、6.12aと6.18カーネルの間で何らかの不具合が発生した。
View full article
About CW 3.1 Who can provide a download link for CodeWarrior 3.1 that runs on Windows XP? The file  name may be Codewarrior-HC(S)08-v3.1.iso.  Thanks a lot. Re: About CW 3.1 I'm really sorry for the inconvenience this might cause you, but the information and files of this software version is no longer available for download, I need to clarify that CodeWarrior 3.1 is a legacy product. The search results indicate that some CodeWarrior versions for specific devices have not been supported in years, and NXP has transitioned away from maintaining certain legacy CodeWarrior implementations.   You could move to a more recent version, The software tool to use 8 bits devices is CodeWarrior for MCUs (Eclipse IDE) v11.1 available for windows 10/11; in this tool you can test with various 8-bit devices if you are interested. Best Regards
View full article
Request for "AES_ACCEL Subsystem Reference Manual" Hi NXP  I am currently analyzing the AES_ACCEL (AES Accelerator) module for my project. The documentation mentions referring to the "AES_ACCEL Subsystem Reference Manual", but I am unable to locate or download it from the product page. Could you please let me know where I can obtain this manual, or how I can gain access to download it? Best regards Re: Request for "AES_ACCEL Subsystem Reference Manual" The document is a secure file. Please follow the secure access registration procedure described here, unless you have already completed it: NXP Secure Access Rights Registration For additional information, please refer to: NXP Secure Access Rights Because this particular file has a higher confidentiality level, access is subject to manual approval. If you have already completed the registration but the file is still not available, please contact your NXP representative or distributor and ask them to request the required access for you.
View full article
s32k396 基本セキュアブートに関する質問 32K396では、HSE FW 0.2.50.0 FULL_MEMが使用され、現在の有効期間はCUST_DELです。 テストプロセス:最初は、システムは正常に動作しました。次に、認証範囲内のアドレス 0x00453FF0 を 0xFF から 0xFE に変更し、AppBL ヘッダー、認証タグ、および IVT は変更しませんでした。IVT bootCfgWord を 0x00000009 に設定しました。電源をオフにしてから再度オンにした後、イメージをダウンロードせずに J-Link Attach 接続を使用し、空の SetupTarget を使用して接続中の RAM/ECC 初期化を無効にしました。この時点で、PC は 0x2040012E で停止しました。0x2040012C から 0x2040012E までの命令は WFI および WFI に戻る分岐であり、JTAG リカバリ待機ループと一致しています。現在、ユーザーのセキュアリカバリアプリケーションは構成されていません。 質問: BSB認証失敗後のこのバージョンの完全な処理プロセスと信頼できる基準を確認してください。JTAGリカバリ待機ループに入った後もGPR3ビット5が0のままなのはなぜですか?このビットは「SBAFブートアプリケーションカーネルがリカバリに入った」ことのみを示し、リカバリパスはHSE FWによってトリガーされることに関係していますか?また、どのステータスビットまたはエラーメッセージを使用して、失敗の原因がAppBL認証失敗であることを明確に確認する必要がありますか? Re: s32k396 Basic Secure Boot qeustion 詳細なテスト説明をありがとうございました。ここで重要なのは、ユーザーのSecure Recoveryアプリケーションが設定されていないということです。 あなたの設定でリカバリーフローがどのように機能するのか、詳しく教えていただけますか?特に: Secure Recoveryアプリケーションが設定されていない場合、AppBL認証失敗後にどのような復旧アクションが期待されますか? JTAGリカバリは明示的に設定され、有効化されていましたか? 観測されたWFIループ自体は予期せぬものとみなされるのか、それともGPR3[5]がクリアされたままであることだけが懸念事項なのか? J-Linkとの接続直後に読み取った、関連する復旧構成情報とHSE/SBAFステータス情報を提供してください。 ユーザーのSecure Recoveryアプリケーションが設定されていなければ、観察されるWFIループは予想されます。したがって、まずはAppBL認証失敗後の想定される回復フローとデバイスの動作を明確にしてください。 Re: s32k396 Basic Secure Boot qeustion gpr3のビット5が設定されていないことを確認しました。これはフラグビットであり、マニュアルにはリカバリモードでは1に設定されるべきと記載されています。なぜリカバリされなかったのでしょうか?詳細なテスト結果を添付します。
View full article
周辺DMA TCD「START」フィールド S32Z2リファレンスマニュアルのバージョン5は1399ページの1に記載しています。 「1. ユーザーがTCDn_CSR[START]フィールドに書き込み、チャネルサービスをリクエストする。」 同じ文書の1354ページにあるTCD CSRのメモリマップには、「START」という名前のCSRのフィールドは表示されていません。TCDn_CSRのどのビットがSTARTビットですか?SWから手動転送を開始しようとしています。 Re: Peripheral DMA TCD "START" FIELD こんにちは、ロバートさん。 ご指摘ありがとうございます。 レジスタマップは TCDn_CSR レジスタとそのオフセットを識別しますが、個々のビットフィールドは一覧表示しません。現場の定義については、同じS32Z2リファレンスマニュアルの1383–1385ページにあるセクション45.3.2.18「TCD制御および状態(TCD0_CSR - TCD31_CSR)」を参照してください。 このセクションでは、 START フィールドが TCDn_CSR のビット 0、つまり TCDn_CSR[0] であることを示しています。 これで、登録簿マップと詳細な登録簿の説明との間の明らかな違いが明確になったことを願います。 よろしくお願いします、 アルド。 Re: Peripheral DMA TCD "START" FIELD ああ、なるほど。ご説明ありがとうございます。
View full article
How to generate exact manual ABZ edge counts (pulse-by-pulse) on i.MX RT1186? I'm using i.MX RT1186 to replace an FPGA. I read a Tamagawa encoder via FLEXIO1, and I need to output an ABZ signal where the number of edges exactly matches the position delta. Because continuous PWM cannot control exact edge counts, I already tried eFlexPWM (SWCOUT/FORCE_OUT). However, when I trigger rapid consecutive updates, the output doesn't match my expectations (e.g., I expected 10 edges but only observed 3). So, are there other dedicated peripherals (like a hardware pulse generator) for this exact requirement, or must I use GPIO bit-banging? Also, since FLEXIO1 is used for T-format, is sharing it for State Mode output a conflict? Thank you. Re: How to generate exact manual ABZ edge counts (pulse-by-pulse) on i.MX RT1186? Dear @rejust , Thanks for your question. To achieve an exact pulse count, a feedback mechanism is needed to count the AB pulse edges that have already been generated. Once the required number of edges is reached, the pulse output can be stopped. Please refer to the diagram below for illustration. You can use a short periodic task, for example a 1 ms task, to dynamically control the start/stop operation and output period of the eFlexPWM based on the number of edges that need to be generated and the number of edges that have actually been generated.   For example, if the encoder position changes by 100 counts within 1 ms, 100 A/B edges need to be generated. Since one complete A/B quadrature cycle contains four edges, this corresponds to 25 A/B cycles within 1 ms. Therefore, the required eFlexPWM frequency is: 25 / 1 ms = 25 kHz Some boundary conditions should also be considered. For example, if only 99 edges( the actual value is obtained by decoding the AB quadrature signals using the eQDC ) are actually generated during this 1 ms interval, the remaining edge should be carried over to the next 1 ms interval instead of being discarded. This prevents the position error from accumulating over time. The periodic task can therefore continuously compare the required number of edges with the number of edges already generated, and adjust the eFlexPWM operation accordingly. When the number of remaining edges is less than or equal to the allowed position error, the eFlexPWM output can be stopped. Best Regards, Shelly   Re: How to generate exact manual ABZ edge counts (pulse-by-pulse) on i.MX RT1186? Dear @ShellyZhang  Thank you for your detailed explanation and diagram. However, I need to first emphasize my application scenario: I want to use the MIMXRT1186XVJ8C to replace an original MCU + FPGA setup. I need to read the encoder signal and simultaneously output an ABZ signal to external devices (used only as a position feedback signal for monitoring/testing purposes). My requirement is to have the output edge count strictly match the position delta, behaving like a direct hardware state machine (e.g., an FPGA pulse generator). Can eFlexPWM, or any other dedicated peripherals on the RT1186, achieve this exact edge-by-edge output? Thank you.
View full article
Peripheral DMA TCD "START" FIELD Version 5 of the S32Z2 Reference Manual states on page 1399 bullet 1. "1.User write to the TCDn_CSR[START] field requests channel service." The memory map for the TCD CSR on page 1354 in the same document does not show any field for the CSR named "START". Which bit of the TCDn_CSR is the START bit? I'm trying to start a manual transfer from SW. Re: Peripheral DMA TCD "START" FIELD Hi Robert, Thank you for pointing this out. The register map identifies the TCDn_CSR register and its offset, but it does not list the individual bit fields. For the field definitions, please refer to Section 45.3.2.18, “TCD Control and Status (TCD0_CSR - TCD31_CSR),” on pages 1383–1385 of the same S32Z2 Reference Manual. This section shows that the START field is bit 0 of TCDn_CSR , i.e. TCDn_CSR[0] .  I hope this clarifies the apparent difference between the register map and the detailed register description. Best regards, Aldo. Re: Peripheral DMA TCD "START" FIELD Ah, gotcha. Thanks for the clarification.
View full article
「AES_ACCELサブシステムリファレンス・マニュアル」の要請 こんにちは、NXPさん 現在、プロジェクトのためにAES_ACCEL(AESアクセラレータ)モジュールを分析しています。 ドキュメントには 「AES_ACCELサブシステムリファレンス・マニュアル」を参照していると書かれていますが、製品ページから見つけたりダウンロードしたりできません。 このマニュアルをどこで入手できるのか、またはダウンロードのアクセス方法を教えていただけますか? よろしくお願いいたします。 Re: Request for "AES_ACCEL Subsystem Reference Manual" この文書は安全なファイルです。すでに手続きを完了している場合は、ここに記載された安全なアクセス登録手順に従ってください。 NXPセキュアアクセス権登録 詳細については、以下を参照してください。 NXPセキュアアクセス権 この特定のファイルはより高い機密性レベルであるため、アクセスは手動承認の対象となります。すでに登録を完了しているのにファイルがまだ利用できない場合は、NXPの担当者または代理店にお問い合わせのうえ、必要なアクセス権の申請をお願いしてください。
View full article
EBトレソス こんにちは!NXPのウェブサイトでEB TRESOSのバージョン32.1.4は入手できますか? Re: EB TRESOS こんにちは、トニーさん。 社内チームに連絡を取り、返答を待っています。 よろしくお願いします、 ロビン Re: EB TRESOS それはまだ存在しないようだ。 Re: EB TRESOS 今すぐダウンロードできるはずです。 S32K3標準ソフトウェア-> 自動車ソフトウェア - EB tresos Studio / AUTOSAR構成ツール -> EB tresos Studio 32.1.4 をクリックしてください。 回复: EB TRESOS ありがとうございます。すべて準備完了です。 Re: EB TRESOS こんにちは、ロビンさん。 EB Tresos Studio 32.1.4が見つかりませんパス上で、EB tresos Studio 30.0.0を一番上位に見つけてください。どこでダウンロードできますか(EB tresos Studio 32.1.4)? Re: EB TRESOS ありがとう。 新しい質問がこちらに投稿されました: https://community.nxp.com/t5/S32K/EB-tresos-Studio-32-1-4/mp/2422512 Re: EB TRESOS コミュニティに新しい質問を投稿していただければ、FlexNetの同僚に連絡し、このバージョンのソフトウェアをあなたのアカウントに追加します。
View full article
AN4908SW 下载 您好, 我的谷歌搜索技巧好像出了问题,因为我到处都找不到“AN4908SW 发动机控制 eTPU 演示应用程序”。 请问有人能提供链接或压缩文件吗? 谢谢您! 回复: AN4908SW download 嗨,Peter,我也在寻找用于 MPC5674F 开发的 AN4908SW 软件包。能否也发到我的邮箱里?谢谢你! Re: AN4908SW download 你好, 非常感谢! 干杯, 何塞 Re: AN4908SW download 你好, 我已经发送到你的邮箱了。 顺祝商祺! Peter
View full article
データベースファイルを共有メモリにアップロードする方法 こんにちは。現在S32G VNP RDB2ボードを使用しています。クライアントからデータベースファイルを共有メモリに配置するように依頼されましたが、データベースファイルを共有メモリにアップロードすることは可能でしょうか? どんなアドバイスでも本当にありがたいです Re: How to upload Database file to share memory こんにちは@Poji9900 S32Gプラットフォーム内でデータベース導入に関する文書やガイドは提供していません。この特定の状況については当社が技術サポートのチャネルでない場合があるため、データベース導入に関しては関連する技術サポートチームにお問い合わせください。 ご不便をおかけして申し訳ありません。 敬具、ミゲル
View full article
How to upload Database file to share memory Hey there, Im currently working with S32G VNP RDB2 board, My client ask me to put one of his database file to shared memory, is it possible to upload database file in to shared memory,  any guidence im really appreciate  Re: How to upload Database file to share memory Hi @Poji9900  We do not provide any documents or guides within the S32G platform for database implementation. We may not be the channel to provide technical support on this specific situation, we recommend contacting the related technical support team on regards of your database implementation. We do apologize for the inconvenience. Best Regards, Miguel
View full article
EB TRESOS Hello! Is EB TRESOS 32.1.4 available on the NXP website? Re: EB TRESOS Hi Tony. I have contacted the internal team and am awaiting their response. Best Regards, Robin Re: EB TRESOS It should be available for download now. Please click on S32K3 Standard Software - > Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool - > EB tresos Studio 32.1.4 Re: EB TRESOS It still doesn't look like it exists. 回复: EB TRESOS Thanks, it's all good. Re: EB TRESOS Thanks. A new question posted here: https://community.nxp.com/t5/S32K/EB-tresos-Studio-32-1-4/m-p/2422512 Re: EB TRESOS Hi Robin, I can't find EB tresos Studio 32.1.4 on the path, just find EB tresos Studio 30.0.0 the highest, Where could I download it(EB tresos Studio 32.1.4)? Re: EB TRESOS Please post a new question in the community, and we will then contact our colleagues at FlexNet to add this version of the software to your account.
View full article
EB TRESOS 你好!EB TRESOS 32.1.4的版本NXP官网有提供吗? Re: EB TRESOS Hi Tony, 我已经联系了内部团队,正在等待他们的答复。 Best Regards, Robin Re: EB TRESOS 看上去它还是不存在 Re: EB TRESOS 现在应该可以下载了。 请点击 S32K3 Standard Software -> Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool -> EB tresos Studio 32.1.4 回复: EB TRESOS 谢谢,已经OK Re: EB TRESOS 谢谢。 这里发布了一个新问题: https://community.nxp.com/t5/S32K/EB-tresos-Studio-32-1-4/mp/2422512 Re: EB TRESOS 嗨,罗宾, 我找不到 EB tresos Studio 32.1.4在路径中,只需找到最高版本的 EB tresos Studio 30.0.0 即可。请问在哪里可以下载到 EB tresos Studio 32.1.4? Re: EB TRESOS 请在社区中发布一个新问题,我们将联系 FlexNet 的同事,将此版本的软件添加到您的帐户中。
View full article
LINUX环境 下开发S32K324咨询   在UBUNT24版本下,使用S32DS进行底层软件配置。此方案是否可行 ?主要疑虑点是linux 下关于S32DS 3.6.11版本 使用config tools 工具生成配置后,RTE是否已经可以生成代码 ? Re: LINUX环境 下开发S32K324咨询 希望能上报此需求并建立更新计划 Re: LINUX环境 下开发S32K324咨询 Hi@han00 这不是bug,只是RTD不适配LINUX系统,我没看到RTD有适配LINUX系统的计划。 Re: LINUX环境 下开发S32K324咨询 @ Senlent 我看到参考链接日期是2024.1.18的,我想确认这个问题是否仍未被修复 Re: LINUX环境 下开发S32K324咨询 Hi@han00 建议使用windows开发,LINUX环境下的RTD生成存在问题。 参考回答: https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/td-p/1791431
View full article
Consulting on S32K324 development in a Linux environment Is it feasible to use S32DS for low-level software configuration under Ubuntu 24? The main concern is with S32DS version 3.6.11 under Linux.After generating the configuration using the config tools, can the RTE generate code ? Re: LINUX环境 下开发S32K324咨询 We hope to report this request and establish an update plan. Re: LINUX环境 下开发S32K324咨询 Hi@ han00 This is not a bug; it's just that RTD is not compatible with Linux systems, and I haven't seen any plans to adapt RTD to Linux systems. Re: LINUX环境 下开发S32K324咨询 @Senlent I see the reference link is dated January 18, 2024. I want to confirm if this issue has still not been fixed. Re: LINUX环境 下开发S32K324咨询 Hi@ han00 It is recommended to use Windows for development, as there are issues with RTD generation under the Linux environment. Suggested answer: https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/td-p/1791431
View full article
AN4908SWのダウンロード こんにちは、 私のGoogle検索がうまくいかず、「AN4908SW Engine Control eTPU Demo Application」がどこにも見つからないようです。 どなたかリンクかzipファイルを教えてもらえますか? よろしくお願いします! 回复: AN4908SW download こんにちは、ピーター。私もMPC5674F開発のためのAN4908SWパッケージを探しています。メールにも送ってもらえますか?ありがとう! Re: AN4908SW download こんにちは、 どうもありがとうございます! 乾杯、 ホセ Re: AN4908SW download こんにちは、 あなたのメールアドレスに送信しました。 よろしくお願いいたします。 ピーター
View full article
i.MX8MP EVKのToFセンサー VL53L8CX SPI通信を有効にする 私たちは、Yocto Linuxを使用したNXP i.MX8MP LPDDR4 EVKにST VL53L8CX ToF(飛行時分)センサーをSPI経由で統合しようとしています。 最初の目的は、基本的なSPI通信を実現し、カスタムLinuxカーネルドライバからVL53L8CXデバイスを正常に検出することです。現段階では、完全な測距機能は必要ありません。 ハードウェア ボード: NXP i.MX8MP LPDDR4 EVK センサー: VL53L8CX ToFセンサー インターフェース: SPI EVKコネクタ: J21拡張コネクタ SPIコントローラー: ECSPI2 チップセレクト: ECSPI2 SS0 CSに使用されるGPIO: GPIO5_IO13 SPIデバイス: spi1.0 SPI速度: 1MHz SPIモード:モード0 デバイスツリー構成は現在以下を使用しています。   &ecspi2 { pinctrl-0 = <&pinctrl_ecspi2 &pinctrl_ecspi2_cs>; cs-gpios = <&gpio5 13 GPIO_ACTIVE_LOW>; status = "okay"; stmvl53l8cx: spi@0 { reg = <0>; compatible = "st,stmvl53l8cx"; spi-max-frequency = <1000000>; }; }; meta-vl53l8cx_8mp/ ├── conf/ │ └── layer.conf ├── レシピズカーネル/ │ ├── Linux/ │ │ ├── ファイル/ │ │ │ └― 0001-add-vl53l8cx-spi-node.patch │ │ └── Linux-imx_%.bbappend │ │ │ └── VL53L8CX/ │ ├── ファイル/ │ │ ├── メイクファイル │ │ └── driver.c │ └── vl53l8cx.bb SPIデバイスが正常に作成されました。   root@imx8mp-lpddr4-evk:~# ls -l /sys/bus/spi/devices/ spi0.0 spi1.0   カスタムドライバーは以下も登録されています:   root@imx8mp-lpddr4-evk:~# ls -l /sys/bus/spi/drivers/ stmvl53l8cx   ドライバープローブ()関数は正常に呼び出されています。 i.MX8MP EVK ECSPI2/J21ハードウェアとデバイスツリーの設定で、VL53L8CXがSPI上で正しく通信していることを確認するために何を検証すべきか、どなたかアドバイスをいただけませんか? 特に、以下の点を確認したいと思います。 ECSPI2 / spi1.0はi.MX8MP LPDDR4 EVKのJ21拡張コネクターで正しいSPIコントローラー/デバイスでしょうか? GPIO5_IO13 / ECSPI2_SS0はJ21の正しいチップセレクトですか? このコネクタにおけるECSPI2のSCK、MOSI、MISO、およびCSピン多重化設定は正しいですか? VL53L8CXには、以下のような追加のデバイスツリー構成が必要ですか? spi-cpol spi-cpha GPIO1/割り込み LPn/リセット/電源GPIO 電源/レギュレータの特性? VL53L8CXは、デバイスIDを読み取る前に、特定のSPIモード、タイミング、または初期化シーケンスを必要としますか? i.MX8MP ECSPIコントローラーでVL53L8CX向けに設定しなければならないことはありますか? spi_write()とspi_read()が0を返すため、 実際のMOSI/MISO電気通信 (例えばロジックアナライザーなど)を検証し、センサーが応答しているかどうかを判断する推奨方法はありますか? また、参考用に カスタムのdriver.cドライバーとカーネルログ も添付しています。 i.MX8MP EVK + J21 + ECSPI2 + VL53L8CX の正しいSPI構成に関するご助言をいただければ幸いです。 カスタムドライバーファイルを添付しました driver.c また、ログも添付しています よろしくお願いします。 Re: Enable SPI Communication for VL53L8CX ToF Sensor on i.MX8MP EVK こんにちは、 @Manuel_Salas さん ご返信ありがとうございます。 さらなる設定作業を進める前に、デバイスIDの読み取りを試みました。しかし、デバイスIDを正常に読み取ることができませんでした。 SPIドライバーは正しくプローブしていますが、チップIDのレジスタ読み取りは期待値を返しません。そのため、VL53L8CXとの通信を確認できず、センサの初期化を進めることができません。 現在、問題の原因を特定するために、SPI構成、デバイスツリー、およびハードウェア接続を確認しています。 また 、ドライバ、ログ、モジュールイメージも添付 しますので、ご覧いただけます。VL53L8CXとの基本的なSPI通信に関して、他に確認すべき点があれば、ぜひご教示いただければ幸いです。 よろしくお願いします、 ヨギ96 Re: Enable SPI Communication for VL53L8CX ToF Sensor on i.MX8MP EVK こんにちは、@yogi96さん お元気でお過ごしのことと思います。 概して、あなたの手順はすべて問題ないようです。 次に試してみるのは、例えばプローブ()関数でチップのIDを読み取るなど、センサのレジスタを読み取ることです。 IDが正しく読み取れた場合は、設定処理を続行します。 また、ドライバが取り付けられているのも見えませんでした。 可能であれば添付してください。 よろしくお願いいたします。 サラス。 Re: Enable SPI Communication for VL53L8CX ToF Sensor on i.MX8MP EVK こんにちは、 以下の方法で試してみましたか? https://www.st.com/en/embedded-software/stsw-img042.html よろしくお願いいたします。 サラス。 Re: Enable SPI Communication for VL53L8CX ToF Sensor on i.MX8MP EVK こんにちは、ありがとうございます@Manuel_Salas ご提案のライブラリは試しましたが、その前に簡単なCプログラム「ユーザー空間ハードウェアドライバ」でデバイスIDを読み取ろうとしたとき、読み取るたびにデバイスIDとリビジョンIDが異なってしまいました。 ログ: 1. root@imx8mp-lpddr4-evk:~# ./read_device_info ================================================== VL53L8CX SPIハードウェア初期発見テスト i.MX8MP EVK Linux Target ================================================== [情報]SPIデバイスマッピング:/dev/spidev1.0 [INFO] アクティブなSPIモード: 3 [情報] 送信ビット/ワード: 8 [情報] 動作速度:50000 Hz [書き込み] レジスタ=0x7FFF 値=0x00 [読み取り] REG=0x0000 TX=40 00 00 00 RX=65 3A 12 C0 [読み取り] REG=0x0001 TX=40 01 00 00 RX=50 15 19 01 [書き込み] レジスタ=0x7FFF 値=0x02 ================================================== 検出レポート ================================================== 解析されたデバイスID:0xC0(期待値:0xF0) 解析されたリビジョンID:0x01(期待値:0x0C ) -------------------------------------------------- 2. root@imx8mp-LPDDR4-EVK:~# ./read_device_info ================================================== VL53L8CX SPIハードウェア初期発見テスト i.MX8MP EVK Linux Target ================================================== [情報]SPIデバイスマッピング:/dev/spidev1.0 [INFO] アクティブなSPIモード: 3 [情報] 送信ビット/ワード: 8 [情報] 動作速度:50000 Hz [書き込み] レジスタ=0x7FFF 値=0x00 [読み取り] REG=0x0000 TX=40 00 00 00 RX=63 C4 02 82 [読み取り] REG=0x0001 TX=40 01 00 00 RX=48 01 25 10 [書き込み] レジスタ=0x7FFF 値=0x02 ================================================== 検出レポート ================================================== 解析されたデバイスID:0x82(期待値:0xF0) 解析されたリビジョンID:0x10(期待値:0x0C) --------------------------------------------------
View full article
如何上传数据库文件到共享内存 您好,我目前正在使用S32G VNP RDB2板,我的客户要求我将他的一个数据库文件放到共享内存中,请问是否可以将数据库文件上传到共享内存中? 任何指导我都非常感激。 Re: How to upload Database file to share memory 嗨@Poji9900 S32G平台内不提供任何数据库部署相关的文档或指南。我们可能无法针对此特定情况提供技术支持,建议您就数据库部署事宜联系相关技术支持团队。由此给您带来的不便,我们深表歉意。 此致敬礼,米格尔
View full article