S32DS Extensions and Updates fails to install PEmicro plugin (v6.2.3.202608261238) — ZLIB input stre Hi NXP Support, I am trying to install packages via S32DS Extensions and Updates in S32 Design Studio, but the installation consistently fails during the Collect phase due to a corrupted PEmicro plugin artifact. Error message: An error occurred while collecting items to be installed session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=). Problems downloading artifact: osgi.bundle,com.pemicro.debug.gdbjtag.pne,6.2.3.202608261238. Unexpected end of ZLIB input stream What I have tried: Searched the local p2 cache (C:\Users\ \.p2\, S32DS eclipse/p2/, and system Temp folder) — the artifact com.pemicro.debug.gdbjtag.pne_6.2.3.202608261238.jar does not exist locally (not even a 0-byte stub), so it is not a stale cache issue. Retried the installation multiple times over different days — the same error occurs every time on the exact same artifact. Try to install on three computers, and they all encounter the same problem. PEmicro appears to be a hard dependency of the packages I need (e.g., S32K3xx development package, S32 Design Studio Debugger Core), so I cannot deselect it in the installation wizard. My environment: S32DS Version: [S32DS.3.5] Build id: 240924 (Update 14) OS: Windows 10 Installation path: D:\NXP\S32DS.3.5\ (no spaces or non-ASCII characters) Request: Could you please: Verify if the artifact com.pemicro.debug.gdbjtag.pne_6.2.3.202608261238.jar on the NXP/PEmicro update server is corrupted? Provide a download link for a previous/stable build of the PEmicro GDB plugin (e.g., 6.2.3 with an earlier timestamp, or 6.2.2) so I can install it offline and bypass the broken artifact? Thank you for your help. Best regards, Yuanbin Jing Re: S32DS Extensions and Updates fails to install PEmicro plugin (v6.2.3.202608261238) — ZLIB input Hi @yuanbin
Try changing the URL under Available S32DS Software Sites from http to https:
VaneB_0-1787934025894.pngVaneB_0-1787934025894.pngVaneB_0-1787934025894.png
Also, this issue may be related to network or proxy restrictions that could be interrupting the download of the required artifacts. Please verify with your IT department whether any firewall, proxy, VPN, or security policies could be affecting access to the S32DS update repositories.
BR, VaneB Re: S32DS Extensions and Updates fails to install PEmicro plugin (v6.2.3.202608261238) — ZLIB input Hi @yuanbin
I am afraid I was not able to reproduce the issue on my side. I successfully updated the PEmicro drivers to version 6.2.3 in my S32DS 3.5 installation without any problems. Based on this, the behavior you are seeing may be related to your setup rather than the plugin itself.
However, since the PEmicro plugin is proprietary software, I am unable to verify its internal integrity or perform a deeper investigation into the plugin components.
I would recommend contacting PEmicro Support directly, as they can provide guidance specific to their software.
Sorry for the inconvenience. Re: S32DS Extensions and Updates fails to install PEmicro plugin (v6.2.3.202608261238) — ZLIB input Hi @VaneB, Thank you for your suggestions. I have already tried changing the URL from http to https in the Available Software Sites settings, but unfortunately the same `Unexpected end of ZLIB input stream` error still occurs on the exact same artifact: osgi.bundle,com.pemicro.debug.gdbjtag.pne,6.2.3.202608261238 Regarding the network/proxy possibility — I have confirmed that: - My machine has no proxy configured - I can successfully install/update other S32DS plugins without any issues - Only the PEmicro plugin fails consistently, every time Since the failing artifact has a very recent build timestamp (20260826), I suspect the file on the update server itself may be corrupted or incomplete. The error happens during the Collect phase, and the artifact does not appear in my local p2 cache at all, which suggests the download stream is being truncated at the source. Could you please: 1. Verify the integrity of `com.pemicro.debug.gdbjtag.pne_6.2.3.202608261238.jar` on the NXP/PEmicro update repository? 2. Alternatively, provide a direct download link to a previous stable build (e.g., 6.2.2 or an earlier 6.2.3 build) so I can install it offline via `Help → Install New Software → Archive`? Thank you again for your help. Best regards, yuanbin
View full article