Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
RTOSプロジェクトにおけるMCALレイヤーでのUART DMAの例 こんにちは、RTOSでDMAを使ってUART通信を実装しようとしています。MCALレイヤーでUARTとDMAを設定できるように、例のプロジェクトを教えてもらえますか? Re: Example for UART DMA in MCAL layer for RTOS Project こんにちは、@ santhu1421 これは以前RTD 6.0.0をベースに、S32K344 MCUを使ってテストしたデモです。この例を参照できます。 Re: Example for UART DMA in MCAL layer for RTOS Project 私はS32K312を使用しています Re: Example for UART DMA in MCAL layer for RTOS Project こんにちは、@ santhu1421 使っているMCUのパーツ番号を教えていただけますか?
View full article
MRF13750H AWR Installation Hello, I need help on how to correctly install the MRF13750H-915MHz model in AWR. Best, Luis
View full article
MRF13750H AWRの設置 こんにちは、 AWRにMRF13750H-915MHzモデルを正しくインストールする方法について助けが必要です。 最高、 ルイス
View full article
Example for UART DMA in MCAL layer for RTOS Project Hello ,  I am trying to impliment UART communication using DMA in RTOS, can you give me example project so that i can configure UART and DMA in MCAL layer Re: Example for UART DMA in MCAL layer for RTOS Project Hi@santhu1421 This is a demo I tested before, based on RTD 6.0.0, using the S32K344 MCU. You can refer to this example. Re: Example for UART DMA in MCAL layer for RTOS Project I am using S32K312 Re: Example for UART DMA in MCAL layer for RTOS Project Hi@santhu1421 Could you please tell the MCU part number you're using?
View full article
RTOS 项目中 MCAL 层 UART DMA 的示例 您好,我正在尝试在RTOS中使用DMA实现UART通信,能否提供一个示例项目,以便我可以在MCAL层配置UART和DMA? Re: Example for UART DMA in MCAL layer for RTOS Project 你好@ santhu1421 这是我之前测试过的一个演示程序,基于 RTD 6.0.0,使用 S32K344 MCU。您可以参考这个例子。 Re: Example for UART DMA in MCAL layer for RTOS Project 我正在使用S32K312 Re: Example for UART DMA in MCAL layer for RTOS Project 你好@ santhu1421 请问您使用的MCU型号是什么?
View full article
i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets Hello NXP Support, we are investigating a reproducible graphics issue on an i.MX8MP platform. Working configuration Yocto Scarthgap Kernel: 6.6.52 Vivante stack: 6.4.11.p2.x Weston 14.0.2.imx Qt 6.8.3 Result: Qt Quick works QOpenGLWindow works No crashes Failing configuration Yocto Wrynose Kernel: 6.18.20 Vivante stack: 6.4.11.p4.4 and 6.4.11.p4.6 Weston 14.0.2.imx Qt 6.8.3 and 6.8.4 Result: QQuickWindow crashes QOpenGLWindow crashes Weston crashes with SIGSEGV We also observed memory corruption symptoms: malloc(): unaligned tcache chunk detected and occasional crashes of unrelated processes after the graphics failure. Qt is probably not the root cause Initially the issue looked like a Qt Quick problem. However, we reduced the test case to a minimal: QOpenGLWindow   without QML, Scene Graph, QRhi, textures, or custom rendering. The failure still occurs. Native EGL tests A simple native Wayland/EGL/GLES3 application is stable: wl_egl_window eglCreateContext glClear eglSwapBuffers   even when resizing up to:   1920x1080   for hours. Additional native EGL tests We created a native Wayland/EGL/GLES3 test using: texture allocation FBO creation render-to-texture glFramebufferTexture2D() glBlitFramebuffer() eglSwapBuffers() The following sizes pass successfully: 500x500 640x480 800x480 900x540 1024x600   The issue starts appearing with larger render targets such as:   1280x720 1280x800   Weston behavior After launching the OpenGL application, Weston crashes: weston.service: Main process exited status=11/SEGV   The Qt application then reports:   The Wayland connection broke. Did the Wayland compositor die?   indicating that Weston crashes first. Vivante userspace differences The following libraries differ between the working and failing systems: libGAL.so libEGL.so libGLESv2.so   The issue is reproducible with both:   6.4.11.p4.4 6.4.11.p4.6   while the older: 6.4.11.p2.x   works on the 6.6 kernel. Questions Are there any known issues in Vivante 6.4.11.p4.x related to: Weston Wayland-EGL FBOs glBlitFramebuffer() large render targets Are there known regressions between p2.x and p4.x? Are there recommended debug options for: galcore libGAL libgbm_viv Weston buffer import paths Any guidance would be greatly appreciated. I attached a simple test app that can reproduce the crash on Kernel 6.18.20 with Vivante stack: 6.4.11.p4.4 and 6.4.11.p4.6 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets I did further investigations. Kernel 6.6.52 with Vivante p6.4.11.p4.4 -> works Kernel 6.18.20 with Vivante p6.4.11.p4.4 -> crashes The findings have now clearly worsened: A direct resize from 500x500 to 1024x600 is already enough to cause a crash. The crash occurs in the OpenGL path, immediately after a swapchain size change. At the same time, the systemd-journal SEGV occurs again. This is a strong indication of memory corruption in the GL/Wayland/Vivante stack, not just an app error. Current Status of the Hypothesis It's not just 1280x720 that's critical. Rather, the decisive factor is the direct "Reconfigure" jump followed by "Present." Sequential, smaller resizes are significantly more robust than a direct jump. The software backend remains stable, confirming that the problem lies in the hardware-GL path. Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets Hello, A Vivante/galcore or buffer-management issue than a Qt problem, especially since the native EGL test also triggers it and Weston is the first process to crash. The fact that it starts with larger render targets and only happens with the p4.x stack is particularly interesting. I’d compare the p2 and p4 GAL/GBM changes and enable galcore/Weston debugging around buffer allocation and import. Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets The main issue was the gpu reserved memory. The SOM I use has only 2GB DDR. So I had to adjust the gpu reserved memory area. I add this to my device tree: &gpu_reserved { reg = <0 0x95000000 0 0x10000000>; }; And now everything works well.
View full article
i.MX8MP - 使用 Qt OpenGL / 大型 EGL 渲染目标时,Vivante 6.4.11.p4.x 导致 Weston 崩溃 您好,NXP技术支持, 我们正在调查 i.MX8MP 平台上的一个可重现的图形问题。 工作配置 约克托·斯卡斯盖普 内核版本:6.6.52 Vivante 堆栈:6.4.11.p2.x Weston 14.0.2.imx Qt 6.8.3 结果: Qt Quick 工作 QOpenGLWindow 工作正常 没有崩溃。 配置失败 约克托·沃诺斯 内核版本:6.18.20 Vivante 堆栈:6.4.11.p4.4 和 6.4.11.p4.6 Weston 14.0.2.imx Qt 6.8.3 和 6.8.4 结果: QQuickWindow崩溃 QOpenGLWindow崩溃 韦斯顿发生 SIGSEGV 故障 我们还观察到了内存损坏的症状: malloc(): unaligned tcache chunk detected 图形故障后,偶尔还会出现无关进程的崩溃。 Qt 可能不是根本原因 最初,这个问题看起来像是 Qt Quick 的问题。 但是,我们将测试用例简化到了最小: QOpenGLWindow   不使用 QML、场景图、QRhi、纹理或自定义渲染。 故障依然发生。 原生 EGL 测试 一个简单的原生 Wayland/EGL/GLES3 应用程序运行稳定: wl_egl_window eglCreateContext glClear eglSwapBuffers   即使调整到最大尺寸:   1920x1080   持续了几个小时。 其他原生 EGL 测试 我们使用以下方法创建了一个原生 Wayland/EGL/GLES3 测试: 纹理分配 FBO创建 渲染到纹理 glFramebufferTexture2D() glBlitFramebuffer() eglSwapBuffers() 以下尺寸通过了验证: 500x500 640x480 800x480 900x540 1024x600   当渲染目标较大时,例如:就会出现这个问题。   1280x720 1280x800   韦斯顿行为 启动 OpenGL 应用程序后,Weston 崩溃了: weston.service: Main process exited status=11/SEGV   然后,Qt应用程序会报告:   The Wayland connection broke. Did the Wayland compositor die?   这表明韦斯顿首先撞车。 Vivante 用户空间差异 以下库在正常运行的系统中与出现故障的系统中有所不同: libGAL.so libEGL.so libGLESv2.so   两种方法均可重现此问题:   6.4.11.p4.4 6.4.11.p4.6   而年长的: 6.4.11.p2.x   适用于 6.6 内核。 问题 Vivante 6.4.11.p4.x 版本是否存在与以下方面相关的已知问题: Weston 韦兰-EGL FBO glBlitFramebuffer() 大型渲染目标 p2.x 和 p4.x 之间是否存在已知的回归关系? 是否有推荐的调试选项? 银河核 libGAL libgbm_viv Weston 缓冲区导入路径 任何指导都将不胜感激。 我附上了一个简单的测试应用程序,它可以在内核 6.18.20 和 Vivante 堆栈 6.4.11.p4.4 和 6.4.11.p4.6 上重现崩溃问题。 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets 我进行了进一步调查。 内核 6.6.52 与 Vivante p6.4.11.p4.4 -> 运行正常 内核 6.18.20 与 Vivante p6.4.11.p4.4 -> 崩溃 研究结果显然已经恶化: 直接将图像尺寸从 500x500 调整到 1024x600 就足以导致崩溃。 崩溃发生在 OpenGL 路径中,紧接着交换链大小的变化。 与此同时,systemd-journal 再次发生 SEGV 错误。 这强烈表明 GL/Wayland/Vivante 堆栈中存在内存损坏,而不仅仅是应用程序错误。 该假设的现状 关键的不仅仅是 1280x720 分辨率。 相反,决定性因素是直接跳转到“重新配置”并接着跳转到“呈现”。 顺序的、较小的尺寸调整比直接跳跃要稳健得多。 软件后端保持稳定,证实问题出在硬件-GL路径上。 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets 你好, 与其说是 Qt 问题,不如说是 Vivante/galcore 或缓冲区管理问题,尤其是原生 EGL 测试也会触发该问题,而且 Weston 是第一个崩溃的进程。它从较大的渲染目标开始,并且只在 p4.x 堆栈中发生,这一点尤其有趣。我会比较 p2 和 p4 GAL/GBM 的变化,并启用 galcore/Weston 调试缓冲区分配和导入功能。 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets 主要问题是GPU预留内存。我使用的SOM只有2GB DDR内存。所以我不得不调整GPU预留内存区域。 我将此添加到我的设备树中: &gpu_reserved { reg = <0 0x95000000 0 0x10000000>; }; 现在一切运转良好。
View full article
MRF13750H AWR 安装 你好, 我需要帮助,了解如何在 AWR 中正确安装 MRF13750H-915MHz 型号。 最好的, 路易斯
View full article
MX95 M7 功能安全功能 您好,关于 i.MX95 的功能安全,我注意到有一份安全手册,但需要签署保密协议。请问这份文件包含哪些内容?我该如何签署保密协议? 此外,i.MX95 M7 内核是否支持功能安全软件框架 (SAF)?据我所知,S32 系列具备此功能。我想确认一下 i.MX95 是否也支持此功能。 关于 SAF 框架,我的理解是它为用户提供 API 来监测当前的 SoC 健康状态(例如内存 ECC、CPU 电压或无响应的 GPIO 等)。 我的理解正确吗?如有任何误解,请您澄清。 Re: MX95 M7 safety functional @yipingwang谢谢你提供的信息。 Re: MX95 M7 safety functional 1.i.MX95 功能安全手册确实是一份受保密协议保护的文件。 您可以从https://www.nxp.com/webapp-signup/ndaReqForm签署新的保密协议。 保密协议签署后,即可与您分享该文件。安全手册通常涵盖安全架构、安全机制、故障模式分析以及获得功能安全认证(例如 IEC 61508 / ISO 26262)的指导等主题。 2. 是的。i.MX95 功能安全解决方案包含 SAF,Cortex-M7 安全执行环境旨在运行使用 SAF 服务的安全应用程序。Cortex-M33 作为运行 SysMgr 和 SAF 基础架构的主要安全处理器,而 Cortex-M7 作为执行安全应用程序和可选 SAF 服务的辅助安全处理器。 3. 您的描述基本正确——SAF 提供 API 来监测 SoC 健康状况,包括内存 ECC 监测、电压监测和 GPIO 诊断等功能。SAF 是一个功能安全中间件/框架,位于应用程序和 SoC 的底层功能安全机制之间。它有助于收集诊断结果、管理故障事件、执行功能安全检查,并在检测到故障时协调系统反应。 Re: MX95 M7 safety functional 请问有人能帮忙吗?
View full article
MX95 M7 セーフティ機能 こんにちは、i.MX95の機能安全についてですが、安全マニュアルがあるのにNDA(秘密保持契約)が必要です。この文書の内容が何か知ってもらえますか?秘密保持契約書(NDA)に署名するにはどうすればよいですか? さらに、i.MX95 M7コアはセーフティソフトウェアフレームワーク(SAF)をサポートしていますか?私の知る限りでは、この機能はS32シリーズで利用可能です。i.MX95でもサポートされているかどうか確認したいです。 SAFフレームワークについてですが、私の理解では、ユーザーが現在のSoCの健康状態(メモリECC、CPU電圧、応答しないGPIOなど)を監視するためのAPIを提供しています。など。 私の理解は正しいでしょうか?誤解があるようでしたら、ご指摘いただけますでしょうか。 Re: MX95 M7 safety functional @yipingwang情報ありがとうございます。 Re: MX95 M7 safety functional 1.i.MX95セーフティマニュアルは確かにNDA保護された文書です。 新しいNDAを歌うこともできます https://www.nxp.com/webapp-signup/ndaReqForm NDAが成立すれば、その文書はあなたに共有できます。安全マニュアルは通常、安全アーキテクチャ、安全機構、故障モード解析、機能安全認証取得のための指針(例:IEC 61508 / ISO 26262)などのトピックを扱っています。 2. はい。i.MX95機能安全ソリューションにはSAFが含まれており、Cortex-M7安全実行環境はSAFサービスを用いた安全アプリケーションを実行するために設計されています。Cortex-M33はSysMgrおよびSAFインフラストラクチャを動かす主要な安全プロセッサとして機能し、Cortex-M7は安全アプリケーションおよびオプションのSAFサービスを実行する補助安全プロセッサとして機能します。 3. あなたの説明は概ね正しいです。SAFは、メモリECC監視、電圧監視、GPIO診断などの機能を含む、SoCの状態を監視するためのAPIを提供します。SAFは、アプリケーションとSoCの基盤となるセーフティメカニズムの間に位置するセーフティミドルウェア/フレームワークです。診断結果の収集、故障イベント情報管理、セーフティチェックの実施、故障検出時のシステムの対応調整を行います。 Re: MX95 M7 safety functional どなたか助けていただけますか?
View full article
i.MX8MP - Qt OpenGL / 大規模EGLレンダーターゲットを使用すると、Vivante 6.4.11.p4.xでWestonがクラッシュする こんにちは、NXPサポートの皆さん、 私たちはi.MX8MPプラットフォーム上の再現可能なグラフィックス問題を調査しています。 動作構成 ヨクト・スカースギャップ カーネル: 6.6.52 Vivanteスタック: 6.4.11.p2.x Weston 14.0.2.imx Qt 6.8.3 結果: Qt Quickは QOpenGLWindowは動作します クラッシュなし 設定エラー ヨクト・ライノーズ カーネル: 6.18.20 Vivanteスタック:6.4.11.p4.4および6.4.11.p4.6 Weston 14.0.2.imx Qt 6.8.3 および 6.8.4 結果: QQuickWindowがクラッシュする QOpenGLWindowがクラッシュする ウェストンがSIGSEGVと衝突 また、メモリ破損の症状も確認されました。 malloc(): unaligned tcache chunk detected グラフィック障害発生後には、無関係なプロセスが時折クラッシュする。 Qtはおそらく根本原因ではない 当初、この問題はQt Quickの問題のように見えた。 しかし、テストケースは最小限に絞りました: QOpenGLWindow   QML、シーングラフ、QRhi、テクスチャ、カスタムレンダリングは使用しません。 故障は依然として発生する。 ネイティブEGLテスト シンプルなネイティブのWayland/EGL/GLES3アプリケーションは安定しています: wl_egl_window eglCreateContext glClear eglSwapBuffers   最大サイズまでリサイズした場合でも:   1920x1080   何時間も。 追加のネイティブEGLテスト 私たちは以下の方法でネイティブのWayland/EGL/GLES3テストを作成しました。 テクスチャ割り当て FBOの作成 テクスチャへのレンダリング glFramebufferTexture2D() glBlitFramebuffer() eglSwapBuffers() 以下のサイズは正常に通過します。 500x500 640x480 800x480 900x540 1024x600   この問題は、以下のようなより大きなレンダリングターゲットで発生し始めます。   1280x720 1280x800   ウェストンの行動 OpenGLアプリケーションを起動した後、Westonはクラッシュします: weston.service: Main process exited status=11/SEGV   Qtアプリケーションは次のように報告します:   The Wayland connection broke. Did the Wayland compositor die?   これは、ウェストンが最初に衝突したことを示唆している。 Vivanteのユーザースペースの違い 正常に動作するシステムと故障しているシステムで異なるライブラリは以下のとおりです。 libGAL.so libEGL.so libGLESv2.so   この問題はどちらの環境でも再現可能です。   6.4.11.p4.4 6.4.11.p4.6   一方、年配の方は: 6.4.11.p2.x   6.6カーネルで動作します。 質問 Vivante 6.4.11.p4.x には、以下の点に関する既知の問題はありますか? Weston ウェイランド-EGL FBO(固定基地運営事業者) glBlitFramebuffer() 大きなレンダリングターゲット p2.xとp4.xの間には既知の回帰関係はありますか? 以下の項目について、推奨されるデバッグオプションはありますか? ガルコア libGAL libgbm_viv Westonバッファのインポートパス 何かご助言いただければ大変ありがたいです。 Vivanteスタックを使ったカーネル6.18.20でクラッシュを再現できる簡単なテストアプリ(6.4.11.p4.4と6.4.11.p4.6)を添付しました Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets 私はさらに調査を進めた。 カーネル6.6.52とVivante p6.4.11.p4.4の組み合わせは動作します。 カーネル6.18.20とVivante p6.4.11.p4.4の組み合わせでクラッシュする 調査結果は明らかに悪化している。 500x500から1024x600への直接的なサイズ変更だけでも、クラッシュを引き起こすのに十分だ。 クラッシュはOpenGLの処理パス内で、スワップチェーンのサイズ変更直後に発生します。 同時に、systemd-journalのSEGVが再び発生します。 これは単なるアプリのエラーではなく、GL/Wayland/Vivanteスタックにおけるメモリ破損の強い兆候です。 仮説の現状 重要なのは1280x720という解像度だけではない。 むしろ、決定的な要因は「再構成」に直接ジャンプし、その後に「提示」を実行することである。 連続的に小さなサイズ変更を行う方が、直接的なサイズ変更よりもはるかに堅牢です。 ソフトウェアバックエンドは安定しており、問題はハードウェア-GL経路にあることが確認されています。 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets こんにちは、 Qtの問題よりもVivante/galcoreやバッファ管理の問題です。特にネイティブEGLテストもトリガーし、Westonが最初にクラッシュするプロセスなので。レンダリングターゲットが大きい場合に発生し、p4.xスタックでのみ発生するという事実は、特に興味深い。p2とp4のGAL/GBMの変更点を比較し、バッファの割り当てとインポートに関するgalcore/Westonのデバッグを有効にします。 Re: i.MX8MP - Weston crash with Vivante 6.4.11.p4.x when using Qt OpenGL / large EGL render targets 主な問題はGPUのリザーブメモリでした。私が使用しているSOMには、2GBのDDRメモリしか搭載されていません。そこでGPUの予約メモリエリアを調整しなければなりませんでした。 これをデバイスツリーに追加します。 &gpu_reserved { reg = <0 0x95000000 0 0x10000000>; }; そして今はすべて順調に機能しています。
View full article
S32G399A IIC構成 こんにちは、 S32G399のI2C4モジュールを使用して外部PMICを設定する予定です。このI2C4モジュールは、Aコアを介して低レベル(クロック周波数、プルアップ/プルダウン抵抗、アドレスなど)で設定できるかどうか教えていただけますでしょうか?現時点ではMコアは使用しません。そのため、S32Gの低レベルI/O設定にはAコアを使用したいと考えています。 MichaelTao_0-1788251860175.pngMichaelTao_0-1788251860175.png Re: S32G399A IIC 配置 こんにちは、 @MichaelTao はい、可能です。AコアはI2C4モジュールで構成できます。 BR チェイン Re: S32G399A IIC 配置 I2Cの低レベルドライバー設定にはS32 Design Studioを試してみるのも良いでしょう
View full article
IPCF_Example_S32R47_to_A53_M7_0 ビルドエラー IPCF_Example_S32R47_to_A53_M7_0 SDKからエクスポートされたデフォルトのプログラムはビルドに失敗し、コンパイルエラーが発生します。 初期トラブルシューティングの結果、問題はタイミング構成に起因しており、3つのクロック出力設定が有効範囲を超えていることが分かりました(スクリーンショット参照)。理論上は起こらないはずなのに、なぜこのエラーがまだ存在しているのか、説明していただけますか?この件の確認にご協力ください。ありがとう! wxh1_1-1788255373531.png S32 SDK for S32K1 Re: IPCF_Example_S32R47_to_A53_M7_0 build error こんにちは、 S32R47製品については、割り当てられたNXPの直接サポートまでお問い合わせください。 petervlna_0-1788264837185.png 根本的な原因としては、S32CTのバージョンミスが考えられます。 よろしくお願いいたします。 ピーター
View full article
[Lin Master] [linstack_config]middleware - BaudRate=10417 bps LIN Bus客戶 要求 baud rate = 10417 bps ,  使用 LDF Explorer 亦支援 10417 baud rate :  CY9_0-1788234587344.png 但是,回到 S32DS , LPUART2 並不支援 該 baudrate  :  CY9_1-1788234668862.png 現在 設備無法溝通, 不確定 是否是 LPUART baud rate 設定造成 !?  有人 能協助確認 嗎?  感謝  S32K144 EVB + S32DSv3.5+RTM401  S32DS-S32PLATFORM  S32SDK-ARMK1 #LIN_BUS   #LIN_Master  #Lin_Master  S32 SDK for S32K1 Re: [Lin Master] [linstack_config]middleware - BaudRate=10417 bps 您可以考虑升级到RTD 3.0.0版本。LIN波特率更加灵活,详见下文。 请注意,您使用的旧版 SDK 4.0.1 已不再受支持,不建议在新设计中使用。 danielmartynek_0-1788261761281.png 此致, 丹尼尔 Re: [Lin Master] [linstack_config]middleware - BaudRate=10417 bps 但我的客户要求使用奇怪的波特率…… [LDF Explorer] 也支持这种奇怪的波特率…… 我认为这种情况可以接受,并且已经向客户承诺会处理好这件事。 那我现在该怎么办? 有什么意见吗? 感谢大家的评论……或者八卦。 Re: [Lin Master] [linstack_config]middleware - BaudRate=10417 bps 你好@CY9 , 遗憾的是,该驱动程序仅支持这些固定的波特率: danielmartynek_0-1788252200254.png 此致, 丹尼尔
View full article
双向交流/直流 + 双向隔离直流/直流系统解决方案/参考设计 Hello 我们正在评估一个双向数字电源系统,想知道是否有适用于这种设置的参考设计或恩智浦解决方案: 系统概念: 双向交流/直流放大器 采用无桥图腾柱的PFC拓扑结构 双向运行(并网逆变器模式和PFC模式) 双向隔离式 DC/DC 级 双有源桥(DAB)拓扑结构 采用数字控制的双向功率流 该系统专为储能系统、双向功率变流器或类似的工业功率平台等应用而设计,目标功率级在千瓦级。 能否请您推荐一个参考设计或解决方案? 我们将从 4 串电池组(标称电压 12.8V)的 1.2kW 逆变器开始。 Re: Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system 图腾柱并非硬性要求,我对拓扑结构比较灵活。我接受这个参考编号:双向交流直流参考设计 您能否也对 DC-DC 级提出一些建议,即使 DAB 不是硬性要求。所以,如果您能推荐一些关于DC-DC电路的参考资料,那就太好了。 Re: Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system 你好,Sahil, 恩智浦半导体针对交流/直流前端设计了两款相关的参考设计: 800W 双向 AC-DC 转换解决方案 (BIDIRECTIONAL-AC-DC-REF-DESIGN) — 一款经过全面验证的双向 AC/DC 变流器,由 MC56F83783 DSC 控制。它支持交流转直流(PFC 模式)和直流转交流(并网逆变器模式)两种操作,模式转换平滑。主要规格:800W @ 220Vac,宽输入范围 85–265Vac,380V 直流母线,峰值效率 >97% @ 220Vac,功率因数 >0.99。文档:UG10208,AN14354。请注意,此设计采用全桥拓扑结构和 LCL 滤波器,而不是图腾柱;它是 NXP 提供的最接近的双向 AC/DC 参考设计。 图腾柱无桥 PFC 变流器 (RDPFC56F82748) — 使用 MC56F83783 / MC56F82748 DSC 实现图腾柱无桥 PFC,功率因数 > 0.99,总谐波失真 < 5%。文档:AN12618、DRM174。该特定参考设计仅在整流器(交流转直流)模式下运行,额定输出功率为 240W / 12V。它可作为图腾柱式 PFC 实现的起点,但本身并不包含双向(逆变器)控制路径。 如果在同一设计中需要图腾柱拓扑的双向操作,建议将 RDPFC56F82748 的 PFC 控制与 BIDIRECTIONAL-AC-DC-REF-DESIGN 的双向控制框架相结合。 BRs,托马斯
View full article
eIQ TSSと移植されたTFLMミドルウェアを使用してKW45B41Z-EVKにAI/MLを実装する こんにちは、NXPコミュニティの皆さん、 私は KW45B41Z-EVK (Cortex-M33)向けのエッジAIアプリケーションを開発しており 、このボード上で機械学習モデルを展開する際にアドバイスをいただきたいです。 KW45 SDKにはデフォルトでeIQ/TFLMミドルウェアが含まれていないため、私の計画は以下の通りです: モデルトレーニング:eIQ Time Series Studio(eIQ TSS)を用いて時系列データのnクラス分類モデルを訓練します。KW45はeIQ TSSのターゲットとしてリストされていないため、モデルをエクスポートするターゲットプラットフォームとしてFRDM-MCXN947(Cortex-M33)を選択しました。 ランタイムデプロイ:FRDM-MCXN947 SDKのmiddleware/eiq/tensorflow-liteフォルダを私のKW45 SDKプロジェクトにポートし、CMSIS-NNと連携させます。 私の質問: MCXN947 SDKからKW45 SDKへのeIQ TFLMミドルウェアの移植は有効でサポートされている方法でしょうか? eIQ TSSでFRDM-MCXN947を選択することは、KW45上で動作するモデルを生成するのに適していますか? KW45B41Z-EVKにAI/MLを実装するための、他に推奨されるワークフローやネイティブなワークフローはありますか? ご協力いただきありがとうございます! Kinetis Wシリーズ・マイクロコントローラ Re: Implementing AI/ML on KW45B41Z-EVK using eIQ TSS and Ported TFLM Middleware NXPサポートチームおよびコミュニティの皆様、こんにちは。 この件についてフォローアップのためご連絡いたしました。現在のプロジェクトのスケジュール上、解決策を見つけることが非常に急務となっているためです。 NXPチームのどなたか、FRDM-MCXN947 SDKからKW45 SDKへのeIQ/TFLMミドルウェアの移植が有効でサポートされている回避策かどうか、簡単な確認をいただけませんか?推奨ワークフローについて簡単なガイダンスや確認があれば、自信を持って開発を進められるよう助かります。 お時間とご協力に、前もって感謝申し上げます! KW45B41Z-EVK EIQ-ツールキットEIQ-TFLITE-MICRO #AI/ML Re: Implementing AI/ML on KW45B41Z-EVK using eIQ TSS and Ported TFLM Middleware こんにちは、 @Srushti_Mulimani さん。お元気でお過ごしでしょうか。   eIQ Time Series Studio (TSS) を使用している場合は、FRDM-MCXW71 からプロジェクトを移植することをお勧めします。eIQ TSSで公式にサポートされているターゲットであり、KW45ともソフトウェア互換性があります。両デバイスは同じCortex-M33コアアーキテクチャと似たメモリプロファイルを共有しているので、生成されるライブラリはあなたのハードウェアにかなり近いはずです。 FRDM-MCXN947のようにハードウェアプロファイルが大きく異なるデバイスをポーティング対象として使用する場合、両デバイス間の利用可能なRAMの違いや、MCXN947特有のNPU加速モデルの生成などにより互換性のないモデルを生成するリスクがあります。 お役に立てば幸いです! よろしくお願いします、 ソフィア。
View full article
Software license expired Hello: ActivationId: 04E9-8F5A-8B1F-F9C8 What procedures are required to extend the validity period of a license? ActivationId: 04E9-8F5A-8B1F-F9C8 What procedures are required to extend the license validity period? Re: 软件许可证过期 Hi, Your S32DS license has been extended. Please activate S32DS again with your old code. 
View full article
RT1172 LT8918 LCDパラレル LCDIFV2 小型層 + 背景アンダーラン 残念ながら、このLCDにはmipi出力を直接接続できないのでLT8918が追加されていますが、問題は起きていないようです。テストパターンはそのデバイス上で正常に実行され、デバッグログにも同期と基本設定の合格が示されています。 しかし、出力に問題が生じます。現在私が持っているコードは、800x1280の画面の中央にある非常にシンプルな小さなメモリバッファ(128x256)のためのものです。実際の出力画面を見る必要はないが、非常に歪んでいるように見える。また、印刷された診断情報には、DMAが1行分の書き込みに必要なデータを十分な速さで取得できていないかのように、アンダーランエラーが多数表示されます。 私はLCDやNXPレジスタの専門家ではありません。どこかで何か愚かな間違いを犯しているのだろうか?不確実な要素は山ほどある。SRAM_OC1は実際にはかなり遅いのでしょうか?タイミングを正しく調整するために、AXIまたはDMAの設定があるのかもしれません。MPUコードでキャッシュしないように設定を変更しましたが、それも間違いかもしれません。残念ながら、デフォルト領域とncache領域の違いは分かりません。他にも考慮すべき点はたくさんあります。例えば、ストライド長を、より小さい128ピクセルのレイヤー0サイズではなく、800ピクセルの行全体に変更してみました。RGBピクセルクロックはMIPIバイトクロックよりも遅いが、MIPIはRGBの24本の並列接続ではなく2本のラインを使用しているため、いずれにしてもMIPIの方がはるかに高速であると予想される。 また、レイヤー0領域をこれほど小さくしている理由は、SDRAMにエラーが発生する可能性があるからです。この不確実性を避けるために、これをより小さなコントロールされた部分に縮小していますが、ここでも何が問題なのか正確には見つけられません。 ここまで来られたのは素晴らしいことだが、これ以上進歩するために何をすればいいのか分からないのは非常に歯がゆい。背景の単色表示はすべて問題なく動作し、テストパターンはきれいな形のバーの領域を作るので、本当の"LCD"の問題ではないと思います。むしろRAMバッファの読み取りやLCDIFv2がパラレル出力に割り当てているのがタイミングの問題のように見えます。 これをどうやってデバッグすればいいですか?ありがとう。 Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun いくつか試してみたところ、少なくとも印刷された診断結果を見る限り、アンダーランエラーのない安定した出力が得られているようです。主な変更点は最初のものだと思いますが、その他の変更点は実際にはもう少し複雑です。しかし、分かりやすくするために列挙しておきます。この設定はまだRGB888のままで、アルファレイヤー描画の実験のために変更したくありません。というのも、まだそれほど良い状態ではないからです。 1. ピクセルクロックを大幅に遅くし、リフレッシュレートを15Hzに近い値にする。DMAには作業のための余分な時間があるのかもしれない?でも、おっしゃる通り、OCRAMは高速なはずです。MPUの設定で、その領域もNCACHE領域として設定しています。 2. 使用されている色は黒と白のみです。緑色の背景を試すと、緑色がRGBパターンにシフトされて毎行(1バイトずれ?)という問題が発生します。 3. RAMレイヤー0の幅を高さ256に合わせるために256に変更します。実際、128の高さでも問題ありませんが、この丸太は256で、ストライドも768に変わるのがわかります。 4. 玄関ポーチと裏庭のビデオ設定がかなり大きくなっています。これが主な原因ではないと思います。もっと速い速度でこれらの設定も試してみましたが、あまり効果はありませんでした。データシートによると、Hfp + Hbp + Hs の最大値は任意の値に設定できますが、ここで合計200を超える値を設定する理由はあるのでしょうか?縦位置設定は、合計で250に制限されています。 とにかく、面白い話です!技術的には、LCDのデータシートには最低22Hzで動作させる必要があると記載されていますが、白い部分にちらつきは見られません。もっと速く走らせたいです。 RT1172のDMAについては全く気にしていなかったのですが、動作速度を上げたり、優先度を上げたりするために何かできることはありますか?LCDIFv2には、これに関する他の設定はありますか?特にOCRAMは本来とても速いはずなのに、こんなに遅くしたのにこんな効果が出たのは驚きです。 Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun 右。本当にありがとうございました!もっと色々なことを試してみましょう。こちらが別のログです。 私はRGB888にこだわりたかったのです。ARGB8888の方がこの用途に適している理由は何かありますか?いつかアルファ版を試してみようかな。 CTRLDESCL5: 0xD8000260 リファレンスマニュアルで確認したところ、BPP設定はビット27〜24で、その「8」はRGB888にうまく入力したことを示しています。最後のバイトは無関係に見え、アルファ設定は無害にずれているように見える。 画面出力は異なって見えるが、修正されていない。もしかしたら改善されたのかも?包み込むようなデザインは健在だが、以前ほど攻撃的な印象ではない。 ピクセルクロックの速度を上げる実験もしてみましたが、効果があるのか悪いのかは分かりません。 もっと動画設定を変えてみることはできますか?25%のHsync設定はここではかなり強力だと思っていたのですが、考えてみれば、これまでこのような設定をしたことがなかったのです。どのような要素が、その場所を特に優れたものにするのでしょうか?Vsyncも関係ありますか?LT8918ブリッジもこれらの設定入力が必要ですが、それも管理できます。入力する数字は推測するしかないのでしょうか? ドライバーはJD9365DA-H3です。参考になれば。タッチスクリーンが付いているという奇妙なパッケージもありますが、私は特に問題ありません。 Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun こんにちは、 @davidpspeedtech さん。 最新情報ありがとうございます!しかし、問題は、設定の一部に一貫性がないことです。 0xD9000260 → ハードウェアにラッチされたフォーマットはARGB8888(32ビット/ピクセル)です。 したがって、stride = 384(=128×3, RGB888)を設定しても、ハードウェアは1行あたり128×4 = 512バイト/行→ずれを取り出し、バッファを越えて読み込み、アンダーランします。 毎回ストライドまたはBPPマクロのみを変更しましたが、ハードウェアは実際には .pixelFormat に従い、ARGB8888のままでした。4つの値は決して一貫していませんでした。 それらをすべて32ビットARGB8888またはRGB888として一度に統一してください。   #define SMALL_LAYER_0_BPP 4U #define SMALL_LAYER_0_STRIDE (SMALL_LAYER_0_WIDTH * 4) /* = 512 */ uint8_t smallLayer0_Buffer0[256][512]; .pixelFormat = kLCDIFV2_PixelFormatARGB8888、 .strideBytes = SMALL_LAYER_0_STRIDE, /* 512、3200ではありません */   CTRLDESCL3 は現在 0x200 (512) を読み取っているはずです。32ビットフレームバッファと24ピンRGB888出力は独立しているため、24ピンリンクに3バイトバッファは必要ありません。 また、これら3回線はeLCDIFビット定義を使用しています。LCDIFv2にはRUNビットがなく、これが制御状態を乱すことがあります。   LCDIFV2->CTRL &= ~LCDIF_CTRL_SFTRST_MASK; LCDIFV2->CTRL &= ~LCDIF_CTRL_CLKGATE_MASK; LCDIFV2->CTRL |= LCDIF_CTRL_RUN_MASK;   Gavin_Jia_0-1788249587860.pngGavin_Jia_0-1788249587860.pngGavin_Jia_0-1788249587860.png 標準APIのみを使用して操作してください。 その他の点について確認させてください。 ストライドは画面幅ではなく、RAMバッファ幅に基づいて計算されます。これは正しいです。 背景色はレジスタ生成(メモリフェッチなし)であるため安定しており、出力パスが正常であることが証明され、障害がレイヤーフェッチパスにあることが特定されます。 原色と二次色の間でカラーバッファがちらつく現象(「まるでバイトが失われたかのよう」)は、まさにアンダーランによってバイトが失われていることが原因です。フォーマットが統一されれば、この現象は解消されるはずです。 帯域幅はボトルネックではない(OCRAM、128幅)。それでもアンダーランが解消されない場合は、ピクセルクロックを下げるか、HBP/HFPを上げて確認してください。 Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun いや、それでは解決しない。実際、ストライドがRGB888の場合は128*3でも、ARGB8888の場合は800*4に設定して画面全体をRAMに収めようとしても、出力は画面の端で歪みが生じる点でかなり似ており、アンダーランエラーが発生します。ファイル内のテキストだけでなく、さまざまな設定を試してみました! #define SMALL_LAYER_0_HEIGHT 256U #define SMALL_LAYER_0_WIDTH 128U #define SMALL_LAYER_0_BPP 3U /* RGB888 */ #define SMALL_LAYER_0_STRIDE (SMALL_LAYER_0_WIDTH*SMALL_LAYER_0_BPP) /*384*/ ~デバッグ出力~ CTRLDESCL3: 0x 180 (ピッチ/ストライド = 384バイト) これもまたうまくいかない。 でも、レイヤー0のストライド設定はRAMバッファ幅に基づいて本来ならLCD画面幅ではなく、右? LT8918へのインターフェースは24ピンのパラレル接続なので、本来RGB888であるべきです。DMAか何かが処理速度に追いついていないのではないかと心配になることもありますが、これはバッファサイズが小さいためSRAM_OC1が不足している状態です。おそらくRGB565も、最上位ビットがRGBピンで正しく出力できるので、似たような出力を持つかもしれません。モノクローム作品にも挑戦してみようかな。 サンプルコードを見ると、RGB888のBPPを3ではなく4に設定している箇所があり、他にも間違いを犯している可能性があります。 「背景領域」を別のレイヤーに配置し、別のメモリにバッファリングする必要があるのでしょうか?背景設定が正しく機能し、設定した単色で出力色が安定している点が気に入っています。白色以外のRAMバッファを使った実験では、画面が原色(RGB)と二次色の間でちらつくことがあり、まるで個々のバイトが失われたかのような現象が見られる。 Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun こんにちは、 @davidpspeedtech さん。 NXP MIMXRTシリーズにご関心をお寄せいただきありがとうございます! ご提供いただいた添付ファイルを確認しましたが、一部の設定を調整する必要があるかもしれません。 CTRLDESCL3: 0x00000C80 (ピッチ/ストライド = 3200バイト) #define SMALL_LAYER_0_BPP 3U /* RGB888 */ #define SMALL_LAYER_0_STRIDE (128 * 3) /* = 384 バイト */ uint8_t smallLayer0_Buffer0[256][384]; --> CTRLDESCL3にプログラムしたピッチ(3200バイト)は実際のバッファレイアウトと一致しません。バッファはRGB888で128×256なので、各行は128×3=384バイトです。   PITCH = 3200の場合、LCDIFv2は1行あたり3200バイト進み、384バイトではなく、各行ごとに有効なデータを大きく超えて到達します。このたった一つの不一致が、ご覧になっている両方の症状を引き起こすのに十分です。各行の開始アドレスが間違っていると画像が歪んだりずれたりし、各行で約8倍もの(しかも無効な)データがフェッチされると出力FIFOが不足し、アンダーランエラーが発生します。   レイヤー記述子をバッファと整合させてください。 CTRLDESCL3 (PITCH) = 384 (0x180)、つまりSMALL_LAYER_0_STRIDE = 128 * 3。 バッファのベースアドレスは64バイト境界にアラインされます。キャッシュ不可のままにするか(現在の設定は正しいです)、表示前にDキャッシュをクリアしてください。 よろしくお願いします、 ギャビン Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun こんにちは、 @davidpspeedtech さん。 記述子は自己整合的になりました: CTRLDESCL5=0xD8000260 (BPP=8=RGB888)、CTRLDESCL3=0x300=768=256×3。おっしゃる通りです。 しかし、根本的な不一致は依然として存在しており、低いクロック周波数によって覆い隠されているだけである。「行ごとに色が変わる、まるで1バイトが失われたかのようだ」という証拠は、メモリダンプがすべて 0xFFFFFFFF であり、センターピクセルが1ピクセルを単一の32ビットワードとして読み取っていることです。つまり、ハードウェアが3バイトをフェッチしている間も、コンテンツは依然として32ビット/ピクセルです。白は各バイトに0xFFされるため隠れています。緑は1行あたりにドリフトします。 ピクセルクロックを下げるとアンダーランは解消されますが、それはOCRAMが遅いからではありません(OCRAMは高速であり、オンチップメモリがボトルネックではありません)。アンダーランは、AXIマスターとしてのLCDIFv2のフェッチスループットに依存します。リフレッシュを~13.5 Hz(18.85 MHz÷ 1000×1400)に下げ、取っ取り要求を3〜4×減らしたので止まりますが、これはパネルの最低限値より低いです。 アンダーランせずに速く走るには、以下の方法が役立つかもしれません。 エンドツーエンドに切り替えARGB8888: .pixelFormat=ARGB8888 、BPP=4、stride=256×4=1024、バッファは4バイト/ピクセルで、ピクセル書き込みコードが32ビットワードを書き込むことを確認してください。理由は2つあります。(a)既存の32ビットコンテンツと一致するため、緑色の問題を修正できます。(b)RMノートに記載されているRGB888はバス上で長さ15のバーストを発行しますが(効率が悪く、アンダーランが発生しやすい)、ARGB8888は32ビットにアラインされ、長さ16のクリーンなバーストを使用します。緑色のダンプで確認してください。行ごとにずれがなく、きれいな繰り返しになっているはずです。 LCDIFv2のb_clk(クロックのルート)を上げて、ピクセルクロックを22Hz以上に復元してください。これが速度を上げるための正しい方法であり、クロックを下げることではありません。LCDIFv2はeDMAを使用しないため、「DMA優先度の上昇」は適用されません。利用可能なレバーはb_clk、バースト長、未処理リクエスト数、そしてTHRES動的優先度閾値です。 JD9365DA-H3パネルのデータシートに記載されているタイミング値を使用し(推測しないでください)、LT8918の入力タイミングをそれに合わせてください。~200の水平ブランキングでも問題ありません。ブランキングが大きいとアンダーランが緩和されますが、htotalが上がり(より高いピクセルクロックが必要)、トレードオフとなります。ルート修正は高いb_clkです。Vsync/垂直ポーチはパネルと一致させる必要がありますが、ラインごとのアンダーランにはほとんど影響しません。 よろしくお願いします、 ギャビン Re: RT1172 LT8918 LCD parallel LCDIFV2 small layer + background underrun 私はNXP初心者なので、最初から正しく設定すべきでしたが、実際にはこの混乱の簡単な解決方法は、BUS_CLK_ROOTをデフォルトの24MHzから200MHzに上げることでした。デフォルト設定を完全に見落としていました。 その後、小さなウィンドウが綺麗に表示されるようになっただけでなく、画面全体も正常に表示され、60Hzの表示クロック(約80MHzのピクセルクロック)で動作するようになった。SDRAMの設定は当然より複雑ですが、OCRAMとSDRAMはどちらもバスクロックによって制限されていたので、それは理にかなっています。 他にもいくつか時計を調整しましたが、おそらくそれらは必要だったのでしょう。ClocksペリフェラルツールでEVKの例を見ると、これらのプロジェクトではこれらの機能が変更されていることがわかります。「clock_config.c」を見ているだけでは気づきにくい。 とにかく、本当にありがとうございました!
View full article
EMI EMC Compliance certificate and test report Hi Team, Could you please help to check and confirm that below mentioned 15W receiver kit is EMI/EMC compliant. P/N: WPR1500-HV Description - High Voltage Wireless Charging Receiver Regards, Parth Bhavsar Re: EMI EMC Compliance certificate and test report Hello @P907 , Thanks for your post. This EVK is mainly for evaluation and pass basic EMI/EMC test to be CE compliance. In general there aren't any major different between our solution and general solution on market. Hope it helps. BR Celeste Re: EMI EMC Compliance certificate and test report Hi Celeste, Thank you for the reply. Could you please help us to share the test report and its results. So, from that we will check which are the basic EMI/EMC test is performed on this EVK. Regards, Parth Bhavsar Re: EMI EMC Compliance certificate and test report Hello @P907 , Of course, I can share them with you. However, these materials are not suitable for sharing on public platforms such as the Community. I will send them to you via private email shortly. Please keep an eye on your inbox. Regards, Celeste Re: EMI EMC Compliance certificate and test report Hi Celeste, Thank you for sharing EMI/EMC test report for the requested EVM. Regards, Parth Bhavsar
View full article
Documentation for the MPC5777C-DEVB2? Hello, My team has been working successfully with the MPC5777CEVB for some years, both in S32 and GHS environments, but we had to purchase some new boards and only the -DEVB2 was available. We are not being able to find documentation on it and, while the board is working fine under S32 (and a pemicro Multilink probe), we are having trouble using it under GHS and the same V4 probe that works with the EVB. It seems we are having problems to perform the JTAG connection, as since the start we cannot read/write registers (thus, we cannot halt or reset the device). Is there any specific jumper/switch configuration that must be performed to enable JTAG debugging under GHS? We are unable to find any manual for the DEVB2, thus we do not know where to start investigating. Thanks, Ricardo Re: Documentation for the MPC5777C-DEVB2? Hello, I see there is SW18 jumper for JTAG / OpenSDA connection. petervlna_0-1788336667191.png This means SW18 determines whether those JTAG signals are connected to: An onboard/OpenSDA debugger path, or The external MCU JTAG connector. Best regards, Peter
View full article