Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt Hi, I'm using the following configuration: S32K388EVB-Q289 S32DS 3.6.8 RTD 7.0.1 I used the provided Eth_InternalLoopback_S32K388 example project as base, and modified it so that it can receive frames from my PC through a media converter. I have added in the RTD fix which was mentioned in Example S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600. I was able to hit the breakpoint in  Eth_43_GMAC_Receive(EthConf_EthCtrlConfig_EthCtrlConfig_0, 0U, &Status); And was able to inspect the Ethernet frame in EthIf_RxIndication(Eth_43_GMAC_apxInternalCfg[PartitionId]->Eth_43_GMAC_apCtrlConfig[CtrlIdx]->EthCtrlEthIfIdx, FrameType, IsBroadcast, MacSrcAddr, Payload, PayloadLength, IngressTimeTuplePtr, RxHandleId); However, when I added a while 1 loop, enabled the Rx Interrupt and linked it to the GMAC0_CH0_RX_IRQHandler I was not able to get any interrupt anywhere. I have attached my project below. James_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.png S32K3 AUTOMOTIVE-RTD  Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt Hello @James_Zhang_SE , I checked the attached project. To enable RX IRQ in RTD7.0.1, you need to change Ingress QueueHandlerFunction and enable QueueInterrupt: PavelL_0-1788263577590.pngPavelL_0-1788263577590.pngPavelL_0-1788263577590.png After that change, I hit breakpoint at GMAC_RxIRQHandler(), resp. at Eth_43_GMAC_Receive(). I also noticed that your RGMII TXCLK is defined as Input -> it should be Output. However, to see your TX frame in Wireshark, you need to change the init sequence accordingly to  Example S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600. So, in your project, it looks like: PavelL_1-1788264277735.pngPavelL_1-1788264277735.pngPavelL_1-1788264277735.png Best regards, Pavel Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt Hi Pavel, Thank you very much for your support. After applying the fixes you suggested, the GMAC driver is now working for me. I do have a few additional questions, and I would appreciate your guidance: Is there any detailed documentation that describes the complete procedure for configuring and using the GMAC driver? I would like to go through the documentation myself first so that I can better understand the driver before asking too many questions. Inside EthIf_RxIndication(), do I need to call Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId); at the end of the function to release the received buffer? There are quite a few GMAC configuration options available. Is there any documentation or reference that explains what each configuration parameter does and how it should be configured? Thank you again for your help. I really appreciate your support. Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt Hi @James_Zhang_SE , Thank you for sharing your update. I am glad to hear that the GMAC driver is now working for you. Regarding your additional questions: 1. The main reference for configuring and using the driver is the Eth_43_GMAC User Manual, which is included in the RTD installation, e.g.: C:\NXP\S32DS.3.6.6_RTD701\S32DS\software\PlatformSDK_S32K3\RTD\Eth_43_GMAC_TS_T40D34M70I1R0\doc\RTD_ETH_43_GMAC_UM.pdf I also recommend reviewing the corresponding Eth_43_GMAC Integration Manual (RTD_ETH_43_GMAC_IM.pdf), saved in the same directory, and the available GMAC example projects.   2. Whether Eth_43_GMAC_ReleaseRxBuffer() must be called depends on the EthCtrlReleaseResourceAfterReception configuration parameter. PavelL_0-1789024403441.png If automatic release after reception is enabled, the driver releases the RX resource after EthIf_RxIndication() returns and you should not release it explicitly. If automatic release is disabled, the received buffer remains allocated after EthIf_RxIndication() returns. In that case, the application must eventually call: Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId);   This mode is useful when the application needs to retain the received data for further processing. However, the buffer must be released after the application has finished using it. Otherwise, the available RX buffers will eventually be exhausted. Please also note that the received Payload pointer should not be used after the corresponding buffer has been released. 3. The Eth_43_GMAC User Manual is also the primary reference for the individual configuration parameters. In addition, S32 Configuration Tools displays a description for many parameters when the corresponding setting is selected or hovered over. For hardware-level behavior, such as MAC filtering, DMA operation, MTL queues, timestamps and interrupt status, please refer to the GMAC/EMAC chapter of the S32K3 Reference Manual. As a practical starting point, I recommend referencing GMAC examples provided by the RTD package. There are also functional lwIP examples on the page: https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-Examples/ta-p/1108990 Please do not hesitate to ask for support in case you observe any issue. A dedicated thread for each topic is preferred. It helps keep us clarity of cases for other users. Best regards, Pavel
View full article
在 IW612 上使用 BlueZ 启用 LE 音频 您好, 我有一块搭载 IW612 芯片组的 FRDM i.MX93 主板。根据芯片组数据表,它支持 LE 音频。 我有兴趣在嵌入式 Linux 镜像(目前使用的是默认的 FRDM Yocto 镜像,内核版本为 6.18-1)上运行 BlueZ 来测试 LE Audio。 在 BlueZ 端,我已经启用了实验性和内核实验性功能来使用 LE 音频,并且我看到 BlueZ 识别出了芯片组的 LE 音频功能。 但是,该功能似乎默认情况下未启用,当我与 LE Audio 耳机配对时,BAP 音频配置文件无法连接。 是否有关于如何在 BlueZ/Linux 中启用 LE Audio 的文档? 提前致谢 Re: Enable LE Audio with BlueZ on IW612 尊敬的@ammar_khallouf_95 , 感谢您的询问。 是的,我们有一份客户文件,请点击链接查看。 https://www.nxp.com/products/IW612 weidong_sun_0-1788306573110.png 文档名称是 UM12155:蓝牙低功耗音频 这是一个安全文件,如果您没有访问权限,请按照以下两个步骤申请访问。 1. 与恩智浦半导体签署保密协议。 通过 NXP 网站 www.nxp.com-->支持-->支持提交工单先购买门票,然后按照说明完成购买。 如果贵公司已与恩智浦签订保密协议,请忽略此步骤。 2. 申请文档访问权限 (1)提交新工单,告诉我们您的 NDA 编号和您要访问的文件。 (2)我们的团队成员,也就是您的新案例负责人,将根据您的保密协议编号向产品管理团队申请访问权限。 谢谢您! 此致, 卫东
View full article
如何在 Linux 系统上通过 OP-TEE 使用 SE051 执行密钥生成、加密/解密和签名/验证操作? 大家好,NXP社区的各位! 我目前正在根据这篇文章中描述的环境,将 Plug and Trust 中间件集成到 OP-TEE 中:如何将 Plug and Trust MW 集成到 OP-TEE 中。 我的目标是利用 SE051 安全元件,从运行在 Linux 上的用户空间应用程序实现以下操作: 生成 AES 密钥并将其存储在 SE051 中。 生成 RSA 密钥对并将其存储在 SE051 中。 使用存储在 SE051 中的 AES 密钥加密文件。 使用存储在 SE051 中的 AES 密钥解密文件。 使用 SE051 中的 RSA 私钥对数据进行签名。 使用 SE051 中的 RSA 公钥验证签名。 使用 SE051 中的 RSA 公钥对数据进行加密。 使用 SE051 中的 RSA 私钥解密数据。 请问各位能否指导我如何以最佳方式完成这些操作?我愿意使用以下任何命令行工具(或它们的组合),前提是这些工具在此 OP-TEE 设置中受支持: openssl 命令(通过 OpenSSL 提供程序) ssscli 工具 pkcs11-tool(通过 PKCS#11 接口) 非常感谢您能提供针对此特定 OP-TEE 环境的任何示例、文档链接或命令使用示例。 SE050 Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? 嗨@Uc_S , 从 Linux 用户空间到 SE051 有三条受支持的路径。这三款产品均可通过 Plug & Trust MW v04.07.01 获取: 通路 库 最适合 PKCS#11 libsss_pkcs11.so 通过 AES、RSA 生成/签名/验证/加密/解密 pkcs11-tool OpenSSL 提供程序 (3.x) libsss_provider.so RSA 签名/验证/加密/解密 openssl pkeyutl ssscli Python CLI 仅密钥注入/配置 OP-TEE 环境的重要提示:在您的 OP-TEE 设置 ( CFG_NXP_SE05X=y ) 中,SE051 由 OP-TEE 内核通过原生 I2C 驱动程序直接访问。Linux 用户空间应用程序不拥有 I2C 总线。以上三条路径均能正常工作,因为 Plug & Trust MW Access Manager ( accessManager ) 或 T1oI2C 套接字接口通过 OP-TEE 的可信世界将命令路由到 SE051。 操作 1:生成 AES 密钥并将其存储在 SE051 中 使用 ssscli 生成指定密钥 ID(SE051 中的对象 ID)的 AES-256 密钥: # Generate AES-256 key at Key ID 0x20000001 ssscli generate aes 0x20000001 256 验证密钥是否存在: ssscli get aes 0x20000001 aes_key_info.txt 注意: AES 密钥是对称的,不能从 SE051 导出。密钥 ID 0x20000001 是一个 32 位对象标识符,持久存储在 SE051 NVM 中。 操作 2:生成 RSA 密钥对并将其存储在 SE051 中 选项 A — 使用 pkcs11-tool (推荐) RSA密钥标签使用 sss: 格式: # Generate RSA-2048 key pair at Key ID 0x10101010 pkcs11-tool --module $PKCS11_MODULE --keypairgen --key-type rsa:2048 --label "sss:10101010" 选项 B — 使用 ssscli ssscli generate rsa 0x10101010 2048 AN13030 第 3.3.8.3 节注释:从外部注入时,RSA 密钥对必须使用 PKCS#8 或传统的 OpenSSL 格式进行 DER 编码。通过 sss_key_store_get_key() 获取时,仅返回公钥。 操作 3:使用 SE051 中的 AES 密钥加密文件 AES 对称加密可通过 SSS API ( sss_cipher_one_go ) 执行,或者,对于命令行使用,可通过小型包装应用程序执行。MW 提供了一个内置的对称示例,位于: simw-top/sss/ex/symmetric/ex_sss_symmetric.c 要直接在命令行中使用,请构建并运行示例: # After building the MW examples: ./se05x_symmetric_aes_cbc_encrypt --keyid 0x20000001 --input plaintext.bin --output ciphertext.bin --iv 00000000000000000000000000000000 MW 支持: kAlgorithm_SSS_AES_ECB 、 kAlgorithm_SSS_AES_CBC 、 kAlgorithm_SSS_AES_CTR 、 kAlgorithm_SSS_AES_GCM 、 kAlgorithm_SSS_AES_CCM (来自 AN13030 的第 3.3.9.1 节)。 操作 4:使用 SE051 中的 AES 密钥解密文件 ./se05x_symmetric_aes_cbc_decrypt --keyid 0x20000001 --input ciphertext.bin --output decrypted.bin --iv 00000000000000000000000000000000 SSS API 使用 kMode_SSS_Decrypt 模式和 sss_cipher_one_go() 进行一次性解密,或使用多步 sss_cipher_init() / sss_cipher_update() / sss_cipher_finish() 序列进行流式传输。 操作 5:使用 SE051 中的 RSA 私钥对数据进行签名 使用 pkcs11-tool (密钥保留在 SE051 中) # Sign with RSA private key (key never leaves SE051) pkcs11-tool --module $PKCS11_MODULE --sign --label sss:10101010 -m SHA256-RSA-PKCS --slot 1 -i in.der -o signature.der 支持通过 PKCS#11 实现的签名机制: SHA256-RSA-PKCS (RSASSA-PKCS1-v1_5,安全散列算法(SHA)-256) SHA1-RSA-PKCS , SHA384-RSA-PKCS , SHA512-RSA-PKCS RSA-PKCS-PSS (PSS 填充) 使用 OpenSSL 提供程序 (v3.x) # 配置 OpenSSL 使用 NXP 提供程序(参见 /etc/ssl/openssl.cnf) openssl pkeyutl -provider nxp -sign -inkey "pkcs11:token=sss;object=sss:10101010;type=private" -in in.txt -out signature.der   操作 6:使用 SE051 中的 RSA 公钥验证签名 步骤 1 — 从 SE051 导出公钥 # Method A: via ssscli ssscli get rsa pub 0x10101010 rsa_pub.der # Method B: via pkcs11-tool pkcs11-tool --module $PKCS11_MODULE --read-object --type pubkey --slot 1 --label sss:10101010 -o pubkey.der # Convert DER to PEM for OpenSSL openssl rsa -in pubkey.der -inform der -out pubkey.pem -outform pem -pubin 步骤 2 — 验证(主机端,无需 SE051) openssl dgst -keyform PEM -verify pubkey.pem -sha256 -signature signature.der in.txt # Expected output: Verified OK 操作 7:使用 SE051 中的 RSA 公钥加密数据 RSA 加密使用公钥(加密时不需要安全元件): # Encrypt with public key (host side) openssl rsautl -encrypt -inkey pubkey.pem -in in.txt -pubin -out crypt.txt 对于 OAEP 衬垫(推荐),请使用: openssl pkeyutl -encrypt -inkey pubkey.pem -pubin > -pkeyopt rsa_padding_mode:oaep > -pkeyopt rsa_oaep_md:sha256 > -in in.txt -out crypt.txt AN13030 第 3.3.5.6 节列出了支持的算法,包括 kAlgorithm_SSS_RSAES_PKCS1_OAEP_SHA256 和 kAlgorithm_SSS_RSAES_PKCS1_V1_5 。 操作 8:使用 SE051 中的 RSA 私钥解密数据 RSA 私钥解密完全在 SE051 内部执行。私钥永远不会离开安全元件。 使用 pkcs11-tool pkcs11-tool --module $PKCS11_MODULE --decrypt --label sss:10101010 --slot 1 -i crypt.txt -o decrypt.txt cat decrypt.txt 使用 OpenSSL 提供程序 (v3.x) openssl pkeyutl -provider nxp -decrypt -inkey "pkcs11:token=sss;object=sss:10101010;type=private" -in crypt.txt -out decrypt.txt AN13030 第 2.3.4 节确认:“在提供程序中添加了 RSA 加密和解密功能”(从 v04.05.03 开始,包含在 v04.07.01 中)。 关键 ID 标签约定 当使用 NXP PKCS#11 库中的 pkcs11-tool 时,密钥 ID 标签格式为: sss: 例如,键 ID 0x10101010 → 标签 sss:10101010 v04.07.00 版本中的重大变更(PKCS#11 v4.7):为了避免字节交换, CKA_ID 属性( --id )现在被视为字节数组。传递ID时不要改变字节序。 PKCS#11 令牌初始化(首次设置) 在使用 pkcs11-tool 之前,您可能需要初始化令牌槽: # Initialize slot 0 pkcs11-tool --module $PKCS11_MODULE --init-token --slot 0 --label "SE051_Token" --so-pin 12345678 # Set user PIN pkcs11-tool --module $PKCS11_MODULE --init-pin --slot 0 --login --so-pin 12345678 --pin 87654321 OpenSSL 3.x 提供程序配置 添加到 /etc/ssl/openssl.cnf (或自定义配置文件): [openssl_init] providers = provider_sect [provider_sect] default = default_sect nxp = nxp_sect [default_sect] activate = 1 [nxp_sect] module = /usr/local/lib/libsss_provider.so activate = 1 OpenSSL 提供程序源代码也可在以下网址获取: https://github.com/NXPPlugNTrust/se05x-openssl-provider 源代码示例(在 simw-top 中) MW 包中的以下内置示例直接演示了这些操作: Operation 示例路径 AES 加密/解密 simw-top/sss/ex/symmetric/ex_sss_symmetric.c RSA签名/验证 simw-top/sss/ex/rsa/ (AN13030 第 5.2.1.2 节) ECC签名/验证 simw-top/sss/ex/ecc/ (AN13030 第 5.2.1.1 节) PKCS#11 脚本 simw-top/sss/plugin/pkcs11/scripts/ OpenSSL 提供程序 RSA 加密 simw-top/sss/plugin/openssl_provider/scripts/openssl_RsaEnc.py OP-TEE 背景下的已知局限性 从 OP-TEE 内核端到 SE051 的 AES 卸载取决于 CFG_NXP_SE05X_CTR_DRV 是否启用。用户空间 AES 通过 PKCS#11 进行加密,这需要经过访问管理器,并且与 OP-TEE 加密驱动程序卸载是分开的。 在 v04.07.01 中,SE051 中的 RSA 密钥生成默认采用 CRT 格式(在 PKCS11 v4.8 中添加了 RSA_CRT 支持)。使用 PKCS11_ENABLE_RSA_KEY_GEN_CRT cmake 选项在 CRT 和普通 RSA 之间切换。 SE051 NVM 有局限性。多次 RSA 密钥对生成可能会耗尽持久存储空间——使用 ssscli delete 删除未使用的对象。 对于并发多进程访问(例如,多个用户空间应用程序),请使用 simw-top/hostlib/hostlib/accessManager 处的访问管理器。使用 -DSMCOM:STRING=JRCP_V1_AM 构建。 参考文档 文档 说明 AN13030 Plug & Trust MW 文档(主要参考资料) AN12660 符合 IEC 62443 标准(SE05x)——包含 SSS API 示例指针 simw-top/doc/ (本地 HTML) 您已安装的版本 v04.08.01 的完整文档 simw-top/doc/plugins/pkcs11.html PKCS#11 独立库文档 simw-top/doc/demos.html 可用演示示例完整列表 希望对您有所帮助。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? 嗨@Uc_S , 当设置 CFG_NXP_SE05X=y 时, OP-TEE 将独占 SE051 的 I2C 总线。Linux DTS 必须禁用该 I2C 控制器(如集成指南中所述)。这从根本上改变了 Plug & Trust MW 的使用方式: 层 谁来运营它 它如何到达SE051 OP-TEE 安全世界 OP-TEE核心 原生 I2C 驱动程序 ( CFG_IMX_I2C=y ) —直接、独占 Linux 用户空间 您的应用程序 ssscli,访问管理器 无法使用 T1oI2C — Linux DTS 中已禁用 I2C 这意味着您现有的带有 -DPTMW_SMCOM=T1oI2C 的 cmake 配置仅适用于 Linux 直接拥有 I2C 的情况。在 OP-TEE 设置中,它适用于下面描述的两种不同的版本场景。 场景 1:MW 版本输入到 OP-TEE ( CFG_NXP_SE05X_PLUG_AND_TRUST= ) 这是最重要的案件。MW在 OP-TEE 中被编译为静态库——您无需为此手动运行 cmake 。当您将 CFG_NXP_SE05X_PLUG_AND_TRUST 指向已解压的 MW 目录时,OP-TEE 的 Makefile 会自动处理集成: CFG_NXP_SE05X_PLUG_AND_TRUST=$HOME/linux-factory/plug-and-trust 您列出的 SMCOM、Host 和 Auth 标志在这里不适用。OP-TEE 通过其自身的原生 I2C 抽象层 ( CFG_IMX_I2C=y ) 驱动 SE051,完全绕过 Linux MW 通信协议栈。 场景 2:Linux 用户空间工具(ssscli / 访问管理器 / 演示) 这里就需要用到你的 cmake 标志了。当 OP-TEE 拥有 I2C 接口时,以下是对必须更改的各项标志位的逐一分析: 必须更改的标志 标志位 您当前的价值 OP-TEE 设置的推荐值 原因 -DPTMW_SMCOM T1oI2C JRCP_V1_AM (如果使用访问管理器) Linux 无法直接使用 I2C;访问管理器提供套接字代理。 -DPTMW_SE05X_Auth PlatfSCP03 None SCP03 通道由 OP-TEE 建立,而非 Linux 用户空间。 -DPTMW_SCP SCP03_SSS None 原因相同——SCP-03归OP-TEE安全世界所有。 保持不变的旗帜 标志位 Value 原因 -DPTMW_Applet SE05X_C 请更正您的 SE051C2 型号(OEF ID A8FA) -DPTMW_SE05X_Ver 07_02 与 OP-TEE 启动日志中显示的 applet 版本 7.2 相符 -DPTMW_Host iMXLinux 仍然运行在 i.MX Linux 上 -DPTMW_HostCrypto OPENSSL 未更改 -DPTMW_RTOS Default 未更改 -DPTMW_OpenSSL 3_0 OpenSSL 3.x 版本保持不变 -DPTMW_FIPS None 未更改 -DPTMW_SBL None 未更改 -DPTMW_mbedTLS_ALT None 未更改 -DPTMW_Log Silent 未更改 -DPTMW_SE_RESET_LOGIC 1 未更改;v04.07.00 版本新增选项 OP-TEE 安装中推荐的 Linux 用户空间工具的 cmake 命令 cd simw-top && mkdir build_optee_linux cmake -S . -B ./build_optee_linux/ -DPTMW_Applet=SE05X_C -DPTMW_SE05X_Ver=07_02 -DPTMW_Host=iMXLinux -DPTMW_SMCOM=JRCP_V1_AM -DPTMW_HostCrypto=OPENSSL -DPTMW_RTOS=Default -DPTMW_mbedTLS_ALT=None -DPTMW_SCP=None -DPTMW_FIPS=None -DPTMW_SBL=None -DPTMW_SE05X_Auth=None -DPTMW_Log=Silent -DCMAKE_BUILD_TYPE=Release -DPTMW_OpenSSL=3_0 -DPTMW_SE_RESET_LOGIC=1 cd build_optee_linux && make -j8 注意: JRCP_V1_AM 要求访问管理器在目标上作为守护进程运行。Access Manager 本身连接到 SE051 — 但请注意以下重要注意事项。 重要提示:访问管理器 I2C 冲突 访问管理器( hostlib/hostLib/accessManager )旨在串行化来自多个 Linux 进程的并发 I2C 访问。然而: 当 OP-TEE 完全禁用 Linux DTS 中的 I2C 接口(如 CFG_NXP_SE05X=y 所要求的)时,访问管理器本身也无法打开 I2C。 这意味着您有两种有效的部署选择: 选项 A:OP-TEE 独家产品(推荐用于生产) OP-TEE 完全拥有 I2C。Linux 用户空间仅使用 OP-TEE PKCS#11 TA ( libckteec.so ) 进行加密操作。在这种模式下,Plug & Trust MW ssscli 和演示程序无法在 Linux 上运行。 Linux App → libckteec.so → OP-TEE PKCS#11 TA → SE051 这是 i.MX Linux 用户指南 (UG10163) 中描述的基于 OP-TEE 的 SE05x 使用的路径。 选项 B:共存(测试/配置) 使用不会禁用 Linux 中 I2C 的 Linux DTS(即,不要应用 lf-6.12.y-i2c-disabled-se050 DTS 补丁)。在此配置中: OP-TEE 使用 SE051 进行加密卸载(RSA/ECC) Linux 用户空间仍然可以使用 T1oI2C (您原来的标志)运行 ssscli / Access Manager 风险:OP-TEE 和 Linux 同时进行 I2C 访问需要谨慎仲裁。 对于此选择,请将 SMCOM、SCP 和 Auth 标志恢复为原始值,并保留原始 I2C DTS(不要禁用它)。 汇总表 用例 SMCOM SCP 身份验证 说明 OP-TEE 内部 MW(用于 OP-TEE 版本的静态库) N/A N/A N/A 无需 cmake;由……处理 CFG_NXP_SE05X_PLUG_AND_TRUST= Linux 用户空间,OP-TEE 专用 I2C JRCP_V1_AM None None 需要 Access Manager,但如果 I2C 被禁用,AM 本身无法访问 SE051。 Linux 用户空间,共存(I2C 共享) T1oI2C SCP03_SSS PlatfSCP03 您原始的标志——如果 Linux DTS 仍然启用了 I2C,则这些标志有效。 Linux 用户空间通过 PKCS#11 TA(OP-TEE 独占) 不适用(无MW版本) N/A N/A 使用 pkcs11-tool / openssl libckteec.so 补充参考 AN13030 修订版 2.4 — 第 4.4 节(i.MX Linux 版本)、第 8.9 节(PKCS#11 独立库)、访问管理器文档 UG10163 i.MX Linux 用户指南— 使用 libckteec.so 的 OP-TEE PKCS#11 命令示例(第 10.4.7 节和 10.4.8 节,第 110-114 页);注意:这些示例使用 OP-TEE 内部安全存储作为密钥后端,而不是直接使用 SE05x — 当通过 CFG_NXP_SE05X=y 将 SE051 配置为 OP-TEE 加密后端时,命令语法相同。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? @Kan_Li 非常感谢您详尽周到的回复。 对三种支持路径的详细说明和命令示例非常有帮助。 关于 OP-TEE 环境,我有一个关于 Linux 根文件系统上 Plug & Trust 中间件的 CMake 构建配置的后续问题。 之前,当直接在 Linux 上运行中间件(不使用 OP-TEE 路由)时,我们使用了以下 CMake 配置标志: -DPTMW_Applet=SE05X_C -DPTMW_SE05X_Ver=07_02 -DPTMW_Host=iMXLinux -DPTMW_SMCOM=T1oI2C -DPTMW_HostCrypto=OPENSSL -DPTMW_RTOS=Default -DPTMW_mbedTLS_ALT=None -DPTMW_SCP=SCP03_SSS -DPTMW_FIPS=None -DPTMW_SBL=None -DPTMW_SE05X_Auth=PlatfSCP03 -DPTMW_Log=Silent -DCMAKE_BUILD_TYPE=Release -DPTMW_OpenSSL=3_0 -DPTMW_SE_RESET_LOGIC=1 请问上述哪些设置需要更改,以及对于此 OP-TEE 设置,它们的推荐新值应该是多少? 细节: 既然 OP-TEE 已经拥有了对 SE051 的直接 I2C 访问(通过 CFG_NXP_SE05X=y),请问在构建 Linux 用户空间中间件/工具(例如 ssscli 或 Access Manager)时,是否需要修改这些 CMake 标志? 具体来说,是否应该更新 Linux 用户空间端的 -DPTMW_SMCOM 选项(例如,从 T1oI2C 更改为 JRCP_V1_AM 或套接字接口)或 -DPTMW_Host 选项,以便通过 OP-TEE 正确路由请求? 以下是我的环境详情: 电路板:MCIMX8M-WEVK 和 OM-SE051ARD Plug and Trust MW 版本:v04.07.01 OP-TEE 操作系统版本:3.19.0 Linux 内核:6.1.151 Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? 非常感谢您如此详尽清晰的解释。 逐个标志位的分析、构建命令示例,以及关于 I2C 冲突的关键注意事项,以及在选项 A(通过 libckteec.so 使用 OP-TEE 独占)和选项 A 之间进行选择的问题。选择 B(共存)明确了我们的设置选项。 这些信息正是我们确定未来架构所需要的。
View full article
[lx2080a][lx2160a] CPUコアをオフにするにはどうすればよいですか? LX2080Aには8コア中4コアを無効化する必要があります。8コアのうち特定の4つのコアをオフにする方法を教えていただけますか? テストのために、rcw_2200_750_3200_19_5_2.rcw ファイルに以下を追加しましたが、起動しません。 .pbi 0x01e00094、0x00000f0 に書き込みます。 。終わり 他に修正が必要な箇所はありますか? Re: [lx2080a][lx2160a] How do I turn off CPU cores? 最初の4つのLX2080Aクラスタをアクティブにしたまま、上位の4つのアクティブコアを無効にする場合は、物理コアビットマップを使用します。 コピー # 物理コア8、10、12、14を無効にする .pbi 0x01e00094、0x00005500 に書き込みます 。終わり Re: [lx2080a][lx2160a] How do I turn off CPU cores? 私たちはそれを適用しました。しかし、起動しなかった。 .pbi 0x01e60060、0x0000000f に書き込みます。 0x01e00094、0x000000f0 に書き込みます 。終わり バージョンが適用されていない状態で、ubootプロンプトのレジスタを次のように読みました。 アクティブコアの数は奇数であるようだ。 > md.l 0x01e00094 01e00094: 00000000 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@........... => MD.L.0x01e60060 01e60060: 0000aaa 000000000000000000000000000000 ................ 01e60070: 000000000000000000000000000000000000................ これが原因でしょうか? ありがとう Re: [lx2080a][lx2160a] How do I turn off CPU cores? コアを無効にするためのターゲットレジスタは正しいですが、変更を以下のようにするだけでは不十分です。 .pbi 0x01e00094、0x00000f0 に書き込みます。 。終わり 完全な32ビット値を使用し、ブート/リリースパスが無効化されたコアを起動しようとしないようにしてください。 .pbi 0x01e00094、0x000000f0 を書き込みます /* COREDISR: コア 4、5、6、7 を無効化します */ 。終わり 0x01e00094 は DCFG + 0x94 です。LX2160A/LX2080A のリファレンスマニュアルには、DCFG のベースアドレスが 0x1E0_0000 であり、COREDISR がオフセット 0x94 にあると記載されています。COREDISRは未使用の物理コアを無効化・クロックゲートするための文書化された仕組みであり、システム準備前にPBIによってプログラム可能です。コア4–7のビット/フィールドはCore 4の無効化からCore 7の無効化に対応しているため、コア0–3を維持し、コア4–7を無効にしたい場合、0x000000f0が期待されるマスクです。 重要な追加項目はブートリリースです。LX2/LS2 4コアケースの場合、文書化された内部ガイダンスは以下のペアリングです: ブートリリース @ 0x01e60060 = 0x0000000f COREDISR @ 0x01e00094 = 0x000000f0 /* Core7:4 を無効にする */ したがって、起動時にリリースされるのはコア0–3のみで、コア4–7は無効化されます。ブートリリースレジスタ BRRL は RST ベース 0x1E6_0000 + 0x60 にあり、そのビット CR0...CR15 は対応するコアをブートホールドオフから解放します。また、COREDISRマスクにプライマリブートコアが含まれていないかも確認してください。RMによるとブートコアはBRCORENBR[CORE_NBR]で識別可能です。 起動失敗を確認するための2つの実用的なチェック方法: パーサー/ツールの曖昧さを避けるため、0x000000f0 を使用してください。0x00000f0 は使用しないでください。 RCW/PBIイメージがSTOP-with-CRCコマンドを使用している場合、PBIを変更した後に再構築すると、PBIのCRCを更新する必要があります。CRCは、Load RCWコマンドからSTOP-with-CRCコマンドまでのすべてのPBIコマンドを対象としています。 起動後、COREDISR とコア無効化ステータスレジスタを読み取って結果を確認します。LX2 実験では、COREDISABLESR @ 0x01E00990 を使用して無効化コアマスクを確認しました。また、COREDISRで無効化されたコアは、後からソフトウェアによって再有効化されてはならないことに注意してください。 「コア0~3を保持し、コア4~7を無効にする」には、COREDISR = 0x000000f0を使用し、ブートリリースマスクがアクティブなコアのみを解放することを確認してください。例:BRRL = 0x0000000f ; そうでない場合、ファームウェアは無効にしたコアを起動しようとする可能性があります。 Re: [lx2080a][lx2160a] How do I turn off CPU cores? .pbi 0x01e00094、0x00005500 に書き込みます 0x01e60060、0x000000aa を書き込む 。終わり 私たちはそれを適用しました。しかし、起動しなかった。 他に調査すべき事項はありますか? Re: [lx2080a][lx2160a] How do I turn off CPU cores? 起動はするが、結果は以下の通りである。 => md.l 0x01e00094 01e00094: 0000aa00 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@........... => md.l 0x01e60060 01e60060: 0000aaaa 00000000 00000000 00000000 ................ 01e60070: 00000000 00000000 00000000 00000000 ................ カーネルは8つのCPUも検出する。 これをLX2080aで試せますか? ありがとうございます。 Re: [lx2080a][lx2160a] How do I turn off CPU cores? 結果は同じようだ。 => md.l 0x01e00094 01e00094: 00008888 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@.......... . => md.l 0x01e60060 01e60060: 0000aaaa 00000000 00000000 00000000 ................ 01e60070: 00000000 00000000 00000000 00000000 ................ Re: [lx2080a][lx2160a] How do I turn off CPU cores? クラスター内のすべてのコアを無効にすると、システムがハングアップするようです。 1つのクラスター内で1つのコアだけを無効にしましょう。 .pbi 0x01e00094、0x00008888 に書き込みます。 0x01e60060、0x00002222 に書き込みます。 。終わり Re: [lx2080a][lx2160a] How do I turn off CPU cores? 以下の設定をお試しください。 .pbi 0x01e00094、0x0000aa00 に書き込みます 0x01e60060、0x000000aa を書き込む 。終わり Re: [lx2080a][lx2160a] How do I turn off CPU cores? LX2160Aのコア番号付けはクラスタグループに対して連続的です。16コアは8つのクラスターに分かれており、各クラスターには2つのコアが含まれています。番号付けは以下のとおりです。 コア0とコア1はクラスター1に属しています コア2とコア3はクラスター2に属しています。 ... そしてクラスター8に属するコア14と15まで続きます クラスタ内のすべてのコアを無効にすると、システムがハングアップします。だから目的を達成することは不可能だ。 Re: [lx2080a][lx2160a] How do I turn off CPU cores? 以下の設定は正しいと思われます。 .pbi 0x01e00094、0x00005500 に書き込みます 0x01e60060、0x000000aa に書き込みます 。終わり `0x01e60060` リリースレジスタの値 `0x0000aaaa` に関して、コア 1、3、5、7、9、11、13、および 15 は無効化されているコア (1 で示される) であり、コア 0、2、4、6、8、10、12、および 14 (0 で示される) は、LX2080A で実際にサポートされているアクティブなコアであると考えられます。 8つのクラスターそれぞれに1つのコアが接続されており、4つのクラスターは無効化しなければなりません。これにより、残りの4つのクラスターそれぞれに1つずつ、4つのアクティブなコアが残ります。しかし、`COREDISR`と`BRRL`を変更した後でも、`BRRL`と`COREDISABLESR`レジスタは引き続き`0x0000aaaa`を表示します。 そこで、クラスタ数が最初8に設定されていた「atf/nxp/soc-lx2160/soc.c'のSoC初期化ルーチンを確認し、クラスタ番号を4に変更してシステムが正常に起動しました。現在、`get_num_cluster()` 内で値を 4 にハードコーディングしていますが、他の提案やフィードバックがあれば歓迎します。 => md.l 0x01e00094 01e00094: 00005500 00000000 00000000 00000000 .U............. => md.l 0x01e60060 01e60060: 0000ffaa 00000000 00000000 00000000 ................ => md.l 0x01e00990 01e00990: 0000ffaa 00000000 00000000 00000000 ... よろしくお願いします。
View full article
Gui Guider 2.0.1 Label Font Size Bug Getting a bug where the displayed font size is much smaller than the true font size for size 20.  Size 21: c_nebe_1-1788222435551.png Size 20: c_nebe_0-1788222422651.png Size 19: c_nebe_2-1788222464898.png It looks to be using the size 14 font in place of the size 20. 回复: Gui Guider 2.0.1 Label Font Size Bug Hi @c_nebe  I tested it on my end. Harry_Zhang_0-1788257251619.png Harry_Zhang_1-1788257276889.png Harry_Zhang_2-1788257288278.png I haven't reproduced the issue you mentioned. BR Harry
View full article
デバイスとの結合を解除することに関して こんにちは、 MCUXpresso SDKバージョン26.03を使ってBLE通信を実装しようとしています。 API関数Gap_RemoveBondについて質問があります。 その注記には、「このAPIは、呼び出し時にアクティブな接続が存在しないことを前提としています」と記載されている。 1.つまり、コネクテッドデバイスがない時だけ使えるということですか? 2. Gap_RemoveBondがアクティブな接続が存在する間に結合を除去できない場合、アクティブな接続が有効な状態で結合情報を除去する方法はありますか? 質問に関する追加情報 3つのデバイスがあると仮定します。 ・周辺機器 ・中央装置A ・中央装置B takuya08_0-1788256233203.pngtakuya08_0-1788256233203.pngtakuya08_0-1788256233203.pngtakuya08_0-1788256233203.png ペリフェラルはすでにセントラルAとセントラルBの両方と結合されています。 ペリフェラルがセントラルAとセントラルBの両方に積極的にコネクテッドされている場合: takuya08_1-1788256275044.pngtakuya08_1-1788256275044.pngtakuya08_1-1788256275044.pngtakuya08_1-1788256275044.png その指摘から、ペリフェラルはセントラルAとBがコネクテッドされている間は結合情報を削除できないと理解しています。 アクティブな接続中に、ボンディング情報を削除する方法はありますか? ペリフェラルがセントラルAにのみ積極的に接続されている場合: takuya08_2-1788256364083.pngtakuya08_2-1788256364083.pngtakuya08_2-1788256364083.pngtakuya08_2-1788256364083.png 周辺機器がセントラルAとセントラルBの両方の結合情報を削除することは不可能でしょうか? それともセントラルBのボンディング情報だけを削除することは可能でしょうか? ペリフェラルがいかなるデバイスにも接続されていない場合: takuya08_3-1788256474725.pngtakuya08_3-1788256474725.pngtakuya08_3-1788256474725.pngtakuya08_3-1788256474725.png このコメントから、この場合、周辺機器はセントラルAとセントラルBの両方の結合情報を削除できると理解しています。 ご協力ありがとうございます。 Re: Regarding Removes the bond with a device @sofiaurueta ご返信ありがとうございます。 あなたの回答から、たとえ1台でも接続されていればボンディング情報は削除できないと理解しました。 ただ、念のためもう一度確認したいです。  2-1788256364083.png2-1788256364083.png2-1788256364083.png ペリフェラルにセントラルAとセントラルBの2つのデバイスの結合情報が保存されており、現在セントラルAにコネクテッドされている場合、以下の挙動のうちどれが起こるのでしょうか? 1.接続されていないセントラルBのボンド情報は削除可能です。 2. 2つの債券情報記録はいずれも削除できません。 Re: Regarding Removes the bond with a device こんにちは、お元気でお過ごしでしょうか。 Gap_RemoveBond() は、アクティブなBLE接続がない場合のみ呼び出せます。APIのドキュメントには、ボンド情報が削除される前にすべての接続を切断することを明記しています。同じ制限はGap_RemoveAllBonds()にも適用されます。 現在、MCUXpresso SDKのBLEホストスタックには、接続がアクティブな間にNVMボンドデータを削除することをサポートするAPIはありません。 アクティブなユースCASEでボンドを除去するための推奨フローは以下の通りです: 関連するコネクテッドピアの連絡先としてGap_Disconnect(deviceId)を呼び出し、切断を確認させるgConnEvtDisconnected_c接続イベント情報を待ってからGap_RemoveBond(nvmIndex)を呼び出します。 よろしくお願いします、 ソフィア。 Re: Regarding Removes the bond with a device こんにちは、 @sofiaurueta 現在、結合情報の削除を検討中です。 答えをいただけますか? ご協力ありがとうございます。
View full article
Regarding Removes the bond with a device Hello, I'm trying to implement BLE communication using MCUXpresso SDK version 26.03. I have a question about the API function Gap_RemoveBond. The remark states, "This API requires that there are no active connections at call time." 1. Does this mean it can only be used when there are no connected devices? 2. If Gap_RemoveBond cannot be used to remove a bond while an active connection exists, is there a way to remove bonding information while an active connection is active? Additional information regarding the question Suppose there are three devices: ・Peripheral device ・Central device A ・Central device B takuya08_0-1788256233203.pngtakuya08_0-1788256233203.pngtakuya08_0-1788256233203.pngtakuya08_0-1788256233203.png The Peripheral device is already bonded with both Central A and Central B. When the Peripheral is actively connected to both Central A and Central B: takuya08_1-1788256275044.pngtakuya08_1-1788256275044.pngtakuya08_1-1788256275044.pngtakuya08_1-1788256275044.png Based on the remark, I understand that the Peripheral cannot delete the bonding information for Central A and B while they are connected. Is there any way to delete bonding information during an active connection? When the Peripheral is actively connected only to Central A: takuya08_2-1788256364083.pngtakuya08_2-1788256364083.pngtakuya08_2-1788256364083.pngtakuya08_2-1788256364083.png Is it impossible for the Peripheral to delete the bonding information for both Central A and Central B? Or is it possible to delete only Central B's bonding information? When the Peripheral is not connected to any device: takuya08_3-1788256474725.pngtakuya08_3-1788256474725.pngtakuya08_3-1788256474725.pngtakuya08_3-1788256474725.png Based on the remark, I understand that the Peripheral can delete the bonding information for both Central A and Central B in this case. Thank you for your help. Re: Regarding Removes the bond with a device @sofiaurueta  Thank you for your response. Based on your answer, I understand that bonding information cannot be deleted if even a single device is connected.  However, I would like to double-check to be sure.  2-1788256364083.png2-1788256364083.png2-1788256364083.png If the peripheral has bond information stored for two devices, Central A and Central B, and it is currently connected to Central A, which of the following behaviors occurs? 1. The bond information for the unconnected Central B can be deleted. 2. Neither of the two bond information records can be deleted. Re: Regarding Removes the bond with a device Hello, hope you are doing well. Gap_RemoveBond() can only be called when there are no active BLE connections. The API documentation explicitly requires that all connections be disconnected before bond information is removed. The same restriction applies to Gap_RemoveAllBonds(). There is currently no API in the MCUXpresso SDK BLE Host Stack that supports deleting NVM bond data while any connection is active. The recommended flow for removing a bond during an active use case is as follows: Call Gap_Disconnect(deviceId) for the relevant connected peers, wait for the gConnEvtDisconnected_c connection event confirming disconnection, then call Gap_RemoveBond(nvmIndex). Best regards, Sofia. Re: Regarding Removes the bond with a device Hello,   @sofiaurueta  We are currently considering removing the bonding information. Could you please provide an answer? Thank you for your help.
View full article
Linux上でOP-TEE経由でSE051でキー生成、エンコン/デック、署名/検証を行う方法は? こんにちは、NXPコミュニティの皆さん、 現在、この投稿「Plug and Trust MWをOP-TEEに統合する方法」で説明されている環境に基づいて、Plug and Trust MiddlewareをOP-TEEに統合する作業を行っています。 私の目標は、SE051のセキュア要素を活用し、Linux上で動作するユーザー空間アプリケーションから以下の操作を実現することです。 AESキーを生成し、SE051に保存します。 RSA鍵ペアを生成し、SE051に保存します。 SE051に保存されたAESキーを使ってファイルを暗号化します。 SE051に保存されているAESキーを使ってファイルを復号します。 SE051でRSA秘密鍵を使用してデータに署名します。 SE051にあるRSA公開鍵を使用して署名を検証します。 SE051でRSA公開鍵を使用してデータを暗号化します。 SE051でRSA秘密鍵を使用してデータを復号します。 これらの手術を達成するための最適な方法について、どなたかアドバイスをいただけませんか?このOP-TEE環境でサポートされている限り、以下のコマンドラインツール(またはそれらの組み合わせ)のいずれかを使用することに抵抗はありません。 openSSLコマンド(OpenSSLプロバイダー経由) ssscliツール pkcs11-tool(PKCS#11インターフェース経由) この特定のOP-TEE環境に関する例、ドキュメントリンク、コマンドの使用例があれば大変ありがたいです。 SE050 Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? こんにちは、 @Uc_S さん。 Linuxユーザー空間からSE051への サポートされた経路は3 つあります。これら3つはすべてPlug & Trust MW v04.07.01で利用可能です。 パス 図書館 最適な用途 PKCS#11 libsss_pkcs11.so AES、RSAキーの生成/署名/検証/エンク/デック pkcs11-tool OpenSSL プロバイダー(3.x) libsss_provider.so RSA署名/検証/エンコード/デコード openssl pkeyutl ssscli Python CLI キーの注入/プロビジョニングのみ OP-TEE環境に関する重要な注意点: OP-TEEセットアップ( CFG_NXP_SE05X=y )では、SE051はOP-TEEコアがネイティブI2Cドライバを通じて直接アクセスします。Linuxユーザー空間アプリケーションはI2Cバスを所有 していません 。上記の3つのパスはすべて正しく動作します。なぜなら、Plug & Trust MWアクセスマネージャー( accessManager )またはT1oI2CソケットインターフェースがOP-TEEの信頼されたワールドを通じてコマンドをSE051にルーティングするためです。 操作1:AESキーを生成し、SE051に保存する ssscli を使って特定のキーID(SE051のオブジェクトID)でAES-256キーを生成します: # Generate AES-256 key at Key ID 0x20000001 ssscli generate aes 0x20000001 256 キーが存在することを確認するには: ssscli get aes 0x20000001 aes_key_info.txt 注意: AESキーは対称的であり、SE051からエクスポートすることはできません。キーID 0x20000001 は、SE051 NVMに永続的に保存される32ビットのオブジェクト識別子です。 操作2:RSA鍵ペアを生成し、SE051に保存する オプションA — pkcs11-tool を使用する(推奨) RSAキーラベルは以下の形式を使用します sss: : # Generate RSA-2048 key pair at Key ID 0x10101010 pkcs11-tool --module $PKCS11_MODULE --keypairgen --key-type rsa:2048 --label "sss:10101010" オプションB — 使用 ssscli ssscli generate rsa 0x10101010 2048 AN13030 セクション 3.3.8.3 注記: RSA キー ペアを外部から注入する場合は、PKCS#8 または従来の OpenSSL フォーマットを使用して DER エンコードする必要があります。 sss_key_store_get_key() を介して取得した場合、公開鍵のみが返されます。 操作3:SE051のAESキーを使ってファイルを暗号化する AES対称暗号化はSSS API( sss_cipher_one_go )またはコマンドライン使用の場合は小型ラッパーアプリケーションを介して行われます。MWには、以下の場所に組み込みの対称例が用意されています。 simw-top/sss/ex/symmetric/ex_sss_symmetric.c コマンドラインから直接使用するには、以下のサンプルをビルドして実行してください。 # After building the MW examples: ./se05x_symmetric_aes_cbc_encrypt --keyid 0x20000001 --input plaintext.bin --output ciphertext.bin --iv 00000000000000000000000000000000 MWは以下をサポートしています: kAlgorithm_SSS_AES_ECB 、 kAlgorithm_SSS_AES_CBC 、 kAlgorithm_SSS_AES_CTR 、 kAlgorithm_SSS_AES_GCM 、 kAlgorithm_SSS_AES_CCM (AN13030の第3.3.9.1節より)。 操作4:SE051のAESキーを使ってファイルを復号する ./se05x_symmetric_aes_cbc_decrypt --keyid 0x20000001 --input ciphertext.bin --output decrypted.bin --iv 00000000000000000000000000000000 SSS APIは、ワンショット復号には sss_cipher_one_go() を使用した kMode_SSS_Decrypt モード、ストリーミングには複数ステップの sss_cipher_init() / sss_cipher_update() / sss_cipher_finish() シーケンスを使用します。 操作5:SE051のRSA秘密鍵を使用してデータに署名する pkcs11-tool を使用します(キーはSE051に保持されます) # Sign with RSA private key (key never leaves SE051) pkcs11-tool --module $PKCS11_MODULE --sign --label sss:10101010 -m SHA256-RSA-PKCS --slot 1 -i in.der -o signature.der PKCS#11でサポートされている手話メカニズム: SHA256-RSA-PKCS (RSASSA-PKCS1-v1_5、SHA-256) SHA1-RSA-PKCS 、 SHA384-RSA-PKCS 、 SHA512-RSA-PKCS RSA-PKCS-PSS (PSSパディング) OpenSSL プロバイダー(v3.x)の使用 # OpenSSLをNXPプロバイダーを使用するように設定してください(/etc/ssl/openssl.cnf参照) openssl pkeyutl -provider nxp -sign -inkey "pkcs11:token=sss;object=sss:10101010;type=private" -in in.txt -out signature.der   操作6:SE051のRSA公開鍵を使用して署名を検証する ステップ1 — SE051から公開鍵をエクスポートする # Method A: via ssscli ssscli get rsa pub 0x10101010 rsa_pub.der # Method B: via pkcs11-tool pkcs11-tool --module $PKCS11_MODULE --read-object --type pubkey --slot 1 --label sss:10101010 -o pubkey.der # Convert DER to PEM for OpenSSL openssl rsa -in pubkey.der -inform der -out pubkey.pem -outform pem -pubin ステップ2 — 検証(ホスト側、SE051は不要) openssl dgst -keyform PEM -verify pubkey.pem -sha256 -signature signature.der in.txt # Expected output: Verified OK 操作7:SE051のRSA公開鍵を使用してデータを暗号化する RSA暗号化は公開鍵を使用します(暗号化にセキュアエレメントは不要です)。 # Encrypt with public key (host side) openssl rsautl -encrypt -inkey pubkey.pem -in in.txt -pubin -out crypt.txt OAEPパディング(推奨)には以下を使用してください。 openssl pkeyutl -encrypt -inkey pubkey.pem -pubin > -pkeyopt rsa_padding_mode:oaep > -pkeyopt rsa_oaep_md:sha256 > -in in.txt -out crypt.txt AN13030 セクション 3.3.5.6 には、 kAlgorithm_SSS_RSAES_PKCS1_OAEP_SHA256 および kAlgorithm_SSS_RSAES_PKCS1_V1_5 を含むサポートされているアルゴリズムがリストされています。 操作8:SE051のRSA秘密鍵を使用してデータを復号化する RSA秘密鍵の復号化は、SE051内部で完全に実行されます。秘密鍵はセキュアエレメントから決して外に出ることはありません。 使用 pkcs11-tool pkcs11-tool --module $PKCS11_MODULE --decrypt --label sss:10101010 --slot 1 -i crypt.txt -o decrypt.txt cat decrypt.txt OpenSSL プロバイダー(v3.x)の使用 openssl pkeyutl -provider nxp -decrypt -inkey "pkcs11:token=sss;object=sss:10101010;type=private" -in crypt.txt -out decrypt.txt AN13030 セクション2.3.4は「RSAの暗号化および復号機能がプロバイダーに追加された」(v04.05.03以降、v04.07.01に含まれます)を確認しています。 キーIDラベルの慣例 NXP PKCS#11ライブラリで pkcs11-tool を使用する場合、Key IDラベル形式は以下の通りです。 sss: 例えば、キーID 0x10101010 →ラベル sss:10101010 バージョン04.07.00 (PKCS#11 v4.7) における互換性のない変更点:バイトスワップを回避するため、 CKA_ID 属性( --id )はバイト配列として扱われるようになりました。エンディアンを変更せずにIDを渡します。 PKCS#11トークンの初期化(初回設定) pkcs11-tool を使用する前に、トークンスロットを初期化する必要がある場合があります。 # Initialize slot 0 pkcs11-tool --module $PKCS11_MODULE --init-token --slot 0 --label "SE051_Token" --so-pin 12345678 # Set user PIN pkcs11-tool --module $PKCS11_MODULE --init-pin --slot 0 --login --so-pin 12345678 --pin 87654321 OpenSSL 3.x プロバイダー構成 /etc/ssl/openssl.cnf (またはカスタム設定ファイル)に追加します。 [openssl_init] providers = provider_sect [provider_sect] default = default_sect nxp = nxp_sect [default_sect] activate = 1 [nxp_sect] module = /usr/local/lib/libsss_provider.so activate = 1 OpenSSLプロバイダーのソースは以下の場所でも利用可能です: https://github.com/NXPPlugNTrust/se05x-openssl-provider ソースコード例(simw-top内) MWパッケージに内蔵された以下の例は、これらの操作を直接示しています: 動作 パス例 AESの暗号化/復号 simw-top/sss/ex/symmetric/ex_sss_symmetric.c RSA署名/検証 simw-top/sss/ex/rsa/ (AN13030のセクション5.2.1.2) ECC署名/検証 simw-top/sss/ex/ecc/ (AN13030のセクション5.2.1.1) PKCS#11 スクリプト simw-top/sss/plugin/pkcs11/scripts/ OpenSSL プロバイダ RSA enc simw-top/sss/plugin/openssl_provider/scripts/openssl_RsaEnc.py OP-TEEにおける既知の制限事項 OP-TEEカーネル側からSE051へのAESオフロードは、 CFG_NXP_SE05X_CTR_DRV 有効化されている必要があります。PKCS#11を経由したユーザー空間AESはアクセス**マネージャ**を経由し、OP-TEEの暗号**ドライバ**オフロードとは別に行われます。 SE051のRSA鍵生成は、バージョン04.07.01でデフォルトでCRT形式となっています(PKCS11 v4.8でサポートが追加され RSA_CRT )。cmakeオプション PKCS11_ENABLE_RSA_KEY_GEN_CRT を使ってCRTと普通のRSAを切り替えてください。 SE051 NVMには制限があります。RSA鍵ペアの生成回数が多いと、永続ストレージが枯渇する可能性があります。使用されていないオブジェクトは ssscli delete で削除してください。 複数のプロセス同時アクセス(例:複数のユーザー空間アプリ)には、 simw-top/hostlib/hostlib/accessManager のアクセスマネージャを使用します。 -DSMCOM:STRING=JRCP_V1_AM で構築します。 参考資料 ドキュメント 説明 AN13030 プラグ&トラストMWドキュメント(主要参照) AN12660 SE05xによるIEC 62443準拠 ― SSS APIの例へのポインタを含む simw-top/doc/ (ローカルHTML) インストール済みバージョンv04.08.01の完全なドキュメント simw-top/doc/plugins/pkcs11.html PKCS#11 スタンドアロンライブラリのドキュメント simw-top/doc/demos.html 利用可能なデモ例の完全なリスト お役に立てば幸いです。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? こんにちは、 @Uc_S さん。 CFG_NXP_SE05X=y が設定されると、OP-TEEはSE051のI2Cバスの独占所有権を取得します。Linux DTSはそのI2Cコントローラを無効にしなければなりません(統合ガイドに記載されています)。これは、Plug & Trust MW の使用方法を根本的に変えるものです。 レイヤ 誰が運営しているのか SE051への到達方法 OP-TEE セキュアワールド OP-TEEコア ネイティブI2Cドライバー( CFG_IMX_I2C=y )— ダイレクト、排他 Linuxユーザースペース あなたのアプリケーション、ssscli、アクセス マネージャ T1oI2Cは使えません — Linux DTSではI2Cが無効化されています つまり、既存のcmake設定はLinuxが直接I2Cを所有している場合にのみ適用される -DPTMW_SMCOM=T1oI2C です。OP-TEEの設定では、以下に説明する2つの異なるビルドシナリオに適用されます。 シナリオ1:MWビルドがOP-TEE( CFG_NXP_SE05X_PLUG_AND_TRUST= )に供給される これが最も重要な事件です。MWはOP-TEE内部で静的ライブラリとしてコンパイルされるため、 cmake 手動で実行する必要はありません。OP-TEEのMakefileは、 CFG_NXP_SE05X_PLUG_AND_TRUST で抽出したMWディレクトリを指定すると、自動的に統合処理を行います。 CFG_NXP_SE05X_PLUG_AND_TRUST=$HOME/linux-factory/plug-and-trust あなたが挙げたSMCOM、Host、およびAuthフラグは、ここでは適用されません。OP-TEEは独自のネイティブI2C抽象化層( CFG_IMX_I2C=y )を介してSE051を駆動し、Linux MW通信スタックを完全にバイパスします。 シナリオ2:Linuxユーザースペースツール(ssscli / Access Manager / デモ) ここで、CMakeのフラグが適用されます。OP-TEEがI2Cを所有する場合、変更が必要な箇所をフラグごとに分析した結果は以下のとおりです。 変更しなければならない旗 フラグ 現在の価値 OP-TEEセットアップの推奨値 理由 -DPTMW_SMCOM T1oI2C JRCP_V1_AM (アクセス マネージャを使う場合) Linuxは直接I2Cを使用できません。アクセス マネージャはソケットプロキシを提供します -DPTMW_SE05X_Auth PlatfSCP03 None SCP03チャネルはLinuxユーザースペースではなくOP-TEEによって確立されています -DPTMW_SCP SCP03_SSS None 同じ理由です。SCP03はOP-TEEセキュアワールドが所有しています。 変わらない旗 フラグ バリュー 理由 -DPTMW_Applet SE05X_C お使いのSE051C2バリアント(OEF ID A8FA)に適合しています。 -DPTMW_SE05X_Ver 07_02 OP-TEEのブートログに見られるアプレットバージョン7.2に一致します。 -DPTMW_Host iMXLinux まだLinux i.MX 動いています -DPTMW_HostCrypto OPENSSL 変更なし -DPTMW_RTOS Default 変更なし -DPTMW_OpenSSL 3_0 OpenSSL 3.x では変更なし -DPTMW_FIPS None 変更なし -DPTMW_SBL None 変更なし -DPTMW_mbedTLS_ALT None 変更なし -DPTMW_Log Silent 変更なし -DPTMW_SE_RESET_LOGIC 1 変更なし。v04.07.00で新しいオプションが追加されました。 LinuxユーザースペースツールのOP-TEEセットアップにおける推奨cmakeコマンド cd simw-top && mkdir build_optee_linux cmake -S . -B ./build_optee_linux/ -DPTMW_Applet=SE05X_C -DPTMW_SE05X_Ver=07_02 -DPTMW_Host=iMXLinux -DPTMW_SMCOM=JRCP_V1_AM -DPTMW_HostCrypto=OPENSSL -DPTMW_RTOS=Default -DPTMW_mbedTLS_ALT=None -DPTMW_SCP=None -DPTMW_FIPS=None -DPTMW_SBL=None -DPTMW_SE05X_Auth=None -DPTMW_Log=Silent -DCMAKE_BUILD_TYPE=Release -DPTMW_OpenSSL=3_0 -DPTMW_SE_RESET_LOGIC=1 cd build_optee_linux && make -j8 注: JRCP_V1_AM アクセスマネージャーがターゲット上でデーモンとして動作している必要があります。アクセスマネージャー自体はSE051に接続しますが、重要な注意点を参照してください。 重要な注意点:アクセスマネージャーとのI2C対立 アクセスマネージャー( hostlib/hostLib/accessManager )は、複数のLinuxプロセスからの同時I2Cアクセスをシリアライズするよう設計されています。しかし: OP-TEEがLinux DTSでI2Cインターフェースを完全に無効にした場合( CFG_NXP_SE05X=y で求められます)、アクセスマネージャー自体もI2Cを起動できません。 つまり、有効なデプロイメントオプションは2つあります。 選択肢A:OP-TEE限定(生産向け推奨) OP-TEEはI2Cを完全に所有しています。Linuxユーザースペースでは、暗号操作にはOP-TEE PKCS#11 TA( libckteec.so )のみを使用しています。このモードでは、Plug and Trust MWのSSSCLIやデモはLinuxからは実行されません。 Linux App → libckteec.so → OP-TEE PKCS#11 TA → SE051 これは i.MX Linux ユーザーガイド(UG10163)で説明されているOP-TEEベースのSE05x使用に関する経路です。 選択肢B:共存(テスト/プロビジョニング) LinuxからI2Cを無効化 しない LinuxのDTSを使いましょう(つまり、 lf-6.12.y-i2c-disabled-se050 DTSパッチを適用しないでください)。この構成では: OP-TEEは暗号化オフロード(RSA/ECC)にSE051を使用します。 Linuxのユーザースペースは、元のフラグを使ってSSSCLIやアクセスマネージャーを T1oI2C 実行できます。 リスク:OP-TEEとLinuxの両方からの同時I2Cアクセスには慎重な仲裁が必要です この選択肢では、 SMCOM、SCP、およびAuthフラグを元の値に戻し、元のI2C DTSを維持してください(無効にしないでください)。 要約表 ユース・ケース SMCOM SCP 認証 備考 OP-TEE内部MW(OP-TEEビルド用の静的ライブラリ) N/A N/A N/A cmakeは不要です。 CFG_NXP_SE05X_PLUG_AND_TRUST= Linuxユーザースペース、OP-TEE独占I2C JRCP_V1_AM None None Access Managerが必要ですが、I2Cを無効にするとAM自体がSE051にアクセスできません Linuxユーザースペース、共存(I2C共有) T1oI2C SCP03_SSS PlatfSCP03 あなたの元のフラグは、Linux DTSがまだI2Cを有効にしている場合に有効です Linuxユーザースペース(PKCS#11 TA経由、OP-TEE限定) 該当なし(MWビルドなし) N/A N/A pkcs11-tool / openssl を libckteec.so 追加参考資料 AN13030 Rev. 2.4 — セクション4.4(i.MX Linux ビルド)、セクション8.9(PKCS#11 スタンドアロンライブラリ)、Access Managerドキュメント UG10163 i.MX Linuxユーザーガイド — libckteec.so を用いたOP-TEE PKCS#11コマンド例(セクション10.4.7および10.4.8、110–114ページ); 注: これらの例はOP-TEE内部セキュアストレージをキーバックエンドとして使用しており、SE05xを直接使うわけではありません。SE051がOP-TEE暗号バックエンドとしてCFG_NXP_SE05X=yを介して設定されている場合もコマンド構文は同じです すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? @Kan_Li 丁寧かつ詳細なご回答をいただき、誠にありがとうございました。 サポートされている3つのパスの詳細な説明とコマンド例は非常に役立ちます。 OP-TEE環境に関して、Linuxのrootfs上のPlug & TrustミドルウェアのCMakeビルド構成について追加の質問があります。 以前は、OP-TEEルーティングなしでLinux上でミドルウェアを直接実行していた際、以下のCMake設定フラグを使用していました: -DPTMW_Applet=SE05X_C -DPTMW_SE05X_Ver=07_02 -DPTMW_Host=iMXLinux -DPTMW_SMCOM=T1oI2C -DPTMW_HostCrypto=OPENSSL -DPTMW_RTOS=Default -DPTMW_mbedTLS_ALT=None -DPTMW_SCP=SCP03_SSS -DPTMW_FIPS=None -DPTMW_SBL=None -DPTMW_SE05X_Auth=PlatfSCP03 -DPTMW_Log=Silent -DCMAKE_BUILD_TYPE=Release -DPTMW_OpenSSL=3_0 -DPTMW_SE_RESET_LOGIC=1 上記の設定のうちどれを変えるべきか、またこのOP-TEEセットアップで推奨される新しい値は何であるべきか教えていただけますか? 詳細: OP-TEEがSE051への直接I2Cアクセス(CFG_NXP_SE05X=y経由)を所有している今、Linuxのユーザー空間ミドルウェアやツール(SSSCLIやアクセス マネージャなど)を構築する際に、これらのCMakeフラグのいずれかを変更する必要があるのか教えていただけますか? 具体的には、-DPTMW_SMCOM(例:T1oI2CからJRCP_V1_AMやソケットインターフェースへの変更)や-DPTMW_Hostのようなオプションは、Linuxユーザー空間向けにOP-TEE経由でリクエストを適切にルーティングするために更新すべきでしょうか? 私の環境情報は以下のとおりです。 基板:MCIMX8M-WEVKおよびOM-SE051ARD Plug and Trust MW バージョン: v04.07.01 OP-TEE OSバージョン:3.19.0 Linuxカーネル:6.1.151 Re: How to perform Key Gen, Enc/Dec, and Sign/Verify with SE051 via OP-TEE on Linux? この非常に詳細かつ明快な説明をいただき、誠にありがとうございました。 フラッグごとの説明、ビルドコマンドの例、特にI2Cの競合と選択肢A(OP-TEE独占、libckteec.so 経由)の選択に関する重要な注意点そして選択肢B(共存)によって、設定オプションが明確になりました。 この情報は、今後のアーキテクチャを決定する上でまさに必要なものでした。
View full article
S32K388 GMAC0 Eth_43_GMACドライバーがRX割り込みを受け取らない こんにちは、 私は以下の設定を使用しています。 S32K388EVB-Q289 S32DS 3.6.8 RTD 7.0.1 提供されたEth_InternalLoopback_S32K388例プロジェクトをベースにし、PCからメディアコンバーター経由でフレームを受け取れるように改良しました。例 S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600で言及されていた RTD 修正を追加しました。ブレークポイントを達成できました Eth_43_GMAC_Receive(EthConf_EthCtrlConfig_EthCtrlConfig_0、0U、&Status); そして、イーサネットフレームを点検できました EthIf_RxIndication(Eth_43_GMAC_apxInternalCfg[PartitionId]->Eth_43_GMAC_apCtrlConfig[CtrlIdx]->EthCtrlEthIfIdx, FrameType, IsBroadcast, MacSrcAddr, Payload, PayloadLength, IngressTimeTuplePtr, RxHandleId); しかし、while 1 ループを追加し、Rx 割り込みを有効にして GMAC0_CH0_RX_IRQHandler にリンクしても、どこにも割り込みが発生しませんでした。プロジェクトを以下に添付しました。 James_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.png S32K3 オートモーティブ-RTD  Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt こんにちは、 @James_Zhang_SE さん、 添付のプロジェクトを確認しました。RTD7.0.1でRX IRQを有効にするには、Ingress QueueHandlerFunctionを変更してQueueInterruptを有効にする必要があります。 PavelL_0-1788263577590.pngPavelL_0-1788263577590.pngPavelL_0-1788263577590.png その変更後、GMAC_RxIRQHandler() でブレークポイントに到達しました。Eth_43_GMAC_Receive() にて。 また、RGMII TXCLKが入力として定義されていますが、出力として定義されるべきです。 ただし、WiresharkでTXフレームを見るには、イニットシーケンスを適切に変更する必要があります。 例S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600 。あなたのプロジェクトでは、次のように見え ます: PavelL_1-1788264277735.pngPavelL_1-1788264277735.pngPavelL_1-1788264277735.png よろしくお願いいたします。 パベル Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt こんにちは、パベルさん。 サポートありがとうございます。ご提案の修正を適用した後、GMACドライバーが動作するようになりました。 いくつか追加の質問がありますので、ご教示いただければ幸いです。 GMACドライバーの設定や使用手順を完全に説明した詳細なドキュメントはありますか?まずは自分でドキュメントを確認して、ドライバのことをもっと理解したいと思っています。 EthIf_RxIndication()の中で、呼び出す必要がありますか? Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId); 関数の最後に受信バッファを解放する処理はありますか? GMACの設定オプションは数多く用意されています。各設定パラメータが何をするのか、どのように設定すべきかを説明するドキュメントや参考文献はありますか? ご協力ありがとうございました。皆さんのサポートに本当に感謝しています。 Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt こんにちは、 @James_Zhang_SE さん。 最新情報のご共有ありがとうございます。GMACドライバーが今あなたのために使えるようになったと聞いて安心しました。 追加のご質問について: 1.ドライバーの設定および使用に関する主な参照は、RTDインストールに含まれているEth_43_GMACユーザーマニュアルです。例:C:\NXP\S32DS.3.6.6_RTD701\S32DS\software\PlatformSDK_S32K3\RTD\Eth_43_GMAC_TS_T40D34M70I1R0\doc\RTD_ETH_43_GMAC_UM.pdf 同じディレクトリに保存されている対応するEth_43_GMAC統合マニュアル(RTD_ETH_43_GMAC_IM.pdf)と、利用可能なGMACサンプルプロジェクトも確認することをお勧めします。   2. Eth_43_GMAC_ReleaseRxBuffer() を呼び出す必要があるかどうかは、EthCtrlReleaseResourceAfterReception 設定パラメータによって決まります。 PavelL_0-1789024403441.png 受信後の自動リリースが有効の場合、ドライバーはEthIf_RxIndication()が戻った後にRXリソースを解放するため、明示的にリリースすべきではありません。 自動解放が無効になっている場合、EthIf_RxIndication() が戻った後も、受信バッファは割り当てられたままになります。その場合、アプリケーションは最終的に以下を呼び出さなければなりません。 Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId);   このモードは、アプリケーションが受信データを保持してさらなるプロセッシングを行う必要がある場合に有用です。ただし、バッファはアプリケーションが使用を終えた後に解放されなければなりません。そうしないと、利用可能な受信バッファが最終的に枯渇してしまう。 また、受信したペイロードポインタは、対応するバッファが解放された後は使用しないでください。 3. Eth_43_GMACユーザーマニュアルは個々の構成パラメータの主要な参照資料でもあります。さらに、S32設定ツールでは、対応する設定を選択またはマウスオーバーすると、多くのパラメーターの説明が表示されます。MACフィルタリング、DMA操作、MTLキュー、タイムスタンプ、割り込み状態などのハードウェアレベルの動作については、S32K3リファレンスマニュアルのGMAC/EMAC章を参照してください。 実用的な出発点として、RTDパッケージで提供されているGMACの例を参照することをお勧めします。このページには、lwIPの機能的なサンプルも掲載されています。 https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-Examples/ta-p/1108990 何か問題を感じたら、遠慮なくサポートをお願いしてください。各トピックごとに専用スレッドを設けることが望ましいです。これにより、他のユーザーにとってケースの明確さを保つことができます。 よろしくお願いいたします。 パベル
View full article
Gui Guider 2.0.1 标签字体大小错误 出现一个bug,显示字体大小(20号字)比实际字体大小小很多。 21号: c_nebe_1-1788222435551.png 20号: c_nebe_0-1788222422651.png 19号尺寸: c_nebe_2-1788222464898.png 它似乎使用的是 14 号字体而不是 20 号字体。 回复: Gui Guider 2.0.1 Label Font Size Bug 嗨@c_nebe 我这边测试过了。 Harry_Zhang_0-1788257251619.png Harry_Zhang_1-1788257276889.png Harry_Zhang_2-1788257288278.png 我没有重现您提到的问题。 BR 哈里
View full article
I cannot get a .mex file generated for a brand new project in either S32DS version Board: FRDM-A-S32K312 (S32K312MINI-EVB) S32DS versions installed side by side: #S32DesignStudio 3.6.5 and 3.6.6 (C:\NXP\S32DS.3.6.5 and C:\NXP\S32DS.3.6.6) RTD installed: S32K3  RTD, version 7.0.0.202601301531 (confirmed under Help > About > Installation Details > Installed Software, screenshot attached — full list at the end of this post AWS-LIBRARIES-S32K3  AUTOMOTIVE-RTD  Issue: The S32K3 RTD/SDK never shows up as attachable — neither when creating a brand-new project nor when trying to attach it to an already-existing one. As a result, I cannot get a .mex file generated in any case, except by copying an existing .mex from an example project into another project. - Creating a project via New > S32DS Application Project completes successfully, but no .mex file is created in the resulting project (no SDK selection step offers the RTD). ivaldes_0-1788256584930.png - On an existing project, following the documented workaround (right-click project > SDKs > Attach/Detach > select all > OK > Apply), the SDK list only shows "FreeMASTER_S32K312" — the S32K3 RTD/PlatformSDK never appears as an option, even though it is confirmed installed  ivaldes_1-1788256618159.png - This happens identically in both 3.6.5 and 3.6.6, so it does not seem to be version-specific. - The only workaround I have found is copying an existing .mex file from one of the example projects into my project — I cannot generate one from scratch for a custom project. I checked the Eclipse workspace log during a fresh project-creation attempt and found these errors around the same timestamp: com.nxp.swtools.serdes.codegen (ERROR): "[TOOL] No script file found while trying to recompile the codegeneration script for SerDes Config Tool" com.nxp.swtools.periphs.model.data (ERROR, repeated ~11 times): "[DATA] You should not reference non-global component "freertos"! See attribute component_id of reference setting "general_tab"/"memory_tab"/etc. in component: freertos" I could not find any existing thread with these exact messages. Question: what determines whether an installed RTD/SDK shows up as attachable in the "SDKs > Attach/Detach" dialog and in the New Project wizard? Is there a way to force S32DS to re-register/re-index an installed RTD as an SDK, or a known cause for these two log errors? Attachments: 1. Installed Software screenshot (RTD confirmed installed) 2. SDKs > Attach/Detach dialog (only FreeMASTER_S32K312 listed) 3. New Project wizard, SDK selection step (empty/incomplete) Installed SDKs (from Help > About S32 Design Studio > Installation Details > Installed Software, filtered by "RTD"): ivaldes_2-1788256655963.png New Project Wizard - Project Management and Settings SDKs Re: I cannot get a .mex file generated for a brand new project in either S32DS version Hi @ivaldes  Could you let me know which toolchain you selected when creating the new application project? The RTDs for S32K3 devices are designed to work with GCC 10.2 BR, VaneB
View full article
[lx2080a][lx2160a] How do I turn off CPU cores? For the LX2080A We need to disable 4 out of the 8 cores. Could you please tell me how to turn off core for specific 4 of the 8 cores? For testing, I added the following to the rcw_2200_750_3200_19_5_2.rcw file, but it will not boot. .pbi write 0x01e00094, 0x00000f0 .end Is there anything else that needs to be modified? Re: [lx2080a][lx2160a] How do I turn off CPU cores? If the intent is to keep the first four LX2080A clusters active and disable the upper four active cores, use the physical-core bitmap: Copy # Disable physical cores 8, 10, 12, 14 .pbi write 0x01e00094, 0x00005500 .end Re: [lx2080a][lx2160a] How do I turn off CPU cores? We applied it. But it didn't boot. .pbi write 0x01e60060,0x0000000f write 0x01e00094,0x000000f0 .end So, with the version not applied, I read the registers from the uboot prompt as follows. It appears that the active core is an odd number. > md.l 0x01e00094 01e00094: 00000000 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@........... => md.l 0x01e60060 01e60060: 0000aaaa 00000000 00000000 00000000 ................ 01e60070: 00000000 00000000 00000000 00000000 ................ Could this be the cause? Thanks Re: [lx2080a][lx2160a] How do I turn off CPU cores? Your target register is correct for disabling cores, but I would not leave the change as only: .pbi write 0x01e00094, 0x00000f0 .end Use a full 32-bit value and make sure the boot/release path does not try to start the disabled cores: .pbi write 0x01e00094, 0x000000f0   /* COREDISR: disable cores 4,5,6,7 */ .end 0x01e00094 is DCFG + 0x94 ; the LX2160A/LX2080A RM lists DCFG base address = 0x1E0_0000 and COREDISR at offset 0x94 . COREDISR is the documented mechanism for disabling/clock-gating unused physical cores, and it can be programmed before system ready by PBI . Bits/fields for cores 4–7 correspond to Core 4 Disable through Core 7 Disable, so 0x000000f0 is the expected mask if you want to keep cores 0–3 and disable cores 4–7 . The important additional item is boot release. For an LX2/LS2 4-core case, the documented/internal guidance is to pair: Boot Release @ 0x01e60060 = 0x0000000f COREDISR     @ 0x01e00094 = 0x000000f0   /* disable Core7:4 */ so only cores 0–3 are released for boot, while cores 4–7 are disabled . The Boot Release Register BRRL is at RST base 0x1E6_0000 + 0x60 , and its bits CR0...CR15 release the corresponding cores from boot holdoff . Also verify that the primary boot core is not included in your COREDISR mask; the RM says the boot core can be identified through BRCORENBR[CORE_NBR] . Two practical checks for the boot failure: Use 0x000000f0 , not 0x00000f0 , to avoid any parser/tool ambiguity. If the RCW/PBI image uses a STOP-with-CRC command, rebuilding after changing PBI must update the PBI CRC; the CRC covers all PBI commands after the Load RCW command through the STOP-with-CRC command. After boot, confirm the result by reading COREDISR and the core-disable status register; an LX2 experiment used COREDISABLESR @ 0x01E00990 to confirm the disabled-core mask . Also note that cores disabled through COREDISR must not be re-enabled by software later . For “keep cores 0–3, disable cores 4–7,” use COREDISR = 0x000000f0 and make sure the boot-release mask releases only the active cores, e.g. BRRL = 0x0000000f ; otherwise firmware may try to start a core you have disabled. Re: [lx2080a][lx2160a] How do I turn off CPU cores? The core numbering in the LX2160A is sequential with respect to the cluster groups. The 16 cores are arranged in 8 clusters, with each cluster containing two cores. The numbering is as follows: Cores 0 and 1 are in Cluster 1 Cores 2 and 3 are in Cluster 2 ... and so on, up to Cores 14 and 15, which are in Cluster 8 Disabling all cores within a cluster causes system to hang. So it is impossible to achieve your purpose. Re: [lx2080a][lx2160a] How do I turn off CPU cores? Please try the following configuration. .pbi write 0x01e00094,0x0000aa00 write 0x01e60060,0x000000aa .end Re: [lx2080a][lx2160a] How do I turn off CPU cores? It seems that disabling all cores within a cluster causes system to hang. Let's only disable one core in one cluster. .pbi write 0x01e00094, 0x00008888 write 0x01e60060, 0x00002222 .end Re: [lx2080a][lx2160a] How do I turn off CPU cores? .pbi write 0x01e00094,0x00005500 write 0x01e60060,0x000000aa .end We applied it. However, it did not boot. Are there any other things to look into? Re: [lx2080a][lx2160a] How do I turn off CPU cores? It boots up, but the result is as follows. => md.l 0x01e00094 01e00094: 0000aa00 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@........... => md.l 0x01e60060 01e60060: 0000aaaa 00000000 00000000 00000000 ................ 01e60070: 00000000 00000000 00000000 00000000 ................ The kernel also detects 8 CPUs. Can you test this on the LX2080a? Thanks, Re: [lx2080a][lx2160a] How do I turn off CPU cores? The results seem to be the same. => md.l 0x01e00094 01e00094: 00008888 00000000 00000000 00000000 ................ 01e000a4: 87360220 00000040 00000000 00000000 .6.@........... => md.l 0x01e60060 01e60060: 0000aaaa 00000000 00000000 00000000 ................ 01e60070: 00000000 00000000 00000000 00000000 ................ Re: [lx2080a][lx2160a] How do I turn off CPU cores? The following settings seem correct. .pbi write 0x01e00094, 0x00005500 write 0x01e60060, 0x000000aa .end Regarding the value `0x0000aaaa` in the `0x01e60060` release register, I think that cores 1, 3, 5, 7, 9, 11, 13, and 15 are the disabled ones (indicated by 1), while cores 0, 2, 4, 6, 8, 10, 12, and 14 (indicated by 0) are the active cores actually supported by the LX2080A. there is one core connected to each of the eight clusters, four clusters must be disabled; this leaves four active cores—one in each of the remaining four clusters. but even after modifying `COREDISR`and `BRRL`, the `BRRL`and `COREDISABLESR` register continues to show `0x0000aaaa`. So, I checked the SoC initialization routine in `atf/nxp/soc-lx2160/soc.c`—where the cluster count was initially set to eight—and successfully booted the system after changing the cluster number to four. Currently, I have hardcoded the value to 4 within `get_num_cluster()`, but I hope that any other suggestions or feedback. => md.l 0x01e00094 01e00094: 00005500 00000000 00000000 00000000 .U.............. => md.l 0x01e60060 01e60060: 0000ffaa 00000000 00000000 00000000 ................ => md.l 0x01e00990 01e00990: 0000ffaa 00000000 00000000 00000000 ................ Thanks,
View full article
IW612でBlueZでLEオーディオを有効にする こんにちは、 私はIW612チップセットを搭載したFRDM i.MX93ボードを持っています。チップセットの日付表によると、LE Audioに対応しています。 私は、組み込みLinuxイメージ(現在はカーネル6.18-1のデフォルトのFRDM Yoctoイメージを使用しています)上でBlueZを使ったLEオーディオをテストしたいと考えています。 BlueZ側では、実験機能とカーネル実験機能にLE Audioを使えるようにしましたが、BlueZはチップセットのLE Audio機能を識別しています。 しかし、この機能はデフォルトでは有効になっておらず、LE AudioヘッドセットとペアリングしてもBAPのオーディオプロファイルが接続されません。 BlueZやLinuxでLE Audioを有効にするためのドキュメントはありますか? 前もって感謝します Re: Enable LE Audio with BlueZ on IW612 親愛なる@ammar_khallouf_95様、 お問い合わせありがとうございます。 はい、お客様向けのドキュメントがあります。リンクをご覧ください。 https://www.nxp.com/products/IW612 weidong_sun_0-1788306573110.png 文書名は UM12155:Bluetooth LE オーディオ このファイルは安全なファイルです。アクセス権がない場合は、以下の2つのステップに従って申請してください。 1. NXPと秘密保持契約(NDA)を締結する。 NXPのウェブサイト(www.nxp.com-->support-->support)からチケットを送信してください。チケットを入手したら、指示に従って完了させてください。 もしあなたの会社がすでにNXPとNDAを結んでいるなら、そのステップは無視してください。 2. 文書のアクセス権を申請する (1) 新しいチケットを提出し、NDA番号とアクセスしたい書類を教えてください。 (2) 私たちのチームメンバーである新しいケースオーナーは、NDA番号に基づいてプロダクトマネジメントチームからアクセス権を申請します。 よろしくお願いします! よろしくお願いいたします。 維東
View full article
S32K388 GMAC0 Eth_43_GMAC 驱动程序未收到 RX 中断 您好, 我使用的是以下配置: S32K388EVB-Q289 S32DS 3.6.8 RTD 7.0.1 我以提供的 Eth_InternalLoopback_S32K388 示例项目为基础,并对其进行了修改,使其可以通过媒体转换器从我的 PC 接收帧。我添加了示例 S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600中提到的 RTD 修复程序。我成功达到了断点 Eth_43_GMAC_Receive(EthConf_EthCtrlConfig_EthCtrlConfig_0, 0U, &Status); 并且能够检查以太网帧 EthIf_RxIndication(Eth_43_GMAC_apxInternalCfg[PartitionId]->Eth_43_GMAC_apCtrlConfig[CtrlIdx]->EthCtrlEthIfIdx, FrameType, IsBroadcast, MacSrcAddr, Payload, PayloadLength, IngressTimeTuplePtr, RxHandleId); 但是,当我添加了一个 while 1 循环,启用了 Rx 中断并将其链接到 GMAC0_CH0_RX_IRQHandler 时,我却无法在任何地方获得任何中断。我的项目文件附在下面。 James_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.pngJames_Zhang_SE_0-1788220964718.png S32K3汽车-RTD Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt 你好@James_Zhang_SE , 我查看了附件中的项目。要在 RTD7.0.1 中启用 RX IRQ,您需要更改 Ingress QueueHandlerFunction 并启用 QueueInterrupt: PavelL_0-1788263577590.pngPavelL_0-1788263577590.pngPavelL_0-1788263577590.png 更改之后,我在 GMAC_RxIRQHandler() 处触发了断点。在 Eth_43_GMAC_Receive()。 我还注意到您的 RGMII TXCLK 被定义为输入 -> 它应该是输出。 但是,要在 Wireshark 中查看您的 TX 帧,您需要相应地更改初始化序列。 例如,S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600 。因此,在您的项目中,它看起来像这样: PavelL_1-1788264277735.pngPavelL_1-1788264277735.pngPavelL_1-1788264277735.png 顺祝商祺! 帕维尔 Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt 你好,帕维尔, 非常感谢您的支持。按照您建议的修复方法操作后,GMAC 驱动程序现在可以正常工作了。 我还有几个问题,希望您能指导我: 是否有详细的文档描述了配置和使用 GMAC 驱动程序的完整步骤?我想先自己仔细阅读一下文档,以便在提出太多问题之前更好地了解驱动程序。 在EthIf_RxIndication() 函数内部,我需要调用吗? Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId); 在函数结束时释放接收缓冲区? GMAC提供了相当多的配置选项。是否有任何文档或参考资料解释每个配置参数的作用以及应该如何配置? 再次感谢您的帮助。我非常感谢您的支持。 Re: S32K388 GMAC0 Eth_43_GMAC driver not getting RX interrupt 你好@James_Zhang_SE , 感谢您分享最新情况。很高兴得知 GMAC 驱动程序现在对您有效。 关于您提出的其他问题: 1.配置和使用驱动程序的主要参考资料是 Eth_43_GMAC 用户手册,该手册包含在 RTD 安装包中,例如:C:\NXP\S32DS.3.6.6_RTD701\S32DS\software\PlatformSDK_S32K3\RTD\Eth_43_GMAC_TS_T40D34M70I1R0\doc\RTD_ETH_43_GMAC_UM.pdf 我还建议查阅保存在同一目录下的相应 Eth_43_GMAC 集成手册 (RTD_ETH_43_GMAC_IM.pdf) 以及可用的 GMAC 示例项目。   2. 是否必须调用 Eth_43_GMAC_ReleaseRxBuffer() 取决于 EthCtrlReleaseResourceAfterReception 配置参数。 PavelL_0-1789024403441.png 如果启用接收后自动释放,驱动程序会在 EthIf_RxIndication() 返回后释放 RX 资源,您不应该显式地释放它。 如果禁用自动释放,则在 EthIf_RxIndication() 返回后,接收缓冲区仍保持分配状态。在这种情况下,应用程序最终必须调用: Eth_43_GMAC_ReleaseRxBuffer(CtrlIdx, RxHandleId);   当应用程序需要保留接收到的数据以进行进一步处理时,此模式非常有用。但是,应用程序使用完毕后,必须释放缓冲区。否则,可用的接收缓冲区最终会耗尽。 另请注意,在相应的缓冲区释放后,不应再使用接收到的有效载荷指针。 3. Eth_43_GMAC 用户手册也是各个配置参数的主要参考资料。此外,S32 配置工具在选择或将鼠标悬停在相应设置上时,会显示许多参数的描述。有关硬件级行为,例如 MAC 过滤、DMA 操作、MTL 队列、时间戳和中断状态,请参阅 S32K3 参考手册的 GMAC/EMAC 章节。 作为实际的起点,我建议参考 RTD 软件包提供的 GMAC 示例。页面上还有一些功能性的 lwIP 示例: https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-Examples/ta-p/1108990 如果您发现任何问题,请随时寻求帮助。建议每个主题单独开一个帖子。这有助于我们清晰地了解案例,以便其他用户使用。 顺祝商祺! 帕维尔
View full article
Enable LE Audio with BlueZ on IW612 Hi, I have the FRDM i.MX93 board with IW612 chipset. According the chipset datsheet it supports LE Audio. I am interested in testing LE Audio with BlueZ running on embedded linux image (currently using the default FRDM Yocto image with kernel 6.18-1) On BlueZ side I have enabled the experimental and kernel experimental features to use LE Audio and I see that BlueZ identifes the LE Audio capabilities of the chipset. However, the feature does not seem to be enabled by default and when I pair with a LE Audio headset I do not get the BAP audio profiles connected. is there a documentation for enabling LE Audio with BlueZ/Linux ? Thanks in advance Re: Enable LE Audio with BlueZ on IW612 Dear @ammar_khallouf_95 , Thanks for the inquiry. Yes, we have a document for customer , see the link, please. https://www.nxp.com/products/IW612 weidong_sun_0-1788306573110.png The document name is  UM12155: Bluetooth LE Audio it is secure file, if you don't have rights to access it, please follow these 2 steps to apply for it. 1. Sign NDA with NXP. Submit a ticket through nxp website, www.nxp.com-->support-->support tickets, then follow guidance to finish it. If your company has already have NDA with NXP, ignore the step, please. 2.  Apply for the access rights for the document (1) Submit a new ticket, tell us your NDA number and the document you want to access. (2) Our team member, your new case owner will apply for the access rights from product management team according to your NDA number. Thanks! Regards, Weidong
View full article
S32 Design Studio for ARM v2.2 License Expired Request Extension Hello, my S32DS license has expired. Activation Code: 04E9-8F5A-8B1F-F9C8 Product Version: S32 Design Studio for ARM v2.2] Please extend the license. Thank you. Re: S32 Design Studio for ARM v2.2 License Expired Request Extension Hi,  your S32DS license has been extended. Please activate S32DS again with your old code
View full article
S32 Design Studio for ARM v2.2 许可证已过期,申请延期 你好, 我的S32DS许可证已过期。 激活码:04E9-8F5A-8B1F-F9C8 产品版本:S32 Design Studio for ARM v2.2] 请延长许可证期限。谢谢。 Re: S32 Design Studio for ARM v2.2 License Expired Request Extension 你好, 您的S32DS许可证已延期。请使用您之前的代码重新激活 S32DS。
View full article
S32 Design Studio for ARM v2.2 ライセンス期限切れのリクエスト延長 こんにちは、 私のS32DSライセンスの有効期限が切れました。 アクティベーションコード:04E9-8F5A-8B1F-F9C8 製品バージョン:Arm v2.2用S32 Design Studio] ライセンス期間を延長してください。ありがとう。 Re: S32 Design Studio for ARM v2.2 License Expired Request Extension こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
.mexファイルが手に入りませんS32DS バージョンの新規プロジェクト用に生成されたファイル 基板:FRDM-A-S32K312(S32K312MINI-EVB) S32DSのバージョンを並行してインストールしました:#S32DesignStudio 3.6.5と3.6.6(C:\NXP\S32DS.3.6.5 および C:\NXP\S32DS.3.6.6) RTDインストール: S32K3 RTD、バージョン7.0.0.202601301531(インストール詳細>>インストールソフトウェアについてヘルプ>で確認済み、スクリーンショット添付 — 全リストはこの投稿の最後に掲載 AWS-LIBRARIES-S32K3  オートモーティブRTD  問題: S32K3のRTD/SDKは、新規プロジェクトを作成しても、既存のプロジェクトにアタッチしようとしても、アタッチ可能として表示されません。その結果、.mexファイルは入手できませんいずれにせよ、既存の.mexをコピーした場合のみ生成されるファイルあるサンプルプロジェクトから別のプロジェクトへ移行する。 - New > S32DS Application Project でプロジェクトを作成する際、.mex ファイルは正常に完了しますが、.mex ファイルは発生しませんファイルは生成されたプロジェクト内で作成されます(SDK選択ステップにはRTDはありません)。 ivaldes_0-1788256584930.png - 既存プロジェクトの場合、ドキュメント化された回避策(プロジェクト> SDKs>アタッチ/デタッチ>「すべての>OK > 適用」を選択すると、SDKリストには「FreeMASTER_S32K312」だけが表示され、S32K3 RTD/PlatformSDKはインストールが確認されているにもかかわらずオプションとして表示されません ivaldes_1-1788256618159.png - これは3.6.5と3.6.6の両方で全く同じように発生します。したがって、バージョン固有のものではないようです。 - 私が見つけた唯一の回避策は、既存の.mexファイルをコピーすることです。サンプルプロジェクトの一つから自分のプロジェクトにファイルを入れることはできません — カスタムプロジェクト用に一から生成することはできません。 新規プロジェクト作成時にEclipseワークスペースのログを確認したところ、ほぼ同じタイムスタンプで以下のエラーが見つかりました。 com.nxp.swtools.serdes.codegen (エラー): "[ツール] SerDes Config Tool のコード生成スクリプトを再コンパイルしようとした際に、スクリプトファイルが見つかりませんでした" com.nxp.swtools.periphs.model.data (ERROR、繰り返し~11回): 「[データ] 非グローバルコンポーネント「freertos」を参照すべきではありません!参照設定の属性component_id「general_tab」/「memory_tab」などをコンポーネント:freertosで参照してください。 これらの正確なメッセージが載った既存のスレッドは見つかりませんでした。 質問:インストールされたRTD/SDKが「SDKs > アタッチ/デタッチ」ダイアログや新規プロジェクトウィザードでアタッチ可能として表示されるかどうかは何が決定しますか?インストール済みRTDをSDKとしてS32DSに再登録・再インデックスさせる方法はありますか?また、これら2つのログエラーの既知の原因はありますか? 添付資料: 1. インストール済みソフトウェアのスクリーンショット(RTDがインストール確認済み) 2. SDKs>アタッチ/デタッチダイアログ(リストFreeMASTER_S32K312のみ) 3. 新しいプロジェクトウィザード、SDK選択ステップ(空/未完了) インストール済みSDKs(ヘルプ> About S32 Design Studio>インストール詳細>インストールソフトウェア、「RTD」でフィルタリング済み): ivaldes_2-1788256655963.png 新規プロジェクト・ウィザード ― プロジェクト管理と設定 SDK Re: I cannot get a .mex file generated for a brand new project in either S32DS version こんにちは、 @ivaldes さん 新しいアプリケーションプロジェクトを作成する際にどのツールチェーンを選んだのか教えていただけますか?S32K3デバイス用のRTDはGCC 10.2で動作するように設計されています。 BR、VaneB
View full article
MX95 M7 safety functional Hi, Regarding the functional safety of i.MX95, I noticed that there is a safety manual available, but it requires an NDA. Could I know what content is in this document? How do I sign an NDA? Additionally, does the i.MX95 M7 core support the Safety Software Framework (SAF)? As far as I know, this feature is available for the S32 series. I would like to check if it is also supported on the i.MX95. Regarding SAF framework, my understanding is that it provides APIs for users to monitor the current SoC health status (such as memory ECC, CPU voltage, or unresponsive GPIOs...etc). Is my understanding correct? Please kindly clarify if there is any misunderstanding. Re: MX95 M7 safety functional @yipingwang  Thank you for the information. Re: MX95 M7 safety functional 1. The i.MX95 Safety Manual is indeed an NDA-protected document. You could sing a new NDA from https://www.nxp.com/webapp-signup/ndaReqForm Once the NDA is in place, the document can be shared with you. The safety manual typically covers topics such as safety architecture, safety mechanisms, failure mode analysis, and guidance for achieving functional safety certifications (e.g., IEC 61508 / ISO 26262). 2. Yes. The i.MX95 functional safety solution includes SAF, and the Cortex-M7 safety execution environment is designed to run safety applications using SAF services. The Cortex-M33 acts as the primary safety processor running SysMgr and SAF infrastructure, while the Cortex-M7 serves as the auxiliary safety processor for executing the safety application and optional SAF services. 3. Your description is largely correct — SAF provides APIs to monitor SoC health, including features like memory ECC monitoring, voltage supervision, and GPIO diagnostics, among others. SAF is a safety middleware/framework that sits between the application and the underlying safety mechanisms of the SoC. It helps collect diagnostic results, manage fault events, execute safety checks, and coordinate the system reaction when a fault is detected. Re: MX95 M7 safety functional Can anyone help?
View full article