Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
Can an eMMC connected to USDHC1 be used as a boot device? Hello, I am checking the Boot ROM behavior of the i.MX 8DualX/8DualXPlus/8QuadXPlus family. According to the reference manual, the recommended boot connections appear to be: eMMC on USDHC0 SD/eSD/SDXC on USDHC1 However, in Figure 5-17, “Expansion device (SD/eSD/SDXC) boot flow”, when SD initialization fails, the flow continues through connector 2 to the MMC initialization flow in Figure 5-16. It appears that the ROM tries the MMC protocol on the same USDHC interface after the SD protocol fails. Does this mean that an eMMC connected to USDHC1 can be detected and used as a Boot ROM boot device, possibly in 4-bit mode? Or is this MMC fallback path intended only for protocol detection, while eMMC boot from USDHC1 is not officially supported? I would also like to confirm whether the ROM switches from USDHC1 to USDHC0 at this point, or whether it continues using the same USDHC1 interface. Thank you. Re: Can an eMMC connected to USDHC1 be used as a boot device? I am trying to understand the boot flow of the i.MX 8DualX/8DualXPlus/8QuadXPlus Boot ROM, especially for SD boot. My current understanding is as follows. After Primary and Secondary Boot fail, the ROM may enter SD/MMC Manufacture Mode, which is described as Recovery Boot. In this mode: The ROM scans SD or MMC devices on USDHC1. A 1-bit data bus is used, regardless of the normal bus-width eFuse setting. If a valid boot image is found, it is loaded and executed. If an eMMC device is connected to USDHC1 and BOOT_MODE[3:0] is set to 0011 (SD boot through USDHC1), is the expected boot sequence as follows? The ROM first attempts the normal Primary Boot using the SD boot flow, but it fails. The ROM then attempts Secondary Boot, which also fails. The ROM enters the SD/MMC Manufacture Mode (Recovery Boot), detects the eMMC device on USDHC1 using the MMC protocol, and successfully boots from it. In other words, with this hardware configuration, would the system be able to boot from the eMMC only during the Recovery/Manufacture Boot stage, rather than during the normal Primary or Secondary Boot stages? Re: Can an eMMC connected to USDHC1 be used as a boot device? Hello, eMMC on USDHC1 cannot be treated as a boot device, the documented primary mapping is eMMC on USDHC0, SD on USDHC1. The USDHC1 fallback/recovery behavior is used by SD/MMC manufacture mode. You can take a look in section 5.11 of reference manual. Best regards. Re: Can an eMMC connected to USDHC1 be used as a boot device? Hello, Yes, your understanding is correct. Please consider that SD/MMC Manufacture Mode will be used "as default boot" with that considered configuration and you will lose this option to recover the device. Best regards.
記事全体を表示
The S32K148 has secure boot functionality, but the bootloader fails to start after JTAG is disabled. Dear NXP, hello: Our company's K148 has two partitions: a bootloader and an application partition. The application partition has a function to disable JTAG. When JTAG is disabled in the application, the bootloader fails to start after a reset, causing the chip to become bricked. Investigation revealed that the bootloader is 32KB, ranging from 0x00 to 0x8000. Disabling JTAG involved writing 0xFFu , 0xFFu , 0xFFu , 0xFFu , 0xFCu, 0x7Fu , 0xFFu , 0xFFu at address 0x408 , causing a change in the flash content. After a reset, the CSEc calculates a different boot_mac value for the bootloader, resulting in the bricking. Does NXP have any mature solutions to resolve this issue? Thank you. Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 K148的key槽.png Hi, @lukaszadrapa According to the manual above, BOOT_MAC is a one-time, irreversible write. Is there an official API that allows changing its value? If so, could you provide this API? Re: 晶振波形异常 Using your company's FS32K144HFT0MLHT MC IMG_20260718_141710.jpg The crystal oscillator is an 8MHz passive crystal oscillator (AV08000009), and the waveform is abnormal. Is this waveform acceptable for your company's MCU, and will it affect normal operation? Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 Hi @vurtual  The common approach is to disable the debug interface during manufacturing, rather than later from the application. In that case, the process can be done in a single production step: reprogram the Flash Configuration Field (FCF) to disable the debug port and then provision the correct BOOT_MAC value (or allow the CSEc to calculate it automatically after the next reset). If you need to disable the debug interface later in the product lifecycle, that is also possible. However, once the FCF is reprogrammed, the BOOT_MAC must be updated as well, since the secure boot calculation includes the modified FCF contents. Otherwise, the secure boot verification will fail. The BOOT_MAC can be updated using the standard SHE memory update protocol, in the same way that CSEc keys are updated. After updating the BOOT_MAC to match the new FCF contents, secure boot should operate correctly with the debug port disabled. Regards, Lukas Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 Hi @vurtual  Where do you see that this is an irreversible operation? That is not correct. BOOT_MAC can be updated.  As I mentioned previously: "The BOOT_MAC can be updated using the standard SHE memory update protocol, in the same way that CSEc keys are updated." This means you can use the CMD_LOAD_KEY command, which is the same command used to import and update regular SHE/CSEc keys. To update BOOT_MAC, you need to generate the M1–M5 values according to the standard SHE key update procedure. The key counter must be incremented, and the update can be authorized using either the MASTER_ECU_KEY or the BOOT_MAC_KEY. Therefore, updating BOOT_MAC is a supported operation and is not irreversible. Regards, Lukas Re: 晶振波形异常 Hello,@ lukaszadrapa Our company uses your FS32K144HFT0MLHT MCU with an 8MHz passive crystal oscillator (AV08000009), and the waveform is abnormal. Is this crystal oscillator waveform acceptable for your MCU? Will it affect the normal operation of the MCU? Thank you. IMG_20260718_141710.jpg Re: 晶振波形异常 Please create new thread for this. Thank you.  Re: 晶振波形异常 OK ,Thank you.
記事全体を表示
CodeWarrior 许可证问题 我们在旧版产品上使用 CodeWarrior 10.6,现在需要将其安装到新电脑上。我找不到 CodeWarrior 10.6 的离线安装包,在线安装也失败了(缺少下载站点)。 我可以找到 10.7 版本的下载。我们拥有 10.6 的永久浮动许可证。这些软件还能在 10.7 系统下运行吗?或者有人能提供一个 10.6 系统的离线安装包吗? 谢谢!
記事全体を表示
AUTOSAR MCAL MPC5744P 您好,请问是否有免费的编译器选项可以用来构建适用于 MPC5744P 的 AUTOSAR MCAL 应用程序? Re: AUTOSAR MCAL MPC5744P 你好, 对于用于 MPC5744P 的旧版 AUTOSAR MCAL 软件包(MPC574xP MCAL 4.x),官方验证的工具链通常是: Wind River Diab Compiler(最常见的资格) 绿山编译器 (GHS) 实际上,MPC5744P AUTOSAR MCAL 没有官方支持的免费编译器。 虽然 MPC5744P 生态系统通过 S32 Design Studio for Power Architecture 支持 GCC 进行通用嵌入式开发,但 MCAL 软件包本身主要是使用 Diab 和 GHS 开发和验证的。 DEVKIT-MPC5744P 信息列出了 GCC(通过 S32DS)、GHS、Cosmic 和其他用于 MPC5744P 开发的通用工具链,但这并不意味着 AUTOSAR MCAL 版本适用于 GCC。 已验证编译器的列表始终包含在 MCAL 软件包的发行说明中。 此致, 彼得
記事全体を表示
UG10215 将 imx708 列为支持的内核驱动程序——应该使用哪个内核驱动程序? 您好, 我正在按照 UG10215(i.MX 95 摄像头移植指南)将 Raspberry Pi Sony IMX708 摄像头集成到基于 i.MX 95 的板上。 文档中的“支持的相机传感器模块列表”表格将 Raspberry Pi Sony imx708 列为支持的参考相机模块。但是,我在linux-imx仓库( lf-6.18.y分支)中找不到对应的驱动程序(例如imx708.c)。😞 https://github.com/nxp-imx/linux-imx/commits/lf-6.18.y/drivers/media/i2c 请问i.MX 95上的imx708传感器应该使用哪个内核驱动程序?IMX708 驱动程序是否包含在公开的 BSP 中? 先行致谢。 Re: UG10215 lists imx708 as supported — which kernel driver should be used? 你好, 我们的标准 电路板支持包 中尚未正式支持此功能,您可以从树莓派源代码中获取驱动程序并使用它: https://github.com/raspberrypi/linux/blob/rpi-6.12.y/drivers/media/i2c/imx708.c 此致敬礼/Saludos, 阿尔多。 Re: UG10215 lists imx708 as supported — which kernel driver should be used? 嗨,阿尔多, 感谢您的回复。 我们的标准 BSP 尚未正式支持此功能。 未来还会支持吗?如果标准 电路板支持包 中不包含对 IMX708 摄像头的支持,为什么 UG10215 中会列出 IMX708 摄像头? 再次感谢 迭戈 Re: UG10215 lists imx708 as supported — which kernel driver should be used? 你好, 是的,我们计划添加此功能,但遗憾的是,我目前无法确定何时会将其添加到标准 电路板支持包 版本中。 它出现在指南中的原因是,它是早期开发阶段测试过的相机之一,但我们的 BSP 并未完全支持它。 此致敬礼/Saludos, 阿尔多。
記事全体を表示
射频功率放大器设计 - MRF13750H 你好!我正在使用 MRF13750H 设计一个 805 MHz 的射频功率放大器,我的设计基于数据手册中的 915 MHz 参考电路。但是,我只能使用 Usimmics 来模拟匹配网络;我无法使用 NXP 用来打开其设计文件的软件。 因此,为了设计匹配网络,我请求 NXP 提供 MRF13750H 915 MHz 参考电路的完整原理图,包括微带线尺寸,因为数据手册中没有提供此信息。如果可能的话,我还想请求提供 805 MHz 的大信号模型阻抗;否则,我将根据 915 MHz 提供的值进行设计。915MHz 参考电路和数据手册附在下方。 另一方面,如果有人知道在 805 MHz 频率下设计匹配网络的其他方法,我将不胜感激。
記事全体を表示
AUTOSAR MCAL MPC5744P Hello, is there any free compiler option to build the AUTOSAR MCAL applications for MPC5744P? Re: AUTOSAR MCAL MPC5744P Hello, For the legacy AUTOSAR MCAL package for MPC5744P (MPC574xP MCAL 4.x), the officially validated toolchains are typically: Wind River Diab Compiler (most commonly qualified) Green Hills Compiler (GHS) In practice, no officially supported free compiler is provided for MPC5744P AUTOSAR MCAL. Although the MPC5744P ecosystem supports GCC through S32 Design Studio for Power Architecture for general embedded development, the MCAL package itself was developed and validated primarily with Diab and GHS. The DEVKIT-MPC5744P information lists GCC (via S32DS), GHS, Cosmic, and other toolchains for MPC5744P development in general, but that does not mean the AUTOSAR MCAL release is qualified for GCC. List of validated compilers is always in release notes supplied with MCAL package. Best regards, Peter
記事全体を表示
RFパワーアンプ設計 - MRF13750H こんにちは!私はこのMRF13750Hを使って805 MHzのRFパワーアンプを設計しており、その設計はデータシートにある915 MHzの基準回路に基づいています。しかし、私はUsimmicsしか対応できないネットワークのシミュレートに使えます。NXPがデザインファイルを開くために使っているソフトウェアにはアクセスできません。 したがって、マッチングネットワークの設計にあたり、データシートには記載されていないマイクロストリップライン寸法を含むMRF13750H 915 MHz参照回路の完全な回路図をNXPに依頼しています。可能であれば、805 MHzの大信号モデルのインピーダンスもお願いしたいです。それ以外の場合は、915 MHzの値に基づいて設計します。915MHzにおける基準回路とデータシートを以下に添付します。 一方で、805MHzでのマッチングネットワーク設計の別の方法を知っている方がいれば、ぜひご意見をいただけるとありがたいです。
記事全体を表示
S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 亲爱的NXP,你好:         我们公司K148上有一个bootloader和app两个分区,在app里面有关闭jtag的功能,当在app中把jtag关了之后reset后bootloader起不来导致芯片变砖。经调查,bootloader有32K,从0x00到0x8000,关闭jtag是在0x408地址处写入了0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFCu, 0x7Fu, 0xFFu, 0xFFu,导致flash内容变化,reset后CSEc计算bootloader的boot_mac的值和原先的不一致导致变砖。请问NXP官方有没有什么成熟的方案来解决此问题?谢谢。 Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 K148的key槽.png  Hi,@lukaszadrapa  根据上面的手册,BOOT_MAC是一次性不可逆写入的。还是说有官方专门的API能变更它的值?如果是 ,能提供这个API接口吗? Re: 晶振波形异常 使用贵公司的FS32K144HFT0MLHT这款MC, IMG_20260718_141710.jpg 晶振为AV08000009这款8MHz的无源晶振,波形异常。请问这样的晶振波形 贵公司的MCU可以接受吗 是否会影响正常使用 Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 嗨@vurtual 通常的做法是在生产过程中禁用调试接口,而不是之后在应用程序中禁用。在这种情况下,该过程可以在一个生产步骤中完成:重新编程 Flash 配置字段 (FCF) 以禁用调试端口,然后配置正确的 BOOT_MAC 值(或者允许 CSEc 在下次 RESET 后自动计算该值)。 如果在产品生命周期的后期需要禁用调试接口,也是可以的。但是,一旦 FCF 被重新编程,BOOT_MAC 也必须更新,因为安全启动计算包括修改后的 FCF 内容。否则,安全启动验证将失败。 BOOT_MAC 可以使用标准的 SHE 内存更新协议进行更新,就像 CSEc 密钥的更新方式一样。在将 BOOT_MAC 更新为与新的 FCF 内容匹配后,禁用调试端口后,安全启动应该可以正常工作。 问候, 卢卡斯 Re: 晶振波形异常 你好,@ lukaszadrapa 我们公司使用贵公司的FS32K144HFT0MLHT这款MCU, 配合晶振为AV08000009这款8MHz的无源晶振,波形异常。请问这样的晶振波形,贵公司的MCU可以接受吗,是否会影响MCU的正常使用,谢谢 IMG_20260718_141710.jpg Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 嗨@vurtual 你从哪里看出这是一项不可逆的操作?那不正确。BOOT_MAC 可以更新。 正如我之前提到的: “BOOT_MAC 可以使用标准的 SHE 内存更新协议进行更新,就像 CSEc 密钥的更新方式一样。” 这意味着您可以使用 CMD_LOAD_KEY 命令,该命令与用于导入和更新常规 SHE/CSEc 密钥的命令相同。 要更新 BOOT_MAC,您需要按照标准 SHE 密钥更新程序生成 M1–M5 值。密钥计数器必须递增,并且可以使用 MASTER_ECU_KEY 或 BOOT_MAC_KEY 授权更新。 因此,更新 BOOT_MAC 是受支持的操作,并且不是不可逆的。 此致, Lukas Re: 晶振波形异常 请为此另开一个帖子。谢谢。 Re: 晶振波形异常 好的,谢谢。
記事全体を表示
UG10215 lists imx708 as supported — which kernel driver should be used? Hi, I'm working on integrating a Raspberry Pi Sony IMX708 camera on an i.MX 95 based board, following UG10215 (i.MX 95 Camera Porting Guide). The document's "List of camera sensors modules supported" table lists the Raspberry Pi Sony imx708 as a supported reference camera module. However, I couldn't find a corresponding driver (e.g. imx708.c) in the linux-imx repository (branch lf-6.18.y😞 https://github.com/nxp-imx/linux-imx/commits/lf-6.18.y/drivers/media/i2c Could you clarify which kernel driver is expected to be used for the imx708 sensor on the i.MX 95? Is the IMX708 driver included in the public BSP? Thanks in advance. Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hello, We do not have it officially supported yet in our standard BSP, you can take the driver from raspberry sources and use it: https://github.com/raspberrypi/linux/blob/rpi-6.12.y/drivers/media/i2c/imx708.c Best regards/Saludos, Aldo. Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hi Aldo, thanks for your reply. We do not have it officially supported yet in our standard BSP Will it be supported in the future? Why is the IMX708 camera listed in UG10215 if support is not included in the standard BSP? Thanks again Diego Re: UG10215 lists imx708 as supported — which kernel driver should be used? Hello, Yes it is planned to be added but, unfortunately, I do not have a due date/version when its going to be added to the standard BSP release. The reason that it appears in the guide is because is one of the cameras that was tested in early development but was not fully supported in our BSP. Best regards/Saludos, Aldo.
記事全体を表示
PCF8563TS 生命周期状态和长期供货情况 你好呀.... 我们目前在我们的一款产品中使用了PCF8563TS RTC,并希望更好地了解其长期生命周期状况。 过去,我们的产品是基于PCF8563BS的,但该芯片最终已达到生命周期结束 (EOL)。因此,我们不得不进行完整的硬件重新设计,以迁移到另一个封装,这产生了额外的工程工作量、验证和制造成本。 鉴于以往的经验,我们想问: 是否有任何迹象表明PCF8563TS即将停产或处于 NRND 状态? 这款设备是否有长期供货计划? NXP能否分享一些关于其预期产品生命周期或路线图的信息? 对于围绕 PCF8563TS 设计新产品的客户,有什么建议吗? 我们理解未来的计划可能会有所改变,但任何关于该设备预期寿命的指导都将有助于我们做出明智的设计决策,并降低未来重新设计的风险。 感谢您的支持。 Re: PCF8563TS Lifecycle Status and Long-Term Availability 我做了一些调查,对于像 PCF8563TS $0.5 这样的芯片,由于存货很大,停止生产并不容易。 Re: PCF8563TS Lifecycle Status and Long-Term Availability 你好,维克多, 感谢您对恩智浦半导体产品的关注,也感谢您给我们提供支持的机会。 我们拥有长期供应计划下的产品,可确保未来 10-15 年的稳定供应。 长寿计划 然而, PCF8563TS 不属于产品延保计划,因此没有停产通知或最后购买日期。具体情况将取决于客户需求。 Alondra_0-1784582617358.png 此致, 阿隆德拉 技术支援 恩智浦半导体
記事全体を表示
UG10215はIMX708をサポートしていると記載されていますが、どのカーネルドライバーを使うべきでしょうか? こんにちは、 私はUG10215(i.MX 95カメラ移植ガイド)に従って、Raspberry PiのSony IMX708カメラをi.MX 95ベースのボードに統合する作業に取り組んでいます。 ドキュメントの「サポートされているカメラセンサーモジュール一覧」の表には、サポートされたリファレンスカメラモジュールとしてRaspberry Pi Sony imx708が記載されています。しかし、linux-imxリポジトリ(lf-6.18.yのブランチ )で対応するドライバー(例:imx708.c)が見つかりませんでした😞 https://github.com/nxp-imx/linux-imx/commits/lf-6.18.y/drivers/media/i2c i.MX 95のIMX708センサにどのカーネルドライバが使われる予定か、詳しく教えていただけますか?IMX708ドライバは公開BSPに含まれていますか? よろしくお願いいたします。 Re: UG10215 lists imx708 as supported — which kernel driver should be used? こんにちは、 標準BSPではまだ公式にサポートされていません。Raspberryソースからドライバーを使ってください: https://github.com/raspberrypi/linux/blob/rpi-6.12.y/drivers/media/i2c/imx708.c よろしくお願いいたします。 アルド。 Re: UG10215 lists imx708 as supported — which kernel driver should be used? こんにちは、アルドさん。 ご返信ありがとうございます。 弊社の標準BSPではまだ正式にサポートされていません。 将来的にサポートされるのでしょうか?標準BSPにサポートが含まれていないのに、なぜIMX708カメラがUG10215に記載されているのでしょうか? 再度、感謝します ディエゴ Re: UG10215 lists imx708 as supported — which kernel driver should be used? こんにちは、 はい、追加する予定ですが、残念ながら、標準のBSPリリースに追加される時期やバージョンはまだ決まっていません。 このカメラがガイドに掲載されている理由は、開発初期段階でテストされたものの、当社のBSPでは完全にはサポートされていなかったカメラの1つだからです。 よろしくお願いいたします。 アルド。
記事全体を表示
PCF8563TS Lifecycle Status and Long-Term Availability Hello there.... We are currently using the PCF8563TS RTC in one of our products and would like to better understand its long-term lifecycle status. In the past, our product was based on the PCF8563BS, which eventually reached End of Life (EOL). As a consequence, we had to perform a complete hardware redesign to migrate to another package, generating additional engineering effort, validation, and manufacturing costs. Considering this previous experience, we would like to ask: Is there any indication that the PCF8563TS is approaching EOL or NRND status? Is there a long-term availability plan for this device? Can NXP share any information regarding its expected product lifecycle or roadmap? Are there any recommendations for customers designing new products around the PCF8563TS? We understand that future plans may be subject to change, but any guidance regarding the expected longevity of this device would help us make informed design decisions and reduce future redesign risks. Thank you for your support. Re: PCF8563TS Lifecycle Status and Long-Term Availability I did some research, and for chips like the PCF8563TS $0.5, which have a large inventory, it's not so easy to stop production. Re: PCF8563TS Lifecycle Status and Long-Term Availability Hello Victor,  Thank you for your interest in NXP Semiconductors products and for the opportunity to support you. We have products under longevity program which ensures a stable supply for the next 10-15 years.  Longevity program  However PCF8563TS is not part of the longevity program there is no discontinuation notice or last purchase date. Will depend on customer's demands Alondra_0-1784582617358.png Best regards, Alondra Technical Support NXP Semiconductors
記事全体を表示
S32K148はセキュアブート機能を備えているが、JTAGを無効にするとブートローダーが起動しない。 NXP様、こんにちは。 弊社のK148には、ブートローダーとアプリケーションパーティションの2つのパーティションがあります。アプリケーションパーティションには、JTAGを無効にする機能があります。アプリケーションでJTAGを無効にすると、リセット後にブートローダーが起動せず、チップが動作不能になります。調査の結果、ブートローダーは32KBで、アドレス0x00から0x8000の範囲であることが判明しました。JTAGを無効にするには、アドレス0x408に0xFFu 、0xFFu 、 0xFFu 、 0xFFu 、 0xFCu 、 0x7Fu 、 0xFFu 、 0xFFuを書き込む必要があり、これによりフラッシュメモリの内容が変更されます。リセット後、CSEcがブートローダーに対して異なるboot_mac値を計算してしまうため、チップが動作不能になります。NXPは、この問題を解決するための成熟したソリューションを提供していますでしょうか?よろしくお願いいたします。 Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 K148的key槽.png こんにちは、 @lukaszadrapa 上記のマニュアルによると、 BOOT_MACは一度だけ書き込まれる不可逆的な値です。この値を変更できる公式APIはありますか?もしあれば、そのAPIを提供していただけますか? Re: 晶振波形异常 御社のFS32K144HFT0MLHT MCを使用しています IMG_20260718_141710.jpg水晶発振器は8MHzの受動型水晶発振器(AV08000009)ですが、波形が異常です。この波形は貴社製MCUにとって許容範囲内でしょうか?また、正常な動作に影響はありますか? Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 こんにちは@vurtual 一般的な方法は、デバッグインターフェースを製造時に無効にすることであり、アプリケーションから後から無効化するのではなく、その場合、このプロセスは単一の生産ステップで完了します:フラッシュ構成フィールド(FCF)を再プログラムしてデバッグポートを無効化し、正しいBOOT_MAC値をプロビジョニングするか(または次のリセット後にCSEcが自動的に計算できるようにします)。 製品ライフサイクルの後半でデバッグインターフェースを無効化する必要がある場合も可能です。しかし、FCFが再プログラムされると、セキュアブートの計算には変更されたFCFの内容が含まれるため、BOOT_MACも更新する必要があります。そうしないと、セキュアブートの検証が失敗します。 BOOT_MACは標準的なSHEメモリ更新プロトコルを用いて更新可能で、CSEcキーの更新と同じ方法で行えます。BOOT_MACを新しいFCFの内容に合わせて更新した後、デバッグポートを無効にした状態でセキュアブートが正しく動作するはずです。 よろしくお願いいたします。 ルーカス Re: 晶振波形异常 この件のために新しいThreadを作成してください。ありがとう。 Re: 晶振波形异常 こんにちは、@ ルカシャドラパ 弊社では、貴社製FS32K144HFT0MLHTマイコンを8MHzのパッシブ水晶発振器(AV08000009)と組み合わせて使用していますが、波形が異常です。この水晶発振器の波形は貴社製マイコンにとって許容範囲内でしょうか?また、マイコンの正常な動作に影響はありますか?よろしくお願いいたします。 IMG_20260718_141710.jpg Re: S32K148有secureboot功能,但是bootloader在jtag关闭后起不来 こんにちは@vurtual これが不可逆的な操作であると、あなたはどこにお考えですか?それは正しくありません。BOOT_MAC更新可能です。 以前にも述べたように: 「BOOT_MACは標準的なSHEメモリ更新プロトコルで更新できます。CSEcキーの更新と同じ方法です。」 つまり、通常のSHE/CSEcキーのインポートや更新に使われるCMD_LOAD_KEYコマンドを使えます。 BOOT_MACを更新するには、標準のSHEキー更新手順に従ってM1~M5の値を生成する必要があります。キーカウンターは増分されなければならず、更新はMASTER_ECU_KEYまたはBOOT_MAC_KEYのいずれかで承認できます。 したがって、BOOT_MACの更新はサポートされている操作であり、元に戻せない操作ではありません。 よろしくお願いいたします。 ルーカス Re: 晶振波形异常 はい、ありがとうございます。
記事全体を表示
PCF8563TSのライフサイクル状況と長期的な供給状況 こんにちは.... 現在、 PCF8563TS RTCを製品の一つに使用しており、その長期的なライフサイクル状況をよりよく理解したいと考えています。 過去には、私たちの製品は PCF8563BSをベースにしており、最終的にはエンド・オブ・ライフ(EOL)に達しました。その結果、別のパッケージへの移行のためにハードウェアの全面的な再設計を行い、追加のエンジニアリング作業、検証、製造コストが発生しました。 こうした過去の経験を踏まえ、私たちは以下の点について質問したいと思います。 PCF8563TSがEOL(販売終了)またはNRND(新製品化)に近づいている兆候はありますか? このデバイスの長期的な供給計画はありますか? NXPは今後の製品ライフサイクルやロードマップについて何かCAN情報を共有できますか? PCF8563TSで新製品をデザインするお客様におすすめはありますか? 今後の計画は変更される可能性があることは理解していますが、この装置の期待される寿命に関する指針があれば、デザイン上の判断を下し、将来の再設計リスクを減らすのに役立ちます。 再開まで今しばらくお待ちください。 Re: PCF8563TS Lifecycle Status and Long-Term Availability 調べてみたところ、PCF8563TS $0.5のように在庫が多いチップでは、生産を止めるのは簡単ではありません。 Re: PCF8563TS Lifecycle Status and Long-Term Availability こんにちは、ビクターさん。 NXPセミコンダクターズの製品にご関心をお寄せいただき、またサポートの機会をいただきありがとうございます。 今後10〜15年間安定した供給を保証する長寿命プログラムの製品もあります。 長寿プログラム しかしPCF8563TSは長寿プログラムには含まれておらず、販売終了の通知や最終購入日はありません。お客様の要望次第です Alondra_0-1784582617358.png 敬具 アロンドラ 技術サポート NXPセミコンダクターズ
記事全体を表示
I.MX6 VPUエンコーディング機能 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> カメラ画像ストリームからH.264へのエンコードを行うためのi.mx6 VPUの評価を行っています。 私はi.MX6でのストリームエンコーディングは全くの初心者なので、センサの選択に惹かれました。私はその点に関して少し疑問を持っています。 1. VPUがH.264エンコーディングでサポートする最大解像度はどれくらいですか? 2. H.264エンコーディングにおいて、最大解像度でサポートされる最大フレームレートはどれくらいですか? 3. VPUがH.264エンコーディングでサポートする入力カラースペースは何ですか? 4. 例えば640×480ピクセルの解像度が低い場合、H.264エンコードで1920×1080ピクセルと比べてより高いフレームレートを得られるのでしょうか? 5. フレームレートはビットレートによって制限されますか? 6.IPUからVPUへストリームをルーティングしてエンコードすることは可能ですか? ありがとうございます グナ グラフィックスとディスプレイ i.MX6Quad Linux マルチメディア Yocto Project Re: I.MX6 VPU Encoding Features こんにちは、アルトゥール 1920x1080 30FPSの動画をデコードしながら、同時に1920x1080 30FPSの動画をエンコードすることは可能ですか?また、この情報が真実であるかどうかについて、文書に明記されていないのでしょうか? Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本当にありがとうございます Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 1.ホリソント解像度は1080ピクセルに制限されていますが、MJPEGのBPプロファイルでは最大8192x8192ピクセルまで画質が設定可能です。 2. ピクセル/秒と動作周波数の直接的な仕様はありません。さらに、VPUのスループットはエンコード処理とデコード処理で異なる。1つの1920x1080@30fpsストリームをエンコードし、1つの1920x1080@30fpsストリームと1つのD1@30fpsストリームをデコードすることができます。 アルトゥール Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> アルトゥール・ペトゥホフ、 ご回答ありがとうございます。 念のため確認ですが、VPUで1600 x 1200(UXGA)h264エンコーディングが@ 352Mhzでもできないということですか? VPUの動作周波数におけるスループットの計算方法は?266MHz動作時のスループットは約72,576,000ピクセル/秒だと読みました。これについて手伝ってもらえますか? Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Q1.VPUがH.264エンコードでサポートする最大解像度はどれくらいですか? Q2.H.264エンコーディングにおいて、最大解像度でサポートされる最大フレームレートはどれくらいですか? A1-2。i.MX6シリーズプロセッサのビデオ処理ユニット(VPU)は 最大1920x1080@30fpsの解像度/フレームレートでビデオストリームをエンコード/デコードします。 Q3.H.264エンコーディングにおいて、VPUがサポートする入力カラースペースは何ですか? A3. サポートされている入力カラースペースは、MJPEG コーデックを除き YUV4:2:0 です。 4:2:0、4:2:2、2:2:4、4:4:4、4:0:0をサポートしています。 Q4.例えば640×480ピクセルの解像度が低い場合、H.264エンコードで1920×1080ピクセルと比べてより高いフレームレートを得られるのでしょうか? A4. はい。 Q5.フレームレートはビットレートによって制限されますか? A5. エンコードされたビデオストリームのビットレートのことでしょうか?もしそうなら、答えはこうです:フレームレートとビットレートの間に直接的な関係はなく、結果となるビットレートは主に使用されるコーデックとエンコードプロファイルに依存します。 Q6.IPUからVPUへストリームをルーティングしてエンコードすることは可能ですか? A6. はい、システムメモリ内のフレームバッファを使用すれば可能です。例えば、IPUはカメラでキャプチャしたフレームをダブルバッファ方式を用いてシステムメモリに保存し、その後VPUがそこからフレームを取り出してエンコードする。 すてきな一日を、 アルトゥール ----------------------------------------------------------------------------------------------------------------------- 注:この記事があなたの質問への回答になっている場合は、「正解」ボタンをクリックしてください。ありがとう! ----------------------------------------------------------------------------------------------------------------------- Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ありがとう。私はそれを使って遊び始めました。 Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 答えは教えられない。 http://www.chipsnmedia.com/ に連絡してみて。 調べた参考文献も答えは出ていません。 http://www.chipsnmedia.com/data/goodsImages/1289972906&&CNM_Brochure_CODA960.pdf https://community.nxp.com/external-link.jspa?url=http %3A% 2F %2Fwww.chipsnmedia.com% 2Fsupport %2Fdown% 2Fcnm-codadx6-datashe… 船内で試してみることをおすすめします。 Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 杜武、 もしそうなら、640 x 480 @ 90fpsで実現することは可能でしょうか? ありがとうございます グナ Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> #1 最大ビットレートや最大クロック周波数は気にしません。 h264エンコードの場合、 1920*1080*30以下の通常の「幅*高さ*フレームレート」であれば問題ないと思います。 #2 i.MX プラットフォームにはDMAやキャッシュの整合性を扱う「物理メモリ 割り当てAPI」が必要です。 「IPU出力」と「VPU入力」が同じメモリと画像フォーマットを共有している場合、コピーや変換は不要です。 Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 杜武、 ご返信ありがとうございます。 いくつか疑問があります。 1.4と5については、 制限が幅×高さ×fpsの場合、VPUがサポートする最大ビットレートはどれくらいですか?ドキュメントには記載されていませんでした。私の知る限り、VPUの動作速度は最大352MHzまで上がることがあります。 2. 6の場合、 SDMAはこれに使えますか?はいの場合、何か制限事項はありますか? ありがとうございます グナ Re: I.MX6 VPU Encoding Features <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 略して: #1,2 1920x1080@30fps #3 YUV422(NV12)、YUV420 #4,5 制限値は「幅×高さ×フレームレート」だと思います。 #6 フォーマット変換かmemcpyが必要になるかもしれません。 詳細は以下をご覧ください。 http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=1337699481071706174845&Parent_pageType…
記事全体を表示
Config Tools for i.MX Config Tools for i.MX 26.06  in this tool i.mx952 not working also 95 , error : cannot download the processor database. Re: Config Tools for i.MX Hi @onkarbhalerao, Thank you for contacting NXP Support. I have tested this on my side and did not observe any issues. Could you please double check your internet connection and try again? If the issue persists, you can manually download the required files using the MCUXpresso SDK Builder Best regards, Chavira
記事全体を表示
I.MX6 VPU Encoding Features We are evaluating i.mx6 VPU for encoding to H.264 from camera image stream. As I am totally new to stream encoding in i.MX6, I am struck in choosing sensor. I am I have some doubts on that front. 1. What is the maximum resolution supported by VPU for H.264 encoding? 2. What is the maximum frame rate supported at maximum resolution for H.264 encoding? 3. What are input color space supported by VPU for H.264 encoding? 4. If you have less resolution say 640*480 pixels, can we get more frame rate compared to 1920*1080 pixels for H.264 encoding? 5. Is frame rate is limited by bit rate? 6. Is it possible to route stream from IPU to VPU for encoding? Thanks, Guna Graphics & Display i.MX6Quad Linux Multimedia Yocto Project Re: I.MX6 VPU Encoding Features Hi Artur is it possible to encode 1920x1080 30 FPS video while 1920x1080 30FPs video is decoded? Also no document specify this information if its true? Re: I.MX6 VPU Encoding Features Thank you so much Re: I.MX6 VPU Encoding Features 1. The horisontal resolution is limited to 1080 pixels except of the MJPEG BP profile where the maximum picture size can be up to 8192x8192 pixels. 2. There is no direct pixels/s vs operating frequency specification. Moreover, the VPU throughput is different for encoding and decoding operations. It can encode one 1920x1080@30fps stream and decode one 1920x1080@30fps stream plus one D1@30fps stream. Artur Re: I.MX6 VPU Encoding Features Artur Petukhov, Thank you for the response. Just to clarify, Does it mean that I cannot do 1600 x 1200 (UXGA) h264 encoding with VPU even if it runs @ 352Mhz? How to calculate the throughput for VPU operating frequency?. I read for 266Mhz operating the throughput is around 72,576,000 pixels/s. Can you help me on this? Re: I.MX6 VPU Encoding Features Q1. What is the maximum resolution supported by VPU for H.264 encoding? Q2. What is the maximum frame rate supported at maximum resolution for H.264 encoding? A1-2. The Video Processing Unit (VPU) of i.MX6 series processors can encode/decode a video streams at up to 1920x1080@30fps resolution/frame rate. Q3. What are input color space supported by VPU for H.264 encoding? A3. Supported input color space is YUV4:2:0 except of the MJPEG codec that supports 4:2:0, 4:2:2, 2:2:4, 4:4:4 and 4:0:0. Q4. If you have less resolution say 640*480 pixels, can we get more frame rate compared to 1920*1080 pixels for H.264 encoding? A4. Yes. Q5. Is frame rate is limited by bit rate? A5. Do you mean the bit rate of encoded video stream? If so, the answer is: there is no direct relation between frame rate and bit rate, the resulting bit rate mostly depends on the codec and encoding profile used. Q6. Is it possible to route stream from IPU to VPU for encoding? A6. Yes, it is possible using the frame buffer in system memory. For example, IPU stores the frames, captured by camera, to system memory using the double-buffer scheme, then VPU takes the frames to encode from there. Have a great day, Artur ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! ----------------------------------------------------------------------------------------------------------------------- Re: I.MX6 VPU Encoding Features Thank you. I am started playing with that. Re: I.MX6 VPU Encoding Features I can't give you the answer, you can contact the http://www.chipsnmedia.com/. All the reference I searched can't answer it either. http://www.chipsnmedia.com/data/goodsImages/1289972906&&CNM_Brochure_CODA960.pdf https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.chipsnmedia.com%2Fsupport%2Fdown%2Fcnm-codadx6-datashe… I suggest you try it on board. Re: I.MX6 VPU Encoding Features Du wu, If that's the case, then is it possible to do 640 x 480 @ 90 fps? Thanks, Guna Re: I.MX6 VPU Encoding Features #1 I don't care the maximum bitrate or maximum clock freq, I just think any regular "width*height*fps" under "1920*1080*30" will be ok for h264 encoding. #2 The i.MX platform must have "physical memory allocator api" which handle DMA and cache coherent. If "IPU output" and "VPU input" share the same memory and the same image format, no copy or convertion is required. Re: I.MX6 VPU Encoding Features Du wu, Thank you for the reply. I have some doubts, 1. For 4 &5,       If the limit is width * height * fps, then what is the maximum bit rate supported by VPU?.I cound not find that in their doc. As far as I know, the speed of operation of VPU can go up to 352Mhz. 2. For 6,         Can SDMA be used for this? If Yes, Is there any limitation with that? Thanks, Guna Re: I.MX6 VPU Encoding Features for short: #1,2 1920x1080@30fps #3 YUV422(NV12), YUV420 #4,5 i think the limit is "width*height*fps". #6 i think you may need format convertion or memcpy. for detail: http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=1337699481071706174845&Parent_pageType…
記事全体を表示
S32K358 + FreeRTOS: PendSV_Handler実行中にランダムなハードフォルトが発生 チームの皆さん、こんにちは。 FreeRTOSを実行しているS32K358で、ランダムなハードフォルトが発生しています。 アプリケーションは長時間正常に動作しますが、突然フリーズします。システムが実行を停止した後、ソフトウェア・ウォッチドッグ(SWT)はサービスされず、最終的にコントローラがリセットされます。 障害は即座に発生するわけではなく、約1~2時間の連続実行後に発生する。 障害発生後に停止すると、コールスタックには以下が表示されます。 PenSV_Handler() ↓ HardFault_Handler() レジスタ値: LR = 0xA5A5A5A5 PC = 0x00407BD9 LR = 0xA5A5A5A5は、有効な戻りアドレスというよりは、メモリ初期化パターンのように見えます。 その他の登録簿: R0 = 0x204011A8 R3 = 0x2040012C R12 = 0x20400010 ご提案やデバッグに関するアドバイスなど、何でもいただければ大変ありがたいです。 Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler こんにちは、 @nirmal_masilamani さん。 FreeRTOSのコンテキスト切り替え時に保存されたタスクコンテキストが破損しているようです。 PendSVはFreeRTOSによってコンテキスト切り替えに使用されるため、PendSV_Handler()内でHardFaultが発生した場合、多くの場合、スケジューラが無効なタスクコンテキストを復元しようとしていることを意味します。 考えられる根本原因の一つは、タスクスタックオーバーフローです。タスクのスタックサイズを増やし、FreeRTOSのスタックオーバーフロー検出機能を有効にすることをお勧めします。 configCHECK_FOR_STACK_OVERFLOW 実装: vApplicationStackOverflowHook()。 さらに、uxTaskGetStackHighWaterMark()を使って各タスクの残りのスタック空間を定期的に監視することもできます。これにより、故障が発生する前にスタック限界に近いタスクを特定するのに役立ちます。 よろしくお願いいたします。 ダニエル Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler こんにちは、 @danielmartynek さん、 ご回答ありがとうございます。 既にスタックサイズを増やしたり、スタックオーバーフローフックを有効にしたりしてみました。 Overflow Hookにdebug CAN msgを追加しましたが、故障発生時にそのメッセージが届きません。 また、障害が発生した際には uxTaskGetStackHighWaterMark()を監視します。 タスク 1 : 1977 × 4 ≈ 7908 バイトの空き容量 タスク2:1971 × 4 ≈ 7884バイトの空き容量 タスク3:3988 × 4 ≈ 15952バイトの空き容量 Re: S32K358 + FreeRTOS: Random HardFault during PendSV_Handler こんにちは、 @nirmal_masilamani さん。 したがって、根本原因としてスタックオーバーフローを除外できるでしょう。 しかし、タスクコンテキストは依然として破損している。プロセッサはLR = 0xA5A5A5A5を復元しており、これがUsageFaultを引き起こします。0xA5A5A5A5 は tskSTACK_FILL_BYTE (0xA5U) から生成されるパターンで、FreeRTOS がタスクスタックを作成する際にタスクスタックを埋めるために使用されます。 danielmartynek_0-1784709240297.png したがって、LRが0xA5A5A5A5になった場合、コンテキストは有効なレジスタ値ではなく、元のスタックフィルパターンが残っている場所から復元されます。 SPが破損した場合に起こり得ます。その場合、PendSV_Handler()はRAM内の誤った場所からタスクコンテキストを復元します。 スタックポインタのアドレスからSRAM領域を特定できるはずです。 MPUとXRDCを使用して、その領域を適切に保護することをお勧めします。 また、FreeRTOS APIを呼び出す割り込み処理はありますか?もしそうなら、FromISR()のバリアントを使っているのか、configMAX_SYSCALL_INTERRUPT_PRIORITYに関して優先順位は正しく設定されているのか? よろしくお願いいたします。 ダニエル
記事全体を表示
S32K358 SWAP ABのMCAL-XDRC構成 以下の3つの質問に答えるのを手伝ってください。 1. 現在、SWAP機能を使用する必要があります。RMモジュール内のXDRCメモリ構成において、フラッシュBブロック:0x800000-0xbffffffを定義する必要はありますか? 2. HSEが占有しているフラッシュメモリ領域0x7D4000-0x7FFFFFをメモリ構成から削除する必要がありますか? 3. core0をOSを実行するプライマリコア、core2をアルゴリズムを実行するセカンダリコアと定義します。次に、Domain_Assgnment_0にCM7_0、CM7_1、GMAC、uSDHC、eDMAを割り当て、Domain_Assgnment_1にCM7_2を割り当てました。これは正しいでしょうか?実際のアプリケーションでは、使用されていないマスターコアを構成から省略できますか? Re: S32K358 SWAP AB的MCAL-XDRC配置 こんにちは、@scott071209 1.アプリケーションまたはブートローダーは、パッシブパーティション内の画像の詳細を消去、プログラム、検証、読み込みを行う必要があります。つまり、パッシブパーティションもXRDCでカバーされる必要があるということだ。 2. AB_SWAPファームウェアの場合、XRDCはリセット時に自動的に設定され、HSE FWアクティブフラッシュエリア、HSE FWパッシブフラッシュエリア、HSE FWデータフラッシュ、HSE UTESTエリアを保護します。この目的にはディスクリプタ12〜15が使われ、この構成はロックされているため、ユーザーが変更することはできません。詳細はHSEファームウェアのリファレンスマニュアルのセクションで確認できます: “14.6.3.3デフォルトのMRC 0構成(AB_SWAP)」 したがって、HSE資源を自社のXRDC構成でカバーする必要はありません。 3. はい、そのようなセットアップを利用できます。マスターが使われていない場合は、設定で省略できます。 ただし、HSEを使用する場合は、ドメイン3もHSE用に構成する必要があります。これはHSEリソースを保護するためではなく、HSEにユーザーデータへのアクセス権を与え、暗号操作を行うためのものです。 S32K358には4つのドメインがあり、HSEは常に利用可能な最高位のドメインに割り当てられます。S32K358の場合はドメイン3です。これは固定されているので、変更できません。RTDの新しいバージョンでは、HSEマスターはXRDC構成でリストにすら含まれていません。なぜなら再構成ができないからです。ドメイン3にHSEのみを配置したい場合は、このドメインにマスターを割り当てる必要はありません。HSE(健康・安全・環境)は既に自動的に組み込まれています。 以前のRTDバージョンでは、HSEを他のドメインに割り当てることが可能でしたが、そのような設定は効果がありませんでした。そのため、削除されました。 よろしくお願いいたします。 ルーカス
記事全体を表示