ATF SSRAM_MAX_ADDR definition inquiry Hi Team,
The RM describes the procedure to initialize SRAM ranges in the following way:
The mapping rule descripte here is 1 -> 64-byte(0x40) The shown bitwise operation is performed to define the ranges in the PRAMIAS and PRAMIAE registers. Which seems to work correctly with SRAMC, SRAMC_1, SRAMC_2 and SRAMC_3 but it does not work with STDBY_SRAM_CFG. This has been confirmed by me and the customer, they were traying to initialize the 32K of STDBY_SRAM, using the calculation in the RM they had: PRAMIAS = 0 PRAMIAE = 0x1FF but only the range 0-0x1FF0 (8K) was initialized. And when they used PRAMIAE = 0x7FF, the complete range was initialized. So the actual mapping rule for Standby SRAM is 1 -> 16byte(0x10)
I found 0x7FF defined in the https://github.com/nxp-auto-linux/arm-trusted-firmware/blob/c9a7f81230064d21e403cfc315cbd3ffdc18752f/plat/nxp/s32/s32cc/s32_sramc.c#L26
#define SSRAM_MAX_ADDR 0x7FF
My question is:
For the Standby SRAM mapping rule, which document have this description? if you know please kindly provide the information with me. Thanks.
With the name MAX ADDR I would expect it to be the the max offset of the Standby range, which is 0x7FFF(32KB), if it is possible add a comment or modify the definition name so it is not confusing?
BRs,
Tianxiang Linux BSP Priority: MEDIUM Re: ATF SSRAM_MAX_ADDR definition inquiry Hi Tianxiang,
Unfortunately, we don't have any such documentation. You need to ask someone from hardware for this. I saw that the validation team uses this forumula which seems to work for this case: https://bitbucket.sw.nxp.com/projects/AMPFVAL/repos/auto-fval/browse/validation/sramc/driver/inc/sramc_soc_config.h#60 . I am not sure if that's the correct one. We talked with people from the hardware teams in order to get the correct settings for SRAM/SSRAM initialization.
Regarding the name of SSRAM_MAX_ADDR, I am not sure if we would rename it. It is only used once and it is given as a parameter to: clear_sramc_range which has its parameters named as offsets so it implies it is not exactly the address (different from clear_sram_range). Best regards, Andrei
記事全体を表示