How to increase the hdmi clock on the imx8Mplus How to increase the HDMI clock in the samsung_phy_pll_cfg function in the drivers/phy/freescale/phy-fsl-samsung-hdmi.c file, given the screen resolution is 800x480 and the clock is 32MHz. Re: How to increase the hdmi clock on the imx8Mplus Shaojun,the problem has been resolved. Thanks for your support. Re: How to increase the hdmi clock on the imx8Mplus Please apply below patch
You may need to add "video=HDMI-A-1:800x480@60" in uboot command line.
diff --git a/drivers/phy/freescale/phy-fsl-samsung-hdmi.c b/drivers/phy/freescale/phy-fsl-samsung-hdmi.c index d1e93e5b9207..221e71ae2341 100644 --- a/drivers/phy/freescale/phy-fsl-samsung-hdmi.c +++ b/drivers/phy/freescale/phy-fsl-samsung-hdmi.c @@ -136,6 +136,15 @@ const struct phy_config samsung_phy_pll_cfg[] = { 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xE0, 0x83, 0x0F, 0x3E, 0xF8, 0x00, 0x00, }, + }, { + 32000000, { + 0x00, 0xD1, 0x36, 0x70, 0xAD, 0xA0, 0x85, 0x42, + 0x4F, 0x30, 0x33, 0x65, 0x00, 0xC1, 0x24, 0x80, + 0x6C, 0xF2, 0x67, 0x00, 0x10, 0x87, 0x30, 0x3A, + 0x74, 0x8F, 0x00, 0x00, 0x08, 0x00, 0x00, 0x00, + 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, + 0x00, 0xE0, 0x83, 0x0F, 0x3E, 0xF8, 0x00, 0x00, + }, }, { 33750000, { 0x00, 0xD1, 0x70, 0xF4, 0x82, 0x01, 0x80, 0x40, Re: How to increase the hdmi clock on the imx8Mplus Will check it.
記事全体を表示