1972546_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1972546_ja-JP

1972546_ja-JP

S32K3 SHEキーの更新

1.K3 HSE_B Firmware RMドキュメントでは、FIDは6ビットで定義されているため、K3はFID-5ビットをサポートしていませんよね?[でK146チップは、FIDは6ビットだけでなく5ビットにも対応しています。

では、S32K3では、FID-5bitでM1-M3を生成すると、SHEキーは更新できないのですね。

JiayuZhou_0-1728703913045.png


2. S32K3 MCALの暗号ドライバでは、SHEキーのM4はキーエレメント2(CRYPTO_KE_MAC_PROOF)に格納され、M5はキーエレメント6(CRYPTO_KE_CIPHER_PROOF)に格納されます。しかし、私の知る限り、M4M5は要素6ではなく、重要な要素2に格納する必要があります。NXPの暗号コードはAUTOSAR規格に準拠していませんか?

JiayuZhou_1-1728704593426.png


Re:S32K3 SHEキーの更新こんにちは、ルカサドラパ、
あなたの図 1.In、S32K3にはS32K1のようなSFEフラグがないため、FID 6ビットのみをサポートし、VERIFY_ONLYビットを構成する必要があるため、FID 5ビットを満たすことはできません。NXPはFID 5bitの使用をサポートするHSEファームウェアを提供していますか?
2.次のRTDはいつ提供されますか?現在のRTDの関連コードを変更する方法を提供できますか?現在、このRTDを使用してSWを開発しており、すでにこの機能を使用する必要があります。
Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:14 PM
Updated by: