Hi,
In imx8mp on customer board.
I have already change debug port from uart2 to uart4 on yocto(Linux 6.1.1_1.0.1 BSP).
And type cmd is OK.
The same modify on Android (Android 13.0.0_2.0.0 (L6.1.22_2.0.0 BSP)),
after booting finish(hdmi show android launcher),debug console can show message
but can't type anything.
I have compare yocto and android modify.
There are 2 file I can't find in Android BSP.
\sources\meta-freescale\conf\machine\include\imx-base.inc
\sources\meta-freescale\conf\machine\include\imx8mp-evk.inc
How to fix it?
Thanks.
Hello,
You are looking for Yocto specific files, that are not available on Android.
For Android you'll need to patch Linux/Uboot/ATF the same way you did for the Linux system you built using Yocto.
Best regards/Saludos,
Aldo.