Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
[MCX A153] LPCMP Beginner's Guide (Japanese Blog) 1. Introduction This article explains the LPCMP ( Low - Power Compulator ) included in the NXP MCX A series ( MCX A153 ), using the sample from the MCUXpresso SDK frdmmcxa153_lpcmp_interrupt and the FRDM-MCXA153 board as examples. LPCMP is a peripheral function that compares the relative magnitudes of two analog inputs and obtains the result as a digital output. It is used in a wide range of applications, including threshold detection, zero-crossing detection, power supply monitoring, and touch input. The MCX A153's LPCMP features a built-in 8-bit DAC and 8-channel analog multiplexer, enabling threshold comparison without the need for additional external components. This sample assigns an external voltage (VDD or GND) to the positive input (P2_2 / CMP0_IN0) of CMP0 and the internal DAC output (≒ VREFI/2 = VDD/2) to the negative input, and turns the LED_RED on/off using rising/falling edge interrupts of the comparison result. (Reading time: 20 minutes) 2. Overview of LPCMP LPCMP consists of the following subblocks: Comparator core : Compares positive and negative inputs to generate a digital output (COUT). 8-bit DAC : Vin is divided using a 256-tap resistor ladder. VREFH0 (VDD) or VREFH1 (VREFI input) can be selected as Vin. Output formula: DACO = Vin / 256 × (DAC_DATA + 1) , DAC_DATA = 0 to 255 Output range: 256 levels from Vin × 1/256 to Vin × 256/256 (= Vin) (0V cannot be output) ANMUX (PMUX / MMUX) : 8:1 analog selector. External pins (IN0-IN5), internal DAC output, and Reserved selector can be assigned to positive/negative inputs. Window / Sampling / Filter : Debouncing, Timing Control Output pin / Interrupt : Three flags: CFR (rising edge), CFF (falling edge), RRF (output change). 3. Internal Block Diagram   3.1 Input Selector and Core   3.2 Built-in DAC When VRSEL = 0, VREFH0 (VDD) becomes Vin, and when VRSEL = 1, VREFH1 (VREFI input) becomes Vin.   4. Unique information in MCX A153 item Content instance CMP0 (used in this sample), CMP1 Analog input pins CMP0_IN0~IN5 Built-in DAC resolution 8-bit (256 levels) DAC reference voltage VDD (VREFH0) or VREFI external input (VREFH1) Interrupt flag CFR (Climate Change), CFF (Climate Fall), RRF (Reduced Output Frequency) Functional clock source Select from FRO12M, FRO HF, CLK_1M, etc. using CLOCK_AttachClk Analog power supply Enable the analog power supply for the CMP/DAC using SPC0 ACTIVE_CFG1.   5. Sample Operation   5.1 Wiring Connect the FRDM-MCXA153 pin headers as follows: signal pin Board Location Destination role VREFI P2_7 J3-1 JP8-2 (VDD) DAC reference voltage Vin (= VDD) CMP0_IN0 P2_2 J2-9 Manually switch between VDD and GND. Plus input LED_RED P3_12 Onboard ― Displaying comparison results By jumpering J3-1 to JP8-2 (VDD), VREFI = VDD, and the Vin of the built-in DAC becomes VDD. DAC_DATA is set to ((LPCMP_DCR_DAC_DATA_MASK >> SHIFT) >> 1) = 127, so DACO ≈ VDD/2. Connecting J2-9 (CMP0_IN0) to VDD lights up LED_RED, and connecting it to GND turns it off.   5.2 Sequence   5.3 Behavior of Comparison Results   6. Clock settings The LPCMP requires a separate function clock (CMP_FUNC) for sampling/filtering, in addition to the bus clock. Furthermore, because it's an analog circuit, the analog power supply for the CMP/DAC must be enabled in the SPC (System Power Controller). hardware_init.c The relevant code is the following three lines: CLOCK_AttachClk(kFRO12M_to_CMP0); /* 1) 機能クロックソースを選択 */ CLOCK_SetClockDiv(kCLOCK_DivCMP0_FUNC, 1U); /* 2) 分周を 1 に設定 (12MHz のまま) */ SPC0->ACTIVE_CFG1 |= ((1U << 16U) | (1U << 20U)); /* 3) CMP0/DAC0 アナログ電源 ON */ Structure of the SPC0->ACTIVE_CFG1 register 6.1 Clock Tree Refer to Figure 46 in the MCX A153 Reference Manual . 6.2 The corresponding bit of SPC ACTIVE_CFG1 bit Content bit16 (CMP0_AEN) Enable the CMP0 analog circuit in Active mode. bit20 (CMP0_DAC_AEN) Enable the CMP0's built-in DAC in Active mode. If you forget to set these two bits, LPCMP_Init() itself won't cause an error, but the comparison result will always remain 0, or the DAC output will not start up. 7. PINMUX Settings pin_mux.c We have set up the following four systems (a total of 5 pins). pin function ALT Setting points P2_2 CMP0_IN0 (analog input) ALT0 Pull-Down, Input Buffer Disable P2_7 VREFI (DAC Reference Voltage) ALT0 Pull-Disable, Input Buffer Disable P3_12 GPIO (LED_RED) ALT0 Output, initial value 1 (light off) P0_2 LPUART0_RX ALT2 Pull-Up P0_3 LPUART0_TX ALT2 Pull-Up   7.1 Precautions when using analog pins When using P2_2 / P2_7 as analog inputs, be sure to disable the digital input buffer . If it is left enabled, a shoot-through current will flow every time the input voltage passes near the logic threshold, leading to increased current consumption, heat generation, and distortion of the analog signal. const port_pin_config_t port2_2_pin16_config = { kPORT_PullDown, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, kPORT_MuxAlt0, kPORT_InputBufferDisable, /* <-- 必須 */ kPORT_UnlockRegister, }; PORT_SetPinConfig(PORT2, 2U, &port2_2_pin16_config);   7.2 PORT / GPIO Clock and Reset Release Before touching PINMUX, you need to supply a clock to the PORT and GPIO you will be using and disable the reset. CLOCK_EnableClock(kCLOCK_GatePORT0); CLOCK_EnableClock(kCLOCK_GatePORT2); CLOCK_EnableClock(kCLOCK_GatePORT3); CLOCK_EnableClock(kCLOCK_GateGPIO3); RESET_ReleasePeripheralReset(kPORT0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT2_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kGPIO3_RST_SHIFT_RSTn); Forgetting this will result in a fault occurring when writing to the GPIO register, or the changes being written not being reflected. 8. Code Explanation Using the SDK API   8.1 Definition of app.h #define DEMO_LPCMP_BASE CMP0 #define DEMO_LPCMP_USER_CHANNEL 0U /* CMP0_IN0 */ #define DEMO_LPCMP_DAC_CHANNEL 7U /* 内蔵 DAC 出力の MUX チャネル */ #define DEMO_LPCMP_IRQ_ID CMP0_IRQn #define DEMO_LPCMP_IRQ_HANDLER_FUNC CMP0_IRQHandler   8.2 Initialization Sequence in main() lpcmp_config_t mLpcmpConfigStruct; lpcmp_dac_config_t mLpcmpDacConfigStruct; BOARD_InitHardware(); /* clocks + pinmux + console */ /* 1) デフォルト設定を取得し、必要箇所だけ上書き */ LPCMP_GetDefaultConfig(&mLpcmpConfigStruct); /* 2) コンパレータ初期化 */ LPCMP_Init(DEMO_LPCMP_BASE, &mLpcmpConfigStruct); /* 3) 内蔵 DAC 設定: Vin = VREFI(=VDD), DAC_DATA = 127 (フルスケールの半分) * DACO = VREFI / 256 * (127 + 1) = VREFI * 128/256 = VREFI/2 */ mLpcmpDacConfigStruct.enableLowPowerMode = false; mLpcmpDacConfigStruct.referenceVoltageSource = kLPCMP_VrefSourceVin2; /* VREFI */ mLpcmpDacConfigStruct.DACValue = ((LPCMP_DCR_DAC_DATA_MASK >> LPCMP_DCR_DAC_DATA_SHIFT) >> 1U); /* = 127 */ LPCMP_SetDACConfig(DEMO_LPCMP_BASE, &mLpcmpDacConfigStruct); /* 4) PMUX = IN0, MMUX = DAC ch7 */ LPCMP_SetInputChannels(DEMO_LPCMP_BASE, DEMO_LPCMP_USER_CHANNEL, DEMO_LPCMP_DAC_CHANNEL); /* 5) 立ち上がり/立ち下がり両エッジ割り込みを有効化 */ LPCMP_EnableInterrupts(DEMO_LPCMP_BASE, kLPCMP_OutputRisingInterruptEnable | kLPCMP_OutputFallingInterruptEnable); EnableIRQ(DEMO_LPCMP_IRQ_ID); while (1) { } /* あとは割り込み駆動 */   8.3 Interrupt Handlers void DEMO_LPCMP_IRQ_HANDLER_FUNC(void) { LPCMP_ClearStatusFlags(DEMO_LPCMP_BASE, kLPCMP_OutputRisingEventFlag | kLPCMP_OutputFallingEventFlag); if (kLPCMP_OutputAssertEventFlag == (kLPCMP_OutputAssertEventFlag & LPCMP_GetStatusFlags(DEMO_LPCMP_BASE))) { LED_ON(); /* V+ > V- (COUT=1) : LED 点灯 */ } else { LED_OFF(); /* V+ < V- (COUT=0) : LED 消灯 */ } SDK_ISR_EXIT_BARRIER; } In both rising and falling interrupts, both flags are cleared first, and then the LED is branched on/off based on kLPCMP_OutputAssertEventFlag (= current COUT).   9. How to operate frdmmcxa153_lpcmp_interrupt Open it in the IDE and build it. Jumper J3-1 (P2_7 / VREFI) to JP8-2 (VDD) to set VREFI = VDD. Write to the target and open a terminal (115200 bps). Connect J2-9 (P2_2 / CMP0_IN0) to VDD with a jumper wire → LED_RED lights up. Reconnect the same pin to GND → LED_RED turns off   10. Common stumbling blocks Symptoms cause handle The LPCMP output is not switching. Forgot to enable the analog power supply for CMP0/DAC in SPC0 ACTIVE_CFG1. SPC0->ACTIVE_CFG1 |= (1<<16) No interruption LPCMP_EnableInterrupts or EnableIRQ(CMP0_IRQn) leak Check both calls DAC output does not start up. VRSEL and VREFI input pin mismatch, VREFI not connected kLPCMP_VrefSourceVin2 When in use, apply the reference voltage to P2_7. Chattering near the threshold Hysteresis 0, filter disabled hysteresisMode Set to Level 1-3, or enable filtering. Fault when writing to GPIO registers PORT clock not supplied / Reset not released CLOCK_EnableClock() And confirm the call to RESET_ReleasePeripheralReset()   11. Summary The LPCMP in the MCX A153 has the following characteristics: With 8 ANMUX inputs and a built-in 8-bit DAC, threshold comparison is possible with minimal external circuitry. The DAC output is DACO = Vin/256 × (DAC_DATA + 1) (DAC_DATA = 0 to 255), with 256 steps ranging from Vin × 1/256 to Vin. Low-power mode, hysteresis, and filtering functions can be configured with a single line of SDK API code. To use (1) Functional Clock Attachment + Divider (2) SPC Analog Power Supply Enable (3) Disable the Input Buffer for analog pins These three points are essential. This sample uses a minimal configuration, but it can be extended to dynamically change thresholds with a DAC, use window mode, or use DMA/external triggers instead of interrupts. We hope this article will be helpful as a starting point for developing applications that use LPCMP. ========================= We are currently unable to respond to comments left in the "Comment" section of this post. We apologize for the inconvenience, but please refer to " Technical Questions to NXP - How to Contact Us( Japanese Blog) " when making an inquiry. (If you are already an NXP distributor or have a relationship with NXP, you may ask your representative directly.) This article explains the LPCMP ( Low - Power Compulator ) included in the NXP MCX A series ( MCX A153 ), using the sample from the MCUXpresso SDK frdmmcxa153_lpcmp_interrupt and the FRDM-MCXA153 board as examples. LPCMP is a peripheral function that compares the relative magnitudes of two analog inputs and obtains the result as a digital output. It is used in a wide range of applications, including threshold detection, zero-crossing detection, power supply monitoring, and touch input. The MCX A153's LPCMP features a built-in 8-bit DAC and 8-channel analog multiplexer, enabling threshold comparison without the need for additional external components. This sample assigns an external voltage (VDD or GND) to the positive input (P2_2 / CMP0_IN0) of CMP0 and the internal DAC output (≒ VREFI/2 = VDD/2) to the negative input, and turns the LED_RED on/off using rising/falling edge interrupts of the comparison result. (Reading time: 20 minutes) MCUXpresso SDK MCX Japanese Blog
View full article
[MCX A153] LPCMP 新手指南(日语博客) 1. 引言 本文以 MCUXpresso SDK 中的 示例和 frdmmcxa153_lpcmp_interrupt FRDM-MCXA153 板为例,解释了 NXP MCX A 系列( MCX A153 ) 中包含的 LPCMP( 低 功耗 计算器 )。 LPCMP 是一种外设功能,用于比较两个模拟输入信号的相对幅度,并将结果以数字输出的形式呈现。它广泛应用于各种场景,包括阈值检测、过零检测、电源监控和触摸输入。MCX A153 的 LPCMP 内置 8 位 DAC 和 8 通道模拟多路复用器,无需额外的外部元件即可实现阈值比较。 此示例将外部电压(VDD 或 GND)分配给 CMP0 的正输入端(P2_2 / CMP0_IN0),将内部 DAC 输出(≒ VREFI/2 = VDD/2)分配给负输入端,并使用比较结果的上升沿/下降沿中断来打开/关闭 LED_RED。 (阅读时间:20分钟) 2. LPCMP概述 LPCMP由以下子模块组成: 比较器核心:比较正负输入以生成数字输出(COUT)。 8 位 DAC :输入电压 Vin 通过 256 抽头电阻梯形电路进行分压。VREFH0 (VDD) 或 VREFH1 (VREFI 输入) 可选择作为输入电压 Vin。 输出公式: DACO = Vin / 256 × (DAC_DATA + 1) ,DAC_DATA = 0 到 255 输出范围:256 级,从 Vin × 1/256 到 Vin × 256/256 (= Vin) (不能输出 0V) ANMUX(PMUX / MMUX) :8:1 模拟选择器。外部引脚(IN0-IN5)、内部 DAC 输出和保留选择器可分配给正/负输入。 窗口/采样/滤波器:去抖动、时序控制 输出引脚/中断:三个标志:CFR(上升沿)、CFF(下降沿)、RRF(输出变化)。 3. 内部框图   3.1 输入选择器和核心   3.2 内置DAC 当 VRSEL = 0 时,VREFH0 (VDD) 变为 Vin;当 VRSEL = 1 时,VREFH1 (VREFI 输入) 变为 Vin。   4. MCX A153 中的独特信息 项目 内容 实例 CMP0(本样本中使用),CMP1 模拟输入引脚 CMP0_IN0~IN5 内置DAC分辨率 8 位(256 级) DAC参考电压 VDD (VREFH0) 或 VREFI 外部输入 (VREFH1) 中断标志 CFR(气候变化)、CFF(气候下降)、RRF(降低输出频率) 功能时钟源 使用 CLOCK_AttachClk 模拟电源 使用 SPC0 ACTIVE_CFG1 启用 CMP/DAC 的模拟电源。   5. 示例操作   5.1 接线 按如下方式连接 FRDM-MCXA153 引脚接头: 信号 别针 董事会位置 目的地 角色 VREFI P2_7 J3-1 JP8-2(VDD) DAC参考电压Vin(= VDD) CMP0_IN0 P2_2 J2-9 手动切换VDD和GND。 加输入 红色 LED P3_12 机上 — 显示对比结果 将 J3-1 跳线连接到 JP8-2 (VDD) 后,VREFI = VDD,内置 DAC 的输入电压 (Vin) 变为 VDD。DAC_DATA 设置为 ((LPCMP_DCR_DAC_DATA_MASK >> SHIFT) >> 1) = 127,因此 DACO ≈ VDD/2。将 J2-9 (CMP0_IN0) 连接到 VDD 会点亮 LED_RED,将其连接到 GND 则会熄灭 LED_RED。   5.2 序列   5.3 对比结果的行为   6. 时钟设置 除了总线时钟外,LPCMP 还需要一个单独的功能时钟 (CMP_FUNC) 用于采样/滤波。此外,由于它是模拟电路,因此必须在 SPC(系统电源控制器)中启用 CMP/DAC 的模拟电源。 hardware_init.c 相关代码如下三行: CLOCK_AttachClk(kFRO12M_to_CMP0); /* 1) 機能クロックソースを選択 */ CLOCK_SetClockDiv(kCLOCK_DivCMP0_FUNC, 1U); /* 2) 分周を 1 に設定 (12MHz のまま) */ SPC0->ACTIVE_CFG1 |= ((1U << 16U) | (1U << 20U)); /* 3) CMP0/DAC0 アナログ電源 ON */ SPC0->ACTIVE_CFG1 寄存器的结构 6.1 时钟树 请参阅MCX A153 参考手册中的图 46。 6.2 SPC ACTIVE_CFG1 的对应位 少量 内容 bit16 (CMP0_AEN) 使 CMP0 模拟电路处于激活状态。 bit20 (CMP0_DAC_AEN) 启用 CMP0 的内置 DAC 并进入激活模式。 如果忘记设置这两个位, LPCMP_Init() 本身不会导致错误,但比较结果将始终为 0,或者 DAC 输出将不会启动。 7. 引脚复用设置 pin_mux.c 我们设置了以下四个系统(共 5 个引脚)。 别针 功能 备用 设置要点 P2_2 CMP0_IN0(模拟输入) 谷丙转氨酶0 下拉输入缓冲区禁用 P2_7 VREFI(DAC 参考电压) 谷丙转氨酶0 拉取禁用,输入缓冲区禁用 P3_12 GPIO(LED_RED) 谷丙转氨酶0 输出,初始值为 1(灯灭) P0_2 LPUART0_RX ALT2 引体向上 P0_3 LPUART0_TX ALT2 引体向上   7.1 使用模拟引脚时的注意事项 当使用 P2_2 / P2_7 作为模拟输入时,请务必禁用数字输入缓冲器。如果启用该缓冲器,则每次输入电压接近逻辑阈值时都会产生直通电流,导致电流消耗增加、发热增多以及模拟信号失真。 const port_pin_config_t port2_2_pin16_config = { kPORT_PullDown, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, kPORT_MuxAlt0, kPORT_InputBufferDisable, /* <-- 必須 */ kPORT_UnlockRegister, }; PORT_SetPinConfig(PORT2, 2U, &port2_2_pin16_config);   7.2 端口/GPIO 时钟和复位释放 在操作 PINMUX 之前,需要为要使用的端口和 GPIO 提供时钟信号,并禁用复位功能。 CLOCK_EnableClock(kCLOCK_GatePORT0); CLOCK_EnableClock(kCLOCK_GatePORT2); CLOCK_EnableClock(kCLOCK_GatePORT3); CLOCK_EnableClock(kCLOCK_GateGPIO3); RESET_ReleasePeripheralReset(kPORT0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT2_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kGPIO3_RST_SHIFT_RSTn); 如果忘记这一点,在写入 GPIO 寄存器时将会出现故障,或者写入的更改不会反映出来。 8. 使用 SDK API 的代码说明   8.1 app.h 的定义 #define DEMO_LPCMP_BASE CMP0 #define DEMO_LPCMP_USER_CHANNEL 0U /* CMP0_IN0 */ #define DEMO_LPCMP_DAC_CHANNEL 7U /* 内蔵 DAC 出力の MUX チャネル */ #define DEMO_LPCMP_IRQ_ID CMP0_IRQn #define DEMO_LPCMP_IRQ_HANDLER_FUNC CMP0_IRQHandler   8.2 main() 函数中的初始化顺序 lpcmp_config_t mLpcmpConfigStruct; lpcmp_dac_config_t mLpcmpDacConfigStruct; BOARD_InitHardware(); /* clocks + pinmux + console */ /* 1) デフォルト設定を取得し、必要箇所だけ上書き */ LPCMP_GetDefaultConfig(&mLpcmpConfigStruct); /* 2) コンパレータ初期化 */ LPCMP_Init(DEMO_LPCMP_BASE, &mLpcmpConfigStruct); /* 3) 内蔵 DAC 設定: Vin = VREFI(=VDD), DAC_DATA = 127 (フルスケールの半分) * DACO = VREFI / 256 * (127 + 1) = VREFI * 128/256 = VREFI/2 */ mLpcmpDacConfigStruct.enableLowPowerMode = false; mLpcmpDacConfigStruct.referenceVoltageSource = kLPCMP_VrefSourceVin2; /* VREFI */ mLpcmpDacConfigStruct.DACValue = ((LPCMP_DCR_DAC_DATA_MASK >> LPCMP_DCR_DAC_DATA_SHIFT) >> 1U); /* = 127 */ LPCMP_SetDACConfig(DEMO_LPCMP_BASE, &mLpcmpDacConfigStruct); /* 4) PMUX = IN0, MMUX = DAC ch7 */ LPCMP_SetInputChannels(DEMO_LPCMP_BASE, DEMO_LPCMP_USER_CHANNEL, DEMO_LPCMP_DAC_CHANNEL); /* 5) 立ち上がり/立ち下がり両エッジ割り込みを有効化 */ LPCMP_EnableInterrupts(DEMO_LPCMP_BASE, kLPCMP_OutputRisingInterruptEnable | kLPCMP_OutputFallingInterruptEnable); EnableIRQ(DEMO_LPCMP_IRQ_ID); while (1) { } /* あとは割り込み駆動 */   8.3 中断处理程序 void DEMO_LPCMP_IRQ_HANDLER_FUNC(void) { LPCMP_ClearStatusFlags(DEMO_LPCMP_BASE, kLPCMP_OutputRisingEventFlag | kLPCMP_OutputFallingEventFlag); if (kLPCMP_OutputAssertEventFlag == (kLPCMP_OutputAssertEventFlag & LPCMP_GetStatusFlags(DEMO_LPCMP_BASE))) { LED_ON(); /* V+ > V- (COUT=1) : LED 点灯 */ } else { LED_OFF(); /* V+ < V- (COUT=0) : LED 消灯 */ } SDK_ISR_EXIT_BARRIER; } 在上升沿和下降沿中断中,两个标志位都会被清除,然后根据 kLPCMP_OutputAssertEventFlag (= 当前 COUT)来控制 LED 的开/关状态。   9. 如何操作 frdmmcxa153_lpcmp_interrupt 在 IDE 中打开并构建。 将跳线 J3-1 (P2_7 / VREFI) 连接到 JP8-2 (VDD)以设置 VREFI = VDD。 向目标写入数据并打开终端(115200 bps)。 用跳线将 J2-9 (P2_2 / CMP0_IN0) 连接到 VDD → LED_RED 亮起。 将同一引脚重新连接到 GND → 红色 LED 熄灭   10. 常见的绊脚石 症状 原因 处理 LPCMP 输出未切换。 忘记在 SPC0 ACTIVE_CFG1 中启用 CMP0/DAC 的模拟电源。 SPC0->ACTIVE_CFG1 |= (1<<16) 无中断 LPCMP_EnableInterrupts 或 EnableIRQ(CMP0_IRQn) 泄漏 检查这两个电话 DAC 输出无法启动。 VRSEL 和 VREFI 输入引脚不匹配,VREFI 未连接 kLPCMP_VrefSourceVin2 使用时,将参考电压施加到 P2_7。 门槛附近传来一阵嘈杂声 滞后为 0,滤波器已禁用 hysteresisMode 设置为 1-3 级,或启用筛选功能。 写入GPIO寄存器时发生故障 端口时钟未提供/复位未释放 CLOCK_EnableClock() 并确认对 RESET_ReleasePeripheralReset() 调用   11. 总结 MCX A153 中的 LPCMP 具有以下特点: 它具有 8 个 ANMUX 输入和一个内置的 8 位 DAC,只需极少的外部电路即可进行阈值比较。 DAC 输出为 DACO = Vin/256 × (DAC_DATA + 1) (DAC_DATA = 0 到 255),有 256 个步长,范围从 Vin × 1/256 到 Vin。 低功耗模式、迟滞和滤波功能可以通过一行 SDK API 代码进行配置。 使用 (1)功能性时钟附件+分隔线 (2)SPC模拟电源使能 (3)禁用模拟引脚的输入缓冲器 这三点至关重要。 本示例采用最小配置,但可以扩展以实现以下功能:使用数模转换器 (DAC) 动态更改阈值、使用窗口模式,或使用 DMA/外部触发器代替中断。我们希望本文能为开发使用 LPCMP 的应用程序提供起点。 ========================= 即使您在本文的“评论”栏留言,我们目前也无法回复。 给您带来不便,我们深感抱歉。请在询问时参阅“NXP技术问题-联系方式(日本博客)”。 (如果您已经是NXP的代理商或与其有合作关系,可以直接向负责人咨询。) 本文以 MCUXpresso SDK 中的 示例和 frdmmcxa153_lpcmp_interrupt FRDM-MCXA153 板为例,解释了 NXP MCX A 系列( MCX A153 ) 中包含的 LPCMP( 低 功耗 计算器 )。 LPCMP 是一种外设功能,用于比较两个模拟输入信号的相对幅度,并将结果以数字输出的形式呈现。它广泛应用于各种场景,包括阈值检测、过零检测、电源监控和触摸输入。MCX A153 的 LPCMP 内置 8 位 DAC 和 8 通道模拟多路复用器,无需额外的外部元件即可实现阈值比较。 此示例将外部电压(VDD 或 GND)分配给 CMP0 的正输入端(P2_2 / CMP0_IN0),将内部 DAC 输出(≒ VREFI/2 = VDD/2)分配给负输入端,并使用比较结果的上升沿/下降沿中断来打开/关闭 LED_RED。 (阅读时间:20分钟) MCUXpresso SDK MCX 日本博客
View full article
General Recommendations for NFC Antenna Design General recommendations for NFC (connected) Tags antennas  Track width -> 0.3 mm  Track spacing -> 0.15 mm / 0.2 mm (Dependent on the manufacturing process.) Copper thickness -> 35 µm Number of turns  Typically, the antenna inductance shall be lower than the maximum value determined by the IC's internal input capacitance. For example, with an internal capacitance of 50 pF, the maximum allowable inductance at 13.56 MHz is approximately 2.7 µH. If a 4-turn antenna results in 2 µH and a 5-turn antenna results in 3 µH, the 4-turn design should be selected. The antenna can then be accurately tuned to resonance using an external capacitor, providing sufficient tuning margin and compensating for component and manufacturing tolerances. Note: Based on practical experience, distributing the antenna turns across multiple PCB layers can increase the effective antenna area. For example, a 4-turn antenna may be implemented as 2 turns on the top layer and 2 turns on the bottom layer, which can improve coupling performance while maintaining the target inductance.  See the impact of the number of turns on the antenna Q factor:  General recommendations for NFC Controllers/Frontends  Track width -> 0.5 mm  Track spacing -> 0.15 mm / 0.2 mm (Dependent on the manufacturing process.) Copper thickness -> 35 µm Number of turns NXP typically recommends selecting the number of turns to achieve an antenna inductance of approximately 1 µH to 1.5 µH. Together with the trace geometry, the inductance determines the antenna Q factor. However, the exact Q factor is generally not critical, as it is typically adjusted using damping resistors during the matching process to achieve the required bandwidth Note: Distributing NFC Reader antenna turns across multiple PCB layers typically offers only marginal performance benefits, except in highly space-constrained designs such as miniature NFC or wireless charging antennas.
View full article
I Tested 10 Data Removal Services: Here Are the Best Data Removal Services for 2026 My 10-Month Experiment: Finding the Best Data Removal Services in 2026 A few months ago, I had a massive wake-up call. I typed my name into a random search engine and was horrified to find my current home address, phone number, and even my relatives' names listed on dozens of sketchy people-search sites. After spending weeks getting targeted spam calls and worrying about AI-powered identity theft, I decided to take action. I spent the last 10 months personally testing the leading data removal services on the market to see which ones actually deliver on their promises. After wasting countless hours trying to do it manually and burning through multiple subscriptions, I found the tools that genuinely protect your digital footprint. If you want to skip my trial and error, here are my top recommendations right out of the gate: 👉 Try Incogni — My #1 overall pick. It’s fully automated, incredibly affordable (~$6.49/mo), and handles the legal heavy lifting globally. 👉 Try DeleteMe — My premium pick. If you have a common name or a complex privacy situation, their human-assisted team and massive 750+ broker database are unmatched. The Wake-Up Call: Why I Started This Journey Let me be real with you: a decade ago, having your data on a data broker site just meant you got a few extra telemarketing calls. In 2026, the stakes are terrifyingly high. Malicious actors are now scraping these exact sites to feed generative AI models. I realized that my exposed biographical data was essentially a blueprint for voice cloning, deepfake impersonation, and hyper-personalized phishing attacks. Privacy is no longer just about avoiding spam; it’s a fundamental layer of personal security. The "Boomerang Effect": Why One-Time Opt-Outs Failed Me When I first started, I tried the DIY route. I found the opt-out pages, submitted my requests, and watched my data disappear. I thought I was safe. But exactly 74 days later, my information was right back up. This is what I call the "Boomerang Effect." Data brokers use automated crawlers that continuously re-scrape public records. A single removal request is practically useless. This harsh reality is exactly why I now exclusively recommend automated data removal services that feature continuous, aggressive re-monitoring. How I Evaluated These Data Protection Services I didn't just read their marketing copy; I put my own data on the line. Over a 10-month period, I graded each data broker removal service on four strict criteria: Long-Term Suppression: Did my data stay hidden, or did it quietly reappear without the service noticing? Scan Frequency: I heavily penalized services that only checked my status once a month. Weekly or real-time scanning is mandatory in 2026. Database Quality: I didn't just count the number of brokers; I checked if they were actually targeting the high-risk, high-traffic people-finder sites. Transparency: Did the dashboard actually show me proof of removal, or just a vague "processing" spinner? My #1 Pick: Incogni (The Set-It-and-Forget-It Champion) My Rating: ★★★★★ 5.0 / 5.0 Cost: ~$6.49/month (Annual Plan) Best For: 90% of users who want maximum protection with zero daily effort. Incogni, built by the cybersecurity veterans at Surfshark, completely blew me away. The setup took me less than three minutes. I essentially gave them power of attorney to act as my legal agent under GDPR and CCPA frameworks. From that moment, their system started firing off legally binding deletion requests to over 180 of the most aggressive data brokers. What I love most about Incogni is the dashboard. It’s clean, real-time, and shows me exactly which brokers had my data and when it was successfully purged. At roughly $6.49 a month, it is hands-down the best value in the industry. It completely neutralizes the "Boomerang Effect" by automatically re-filing requests the second a broker tries to re-list me. My Pros: Unbeatable price-to-performance ratio. True global reach (leverages strict EU GDPR laws even if you are outside the EU). Zero manual effort required on my end. My Cons: The broker list (180+) is highly curated but smaller than DeleteMe’s. No dedicated human case manager for highly unusual edge cases. 👉 Check out my Incogni setup here My #2 Pick: DeleteMe (The Heavyweight for Complex Cases) My Rating: ★★★★★ 4.8 / 5.0 Cost: ~$10.75/month (Annual Plan) Best For: Users with common names, multiple past addresses, or high-risk profiles. If Incogni is a highly efficient sniper, DeleteMe is a full tactical squad. They cover a staggering 750+ data brokers—the largest network I’ve seen. But the real reason I keep DeleteMe in my arsenal (and recommend it to my family members with very common names) is their hybrid approach. They use automation, but they also employ actual human privacy experts who manually fight with stubborn brokers that try to reject automated requests. Every quarter, I get a detailed, documented report showing exactly what my dedicated team did. It’s more expensive, but for complex digital footprints, that human oversight is worth every penny. My Pros: Massive 750+ broker database. Real humans handle the stubborn, hard-to-remove sites. Excellent family plans to cover your spouse and kids. My Cons: Noticeably more expensive than Incogni. Reporting is quarterly, so you don't get that instant dopamine hit of real-time dashboard updates. Review DeleteMe's plans here The Best Incogni Alternatives I Tested While Incogni and DeleteMe took the top spots, I know everyone has different needs. Here are my quick takes on the other major players if you are looking for Incogni alternatives: Optery (#3): I loved their transparency. They actually show you screenshots of your exposed profiles before they remove them. Great for visual learners on a budget (~$3.99/mo). Aura (#4): If you want to kill two birds with one stone, Aura bundles data privacy services with a top-tier VPN, antivirus, and credit monitoring. Privacy Bee (#5): This is for the privacy nerds. It offers incredibly granular control over what data types are targeted, though the learning curve is a bit steep. OneRep (#6): Fast and aggressive automation. A solid runner-up for speed, though their customer support isn't quite as responsive as Incogni's. The DIY Approach: How I Tried to Remove My Data for Free (And Failed) People always ask me how to remove personal information from internet databases without paying. I tried it. Here is what my weekend looked like: I searched my name on Spokeo, Whitepages, BeenVerified, and MyLife. I hunted for the "Do Not Sell My Info" links, usually hidden in tiny font at the bottom of the page. I uploaded my ID, verified my email, and filled out CAPTCHAs. I set a calendar reminder to do it all again in 60 days. It took me 14 hours. Two months later, 80% of my data was back online. Unless your risk profile is incredibly low and you value your free time at less than $2 an hour, paying a data removal service like Incogni is an absolute no-brainer. Your time is worth more than the cost of a couple of coffees a month. Frequently Asked Questions (From My Inbox) Do data broker removal services actually work? Yes, but only if they include continuous re-monitoring. My 10-month test proved that one-and-done services are a scam. Brokers re-scrape public records constantly. Tools like Incogni and DeleteMe work because they act as relentless legal watchdogs, suppressing your data on an endless loop. Is Incogni better than DeleteMe? For the vast majority of my readers, yes. Incogni offers a better price, global legal reach, and a real-time dashboard. I only tell people to upgrade to DeleteMe if they have a highly complex digital footprint (multiple marriages, lots of past addresses) or if they specifically want human agents fighting on their behalf. What happens if I cancel my subscription? This is a common fear. If you cancel a service like Incogni or DeleteMe, they stop sending new suppression requests. Because of the "Boomerang Effect," data brokers will eventually re-scrape your info from public records and re-list you within a few months. Think of these services like a gym membership for your privacy—you have to keep it active to stay protected. My Final Verdict on Protecting Your Digital Footprint Living in 2026 means accepting that the data broker economy is relentless. Your personal information is being packaged and sold right now, feeding AI scams and social engineering attacks. Doing nothing is an active choice to remain vulnerable. After hundreds of hours of testing, my advice is simple: Start with Incogni to automate your baseline protection globally. If your situation is messy or you want the absolute widest net cast across 750 brokers, upgrade to DeleteMe. Pair your chosen service with a good password manager, enable hardware-key 2FA, and stop letting the internet treat your private life like public property. Take back control today. Re: I Tested 10 Data Removal Services: Here Are the Best Data Removal Services for 2026 Hi Jakyz Thank you for reaching out to NXP and for your interest in our products. Could you please let us know if your inquiry is related to any specific NXP product or device? We would be happy to assist you further if so. Pls review our NXP website to find which part do you need:  https://www.nxp.com/ If your question is not related to NXP products, we’re afraid we may have limited ability to provide detailed support in this case. We truly appreciate your understanding. Please feel free to share more details if applicable — we’re always glad to help where we can. BR Lina 
View full article
我测试了 10 款数据清除服务:以下是 2026 年最佳数据清除服务 我的十个月实验:寻找2026年最佳数据清除服务 几个月前,我经历了一次巨大的觉醒。我随便在一个搜索引擎里输入了自己的名字,结果惊恐地发现,我的家庭住址、电话号码,甚至我亲戚的名字都列在几十个可疑的寻人网站上。在连续几周接到针对性的垃圾电话,并担心人工智能驱动的身份盗窃后,我决定采取行动。过去 10 个月,我亲自测试了市场上领先的数据删除服务,看看哪些服务真正兑现了承诺。 在浪费了无数时间尝试手动操作并消耗了多种订阅服务后,我终于找到了真正能够保护您的数字足迹的工具。如果你不想经历我的摸索过程,以下是我开门见山的最佳建议: 👉 试试 Incogni——我的首选。它完全自动化,价格极其实惠(每月约 6.49 美元),而且可以处理全球范围内的繁琐法律事务。 👉 试试 DeleteMe——我的首选高级服务。如果您的名字很常见,或者您的隐私情况比较复杂,他们专业的客服团队和超过 750 家经纪公司的庞大数据库绝对是您的最佳选择。 觉醒时刻:我为何踏上这段旅程 说实话,十年前,把你的数据放在数据经纪网站上,只意味着你会接到一些额外的电话推销。2026年,形势将变得异常严峻。恶意行为者现在正在抓取这些网站的数据,以训练生成式人工智能模型。我意识到,我泄露的个人信息实际上成了语音克隆、深度伪造冒充和高度个性化网络钓鱼攻击的蓝图。隐私不再仅仅是避免垃圾邮件;它是个人网络安全的基本层。 “回旋镖效应”:为什么一次性退出机制对我无效 我刚开始的时候,尝试过自己动手做。我找到了退出页面,提交了请求,然后眼睁睁地看着我的数据消失了。我以为自己很安全。但74天后,我的信息就恢复了。 这就是我所说的“回旋镖效应”。数据经纪商使用自动爬虫程序不断重新抓取公共记录。单个删除请求几乎毫无用处。正是由于这种残酷的现实,我现在只推荐具有持续、积极的重新监控功能的自动化数据删除服务。 我如何评估这些数据保护服务 我不仅阅读了他们的营销文案,我还投入了自己的数据进行验证。在 10 个月的时间里,我根据四个严格的标准对每个数据经纪商删除服务进行了评分: 长期抑制:我的数据是否一直被隐藏,还是在服务提供商未察觉的情况下悄悄重新出现? 扫描频率:我严厉处罚了那些每月只检查一次我状态的服务。2026年起,每周或实时扫描将成为强制性要求。 数据库质量:我不仅统计了经纪人的数量,还检查了他们是否真的瞄准了高风险、高流量的寻人网站。 透明度:控制面板是否真的向我显示了移除的证明,还是仅仅显示了一个模糊的“正在处理”的旋转图标? 我的首选:Incogni(一劳永逸的冠军) 我的评分: ★★★★★ 5.0 / 5.0 费用:约 6.49 美元/月(年付计划) 最适合: 90% 的用户,他们希望获得最大程度的保护,而无需任何日常操作。 由 Surfshark 的网络安全资深人士打造的 Incogni 让我彻底惊艳。安装过程不到三分钟。我实际上授予了他们代理权,让他们根据 GDPR 和 CCPA 框架作为我的法律代理人。从那一刻起,他们的系统开始向 180 多家最激进的数据经纪商发出具有法律约束力的删除请求。 我最喜欢 Incogni 的地方就是它的仪表盘。它干净、实时,并准确地向我显示哪些经纪商拥有我的数据以及何时成功清除这些数据。每月大约只需 6.49 美元,绝对是业内性价比最高的选择。它通过在经纪人试图重新挂牌出售我的产品时立即自动重新提交请求,完全消除了“回旋镖效应”。 我的优点: 无与伦比的性价比。 真正的全球覆盖(即使您身处欧盟以外,也能利用严格的欧盟 GDPR 法规)。 我这边无需任何人工操作。 我的缺点: 经纪人列表(180+)经过精心筛选,但比 DeleteMe 的经纪人列表要小。 对于极其特殊的极端案例,没有专用的人工个案经理。 👉 点击此处查看我的隐身设置 我的第二个选择:DeleteMe(处理复杂案例的重量级选手) 我的评分: ★★★★★ 4.8 / 5.0 费用:约 10.75 美元/月(年度计划) 最适合:姓名常见、曾居住过多个地址或高风险我的。 如果说 Incogni 是一个高效的狙击手,那么 DeleteMe 就是一个完整的战术小队。他们覆盖了超过 750 家数据经纪商——这是我见过的最大的网络。但我之所以一直使用 DeleteMe(并向名字很常见的家人推荐它),真正的原因是它采用的混合方法。他们使用自动化技术,但也雇佣真正的隐私专家,手动与试图拒绝自动化请求的顽固经纪人作斗争。 每个季度,我都会收到一份详细的、有据可查的报告,其中详细列出了我的专用的团队具体做了哪些工作。虽然成本更高,但对于复杂的数字足迹而言,这种人工监管绝对物有所值。 我的优点: 庞大的经纪商数据库,包含超过750家经纪商。 那些顽固难除的黑点都由真人处理。 优秀的家庭保险计划,可保障您的配偶和子女。 我的缺点: 比 Incogni 贵得多。 报告是按季度发布的,所以你无法获得实时仪表盘更新带来的那种即时多巴胺刺激。 点击此处查看DeleteMe的计划 我测试过的最佳 Incogni 替代方案 虽然 Incogni 和 DeleteMe 位居榜首,但我知道每个人的需求都不同。如果您正在寻找Incogni 的替代方案,以下是我对其他主要参与者的简要看法: Optery(#3):我喜欢它们的透明度。他们会在删除你的个人资料之前,先给你看泄露资料的截图。非常适合预算有限(每月约 3.99 美元)的视觉学习者。 Aura(#4):如果您想一举两得,Aura 将数据隐私服务与顶级 VPN、防病毒软件和信用监控服务捆绑在一起。 Privacy Bee(#5):这是为隐私爱好者准备的。它对目标数据类型提供了极其精细的控制,但学习曲线有点陡峭。 OneRep(排名第6):快速高效的自动化。速度方面表现出色,位列第二,不过他们的客户支持响应速度不如 Incogni。 DIY方法:我是如何尝试免费删除数据(但失败了)的 人们总是问我如何才能免费从互联网数据库中删除个人信息。我试过了。这就是我周末的安排: 我在 Spokeo、Whitepages、BeenVerified 和 MyLife 上搜索了我的名字。 我到处寻找“请勿出售我的信息”链接,它们通常以很小的字体隐藏在页面底部。 我上传了我的身份证件,验证了我的邮箱,并填写了验证码。 我设置了日历提醒,60天后再重复一遍。 我花了14个小时。两个月后,我的数据有 80% 恢复在线。除非你的风险承受能力极低,而且你认为你的空闲时间价值低于每小时 2 美元,否则付费使用像 Incogni 这样的数据删除服务绝对是明智之举。你的时间比一个月几杯咖啡的钱更有价值。 常见问题解答(来自我的收件箱) 数据经纪商移除服务真的有效吗? 是的,但前提是它们包含持续的再监测。我历时 10 个月的测试证明,一次性服务都是骗局。经纪人会不断地重新抓取公共记录。Incogni 和 DeleteMe 等工具之所以有效,是因为它们就像无情的法律监督者,不断地压制你的数据。 Incogni 比 DeleteMe 更好吗? 对于我的绝大多数读者来说,答案是肯定的。Incogni 提供更优惠的价格、全球法律服务范围和实时仪表盘。我只建议那些拥有非常复杂的数字足迹(多次婚姻、很多过去的住址)或者特别希望由人工代理人代表他们争取权益的人升级到 DeleteMe。 如果我取消订阅会怎样? 这是人们普遍的担忧。如果您取消 Incogni 或 DeleteMe 等服务,他们将停止发送新的屏蔽请求。由于“回旋镖效应”,数据经纪人最终会在几个月内从公共记录中重新抓取你的信息,并重新将你列入名单。把这些服务想象成保护隐私的健身房会员卡——你必须保持会员资格才能受到保护。 关于保护你的数字足迹的最终结论 生活在 2026 年意味着要接受数据经纪经济的残酷现实。您的个人信息现在正被打包出售,为人工智能诈骗和社会工程攻击提供资金。什么都不做就等于主动选择让自己处于弱势地位。 经过数百小时的测试,我的建议很简单:从 Incogni 开始,实现全球基础防护的自动化。如果你的情况很混乱,或者你想在 750 家经纪商中进行最广泛的筛选,请升级到 DeleteMe。 将您选择的服务与一款优秀的密码管理器搭配使用,启用硬件密钥双因素身份验证,并停止让互联网将您的私生活当作公共财产。今天就重新掌控自己的命运。 Re: I Tested 10 Data Removal Services: Here Are the Best Data Removal Services for 2026 嗨Jakyz 感谢您联系恩智浦半导体并对我们的产品感兴趣。 请问您的咨询是否与恩智浦的任何特定产品或设备有关?请与我们联系。 如果您需要进一步的帮助,我们很乐意效劳。 请访问我们的恩智浦(NXP)网站,查找您需要的零件: https://www.nxp.com/ 如果您的问题与恩智浦产品无关,恐怕我们在这方面提供详细支持的能力有限。非常感谢您的理解。 如有需要,请随时分享更多详情——我们非常乐意尽我们所能提供帮助。 BR 莉娜
View full article
10種類のデータ削除サービスをテストしました:2026年版、最高のデータ削除サービスはこちら 私の10ヶ月間の実験:2026年に最高のデータ削除サービスを見つける 数ヶ月前、私は大きな衝撃を受けた。自分の名前を適当な検索エンジンに入力すると、現在のホーム住所、電話番号、さらには親戚の名前までもが、怪しい検索サイトに何十もの登録されているのを見て愕然としました。数週間も標的型スパム電話を受け続け、AIを利用した個人情報盗難を心配していた私は、行動を起こすことにした。私は過去10ヶ月間、マーケットにある主要な データ削除サービスを 自らテストし、どれが約束を果たすかを見極めました。 手作業で何時間も無駄にし、複数のサブスクリプションを浪費した後、ようやく自分のデジタルフットプリントを真に保護してくれるツールを見つけました。私の試行錯誤を省きたいなら、まず最初に私のおすすめを以下に挙げます。 👉 Incogniを試してみてください。私の一番のおすすめです。完全自動化されていて、驚くほど手頃な価格(月額約6.49ドル)で、世界中の法務手続きを代行してくれます。 👉 DeleteMeを試してみてください — 私のプレミアムピックです。共通の名前や複雑なプライバシー状況をお持ちでも、彼らの人間支援チームと膨大な750+のブローカーデータベースは比類なきものです。 目覚めのきっかけ:私がこの旅を始めた理由 正直に言うと、10年前は、データブローカーのサイトに自分のデータが掲載されるということは、せいぜいテレマーケティングの電話が少し増える程度だった。2026年、事態は恐ろしいほど深刻だ。悪意のある者たちは、これらのサイトをスクレイピングして生成AIモデルに提供しています。私の露出した伝記データは、実質的に音声クローン、ディープフェイクなりすまし、超パーソナライズされたフィッシング攻撃の設計図であることに気づきました。プライバシーはもはやスパムを避けるだけのものではありません。それは個人のセキュリティの根本的な層です。 「ブーメラン効果」:なぜ一度限りのオプトアウトは私には効果がなかったのか 最初に始めた頃は、自分で全てをやってみようと試みました。私はオプトアウトページを見つけ、リクエストを送信し、自分のデータが消えていくのを見守った。私は安全だと思っていた。しかし、ちょうど74日後、私の情報はすぐに元に戻った。 これが私が「ブーメラン効果」と呼ぶものです。データブローカーは、公開されている記録を継続的に収集する自動クローラーを使用する。削除依頼が1件だけでは、ほとんど意味がありません。こうした厳しい現実があるからこそ、私は現在、継続的かつ積極的な再監視機能を備えた自動データ削除サービスのみを推奨しているのです。 これらのデータ保護サービスをどのように評価したか 私は彼らの宣伝文句を読んだだけではなく、自分のデータも投入して検証した。私は10ヶ月間にわたり、各データブローカーの削除サービスを4つの厳格な基準に基づいて評価しました。 長期的なデータ隠蔽:私のデータは隠されたままだったのか、それともサービス提供者が気づかないうちにひっそりと再出現したのか? スキャン頻度:月に一度しかステータスを確認しないサービスには、厳しいペナルティを課しました。2026年には、週次またはリアルタイムのスキャンが義務付けられる。 データベースの品質: 単にブローカーの数を数えただけでなく、彼らが実際に高リスクでアクセス数の多い人探しサイトをターゲットにしているかどうかも確認しました。 透明性: ダッシュボードは実際に削除の証拠を示していたのでしょうか、それとも漠然とした「プロセッシング」スピナーだけだったのでしょうか? 私のイチオシ:インコグニ(設定したらあとはお任せの王者) 私の評価: ★★★★★ 5.0 / 5.0 費用: 月額~$6.49(年間プラン) 最適: 日々の努力ゼロで最大限の保護を求めるユーザーの90%。 Surfsharkのサイバーセキュリティのベテランたちが開発したIncogniは、私を完全に驚かせた。セットアップには3分もかかりませんでした。私は基本的に、GDPRおよびCCPAの枠組みの下で、彼らに私の法的代理人として行動する権限を与えました。その瞬間から、彼らのシステムは、最も攻撃的なデータブローカー180社以上に対し、法的拘束力のある削除要求を次々と送信し始めた。 Incogniで一番気に入っているのはダッシュボードです。これはクリーンでリアルタイムであり、どのブローカーが私のデータを保持していたか、そしていつデータが正常に削除されたかを正確に示してくれます。月額約6.49ドルという価格は、間違いなく業界で最もお得な価格です。ブローカーが私の物件を再掲載しようとした瞬間に自動的に再申請を行うことで、「ブーメラン効果」を完全に無効化します。 私の長所: 比類のない価格性能比。 真のグローバル展開(EU域外にいても、厳格なEU一般データ保護規則(GDPR)を活用できます)。 私の側では一切の手作業は必要ありません。 私の短所: ブローカーリスト(180以上)は厳選されているが、DeleteMeのリストよりは少ない。 非常に特殊な例外CASEに対して専任の人間のCASEマネージャがいないこと。 👉 私のIncogniの設定はこちらをご覧ください 私の#2のおすすめ:DeleteMe(複雑なCASE向けのヘビー級) 私の評価: ★★★★★ 4.8 / 5.0 費用:月額約10.75ドル(年次計画) 最適な対象: 共通名、複数の過去住所、または高リスクプロファイルのユーザー。 インコグニが非常に効率的なスナイパーだとすれば、デリートミーは完全な戦術部隊だ。彼らは750社以上のデータブローカーを網羅しており、私がこれまで見た中で最大のネットワークだ。しかし、私がDeleteMeを武器庫に置き続け(そして非常に一般的な名前を持つファミリにも勧める)本当の理由は、彼らのハイブリッドなアプローチにあります。彼らはオートメーションを利用していますが、実際の人間のプライバシー専門家も雇い、頑固なブローカーが自動リクエストを拒否しようと手作業で戦っています。 毎四半期、専任チームが何をしたかを詳細に文書化した報告書を受け取ります。費用は高くなりますが、複雑なデジタルフットプリントに関しては、人間の監視による確認は費用に見合う価値があります。 私の長所: 750社以上のブローカーを擁する大規模なデータベース。 頑固で除去しにくい部位は、実際に人間が対処します。 配偶者や子どもをカバーする優れたファミリプラン。 私の短所: Incogniよりも明らかに高価です。 報告は四半期ごとに行われるため、リアルタイムのダッシュボード更新による即座のドーパミンの刺激はありません。 DeleteMeの計画はこちらでご確認ください 私が試した中で最高のIncogni代替アプリ IncogniとDeleteMeがトップの座を獲得しましたが、人それぞれニーズが異なることは承知しています。Incogniの代替となる主要なサービスをお探しの方のために、他の主要サービスについて簡単に紹介します。 Optery(#3):彼らの透明性が気に入りました。彼らは、あなたの公開されたプロフィールを削除する前に、実際にスクリーンショットを見せてくれます。予算を抑えたい視覚学習者に最適です(月額約3.99ドル)。 Aura (#4): 一石二鳥を狙うなら、Auraはデータ プライバシーサービス に最高級のVPN、ウイルス対策、クレジットモニタリングを組み合わせて提供しています。 プライバシービー2: これはプライバシーオタクのためのものだ。対象となるデータタイプを非常に細かく制御できるという利点があるが、習得にはやや時間がかかる。 OneRep (#6): 迅速かつ積極的なオートメーション。スピード面では堅実な次点ですが、カスタマーサポートはIncogniほどの対応は良くありません。 DIYアプローチ:無料でデータを削除しようと試みた方法(そして失敗した方法) 人々はいつも私に、お金を払わずにインターネット上のデータベースから個人情報を削除する方法を尋ねてきます。試してみました。私の週末はこんな感じでした。 Spokeo、Whitepages、BeenVerified、MyLifeで自分の名前を検索しました。 私は「個人情報の販売を拒否する」というリンクを探したが、それはたいていページの最下部に小さな文字で隠されていた。 私は身分証明書をアップロードし、メールアドレスを確認し、CAPTCHAを入力しました。 60日後に同じことをもう一度行うように、カレンダーにリマインダーを設定しました。 14時間かかりました。2か月後、私のデータの80%が復旧した。リスク許容度が極めて低く、自由時間を時給2ドル未満と評価するのでない限り、Incogniのようなデータ削除サービスに料金を支払うことは、全く迷う必要のない選択です。あなたの時間は、月にコーヒー2杯分の値段よりもずっと価値があります。 よくある質問(受信箱から) データブローカーによるデータ削除サービスは本当に効果があるのか? はい、ただし継続的な再監視が含まれている場合に限ります。10ヶ月間のテストの結果、一度きりのサービスというのは詐欺であることが証明されました。ブローカーは公的記録を絶えず再収集している。IncogniやDeleteMeのようなツールが機能するのは、それらが執拗な法的監視役として働き、あなたのデータを際限なく抑制するからです。 IncogniはDeleteMeより優れていますか? 私の読者の大多数にとって、答えはイエスです。Incogniは、より優れた価格、グローバルな法的サービス範囲、そしてリアルタイムのダッシュボードを提供します。私がDeleteMeへのアップグレードを勧めるのは、デジタルフットプリントが非常に複雑な場合(複数回の結婚歴、多数の過去の住所など)か、あるいは人間のエージェントに自分の代わりに戦ってもらいたい場合のみです。 定期購読を解約するとどうなりますか? これはよくある不安です。IncogniやDeleteMeのようなサービスを解約すると、新たな配信停止リクエストの送信が停止されます。「ブーメラン効果」のため、データブローカーは数ヶ月以内に公開記録からあなたの情報を再び収集し、あなたを再びリストに掲載するでしょう。これらのサービスはプライバシーのためのジム会員権のようなものだと考えてください。保護のためには有効にしておく必要があります。 デジタルフットプリントの保護に関する私の最終的な結論 2026年に生きるということは、データブローカー経済が容赦なく続くことを受け入れることを意味する。あなたの個人情報は今まさにパッケージ化され販売されており、AI詐欺やソーシャルエンジニアリング攻撃の餌となっています。何もしないということは、脆弱な状態に留まることを積極的に選択しているのと同じだ。 数百時間に及ぶテストの結果、私の助言はシンプルです。まずはIncogniを使って、グローバルなベースライン保護を自動化することから始めましょう。状況が複雑な場合や、750社のブローカーに最大限にアプローチしたい場合は、DeleteMeにアップグレードしてください。 選んだサービスを良いパスワードマネージャーと組み合わせ、ハードウェアキーの2段階認証を有効にし、インターネットがあなたの私生活を公共の所有物のように扱うのをやめましょう。今日こそ主導権を取り戻そう。 Re: I Tested 10 Data Removal Services: Here Are the Best Data Removal Services for 2026 こんにちは、 Jakyzさん NXPにご連絡いただき、また当社の製品にご関心をお寄せいただき、ありがとうございます。 ご質問が特定のNXP製品やデバイスに関連していれば教えていただけますか? もしSOであれば、さらにお手伝いいたします。 必要な部品については、NXPのウェブサイトをご確認ください。 https://www.nxp.com/ もしご質問がNXP製品に関係ない場合、このCASEに関して詳細なサポートは限られている可能性があります。ご理解いただき、誠にありがとうございます。 もし詳細があれば、ぜひお気軽に共有してください。できる限りお手伝いできることをいつでも喜んでいたします。 BR リナ
View full article
恩智浦微控制器 - MCX 概览页面(日语博客) 介绍   在开发工业和物联网设备时,不仅需要处理能力,还需要模拟性能来精确捕获传感器信号、实时控制、通信接口、安全性、功耗以及允许长期产品部署的开发环境。 NXP 的 MCX 是一款基于 Arm Cortex-M 内核的微控制器产品组合,可满足从通用控制到高性能边缘处理、低功耗运行、功能安全和无线通信等各种嵌入式设备需求。 本页面概述了MCX的各项特性、基于其功能性选择MCX的原因、各系列产品之间的区别,以及帮助您入门开发的资源。请以此作为产品选择的起点。   目录   1. 从功能角度选择MCX的原因 2. MCX系列简介 3. 评估和发展入门资源 4. 结论     1. 从功能角度选择MCX的原因   我们汇总了已采用MCX的用户对其功能的反馈!我们将介绍其规格以及相关文章。 功能 专题文章及精选文章 安全 根据产品和系列的不同,可能包含安全启动、安全更新、Arm TrustZone、加密加速器、密钥管理和生命周期管理等功能。 ✓提供安全功能,为遵守网络安全法规(如CRA )和国家/地区认证/标签系统(如日本的JC-STAR)奠定基础。 ✓使用 MCX N,信任根可以在硬件(内部 ROM)中实现,从而使安全启动更加安全。 ✓ MCX A5 还具有PQC(后量子密码学)功能。 ✓部分产品已获得 SESIP 等第三方认证,可作为证据使用。 NXP Security - 摘要页面(日语博客) 16位ADC 部分产品配备 16 位 ADC、多个 ADC、差分输入和内部/外部触发。 ✓高分辨率地捕获传感器信号、电机电流、位置信息等,减少了对外部组件的需求。 [MCX A153] ADC模块基础知识及使用方法 FlexIO 一款灵活的外设,可用于通用串行通信、定时生成等。 ✓您可以选择您喜欢的通信接口:UART、SPI 或 I²C。 ✓还可以进行定时设置和自定义专有协议。 内容发布计划于2026年11月进行。 边缘人工智能 MCX N 系列中的某些产品配备了 eIQ Neutron NPU。 ✓ EdgeAI 的入门级型号。 ✓ 通过使用 eIQ 工具 ,我们支持从转换推理模型到在微控制器上实现 图像 识别 、 异常检测 和其他推理过程的一切操作。 【简介】MCX N947:AI/ML图像识别示例代码实现 eIQ时间序列工作室(时间序列模型开发工具)概述及使用方法 其他显著特点 电机控制、I3C、CAN FD、以太网、USB、功能安全、低功耗、开发环境等。 “FRDM 会议室”内提供各种内容。   *并非所有MCX产品都具备安全特性、16位ADC、FlexIO和边缘AI功能。购买前请查看适用系列和型号的规格说明。 返回页面顶部   功能以外的特性 除了上述功能外,它还具有以下特点: ✓产品线丰富——您可以根据性能、内存、外设和包装等方面的需求,选择最合适的产品。 ✓支持长期设计——稳定供应和长期产品供应—— ✓共享开发经验– 从产品选择到开发,以及早期实施实际设备测试 –       2. MCX系列简介   MCX系列针对每种应用都具有独特的功能,并提供多种型号。请参考以下内容选择合适的系列。   系列 主要特点和功能 易于考虑的用途 MCX N 高性能/人工智能 配备人工智能加速器(NPU) 双核Cortex-M33处理器,最高频率可达150MHz 高达 2 MB 的闪存,512 KB 的 SRAM,184 个引脚 eIQ Neutron NPU,高安全性,摄像头,显示器,音频等。 边缘人工智能、图像、音频、人机交互、高安全性 MCX A 通用电机控制 通用微控制器 Arm Cortex-M33,最高频率可达 240MHz 高达 1 MB 的闪存,256 KB 的 SRAM,144 个引脚 模拟、ADC、运算放大器、PWM、USB、CAN FD、I3C 等。 传感、控制、电机、人机界面 MCX L 超低功耗 低功耗运行 双核 Arm Cortex-M33 处理器,最高频率 96 MHz + Arm Cortex-M0+ 处理器,频率 10 MHz 高达 512 KB 的闪存,128 KB 的 SRAM,184 个引脚。 适用于连续传感和始终开启应用的配置 传感器节点、智能电表、电池设备 MCX C 适合初学者且价格低廉 成本效益 Arm Cortex-M0+,最高频率可达 48MHz 高达 256 KB 的闪存和 32 KB 的 SRAM,64 针连接器。 低功耗、模拟、USB、段式液晶显示等。 基本控制,低成本设备 MCX E 安全可靠 5V兼容微控制器 Arm Cortex-M4F/M7,最高频率可达 160MHz 高达 4 MB 的闪存,128 KB 的 SRAM,172 个引脚 功能安全、CAN FD、以太网、TSN、电机控制等。 工业控制、电机、运输、医疗 MCX W 短距离无线 低功耗微控制器,具备短距离无线功能 Arm Cortex-M33,最高频率可达96MHz 最高 2 MB 闪存,256 KB SRAM Bluetooth LE、Matter、Thread、Zigbee 等(因产品而异) 智能家居、传感器、智能能源 RW612 具备 Wi-Fi 功能 兼容 Wi-Fi 6 的微控制器 Arm Cortex-M33,最高频率可达 260MHz 四路 FlexSPI 闪存接口,1.2MB SRAM 集成了 Wi-Fi 6、蓝牙 LE 5.4 和 802.15.4。 Wi-Fi 设备、工业和智能家居   *虽然 RW612 不属于 MCX W 系列,但它在这里被列为支持 Wi-Fi 的 MCU。 返回页面顶部     3. 评估和发展入门资源 所有用于启动评估和开发的资源都汇总在“ FRDM 会议室”中。如果您希望继续进行评估和开发,请参阅该会议室。 资源示例 说明 FRDM开发板 负责评估和开发MCX产品的委员会。 价格低廉,并且与 Arduino 和 PMOD 等外形尺寸兼容。 开发环境 MCUXpresso 开发者体验 使用 SDK 创建、构建和调试项目。 SDK/RTOS 使用 NXP SDK 示例和 Zephyr OS 进行软件开发。 应用渠道中心 搜索与目标设备兼容的示例代码和应用程序示例。 返回页面顶部     4. 结论 MCX 是一个产品组合,可满足工业和物联网设备的广泛需求,从通用控制、传感和电机控制到边缘人工智能、功能安全、超低功耗和无线通信。 首先,请查看产品页面,找到最符合您需求的系列产品,然后使用 FRDM 开发板和 MCUXpresso 开始您的实际评估。有关如何使用各项功能和评估流程的具体说明,我们将陆续发布在 NXP 社区技术博客上,您也可以在“FRDM 开发板专区”中找到相关信息。 查看MCX产品组合 查看“FRDM 会议室” 返回页面顶部     ========================== 我们目前无法回复此帖子“评论”部分留下的评论。 对于由此造成的不便,我们深表歉意,但在进行咨询时,请参考“ NXP 技术问题 - 如何联系我们(日语博客) ”。 (如果您已经是恩智浦的分销商或与恩智浦有合作关系,您可以直接咨询您的代表。) NXP 的 MCX 是一款基于 Arm Cortex-M 内核的微控制器产品组合,可满足从通用控制到高性能边缘处理、低功耗运行、功能安全和无线通信等各种嵌入式设备需求。 本页面概述了MCX的各项特性、基于其功能性选择MCX的原因、各系列产品之间的区别,以及帮助您入门开发的资源。请以此作为产品选择的起点。 MCX 日本博客
View full article
NXP Microcontrollers - MCX Summary Page (Japanese Blog) Introduction   In developing industrial and IoT devices, not only processing power is required, but also analog performance to accurately capture sensor signals, real-time control, communication interfaces, security, power consumption, and a development environment that allows for long-term product deployment. NXP's MCX is a microcontroller portfolio based on the Arm Cortex-M core, addressing a wide range of embedded device requirements, from general-purpose control to high-performance edge processing, low-power operation, functional safety, and wireless communication. This page summarizes the features of MCX, the reasons why it's chosen based on its functionality, the differences between each series, and resources to get you started with development. Please use this as a starting point for product selection.   table of contents   1. Reasons why the MCX is chosen from a functional standpoint 2. Introduction to the MCX Series 3. Resources for getting started with evaluation and development 4. In conclusion     1. Reasons why the MCX is chosen from a functional standpoint   We've compiled feedback from users who have adopted MCX regarding its functionality! We'll introduce not only the specifications but also related articles. function Features & Featured Articles security Depending on the product and series, features such as secure boot, secure updates, Arm TrustZone, cryptographic accelerators, key management, and lifecycle management are included. ✓ Provides security functions that serve as a foundation when considering compliance with cybersecurity regulations such as CRA , and national/regional certification/labeling systems such as Japan's JC-STAR . ✓ With MCX N, the Root of Trust can be implemented in hardware (internal ROM) , making secure boot more secure. ✓ The MCX A5 also features PQC (Post-Quantum Cryptography) functionality. ✓ Some products have obtained third-party certifications such as SESIP, and can be used as evidence. NXP Security - Summary Page (Japanese Blog) 16-bit ADC Some products feature 16-bit ADCs, multiple ADCs, differential inputs, and internal/external triggers. ✓ Captures sensor signals, motor current, position information, etc. with high resolution , reducing the need for external components. [MCX A153] Basics and Usage of the ADC Module FlexIO A flexible peripheral that can be used for general-purpose serial communication, timing generation, and more. ✓ You can choose your preferred communication interface: UART, SPI, or I²C. ✓ Timing settings and customization to proprietary protocols are also possible. Content release scheduled for November 2026. Edge AI Some products in the MCX N series are equipped with the eIQ Neutron NPU. ✓ An entry-level model of EdgeAI. ✓ By using eIQ tools , we support everything from converting inference models to implementing them on microcontrollers for image recognition , anomaly detection , and other inference processes. [Introduction] MCX N947: AI/ML Image Recognition Sample Code Implementation Overview and usage of eIQ Time Series Studio (time series model development tool) Other notable features Motor control, I3C, CAN FD, Ethernet, USB, functional safety, low power consumption, development environment, etc. Various content is available in the "FRDM Board Room".   *Security features, 16-bit ADC, FlexIO, and Edge AI are not common to all MCX products. Please check the specifications of the applicable series and model number when considering your purchase. Return to top of page   Features other than functionality In addition to its functionality, it also has the following features: ✓ Extensive lineup – Choose the product that best suits your needs in terms of performance, memory, peripherals, and packaging. ✓Supporting long-term design – stable supply & long-term product supply – ✓ Shared Development Experience – From Product Selection to Development, Early Implementation of Actual Device Testing –       2. Introduction to the MCX Series   The MCX series has unique features for each application and is offered in various forms. Please use the following as a starting point for selecting a series.   series Main features and functions Easy-to-consider uses MCX N High performance/AI Equipped with an AI accelerator (NPU) Dual Arm Cortex-M33 @ up to 150 MHz Up to 2 MB of flash memory, 512 KB of SRAM, 184 pins eIQ Neutron NPU, high security, camera, display, audio, etc. Edge AI, images, audio, HMI, high security MCX A General-purpose motor control General-purpose microcontroller Arm Cortex-M33 @up to 240MHz Up to 1 MB of flash memory, 256 KB of SRAM, 144 pins Analog, ADC, op-amp, PWM, USB, CAN FD, I3C, etc. Sensing, control, motors, HMI MCX L Ultra low power consumption Low power operation Dual Arm Cortex-M33 @ up to 96 MHz + Arm Cortex-M0+ @ 10 MHz Up to 512 KB of flash memory, 128 KB of SRAM, 184 pins. Configuration for continuous sensing and always-on applications Sensor nodes, smart meters, battery devices MCX C Beginner-friendly and low-cost Cost efficiency Arm Cortex-M0+ @up to 48MHz Up to 256 KB of flash memory and 32 KB of SRAM, 64-pin connector. Low power consumption, analog, USB, segment LCD, etc. Basic control, low-cost equipment MCX E Safe and robust 5V compatible microcontroller Arm Cortex-M4F/M7 @up to 160MHz Up to 4 MB of flash memory, 128 KB of SRAM, 172 pins Functional safety, CAN FD, Ethernet, TSN, motor control, etc. Industrial control, motors, transportation, medical MCX W short range wireless Low-power microcontroller with short-range wireless capabilities Arm Cortex-M33 @up to 96MHz Up to 2 MB of flash memory, 256 KB of SRAM Bluetooth LE, Matter, Thread, Zigbee, etc. (varies depending on the product) Smart home, sensors, smart energy RW612 Wi-Fi enabled Wi-Fi 6 compatible microcontroller Arm Cortex-M33 @up to 260MHz Quad FlexSPI flash interface, 1.2MB SRAM Integrates Wi-Fi 6, Bluetooth LE 5.4, and 802.15.4. Wi-Fi devices, industrial and smart home   *Although the RW612 is not part of the MCX W series, it is listed here as a Wi-Fi enabled MCU. Return to top of page     3. Resources for getting started with evaluation and development All resources for starting evaluation and development are compiled in the " FRDM Board Room ." Please refer to this if you wish to proceed with evaluation and development. Resource examples explanation FRDM development board A board for evaluating and developing MCX products. Inexpensive and compatible with form factors such as Arduino and PMOD. Development environment MCUXpresso Developer Experience Project creation, building, and debugging using the SDK. SDK / RTOS Software development using NXP SDK samples and Zephyr OS. Application Channel Hub Search for sample code and application examples compatible with the target device. Return to top of page     4. In conclusion MCX is a portfolio that addresses a wide range of requirements for industrial and IoT equipment, from general-purpose control, sensing, and motor control to edge AI, functional safety, ultra-low power consumption, and wireless communication. First, check the product page for the series that best suits your needs, and then begin your hands-on evaluation with the FRDM development board and MCUXpresso. Specific instructions on how to use the features and evaluation procedures are being published sequentially on the NXP Community Tech Blog, which is also introduced in the "FRDM Board Room." View the MCX product portfolio View the "FRDM board room" Return to top of page     ========================== We are currently unable to respond to comments left in the "Comment" section of this post. We apologize for the inconvenience, but please refer to " Technical Questions to NXP - How to Contact Us (Japanese Blog) " when making inquiries. (If you are already an NXP distributor or have a relationship with NXP, you may ask your representative directly.) NXP's MCX is a microcontroller portfolio based on the Arm Cortex-M core, addressing a wide range of embedded device requirements, from general-purpose control to high-performance edge processing, low-power operation, functional safety, and wireless communication. This page summarizes the features of MCX, the reasons why it's chosen based on its functionality, the differences between each series, and resources to get you started with development. Please use this as a starting point for product selection. MCX Japanese Blog
View full article
NXPマイコン - MCXまとめページ (日本語ブログ) はじめに   産業機器やIoT機器の開発では、処理性能だけでなく、センサ信号を正確に取り込むアナログ性能、リアルタイム制御、通信インターフェース、セキュリティ、消費電力、そして長期的に製品を展開できる開発環境が求められます。 NXPのMCXは、Arm Cortex-Mコアをベースに、汎用制御から高性能なエッジ処理、低消費電力動作、機能安全、無線通信まで、さまざまな組込み機器の要件に対応するマイコン・ポートフォリオです。 本ページでは、MCXの特長、機能面から選ばれる理由、各シリーズの違い、開発を始めるためのリソースをまとめます。製品選定の入口として、ぜひご活用ください。   目次   1.機能面からMCXが選ばれる理由 2.MCXシリーズの紹介 3.評価・開発を始めるためのリソース 4.さいごに     1.機能面からMCXが選ばれる理由   MCXの機能面で、採用いただいたユーザー様からの声をピックアップしました!単なる仕様だけでなく、関連する記事も併せて紹介します。 機能 特長 & ピックアップ記事 セキュリティ 製品・シリーズに応じて、セキュアブート、セキュアアップデート、Arm TrustZone、暗号アクセラレータ、鍵管理、ライフサイクル管理などを搭載。 ✓ CRAなどのサイバーセキュリティ規制や、日本のJC-STARのような各国・地域の認証/ラベリング制度への対応を検討する際の基盤となるセキュリティ機能を提供。 ✓ MCX Nでは、Root of Trustをハードウェア(内部ROM)で持たせることができ、セキュアブートがより安全に。 ✓ MCX A5からPQC(耐量子暗号)の機能も備えています。 ✓ SESIP等の第3者認証を取得した製品もあり、エビデンスとしても活用可能。 NXPのセキュリティ ~まとめページ~ (日本語ブログ) 16ビットADC 一部製品に16ビットADC、複数ADC、差動入力、内部・外部トリガなどを搭載。 ✓ センサ信号、モータ電流、位置情報などを高い分解能で取り込み、外付け部品を削減。 [MCX A153] ADCモジュールの基本と使い方 FlexIO 汎用のシリアル通信やタイミング生成などに利用できる柔軟なペリフェラル。 ✓ UART、SPI、I²C好きな通信インターフェースとして選択可。 ✓ タイミング設定や独自プロトコルへのカスタマイズ対応も可能。 コンテンツ公開予定 (2026年11月) Edge AI MCX Nシリーズの一部製品にeIQ Neutron NPUを搭載。 ✓ EdgeAIのエントリーモデル。 ✓ 画像認識、異常検知などの推論をeIQツールを使用することで、推論モデルの変換からマイコンにインプリまでを支援。 [入門]MCX N947: AI/ML画像認識サンプルコード実装 eIQ Time Series Studio(時系列モデル開発ツール)の概要と使い方 その他 注目機能 モータ制御、I3C、CAN FD、Ethernet、USB、機能安全、低消費電力、開発環境等々。 「FRDMボードの部屋」に各種コンテンツを準備   ※セキュリティ機能、16ビットADC、FlexIO、Edge AI、はMCX全製品に共通するものではありません。検討時に、対象シリーズ・型番の仕様をご確認ください。 ページ上部へ戻る   機能面以外の特長 機能面以外にも下記のような特長があります。  ✓ 豊富なラインアップ ~必要な性能/メモリ/ペリフェラル/パッケージから製品を選択~  ✓ 長期設計を支援 ~安定供給 & 長期製品供給~  ✓ 共通の開発体験 ~製品選定から開発まで、早期に実機検証を開始~       2.MCXシリーズの紹介   MCXは用途ごとに特長を持ち、シリーズ展開しています。以下はシリーズ選定の入口としてご利用ください。   シリーズ 主な特長・機能 検討しやすい用途 MCX N 高性能・AI AIアクセラレータ(NPU)搭載 デュアルArm Cortex-M33 @最大150 MHz 最大2 MBのフラッシュ、512 KBのSRAM、184ピン eIQ Neutron NPU、高セキュリティ、カメラ、ディスプレイ、オーディオなど Edge AI、画像、音声、HMI、高セキュリティ MCX A 汎用・モータ制御 汎用マイコン Arm Cortex-M33 @最大240 MHz 最大1 MBのフラッシュ、256 KBのSRAM、144ピン アナログ、ADC、オペアンプ、PWM、USB、CAN FD、I3Cなど センシング、制御、モータ、HMI MCX L 超低消費電力 低消費電力動作 デュアルArm Cortex-M33 @最大96 MHz + Arm Cortex-M0+ @10 MHz 最大512 KBのフラッシュ、128 KBのSRAM、184ピン 常時センシング、Always-on用途向けの構成 センサノード、スマートメータ、バッテリ機器 MCX C 入門・低コスト コスト効率 Arm Cortex-M0+ @最大48 MHz 最大256 KBのフラッシュと32 KBのSRAM、64ピン 低消費電力、アナログ、USB、セグメントLCDなど 基本制御、低コスト機器 MCX E 安全・堅牢 5V対応マイコン Arm Cortex-M4F / M7 @最大160 MHz 最大4 MBのフラッシュ、128 KBのSRAM、172ピン 機能安全、CAN FD、Ethernet、TSN、モータ制御など 産業制御、モータ、輸送、医療 MCX W 近距離無線 省電力の近距離無線対応マイコン Arm Cortex-M33 @最大96 MHz 最大2 MBのフラッシュ、256 KBのSRAM Bluetooth LE、Matter、Thread、Zigbeeなど(製品により異なる) スマートホーム、センサ、スマートエネルギー RW612 Wi-Fi対応 Wi-Fi 6対応マイコン Arm Cortex-M33 @最大260 MHz Quad FlexSPIフラッシュI/F、1.2MBのSRAM Wi-Fi 6、Bluetooth LE 5.4、802.15.4を統合 Wi-Fi機器、産業・スマートホーム   ※RW612はMCX Wシリーズの一製品ではないですが、Wi-Fi対応MCUとして紹介しています。 ページ上部へ戻る     3.評価・開発を始めるためのリソース 評価・開発を始めるためのリソースはすべて「FRDMボードの部屋」にまとめています。評価、開発を進めたい方はこちらをご参考ください。 リソース例 説明 FRDM開発ボード MCX製品の評価・開発をするためのボード。 安価で、Arduino, PMODなどにフォームファクターに対応。 開発環境 MCUXpresso Developer Experience SDKを用いたプロジェクト作成、ビルド、デバッグ。 SDK / RTOS NXP SDKのサンプルやZephyr OSを利用したソフトウェア開発。 Application Code Hub 対象デバイスに対応するサンプルコードやアプリケーション例の検索。 ページ上部へ戻る     4.さいごに MCXは、汎用制御、センシング、モータ制御、Edge AI、機能安全、超低消費電力、無線通信まで、産業機器・IoT機器のさまざまな要件に対応するポートフォリオです。 まずは用途に近いシリーズの製品ページを確認し、FRDM開発ボードとMCUXpressoで実機評価を始めてみてください。具体的な機能の使い方や評価手順は、「FRDMボードの部屋」内でも紹介しているNXP CommunityのTech Blogで順次公開しています。 MCX製品ポートフォリオを見る 「FRDMボードの部屋」を見る ページ上部へ戻る     =========================​ 本投稿の「Comment」欄にコメントをいただいても、現在返信に対応しておりません。​ お手数をおかけしますが、お問い合わせの際には「NXPへの技術質問 - 問い合わせ方法 (日本語ブログ)」をご参照ください。​ (既に弊社NXP代理店、もしくはNXPとお付き合いのある方は、直接担当者へご質問いただいてもかまいません。) NXPのMCXは、Arm Cortex-Mコアをベースに、汎用制御から高性能なエッジ処理、低消費電力動作、機能安全、無線通信まで、さまざまな組込み機器の要件に対応するマイコン・ポートフォリオです。 本ページでは、MCXの特長、機能面から選ばれる理由、各シリーズの違い、開発を始めるためのリソースをまとめます。製品選定の入口として、ぜひご活用ください。 MCX 日本語ブログ
View full article
T4240QDS RGMII 以太网需要在现代内核的设备树中添加固定链路节点 你好, 为了使 T4240QDS RGMII 以太网在现代内核上工作,我采取了在设备树中添加固定链路节点的方法。如果没有进行此修改,尝试启动设备时会显示“SIOCSIFFLAGS: No such device”(ifconfig)或“RTNETLINK answers: No such device”(ip link),日志中没有任何明显的错误。 在 fman 以太网下插入一个固定链路节点可以解决此问题,请参见附图。 我发帖是为了让其他人可以通过搜索找到解决方案,但也想知道这是否是预期/已知的行为?有什么办法能让自动协商功能正常工作吗? 另附上未进行此设备树修改的主线内核的启动日志(以太网无法工作)。使用最新的 nxp-qoriq/linux 内核 6.12 也观察到了同样的行为。 QorIQ T4 设备 Re: T4240QDS RGMII ethernet requires adding fixed-link node in device tree on modern kernel 固定链路是一种权宜之计,并非自动协商的根本解决方案。它绕过正常的 PHY 连接,并告诉 Linux 假定为固定链路。 你的症状表明你存在 PHY 发现/依恋问题。要恢复自动协商,请检查 MAC 的 phy 句柄、MDIO 总线/复用器配置、PHY 地址和已启用的 PHY 驱动程序。
View full article
USB VID/PID 程序仍然处于活动状态吗? 你好, 我们是一家小型公司,正在开发基于 LPC5528 的带 USB CDC 接口的家庭控制器。预计销量远低于1万台。我们希望通过 USB VID/PID 程序申请 NXP VID 下的 PID。 程序常见问题解答 (contact.nxp.com/vid-usb-app) 中链接的申请表不可用,案例门户拒绝了我们的帐户,因为它不是在公司域名上注册的。 该项目目前是否仍在进行?如果仍在进行,目前的申请方式是什么? 谢谢你! Re: USB VID/PID program still active ? 是的,NXP USB VID/PID 程序仍然有效。旧版网页表单(`contact.nxp.com/vid-usb-app`)已被弃用,不再可用。 目前官方的申请方式是通过 NXP 社区门户网站直接创建支持工单。 以下是获取免费PID的步骤: 1. **前往 NXP 社区页面**:导航至 NXP 官方 USB VID/PID 程序页面:[链接] NXP USB VID/PID 程序 2. **创建支持工单**:在该页面的底部,您会看到一个标题为“如需更多详细信息,请创建支持工单”的部分。点击它。 3. **填写工单**:您需要在工单中提供以下详细信息: - 您的公司名称 - 您需要的 PID 数量(最多免费提供 3 个) - 简要描述您的产品及其用途 4. **等待批准**:NXP 将审核您的请求。请注意,从提交申请到收到分配的 PID,整个过程可能需要长达一个月的时间。 **LPC5528 项目重要提示:** - **资格**:LPC 系列(Cortex-M)完全包含在该计划的覆盖范围内。 - **销量限制**:由于您的预期销量低于 10,000 件,因此您符合此计划的资格。如果您的生产批量超过 10,000 台,您需要从 USB.org 获取您自己的 VID。 - **USB 标志**:使用 NXP VID 并不授予您使用 USB-IF 商标标志的许可。如果您想使用该标志,您必须通过 USB-IF 认证流程并拥有自己的 VID。 Re: USB VID/PID program still active ? 非常感谢您的帮助,但很遗憾,我还是原地打转。 由于我们无法将您的电子邮件与公司关联,因此您没有资格在案件门户网站上创建新案件。请使用您的公司邮箱地址登录 NXP.com 或通过 NXP 社区提出您的问题。 我总是得到这样的结果:尽管我们是一家专业的小型工程公司,但我们没有功能域,因为我们不需要它。我认为我们的 GMX 电子邮件地址不被接受,这是最大的问题。 亲切的问候 托马斯 Re: USB VID/PID program still active ? 你好@Thomas_Mundhenke 是的,db16122 的描述是正确的。我会给你发一封私人邮件。请把所有相关信息发给我。谢谢。 BR 爱丽丝
View full article
Coupon claim i am a student, and i want to buy some board which is available with open public coupons i successfully found one but the thing is i want 2-3 boards and the coupon allows one claim on one account, So is it okay if i create one more account and order again by claiming the coupon if it is allowed then it would be helpful. Board Design MCXA Re: Coupon claim Hi Moksh Thanks for reaching out. Based on the coupon usage rules, each account can use one coupon. If you would like to purchase additional boards, you may try registering another account and check whether another coupon is available and eligible for use. For further assistance with board purchases, coupon eligibility, or order placement, we recommend contacting our Online Purchase Team at [email protected]. They will be able to provide further guidance and help resolve any issues during the ordering process. Thank you and have a nice day. BR Lina 
View full article
MPC57xx MBD互換性 こんにちは、 MPC57xxシリーズ用にインストールされたモデルベースデザインツールボックスはバージョン「3.2.0」で、MATLAB/SimulinkのR2016aからR2020aリリース用にドキュメント化されています。同じバージョンをMATLAB R2025b版でも使えますか? もしそうでなければ、MATLAB R2025bにはMPC57xx mbd toolboxのどのバージョンが必要ですか? 問題点:matlab r2025bでMPC57xxベースのコントローラプロジェクトを実行しようとしています。モデルをMatlabで実行すると、ソフトウェアがクラッシュします。 Re: MPC57xx MBD compatibility バージョン3.2.0の公式ドキュメント対象となるのは、MATLAB/SimulinkのリリースR2016aからR2020aまでのみです。R2025bで動かそうとするとインターフェースの互換性が悪化し、MPC57xxモデルを動かそうとするとMATLABがクラッシュするのです。 **現状:** NXPコミュニティの報告によると、MPC57xx用のMBDTはMATLAB 2025a、ましてやR2025bで成功裏にインストールできませんでした。NXPはMATLAB R2025bをサポートするMPC57xx MBDツールボックスの新しいバージョンをリリースしていません。 **選択肢:** | オプション | 何をすべきか | 最適な対象 | |--------|-----------|----------| | **MATLABのダウングレード** | MBD Toolbox 3.2.0を使用してMATLAB R2019bまたはR2020aをインストールします|既存のSimulinkモデルを維持すること;最早の解決策 | |**S32 Design Studioへの移行** |アルゴリズムデザインのみにSimulinkを使用し、Embedded CoderでANSI Cコードを生成し、底層ドライバ付きのS32 Design Studioに統合 |R2025bを使用必須;移行時間を投資する意思がある | |**S32設定ツールを使用** |ピン、クロック、ペリフェラルをグラフィカルに設定して、底層初期化コードを自動生成する |新規プロジェクトや重构設定を希望する方 | **推奨事項:** 既存のSimulinkモデルがコア資産である場合、最も安全な方法は**MATLAB R2020a**にダウングレードすることです。これはMBD Toolbox 3.2.0で公式にサポートされている最高バージョンで、現在のワークフローを維持します。もしR2025bを使う必要があるなら、「MBD自動コード生成」から「Simulinkアルゴリズム+S32 Design Studio統合」ワークフローに移行する必要があります。
View full article
S32K314のPLLロックアウトにより、再起動問題が発生しました。 水晶発振器のレイアウトに誤りがあったため、デジタル信号からの干渉が発生し、以下の問題が発生しました。 Power_Ip_MC_RGM_GetResetReason() は 0x05 を返します 8MHzの水晶発振器を120倍することで、PLL出力は960MHz、動作クロックは160MHz(PHI0、PHI1)となる。低温環境下では再起動を起こしやすい。 8MHzの水晶発振器と80倍の乗算器に変更したところ、PLL出力は640MHz、動作クロックは160MHz(PHI0、PHI1)となり、再起動の問題は発生しなくなりました。 質問: 水晶発振器が受ける干渉は変化していません。変更されたのはPLLの乗算係数のみです。動作メインクロック周波数160MHzも変更されていません。ここで改善された耐干渉対策の技術的な説明は何でしょうか?温度に関連する要因は何でしょうか?よろしくお願いいたします。 Re: S32K314的PLL失锁造成重启的问题 こんにちは@ Allen_zhang_202 4 以下は単なる経験的分析である。 PHI0とPHI1はどちらも最終的には160MHzで動作しますが、PLLの内部動作状態は2つの構成で全く異なります。 8 MHz × 120 = 960 MHz、それを160 MHzで割る 8 MHz × 80 = 640 MHz、それを160 MHzで割る 問題はおそらく最終的な160MHzではなく、PLLの内部VCO動作周波数、ループマージン、ロックイン検出マージン、および低温時の水晶発振器駆動能力にあると考えられます。PLLの内部周波数を960MHzから640MHzに下げることで、PLLのロックインマージンが増加し、同じ水晶発振器の干渉によってPLLのロックが失われる可能性が低くなります。 しかし、これは「PLLの干渉耐性を高める」ようなものであり、水晶発振器のレイアウト問題を実際に解決するものではないことに注意することが重要です。 Re: S32K314的PLL失锁造成重启的问题 こんにちは、センレント こんにちは。ご返信ありがとうございます。添付ファイルについてお伺いしたいのですが、S32K314 に適用できるものでしょうか?もし適用できない場合、S32K314 に適用できる新しいドキュメントはありますでしょうか?もしあれば、教えていただけると幸いです。よろしくお願いいたします。 Re: S32K314的PLL失锁造成重启的问题 こんにちは@ Allen_zhang_202 4 申し訳ありませんが、S32K3に関する該当ドキュメントは存在しません。 AN535は2006年に発行されたため、かなり古いアプリケーションノートです。基本的なメカニズムを理解するには十分ですが、最も包括的なアプリケーションノートとは言えないかもしれません。 S32K3と完全互換。
View full article
クーポン利用 私は学生で、オープンパブリッククーポンで入手可能なボードを購入したいと思っています 見つけましたが、2〜3つのボードが欲しいのに、クーポンは1アカウントで1回のクレームができるのですが、 もう一つアカウントを作成してクーポンを請求して再度注文しても大丈夫でしょうか? もし許可されれば、それは役に立ちます。 ボード設計 MCXA Re: Coupon claim こんにちは、モクシュさん ご連絡ありがとうございます。 クーポン使用ルールに基づき、 各アカウントは1つのクーポンを使用CANできます。追加のボードを購入したい場合は、別のアカウントを登録して、別のクーポンが利用可能かどうか、また使用できるかどうかを確認してみてください。 基板の購入、クーポンの利用資格、または注文方法についてさらにサポートが必要な場合は、オンライン購入チーム([email protected])までお問い合わせください。 彼らはさらなる指導を提供し、ご注文過程で問題を解決する手助けをしてくれます。 ありがとうございました。良い一日をお過ごしください。 BR リナ
View full article
The S32K314's PLL lockout caused a restart issue. An error in the crystal oscillator layout caused interference from digital signals, resulting in the following issues: Power_Ip_MC_RGM_GetResetReason() returns 0x05 The 8MHz crystal oscillator, multiplied by 120, has a PLL output of 960MHz and a working clock of 160MHz (PHI0, PHI1). It is prone to restarting at low temperatures. After modifying it to an 8MHz crystal oscillator with an 80x multiplier, the PLL output is 640MHz, and the operating clock is 160MHz (PHI0, PHI1), the rebooting issue no longer occurs. Question: The interference experienced by the crystal oscillator remains unchanged; only the PLL multiplication factor has been modified. The operating main clock frequency of 160MHz also remains unchanged. What is the technical explanation for the improved anti-interference measures here? What are the temperature-related factors? Thank you! Re: S32K314的PLL失锁造成重启的问题 Hi@ Allen_zhang_202 4 The following is just an empirical analysis Although both PHI0 and PHI1 ultimately operate at 160 MHz, the internal operating states of the PLL are completely different in the two configurations: 8 MHz × 120 = 960 MHz, then divided to 160 MHz 8 MHz × 80 = 640 MHz, then divided to 160 MHz The problem likely lies not in the final 160 MHz, but in the PLL's internal VCO operating frequency, loop margin, lock-in detection margin, and crystal oscillator driving capability at low temperatures. Reducing the PLL's internal frequency from 960 MHz to 640 MHz increases the PLL's lock-in margin, making it less likely for the same crystal oscillator interference to trigger a PLL loss of lock. However, it is important to note that this is more like increasing the "PLL's tolerance to interference" and does not actually solve the crystal oscillator layout problem. Re: S32K314的PLL失锁造成重启的问题 Hi Senlent Hello, thank you very much for your reply. I would also like to ask about the attached file, which is applicable to the S32K314. If not, are there any newer documents applicable to the S32K314? If so, please let me know. Thank you! Re: S32K314的PLL失锁造成重启的问题 Hi@ Allen_zhang_202 4 Sorry, there is no such document for S32K3. AN535 was released in 2006, making it a fairly old application note. While it's perfectly adequate for understanding the underlying mechanisms, it may not be the most comprehensive application. Fully compatible with S32K3.
View full article
MPC57xx MBD compatibility Hi,  The installed Model-Based Design Toolbox for MPC57xx Series is version "3.2.0", which is documented for MATLAB/Simulink releases R2016a through R2020a. Can I use the same version in MATLAB R2025b version also?  If not, which version of mpc57xx mbd toolbox is needed for MATLAB R2025b? Issue: I'm trying to run a mpc57xx based controller project in my matlab r2025b. Whenever the model is run in matlab, the software is crashing.  Re: MPC57xx MBD compatibility The official documentation for version 3.2.0 only covers MATLAB/Simulink releases R2016a through R2020a. Attempting to run it on R2025b causes interface incompatibility, which is why your MATLAB is crashing when you try to run your MPC57xx model. **Current status:** According to NXP Community reports, the MBDT for MPC57xx couldn't even install successfully on MATLAB 2025a, let alone R2025b. NXP has not released a newer version of the MPC57xx MBD Toolbox that supports MATLAB R2025b. **Your options:** | Option | What to do | Best for | |--------|-----------|----------| | **Downgrade MATLAB** | Install MATLAB R2019b or R2020a with MBD Toolbox 3.2.0 | Keeping your existing Simulink models; fastest fix | | **Migrate to S32 Design Studio** | Use Simulink for algorithm design only, generate ANSI C code via Embedded Coder, then integrate into S32 Design Studio with底层 drivers | Must use R2025b; willing to invest migration time | | **Use S32 Configuration Tools** | Graphically configure pins, clocks, and peripherals to auto-generate底层 initialization code | New projects or willing to重构 configuration | **Recommendation:** If your existing Simulink model is a core asset, the safest approach is to **downgrade to MATLAB R2020a** — that's the highest version officially supported by MBD Toolbox 3.2.0 and will preserve your current workflow. If you must use R2025b, you'll need to migrate from "MBD automatic code generation" to a "Simulink algorithm + S32 Design Studio integration" workflow.
View full article
USB VID/PID program still active ? Hello, we are a small company developing a home controller based on the LPC5528 with a USB CDC interface. Expected volume is well below 10,000 units. We would like to apply for a PID under the NXP VID via the USB VID/PID program. The application form linked in the program FAQ (contact.nxp.com/vid-usb-app) is unavailable, and the Case Portal rejects our account because it is not registered on a company domain. Is the program still active, and if so, what is the current way to apply? Thank you! Re: USB VID/PID program still active ? Yes, the NXP USB VID/PID program is still active. The old web form (`contact.nxp.com/vid-usb-app`) has been deprecated and is no longer available. The current official way to apply is by **creating a support ticket** directly through the NXP Community portal. Here are the steps to get your free PID(s): 1. **Go to the NXP Community page**: Navigate to the official NXP USB VID/PID Program page: [链接] NXP USB VID/PID Program 2. **Create a Support Ticket**: At the bottom of that page, you will see a section titled **"For more details, please create a support ticket"**. Click on it. 3. **Fill out the Ticket**: You will need to provide the following details in the ticket: - Your company name - The number of PIDs you need (up to 3 are provided for free) - A brief description of your product and its purpose 4. **Wait for Approval**: NXP will review your request. Please note that the process can take up to a month from submission to receiving your assigned PID(s). **Important Notes for Your LPC5528 Project:** - **Eligibility**: The LPC series (Cortex-M) is fully covered under this program. - **Volume Limit**: Since your expected volume is below 10,000 units, you qualify for this program. If your production run exceeds 10,000 units, you would need to obtain your own VID from USB.org. - **USB Logo**: Using the NXP VID does not grant you the license to use the USB-IF trademarked logo. If you wish to use the logo, you must go through the USB-IF certification process and have your own VID. Re: USB VID/PID program still active ? Thanks a lot for your help, but unfortunately I'm running in circles As we are not able to link your email with a company, you are not eligible to create a new case on the Case Portal. Please use your company email address to log into NXP.com or raise your question via NXP community. Thats what I always get, despite we're a professional small engeneering office we don't own a domain simply because we don't need it. I think our gmx e-mail adress is not accepted, thats the biggets issue. Kind regards Thomas Re: USB VID/PID program still active ? Hello @Thomas_Mundhenke  Yes, what db16122 described is correct. I will send you a private email. Please send me all the relevant information. Thank you. BR Alice
View full article
S32K314的PLL失锁造成重启的问题 因晶振布局出现错误,造成晶振受到数字信号的干扰出现: Power_Ip_MC_RGM_GetResetReason() 返回值0x05 8MHZ的晶振,120倍频,PLL的输出是960MHZ,工作时钟160MHZ(PHI0,PHI1)低温下很容易出现重启。 修改为8MHZ晶振,80倍频,PLL的输出是640MHZ,工作时钟160MHZ(PHI0,PHI1),不出现重启了。 请教问题点: 晶振受到的干扰没有变,只修改了PLL倍频系数,工作主时钟160MHZ也没有变,此处提高了抗干扰的技术解释点是什么,与温度相关的点是什么,感谢! Re: S32K314的PLL失锁造成重启的问题 Hi@Allen_zhang_202 4 以下只是经验分析 虽然最终的 PHI0/PHI1 都是 160 MHz,但两种配置下 PLL 内部的工作状态完全不同: 8 MHz × 120 = 960 MHz,再分频到 160 MHz 8 MHz × 80 = 640 MHz,再分频到 160 MHz 问题很可能不在最终的 160 MHz,而在于 PLL 内部 VCO 工作频率、环路裕量、锁定检测裕量以及低温下晶振驱动能力。将 PLL 内部频率从 960 MHz 降到 640 MHz 后,PLL 的锁定裕量增大,因此同样的晶振干扰不再容易触发 PLL Loss of Lock。 但需要特别提醒:这更像是提高了“PLL 对干扰的容忍度”,并没有真正解决晶振布局问题。 Re: S32K314的PLL失锁造成重启的问题 hi Senlent 你好,非常感谢您的回复,再请问附图的文件,适用于S32K314,如果没有,是否有更新的资料适用于S32K314,如果有麻烦请告知,谢谢! Re: S32K314的PLL失锁造成重启的问题 Hi@Allen_zhang_202 4 很抱歉,S32K3没有这样的文档. AN535的发布日期是2006年,相当早的应用笔记了,用于了解其中的机制是完全可以的,但是可能并不是 完全适用于S32K3。
View full article
MPC57xx MBD 兼容性 你好, 已安装的 MPC57xx 系列基于模型的设计工具箱版本为“3.2.0”,其文档适用于 MATLAB/Simulink 版本 R2016a 至 R2020a。我可以在MATLAB R2025b版本中使用相同的版本吗? 如果不是,MATLAB R2025b 需要哪个版本的 mpc57xx mbd 工具箱? 问题:我正在尝试在我的 matlab r2025b 中运行一个基于 mpc57xx 的控制器项目。每当在MATLAB中运行该模型时,软件都会崩溃。 Re: MPC57xx MBD compatibility 3.2.0 版本的官方文档仅涵盖 MATLAB/Simulink R2016a 至 R2020a 版本。尝试在 R2025b 上运行它会导致接口不兼容,这就是为什么当您尝试运行 MPC57xx 模型时 MATLAB 会崩溃的原因。 **当前状态:**根据 NXP 社区的报告,MPC57xx 的 MBDT 甚至无法在 MATLAB 2025a 上成功安装,更不用说 R2025b 了。NXP 尚未发布支持 MATLAB R2025b 的 MPC57xx MBD 工具箱的新版本。 您的选择: | 选项 | 怎么做 | 最适合 | |--------|-----------|----------| | **降级 MATLAB** | 使用 MBD Toolbox 3.2.0 安装 MATLAB R2019b 或 R2020a| 保留您现有的 Simulink 模型;最快的修复方法 | | **迁移至 S32 Design Studio** | 仅使用 Simulink 进行算法设计,通过 Embedded Coder 生成 ANSI C 代码,然后将其与底层驱动程序集成到 S32 Design Studio 中 | 必须使用 R2025b 版本;愿意投入迁移时间 | | **使用 S32 配置工具** | 以图形方式配置引脚、时钟和外设,自动生成底层初始化代码 | 适用于新项目或希望重构配置 | **建议:**如果您的现有 Simulink 模型是核心资产,最安全的方法是**降级到 MATLAB R2020a**——这是 MBD Toolbox 3.2.0 官方支持的最高版本,并且可以保留您当前的工作流程。如果您必须使用 R2025b,则需要从“MBD 自动代码生成”迁移到“Simulink 算法 + S32 Design Studio 集成”工作流程。
View full article