Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
MC33PF8100A0TS 参考資料 こんにちは。MC33PF8100A0tsの設計参考資料はありますか? 1. プログラミングポートをどのように設計すればよいか? 2. 参考設計図はありますか? ご確認いただけますでしょうか?ありがとうございます。 Re: MC33PF8100A0TS参考资料 PF8100のGUIを使用してソフトウェアをフラッシュした後、インターフェースの接続図が記載されているユーザーマニュアルをダウンロードしてください。 PF8200/PF8100プログラミングボード | NXPセミコンダクターズ FRDM-KL25Zはこの制御基板を使用しており、そのプロセスは簡単ではありません。ソケットに直接コードを書き込む方が良いでしょう。 Re: MC33PF8100A0TS参考资料 はい、初期プロトタイプのデバッグ段階では、チップは基板に半田付けされています。 Re: MC33PF8100A0TS参考资料 こんにちは、ボブ 製品の回路基板をプログラムする予定ですか?
記事全体を表示
FS2643D H世代:S32K376NHT1MJBSTの本格的なOTP/オーダー可能なサポート こんにちは、 S32K376NHT1MJBST対応するFS2643D H世代の生産構成について教えていただけますか? 1. この組み合わせに対応する、既存のプログラム済み生産発注書およびOTP構成はありますか?もしそうであれば、正確な注文コード、OTP ID/リビジョン、該当する設定レポートおよびプログラミング/設定ファイルのリンクを特定してください。 2. カスタムOTPが必要な場合、互換性のある構成と本番プログラム部品を得るために、どのNXPまたは認可チャネルプロセスを使用すべきか?これは、ブランクデバイスを用いたエンジニアリングのエミュレーション/プログラミングとは区別してください。 3. MFS2643HMDA0ADとMFS2643HMDA0UDは該当するブランク開発バリアントであり、ADとUDの違いはパッケージ、組み立て、ご注文の適用性にどのような影響を与えるか? 公開されているFS26標準構成例とS32K376POCページを確認しました。後者はFS2633ベースのボードについて説明しており、その構成はFS2643Dにそのまま適用できるとは想定されていません。これらの詳細が公開されていない場合は、正確な該当書類または適切なサポートルートをご指摘ください。 よろしくお願いします。 Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST こんにちは、ジョナス 以下のコメントをご覧ください。 1. この組み合わせに対応する、既存のプログラム済み生産発注書およびOTP構成はありますか?もしそうであれば、正確な注文コード、OTP ID/リビジョン、該当する設定レポートおよびプログラミング/設定ファイルのリンクを特定してください。 [gw]以下は推奨事項です。まず、このパワーツリーがS32K376に適しているかどうかを評価してください。 https://www.nxp.com/products/FS26 2. カスタムOTPが必要な場合、互換性のある構成と本番プログラム部品を得るために、どのNXPまたは認可チャネルプロセスを使用すべきか?これは、ブランクデバイスを用いたエンジニアリングのエミュレーション/プログラミングとは区別してください。 [gw]上記の回答をご覧ください。 3. MFS2643HMDA0ADとMFS2643HMDA0UDは該当するブランク開発バリアントであり、ADとUDの違いはパッケージ、組み立て、ご注文の適用性にどのような影響を与えるか? [gw] A0 は空白部分を意味します。以下は FS26 の命名規則です。UD サフィックスは見つかりませんでした。 回路図デザインが終わったら、再度確認のために当社にご連絡ください。 よろしくお願いします!
記事全体を表示
S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello, Could you please identify the applicable power-estimation tool and supply-current data for S32K376NHT1MJBST? Does S32K-PET support this exact derivative? Which tool and device-dataset revisions should be used? If it is not supported, what is the recommended current NXP method? For externally supplied V15 with the external NMOS V11 regulator arrangement, how should reported demand be attributed to V15, V11, VDD_HV_A/B and other analog/bias supplies? Please identify what is included or excluded, especially regulator losses, shared core/lockstep demand, I/O loading and peripheral currents, so these are not counted twice. Which applicable public documents, data or characterization method cover worst-case supply current versus voltage/temperature, and peaks during reset, startup, wake and clock/mode changes? Please distinguish typical/average estimates from guaranteed limits and identify their conditions. The public PET page and setup guide have been reviewed. Their family-level support listing and initial average-power scope do not identify the exact derivative or all physical-supply contributions. We are seeking the applicable sources and method, not an application-specific current result without a defined operating profile. Please point to the appropriate public material or support route if these details are not public. Thank you. Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello @JonasGranlund, 1. As of now, the S32K PET tool does not support S32K39/37/36 devices. The recommended method is to refer to S32K396's Data Sheet (Rev. 5) for supply current data, specifically: 6.7 Supply currents (Standby and RUN mode tables) 6.9 Cyclic wake-up average current calculation 2. The datasheet supply current tables report current at the following rails independently: VDD_HV_A is catalogued as the main I/O and analog supply, and it covers both I/O pads in the VDD_HV_A bank and all analog blocks.  VDD_HV_B is the secondary I/O supply and covers I/O pads in the VDD_HV_B bank only. You can refer to "S32K39_and_S32K37_IOMUX.xlsx" attachment inside the Reference Manual in order to identify which pin belongs to which power domain. V11 is generated by V15 using external NMOS. The external V1.5 power supply should be turned off before entering LPM mode. IO load current is not included in measurements. The actual current requirements for IOs will depend on the I/O configuration in the application. Refer to the DC characteristics tables in the S32K39 Data sheet. Lockstep/dual-core demand is included in the core supply figures in the data sheet; the power consumption is specified to be the same because there are no separate specifications depending on the load of the cores. 3. Data Sheet values include ambient temperature, typical and maximum values.  As far as I know, there are no specific S32K39 documents detailing worst-case scenario currents, peaks during reset, etc. However, S32K3 Low Power Management AN and demos document provide power mode transitions, clock operation in low-power modes, hardware considerations and quiescent current. It is focused on a more family-level, referencing S32K3xx in general, rather than S32K39-37-36 specifics. I've also sent you a private message in community sharing S32K3 Low Power Lab presentation, which explains S32K3 low power behavior and considerations. Best regards, Julián
記事全体を表示
トリメンションSR250 — 試作前のライセンスとレーダーデータの質問 FRDM-RW612と「SR250 UWBIoT for Zephyr」(github.com/nxp-uwb/sr250-uwbiot-zephyr)を用いたSR250UWBSHIELDを基に研究プロトタイプを計画しています。これはタグフリーのUWBレーダーで、ビルディング資材の背後にいる人を探知し、検索救助に使用されます。ソフトウェアライセンス(LA_OPT_Online Code Hosting v1.4)を受け入れる前に、以下の5つの質問に簡潔にお答えいただけると幸いです。 1. レーダーデータ:レーダーモードでSR250は複雑なI/Q(位相保持)としてCIRをホストに届けますか?複数の受信アンテナからCIRを同時にキャプチャし、ホストが到着角度を推定できるのでしょうか? 2. 結果共有:セクション3.8は「ライセンスソフトウェアの使用に関連する報告」をNXP以外の者に配布することを禁止しています。これは、私自身の測定結果やテストラボ、外部査読者、お客様、科学論文と共有したログも含まれますか?もしそうなら、NXPは書面での許可を出せますか? 3. 自社ソフトウェア:私自身のホスト側信号プロセッシング(PC上で動作し、CIRデータを受信し、NXPコードを含まない)は、セクション1.3および5の下で「派生作品」として扱われますか? 4. 製品経由:プロトタイプが成功した場合、v1.4は自社のPCBにSR250を搭載した機器の商業販売を許可し、お客様向けのファームウェアアップデートも含めて提供できますか?それとも別途合意が必要でしょうか? 5. コンプライアンス:SR250UWBSHIELDのEU適合宣言全文はどこで入手できますか?レーダーモードはカバーされていますか? ご返信よろしくお願いします。 Re: Trimension SR250 — licensing and radar data questions before prototyping こんにちは、 プライベートメッセージを送りました! よろしくお願いいたします。 リカルド
記事全体を表示
FS2643D H 代:生产 OTP/可订购支持 S32K376NHT1MJBST 你好, 请问能否说明一下 S32K376NHT1MJBST 支持的 FS2643D H 代生产配置? 1. 是否存在针对此组合的已编程生产可订购和OTP配置?如果是,请提供确切的订单代码、OTP ID/版本以及适用的配置报告和编程/配置文件链接。 2. 如果需要定制 OTP,应该使用 NXP 的哪个流程或授权渠道来获得兼容的配置和生产编程部件?请将此与空白设备工程仿真/编程区分开来。 3. MFS2643HMDA0AD 和 MFS2643HMDA0UD 是否是适用的空白开发变体?它们的 AD/UD 差异对封装、组装和订购适用性有何意义? 已审查公开的 FS26 标准配置示例和 S32K376POC 页面。后者描述的是基于 FS2633 的板;其配置不被认为可以转移到 FS2643D。如果这些信息不公开,请指出适用的具体文件或正确的求助途径。 谢谢! Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST 嗨,乔纳斯 请看下方评论: 1. 是否存在针对此组合的已编程生产可订购和OTP配置?如果是,请提供确切的订单代码、OTP ID/版本以及适用的配置报告和编程/配置文件链接。 [gw]以下是推荐配置,请先评估此电源树是否适用于 S32K376。 https://www.nxp.com/products/FS26 2. 如果需要定制 OTP,应该使用 NXP 的哪个流程或授权渠道来获得兼容的配置和生产编程部件?请将此与空白设备工程仿真/编程区分开来。 [gw]请看上面的答案。 3. MFS2643HMDA0AD 和 MFS2643HMDA0UD 是否是适用的空白开发变体?它们的 AD/UD 差异对封装、组装和订购适用性有何意义? [gw] A0 表示空白部分,以下是 FS26 的名称规则,我没有找到 UD 后缀。 请注意,原理图设计完成后请发送给我们进行复核。 谢谢您!
記事全体を表示
Trimension SR250 — licensing and radar data questions before prototyping I am planning a research prototype based on the SR250UWBSHIELD with FRDM-RW612 and "SR250 UWBIoT for Zephyr" (github.com/nxp-uwb/sr250-uwbiot-zephyr). It is a tag-free UWB radar for detecting people behind building materials, for search-and-rescue use. Before accepting the software license (LA_OPT_Online Code Hosting v1.4), I would appreciate short answers to five questions: 1. Radar data: In radar mode, does the SR250 deliver CIR to the host as complex I/Q (phase preserved)? Can it capture CIR from more than one RX antenna simultaneously, so that the host can estimate angle of arrival? 2. Sharing results: Section 3.8 prohibits distributing "reports associated with the use of the Licensed Software" to anyone other than NXP. Does this cover my own measurement results and logs shared with test labs, external reviewers, customers or scientific publications? If so, can NXP give written permission? 3. Own software: Is my own host-side signal processing (running on a PC, receiving CIR data, containing no NXP code) treated as a "Derivative Work" under Sections 1.3 and 5? 4. Product path: If the prototype succeeds, does v1.4 allow commercial sale of a device with SR250 on my own PCB, including firmware updates for customers? Or would a separate agreement be needed? 5. Compliance: Where can I find the full EU Declaration of Conformity for SR250UWBSHIELD? Does it cover radar mode? Thank you very much. Re: Trimension SR250 — licensing and radar data questions before prototyping Hello, I sent you a private message! Regards, Ricardo
記事全体を表示
Trimension SR250——原型制作前的许可和雷达数据问题 我正在计划基于 SR250UWBSHIELD、FRDM-RW612 和“SR250 UWBIoT for Zephyr”(github.com/nxp-uwb/sr250-uwbiot-zephyr)的研究原型。它是一种无需标签的超宽带雷达,用于探测建筑物材料后面的人员,可用于搜救。在接受软件许可协议(LA_OPT_Online Code Hosting v1.4)之前,我希望您能简要回答以下五个问题: 1. 雷达数据:在雷达模式下,SR250 是否以复数 I/Q(相位保持)的形式向主机提供 CIR?它能否同时从多个接收天线捕获 CIR,以便主机可以估计到达角? 2. 分享结果:第 3.8 节禁止向 NXP 以外的任何人分发“与使用许可软件相关的报告”。这是否涵盖我自己的测量结果和与测试实验室、外部审阅者、客户或科学出版物共享的日志?如果可以,恩智浦能否提供书面许可? 3. 自己的软件:我自己的主机端信号处理(在 PC 上运行,接收 CIR 数据,不包含 NXP 代码)是否被视为第 1.3 节和第 5 节中的“衍生作品”? 4. 产品路径:如果原型成功,v1.4 是否允许我在自己的 PCB 上进行带有 SR250 的设备的商业销售,包括为客户提供固件更新?或者是否需要另行签订协议? 5. 合规性:我可以在哪里找到 SR250UWBSHIELD 的完整欧盟符合性声明?它是否支持雷达模式? 非常感谢。 Re: Trimension SR250 — licensing and radar data questions before prototyping 你好, 我给你发了私信! 此致, 里卡多
記事全体を表示
Licensing question: LA_OPT Online Code Hosting v1.4 (SR250 UWBIoT) — sharing results, AI tools, own Hello,  On the advice of NXP support chat, I'm posting my licensing questions here for the licensing team.  I plan a research prototype with SR250UWBSHIELD + FRDM-RW612, using software from github.com/nxp-uwb/sr250-uwbiot-zephyr and github.com/nxp-appcodehub/an-sr250-uwb-plug-and-play-demo (SR250 FW 01.41.04). Both are under "LA_OPT_Online Code Hosting NXP_Software_License – v1.4 May 2025". I have not accepted the license yet and would like to clarify the following first:  1. Section 3.8: Does the restriction on distributing "reports associated with the use of the Licensed Software" cover my own measurement results, logs and test reports? I would share them with a test laboratory, external reviewers, customers or in a scientific publication.  2. AI tools (Sections 3.2 / 3.8): I develop with AI assistants (e.g. ChatGPT, Claude). May I (a) share my results and reports with such services, and (b) let an AI assistant read and work with the Licensed Software and NXP documentation (e.g. UM12508), on my own computer or via a cloud service?  3. Own software (Sections 1.3 / 5): Is my own PC-side signal-processing software, which only receives CIR data and contains no NXP code, a "Derivative Work"? Do Sections 5.1–5.2 apply to it?  4. Product (Section 2.1): Does v1.4 allow selling a device with the SR250 (NXP board, third-party SR250 module or bare SR250UK on my own PCB) and this firmware, including firmware update files for customers? Or is a separate agreement required?  5. Licensee: If I accept the license as an individual now, does it carry over to a company I may set up later?  A written answer, or a contact at the NXP licensing/legal team, would be much appreciated. Thank you!
記事全体を表示
MC33PF8100A0TS参考资料 你好,又MC33PF8100A0ts的设计参考资料吗?  1. 如何设计烧写口? 2.参考设计原理图有吗? 帮忙看看,谢谢。 Re: MC33PF8100A0TS参考资料 用我们的PF8100的GUI 烧录,然后下载usermanual上面有接口的连接示意图: PF8200/PF8100 Programming Board | NXP Semiconductors FRDM-KL25Z用的是这个控制板,这一套操作下来也不简单,还不如直接在socket上烧写。 Re: MC33PF8100A0TS参考资料 是的,初期样板调试是芯片焊在板子上。 Re: MC33PF8100A0TS参考资料 HI Bob 您是要在产品的板子上做烧写吗?
記事全体を表示
FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hello, Could you please clarify the supported FS2643D H-generation production configuration for S32K376NHT1MJBST? 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? The public FS26 standard-configuration examples and the S32K376POC page have been reviewed. The latter describes an FS2633-based board; its configuration is not being assumed transferable to FS2643D. Please point to the exact applicable documents or the correct support route if these details are not public. Thank you. Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hi Jonas Please see comment below: 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. [gw]Below is the recommend please firstly evaluate this power tree is suitable or not for S32K376 https://www.nxp.com/products/FS26 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. [gw]Please see answer above. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? [gw] A0 means blank part, Below is the name rule of FS26,I didn't find the UD suffix. Please note that after you finish schematic design please send to us for double check. Thanks!
記事全体を表示
S32K376NHT1MJBST:適用可能な電力推定器および電源ごとの電流データ こんにちは、 S32K376NHT1MJBSTに適用される電力推定ツールと供給電流データを教えていただけますか? S32K-PETはこの派生モデルをサポートしていますか?どのツールとデバイスデータセットの改訂版を使用すべきですか?もしサポートされていない場合、現在の推奨されているNXP方法は何ですか? 外部供給のV15に外部NMOSのV11レギュレータ配置がある場合、報告された需要はV15、V11、VDD_HV_A/Bおよびその他のアナログ/バイアス供給にどのように帰属すべきでしょうか?特にレギュレーター損失、共有コア/ロックステップ需要、I/O負荷、ペリフェラル電流などを含め、何が含まれているか、何が除外されているかを特定してください。これらが二重にカウントされないようにするためです。 どの適用可能な公文書、データ、特性評価方法が、最悪のケースの電源電流と電圧/温度、リセット、起動、ウェイク、クロック/モード変更時のピークをカバーしていますか?標準値/平均値と保証限度額を区別し、それぞれの条件を明記してください。 公開されているPETページとセットアップガイドを確認しました。ファミリレベルの支援リストと初期の平均出力範囲では、正確な微分やすべての物理的供給貢献は特定されていません。私たちは、定義された運用プロファイルのない応用特有の現行結果ではなく、適用される情報源と方法を求めています。 これらの詳細が公開されていない場合は、適切な公開資料やサポートルートをご紹介ください。 よろしくお願いします。 Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data こんにちは、@JonasGranlund さん。 1.現時点で、S32K PETツールはS32K39/37/36デバイスをサポートしていません。推奨される方法は、S32K396のデータシート(Rev.5) 供給電流データについては、具体的には: 6.7 供給電流(スタンバイモードおよび動作モードの表) 6.9 周期的なウェイクアップ平均電流の計算 2. データシートの供給電流表には、以下のレールにおける電流が個別に記載されています。 VDD_HV_A メインのI/Oおよびアナログ電源としてカタログ化されており、VDD_HV_AバンクのI/Oパッドとすべてのアナログブロックをカバーしています。 VDD_HV_Bは二次I/O電源であり、VDD_HV_Bバンク内のI/Oパッドのみを対象としています。どのピンがどのパワードメインに属しているかを特定するために、リファレンスマニュアル内の「S32K39_and_S32K37_IOMUX.xlsx」アタッチメントを参照できます。 V11は、外部NMOSを用いてV15によって生成される。LPMモードに入る前に、外部V1.5電源をオフにしてください。 IO負荷電流は測定値に含まれていません。IOの現在の要件は、アプリケーションのI/O構成によって異なります。S32K39データシートのDC特性表を参照してください。 データシートのコア供給量には、ロックステップ/デュアルコア動作時の需要が含まれています。コアの負荷に応じて個別の仕様が定められていないため、消費電力は同じ値として規定されています。 3.データシートの値には、周囲温度、標準値、最大値が含まれます。 私の知る限り、最悪のシナリオの電流やリセット時のピークなどを詳述したS32K39の文書は存在しません。しかし、S32K3の低電力パワーマネージメントANおよびデモでは、電源モードの遷移、低消費電力モードのクロック動作、ハードウェアの考慮事項、静止電流が記載されています。よりファミリレベルに焦点を当てており、S32K39-37-36の詳細ではなく、S32K3xx全体を指しています。 S32K3の低消費電力動作と留意事項について説明したS32K3低消費電力ラボのプレゼンテーションを、コミュニティ共有のプライベートメッセージでお送りしました。 よろしくお願いします、 ジュリアン
記事全体を表示
i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support Hello NXP Support Team, I am evaluating the i.MX 93 platform for an EVSE application and came across the EVSE-IMX93 development kit. I would like to clarify the available Linux images and their compatibility with a potential custom carrier-board design. Our intention is to use the MCIMX93-SOM and develop a simplified custom carrier board based on the original NXP carrier-board design. We would retain the same SOM connector and pin assignments while removing unused peripherals and circuitry. As I am relatively new to the i.MX processor platform and Yocto-based development, I am looking for a straightforward, ready-to-use Linux solution to get started before moving towards customisation. Could you please clarify the following? Is a ready-to-use Ubuntu or Debian 13 (Trixie) image available for the i.MX 93, preferably a general-purpose server/minimal Linux image? Can this image be downloaded and flashed directly onto a microSD card to boot the board, without requiring a Yocto build? Does the available image support standard Linux functionality such as apt, Python 3, SSH, systemd and networking? Does it include support for CAN/CAN-FD (SocketCAN), Wi-Fi, Ethernet and MQTT? Can packages such as Mosquitto be installed using apt? Can the same prebuilt image be used with our proposed custom carrier board, provided we retain the original SOM connector and relevant hardware connections? Would only device-tree or configuration changes be required? If such an image is available, could you please share the direct download link, supported board details and installation instructions? Our objective is to use the i.MX 93 as a general-purpose Linux platform for running the EVerest framework and other EVSE application software, while avoiding the need to maintain a Yocto build initially. Thank you for your assistance. Kind regards Ganesh Bhagwat Re: i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support Hello,  Yes, there is a Debian Linux SDK compatible with the i.mx93 platform, you can build the image through the implementation of "Flexbuild" instead of Yocto and flash the image with the  flexinstaller tool , more information about supported packages of the distro is available here: DEBIAN-SDK  Debian Software Release Notes LDLSDK_26.06
記事全体を表示
MC33PF8100A0TS Reference Material Hello, do you have any design reference materials for the MC33PF8100A0ts? 1. How to design the programming port? 2. Do you have a reference design schematic? Could you please take a look? Thank you. Re: MC33PF8100A0TS参考资料 Flash the software using our PF8100 GUI, then download the user manual which contains a connection diagram of the interfaces: PF8200/PF8100 Programming Board | NXP Semiconductors The FRDM-KL25Z uses this control board, and the whole process is not simple. It's better to just burn the code directly onto the socket. Re: MC33PF8100A0TS参考资料 Yes, in the initial prototype debugging, the chip is soldered onto the board. Re: MC33PF8100A0TS参考资料 HI Bob Are you planning to program the product's circuit board?
記事全体を表示
电池包主动均衡方案 你好,在网站上没有找到电池包主动均衡的方案,只有一段电池储能解决方案的演示视频,论坛里也没搜到相关的文章。我想找找这方面的文章,有推荐吗?谢谢。 Re: 电池包主动均衡方案 这个太老了,主动均衡应该是后续新能源的趋势吧。 Re: 电池包主动均衡方案 Hi Bob 我们不做主动均衡的IC,这方面的资料不多,附件这个希望能对您有所帮助是很老的app note了
記事全体を表示
i.MX 93 – プリビルドのUbuntu/Debian Linuxイメージおよびカスタムキャリアボードサポート こんにちは、NXPサポートチームの皆さん、 私はEVSEアプリケーション用に i.MX 93プラットフォームを評価しているところ、EVSE-IMX93開発キットに出会いました。 利用可能なLinuxイメージと、それらが潜在的なカスタムキャリアボードデザインとの互換性について明確にしたいと思います。 私たちの意図は、MCIMX93-SOMを用いて、元のNXPキャリアボードデザインを基にした簡素化されたカスタムキャリアボードを開発することです。使用していないペリフェラルや回路を除去しつつ、SOMコネクタとピンの割り当ては同じままにします。 私は i.MX プロセッサプラットフォームとYoctoベースの開発にはまだ比較的新しいため、カスタマイズに進む前にすぐに使えるLinuxソリューションを探しています。 以下の点を明確にしていただけますか? i.MX 93用の 使いやすいUbuntuやDebian 13(Trixie)イメージ はありますか ?できれば汎用サーバーや最小限のLinuxイメージが望ましいです。 このイメージは、Yoctoビルドなしで直接microSDカードにダウンロードしてフラッシュしてボードを起動できますか? 利用可能な画像はapt、Python 3、SSH、systemd、networkingなどの標準的なLinux機能をサポートしていますか? CAN/CAN-FD(SocketCAN)、Wi-Fi、イーサネット、MQTT のサポートは含まれています か?Mosquittoのようなパッケージはaptでインストールできますか? 元のSOMコネクタと関連するハードウェア接続を保持すれば、同じプリビルドイメージを提案しているカスタムキャリアボードに使うことは可能でしょうか?デバイスツリーまたは設定の変更のみが必要となるのでしょうか? もしそのような画像があれば、直接ダウンロードリンク、対応ボードの詳細、インストール手順を共有していただけると助かります。 私たちの目標は、i.MX 93をEVerestフレームワークやその他のEVSEアプリケーションソフトウェアを動かす汎用Linuxプラットフォームとして活用しつつ、最初にYoctoビルドの保守を回避することです。 ご協力ありがとうございました。 敬具 ガネーシュ・バグワット Re: i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support こんにちは、 はい、i.mx93プラットフォームに対応したDebian Linux SDKがあります。Yoctoではなく「Flexbuild」の実装を通じてイメージを構築し、flexinstallerツールでイメージをフラッシュできます。ディストリビューションのサポートパッケージについてはこちらで詳しくご覧いただけます: DEBIAN-SDK Debianソフトウェアリリースノート LDLSDK_26.06
記事全体を表示
バッテリーパックのアクティブバランシングソリューション こんにちは。ウェブサイトでアクティブバッテリーパックバランシングの解決策を探したのですが、バッテリーエネルギー貯蔵ソリューションのデモビデオしか見つかりませんでした。フォーラムでも関連する記事が見つかりませんでした。何かおすすめはありますか? よろしくお願いします。 Re: 电池包主动均衡方案 それは時代遅れだ。新しいエネルギー源においては、アクティブバランシングが将来のトレンドとなるべきだ。 Re: 电池包主动均衡方案 こんにちは、ボブ。 弊社ではアクティブバランシングICを製造しておらず、この件に関する情報もあまりありません。添付ファイルは古いアプリケーションノートですが、お役に立てれば幸いです。
記事全体を表示
From MC33816 to PT2001 design tips(CN) The C33PT2000AF and MC33816 wafers are manufactured at NXP's Chandler fab in the US, and production will cease due to the fab's impending closure. Currently, the official website states the last buy date as August 6, 2027, and the last delivery date as August 6, 2028 (specific dates are subject to change). The MC33PT2001 wafers are currently sourced from NXP's Austin fab in the US and are not affected by this discontinuation. Therefore, it is recommended that relevant customers replace their existing MC33PT2000AF and MC33816 wafers with MC33PT2001 wafers. Migrating a system from MC33816 to MC33PT2001 is not complicated. The hardware is basically pin-to-pin compatible, with only the voltage of pin 20 changing from 2.5V to 1.5V. This basically does not require any changes to the external circuitry. The internal registers are mostly compatible, only the Threshold register bit field has changed. MC33816: 0x18A Vds_threshold_hs Because each threshold in PT2001 becomes 4 bits, it is split into: 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS An additional 0x1B4 batt_result register was added to store the ADC conversion result of the VBATT pin. In summary, migrating from MC33816 to MC33PT2001 is quite convenient. Small Engine Driver
記事全体を表示
From MC33816 to PT2001 design tips(CN) C33PT2000AF和MC33816由于晶圆产自NXP美国Chandler工厂, 由于Chandler 工厂即将关闭,所以将停产。目前官网信息,last time buy date 为2027年8月6日,last time delivery date为2028年8月6日(具体日期以官网为准)。MC33PT2001晶圆目前来自NXP美国Austin工厂,不涉及本次停产,所以建议相关客户用MC33PT2001替代原有使用的MC33PT2000AF和MC33816的项目。 系统如果是从MC33816迁移到MC33PT2001并不复杂,硬件上基本Pin to Pin兼容, 仅是pin 20电压由2.5V变为1.5V,基本可以不涉及外围电路改变。 内部寄存器也是大部分是兼容的,仅是Threshold register bit field改变了 MC33816: 0x18A Vds_threshold_hs PT2001因为每个 threshold 变成4 bit,所以拆成: 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS 另外增加了一个0x1B4  batt_result寄存器用于放VBATT pin的ADC转换结果。 总之,如果是从MC33816迁移至MC33PT2001还是非常方便的。 Small Engine Driver
記事全体を表示
MC33816からPT2001への設計ヒント(中国語) C33PT2000AFおよびMC33816ウェハは、NXPの米国チャンドラー工場で製造されていますが、同工場の閉鎖に伴い生産が中止されます。現在、公式ウェブサイトでは最終購入日が2027年8月6日、最終納品日が2028年8月6日と記載されています(具体的な日付は変更される可能性があります)。MC33PT2001ウェハは現在、NXPの米国オースティン工場から供給されており、今回の生産中止の影響を受けません。したがって、該当するお客様は、既存のMC33PT2000AFおよびMC33816ウェハをMC33PT2001ウェハに交換することをお勧めします。 MC33816からMC33PT2001へのシステム移行は複雑ではありません。ハードウェアは基本的にピン互換性があり、20番ピンの電圧が2.5Vから1.5Vに変更されるだけです。そのため、外部回路の変更は基本的に必要ありません。 内部レジスタはほとんど互換性がありますが、しきい値レジスタのビットフィールドのみが変更されています。 MC33816: 0x18A Vds_threshold_hs PT2001では各しきい値が4ビットになるため、以下のように分割されます。 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS VBATTピンのADC変換結果を格納するために、追加の0x1B4 batt_resultレジスタが追加されました。 要約すると、MC33816からMC33PT2001への移行は非常に簡単です。 小型エンジンドライバー
記事全体を表示
[MCX A153] LPCMP入門ガイド(日本語ブログ) 1. はじめに 本記事では、NXP MCX A シリーズ (MCX A153) に搭載されている LPCMP (Low-Power Comparator) を、MCUXpresso SDK の frdmmcxa153_lpcmp_interrupt サンプルと、FRDM-MCXA153ボードを題材に解説します。 LPCMP は 2 つのアナログ入力の大小関係を比較し、結果をデジタル出力として得る周辺機能で、しきい値検出、ゼロクロス検出、電源監視、タッチ入力など幅広い用途に使われます。MCX A153 の LPCMP は内蔵 8bit DAC と 8ch アナログマルチプレクサを備えており、外付け部品を増やすことなくしきい値比較が可能です。 本サンプルは、CMP0 の正入力 (P2_2 / CMP0_IN0) に外部電圧 (VDD または GND)、負入力に内蔵 DAC 出力 (≒ VREFI/2 = VDD/2) を割り当て、比較結果の立ち上がり/立ち下がりエッジ割り込みで LED_RED を点灯/消灯させます。 (読了:20分) 2. LPCMP の概要 LPCMP は以下のサブブロックで構成されます。 コンパレータコア: プラス入力 / マイナス入力を比較しデジタル出力 (COUT) を生成 8bit DAC: 256 タップの抵抗ラダーで Vin を分圧。VREFH0 (VDD) または VREFH1 (VREFI 入力) を Vin として選択可能 出力式: DACO = Vin / 256 × (DAC_DATA + 1) 、DAC_DATA = 0〜255 出力範囲: Vin × 1/256 〜 Vin × 256/256 (= Vin) の 256 段階 (0V は出力できない) ANMUX (PMUX / MMUX): 8:1 のアナログセレクタ。外部ピン (IN0〜IN5)、内部 DAC 出力、Reservedセレクタを正/負入力に割り当て可能 ウィンドウ / サンプリング / フィルタ: チャタリング除去、タイミング制御 出力ピン / 割り込み: CFR (立ち上がり)、CFF (立ち下がり)、RRF (出力変化) の 3 フラグ 3. 内部ブロック図   3.1 入力セレクタとコア   3.2 内蔵 DAC VRSEL = 0 で VREFH0 (VDD)、VRSEL = 1 で VREFH1 (VREFI 入力) が Vin となります。   4. MCX A153 における固有情報 項目 内容 インスタンス CMP0 (本サンプル使用), CMP1 アナログ入力ピン CMP0_IN0〜IN5 内蔵 DAC 分解能 8bit (256 段階) DAC 基準電圧 VDD (VREFH0) または VREFI 外部入力 (VREFH1) 割り込みフラグ CFR (立ち上がり), CFF (立ち下がり), RRF (出力変化) 機能クロック源 FRO12M, FRO HF, CLK_1M 等から CLOCK_AttachClk で選択 アナログ電源 SPC0 ACTIVE_CFG1 で CMP / DAC 用アナログ電源を有効化   5. サンプルの動作   5.1 配線 FRDM-MCXA153 のピンヘッダで以下のように接続します。 信号 ピン Board Location 接続先 役割 VREFI P2_7 J3-1 JP8-2 (VDD) DAC 基準電圧 Vin (= VDD) CMP0_IN0 P2_2 J2-9 VDD または GND を手動で切替 プラス入力 LED_RED P3_12 オンボード ― 比較結果の表示 J3-1 を JP8-2 (VDD) にジャンパすることで VREFI = VDD となり、内蔵 DAC の Vin が VDD になります。DAC_DATA は ((LPCMP_DCR_DAC_DATA_MASK >> SHIFT) >> 1) = 127 が設定されるため、DACO ≒ VDD/2 です。J2-9 (CMP0_IN0) を VDD に繋ぐと LED_RED 点灯、GND に繋ぐと消灯します。   5.2 シーケンス   5.3 比較結果の挙動   6. クロック設定 LPCMP はバスクロックとは別に、サンプリング/フィルタ用の機能クロック (CMP_FUNC) を要求します。また、アナログ回路のため SPC (System Power Controller) で CMP / DAC 用アナログ電源を有効化する必要があります。 hardware_init.c の該当コードは以下の 3 行です。 CLOCK_AttachClk(kFRO12M_to_CMP0); /* 1) 機能クロックソースを選択 */ CLOCK_SetClockDiv(kCLOCK_DivCMP0_FUNC, 1U); /* 2) 分周を 1 に設定 (12MHz のまま) */ SPC0->ACTIVE_CFG1 |= ((1U << 16U) | (1U << 20U)); /* 3) CMP0/DAC0 アナログ電源 ON */ SPC0->ACTIVE_CFG1 レジスタの構造 6.1 クロックツリー MCX A153 リファレンスマニュアル Figure 46参照。 6.2 SPC ACTIVE_CFG1 の該当ビット ビット 内容 bit16 (CMP0_AEN) Active モードで CMP0 アナログ回路を有効化 bit20 (CMP0_DAC_AEN) Active モードで CMP0 内蔵 DAC を有効化 この 2 ビットを立て忘れると、 LPCMP_Init() 自体はエラーにならないものの、比較結果が常に 0 のまま、あるいは DAC 出力が立ち上がらないという症状になります。 7. PINMUX 設定 pin_mux.c では以下 4 系統 (計 5 ピン) をセットアップしています。 ピン 機能 ALT 設定ポイント P2_2 CMP0_IN0 (アナログ入力) ALT0 Pull-Down、Input Buffer Disable P2_7 VREFI (DAC 基準電圧) ALT0 Pull-Disable、Input Buffer Disable P3_12 GPIO (LED_RED) ALT0 出力、初期値 1 (消灯) P0_2 LPUART0_RX ALT2 Pull-Up P0_3 LPUART0_TX ALT2 Pull-Up   7.1 アナログピンでの注意点 アナログ入力として使う P2_2 / P2_7 では、必ずデジタル Input Buffer を Disable にします。これを有効のままにすると、入力電圧がロジック閾値付近を通過するたびにシュートスルー電流が流れ、消費電流増加や発熱、さらにアナログ信号の歪みに繋がります。 const port_pin_config_t port2_2_pin16_config = { kPORT_PullDown, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, kPORT_MuxAlt0, kPORT_InputBufferDisable, /* <-- 必須 */ kPORT_UnlockRegister, }; PORT_SetPinConfig(PORT2, 2U, &port2_2_pin16_config);   7.2 PORT / GPIO クロックとリセット解除 PINMUX を触る前に、使用する PORT と GPIO にクロックを供給し、リセットを解除する必要があります。 CLOCK_EnableClock(kCLOCK_GatePORT0); CLOCK_EnableClock(kCLOCK_GatePORT2); CLOCK_EnableClock(kCLOCK_GatePORT3); CLOCK_EnableClock(kCLOCK_GateGPIO3); RESET_ReleasePeripheralReset(kPORT0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT2_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kGPIO3_RST_SHIFT_RSTn); これを忘れると GPIOレジスタへの書き込みでフォルトが発生する、または書いても反映されない現象が起こります。 8. SDK API を用いたコード解説   8.1 app.h の定義 #define DEMO_LPCMP_BASE CMP0 #define DEMO_LPCMP_USER_CHANNEL 0U /* CMP0_IN0 */ #define DEMO_LPCMP_DAC_CHANNEL 7U /* 内蔵 DAC 出力の MUX チャネル */ #define DEMO_LPCMP_IRQ_ID CMP0_IRQn #define DEMO_LPCMP_IRQ_HANDLER_FUNC CMP0_IRQHandler   8.2 main() 中の初期化シーケンス lpcmp_config_t mLpcmpConfigStruct; lpcmp_dac_config_t mLpcmpDacConfigStruct; BOARD_InitHardware(); /* clocks + pinmux + console */ /* 1) デフォルト設定を取得し、必要箇所だけ上書き */ LPCMP_GetDefaultConfig(&mLpcmpConfigStruct); /* 2) コンパレータ初期化 */ LPCMP_Init(DEMO_LPCMP_BASE, &mLpcmpConfigStruct); /* 3) 内蔵 DAC 設定: Vin = VREFI(=VDD), DAC_DATA = 127 (フルスケールの半分) * DACO = VREFI / 256 * (127 + 1) = VREFI * 128/256 = VREFI/2 */ mLpcmpDacConfigStruct.enableLowPowerMode = false; mLpcmpDacConfigStruct.referenceVoltageSource = kLPCMP_VrefSourceVin2; /* VREFI */ mLpcmpDacConfigStruct.DACValue = ((LPCMP_DCR_DAC_DATA_MASK >> LPCMP_DCR_DAC_DATA_SHIFT) >> 1U); /* = 127 */ LPCMP_SetDACConfig(DEMO_LPCMP_BASE, &mLpcmpDacConfigStruct); /* 4) PMUX = IN0, MMUX = DAC ch7 */ LPCMP_SetInputChannels(DEMO_LPCMP_BASE, DEMO_LPCMP_USER_CHANNEL, DEMO_LPCMP_DAC_CHANNEL); /* 5) 立ち上がり/立ち下がり両エッジ割り込みを有効化 */ LPCMP_EnableInterrupts(DEMO_LPCMP_BASE, kLPCMP_OutputRisingInterruptEnable | kLPCMP_OutputFallingInterruptEnable); EnableIRQ(DEMO_LPCMP_IRQ_ID); while (1) { } /* あとは割り込み駆動 */   8.3 割り込みハンドラ void DEMO_LPCMP_IRQ_HANDLER_FUNC(void) { LPCMP_ClearStatusFlags(DEMO_LPCMP_BASE, kLPCMP_OutputRisingEventFlag | kLPCMP_OutputFallingEventFlag); if (kLPCMP_OutputAssertEventFlag == (kLPCMP_OutputAssertEventFlag & LPCMP_GetStatusFlags(DEMO_LPCMP_BASE))) { LED_ON(); /* V+ > V- (COUT=1) : LED 点灯 */ } else { LED_OFF(); /* V+ < V- (COUT=0) : LED 消灯 */ } SDK_ISR_EXIT_BARRIER; } Rising / Falling どちらの割り込みでも一旦両方のフラグをクリアし、その後 kLPCMP_OutputAssertEventFlag (= 現在の COUT) を見て LED をオン/オフ分岐します。   9. 動かし方 frdmmcxa153_lpcmp_interrupt を IDE で開きビルド J3-1 (P2_7 / VREFI) を JP8-2 (VDD) にジャンパ して VREFI = VDD にする ターゲットに書き込み、ターミナル (115200 bps) を開く J2-9 (P2_2 / CMP0_IN0) をジャンパ線で VDD に接続 → LED_RED 点灯 同ピンを GND に繋ぎ替え → LED_RED 消灯   10. よくあるつまずき 症状 原因 対処 LPCMPの出力が切り替わらない SPC0 ACTIVE_CFG1 の CMP0/DAC アナログ電源有効化忘れ SPC0->ACTIVE_CFG1 |= (1<<16) 割り込みが入らない LPCMP_EnableInterrupts または EnableIRQ(CMP0_IRQn) 漏れ 両方の呼び出しを確認 DAC 出力が立ち上がらない VRSEL と VREFI 入力ピンの不一致、VREFI 未接続 kLPCMP_VrefSourceVin2 使用時は P2_7 に基準電圧を印加 しきい値付近でチャタリング ヒステリシス 0、フィルタ無効 hysteresisMode を Level1〜3 に、またはフィルタ有効化 GPIOレジスタ書き込みでフォルト PORT クロック未供給 / リセット未解除 CLOCK_EnableClock() と RESET_ReleasePeripheralReset() の呼び出しを確認   11. まとめ MCX A153 の LPCMP は、以下の特徴を持ちます。 8 入力 ANMUX + 内蔵 8bit DAC により外付け回路最小でしきい値比較が可能 DAC 出力は DACO = Vin/256 × (DAC_DATA + 1) (DAC_DATA = 0〜255) で、Vin×1/256 〜 Vin の 256 段階 低消費電力モードやヒステリシス、フィルタ機能を SDK API 1 行で設定可能 使用するには  (1) 機能クロック Attach + Divider  (2) SPC アナログ電源 Enable  (3) アナログピンの Input Buffer Disable の 3 点が必須 本サンプルは最小構成ですが、しきい値を DAC で動的に変える、ウィンドウモードを使う、割り込みの代わりに DMA / 外部トリガとして使用するといった拡張も可能です。LPCMP を使うアプリ開発の出発点として本記事がお役に立てば幸いです。 ========================= 本投稿の「Comment」欄にコメントをいただいても、現在返信に対応しておりません。 お手数をおかけしますが、お問い合わせの際には「NXPへの技術質問 - 問い合わせ方法 (日本語ブログ)」をご参照ください。 (既に弊社NXP代理店、もしくはNXPとお付き合いのある方は、直接担当者へご質問いただいてもかまいません。) 本記事では、NXP MCX A シリーズ (MCX A153) に搭載されている LPCMP (Low-Power Comparator) を、MCUXpresso SDK の frdmmcxa153_lpcmp_interrupt サンプルと、FRDM-MCXA153ボードを題材に解説します。 LPCMP は 2 つのアナログ入力の大小関係を比較し、結果をデジタル出力として得る周辺機能で、しきい値検出、ゼロクロス検出、電源監視、タッチ入力など幅広い用途に使われます。MCX A153 の LPCMP は内蔵 8bit DAC と 8ch アナログマルチプレクサを備えており、外付け部品を増やすことなくしきい値比較が可能です。 本サンプルは、CMP0 の正入力 (P2_2 / CMP0_IN0) に外部電圧 (VDD または GND)、負入力に内蔵 DAC 出力 (≒ VREFI/2 = VDD/2) を割り当て、比較結果の立ち上がり/立ち下がりエッジ割り込みで LED_RED を点灯/消灯させます。 (読了:20分) MCUXpresso SDK MCX 日本語ブログ
記事全体を表示