Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32K3 UTEST program generates hardfault Hello, I am trying to create a test application to restrict JTAG/debug access by setting a 16 byte password (without HSE) for an S32K312. Previously my approach was 2 staged - I had one program to set the password, and another to advance the lifecycle, and this seemingly worked fine. I am now trying to combine both into a single sequence to integrate into my main application eventually, but I am facing issues where the MCU generates a hardfault when I try to program the password. I can confirm that before trying to program the password, there is no password set (0xFF throughout) and even though a hardfault was generated, the password has actually been programmed - this must have been why my previous 2 staged approach worked, as even if the first stage hardfaulted, I would not have noticed and simply programmed the second stage. Below is my code snippet. Do note that I have also set the lifecycle configuration word address in the startup script, to be included in the IVT. There are no other modifications to the startup script or linker. #define MASTER_ID (0U) #define CUST_DB_PSWD_A_ADDR (0x1B000080U) #define CUST_DB_PSWD_A_SECTOR (C40_UTEST_ARRAY_0_S000) #define CUST_DB_PSWD_A_LENGTH (16U) #define LC_CONFIGURATION_WORD_ADDR (0x005A6000) #define LC_CONFIGURATION_WORD_SECTOR (C40_CODE_ARRAY_0_BLOCK_1_S211) #define LC_CONFIGURATION_WORD_LENGTH (8U) uint8_t cust_db_pswd_a[CUST_DB_PSWD_A_LENGTH] __attribute__((aligned(4))) = { 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23, 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23 }; uint8_t lc_configuration_word[LC_CONFIGURATION_WORD_LENGTH] __attribute__((aligned(4))) = { 0xBA, 0xBA, 0xBA, 0xBA, 0x0, 0x0, 0x0, 0x0 }; /* Minimum data length 8 bytes */ int main(void) { Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); C40_Ip_Init(&C40_Ip_InitCfg); /* PROGRAMMING ADKP */ if (C40_Ip_GetLock(CUST_DB_PSWD_A_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(CUST_DB_PSWD_A_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceWrite(CUST_DB_PSWD_A_ADDR, CUST_DB_PSWD_A_LENGTH, cust_db_pswd_a, MASTER_ID); /* Hardfaults here, but UTEST program is actually successful */ while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; /* ADVANCING LC */ if (C40_Ip_GetLock(LC_CONFIGURATION_WORD_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceSectorErase(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); while (C40_Ip_MainInterfaceSectorEraseStatus() == C40_IP_STATUS_BUSY) ; C40_Ip_MainInterfaceWrite(LC_CONFIGURATION_WORD_ADDR, LC_CONFIGURATION_WORD_LENGTH, lc_configuration_word, MASTER_ID); while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; while (true) ; return 0U; }   my .mex configuration is as such -  Any inputs as to what I am doing wrong? With regards, Hareesh S Re: S32K3 UTEST program generates hardfault Hi Please check the value of "21.7.1.3 Module Configuration Status (MCRS)" at address 0x402EC004.  If MCRS[RWE] = 1, it means that an RWW error occurred during a previous read. Then please read the discussion in  "Hard Fault in C40_Ip_MainInterfaceHVJobStatus api when flash is erase in s32k312". Best Regards, Robin Re: S32K3 UTEST program generates hardfault Hello @Robin_Shen, Thanks for reverting back - It was indeed a RWW error as you had suggested. I assumed the UTEST section was a different block and hence flash erase/program functions could run from flash but apparently not. Moving the functions to RAM solved my issues. With regards, Hareesh S
View full article
i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? Hi all, we are looking at using an i.MX 8M Plus board to loop short MP4 clips (4–10 seconds each, H.264, 3840x2160 at 24 fps) on a 1080p HDMI display. The clips come from an AI video generator, e.g. the Gemini Omni Flash model on Veo3 AI, which exports up to 4K (disclosure: I work with Veo3 AI, an independent service, not affiliated with Google). Before setting this up I would like to check the approach. A pipeline like this is what I had in mind: gst-launch-1.0 filesrc location=clip.mp4 ! qtdemux ! h264parse ! vpudec ! imxvideoconvert_g2d ! video/x-raw,width=1920,height=1080 ! waylandsink Questions: Can the 8M Plus VPU decode 4K H.264 at 24 fps in real time, or is it better to transcode the clips to 1080p before copying them to the board? Is imxvideoconvert_g2d the right element for the 4K to 1080p downscale, or is there a zero-copy path into waylandsink? For looping a playlist of clips, is there a recommended way to avoid a black frame between files? Thanks for any pointers. Re: i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? Hi @ethancaldwell  1. imx8mp vpu can decoding 4K video without HW limitation, but only guarantee 1080p performance, and we did SW limitation to 1080p. If you must use 4K, you need to change the source code. So, it's better to transcode the clips to 1080p. 2. please use imxvideoconvert_g2d for scaling. 3. Currently, there is no official, direct solution for seamless switching between multiple files in `gst-launch`. It is recommended to mux multiple files into a single long video beforehand, and then set that single file to play on a loop. B.R
View full article
i.MX 适用于安卓车载主机 – 兼容性,电路板支持包。 产品型号:i.MX 8M Plus / i.MX 95 / i.MX 8QuadXPlus / i.MX 8QuadMax 你好, 我们正在评估 NXP i.MX 应用处理器(i.MX 8M Plus、i.MX 95、i.MX 8QuadXPlus / 8QuadMax),以用于基于 Android 的售后汽车主机。我们想了解哪个部件最符合我们的需求,以及价格和支持条款。如果以上产品均不合适,请从恩智浦的产品组合中推荐其他适合我们开发的替代部件。 产品要求 平台 - Android (AOSP) 13 或更高版本,并包含电路板支持包。源代码(引导加载程序、内核、HAL) - 4 GB DDR4/LPDDR4、64 GB eMMC - 八核处理器(或同等性能的处理器) 优先考虑工业级(-40 至 85 °C)或汽车级(AEC-Q100)温度等级。 展示 - 9英寸1280×800面板,首选LVDS接口(MIPI DSI接口亦可) - 通过 I2C 实现电容式触摸 - 显示颜色调整(对比度、饱和度、色温) 相机和视频 - 通过外部4通道解码器,使用MIPI CSI-2(虚拟通道)连接4个AHD 720p/1080p摄像头,实现360°环绕视角。 - 通过 CVBS 解码器支持 CVBS 倒车摄像头、前置/右摄像头和 AV-IN 视频输入 - 支持 H.264/H.265 1080p 解码;支持多流 H.264 编码,用于前后摄像头录制(例如 4 × 720p) - 具备用于 2D/3D 360° 拼接的 GPU 功能 声音的 - 支持 I2S/TDM(至少一个 8 通道 TDM 端口,共 3 个端口),用于多通道编解码器、FM/AM 调谐器和蓝牙语音 - S/PDIF 输出 - 音频处理,包括 8 段均衡器、跨界、低音炮滤波器和回声消除(请问 HiFi4 DSP 及其软件框架是否可以在 Android 系统下用于此功能) 连接和 I/O - 3 个 USB 2.0 接口(其中一个支持 OTG 功能),用于手机投屏、媒体播放和配件连接。 - 用于 Wi-Fi/蓝牙模块(2.4/5 GHz,蓝牙 5.0 双连接)的 SDIO - 5 个 UART 接口(车载接口盒、附件、蓝牙 HCI、GNSS、调试) - 3 个 I2C 接口、1 个 SPI 接口、2 个以上的 SAR-ADC 通道、3 个 PWM 接口、约 20 个 GPIO 接口 - 可选的:4G LTE(集成或通过 USB/PCIe 模块) 应用功能(请注明您的平台上任何可用或可授权的软件) - 支持 Apple CarPlay 和 Android Auto(有线/无线),手机镜像 - 360°环绕视图(AVM)库 - 音频DSP/音效包 请求提供的信息 1. 以上各部件是否符合我们的要求,以及您推荐的部件 2. 数据手册、硬件设计指南、参考原理图和推荐的电源管理集成电路/存储器 3. Android 电路板支持包。:可用版本(AOSP 和 Android Automotive)、内核版本、路线图、源代码可用性以及提供方式(公开下载、保密协议、许可协议) 4. 任何 SDK 许可费或单位版税(包括 HiFi4 DSP 软件) 5. 评估套件/SOM的可用性、价格和交货时间 6. SoC(或SOM)年产量分别为1万、5万和10万颗时的单价,另加最小起订量和交货周期。 7. 产品寿命/供应承诺 8. 技术支持模式,以及在印度的设计合作伙伴或代理商 谢谢! 此致, 诗条门·托马斯 Re: i.MX for Android car head unit – suitability, BSP 你好, 根据所述要求,我会将i.MX 95和i.MX 8QuadMax列入候选名单。最佳选择主要取决于相机/视频性能还是 HiFi4/音频和汽车软件成熟度哪个才是首要考虑因素。 i.MX95 i.MX 95 是相机和视频工作负载的最佳选择。它提供: 最多六个 Cortex-A55 应用核心 4K H.264/H.265 视频编码和解码 ISP 支持通过 MIPI 虚拟通道连接多个 1080p 流和最多八个摄像头。 支持两个四通道 MIPI-CSI 接口、LVDS 显示和 MIPI-DSI 显示。 多种 UART 和 I2C 接口、ADC 输入、15 通道 I2S/TDM 以及 S/PDIF 接口 汽车和扩展工业温度选项 这使其非常适合四通道 AHD 解码器、CVBS 解码器输入、环绕视图处理和多流录制,前提是所选解码器通过支持的 CSI-2/V4L2 或 Android 摄像头接口公开其流。 选择前需要核实的几点: 确切的 AHD/CVBS 解码器及其 Android 摄像头或 EVS 驱动程序支持 摄像机配置是否在可用车道带宽内使用 CSI 虚拟通道 如果显示器选择 MIPI-DSI,则 MIPI-CSI/DSI 多路复用会比较复杂;LVDS 可能会释放更多 CSI 资源。 由于处理器文档中列出了两个定时器/PWM模块,因此需要三个PWM输出。 HiFi4 DSP 可用性。i.MX 95 的文档中没有列出 HiFi4 DSP,因此音频算法可能需要在应用程序核心或实时核心上运行,或者在外部音频 DSP 上运行。 产品信息: i.MX 95 i.MX8QM 如果汽车认证、HiFi4 音频处理、外围设备覆盖范围和 Android Automotive 功能是主要优先事项,那么 i.MX 8QuadMax 是更好的选择。它提供: 两个 Cortex-A72 应用核心和四个 Cortex-A53 应用核心,外加两个 Cortex-M4F 核心 符合汽车行业 AEC-Q100 标准的订购选项 硬件视频、图形和摄像头处理,支持多摄像头输入 HiFi4 DSP、多个 SAI/ESAI 接口以及用于多声道音频设计的 S/PDIF 接口 具备满足所述车辆接口要求的充足 UART、I2C、SPI、PWM 和 ADC 资源 NXP Android Automotive 在 i.MX 8QuadMax 换成产品名,如“i.mx8-mek是……” 上的支持 主要的缺点是它的架构比 i.MX 95 更老,因此应该使用完整的四摄像头、CVBS、环视和录制工作负载来衡量可用的视频处理和 CPU 裕量。还必须检查确切的摄像头解码器、同时流数和 Android 摄像头集成情况。 产品信息: i.MX 8 应用处理器 i.MX8MPlus i.MX 8M Plus 对工业多媒体设计很有吸引力,因为它包括 HiFi4、LVDS/MIPI-DSI、两个 MIPI-CSI 接口以及 1080p 级 H.264/H.265 视频支持。但是,它有四个 Cortex-A53 内核,是工业级而非汽车级认证,并且只有两个 CSI 摄像头接口。因此,与 i.MX 95 或 i.MX 8QuadMax 相比,它不太适合满足完整的多摄像头车载单元需求。 产品信息: i.MX 8M Plus i.MX8QXP i.MX 8QuadXPlus 提供四个 Cortex-A35 内核和一个 Cortex-M4F 内核,以及多媒体、显示、摄像头和 HiFi4 功能。但是,它的 CPU 性能低于要求的级别。与 i.MX 8QuadMax 和 i.MX 95 相比,它也不是目前首选的 Android Automotive 平台。 Android 电路板支持包。 NXP 的公开 Android 电路板支持包。页面目前列出了对 i.MX 8M Plus、i.MX 8QuadMax/8QuadXPlus 和 i.MX 95 评估平台的 Android 16 支持。构建源代码包和文档通过 NXP 软件门户提供。应确认所选版本的确切源代码和二进制文件覆盖范围、许可条款以及生产再分发权。 目前公开的 Android Automotive 资料主要集中在 i.MX 8QuadMax 和 i.MX 95 平台上。Android Automotive 支持与 Android Auto 手机投影应加以区分。 适用于 i.MX 应用处理器的 Android 电路板支持包 适用于 i.MX 应用处理器的 Android Automotive 电路板支持包。 Apple CarPlay、Android Auto 手机投影、无线连接、AVM/环视库、音频效果包和 HiFi4 软件框架可能需要单独的认证、合作伙伴软件、专业服务或商业许可。不应仅仅因为 SoC 支持所需的硬件接口就假定它们会被包含在内。 总之,选拔路径如下: 如果 HiFi4、汽车认证、音频 I/O、PWM 资源和已建立的 Android Automotive 路径是主要决策因素,请选择 i.MX 8QuadMax。 如果摄像机/视频性能、未来处理裕量和虚拟通道摄像机支持更为重要,并且可以接受外部音频 DSP 或软件音频实现,则选择 i.MX 95。 只有在降低摄像头数量、性能和汽车要求的情况下,才将 i.MX 8M Plus 和 i.MX 8QuadXPlus 作为备选方案。 此致敬礼/Saludos, 阿尔多。
View full article
S32K3をリセットすると、fs26もリセットされますか? S32K3とFS26を使用している場合、電源投入時にFS26とS32K3の初期化が正常に完了し、FS26は通常モードに入ります。この状態でソフトウェアを使用してソフトリセットを実行した場合、ソフトリセット完了後、初期化プロセス中にFS26を再度初期化する必要はありますか? ご指導をお願いいたします。ありがとうございます。 Re: S32K3复位,会让fs26复位吗? はい、どうもありがとうございました! Re: S32K3复位,会让fs26复位吗? 基本的には以上です。 Re: S32K3复位,会让fs26复位吗? S32K3の初期化処理中は、S32K3によってプルダウンされます。初期化が完了するとプルダウンは解除されます。つまり、必ず初期化状態になります。 Re: S32K3复位,会让fs26复位吗? FS26のRSTBが外部からの力によって強制的にローレベルに引き下げられた場合、INIT状態に入ります。また、8秒以上ローレベルに引き下げられた場合、ディープFSモードに入ります。 Re: S32K3复位,会让fs26复位吗? 通常モードに入った後は、FS26レジスタは変更しません。ソフトリセット処理中は、S32K3のRSTBが変化します。このピンはFS26にも接続されており、FS26はこのピンの変化に基づいて関連する動作を実行します。 Re: S32K3复位,会让fs26复位吗? こんにちは、 zuozuo S32Kのみがリセットされ、FS26レジスタの値が変更されず、FS26が正常な状態のままであれば、FS26を初期化する必要はありません。
View full article
PN7220 Currently, we are observing failures in certain NFC XTS test cases on the supported PN7XX chips. Could you please clarify if Google plans to remove the relevant Type B and Type F Card Emulation test items from future XTS test suites? Also, has NXP confirmed this specific aspect with Google? Re: PN7220 Hello @Max4  For the PN7220, you can apply to NXP for a waiver statement and submit it to Google for testing. Best Rgeards, kelly
View full article
MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: Hello Everyone, Currently I am working on a BMS design.  The Main components/design highlights are: 1. MCU: S32k312 2. Network Isolator: MC33664 3. AFE: MC33771 4. Communication mode: TPL Isolation is as shown below: Also,  MCU to MC33664 Comms from Dual SPI.  MC33664 to MC33771C is TPL.  SPI Configuration is set as follows:     1. Wakeup Sequence:    Wake up sequence is pulling the VCOM high keeping it stable at 5V.  2. First Command  First command is a Software Reset command through Global Write with CID set to 0x00.    This is followed by Second Command after a 500 mS delay.  3. Second Command  Second command is a read command to read the Init (0x01) Register to verify the comms.    Second command is failing because it is expected to read 2 frames of 6 Bytes i.e. the echo and the read response but only echo is generated but not the read response.  4. Read Command and Read Response on the TPL Line:    The first pulse train shown in this image is the echo of the read command sent which is properly translated to SPI by MC33664. The second pulse train the actual response from the AFE on the TPL which the MC33664 is failing to translate to the SPI. The visual difference here is that the voltage levels of the echo and read response are different on the TPL which is a suspect to investigate.  Additional Diagnostic Signal Captures:  RDTX+ and RDTX- before the isolator.    2. RDTX+ and RDTX- after the isolator.      Conclusion:  The TPL comms are accepted by the AFE and is producing the responses but the MC33664 is not translating the responses back to SPI RX line which is causing communication timeout failure.  Please help !! Thank you in advance. Re: MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: Hello, Please verify that the wake-up is generated through the MC33664 CSB_TX timing after enabling the MC33664, rather than by forcing VCOM high. Since the AFE response appears on the TPL line, please focus next on the MC33664 receive path and check CSB_RX, SCLK_RX, DATA_RX, SPI mode, 48-bit frame timing, and the signal at both the MC33664 SPI RX pins and the S32K312 pins.  Please note that we do not have a ready made, tested software and evaluation-board combination for the exact S32K312 + MC33664 + MC33771C configuration, so the SPI driver and dual-SPI receive implementation require application specific validation.
View full article
PN7220 現在、サポートされているPN7XXチップの特定のNFC XTSテストケースで故障が確認されています。今後のXTSテストスイートから、関連するType BおよびType Fカードエミュレーションテスト項目を削除する予定があるのか、ご確認いただけますか?また、NXPはこの点についてGoogleと確認済みでしょうか? Re: PN7220 こんにちは、 @Max4さん PN7220については、NXPに免除申請書を申請し、Googleに提出してテストを受けることができます。 よろしくお願いいたします。 ケリー
View full article
Androidカーヘッドユニット i.MX – 適合性、BSP 部品番号:i.MX 8M Plus / i.MX 95 / i.MX 8QuadXPlus / i.MX 8QuadMax こんにちは、 私たちは、Androidベースのアフターマーケットカーヘッドユニット用に、NXP i.MX アプリケーションプロセッサ(i.MX 8M Plus、i.MX 95、i.MX 8QuadXPlus / 8QuadMax)を評価しています。どの部品が最も私たちの要件に合っているのか、価格やサポート条件についても知りたいと思っています。これらのいずれも適切でない場合は、NXPの製品ポートフォリオの中から、弊社の開発に適した代替部品をご提案ください。 製品要件 プラットフォーム - Android (AOSP) 13以降、BSPソース(ブートローダー、カーネル、HALs)を使用 - 4GB DDR4/LPDDR4、64GB eMMC - オクタコアクラスCPU(または同等の性能) - インダストリアル(-40〜85°C)またはオートモーティブ(AEC-Q100)温度グレードが推奨されます 画面 - 9インチ、1280×800ピクセルのパネル、LVDS推奨(MIPI DSIも可) - I2C経由の静電容量式タッチ - ディスプレイの色調整(コントラスト、彩度、色温度) カメラとビデオ - 4台× AHD 720p/1080pカメラを、MIPI CSI-2(仮想チャネル)で外部4チャネルデコーダー経由で360°サラウンドビューを使用。 - CVBSバックカメラ、前後カメラ、CVBSデコーダーによるAV-INビデオ - H.264/H.265 1080pデコード;前後録画用のマルチストリームH.264エンコード(例:4×720p) - 2D/3Dの360°ステッチング対応GPU機能 オーディオ - I2S/TDM(少なくとも1つの8チャネルTDMポート、合計3ポート)はマルチチャネルコーデック、FM/AMチューナー、Bluetooth音声用 - S/PDIF出力 - 8バンドEQ、クロスオーバー、サブウーファーフィルター、エコーキャンセリングのオーディオプロセッシング(Android上でHiFi4 DSPおよびそのソフトウェアフレームワークが使用可能かご確認ください) コネクティビティとI/O - 3 × USB 2.0(1つのOTG)で電話プロジェクション、プレスリリース、製品ニュース、アクセサリ用 - Wi-Fi/Bluetoothモジュール用のSDIO(2.4/5 GHz、BT 5.0デュアル接続) - 5 × UART(車載インターフェースボックス、アクセサリ、BT HCI、GNSS、DEBUG) - 3 × I2C、1 × SPI、2+ SAR-ADCチャネル、3× PWM、~20 GPIO - オプション:4G LTE(統合型またはUSB/PCIeモジュール経由) アプリケーションの機能(プラットフォーム上で利用可能なまたはライセンス可能なソフトウェアを記載してください) - Apple CarPlayおよびAndroid 車載(有線/無線)、電話ミラーリング - 360°サラウンドビュー(AVM)ライブラリ - オーディオDSP/効果音パッケージ 情報提供 1. 上記の各部品が当社の要件および推奨する部分に適合していること 2. データシート、ハードウェアデザインガイド、参照回路図および推奨PMIC/メモリ 3. Android BSP:利用可能なバージョン(AOSPおよびAndroid オートモーティブ)、カーネルバージョン、ロードマップ、ソースの入手可能性、および提供方法(公開ダウンロード、NDA、ライセンス契約) 4. SDKsのライセンス料やユニットごとのロイヤリティ(HiFi4 DSPソフトウェアを含む) 5. 評価キット/SOMの入手可能性、価格およびリードタイム 6. SoC(またはSOM)のユニット価格(年間10K、50K、100Kユニット)、さらにMOQおよびリードタイム 7. 製品の耐久性/供給コミットメント 8. 技術サポートモデルおよびインドにおけるデザインパートナーまたは代理店 よろしくお願いします。 よろしくお願いします、 四条門トーマス Re: i.MX for Android car head unit – suitability, BSP こんにちは、 記載された要件に基づくと、 i.MX 95とi.MX 8QuadMaxを候補として挙げます。最適な選択は主にカメラ/映像性能かHiFi4/オーディオ・自動車ソフトウェアの成熟度のどちらが優先度が高いかによります。 i.MX95 i.MX 95は、カメラおよびビデオ撮影のワークロードにおいて最も有力な候補である。提供するもの: 最大6つのCortex-A55アプリケーションコア 4K H.264/H.265ビデオのエンコードとデコード 複数の1080pストリームと最大8台のカメラをMIPI仮想チャネル経由でサポートするISP 2つの4レーンMIPI-CSIインターフェース、LVDSディスプレイサポート、MIPI-DSIディスプレイサポート 複数のUARTおよびI2Cインターフェース、ADC入力、15レーンI2S/TDM、S/PDIF オートモーティブおよび拡張インダストリアル用の温度オプション これにより、選択されたデコーダーが対応するCSI-2/V4L2またはAndroidカメラインターフェースを通じてストリームを露出すれば、4チャネルAHDデコーダー、CVBSデコーダー入力、サラウンドビュープロセッシング、マルチストリーム録画に適しています。 選択する前に確認すべき点: 正確なAHD/CVBSデコーダーとAndroidカメラまたはEVSドライバのサポート カメラ構成が利用可能なレーン帯域幅内でCSI仮想チャネルを使用しているかどうか MIPI-DSIがディスプレイに選択された場合、MIPI-CSI/DSI多重化が行われます。LVDSを使用すると、より多くのCSIリソースが利用可能になる可能性があります。 プロセッサのドキュメントには2つのタイマー/PWMブロックが記載されているため、3つのPWM出力の要件があります HiFi4 DSPの利用可能性。i.MX 95のドキュメントにはHiFi4 DSPが記載されていないため、オーディオアルゴリズムはアプリケーションコアやリアルタイムコア、または外部オーディオDSP上で動作する必要がある場合があります 製品情報: i.MX 95 i.MX8QM i.MX 8QuadMaxは、自動車認証、HiFi4オーディオプロセッシング、ペリフェラルカバレッジ、Android オートモーティブのイネーブルメントが主な優先事項である場合により適しています。提供するもの: Cortex-A72 2基とCortex-A53アプリケーションコア4基、さらにCortex-M4Fコア 2基 オートモーティブAEC-Q100対応ご注文オプション ハードウェアビデオ、グラフィックス、カメラプロセッシング、複数のカメラ入力に対応しています HiFi4 DSP、複数のSAI/ESAIインターフェース、そしてマルチチャネルオーディオデザイン用のS/PDIF対応 車載インターフェース要件を満たすために十分なUART、I2C、SPI、PWM、ADCリソース NXP Android オートモーティブの i.MX 8QuadMax MEKサポート 主なトレードオフは、i.MX 95よりも古いアーキテクチャであるため、利用可能なビデオプロセッシングやCPUの余裕は、4カメラ、CVBS、サラウンドビュー、録画の全負荷と合わせて測定されるべきだということです。カメラのデコーダー、同時配信数、Androidカメラとの連携も確認する必要があります。 製品情報: i.MX 8アプリケーションプロセッサ i.MX8MPlus i.MX 8M Plusは、HiFi4、LVDS/MIPI-DSI、2つのMIPI-CSIインターフェース、1080pクラスのH.264/H.265ビデオサポートを含むため、インダストリアルマルチメディアデザインに魅力的です。しかし、4つのCortex-A53コアを搭載しており、オートモーティブではなく、インダストリアルの認証で、CSIカメラインターフェースは2つだけです。したがって、i.MX 95やi.MX 8QuadMaxに比べて、完全なマルチカメラヘッドユニットの要件には適していません。 製品情報: i.MX 8M Plus i.MX8QXP i.MX 8QuadXPlusは、4つのCortex-A35コアと1つのCortex-M4Fコアを備え、マルチメディア、ディスプレイ、カメラ、HiFi4機能を備えています。しかし、そのCPU性能は要求されたクラスを下回っている。また、i.MX 8QuadMaxや i.MX 95と比べて現在のAndroid Automotiveプラットフォームとしては推奨されていません。 Android BSP NXPの公開Android BSPページでは、現在 i.MX 8M Plus、i.MX 8QuadMax/8QuadXPlus、i.MX 95の評価プラットフォームに対するAndroid 16サポートが掲載されています。ビルドソースパッケージやドキュメントはNXPソフトウェアポータルを通じて提供されています。選択したリリースについて、正確なソースコードとバイナリの提供範囲、ライセンス条項、および製品版の再配布権を確認する必要があります。 現在公開されているAndroid オートモーティブの資料は、i.MX 8QuadMaxおよび i.MX 95プラットフォームに焦点を当てています。Android オートモーティブのサポートは、Android 車載の電話プロジェクションとは区別されるべきです。 i.MX アプリケーションプロセッサ向けAndroid BSP Android オートモーティブ BSP for i.MXアプリケーション・プロセッサ Apple CarPlay、Android 車載の電話プロジェクション、ワイヤレス・コネクティビティ、AVM/サラウンドビューライブラリ、オーディオエフェクトパッケージ、HiFi4ソフトウェアフレームワークは、別途認証、パートナーソフトウェア、プロフェッショナルサービス、または商用ライセンスを必要とする場合があります。SoCが必要なハードウェアインターフェースをサポートしているからといって、それらが含まれていると考えるべきではありません。 要約すると、選考プロセスは以下のようになります。 HiFi4、自動車資格、オーディオI/O、PWMリソース、確立されたAndroid オートモーティブの経路が主な判断要素であれば、8QuadMax i.MX 選択してください。 カメラ/映像性能、FUTUREのプロセッシング余裕、仮想チャネルカメラのサポートがより重要で、外部オーディオDSPやソフトウェアオーディオ実装が許容される場合は i.MX 95を選択してください。 カメラ数、性能、オートモーティブ要件が減った場合 i.MX、8M Plusと i.MX 8QuadXPlusは副次オプションとして残しておくのが良いでしょう。 よろしくお願いいたします。 アルド。
View full article
PN7220 目前,我们发现支持的 PN7XX 芯片在某些 NFC XTS 测试用例中出现故障。请问谷歌是否计划从未来的 XTS 测试套件中移除相关的 B 型和 F 型卡模拟测试项?另外,NXP是否已向谷歌确认过这一具体方面? Re: PN7220 你好@Max4 对于 PN7220,您可以向 NXP 申请豁免声明,并将其提交给 Google 进行测试。 此致敬礼, 凯莉
View full article
MCU (S32k312) 至 MC33664 (网络隔离器) 至 MC33771C (AFE) 通信无响应诊断: 大家好, 目前我正在进行电池管理系统(BMS)的设计工作。 主要元器件/设计亮点如下: 1. MCU:S32k312 2. 网络隔离器:MC33664 3. AFE:MC33771 4. 通信方式:TPL 隔离情况如下所示: 还, MCU 与 MC33664 通过双 SPI 进行通信。 MC33664 至 MC33771C 是 TPL。 SPI配置设置如下:    1.唤醒序列:    唤醒序列将 VCOM 拉高,使其稳定在 5V。  2. 第一条命令  第一个命令是通过全局写入执行的软件 RESET 命令,CID 设置为 0x00。    随后,在延迟 500 毫秒后发出第二个命令。  3. 第二条命令  第二条命令是读取 Init (0x01) 寄存器的READ命令,用于验证通信。    第二个命令失败,因为它应该读取 2 个 6 字节的帧,即回显和读取响应,但只生成了回显,没有生成读取响应。  4. 在 TPL 线上READ命令和读取响应:    图中显示的第一组脉冲是发送的READ命令的回波,MC33664 已将其正确翻译为 SPI 信号。第二组脉冲是 TPL 上 AFE 的实际响应,MC33664 未能将其翻译为 SPI 信号。此处的视觉差异在于 TPL 上回波和读取响应的电压等级不同,这可能是需要调查的原因。  其他诊断信号捕获:  隔离器之前的 RDTX+ 和 RDTX-。    2. 隔离器后的 RDTX+ 和 RDTX-。      结论:  AFE 接受 TPL 通信并产生响应,但 MC33664 没有将响应已翻译回 SPI RX 线,导致通信超时失败。  请帮帮我!! 先感谢您。 Re: MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: 你好, 请验证在启用 MC33664 后,是否通过 MC33664 CSB_TX 时序产生唤醒,而不是通过强制 VCOM 为高电平产生唤醒。 由于AFE响应出现在TPL线上,接下来请重点检查MC33664接收路径,并检查CSB_RX、SCLK_RX、DATA_RX、SPI模式、48位帧时序,以及MC33664 SPI RX引脚和S32K312引脚上的信号。 请注意,我们没有针对 S32K312 + MC33664 + MC33771C 配置的现成、经过测试的软件和评估板组合,因此 SPI 驱动程序和双 SPI 接收实现需要针对特定应用进行验证。
View full article
Will resetting the S32K3 cause the fs26 to reset? Now, using S32K3 and FS26, during power-on, the initialization of FS26 and S32K3 is completed normally, and FS26 enters normal mode. If I use software to perform a soft reset at this time, after the soft reset is completed, is it necessary to initialize FS26 again during the initialization process? Requesting guidance, thank you. Re: S32K3复位,会让fs26复位吗? Okay, thank you very much! Re: S32K3复位,会让fs26复位吗? That's basically it. Re: S32K3复位,会让fs26复位吗? During the initialization process of S32K3, it will be pulled low by S32K3. It will be released after the initialization is completed. In other words, it will definitely be brought to the init state. Re: S32K3复位,会让fs26复位吗? If the RSTB of FS26 is forcibly pulled low by an external force, it will enter the INIT state; or if it is pulled low for more than 8 seconds, it will enter Deep FS mode. Re: S32K3复位,会让fs26复位吗? After entering normal mode, I will not modify the FS26 register. During the soft reset process, the RSTB of the S32K3 will change. This pin is also connected to the FS26, and the FS26 will perform related actions based on the change of this pin. Re: S32K3复位,会让fs26复位吗? Hi zuozuo If only the S32K is reset without changing the FS26 register value, and FS26 is still in normal state, then there is no need to initialize FS26.
View full article
i.MX for Android car head unit – suitability, BSP Part number: i.MX 8M Plus / i.MX 95 / i.MX 8QuadXPlus / i.MX 8QuadMax Hello, We are evaluating NXP i.MX applications processors (i.MX 8M Plus, i.MX 95, i.MX 8QuadXPlus / 8QuadMax) for an Android-based aftermarket car head unit. We would like to understand which part best meets our requirements, along with pricing and support terms. If none of these is suitable, please suggest an alternative part from NXP's portfolio for our development. PRODUCT REQUIREMENTS Platform - Android (AOSP) 13 or later, with BSP source (bootloader, kernel, HALs) - 4 GB DDR4/LPDDR4, 64 GB eMMC - Octa-core class CPU (or equivalent performance) - Industrial (-40 to 85 °C) or automotive (AEC-Q100) temperature grade preferred Display - 9" 1280×800 panel, LVDS preferred (MIPI DSI acceptable) - Capacitive touch over I2C - Display colour adjustment (contrast, saturation, colour temperature) Camera and video - 4 × AHD 720p/1080p cameras via an external 4-channel decoder on MIPI CSI-2 (virtual channels), for 360° surround view - CVBS reverse camera, front/right camera and AV-IN video via a CVBS decoder - H.264/H.265 1080p decode; multi-stream H.264 encode for front/rear recording (e.g. 4 × 720p) - GPU capability for 2D/3D 360° stitching Audio - I2S/TDM (at least one 8-channel TDM port, 3 ports in total) for a multi-channel codec, FM/AM tuner and Bluetooth voice - S/PDIF output - Audio processing for an 8-band EQ, crossover, subwoofer filter and echo cancellation (please advise whether the HiFi4 DSP and its software framework can be used for this under Android) Connectivity and I/O - 3 × USB 2.0 (one OTG) for phone projection, media and accessories - SDIO for a Wi-Fi/Bluetooth module (2.4/5 GHz, BT 5.0 dual connection) - 5 × UART (vehicle interface box, accessory, BT HCI, GNSS, debug) - 3 × I2C, 1 × SPI, 2+ SAR-ADC channels, 3 × PWM, ~20 GPIO - Optional: 4G LTE (integrated or via USB/PCIe module) Application features (please indicate any software available or licensable on your platform) - Apple CarPlay and Android Auto (wired/wireless), phone mirroring - 360° surround view (AVM) library - Audio DSP / sound-effect packages INFORMATION REQUESTED 1. Suitability of each part above against our requirements, and the part you recommend 2. Datasheet, hardware design guide, reference schematics and recommended PMIC/memory 3. Android BSP: available versions (AOSP and Android Automotive), kernel version, roadmap, source availability, and how it is provided (public download, NDA, licence agreement) 4. Any SDK licence fees or per-unit royalties (including HiFi4 DSP software) 5. Evaluation kit / SOM availability, price and lead time 6. Unit pricing for the SoC (or SOM) at 10K, 50K and 100K units per year, plus MOQ and lead time 7. Product longevity / supply commitment 8. Technical support model, and design partners or distributors in India Thank you. Best regards, Shijomon Thomas Re: i.MX for Android car head unit – suitability, BSP Hello, Based on the requirements described, I would shortlist the i.MX 95 and i.MX 8QuadMax. The best choice depends mainly on whether camera/video performance or HiFi4/audio and automotive software maturity has the highest priority. i.MX95 The i.MX 95 is the strongest candidate for the camera and video workload. It provides: Up to six Cortex-A55 application cores 4K H.264/H.265 video encode and decode An ISP supporting multiple 1080p streams and up to eight cameras through MIPI virtual channels Two four-lane MIPI-CSI interfaces, LVDS display support, and MIPI-DSI display support Multiple UART and I2C interfaces, ADC inputs, 15-lane I2S/TDM, and S/PDIF Automotive and extended-industrial temperature options This makes it a good fit for a four-channel AHD decoder, CVBS decoder inputs, surround-view processing, and multi-stream recording, provided that the selected decoders expose their streams through a supported CSI-2/V4L2 or Android camera interface. Points to verify before selecting it: The exact AHD/CVBS decoder and its Android camera or EVS driver support Whether the camera configuration uses CSI virtual channels within the available lane bandwidth The MIPI-CSI/DSI multiplexing if MIPI-DSI is selected for the display; LVDS may leave more CSI resources available The requirement for three PWM outputs, since the processor documentation lists two Timer/PWM blocks HiFi4 DSP availability. The i.MX 95 documentation does not list a HiFi4 DSP, so audio algorithms may need to run on the application or real-time cores, or on an external audio DSP Product information: i.MX 95 i.MX8QM The i.MX 8QuadMax is the better fit when automotive qualification, HiFi4 audio processing, peripheral coverage, and Android Automotive enablement are the main priorities. It provides: Two Cortex-A72 and four Cortex-A53 application cores, plus two Cortex-M4F cores Automotive AEC-Q100-qualified ordering options Hardware video, graphics, and camera processing, with support for multiple camera inputs HiFi4 DSP, multiple SAI/ESAI interfaces, and S/PDIF for the multi-channel audio design Sufficient UART, I2C, SPI, PWM, and ADC resources for the stated vehicle-interface requirements NXP Android Automotive support on the i.MX 8QuadMax MEK The main trade-off is that it is an older architecture than the i.MX 95, so the available video-processing and CPU headroom should be measured with the complete four-camera, CVBS, surround-view, and recording workload. The exact camera decoder, simultaneous stream count, and Android camera integration must also be checked. Product information: i.MX 8 applications processors i.MX8MPlus The i.MX 8M Plus is attractive for industrial multimedia designs because it includes HiFi4, LVDS/MIPI-DSI, two MIPI-CSI interfaces, and 1080p-class H.264/H.265 video support. However, it has four Cortex-A53 cores, industrial rather than automotive qualification, and only two CSI camera interfaces. It is therefore less suitable for the complete multi-camera head-unit requirement than the i.MX 95 or i.MX 8QuadMax. Product information: i.MX 8M Plus i.MX8QXP The i.MX 8QuadXPlus provides four Cortex-A35 cores and one Cortex-M4F core, together with multimedia, display, camera, and HiFi4 capabilities. However, its CPU performance is below the requested class. It is also not the preferred current Android Automotive platform compared with the i.MX 8QuadMax and i.MX 95. Android BSP NXP's public Android BSP page currently lists Android 16 support for the i.MX 8M Plus, i.MX 8QuadMax/8QuadXPlus, and i.MX 95 evaluation platforms. Build-source packages and documentation are provided through the NXP software portal. The exact source and binary coverage, license terms, and production redistribution rights should be confirmed for the selected release. The current public Android Automotive materials focus on the i.MX 8QuadMax and i.MX 95 platforms. Android Automotive support should be distinguished from Android Auto phone projection. Android BSP for i.MX applications processors Android Automotive BSP for i.MX applications processors Apple CarPlay, Android Auto phone projection, wireless connectivity, AVM/surround-view libraries, audio-effect packages, and HiFi4 software frameworks may require separate certification, partner software, professional services, or commercial licenses. They should not be assumed to be included solely because the SoC supports the required hardware interfaces. In summary the path for selection would be: Select i.MX 8QuadMax if HiFi4, automotive qualification, audio I/O, PWM resources, and the established Android Automotive path are the primary decision factors. Select i.MX 95 if camera/video performance, future processing headroom, and virtual-channel camera support are more important, and an external audio DSP or software audio implementation is acceptable. Keep i.MX 8M Plus and i.MX 8QuadXPlus as secondary options only if the camera count, performance, and automotive requirements are reduced. Best regards/Saludos, Aldo.
View full article
S32K3复位,会让fs26复位吗? 现在使用S32K3和fs26,在上电过程中,正常完成fs26和s32k3的初始化工作,fs26进入正常模式,假如我此时使用软件进行软复位,执行完软复位之后,在初始化过程中还需要初始化fs26吗? 请求指导,谢谢 Re: S32K3复位,会让fs26复位吗? 好的,非常感谢! Re: S32K3复位,会让fs26复位吗? 对的基本上这样了。 Re: S32K3复位,会让fs26复位吗? S32K3在重启初始化,开始过程中,会被s32k3拉低,之后初始化完成,才会被释放,也就是他肯定会被带到init状态? Re: S32K3复位,会让fs26复位吗? 假如FS26的RSTB被外部拉强制拉低,他会进入INIT的状态,或者外部拉低8s以上就进入了Deep FS模式 Re: S32K3复位,会让fs26复位吗? 进入normal之后,我不会修改fs26寄存器,在执行软复位过程中,s32k3的rstb会发生变化,此引脚也连接fs26,fs26会根据此引脚变化,进行相关的动作? Re: S32K3复位,会让fs26复位吗? Hi zuozuo 假如是只是复位S32K并没有更改FS26的寄存器值,而且FS26还在normal状态下,这个时候无需初始化FS26.
View full article
MCU(S32k312)からMC33664(ネットワークアイソレータ)からMC33771C(AFE)通信無応答診断: 皆さん、こんにちは。 現在、BMSの設計に取り組んでいます。 主な構成要素/デザインのハイライトは以下の通りです: 1. MCU:S32k312 2. ネットワークアイソレータ:MC33664 3. AFE:MC33771 4. 通信モード:TPL アイソレータは以下の通りです: それから、 MCUからデュアルスパイからのMC33664通信へ。 MC33771C MC33664はTPLです。  SPI構成は以下の通りに設定されます:    1.起動シーケンス:    ウェイクアップシーケンスはVCOMをハイレベルに引き上げ、5Vで安定させます。  2. 最初の命令  最初のコマンドは、CIDを0x00に設定したグローバル書き込みによるソフトウェアリセットコマンドです。    これに続いて、500ミリ秒の遅延の後、第2コマンドが送信されます。  3. 第二の命令  2 番目のコマンドは、通信を確認するために Init (0x01) レジスタを読み取る読み取りコマンドです。    2番目のコマンドが失敗するのは、6バイトのフレームを2つ(つまり、エコーと読み取り応答)読み込むことが期待されているにもかかわらず、エコーのみが生成され、読み取り応答が生成されないためです。  4. TPL回線での読み取りコマンドと読み取り応答:    この画像に示されている最初のパルス列は、MC33664によってSPIに正しく変換された読み出しコマンドのエコーです。2番目のパルス列は、TPL上のAFEからの実際の応答ですが、MC33664はこれをSPIに変換できていません。ここで視覚的にわかる違いは、エコーと読み出し応答の電圧レベルがTPL上で異なっていることであり、これが調査すべき原因と考えられます。  追加の診断信号キャプチャ:  アイソレータの前にRDTX+とRDTX-を配置します。    2. アイソレータ後のRDTX+とRDTX-。      結論:  TPL通信はAFEによって受け入れられ、応答が生成されますが、MC33664が応答をSPI RXラインに変換しないため、通信タイムアウトエラーが発生します。 助けてください!! よろしくお願いします。 Re: MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: こんにちは、 MC33664を有効にした後、ウェイクアップがVCOMを強制的にハイにするのではなく、MC33664のCSB_TXタイミングによって生成されることを確認してください。 AFE応答がTPLラインに現れるため、次にMC33664の受信経路に注目し、CSB_RX、SCLK_RX、DATA_RX、SPIモード、48ビットフレームタイミング、およびMC33664のSPI RXピンとS32K312ピンの両方の信号を確認してください。 なお、S32K312 + MC33664 + MC33771C構成のための既成のテスト済みソフトウェアと評価ボードの組み合わせは存在しないため、SPIドライバおよびデュアルSPI受信実装はアプリケーション固有の検証が必要です。
View full article
Q3 2026 | MCUXpresso Software, Tools & Developer Quarterly Update MCUXpresso 26.09 Has Arrived: Here's What's New If your workflow includes MCUXpresso, this release is worth a closer look. Here's a breakdown of what's new and why it matters. EdgeFast Open MCUXpresso SDK 26.09.00 migrates from the EdgeFast Bluetooth stack for i.MX RT and MCX devices connected to an NXP radio co-processor (e.g., IW6xx devices) to the EdgeFast Open Bluetooth stack. EdgeFast Open is an open-source Bluetooth host stack based on the stack from the Zephyr community. This migration will make Bluetooth-based applications smaller size (Flash and RAM) due to architecture changes versus the previously used EdgeFast Bluetooth stack. Given that EdgeFast Bluetooth adopted Zephyr Bluetooth stack API’s the migration from EdgeFast Bluetooth to EdgeFast Open is expected to be minimally disruptive. For uses who want to continue using the EdgeFast Bluetooth stack, this continues to be supported and maintained on the SDK 26.06.00-LTS release that was introduced in Q2. Documentation SDK release notes have been updated to improve the quality, and relevance of results when using the built-in search tools. Example product documentation has also been reworked to improve readability, and useability in the web-based interface. Security updates Migration to MBEDTLS 3.x has been complete for all middleware components that depend on security. MBEDLS 4.2 is starting to be introduced into MCUXpresso SDK, offering a gradual transition to the next MBEDTLS LTS release. RTOS updates Updated FreeRTOS kernel and libraries for improved reliability, security and ecosystem compatibility New product introduction support MCXE327, MCXN556S (123-WLCSP), MCXN947T, MCXC352/353, MCXA556/557 (WLCSP), i.MX RT2660 , i.MX 93 Cortex-A55, i.MX 8M Mini Cortex-A53, i.MX 95 Cortex-A55, FRDM-IMXRT1152, FRDM-MCXE32B, KW43-LOC, MCXW70-LOC.   Toolchain and IDE updates IAR Embedded Workbench for Arm updated to v9.70.2 MCUXpresso toolchain components aligned with the 26.06.00 release Learn more: SDK documentation and GitHub Release Notes Over the past three months, the MCUXpresso for Visual Studio Code team has delivered a series of updates focused on productivity, usability, and next-generation development workflows. Experimental Agentic AI Toolkit The headline feature this quarter is experimental access to the Agentic AI Toolkit, enabling developers to interact with MCUXpresso through AI coding assistants such as GitHub Copilot. Developers can install repositories, create and build projects, program devices, perform debugging tasks, and execute MCUXpresso-specific workflows directly from AI chat sessions. Energy Measurement with MCU-Link Pro LinkServer 26.09 introduces Target Power and Energy Measurement support for MCU-Link Pro and NXP development boards with power measurement circuits, providing visibility into device power and energy consumption directly within the development workflow. It includes both command-line and standalone GUI usage of the features. This helps developers better understand and optimize energy usage on their target hardware, up to CI/CD integration, and automated testing. Easier Project Management July and August releases delivered numerous customer-requested improvements that simplify everyday development, including faster project imports, improved repository management, more reliable project conversion from MCUXpresso IDE, better build configuration handling, and enhanced archive support. Better DSP and eIQ Example Support Developers working with DSP and eIQ examples will benefit from improved build automation that eliminates unnecessary toolchain errors when using supplied binaries, reducing setup complexity and improving the out-of-box experience. Experimental Secure Debug Authentication An additional experimental feature, Secure Debug Authentication, adds support for authenticating with protected devices before establishing a debug session when required by the device security configuration. Explore the latest updates in the Visual Studio Marketplace Changelog and discover how MCUXpresso for VS Code continues to make embedded development more productive, intelligent, and efficient. Learn more: MCUXpresso VS Code Documentation and Extension Change Log MCUXpresso Secure Provisioning Tool (SEC) 26.09 - Broad coverage, stronger security, one unified tool MCX Family Support & Improvement Added support for MCX E32x, L14x and W70x Secure Installer erasure improvement for MCX A1xx/2xx/3xx and L14x, L25x Other significant updates Added support for i.MX RT1150, i.MX RT1185/118C, KW43 and i.MX 943 processors Debug authentication integrated into VS Code Six clicks to secure your IP Blog — Prototype to secure deployment in six clicks Video — Six steps to secure your IP with MCUXpresso Training — How to build a secure image with MCUXpresso Secure Provisioning Tool Learn more: MCUXpresso Secure Provisioning Tool   SPSDK 3.11.0 - Build your own secure production workflow New features include: Added IPED tool for external flash encryption (nxpimage) Added debug mailbox command for MCX C1xx devices (nxpdebugmbox)   New devices supported include i.MX RT1150/1152, MCX A557, MCX E32x, MCX W70 and KW43 families. Learn more: SPSDK Config Tools 26.09 – Faster setup, timely insights MCU Tools Now support preliminary public releases of processor data i.MX Updates DDR Tool extended with new boards and memories System Manager has updated validation engine Learn more: MCUXpresso Config tools and Config tools for i.MX release notes Real-Time Edge 3.5 Released in July Fast Boot: Enables boot of two Cortex-A cores in parallel and decreases boot time especially for use cases with RTOS on Cortex-A core. Consolidated Images: Leveraging Yocto Multiconfig to enable single system image covering multiple boards (from same family). Updated Base: Now rebased on Linux Kernel 6.18.20 / Yocto Wrynose. GUI Guider v2.0.1 Released in August Figma-to-GUI Guider import New UI for GUI Guider Visual flowchart-style event system Added FRDM-MCXA577, FRDM-MXCA287 & FRDM-MXCA266 LVGL v9.4 support across MCX, RW, i.MX RT and i.MX platforms MCU on Eclipse Installing MCUXpresso Installer in DevContainer | MCU on Eclipse   Tool Time | LinkedIn Live Event Tool Demonstrations July – Serial Memory Tool – a smarter way to configure and work with serial memory in VS Code August – MCUXpresso Installer – create consistent development environments and simplify your setup experience September – G-Knob – Connecting click shields to FRDM Boards using MCUXpresso Tools EdgeVerse Techcast | Apple • Spotify • YouTube Audit Alert: Andrei's Expert Take on NXP's Software Suite Steering Success: Automotive Developers Take the Wheel in the Application Code Hub Empowering Developers with Long-Term Support in MCUXpresso SDK Winning with Efficient Performance: Why Architecture Matters More Than Clock Speed The Sound of Smart Glasses: Building Conversational AI at the Edge Unlocking Embedded Development: Insights from DigiKey's Experts and Tech Forum Application Code Hub | Spotlights RW612 Connectivity Momentum BLE Relay: Multi Peripheral to Single Central Connection RW612 Wi-Fi Secure MQTT Demonstration Wi‑Fi Access Point to Ethernet Layer‑2 Bridging Wi-Fi Sensing using Sniffer on RW61x with Zephyr OS MCXC162 focused on Low-Power and Motor Control Low Power Presence Detection Low Power Temperature Sensing One shunt FOC on MCXC162 Remote-System Architectures Wireless UART Throughput on RT1060EVKC and IW416 Servo Motor Multi-Control via Wireless UART High-Value Peripheral Enablement NFC Controller on MCXC242, 6-Color ePaper Display on MCXA266 AI enablement Agentic AI Network Management System (i.MX 8M Plus / 95 - Ara240)  
View full article
MCUXpresso Tooltime Episodes NXP LinkedIn Live series Tool Time: practical embedded development, on demand Catch up on conversations and demonstrations featuring NXP development tools, SDK workflows, board enablement, debugging, visualization, configuration and user-interface design. Browse past episodes See how the MCUXpresso ecosystem comes together Tool Time brings developers closer to the software and workflows used to build with NXP microcontrollers. Across the series, the episodes cover MCUXpresso SDK releases, VS Code integration, CMake and Kconfig projects, Configuration Tools, GUI Guider, FreeMASTER, LinkServer, Serial Memory Tool, MCUXpresso Installer, cloud connectivity and FRDM board expansion. Use this replay library to explore each topic, meet the hosts and guests, and go directly to the available LinkedIn episode. What the series provides Focused sessions on MCUXpresso tools and embedded-development workflows Topics spanning setup, configuration, build systems, debug, visualization and prototyping Conversations with NXP specialists and ecosystem guests Direct links to rewatch each available episode on LinkedIn Watch past episodes Choose an episode and select Watch on LinkedIn. Newest episodes are listed first. NOVEMBER 2026   |   EMBEDDED UI with GUI GUIDER From Prompt to Embedded UI with GUI Guider Describe the GUI you want and let AI help bring the concept to life. Host: Mike Susen   Guest: Zhenhua Luo Watch on LinkedIn OCTOBER 2026   |   AGENTIC AI Introducing our new Agentic AI Toolkit Explore how AI agents can discover, understand and use products to help improve customer enablement. Host: Kyle Dando   Guest: Marius-Lucian Andrei Watch on LinkedIn SEPTEMBER 2026   |   HARDWARE EXPANSION Adding a click shield to a FRDM board (G-Knob) A Tool Time episode focused on adding a G-Knob click shield to a FRDM board. Host: Kyle Dando   Guest: Patrik Fillner Watch on LinkedIn AUGUST 2026   |   INSTALLATION MCUXpresso Installer A focused discussion and demonstration of MCUXpresso Installer. Host: Jose Ocampo Hernandez   Guest: Alexandra Maracine Watch on LinkedIn JULY 2026   |   SERIAL MEMORY Serial Memory Tool A Tool Time session featuring the Serial Memory Tool. Host and guest: Patrik Fillner Watch on LinkedIn JUNE 2026   |   DEBUG LinkServer A focused episode covering LinkServer. Host: Kyle Dando   Guest: Cristian Lupascu Watch on LinkedIn MAY 2026   |   DATA VISUALIZATION FreeMASTER data visualization A Tool Time session focused on FreeMASTER data visualization. Host: Kyle Dando   Guest: Patrik Fillner Watch on LinkedIn APRIL 2026   |   EMBEDDED GUI GUI Guider A focused discussion and demonstration of GUI Guider. Host: Kyle Dando   Guest: Mike Susen Watch on LinkedIn MARCH 2026   |   CONFIGURATION MCUXpresso Configuration Tools A Tool Time episode focused on MCUXpresso Configuration Tools. Host: Patrik Fillner   Guest: Petr Hradsky Watch on LinkedIn FEBRUARY 2026   |   CLICK BOARDS 6 clicks A Tool Time episode titled “6 clicks.” Host: Kyle Dando   Guest: Stella Or Watch on LinkedIn JANUARY 2026   |   BUILD CONFIGURATION CMake and Kconfig projects on FRDM-MCXN947 A session on CMake and Kconfig projects using the FRDM-MCXN947. Host: Kyle Dando   Guest: Jose Ocampo Hernandez Watch on LinkedIn DECEMBER 2025   |   CLOUD CONNECTIVITY Bluetooth to Cloud on MCX W71 and RW612 A Bluetooth-to-cloud project running on the MCX W71 and RW612. Host: Kyle Dando   Guest: Chris Gammell, Golioth Watch on LinkedIn NOVEMBER 2025   |   RELEASE HIGHLIGHTS SDK 25.10, VS Code and Configuration Tools A session covering the 25.10 SDK release, VS Code integration and streamlined Configuration Tools. Host: Kyle Dando   Guest: Jose Ocampo Hernandez Watch on LinkedIn OCTOBER 2025   |   SERIES OVERVIEW MCUXpresso IDEs, SDK, Configuration and Security A session covering MCUXpresso IDEs, SDK, Configuration Tools and security tooling. Host: Kyle Dando Replay link not listed Episode links open LinkedIn in a new browser tab. LinkedIn sign-in may be required to view some replays. Application Code Hub FreeMASTER LinkServer MCUXpresso Config Tools MCUXpresso for VS Code MCUXpresso SDK
View full article
SAF Framework License query Hello, We are evaluating the NXP S32K series for a safety-critical railway product and exploring the S32K3 Safety Software Framework (SAF). We have following queries regarding the license. Can a SAF Single Project License be used by multiple engineers working on the same project from multiple location ( USA, India)? Within the same project, we have multiple boards that use the same S32K3 MCU family. Can a SAF Single Project License be used across all such boards as long as they belong to the same project? Re: SAF Framework License query Hello @beherehardik, This topic is outside the scope of our online technical support. If your company has NXP FAEs assigned , please contact them directly. Otherwise, please reach out to your local distributor for further assistance. Thank you for your understanding. Regards, Daniel
View full article
PN5190B2HN/C131Y chip FW version The manual for PN5190B2HN/C131Y states that it has built-in Firewall 3.2. However, the official Firewall is only updated to Firewall 3.08. What is the difference between these two? I'd like to know the import time for FW version 3.07 and above. Re: PN5190B2HN/C131Y 芯片FW版本 Initialized with FW 3.2, supports encrypted firmware download. For the version history about FW3.07 please refer the link below: RN00066: PN5190 B2 firmware release v03.08 | NXP Semiconductors
View full article
SAF框架许可证查询 你好, 我们正在评估 NXP S32K 系列产品在安全至关重要的铁路产品中的应用,并探索 S32K3 功能安全软件框架 (SAF)。 关于许可证,我们有以下疑问。 SAF 单项目许可证是否可以供多个工程师在多个地点(例如美国、印度)使用,共同完成同一个项目? 在同一个项目中,我们有多个板使用相同的 S32K3 MCU 系列。SAF 单一项目许可证是否可以在所有属于同一项目的板上使用? Re: SAF Framework License query 你好@beherehardik , 此主题超出我们的在线技术支持范围。 如果贵公司已指派 NXP FAE,请直接与他们联系。否则,请联系您当地的代理商以获取进一步帮助。 感谢您的理解。 问候, 丹尼尔
View full article
rt1180 フラッシュメモリ上のプログラム こんにちは、 RT1180で変な問題があります。M33でMCUXpresso提案のデフォルト設定で新しいプロジェクトを作成し、Flashにコンパイルしてダウンロードすると、プログラムは問題なく動作します。デフォルトの「Hello Word」を正しく印刷すれば、すべての作業が問題なく進みます。 M7で新しいプロジェクトを使って同じことを行うと、コンパイルは正しく行われますが、デバッグしようとすると、次のような結果になります。 LinkServer RedlinkMulti Driver v24.12(2024年12月18日 18:34:07 - crt_emu_cm_redlinkビルド869) C:/Users/colombos/Documents/MCUXpressoIDE_24.12.148/workspace/MIMXRT1189_Project_m7/Debug\MIMXRT1189xxxxx.xmlでチップXMLファイルを発見 既存のLinkServerプロセスに再接続しました。 ============= スクリプト: RT1180_connect_M33_wake_M7_ITC.scp ============= RT1180 Connect M33およびWake M7 to ITCスクリプト DpID = 5BA02477 APID = 0x74770001 ************ シリアルダウンローダーモードに入るには runBootLoader を実行してください ************* PC = 1001BC6A、SP = 2001FFF4 DpID = 5BA02477 APID = 0x74770001 R15 = 0x1001C086 ********** CM33を初期化します ************ 0xE000E180 + 0x00000040 を 0xFFFFFFFF で埋めます 0xE000E280 + 0x00000040 を 0xFFFFFFFF で埋めます 0x201E0000 + 0x00020000 を 0x00000000 で埋めます 0x20200008 + 0x0001FFF8 を 0x00000000 で埋めます ************* CM7 を有効にする ************** ************ 時計の準備 ************* ******** 着陸ゾーンの作成 ********* 0x303C0000 + 0x00020000 を 0x00000000 で埋めます 0x303E0000 + 0x00020000 を 0x00000000 で埋めます 0x30400000 + 0x00020000 を 0x00000000 で埋めます 0x30420000 + 0x00020000 を 0x00000000 で埋めます ************* キックオフ CM7 ************** 応答1:0xE1D20206 応答2:0x000000D6 TAP 0: 5BA02477 AP 0: APID: 74770001 ROMテーブル: 00000002 TAP 0: 5BA02477 AP 1: APID: 44770002 ROMテーブル: 80000003 TAP 0: 5BA02477 コア 2: M7 APID: 74770001 ROM テーブル: E00FD003* TAP 0: 5BA02477 コア 3: M33 APID: 74770001 ROM テーブル: E00FF003 APID = 0x74770001 ============= スクリプト終了 ============================================== プローブファームウェア:MCU-LINK搭載(r1E2) CMSIS-DAP V3.153(NXPセミコンダクターズ) シリアル番号:OK1PG5OV03J1X VID:PID: 1FC9:0143 USBパス: 0001:002a:00 適切なコアを検索した後、コア2のメモリを使用する (30) エミュレーター接続済み デバッグインターフェースタイプ = CoreSight DP(DAP DP ID 5BA02477)over SWD TAP 0 プロセッサタイプ = DAP AP 2 上の Cortex-M7(CPU ID 00000C27) ハードウェアブレークポイントの数 = 8 フラッシュパッチの数 = 0 ハードウェアウォッチポイントの数 = 4 プローブ(0): 接続済み&リセット。DPID: 5BA02477。CPUID: 00000C27。情報: デバッグプロトコル:SWD。RTCK: 無効です。ベクターキャッチ:無効。 CoreSightデバッグROMの内容: RBASE E00FD000: CID B105100D PID 000008E88C ROM (タイプ 0x1) ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (タイプ 0x1) ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (タイプ 0x1) ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (タイプ 0x0) ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (タイプ 0x0) ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (タイプ 0x0) ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (タイプ 0x0) ROM 2 E0041000:CID B105900D PID 04001BB975 CSt ARM ETMv4.0 タイプ0x13 トレースソース - コア ROM 2 E0042000: CID B105900D PID 04004BB906 CSt タイプ 0x14 デバッグ制御 - トリガー、例:ECT ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTFタイプ 0x12 トレースリンク - トレースファンネル/ルーター CM7 Rev. 7.0 DTCM: 512KB ITCM: 512KB LoUU: レベル2: LoC: レベル2 レベル1キャッシュタイプ:命令+データ ICache 32K: WT: Y WB: Y RA: Y WA: Y NumSets: 512 Assoc: 2 LineSize: 8 DCache 32K: WT: Y WB: Y RA: Y WA: Y NumSets: 256 Assoc: 4 LineSize: 8 NXP: MIMXRT1189xxxxx SFDP JEDEC ID MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfxを使用してSPI上のv.2外部フラッシュデバイスを検査しました。 イメージ「iMXRT1180_SFDP_FlexSPI1_A_QSPI 2024年12月18日 17:30:53」 フラッシュドライバーの開MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfx フラッシュドライバーを実行するためにVECTRESETを送信する ドライバ起動タイムアウト後(302 5msのリトライ) ドライバーアドレス 開始: 20000000 エントリー番号: 2000009D 終了: 2000075C スタック: 20002760 メールボックス:2000A760 ドライバ登録状態 R0: 00000000 R1: 00000000 R2: 00000000 R3: 00000000 R4: 2000A760 R5: 00000000 R6: 00000000 R7: 00000000 R8: 00000000 R9: 00000000 R10: 00000000 R11: 00000000 R12: 00000000 SP: 20002740 LR:FFFFFFF9(メインThreadからの例外) PC: E7FEE7FE xPSR: 40000003 MSP: 20002740 PSP: 20002760 CFBP: 00000001 (CONTROL=0x0、FAULTMASK=0x0、BASEPRI=0x0、PRIMASK=0x1) MSP でのスタック例外情報 2000275C: xPSR: 41000000 20002758: VECTPC: 200000A2 20002754: LR: 2000009D 20002750: R12: 00000000 2000274C: R3: 00000000 20002748: R2: 00000000 20002744: R1: 00000000 20002740: R0: 00000000 例外レジスタ E000ED04: ICSR: 00400803 (ISRPENDING、VECTPEND=0(なし)、RETTOBASE、VECTACTIVE=3(ハードフォルト)) E000ED08: VTOR: 00000000 TBLBASE=0(INCODE)、TBLOFF=0x0 E000ED28: MMFSR: 01 (IACCVIOL) E000ED29: BFSR: 00 E000ED2A: UFSR: 0001 (未定義STR) E000ED2C: HFSR: 40000000 (強制) E000ED30: DFSR: 00000001 (停止) E000ED3C: AFSR: 00000000 E000ED24: SHCSR: 00000000 E000ED34: MMAR: 00000000 E000ED38: BFAR: 00000000 E000EDFC: DEMCR: 01000000 (TRCENA) VECTPC命令数約41000000 40FFFFFC:(読めません - Nn(05)。DAPアクセスにおけるワイヤーACK故障) 40FFFFFE:(読めない) Flash Driver V.2の起動失敗 - rc Ef(34):フラッシュ初期化タイムアウト。 チップの初期化に失敗しました - Ef(34): フラッシュの初期化がタイムアウトしました。 フラッシュドライバーの初期化に失敗MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfx この問題を解決するのを手伝ってください。 私はMCUXpresso 24.12ビルド148とSDKs 24.12.00を使っていて、最近MCU-Linkをバージョン3.153にアップデートしようとしました デモボードは以下のとおりです。 SCH-5077 REV C3 700-5077 REV C1(ペンで署名されている) シモーネ Re: rt1180 program on flash これは依然として非常に妥当な質問だと思います。製品はもはやプリプロダクション段階ではありませんが、問題は依然として残っています。外部フラッシュからM7コアコードを実行するようにデバイスをどのように設定すればよいでしょうか。 Re: rt1180 program on flash こんにちは。お元気ですか? RT1180は製品がまだプリプロダクション段階です。詳細については、NXPの担当者までお問い合わせください。 よろしくお願いします、 オマール Re: rt1180 program on flash 必要に応じてプロジェクト
View full article