[SPSDK][i.MX95] nxpele read-common-fuse fails Hi, I'm working on enabling secure boot on an IMX95 19x19 EVK board. I've successfully signed my images using the SPSDK. Now, before writing the fuses, i wanted to read them using `nxpele` but i'm getting the error below. ``` $ nxpele -f mimx9596 -d uboot_serial -p /dev/ttyUSB2 read-common-fuse --index 136 SPSDKParsingError: SPSDK: Message SIZE in response is invalid: 0x4 See debug log file: /home/user/.local/state/spsdk/3.11.0/log/debug.log for more info ``` and in the logs it says the following: ``` $ tail -60 /home/user/.local/state/spsdk/3.11.0/log/debug.log raise SPSDKParsingError(f"Message SIZE in response is invalid: {hex(size)}") spsdk.exceptions.SPSDKParsingError: SPSDK: Message SIZE in response is invalid: 0x4 DEBUG:spsdk:*************************************************** (206ms since start, spsdk_logger.py:212) DEBUG:spsdk:* SPSDK DEBUG LOGGING STARTED 2026-09-03 15:58:44 * (207ms since start, spsdk_logger.py:213) DEBUG:spsdk:* SPSDK version: 3.11.0 * (207ms since start, spsdk_logger.py:215) DEBUG:spsdk:* Python version: 3.14.4 * (207ms since start, spsdk_logger.py:216) DEBUG:spsdk:* OS version: Linux-6.12.95+deb13-amd64-x86_64-with-glibc2.43 * (208ms since start, spsdk_logger.py:217) DEBUG:spsdk:* Last command: ['/usr/bin/../lib/spsdk/bin/nxpele', '-f', 'mimx9596', '-d', 'uboot_serial', '-p', '/dev/ttyUSB2', 'read-common-fuse', '--index', '136'] * (208ms since start, spsdk_logger.py:218) DEBUG:spsdk:*************************************************** (208ms since start, spsdk_logger.py:219) TRACE:spsdk.uboot.uboot:Uboot WRITE -> invalid (210ms since start, __init__.py:50) DEBUG:spsdk.uboot.uboot:Uboot READ UNTIL <- => (210ms since start, uboot.py:271) DEBUG:spsdk.uboot.uboot:Checking if the serial console is open by sending invalid command: "invalid\r\nUnknown command 'invalid' - try 'help'\r\nu-boot=> " (224ms since start, uboot.py:209) DEBUG:spsdk.utils.database:Current database finger print hash: f0f0598d4e6ae6c755d693693f232e30537cfb3b (226ms since start, database.py:1967) DEBUG:spsdk.utils.database:Loaded database from cache: /tmp/spsdk-cache-1001/spsdk/3.11.0/db_data_25a661a55aac_3.11.0.cache (226ms since start, database.py:1976) DEBUG:spsdk.utils.misc:Loading text file from /usr/lib/spsdk/lib/python3.14/site-packages/spsdk/data/devices/mimx9596/database.yaml (226ms since start, misc.py:312) INFO:spsdk.ele.ele_comm:ELE communicator is using 196608 B size buffer at 92800000 address in mimx9596, Revision: latest target. DEBUG:spsdk.ele.ele_comm:ELE msg 0x92800000 0x30000 0602971788000000 (245ms since start, ele_comm.py:502) TRACE:spsdk.uboot.uboot:Uboot WRITE -> ele_message 0x92800000 0x30000 0602971788000000 (246ms since start, __init__.py:50) DEBUG:spsdk.uboot.uboot:Uboot READ UNTIL <- => (246ms since start, uboot.py:271) DEBUG:spsdk.ele.ele_comm:Raw ELE message output: ele_message 0x92800000 0x30000 0602971788000000 060497e1d60000000000000000000200u-boot=> (256ms since start, ele_comm.py:422) DEBUG:spsdk.ele.ele_comm:Stripped output: 060497e1d600000000000000 (256ms since start, ele_comm.py:460) DEBUG:spsdk.apps.utils.utils:SPSDK: Message SIZE in response is invalid: 0x4 (257ms since start, utils.py:182) Traceback (most recent call last): File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/utils/utils.py", line 172, in wrapper retval = function(*args, **kwargs) File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py", line 2189, in safe_main sys.exit(main()) # pylint: disable=no-value-for-parameter ~~~~^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py", line 1631, in __call__ return self.main(*args, **kwargs) ~~~~~~~~~^^^^^^^^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py", line 1552, in main rv = self.invoke(ctx) File "/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py", line 2032, in invoke return _process_result(sub_ctx.command.invoke(sub_ctx)) ~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py", line 1415, in invoke return ctx.invoke(self.callback, **ctx.params) ~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py", line 910, in invoke return callback(*args, **kwargs) File "/usr/lib/spsdk/lib/python3.14/site-packages/click/decorators.py", line 46, in new_func return f(get_current_context().obj, *args, **kwargs) File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py", line 575, in cmd_read_common_fuse ele_read_common_fuse(handler, index) ~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py", line 588, in ele_read_common_fuse ele_handler.send_message(read_common_fuse_msg) ~~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_comm.py", line 519, in send_message msg.decode_response(response) ~~~~~~~~~~~~~~~~~~~^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_message.py", line 1235, in decode_response super().decode_response(response) ~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^ File "/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_message.py", line 346, in decode_response raise SPSDKParsingError(f"Message SIZE in response is invalid: {hex(size)}") spsdk.exceptions.SPSDKParsingError: SPSDK: Message SIZE in response is invalid: 0x4 ``` Note: i'm using `SPSDK 3.11.0` I've created an issue also on SPSDK's github page https://github.com/nxp-mcuxpresso/spsdk/issues/116#issue-5346231614 Any help is very much appreciated. Thank you, BR, Re: [SPSDK][i.MX95] nxpele read-common-fuse fails Hi joanxie I'm using linux BSP version LF6.18.20_2.0.0 (yocto wrynose) And here is the output of nxpele get-info $ nxpele -f mimx9596 -d uboot_serial -p /dev/ttyUSB2 get-info
ELE get info ends successfully:
Command: 0xda
Version: 4
Length: 256
SoC ID: SocId:Unknown_0x9590 - 0x9590
SoC version: B000
Life Cycle: OEM_OPEN - 0x0010
SSSM state: 4
Attest API version: 0
UUID: bc193865d65e45f193b55cc234303a0f
SHA256 ROM PATCH: d5d2cdc98cb54b64bffb00687edcd994ebfdd762275a66a858d928ae2fcff494
SHA256 FW: 525f972dbb772acd9f461bfc148d29beb5dc2f2e9693ff1b9ace182a8ffd8131
Advanced information:
OEM SRKH: 0000000000000000000000000000000000000000000000000000000000000000
CSAL state: EdgeLock secure enclave random context initialization succeed - 0x02
TRNG state: TRNG entropy is valid and ready to be read - 0x03
OEM PQC SRKH: 00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000 Re: [SPSDK][i.MX95] nxpele read-common-fuse fails could you tell me what ele fw version do you use for this command? let me double check it Re: [SPSDK][i.MX95] nxpele read-common-fuse fails I reproduced this issue, and I checked internal data base, this is existed issue and will fixe on spsdk 3.12.0
記事全体を表示