Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Trimension SR250——原型制作前的许可和雷达数据问题 我正在计划基于 SR250UWBSHIELD、FRDM-RW612 和“SR250 UWBIoT for Zephyr”(github.com/nxp-uwb/sr250-uwbiot-zephyr)的研究原型。它是一种无需标签的超宽带雷达,用于探测建筑物材料后面的人员,可用于搜救。在接受软件许可协议(LA_OPT_Online Code Hosting v1.4)之前,我希望您能简要回答以下五个问题: 1. 雷达数据:在雷达模式下,SR250 是否以复数 I/Q(相位保持)的形式向主机提供 CIR?它能否同时从多个接收天线捕获 CIR,以便主机可以估计到达角? 2. 分享结果:第 3.8 节禁止向 NXP 以外的任何人分发“与使用许可软件相关的报告”。这是否涵盖我自己的测量结果和与测试实验室、外部审阅者、客户或科学出版物共享的日志?如果可以,恩智浦能否提供书面许可? 3. 自己的软件:我自己的主机端信号处理(在 PC 上运行,接收 CIR 数据,不包含 NXP 代码)是否被视为第 1.3 节和第 5 节中的“衍生作品”? 4. 产品路径:如果原型成功,v1.4 是否允许我在自己的 PCB 上进行带有 SR250 的设备的商业销售,包括为客户提供固件更新?或者是否需要另行签订协议? 5. 合规性:我可以在哪里找到 SR250UWBSHIELD 的完整欧盟符合性声明?它是否支持雷达模式? 非常感谢。 Re: Trimension SR250 — licensing and radar data questions before prototyping 你好, 我给你发了私信! 此致, 里卡多
View full article
Licensing question: LA_OPT Online Code Hosting v1.4 (SR250 UWBIoT) — sharing results, AI tools, own Hello,  On the advice of NXP support chat, I'm posting my licensing questions here for the licensing team.  I plan a research prototype with SR250UWBSHIELD + FRDM-RW612, using software from github.com/nxp-uwb/sr250-uwbiot-zephyr and github.com/nxp-appcodehub/an-sr250-uwb-plug-and-play-demo (SR250 FW 01.41.04). Both are under "LA_OPT_Online Code Hosting NXP_Software_License – v1.4 May 2025". I have not accepted the license yet and would like to clarify the following first:  1. Section 3.8: Does the restriction on distributing "reports associated with the use of the Licensed Software" cover my own measurement results, logs and test reports? I would share them with a test laboratory, external reviewers, customers or in a scientific publication.  2. AI tools (Sections 3.2 / 3.8): I develop with AI assistants (e.g. ChatGPT, Claude). May I (a) share my results and reports with such services, and (b) let an AI assistant read and work with the Licensed Software and NXP documentation (e.g. UM12508), on my own computer or via a cloud service?  3. Own software (Sections 1.3 / 5): Is my own PC-side signal-processing software, which only receives CIR data and contains no NXP code, a "Derivative Work"? Do Sections 5.1–5.2 apply to it?  4. Product (Section 2.1): Does v1.4 allow selling a device with the SR250 (NXP board, third-party SR250 module or bare SR250UK on my own PCB) and this firmware, including firmware update files for customers? Or is a separate agreement required?  5. Licensee: If I accept the license as an individual now, does it carry over to a company I may set up later?  A written answer, or a contact at the NXP licensing/legal team, would be much appreciated. Thank you!
View full article
imx95 CRA Hi NXP           我需要移植欧盟的CRA,请问官方哪个地方有移植的文档(可以发下链接吗) Linux Re: imx95 CRA Hi @yrj  CRA 不是可以直接移植的软件组件,而是产品需要满足的网络安全法规。 如果你是要在i.MX 平台上落地 CRA 要求,建议优先看以下资料: 1. NXP 官方 CRA 专题入口 页面的 Documentation 栏目列出了应用笔记、白皮书和培训资料,也介绍了安全启动、安全更新、密钥管理等安全能力与法规要求之间的对应关系。   2.i.MX 平台相关应用笔记 这份文档介绍如何利用 i.MX 93支持 OEM 实现 CRA 要求。 3. 产品整体合规实施白皮书 介绍安全产品设计及生命周期方面的合规要求,适合先建立产品级实施框架,而不只是关注 BSP 或某个安全功能。 4. 欧盟官方实施指南 法规发布方的实施入口,包含 Commission guidance、FAQ、制造商义务、符合性评估、漏洞报告义务等资料。判断产品需要满足哪些要求,应以这类欧盟官方资料为依据。 Best Regards, Zhiming Re: imx95 CRA HI @Zhiming_Liu           您说的对,我描述的太通俗了          我现在参考文档对uboot 、Image、imx95-xxx.dtb,进行了签名与验证。          我现在是疑问是rootfs是否也需要签名呢,暂时没有看到rootfs的签名资料,是不需要吗? Re: imx95 CRA HI @Zhiming_Liu        dm-verity只读的,有dm-crypt的文档吗 Re: imx95 CRA Hi @yrj  文件系统一般用dm-verity。你可以参考这个文档来使能文件系统的保护:https://www.nxp.com/docs/en/application-note/AN15078.pdf Best Regards, Zhiming Re: imx95 CRA Hi @yrj  请参考下面文档中的:10.5.5 DM-Crypt usage on i.MX Platforms without CAAM hardware IP https://www.nxp.com/docs/en/user-guide/UG10163.pdf Best Regards, Zhiming
View full article
MC33PF8100A0TS参考资料 你好,又MC33PF8100A0ts的设计参考资料吗?  1. 如何设计烧写口? 2.参考设计原理图有吗? 帮忙看看,谢谢。 Re: MC33PF8100A0TS参考资料 用我们的PF8100的GUI 烧录,然后下载usermanual上面有接口的连接示意图: PF8200/PF8100 Programming Board | NXP Semiconductors FRDM-KL25Z用的是这个控制板,这一套操作下来也不简单,还不如直接在socket上烧写。 Re: MC33PF8100A0TS参考资料 是的,初期样板调试是芯片焊在板子上。 Re: MC33PF8100A0TS参考资料 HI Bob 您是要在产品的板子上做烧写吗?
View full article
i.MX95: neutron_perf.sh shows false 100% NPU Load (perf_counters line is read byte by byte) Hello, On i.MX95, neutron_perf.sh (eiq-examples-npu-utils, UG10166 section 8.4.5.1) sometimes shows 100% NPU Load while the actual load is about 60%. Environment - Board: IMX95LPD5EVK-19 - BSP: LF_6.18.20_2.0.0 (neutron_perf.sh is the same in lf-6.18.37_2.1.0) - eIQ Neutron SDK 3.2.3 Steps to reproduce 1. Convert the MobileNet model in the BSP (mobilenet_v1_1.0_224_quant.tflite in the TensorFlow Lite examples folder) with neutron-compiler for imx95. 2. On the board, run benchmark_model with the converted model and the Neutron delegate in the background, and run neutron_perf.sh at the same time. 3. The actual load is about 60%, but 100% was shown 11 times in 60 seconds. Cause 1. The perf_counters file in debugfs is not seekable, so the bash "read" command reads it one byte at a time. The driver function perf_counters_read() rebuilds the line on every read call, so one line mixes values from different moments, and some values break. In our test, 52 of 300 reads with "read" were broken, and 0 of 300 with "cat". 2. When a 32-bit counter reaches its maximum value, the driver resets it to 0. The script takes the absolute value of the negative difference, which gives 100%. Proposed fix (tested: no 100% in the same test) 1. Read the whole line at once (for example with cat), and then split it into the variables. 2. When the NACT difference is negative, add 2 to the power of 32 instead of taking the absolute value. We can share the patch if needed. On the driver side, using seq_file for perf_counters would probably also prevent cause 1 (not verified). Note: even with the fix, the NPU Load drops for one interval each time NACT reaches its maximum value (about every 7 seconds at 60% load), because NACT stops there until the next read resets it. Questions 1. Is this a known issue? 2. Could the fix be included in a future BSP release? Thank you. Re: i.MX95: neutron_perf.sh shows false 100% NPU Load (perf_counters line is read byte by byte) Hello, This is a gentle follow-up, as there has been no reply for two weeks. To make the report easier to review, I have attached the proposed fix as a patch (neutron_perf_fix.patch.txt). It changes only two lines of neutron_perf.sh, as described in my first post: 1. Read the perf_counters line all at once with cat, and then split it into the variables. 2. When the NACT difference is negative, add 2 to the power of 32 instead of taking the absolute value. The patch is against npu_utils/neutron_perf.sh in the nxp-imx/eiq-example repository on GitHub (branch lf-6.18.20_2.0.0). This is the script described in UG10166 (i.MX Machine Learning User's Guide), section 8.4.5.1: https://www.nxp.com/docs/en/user-guide/UG10166.pdf Could someone from NXP check the two questions in my first post? 1. Is this a known issue? 2. Could this issue be fixed in a future BSP release? The attached patch is only a suggestion. A different fix, for example on the driver side, is also fine. Thank you.
View full article
s32k31XEVB-Q100評価ボード上でS32K311およびFS23用のSPIを設定 こんにちは、 私はs32k31XEVB-Q100評価ボード上のS32K311とFS23間の通信用にSPIを設定しようとしています。 そこで、LPSPI0のピンを設定しました。 データシートによると、まずCLKが起動し、次にCSがLOWになる必要がある。 S32DSでこの動作をどのように設定すればよいですか? しかし、SPIデータを見ると、まずCSがLOWになり、次にCLKがトグルし始めることがわかります。 Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board こんにちは、 @john_2 図中のSCLK信号の開始位置に関して、若干の誤解があるかもしれません。図には、CSがLOWになる前にSCLKがトグルを開始する必要があるとは示されていません。むしろ、CSがアサートされる前にSCLKがすでにアイドル状態のLOWレベルになっている必要があることを示している。 CS信号がLOWになると、最初のSCLKエッジは、指定されたPCS-SCK遅延時間の後に発生します。したがって、LPSPI0をSCLKアイドルLOW(CPOL = 0)に設定し、FS23のタイミング要件に従ってPCS-to-SCK遅延を設定する必要があります。 BR、VaneB Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board 情報ありがとうございます 😄 これらが必要だったんです。 しかし、通信はまだ正常に機能していません。 私はLpspiとSbc_fs23_Ipドライバを使っています。 M_DEV_PROG_IDを読み取りたい でも、部品の順番自体が間違っていると思うのですが? つまり、最初のバイトは00000010であるべきでしょうか? 私が設定した構成では Lpspiドライバー データシートを正しく理解していれば、SpiTransferStartはMSBであるべきですよね?しかし、ロジックアナライザでは、CRCは最初のバイトに、アドレスは最後のバイトに表示されます。 スピジェネラル および Sbc_fs23_Ip-GeneralConfig
View full article
FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hello, Could you please clarify the supported FS2643D H-generation production configuration for S32K376NHT1MJBST? 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? The public FS26 standard-configuration examples and the S32K376POC page have been reviewed. The latter describes an FS2633-based board; its configuration is not being assumed transferable to FS2643D. Please point to the exact applicable documents or the correct support route if these details are not public. Thank you. Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hi Jonas Please see comment below: 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. [gw]Below is the recommend please firstly evaluate this power tree is suitable or not for S32K376 https://www.nxp.com/products/FS26 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. [gw]Please see answer above. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? [gw] A0 means blank part, Below is the name rule of FS26,I didn't find the UD suffix. Please note that after you finish schematic design please send to us for double check. Thanks!
View full article
DSP56F807PY80E:在 1.6V 输入电压下,ADC 读数与预期的 2048 个计数不符 NXP社区的各位朋友,大家好! 我正在排查一块使用DSP56F807PY80E的电路板上的 ADC 偏移问题。在设备引脚上测得的电压如下: 引脚功能测量电压 102–109 ANA0–ANA7 输入 1.60伏 99 和 110 VREF 和 VREF2 3.20伏 88、100 和 111 VDDA 3.30伏 对于没有偏移校正的单端转换,我预计计数约为 2048 ,因为输入电压是参考电压的一半: ADC计数 = (1.60 / 3.20) × 4096 = 2048 然而,ADC读数与预期值有所不同。 请问有人能提供一些建议吗? 我应该检查哪些ADC配置和偏移寄存器? 这种差异是否与 ADC 结果寄存器的读取或移位方式有关? RESET或重新初始化ADC并验证其偏移的推荐步骤是什么? 任何指导或初始化代码示例都将不胜感激。 感谢您的支持。 Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input 你好@Hari0369 , 感谢您提供如此详细的信息。 对于理想的 12 位转换,您的计算是正确的。输入电压为 1.60 V,参考电压为 3.20 V,预期结果约为 2048 个计数。 我建议首先检查的是如何读取ADC结果。 在 DSP56F807 上,12 位 ADC 结果存储在 ADRSLT 位 14-3 中。如果没有应用偏移量,2048 个计数在原始 ADRSLT 寄存器中将显示为大约 0x4000。 所以,请先将原始结果右移 3 位,然后再与 2048 进行比较: ADC 值 = ADRSLTn > 3 根据您的测试条件,您应该看到大致如下: 原始 ADRSLT 值:0x4000 之后 > 3 : 0x0800 = 2048 我还建议检查以下ADC设置: - 检查 ADLST1/ADLST2,确保已选择正确的模拟输入。 - 检查 ADCR1.CHNCFG 并确保已选择单端操作。 - 检查 ADSDIS 并确保您使用的采样槽已启用。 - 检查相应的 ADOFS 寄存器。本次测试请将偏移量设置为 0x0000。 - 检查 ADCR2,确保 ADC 时钟和采样配置正确。 - 确保您读取的 ADRSLT 寄存器与您配置的采样槽相匹配。   为了获得清晰的测试结果,我建议只使用一个ADC通道。 首先,停止 ADC,并等待 ADSTAT.CIP 指示 ADC 处于空闲状态。然后禁用未使用的采样槽,并配置一个已知的通道。将相应的 ADOFS 寄存器设置为 0x0000,并仅启用要测试的采样槽。 之后,开始一次转换并保存原始 ADRSLT 值。然后将此值右移 3 位,并将结果与预期的 ADC 计数进行比较。   如果结果仍然与预期不符,请您提供以下数值? - ADCR1 - ADCR2 - ADLST1/ADLST2 - ADSDIS - 相应的 ADOFS 值 - 原始 ADRSLT 值 这些值应该有助于我们确定差异是来自结果格式、ADC 配置、偏移设置还是模拟输入路径。 希望对您有所帮助。 BR 塞莱斯特 Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input 你好@Celeste_Liu , 感谢您分享详细信息和故障排除建议。 我使用相同的固件对大约 500 个 DSP 控制器进行了编程。大多数设备运行正常,但约有 10 台设备的 ADC 读数与相同测试条件下的预期计数不同。 据我了解,数据手册规定ADC偏移电压范围为-90 mV至+10 mV,典型值为-25 mV。请问 RESET 或重新初始化 DSP 或 ADC 是否可以使读数更接近在 1.60 V 输入和 3.20 V 参考电压下预期的 2048 个计数?如果可以的话,能否请您分享一下推荐的步骤? 感谢您的支持。 Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input 你好@Hari0369 , 感谢您提供的补充信息。 重新初始化 ADC 可以帮助排除 ADC 配置或状态问题,但通常不会改变设备固有的 ADC 偏移。 数据手册规定 ADC 偏移电压范围为 -90 mV 至 +10 mV,典型值为 -25 mV。当 VREF = 3.20 V 时,1 LSB 约为 0.781 mV,因此与理想的 2048 个计数可能会有一些差异。 对于受影响的单元,我建议进行以下检查: 停止 ADC,并等待 ADSTAT.CIP 指示 ADC 处于空闲状态。 使用与正常单元相同的配置重新初始化ADC。 确保相应的 ADOFS 寄存器设置为 0x0000。 执行多次转换,并比较重新初始化前后的平均结果。 完成一次断电重启后,重复测试。 如果同一组设备始终显示相同的偏移,请将一台正常设备和一台受影响设备在 1.60 V 输入和 3.20 V 参考电压下的实际 ADC 计数发送给我们。然后我们可以将该差异与ADC规格进行比较。 BR 塞莱斯特
View full article
DSP56F807PY80E: 1.6V入力時のADC読み取り値が期待される2048カウントと異なる こんにちは、NXPコミュニティの皆さん、 DSP56F807PY80E を搭載したボードで、ADC オフセットの問題をトラブルシューティングしています 。デバイスのピンで測定された電圧は以下のとおりです。 ピンの機能 測定電圧 102~109 ANA0~ANA7入力 1.60V 99と110 VREFとVREF2 3.20V 88、100、111 VDDA 3.30V オフセット補正のないシングルエンド変換の場合、 入力電圧が基準電圧の半分であるため、 約 2048カウントになると 予想されます。 ADCカウント = (1.60 / 3.20) × 4096 = 2048 しかし、ADCの測定値はこの予想値とは異なっている。 どなたかアドバイスをいただけませんか: どのADC設定レジスタとオフセットレジスタを確認すればよいですか? この違いは、ADCの結果レジスタの読み込みやシフトの仕方に関係しているのでしょうか? ADCをリセットまたは再初期化し、オフセットを確認するための推奨手順は何ですか? 何かご指導や初期化コードの例があれば幸いです。 再開まで今しばらくお待ちください。 Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input こんにちは、 @Hari0369 さん。 詳細な情報ありがとうございます。 理想的な12ビット変換の場合、あなたの計算は正しいです。入力電圧が1.60V、基準電圧が3.20Vの場合、予想される結果は約2048カウントです。 まず最初に確認すべきことは、ADCの結果がどのように読み取られるかということです。 DSP56F807では、12ビットADCの結果はADRSLTビット14~13に格納されます。オフセットを適用しない場合、2048カウントは生のADRSLTレジスタでは約0x4000として表示されます。 ですので、2048と比較する前に生の結果を右に3ビットシフトしてください: ADC値 = ADRSLTn > 3 テスト条件では、おおよそ以下の値が表示されるはずです。 生のADRSLT値:0x4000 3 の後 : 0x0800 = 2048 また、以下のADC設定も確認することをお勧めします。 - ADLST1/ADLST2を確認し、正しいアナログ入力が選択されているか確認してください。 - ADCR1.CHNCFG を確認し、シングルエンド動作が選択されていることを確認してください。 - ADSDISを確認し、使用しているサンプルスロットが有効になっていることを確認してください。 - 対応するADOFSレジスタを確認してください。このテストでは、オフセットを0x0000に設定してください。 - ADCR2を確認し、ADCクロックとサンプリング構成が正しいことを確認してください。 - 読み取ったADRSLTレジスタが、設定したサンプルスロットと一致していることを確認してください。   クリーンなテストには、ADCチャネルを1つだけ使うことをおすすめします。 まず、ADCを停止し、ADSTAT.CIPがADCがアイドル状態であることを示すまで待ちます。次に、使われていないサンプルスロットを無効にし、既知のチャネルを1つ設定します。対応するADOFSレジスタを0x0000に設定し、テストしたいサンプルスロットのみを有効にしてください。 その後、変換を1つ開始し、生のADRSLT値を保存します。次に、この値を3ビット右にシフトし、その結果を期待されるADCカウントと比較します。   それでも結果が予想と異なる場合は、以下の値を教えていただければ幸いです。 - ADCR1 - ADCR2 - ADLST1/ADLST2 - ADSDIS - 対応するADOFS値 - 生のADRSLT値 これらの値は、結果フォーマット、ADC構成、オフセット設定、またはアナログ入力経路による差を判断するのに役立ちます。 お役に立てば幸いです。 BR セレステ Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input こんにちは、 @Celeste_Liu さん。 詳細情報とトラブルシューティングのご提案をいただき、ありがとうございます。 同じファームウェアを使って約500台のDSPコントローラをプログラムしました。ほとんどのユニットは期待どおりに動作しますが、約10台のユニットでは、同じテスト条件下で予想されるカウントとは異なるADC値を示します。 データシートには、ADCオフセット電圧の範囲が-90mV~+10mVで、標準値が-25mVであると記載されていることを理解しています。DSPやADCをリセットまたは再初期化することで、1.60V入力と3.20Vの基準で予想される2048カウントに近づけるかどうか、教えていただけますか?もしそうなら、推奨される手順を教えていただけますか? 再開まで今しばらくお待ちください。 Re: DSP56F807PY80E: ADC reading differs from expected 2048 counts at 1.6 V input こんにちは、 @Hari0369 さん。 追加情報ありがとうございます。 ADCを再初期化することでADCの設定や状態の問題を除外するのに役立ちますが、通常はデバイスのADCオフセット自体は変わりません。 データシートでは、ADCオフセット電圧は-90mV~+10mVの範囲で、標準値は-25mVと規定されている。VREF = 3.20 Vの場合、1 LSBは約0.781 mVであり、理想的な2048カウントとは多少の違いが期待されます。 影響を受ける機器については、以下の点を確認することをお勧めします。 ADCを停止し、ADSTAT.CIPがADCがアイドル状態であることを示すまで待ちます。 通常ユニットで使用されている設定と同じ設定でADCを再初期化してください。 対応するADOFSレジスタが0x0000に設定されていることを確認してください。 複数の変換を実行し、再初期化前と再初期化後の平均結果を比較する。 電源を完全に投入してから再度テストを行ってください。 同じユニットで常に同じオフセット値が表示される場合は、入力電圧1.60V、基準電圧3.20Vにおける、正常なユニットと影響を受けているユニットそれぞれの実際のADCカウント値を弊社までお送りください。その差をADC仕様と比較できます。 BR セレステ
View full article
IMX93 功率 您好, 我正在研究imx93处理器,在frdm-imx93评估套件中,vdd_soc_0v8的电流被设定为1.5A,但根据数据手册,最大电流额定值为2.7A,且没有提及电流范围。那么,1.5A的电流值是基于什么计算得出的呢?此外,为了进行功耗计算,我需要知道右侧信号(PFA)的电流值……请帮我解答一下。 请问您能否确认 imx9352 和 imx9351 的电源树是否相同? FRDM 培训 Re: IMX93 Power imx9352 和 imx9351 的电源树应该不同,因为 9352 有两个 A55 核心,而 9351 只有一个 A55 核心。 根据官方网站,EVK 板有两种类型:i.Mx93evk 和 FRDMi.Mx93 evk。这两个板都共享 i.mx9352 的某些部件号,并且在测试模式下出现的最快电流模式如下:1256.9mA。有关功率测量的详细信息,请参阅 AN13917 i.MX 93 功耗测量 6.8.2 2 x CA55 Stream + PXP + CM33 CoreMark + NPU 当用例运行时,系统状态如下: 1.CPU频率设置为最大值1.7GHz。 2. DDR 数据速率设置为 3733 MT/s。 3. LCDIF 和 PXP 用于 GUI 渲染和显示。 4. CA55 用于流。 5.CM33用于CoreMark和NPU测试。 Re: IMX93 Power 嗨@Navya , Q1&A:这是 FRDM 板设计中这些引脚上可能消耗的最大电流。 i.MX93 的 VDD_SOC 最大电流为 2700 mA。因此,FRDM 是低功耗设计。如果您有相同的需求,可以参考它。 如果没有,您可以参考 i.MX93 EVK 设计。 对于右侧的功率,您可以进行计算,它就是您所指的近似值: Q2&A:两者都采用相同的 i.MX93 系列电源架构。 希望这对您有所帮助。 祝你今天过得愉快 顺祝商祺! Rita
View full article
MC33PF8100A0TS Reference Material Hello, do you have any design reference materials for the MC33PF8100A0ts? 1. How to design the programming port? 2. Do you have a reference design schematic? Could you please take a look? Thank you. Re: MC33PF8100A0TS参考资料 Flash the software using our PF8100 GUI, then download the user manual which contains a connection diagram of the interfaces: PF8200/PF8100 Programming Board | NXP Semiconductors The FRDM-KL25Z uses this control board, and the whole process is not simple. It's better to just burn the code directly onto the socket. Re: MC33PF8100A0TS参考资料 Yes, in the initial prototype debugging, the chip is soldered onto the board. Re: MC33PF8100A0TS参考资料 HI Bob Are you planning to program the product's circuit board?
View full article
电池包主动均衡方案 你好,在网站上没有找到电池包主动均衡的方案,只有一段电池储能解决方案的演示视频,论坛里也没搜到相关的文章。我想找找这方面的文章,有推荐吗?谢谢。 Re: 电池包主动均衡方案 这个太老了,主动均衡应该是后续新能源的趋势吧。 Re: 电池包主动均衡方案 Hi Bob 我们不做主动均衡的IC,这方面的资料不多,附件这个希望能对您有所帮助是很老的app note了
View full article
Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board Hello, I am trying to configure the SPI for the communication between a S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board. Therefore I configured the pins on LPSPI0. According to the Datasheet first the CLK has to start and then the CS has to go LOW. How can I configure this behavior in S32DS? But When I see the SPI Data I see that first the CS goes to LOW and then the CLK starts toggling Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board Hi @john_2  There may be a small misunderstanding regarding the beginning of the SCLK signal in the diagram. The diagram does not indicate that SCLK needs to start toggling before CS goes LOW. Instead, it shows that SCLK must already be at its idle LOW level before CS is asserted. Once CS goes LOW, the first SCLK edge occurs after the specified PCS-to-SCK delay. Therefore, you should configure LPSPI0 with SCLK idle LOW (CPOL = 0) and configure the PCS-to-SCK delay according to the FS23 timing requirement. BR, VaneB Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board Thanks for the Information 😄 I needed these. But the Communication is still not working correctly. I am using the Lpspi and Sbc_fs23_Ip driver. I want to read the M_DEV_PROG_ID But I think the bits itself are in the wrong order? I.e. the first Byte should be 00000010 ? In the configuration I have  LpspiDriver If I understood the Datasheed correct, the SpiTransferStart should be MSB? But then the CRC is shown in the first Byte and the Address in the last Byte (in the LogicAnalyzer) SpiGeneral and Sbc_fs23_Ip- GeneralConfig
View full article
在 s32k31XEVB-Q100 评估板上配置 S32K311 和 FS23 的 SPI 你好, 我正在尝试配置 s32k31XEVB-Q100 评估板上的 S32K311 和 FS23 之间的 SPI 通信。 因此,我配置了 LPSPI0 上的引脚。 根据数据手册,首先 CLK 必须启动,然后 CS 必须变为低电平。 如何在S32DS中配置此行为? 但是当我查看SPI数据时,我发现首先CS变为低电平,然后CLK开始切换。 Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board 嗨@john_2 图中 SCLK 信号的起始位置可能存在一些误解。图表并未表明 SCLK 需要在 CS 变为低电平之前开始切换。相反,这表明在 CS 被钳位之前,SCLK 必须已经处于空闲的低电平。 CS 变为低电平后,第一个 SCLK 边沿会在指定的 PCS 到 SCK 延迟后出现。因此,您应该将 LPSPI0 配置为 SCLK 空闲低电平 (CPOL = 0),并根据 FS23 时序要求配置 PCS 到 SCK 的延迟。 BR,VaneB Re: Configure SPI for S32K311 and FS23 on a s32k31XEVB-Q100 Evaluation Board 谢谢你提供的信息 😄 我需要这些。 但是通讯仍然无法正常工作。 我正在使用Lpspi和Sbc_fs23_Ip驱动程序。 我想读取 M_DEV_PROG_ID 但我认为这些部件的顺序错了? 也就是说,第一个字节应该是 00000010 吗? 在我的配置中 Lpspi驱动程序 如果我理解数据表没错,SpiTransferStart 应该是 MSB 吗?但是,在逻辑分析仪中,CRC校验值显示在第一个字节,地址显示在最后一个字节。 SpiGeneral 和 Sbc_fs23_Ip-通用配置
View full article
バッテリーパックのアクティブバランシングソリューション こんにちは。ウェブサイトでアクティブバッテリーパックバランシングの解決策を探したのですが、バッテリーエネルギー貯蔵ソリューションのデモビデオしか見つかりませんでした。フォーラムでも関連する記事が見つかりませんでした。何かおすすめはありますか? よろしくお願いします。 Re: 电池包主动均衡方案 それは時代遅れだ。新しいエネルギー源においては、アクティブバランシングが将来のトレンドとなるべきだ。 Re: 电池包主动均衡方案 こんにちは、ボブ。 弊社ではアクティブバランシングICを製造しておらず、この件に関する情報もあまりありません。添付ファイルは古いアプリケーションノートですが、お役に立てれば幸いです。
View full article
From MC33816 to PT2001 design tips(CN) The C33PT2000AF and MC33816 wafers are manufactured at NXP's Chandler fab in the US, and production will cease due to the fab's impending closure. Currently, the official website states the last buy date as August 6, 2027, and the last delivery date as August 6, 2028 (specific dates are subject to change). The MC33PT2001 wafers are currently sourced from NXP's Austin fab in the US and are not affected by this discontinuation. Therefore, it is recommended that relevant customers replace their existing MC33PT2000AF and MC33816 wafers with MC33PT2001 wafers. Migrating a system from MC33816 to MC33PT2001 is not complicated. The hardware is basically pin-to-pin compatible, with only the voltage of pin 20 changing from 2.5V to 1.5V. This basically does not require any changes to the external circuitry. The internal registers are mostly compatible, only the Threshold register bit field has changed. MC33816: 0x18A Vds_threshold_hs Because each threshold in PT2001 becomes 4 bits, it is split into: 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS An additional 0x1B4 batt_result register was added to store the ADC conversion result of the VBATT pin. In summary, migrating from MC33816 to MC33PT2001 is quite convenient. Small Engine Driver
View full article
From MC33816 to PT2001 design tips(CN) C33PT2000AF和MC33816由于晶圆产自NXP美国Chandler工厂, 由于Chandler 工厂即将关闭,所以将停产。目前官网信息,last time buy date 为2027年8月6日,last time delivery date为2028年8月6日(具体日期以官网为准)。MC33PT2001晶圆目前来自NXP美国Austin工厂,不涉及本次停产,所以建议相关客户用MC33PT2001替代原有使用的MC33PT2000AF和MC33816的项目。 系统如果是从MC33816迁移到MC33PT2001并不复杂,硬件上基本Pin to Pin兼容, 仅是pin 20电压由2.5V变为1.5V,基本可以不涉及外围电路改变。 内部寄存器也是大部分是兼容的,仅是Threshold register bit field改变了 MC33816: 0x18A Vds_threshold_hs PT2001因为每个 threshold 变成4 bit,所以拆成: 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS 另外增加了一个0x1B4  batt_result寄存器用于放VBATT pin的ADC转换结果。 总之,如果是从MC33816迁移至MC33PT2001还是非常方便的。 Small Engine Driver
View full article
MC33816からPT2001への設計ヒント(中国語) C33PT2000AFおよびMC33816ウェハは、NXPの米国チャンドラー工場で製造されていますが、同工場の閉鎖に伴い生産が中止されます。現在、公式ウェブサイトでは最終購入日が2027年8月6日、最終納品日が2028年8月6日と記載されています(具体的な日付は変更される可能性があります)。MC33PT2001ウェハは現在、NXPの米国オースティン工場から供給されており、今回の生産中止の影響を受けません。したがって、該当するお客様は、既存のMC33PT2000AFおよびMC33816ウェハをMC33PT2001ウェハに交換することをお勧めします。 MC33816からMC33PT2001へのシステム移行は複雑ではありません。ハードウェアは基本的にピン互換性があり、20番ピンの電圧が2.5Vから1.5Vに変更されるだけです。そのため、外部回路の変更は基本的に必要ありません。 内部レジスタはほとんど互換性がありますが、しきい値レジスタのビットフィールドのみが変更されています。 MC33816: 0x18A Vds_threshold_hs PT2001では各しきい値が4ビットになるため、以下のように分割されます。 1AEh: HS1–HS4 VDS 1AFh: HS5 VDS 1B0h: HS1–HS4 VSRC 1B1h: HS5 VSRC 1B2h: LS1–LS4 VDS 1B3h: LS5–LS6 VDS VBATTピンのADC変換結果を格納するために、追加の0x1B4 batt_resultレジスタが追加されました。 要約すると、MC33816からMC33PT2001への移行は非常に簡単です。 小型エンジンドライバー
View full article
KW43 Knowledge Hub The KW43 product family is a low-power, secure, single-chip wireless MCU that integrates a high performance, Bluetooth Low Energy, Bluetooth Channel Sounding, EdgeLock Secure Accelerators, and various MCU peripherals targeted for Automotive applications. The KW43 family utilizes an Arm® Cortex®-M33 core (Armv8-M architecture) running up to 96 MHz for customer applications. The family includes memory configurations of up to 1.5MB flash and 256 KB SRAM across all listed part numbers. All devices in the family integrate a state-of-the-art, scalable security architecture including Arm’s TrustZone®-M, a resource domain controller and an isolated EdgeLock Secure Accelerators supporting hardware cryptographic accelerators, random number generators and key generation, storage, and management along with secure debug. All members of the KW43 family are designed to be compliant to a SESIP Level 3 certification following the Arm PSA Level 3 profile. KW43 uses dual Arm Core Cortex-M33 (‘CM33’) and supports multiple interfaces and security features. One is for application and system use and other is for radio link layer and both cores share a common flash of 1.5 MB. The devices include a full certified Bluetooth LE 6.x controller stack with support for up to 10 simultaneous connections in any controller/peripheral combination. The multiprotocol radio subsystem integrated in the KW43 Family is energy efficient and is designed for Wi-Fi coexistence. The radio is supported with tested software stacks for Bluetooth Low Energy for standalone and hosted applications to enable a range of Automotive, IoT and industrial applications. There is also software and hardware support for 2.4 GHz proprietary protocols. To address ranging requirements, the Localization Engine (LCE) is integrated into the system for enhanced localization performance. The KW43 series is supported by the MCUXpresso Developer Experience to optimize, ease and help accelerate embedded system development. Early access program The KW43 is in pre-production, developers can get started today with the KW45/KW47, which is pin and software compatible.   you can request access contacting NXP sales team - Pascal Bernard ([email protected]) Join KW47 early access program here: KW43 Early Access Training Bluetooth Low energy 6.0 NXP Introduction Interested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology.                2024: Channel Sounding              2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth AI Assistant - Amber Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview Bluetooth_7.0_Feature_Overview - (HDT not supported in KW43) Bluetooth Core Specification Core Specification 4.0 Core Specification 4.1 Bluetooth 4.1 FAQ Core Specification 4.2 Bluetooth 4.2 FAQ Core Specification 5.0 Core Specification 5.1 Core Specification 5.2 Core Specification 5.3 Core Specification 5.4 Core Specification 6.0 Core Specification 6.1 Core Specification 6.2 Core Specification 6.3 Core Specification 7.0 - (HDT not supported in KW43, TAK supported) RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Useful Links How to import and run demo examples with MCUXpresso for Visual Studio Code: This article gives information on how to import and run demo examples from the new SDK with ARM GCC toolchain, in MCUXpresso for Visual Studio Code. [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide: This article describes a simple process for enabling the user controls the radio through serial commands. KW43
View full article
KW45ナレッジハブ KW45の3コア・アーキテクチャには、96 MHzのCM33アプリケーション・コア、専用のCM3無線コア、分離型のEdgeLockセキュア・エンクレーブが統合されています。専用のSRAMを備えたフラッシュ・ベースの無線コアにより、高度な設定とアップグレードが可能なソフトウェア実装の無線が得られ、メイン・コア上のリソースをお客様のアプリケーション領域に活用できます。 Bluetooth Low Energy 5.3準拠の無線は、最大24のセキュアな同時接続に対応しています。EdgeLockセキュア・エンクレーブの分離された実行環境は、一連の暗号化アクセラレータ、キー・ストア処理、セキュアなライフサイクル管理を備え、メイン・コアのセキュリティ負荷を最小限に抑えます。 さらに、KW45 MCUにはFlexCANが搭載され、車載用または産業用CAN通信ネットワークへのシームレスな統合を実現できます。FlexCANモジュールは、CANのフレキシブル・データ・レート(CAN FD)に対応でき、帯域幅の拡大とレイテンシの低減に役立ちます。 KW45のブロック図 KW45アーキテクチャブロック図 書類 リファレンス・マニュアル Datasheet Errata Secure Referenceマニュアル** 認証 SESIP認定 SESIP ST PSA認証 RED 認証 欧州連合適合宣言書(EVK) 欧州連合適合宣言書(LOC) 日本MIC KW45-LOC _TELEC-20250221 添付ファイルをご覧ください Bluetooth仕様 Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview Bluetooth_5.2_機能_概要 Bluetooth_5.3_機能_概要 Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview 評価ボード KW45 KW45-EVK KW45-EVK回路図 KW45-EVK 設計ファイル KW45-EVKユーザー・マニュアル KW45-LOCユーザーマニュアル KW45-EVKスタート・ガイド アプリケーション・ノート ソフトウェア、ハードウェア、ペリフェラル: AN14122:KW45でのRTCの使用方法 このアプリケーション・ノートでは、BLEデモでRTCペリフェラルを構成および使用する方法について説明します。 AN14141:KW45 Bluetooth Low Energy用接続スタックでウォッチドッグ・タイマ・モジュールを有効にする このアプリケーション・ノートでは、接続スタック・デモにWDOGタイマを実装するプロセスについて説明します。 AN13855:KW45/K32W1でOTAPクライアント・サービスをBluetooth LEペリフェラル機器に統合する このアプリケーション・ノートでは、Over the Air Programming(OTAP)クライアント・サービスをBLEペリフェラル機器に統合するステップとプロセスを説明します。 AN13584:Kinetis KW45およびK32W1ロードプル・レポート このアプリケーション・ノートでは、ロードプル特性での測定方法と関連する結果について説明します。 AN13860:OTAPツールを使用してKW45/K32W1にファームウェアの更新イメージを作成する このアプリケーション・ノートでは、OTAPを使ってKW45ボードでイメージを作成および更新するステップについて説明します。 AN14077:KW45(1MB)からKW45(512kB)に移行するステップ このアプリケーション・ノートでは、1MBフラッシュから512kBフラッシュへの移行に必要な初期ステップについて説明します。 電力管理: AN13230:Kinetis KW45およびK32W1 Bluetooth LEの電力消費分析 このアプリケーション・ノートでは、KW45ワイヤレスMCUの電力消費、ハードウェアの設計、低電力動作向けの最適化に関する情報を紹介します。 AN13831:KW45/K32W1電力管理ハードウェア このアプリケーション・ノートでは、KW45/K32W1 MCUで電力管理専用の各種モジュールの使用方法について説明します。 RF: AN13687:K32W1による802.15.4アプリケーションの接続テスト このアプリケーション・ノートでは、K32W1 802.15.4のRF性能を実行するために接続テスト・ツールを使用する方法について説明します。 AN13728:KW45 RFシステムでのBluetooth LEおよびIEEE 802.15.4アプリケーションの評価レポート このアプリケーション・ノートでは、BLE(2FSK変調)およびIEEE 802.15.4(OQPSK変調)でKW45ボードを使用する場合の無線周波数(RF)評価テストの結果を報告します。テストの実行時に使用可能なセットアップとツールについても説明します。 AN14098:KW45-LOC RFテスト・レポート このアプリケーション・ノートでは、KW45B41Zローカライゼーション・ボードの基本的なRFテストの結果を報告します。  AN13228:KW45-EVK RFシステムでのBLEアプリケーションに関する評価レポート このアプリケーション・ノートでは、2つの周波数シフト・キー変調を用いて、BLEアプリケーションでKW45B41Z-EVKを使用する場合のRF評価テストの結果を報告します。 AN13229:BLEアプリケーションで、KW45-EVKとRFシステムの共存に関する評価レポート このアプリケーション・ノートでは、KW45B41Z-EVKをBLEアプリケーション(2FSK変調)で使用する場合のRF評価テストの結果を報告します。 AN13512:Kinetisワイヤレス・ファミリ製品のBLEとWi-Fiアプリケーションとの共存 このアプリケーション・ノートでは、K32W1/4X低エネルギー製品のWi-Fi信号に対する耐性、およびWi-Fiとの共存状態の改善方法を取りあげます。  セキュリティ: AN13859:KW45/K32W1システム内プログラミング(ISP)ユーティリティ このアプリケーション・ノートでは、ISPモードでKW45/K32W1 MCUを起動するステップと、MCUと通信するために多様なシリアル接続を確立するステップについて説明します。 AN1403:量産時に、シリアル・ワイヤ・デバッグ(SWD)を介してアプリケーションと無線ファームウェア用にKW45フラッシュをプログラミングする このアプリケーション・ノートでは、量産時にSWDを介して必要なすべての設定を書き込み、焼き込み、プログラミングするステップについて説明します。  AN13883:SPSDKを使用してISP経由でKW45無線ファームウェアを更新する このアプリケーション・ノートでは、ISPモードでKW45/K32W1 MCUを起動するステップと、セキュア・バイナリで無線ファームウェアを更新するステップを説明します。 AN14109:SECツールを使用してKW45およびK32W148セキュアにブートするこのアプリケーション・ノートでは、SEC GUIツールで署名済みイメージとセキュア・バイナリを使用して、KW45/K32W1 MCUをセキュアにブートするステップを説明します。 AN13838:SPSDKコマンド・ライン・ツールを使用してKW45およびK32W148をセキュアにブートする このアプリケーション・ノートでは、SPSDKコマンド・ライン・ツールで署名済みイメージとセキュア・バイナリを使用して、KW45/K32W1 MCUをセキュアにブートするステップを説明します。 AN13931:KW45およびK32W148でのライフサイクルを管理する このアプリケーション・ノートでは、SEC GUIとSPSDKコマンド・ライン・ツールを使用してKW45/K32W1 MCUのライフサイクルを移行するステップを説明します。  AN14174:NPXを使用して、KW45/K32W148のフラッシュ暗号化を実行する このアプリケーション・ノートでは、KW45/K32W1 MCUでオンザフライ暗号化を有効にするステップを説明します。 AN14158:KW45/K32W148で認証をデバッグするこのアプリケーション・ノートでは、フィールドでアプリケーションをセキュアにデバッグするためにデバッグ認証を実行する方法を説明します。  AN14544:MPUおよびMCU向けのEdgeLock 2GOサービス このアプリケーション・ノートでは、NXPデバイス向けのEL2GOサービスを紹介します。このサービスにより信頼できない環境でも信頼できる形でデバイスをプロビジョニングできます。  サポート KW45に関して疑問点がある場合は、ワイヤレスMCUコミュニティ(こちら)に質問を投稿しましょう! 便利なリンク リファレンスデザイン - NXP Community [MCUXSDK]KW4x、MCXW7x、MCXW2xにGitHub SDKを使用する方法 - NXPコミュニティ GitHub SDKの使用方法をステップ別に紹介しています。 [MCUXSDK]GitHub SDK - Bluetooth LEプラットフォームのドキュメント - NXPコミュニティ BLEプラットフォーム用ドキュメントを提供しています。  KW45/KW47/MCXW71/MCXW72でのSignal Frequency Analyzer(SFA)モジュールを使用したクロック測定 - NXPコミュニティ:このコミュニティでは、Signal Frequency Analyzerの使用方法に関する手順を提示しています。 KW45(自動車)またはK32W1/MCXW71(IoT/産業)で初めてPCBを適切に構築する最良の方法... コミュニティ : KW45またはK32W148、およびMCXW7を使用してPCBを構築するためのリンクと、無線性能、低電力、無線認証(CE/FCC/ICC)に関するあらゆる要素を掲載しています。 HCI_bbをKinetisファミリ製品で使用してDTMモードにアクセスする方法:この記事は次の2つの部分に分かれています。 HCI_bbバイナリを Kinetis製品へフラッシュする方法。 R&S CMW270を使用してRF測定を行う BLE HCIアプリケーションによるトランスミッタ/レシーバテストコマンドの設定:この記事では、ユーザーはどのようにすればシリアルコマンドをデバイスに送信できるかを示す手順を説明します。 Bluetooth LE HCI Black Boxクイックスタートガイド:この記事では、ユーザーが無線をシリアルコマンドで制御できるようにするためのシンプルなプロセスを説明します。 Kinetis(K32/38/KW45およびK32W1/MCXW71)パワー・プロファイル・ツール:Kinetis(KW35/KW38/KW45)およびMCX W7x(MCX W71)パワー・プロファイル・ツールに的を絞ったページです。お使いのアプリケーション(自動車またはIoT)での電力消費量を試算したり、ソリューションのバッテリ寿命を評価したりするのに役立ちます。 KW45/K32W1 32MHzおよび32kHzの発振余裕度:この記事では、回路の発振余裕度の適切な構成について説明しています。 KW45ベースのCSの1対多デモ NXP - チャネル・サウンディング   トレーニング BLE Introduction  RFスイッチの比較 吸収型と反射型 規格の比較 ETSI/FCC/ARIB要件 BLEチャネルサウンディング - 概要 BLEチャネル・サウンディング - RFハードウェア BLEチャネル・サウンディング - ANSYSモデリング・ツール BLEチャネル・サウンディング - アンテナのプロトタイプの検証測定 機器 ワイヤレス機器:この記事には、プロジェクト策定に役立つ機器へのリンクが掲載されています。 開発ツール  SDKビルダ: MCUXpresso SDKは、オープンソースのドライバ、ミドルウェア、リファレンス例のアプリケーションを提供し、ソフトウェア開発を加速させます。 SDK GitHub:GitHubで公開されているSDKのオープンソースのドライバ、ミドルウェア、リファレンス例 NXP MCUXpresso:MCUXpresso IDEは高度な編集、コンパイル、デバッグ機能を提供し、MCU固有のデバッグ機能も追加されています。すべての汎用Arm Cortex-Mとの接続をサポートします。 NXP SPSDK:信頼性が高く使いやすいPython SDK統合ライブラリです。NXP MCUポートフォリオ全体で動作するので、お客様のクイックプロトタイピングから本番環境デプロイまで対応する強力な基盤となります。 NXP SECツール:GUIベースのアプリケーションMCUXpresso Secure Provisioning Toolは、NCP MCUデバイスのブータブル実行ファイルの生成とプロビジョニングをシンプル化するものです。 NXP OTAP Tool:ユーザーがNXP開発ボードのOver-the Air)ファームウェア・アップデートを実行するのに役立つアプリケーションです。 Config Tool: 構成ツールの統合スイート「MCUXpresso Config Tools」を利用すると、開発者はカスタムSDKをすばやく構築したり、ピン、クロック、ペリフェラルを利用して初期化Cコードを生成したり、カスタム・ボード・サポート用の値を登録したりできます。 ワイヤレスMCU用のSDKの例:ワイヤレスの例では、多くの一般的なBluetooth構成を取りあげています。 **セキュア・ファイルには追加のアクセス権をリクエストする必要があります。  ハンズオン・トレーニング 製品: K32W1 プロトコル:802.15.4 プロトコル:BLE→コネクティビティ プロトコル:Bluetooth プロトコル:Matter プロトコル:Thread プロトコル:Zigbee
View full article