I am implementing MBDT through the example file attached below.
I checked that the S32 Design Studio for ARM Version 2.2 program works normally for the same file.
However, I don't know if the S32 Design Studio for S32 Platform 3.4 program doesn't work as below.
S32 Design Studio for ARM Version 2.2 creates libm.a file and builds well.
However, libm.a file is not generated in program S32 Design Studio for S32 Platform 3.4
This issue was being helped in the link below, and I posted it to get more help.
已解决! 转到解答。
Hello Sangho Lee, @autics
Yes, there is a migration Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2 - NXP Co...
But I have a simpler method, that worked on my setup, and you need to follow the steps:
Open Matlab r2021a and the GPIO model gpio_s32k144.mdl, then press Ctrl+B to build and flash on the board:
Open the S32 Design Studio IDE for Arm® 2.2 and import the ProjectInfo.xml:
Hope you can follow the steps above and it works on your side,
Stefan V.
Hello Sangho Lee,
The S32K1xx Family is supported by the S32 Design Studio IDE for Arm® based MCUs and it has the Integrated NXP Software:
With this IDE you can get the best results for S32K1 Family of Microcontrollers.
The latest Model-Based Design Toolbox for S32K1xx version 4.3.0 has been designed and tested using S32 Design Studio IDE for Arm® and it is using the S32K SDK.
Download and install the S32 Design Studio v3.4 S32K1 Service Pack 1 released! - NXP Community
| S32 Design Studio 3.4 S32K1xx Service Pack 1 for offline use | 2.6 GB | SW32K1_S32DS_3.4.1_D2106.zip |
To add S32K1 support, open the S32DS Extension and Updates and check if the S32K1XXX packages are installed:
Then open Matlab r2021a and the GPIO model gpio_s32k144.mdl, then press Ctrl+B to build and flash on the board:
After this open the S32 Design Studio for S32 Platform and Import Info XML as S32DS Project:
Then select the ProjectInfo.xml file from C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K1xx\S32_Examples\s32k14x\gpio\gpio_s32k144_mbd_rtw:
Then open project settings in S32DS for S32 Platform and go to C/C++ Build -> Settings -> Tool Settings -> Standard S32DS C Linker -> Libraries:
And add ":" on each entry, this will be modified to ":S32K14x_AMMCLIB.a" and ":libm.a".
To migrate the project please follow the steps in Solved: Migrate prj from S32DS for ARM version2018.R1 TO S32 platform 3.4 - NXP Community
Hope this helps,
Stefan V.
Hello Sangho Lee, @autics
Yes, there is a migration Video: Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2 - NXP Co...
But I have a simpler method, that worked on my setup, and you need to follow the steps:
Open Matlab r2021a and the GPIO model gpio_s32k144.mdl, then press Ctrl+B to build and flash on the board:
Open the S32 Design Studio IDE for Arm® 2.2 and import the ProjectInfo.xml:
Hope you can follow the steps above and it works on your side,
Stefan V.