Cannot launch debug session for MPC5748G from S32 Design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot launch debug session for MPC5748G from S32 Design studio

3,590件の閲覧回数
Vkatrenikona
Contributor I

Greetings,

I am new to NXP platform and trying to flash  LED blink example on MPC5748G-DEVKIT. I followed following steps. I see this error.

Error in services launch sequence
PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.

Debugging settings look like:

Vkatrenikona_0-1611163178639.png

Kindly help me to resolve this issue. Also if anyone can provide any debugging steps to make sure the board I purchased is in good shape would be a great help.

Thanks and regards,

Himateja Katrenikona

0 件の賞賛
返信
6 返答(返信)

3,574件の閲覧回数
Vkatrenikona
Contributor I

@lukaszadrapa  Thank you for sharing this with me. I will try to update the firmware on my board. How to make sure that the OpenSDA has updated firmware v1.10 after these steps?

Thanks and regards,

Himateja Katrenikona

0 件の賞賛
返信

3,556件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at this thread:

https://community.nxp.com/t5/S32-Design-Studio/Unable-to-start-debug-session-on-MPC5748G-board-downl...

There's a post from Jiri Kral (02-07-2019 05:09 AM) where it is described how to get firmware version.

Regards,

Lukas

 

0 件の賞賛
返信

3,579件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Himateja,

I would try to update the OpenSDA firmware. The procedure is described here:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/t...

Latest version is 1.10.

Please let me know if it doesn't help.

Regards,

Lukas

 

 

0 件の賞賛
返信

3,536件の閲覧回数
Vkatrenikona
Contributor I

Hi Lukas,

Updating hardware did not help me to resolve the issue. Apologies for delay in my update.

Thanks and regards,

Himateja Katrenikona

0 件の賞賛
返信

3,510件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Himateja,

I got recommendation from Jiri to try erase from PROGPPCNEXUS tool. You can take a look at this:

https://community.nxp.com/t5/S32-Design-Studio/MPC5777C-update-DCF-record/m-p/791557

See post marked as solution. It shows where to download the tool, how to connect. Then select the right PCP file for normal flash (not UTEST) and try to erase the flash. (do not follow the programming of UTEST, that's something different).

Regards,

Lukas

 

0 件の賞賛
返信

3,522件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @jirikral ,

could you please help with this? Any idea?

Thanks,

Lukas

 

0 件の賞賛
返信