MPC5xxx ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5xxx Knowledge Base

ラベル

ディスカッション

ソート順:
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop, initializes and display notice via UART terminal and then terminal ECHO. * * ------------------------------------------------------------------------------ * Test HW:        XPC563MKIT * MCU:            PPC5633MMLQ80 * Fsys:           80/60/40/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
記事全体を表示
This example contains On-line BIST configuration for MPC5746R in GreenHills compiler. For more details refer to application note AN5427 * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     b21190(Vlna Peter)  Initial Version 1.1    Nov-11-2015    b21190(Vlna Peter)  Added PPL0 200MHz as system clock 1.2    Dec-02-2015    b21190(Vlna Peter)  Added Flash controller init 1.3     May-24-2016    nxa13250(Vlna Peter)Added Online BIST *******************************************************************************/* ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     b21190(Vlna Peter)  Initial Version 1.1    Nov-11-2015    b21190(Vlna Peter)  Added PPL0 200MHz as system clock 1.2    Dec-02-2015    b21190(Vlna Peter)  Added Flash controller init 1.3     May-24-2016    nxa13250(Vlna Peter)Added Online BIST *******************************************************************************/
記事全体を表示
******************************************************************************** * Detailed Description: * This example content a basic PMPLL initialization and *  configuration of Mode Entry module and Clock Generation *  module for core1 and start of core0 and core0s from Core_Init function. * Also containts Lauterbach multicore multi-Trace32 view script for multicore * debugging puproses ******************************************************************************** * Test HW:  Test HW:  MPC57xx Motherboard + MPC5777M_512DS minimodule, MPC5777M, * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Jun-09-2015     b21190(Vlna Peter)  Initial Version 1.1     Sep-20-2016     b21190(Vlna Peter)  core0+core0s boot function added *******************************************************************************
記事全体を表示
Detailed Description:                      This config tool simplifies DCF records calculation for MPC5777M device.                 Look at HowToUse sheet for simple guideline, then work with DCF sheet                 Notes: - Macros have to be enabled!         BR, Petr
記事全体を表示
******************************************************************************** * Detailed Description: * DRUN with PLL 160MHz active. * Example of INTC configuration. PIT timer is triggering an * interrupt which is served in PIT ISR. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N06M * Target :  Internal Flash * Fsys:     160 MHz PLL * ******************************************************************************** Revision History: 1.0     Oct-29-2014     b21190(Vlna Peter)  Initial Version 1.1    Nov-20-2014    b21190(Vlna Peter)  Modified for Cut2.0 1.2    Apr-23-2015    b21190(Vlna Peter)  Added INTC driver and PIT ISR 1.3    May-14-2015    b21190(Vlna Peter)  Dissabling SWT in Startup code 1.4     Jun-06-2017    b21190(Vlna Peter)  ported for MPC5746C *******************************************************************************/
記事全体を表示
******************************************************************************** * Detailed Description: * * This example shows how to use SPI module in extended SPI mode * - DSPI3 is configured as a master * - SPI1 is configured as a slave * - Frame size is configured to 32bit * - Two writes are necessary to load one 32bit frame to TX FIFO * - For more details about the timing settings see application note AN4830 * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH ********************************************************************************
記事全体を表示
Detailed Description:                      This config tool simplifies DCF records calculation for S32R274 device.                 Look at HowToUse sheet for simple guideline, then work with DCF sheet                 Notes: - Macros have to be enabled!         BR, Petr
記事全体を表示
******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and cyclically converts PMC * internal channel as specified by macros CHOOSEN_PMC_ADC_CHNL, * CHOOSEN_PMC_ADC_SCALE and CHOOSEN_PMC_ADC_COMMAND to check particular voltage * level, displaying it into terminal window. * No external connection required excluding terminal via eSCI. * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU:             PPC5676RDMVY1 3N23A * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            180MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  default ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * This example content a driver for CGM module configuration. * ------------------------------------------------------------------------------ * Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P, * silicon mask set 1N65H * Target :  internal_FLASH* ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * * Simple LINFlex UART mode transmit and receive without interrupts (polled UART) * TXFIFO and RXFIFO macro is used to select between buffer and FIFO mode * * PIT channel 0 is also used to generate 1sec interrupt where PA0 pin is toggled. * * EVB connection: * *   Motherboard *   J14 - SCI_RX OFF *   J13 - SCI_TX OFF *   J25 - SCI_PWR ON * * See results on PC terminal (19200, 8N1, None). * ------------------------------------------------------------------------------ * Test HW:  MPC5777M, MPC57xx Motherboard + MPC5777M_512DS minimodule * Maskset:  0N78H * Target :  RAM, internal_FLASH * Fsys:     600 MHz PLL1 with 40 MHz crystal reference, *        core2 at 200MHz generated from PPL1 * Terminal: 19200, 8N1 ********************************************************************************
記事全体を表示
Detailed Description:                      This config tool simplifies DCF records calculation for MPC5744P device.                 Look at HowToUse sheet for simple guideline, then work with DCF sheet                 Notes: - Macros have to be enabled!         BR, Petr
記事全体を表示
******************************************************************************** Detailed Description:  Example shows MCU's temperature measurement with the help of TSENS.  Calibration constants for TSENS0 are read from Test Flash and  SARADC_B is set to measure Vbg and TSENS outputs.  Calculated internal temperature can be displayed on the Terminal.  EVB connection:    Motherboard    J14 - SCI_RX ON    J13 - SCI_TX ON    J25 - SCI_PWR ON    See results on PC terminal (19200, 8N1, None). You should see following text  (with different values for sure)  TSENS - temperature measurement  press any key to continue...  TSENS's calibration constants read from Test Flash  TSCA = 184  TSCB = 21    T = (232 + TSCA * 2^-6) * TSENS_code / VBG_code - (273 + TSCB * 2^-4) [degC]  ----------------------------------------------------------------------------  VBG_code   =  251  TSENS_code =  339  TSENS temp = 42.91 degC  ------------------------------------------------------------------------------  Test HW:  MPC5777M  Maskset:  0N50N  Target :  RAM, internal_FLASH  Fsys:     600 MHz PLL1 with 40 MHz crystal reference  Terminal: 19200baud, 8N1 ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Preparation, configuration and execution of ONLINE(SHUTDOWN) build-in self-test. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * ******************************************************************************** Revision History: 1.0     Apr-04-2016     b21190(Vlna Peter)  Initial Version 1.1    Apr-28-2017     b21190(Vlna Peter)  Added cut 1N65H (2.1) *******************************************************************************/
記事全体を表示
******************************************************************************** * Detailed Description: * * eMIOS0 ch0 is set to SAIC mode generating interrupt on falling edge. * The IGF ch16, connected to eMIOSch0, is set to filter low pulses <1.5us * Intergation filter type is used for falling edge with given threshold. * eMIOS interrupt is called if input signal low pulse is longer than 1.5us. * * ------------------------------------------------------------------------------ * Test HW: MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU: PPC5777CMM03 2N45H CTZZS1521A * Fsys: PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * use USB connector (J21) on minimodule * * EVB connection: ETPUA30 (PortP P23-15) --> USER_LED_1 (P7-1) * ETPUA31 (PortP P23-14) --> USER_LED_2 (P7-2) * * eMIOS ch0 (PortG P14-16)--> connect external pulse signal * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * setup clock for peripherals, setup access right for Masters and Peripherals * on AIPS_0 * * DMA transfers block of data from variable TransmitBuffer to the variable * ReceiveBuffer. Both variables are placed in SRAM. * * ICache and DCache are both disabled in startup file using CACHE_ENABLE macro. * You can change the value of the macro at the following path: * project Properties/C/C++ General/Paths and Symbols/Symbols * If you change the value to 1, ICahce and DCache will be enabled in startup. * * * ------------------------------------------------------------------------------ * Test HW:         MPC5775K-356DS, MPC57xx Motherboard * MCU:             PPC5775KMMY3A 0N38M * Fsys:            PLL0 266MHz *                    Z4 Core 133MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  default * ********************************************************************************
記事全体を表示
This document shows, how to use CodeWarrior 10.6 to program QSPI flash for Power Architecture microcontrollers.   1) Create new project for appropriate microcontroller. 2) Open Debug configuration and duplicate one of the target.   3) Rename duplicated target (optional) 4) Choose the duplicated (renamed) target and click Edit button in Target settings tab.   5) In new screen, click Advanced Programming Options.   6) Check Use Alternative Algorithm and choose the algorithm you want to use. Algorithms are place in CodeWarrior installation folder. Full path is CodeWarrior_installation_folder\MCU\bin\plugins\support\EPPC\gdi\P&E\   7) On the screen Debug configuration, choose the file you want to program to QSPI flash.   Click Apply and Debug.
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, third LED by software * loop, initializes and display notice via UART terminal and then terminal ECHO. * Second core is started and second LED blinking is being performed by it. * The example configures the device for maximum performance (OPTIMIZATIONS_ON) * by initialization of instruction cache and enabling of branch prediction. * Example suppose MCU is configured for DPM (Decoupled-parallel mode). * Its intention is to offer advanced startup code additional to CW stationery. * * ------------------------------------------------------------------------------ * Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon * Target :         internal_FLASH, RAM * Fsys:            120 MHz PLL0 * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  default * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, * initializes and display notice via UART terminal and then terminal ECHO. * * You can choose TRK or Minimodule version using USED_BOARD macro * * ------------------------------------------------------------------------------ * Test HW:         XPC560P 100LQFP, XPC56XX EVB MOTHEBOARD Rev.B, TRK-MPC5604P Rev.B * MCU:             PPC5604PEFMLL 0M36W * Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFLEX_0 * Fsys:            64/40 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  Jumper J8 1st position fit LED1 connected to PE4, jumpers J22,23 position 2-3 fit SCI tx and rx connected * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * setup clock for peripherals, * * Initializes the MCU including the FlexCAN peripherals. * Configures the FlexCAN to transmit and receive a CAN message. * * In this config, CAN_0 transmits a message. CAN_2 receives the message. * CAN_0 MB0 is configured to send data. * * CAN_2 MB0 is configured to receive a message, interrupt is used. * * * ------------------------------------------------------------------------------ * Test HW:         MPC5746R-176LQFP, MPC57xx Motherboard * MCU:             PPC5743R 1N83M * Fsys:            PLL0 200MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, debug_ram mode) * EVB connection: * * Jumpers j37 and j38 on motherboard must be in position 2-3 * * Connect CAN P5.2 to CAN2 P4.2 on motherboard * Connect CAN P5.1 to CAN2 P4.1 on motherboard * * ******************************************************************************** Revision History: Version  Date         Author              Description of Changes 1.0      Jun-07-2017  Martin Kovar      Initial version
記事全体を表示
******************************************************************************** * Detailed Description: * Example shows MCU's temperature measurement using internal temperature sensor. * After basic initialization, the code initializes and calibrates eQADC, reads * test flash content and performs all necessary ADC measurement to calculate die * temperature. Results are then displayed in the terminal window. * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B * MCU:             PPC5674FMVYA264 * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            264/200/150/60 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  default * ********************************************************************************
記事全体を表示