******************************************************************************** * Detailed Description: * Purpose of the example is to show how to simulate Multi-bit or Single-bit ECC * error in FlexCAN RAM (user must choose it in the option at the end of * main function). * Example configures FlexCAN module, initializes ECC for all FlexCAN RAMs, then * it injects ECC error to the Message Buffer 9. * When corrupted data is accessed the IVOR1 exception handler is called in case * of multi-bit ECC error (IVOR1 exception occurs) and FCCU_Alarm_Interrupt * handler is called in case of single-bit ECC error (FCCU interrupt occurs). * Both function calls MEMU handler. * Reported FlexCAN ECC error address is corrected according RM, section 7.12.2.3 * The example displays notices in the terminal window (connector J19 on * MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * ------------------------------------------------------------------------------ * Test HW: MPC57xx_Motherboard + MPC5744P-144DC * MCU: PPC5744PFMLQ8,0N15P,QQAA1515N, Rev2.1B * Fsys: 200 MHz PLL with 40 MHz crystal reference * Debugger: Lauterbach Trace32 * Target: internal_FLASH, RAM * Terminal: 19200-8-no parity-1 stop bit-no flow control * EVB connection: default ********************************************************************************
查看全文