SDK Importing Help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
692件の閲覧回数
joseph_lindula
Contributor IV

Hello, my work computer is not connected to the internet so I have to download the SDK from another computer and manually install it. I have some instructions:

https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/Importing-an-MCUXpresso-SDK-into-MCUXpres...

These instructions are from 2017 and the Windows>Preferences Window looks a little different. There is no SDK Options listed under the MCUXpresso IDE.

Here is my view:

nxp.png

Can anyone help me with installing an SDK manually please?

Here is where I download the SDK which is pretty helpful, better than other vendors:

https://mcuxpresso.nxp.com/en

 

Thank you 

タグ(1)
0 件の賞賛
返信
1 解決策
666件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @joseph_lindula 

To install SDK package to MCUXpresso IDE, pls follow steps:

1. Select the board and download the package from  https://mcuxpresso.nxp.com/en/select 

2. Make sure select toolchain as "All" or "MCUXpresso IDE", online build the package and download the zip file

ZhangJennie_0-1739442812657.png

3. Open MCUXpresso IDE. Drag the SDK zip file to IDE "Installed SDKs" window

ZhangJennie_1-1739443347878.png

 

Hope this helps,

Jun Zhang

 

元の投稿で解決策を見る

2 返答(返信)
597件の閲覧回数
joseph_lindula
Contributor IV

Thank you very much. 

0 件の賞賛
返信
667件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @joseph_lindula 

To install SDK package to MCUXpresso IDE, pls follow steps:

1. Select the board and download the package from  https://mcuxpresso.nxp.com/en/select 

2. Make sure select toolchain as "All" or "MCUXpresso IDE", online build the package and download the zip file

ZhangJennie_0-1739442812657.png

3. Open MCUXpresso IDE. Drag the SDK zip file to IDE "Installed SDKs" window

ZhangJennie_1-1739443347878.png

 

Hope this helps,

Jun Zhang